]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - .gitignore
gpu: ion: omap: re-populate flags parameters into buffer
[android-sdk/kernel-video.git] / .gitignore
1 #
2 # NOTE! Don't add files that are generated in specific
3 # subdirectories here. Add them in the ".gitignore" file
4 # in that subdirectory instead.
5 #
6 # NOTE! Please use 'git ls-files -i --exclude-standard'
7 # command after changing this file, to see if there are
8 # any tracked files which get ignored after the change.
9 #
10 # Normal rules
11 #
12 .*
13 *.o
14 *.o.*
15 *.a
16 *.s
17 *.ko
18 *.so
19 *.so.dbg
20 *.mod.c
21 *.i
22 *.lst
23 *.symtypes
24 *.order
25 modules.builtin
26 *.elf
27 *.bin
28 *.gz
29 *.bz2
30 *.lzma
31 *.xz
32 *.lzo
33 *.patch
34 *.gcno
36 #
37 # Top-level generic files
38 #
39 /tags
40 /TAGS
41 /linux
42 /vmlinux
43 /vmlinuz
44 /System.map
45 /Module.markers
46 /Module.symvers
48 #
49 # Debian directory (make deb-pkg)
50 #
51 /debian/
53 #
54 # git files that we don't want to ignore even it they are dot-files
55 #
56 !.gitignore
57 !.mailmap
59 #
60 # Generated include files
61 #
62 include/config
63 include/generated
64 arch/*/include/generated
66 # stgit generated dirs
67 patches-*
69 # quilt's files
70 patches
71 series
73 # cscope files
74 cscope.*
75 ncscope.*
77 # gnu global files
78 GPATH
79 GRTAGS
80 GSYMS
81 GTAGS
83 *.orig
84 *~
85 \#*#
87 #
88 # Leavings from module signing
89 #
90 extra_certificates
91 signing_key.priv
92 signing_key.x509
93 x509.genkey