]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - Documentation/ABI/testing/sysfs-devices-power
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/dtor/input
[android-sdk/kernel-video.git] / Documentation / ABI / testing / sysfs-devices-power
1 What:           /sys/devices/.../power/
2 Date:           January 2009
3 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
4 Description:
5                 The /sys/devices/.../power directory contains attributes
6                 allowing the user space to check and modify some power
7                 management related properties of given device.
9 What:           /sys/devices/.../power/wakeup
10 Date:           January 2009
11 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
12 Description:
13                 The /sys/devices/.../power/wakeup attribute allows the user
14                 space to check if the device is enabled to wake up the system
15                 from sleep states, such as the memory sleep state (suspend to
16                 RAM) and hibernation (suspend to disk), and to enable or disable
17                 it to do that as desired.
19                 Some devices support "wakeup" events, which are hardware signals
20                 used to activate the system from a sleep state.  Such devices
21                 have one of the following two values for the sysfs power/wakeup
22                 file:
24                 + "enabled\n" to issue the events;
25                 + "disabled\n" not to do so;
27                 In that cases the user space can change the setting represented
28                 by the contents of this file by writing either "enabled", or
29                 "disabled" to it.
31                 For the devices that are not capable of generating system wakeup
32                 events this file is not present.  In that case the device cannot
33                 be enabled to wake up the system from sleep states.
35 What:           /sys/devices/.../power/control
36 Date:           January 2009
37 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
38 Description:
39                 The /sys/devices/.../power/control attribute allows the user
40                 space to control the run-time power management of the device.
42                 All devices have one of the following two values for the
43                 power/control file:
45                 + "auto\n" to allow the device to be power managed at run time;
46                 + "on\n" to prevent the device from being power managed;
48                 The default for all devices is "auto", which means that they may
49                 be subject to automatic power management, depending on their
50                 drivers.  Changing this attribute to "on" prevents the driver
51                 from power managing the device at run time.  Doing that while
52                 the device is suspended causes it to be woken up.
54 What:           /sys/devices/.../power/async
55 Date:           January 2009
56 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
57 Description:
58                 The /sys/devices/.../async attribute allows the user space to
59                 enable or diasble the device's suspend and resume callbacks to
60                 be executed asynchronously (ie. in separate threads, in parallel
61                 with the main suspend/resume thread) during system-wide power
62                 transitions (eg. suspend to RAM, hibernation).
64                 All devices have one of the following two values for the
65                 power/async file:
67                 + "enabled\n" to permit the asynchronous suspend/resume;
68                 + "disabled\n" to forbid it;
70                 The value of this attribute may be changed by writing either
71                 "enabled", or "disabled" to it.
73                 It generally is unsafe to permit the asynchronous suspend/resume
74                 of a device unless it is certain that all of the PM dependencies
75                 of the device are known to the PM core.  However, for some
76                 devices this attribute is set to "enabled" by bus type code or
77                 device drivers and in that cases it should be safe to leave the
78                 default value.
80 What:           /sys/devices/.../power/wakeup_count
81 Date:           September 2010
82 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
83 Description:
84                 The /sys/devices/.../wakeup_count attribute contains the number
85                 of signaled wakeup events associated with the device.  This
86                 attribute is read-only.  If the device is not enabled to wake up
87                 the system from sleep states, this attribute is not present.
89 What:           /sys/devices/.../power/wakeup_active_count
90 Date:           September 2010
91 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
92 Description:
93                 The /sys/devices/.../wakeup_active_count attribute contains the
94                 number of times the processing of wakeup events associated with
95                 the device was completed (at the kernel level).  This attribute
96                 is read-only.  If the device is not enabled to wake up the
97                 system from sleep states, this attribute is not present.
99 What:           /sys/devices/.../power/wakeup_abort_count
100 Date:           February 2012
101 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
102 Description:
103                 The /sys/devices/.../wakeup_abort_count attribute contains the
104                 number of times the processing of a wakeup event associated with
105                 the device might have aborted system transition into a sleep
106                 state in progress.  This attribute is read-only.  If the device
107                 is not enabled to wake up the system from sleep states, this
108                 attribute is not present.
110 What:           /sys/devices/.../power/wakeup_expire_count
111 Date:           February 2012
112 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
113 Description:
114                 The /sys/devices/.../wakeup_expire_count attribute contains the
115                 number of times a wakeup event associated with the device has
116                 been reported with a timeout that expired.  This attribute is
117                 read-only.  If the device is not enabled to wake up the system
118                 from sleep states, this attribute is not present.
120 What:           /sys/devices/.../power/wakeup_active
121 Date:           September 2010
122 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
123 Description:
124                 The /sys/devices/.../wakeup_active attribute contains either 1,
125                 or 0, depending on whether or not a wakeup event associated with
126                 the device is being processed (1).  This attribute is read-only.
127                 If the device is not enabled to wake up the system from sleep
128                 states, this attribute is not present.
130 What:           /sys/devices/.../power/wakeup_total_time_ms
131 Date:           September 2010
132 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
133 Description:
134                 The /sys/devices/.../wakeup_total_time_ms attribute contains
135                 the total time of processing wakeup events associated with the
136                 device, in milliseconds.  This attribute is read-only.  If the
137                 device is not enabled to wake up the system from sleep states,
138                 this attribute is not present.
140 What:           /sys/devices/.../power/wakeup_max_time_ms
141 Date:           September 2010
142 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
143 Description:
144                 The /sys/devices/.../wakeup_max_time_ms attribute contains
145                 the maximum time of processing a single wakeup event associated
146                 with the device, in milliseconds.  This attribute is read-only.
147                 If the device is not enabled to wake up the system from sleep
148                 states, this attribute is not present.
150 What:           /sys/devices/.../power/wakeup_last_time_ms
151 Date:           September 2010
152 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
153 Description:
154                 The /sys/devices/.../wakeup_last_time_ms attribute contains
155                 the value of the monotonic clock corresponding to the time of
156                 signaling the last wakeup event associated with the device, in
157                 milliseconds.  This attribute is read-only.  If the device is
158                 not enabled to wake up the system from sleep states, this
159                 attribute is not present.
161 What:           /sys/devices/.../power/wakeup_prevent_sleep_time_ms
162 Date:           February 2012
163 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
164 Description:
165                 The /sys/devices/.../wakeup_prevent_sleep_time_ms attribute
166                 contains the total time the device has been preventing
167                 opportunistic transitions to sleep states from occurring.
168                 This attribute is read-only.  If the device is not enabled to
169                 wake up the system from sleep states, this attribute is not
170                 present.
172 What:           /sys/devices/.../power/autosuspend_delay_ms
173 Date:           September 2010
174 Contact:        Alan Stern <stern@rowland.harvard.edu>
175 Description:
176                 The /sys/devices/.../power/autosuspend_delay_ms attribute
177                 contains the autosuspend delay value (in milliseconds).  Some
178                 drivers do not want their device to suspend as soon as it
179                 becomes idle at run time; they want the device to remain
180                 inactive for a certain minimum period of time first.  That
181                 period is called the autosuspend delay.  Negative values will
182                 prevent the device from being suspended at run time (similar
183                 to writing "on" to the power/control attribute).  Values >=
184                 1000 will cause the autosuspend timer expiration to be rounded
185                 up to the nearest second.
187                 Not all drivers support this attribute.  If it isn't supported,
188                 attempts to read or write it will yield I/O errors.
190 What:           /sys/devices/.../power/pm_qos_latency_us
191 Date:           March 2012
192 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
193 Description:
194                 The /sys/devices/.../power/pm_qos_resume_latency_us attribute
195                 contains the PM QoS resume latency limit for the given device,
196                 which is the maximum allowed time it can take to resume the
197                 device, after it has been suspended at run time, from a resume
198                 request to the moment the device will be ready to process I/O,
199                 in microseconds.  If it is equal to 0, however, this means that
200                 the PM QoS resume latency may be arbitrary.
202                 Not all drivers support this attribute.  If it isn't supported,
203                 it is not present.
205                 This attribute has no effect on system-wide suspend/resume and
206                 hibernation.
208 What:           /sys/devices/.../power/pm_qos_no_power_off
209 Date:           September 2012
210 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
211 Description:
212                 The /sys/devices/.../power/pm_qos_no_power_off attribute
213                 is used for manipulating the PM QoS "no power off" flag.  If
214                 set, this flag indicates to the kernel that power should not
215                 be removed entirely from the device.
217                 Not all drivers support this attribute.  If it isn't supported,
218                 it is not present.
220                 This attribute has no effect on system-wide suspend/resume and
221                 hibernation.
223 What:           /sys/devices/.../power/pm_qos_remote_wakeup
224 Date:           September 2012
225 Contact:        Rafael J. Wysocki <rjw@sisk.pl>
226 Description:
227                 The /sys/devices/.../power/pm_qos_remote_wakeup attribute
228                 is used for manipulating the PM QoS "remote wakeup required"
229                 flag.  If set, this flag indicates to the kernel that the
230                 device is a source of user events that have to be signaled from
231                 its low-power states.
233                 Not all drivers support this attribute.  If it isn't supported,
234                 it is not present.
236                 This attribute has no effect on system-wide suspend/resume and
237                 hibernation.