1 DMA with ISA and LPC devices
2 ============================
4 Pierre Ossman <drzeus@drzeus.cx>
6 This document describes how to do DMA transfers using the old ISA DMA
7 controller. Even though ISA is more or less dead today the LPC bus
8 uses the same DMA system so it will be around for quite some time.
10 Part I - Headers and dependencies
11 ---------------------------------
13 To do ISA style DMA you need to include two headers:
15 #include <linux/dma-mapping.h>
16 #include <asm/dma.h>
18 The first is the generic DMA API used to convert virtual addresses to
19 physical addresses (see Documentation/DMA-API.txt for details).
21 The second contains the routines specific to ISA DMA transfers. Since
22 this is not present on all platforms make sure you construct your
23 Kconfig to be dependent on ISA_DMA_API (not ISA) so that nobody tries
24 to build your driver on unsupported platforms.
26 Part II - Buffer allocation
27 ---------------------------
29 The ISA DMA controller has some very strict requirements on which
30 memory it can access so extra care must be taken when allocating
31 buffers.
33 (You usually need a special buffer for DMA transfers instead of
34 transferring directly to and from your normal data structures.)
36 The DMA-able address space is the lowest 16 MB of _physical_ memory.
37 Also the transfer block may not cross page boundaries (which are 64
38 or 128 KiB depending on which channel you use).
40 In order to allocate a piece of memory that satisfies all these
41 requirements you pass the flag GFP_DMA to kmalloc.
43 Unfortunately the memory available for ISA DMA is scarce so unless you
44 allocate the memory during boot-up it's a good idea to also pass
45 __GFP_REPEAT and __GFP_NOWARN to make the allocater try a bit harder.
47 (This scarcity also means that you should allocate the buffer as
48 early as possible and not release it until the driver is unloaded.)
50 Part III - Address translation
51 ------------------------------
53 To translate the virtual address to a physical use the normal DMA
54 API. Do _not_ use isa_virt_to_phys() even though it does the same
55 thing. The reason for this is that the function isa_virt_to_phys()
56 will require a Kconfig dependency to ISA, not just ISA_DMA_API which
57 is really all you need. Remember that even though the DMA controller
58 has its origins in ISA it is used elsewhere.
60 Note: x86_64 had a broken DMA API when it came to ISA but has since
61 been fixed. If your arch has problems then fix the DMA API instead of
62 reverting to the ISA functions.
64 Part IV - Channels
65 ------------------
67 A normal ISA DMA controller has 8 channels. The lower four are for
68 8-bit transfers and the upper four are for 16-bit transfers.
70 (Actually the DMA controller is really two separate controllers where
71 channel 4 is used to give DMA access for the second controller (0-3).
72 This means that of the four 16-bits channels only three are usable.)
74 You allocate these in a similar fashion as all basic resources:
76 extern int request_dma(unsigned int dmanr, const char * device_id);
77 extern void free_dma(unsigned int dmanr);
79 The ability to use 16-bit or 8-bit transfers is _not_ up to you as a
80 driver author but depends on what the hardware supports. Check your
81 specs or test different channels.
83 Part V - Transfer data
84 ----------------------
86 Now for the good stuff, the actual DMA transfer. :)
88 Before you use any ISA DMA routines you need to claim the DMA lock
89 using claim_dma_lock(). The reason is that some DMA operations are
90 not atomic so only one driver may fiddle with the registers at a
91 time.
93 The first time you use the DMA controller you should call
94 clear_dma_ff(). This clears an internal register in the DMA
95 controller that is used for the non-atomic operations. As long as you
96 (and everyone else) uses the locking functions then you only need to
97 reset this once.
99 Next, you tell the controller in which direction you intend to do the
100 transfer using set_dma_mode(). Currently you have the options
101 DMA_MODE_READ and DMA_MODE_WRITE.
103 Set the address from where the transfer should start (this needs to
104 be 16-bit aligned for 16-bit transfers) and how many bytes to
105 transfer. Note that it's _bytes_. The DMA routines will do all the
106 required translation to values that the DMA controller understands.
108 The final step is enabling the DMA channel and releasing the DMA
109 lock.
111 Once the DMA transfer is finished (or timed out) you should disable
112 the channel again. You should also check get_dma_residue() to make
113 sure that all data has been transferred.
115 Example:
117 int flags, residue;
119 flags = claim_dma_lock();
121 clear_dma_ff();
123 set_dma_mode(channel, DMA_MODE_WRITE);
124 set_dma_addr(channel, phys_addr);
125 set_dma_count(channel, num_bytes);
127 dma_enable(channel);
129 release_dma_lock(flags);
131 while (!device_done());
133 flags = claim_dma_lock();
135 dma_disable(channel);
137 residue = dma_get_residue(channel);
138 if (residue != 0)
139 printk(KERN_ERR "driver: Incomplete DMA transfer!"
140 " %d bytes left!\n", residue);
142 release_dma_lock(flags);
144 Part VI - Suspend/resume
145 ------------------------
147 It is the driver's responsibility to make sure that the machine isn't
148 suspended while a DMA transfer is in progress. Also, all DMA settings
149 are lost when the system suspends so if your driver relies on the DMA
150 controller being in a certain state then you have to restore these
151 registers upon resume.