1 <refentry id="vidioc-expbuf">
3 <refmeta>
4 <refentrytitle>ioctl VIDIOC_EXPBUF</refentrytitle>
5 &manvol;
6 </refmeta>
8 <refnamediv>
9 <refname>VIDIOC_EXPBUF</refname>
10 <refpurpose>Export a buffer as a DMABUF file descriptor.</refpurpose>
11 </refnamediv>
13 <refsynopsisdiv>
14 <funcsynopsis>
15 <funcprototype>
16 <funcdef>int <function>ioctl</function></funcdef>
17 <paramdef>int <parameter>fd</parameter></paramdef>
18 <paramdef>int <parameter>request</parameter></paramdef>
19 <paramdef>struct v4l2_exportbuffer *<parameter>argp</parameter></paramdef>
20 </funcprototype>
21 </funcsynopsis>
22 </refsynopsisdiv>
24 <refsect1>
25 <title>Arguments</title>
27 <variablelist>
28 <varlistentry>
29 <term><parameter>fd</parameter></term>
30 <listitem>
31 <para>&fd;</para>
32 </listitem>
33 </varlistentry>
34 <varlistentry>
35 <term><parameter>request</parameter></term>
36 <listitem>
37 <para>VIDIOC_EXPBUF</para>
38 </listitem>
39 </varlistentry>
40 <varlistentry>
41 <term><parameter>argp</parameter></term>
42 <listitem>
43 <para></para>
44 </listitem>
45 </varlistentry>
46 </variablelist>
47 </refsect1>
49 <refsect1>
50 <title>Description</title>
52 <note>
53 <title>Experimental</title>
54 <para>This is an <link linkend="experimental"> experimental </link>
55 interface and may change in the future.</para>
56 </note>
58 <para>This ioctl is an extension to the <link linkend="mmap">memory
59 mapping</link> I/O method, therefore it is available only for
60 <constant>V4L2_MEMORY_MMAP</constant> buffers. It can be used to export a
61 buffer as a DMABUF file at any time after buffers have been allocated with the
62 &VIDIOC-REQBUFS; ioctl.</para>
64 <para> To export a buffer, applications fill &v4l2-exportbuffer;. The
65 <structfield> type </structfield> field is set to the same buffer type as was
66 previously used with &v4l2-requestbuffers;<structfield> type </structfield>.
67 Applications must also set the <structfield> index </structfield> field. Valid
68 index numbers range from zero to the number of buffers allocated with
69 &VIDIOC-REQBUFS; (&v4l2-requestbuffers;<structfield> count </structfield>)
70 minus one. For the multi-planar API, applications set the <structfield> plane
71 </structfield> field to the index of the plane to be exported. Valid planes
72 range from zero to the maximal number of valid planes for the currently active
73 format. For the single-planar API, applications must set <structfield> plane
74 </structfield> to zero. Additional flags may be posted in the <structfield>
75 flags </structfield> field. Refer to a manual for open() for details.
76 Currently only O_CLOEXEC is supported. All other fields must be set to zero.
77 In the case of multi-planar API, every plane is exported separately using
78 multiple <constant> VIDIOC_EXPBUF </constant> calls. </para>
80 <para> After calling <constant>VIDIOC_EXPBUF</constant> the <structfield> fd
81 </structfield> field will be set by a driver. This is a DMABUF file
82 descriptor. The application may pass it to other DMABUF-aware devices. Refer to
83 <link linkend="dmabuf">DMABUF importing</link> for details about importing
84 DMABUF files into V4L2 nodes. It is recommended to close a DMABUF file when it
85 is no longer used to allow the associated memory to be reclaimed. </para>
87 </refsect1>
88 <refsect1>
89 <section>
90 <title>Examples</title>
92 <example>
93 <title>Exporting a buffer.</title>
94 <programlisting>
95 int buffer_export(int v4lfd, &v4l2-buf-type; bt, int index, int *dmafd)
96 {
97 &v4l2-exportbuffer; expbuf;
99 memset(&expbuf, 0, sizeof(expbuf));
100 expbuf.type = bt;
101 expbuf.index = index;
102 if (ioctl(v4lfd, &VIDIOC-EXPBUF;, &expbuf) == -1) {
103 perror("VIDIOC_EXPBUF");
104 return -1;
105 }
107 *dmafd = expbuf.fd;
109 return 0;
110 }
111 </programlisting>
112 </example>
114 <example>
115 <title>Exporting a buffer using the multi-planar API.</title>
116 <programlisting>
117 int buffer_export_mp(int v4lfd, &v4l2-buf-type; bt, int index,
118 int dmafd[], int n_planes)
119 {
120 int i;
122 for (i = 0; i < n_planes; ++i) {
123 &v4l2-exportbuffer; expbuf;
125 memset(&expbuf, 0, sizeof(expbuf));
126 expbuf.type = bt;
127 expbuf.index = index;
128 expbuf.plane = i;
129 if (ioctl(v4lfd, &VIDIOC-EXPBUF;, &expbuf) == -1) {
130 perror("VIDIOC_EXPBUF");
131 while (i)
132 close(dmafd[--i]);
133 return -1;
134 }
135 dmafd[i] = expbuf.fd;
136 }
138 return 0;
139 }
140 </programlisting>
141 </example>
142 </section>
143 </refsect1>
145 <refsect1>
146 <table pgwide="1" frame="none" id="v4l2-exportbuffer">
147 <title>struct <structname>v4l2_exportbuffer</structname></title>
148 <tgroup cols="3">
149 &cs-str;
150 <tbody valign="top">
151 <row>
152 <entry>__u32</entry>
153 <entry><structfield>type</structfield></entry>
154 <entry>Type of the buffer, same as &v4l2-format;
155 <structfield>type</structfield> or &v4l2-requestbuffers;
156 <structfield>type</structfield>, set by the application. See <xref
157 linkend="v4l2-buf-type" /></entry>
158 </row>
159 <row>
160 <entry>__u32</entry>
161 <entry><structfield>index</structfield></entry>
162 <entry>Number of the buffer, set by the application. This field is
163 only used for <link linkend="mmap">memory mapping</link> I/O and can range from
164 zero to the number of buffers allocated with the &VIDIOC-REQBUFS; and/or
165 &VIDIOC-CREATE-BUFS; ioctls. </entry>
166 </row>
167 <row>
168 <entry>__u32</entry>
169 <entry><structfield>plane</structfield></entry>
170 <entry>Index of the plane to be exported when using the
171 multi-planar API. Otherwise this value must be set to zero. </entry>
172 </row>
173 <row>
174 <entry>__u32</entry>
175 <entry><structfield>flags</structfield></entry>
176 <entry>Flags for the newly created file, currently only <constant>
177 O_CLOEXEC </constant> is supported, refer to the manual of open() for more
178 details.</entry>
179 </row>
180 <row>
181 <entry>__s32</entry>
182 <entry><structfield>fd</structfield></entry>
183 <entry>The DMABUF file descriptor associated with a buffer. Set by
184 the driver.</entry>
185 </row>
186 <row>
187 <entry>__u32</entry>
188 <entry><structfield>reserved[11]</structfield></entry>
189 <entry>Reserved field for future use. Must be set to zero.</entry>
190 </row>
191 </tbody>
192 </tgroup>
193 </table>
195 </refsect1>
197 <refsect1>
198 &return-value;
199 <variablelist>
200 <varlistentry>
201 <term><errorcode>EINVAL</errorcode></term>
202 <listitem>
203 <para>A queue is not in MMAP mode or DMABUF exporting is not
204 supported or <structfield> flags </structfield> or <structfield> type
205 </structfield> or <structfield> index </structfield> or <structfield> plane
206 </structfield> fields are invalid.</para>
207 </listitem>
208 </varlistentry>
209 </variablelist>
210 </refsect1>
212 </refentry>