]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - Documentation/arm64/legacy_instructions.txt
Merge branch 'p-ti-linux-3.14.y-common' into p-ti-linux-3.14.y-android
[android-sdk/kernel-video.git] / Documentation / arm64 / legacy_instructions.txt
1 The arm64 port of the Linux kernel provides infrastructure to support
2 emulation of instructions which have been deprecated, or obsoleted in
3 the architecture. The infrastructure code uses undefined instruction
4 hooks to support emulation. Where available it also allows turning on
5 the instruction execution in hardware.
7 The emulation mode can be controlled by writing to sysctl nodes
8 (/proc/sys/abi). The following explains the different execution
9 behaviours and the corresponding values of the sysctl nodes -
11 * Undef
12   Value: 0
13   Generates undefined instruction abort. Default for instructions that
14   have been obsoleted in the architecture, e.g., SWP
16 * Emulate
17   Value: 1
18   Uses software emulation. To aid migration of software, in this mode
19   usage of emulated instruction is traced as well as rate limited
20   warnings are issued. This is the default for deprecated
21   instructions, .e.g., CP15 barriers
23 * Hardware Execution
24   Value: 2
25   Although marked as deprecated, some implementations may support the
26   enabling/disabling of hardware support for the execution of these
27   instructions. Using hardware execution generally provides better
28   performance, but at the loss of ability to gather runtime statistics
29   about the use of the deprecated instructions.
31 The default mode depends on the status of the instruction in the
32 architecture. Deprecated instructions should default to emulation
33 while obsolete instructions must be undefined by default.
35 Note: Instruction emulation may not be possible in all cases. See
36 individual instruction notes for further information.
38 Supported legacy instructions
39 -----------------------------
40 * SWP{B}
41 Node: /proc/sys/abi/swp
42 Status: Obsolete
43 Default: Undef (0)
45 * CP15 Barriers
46 Node: /proc/sys/abi/cp15_barrier
47 Status: Deprecated
48 Default: Emulate (1)
50 * SETEND
51 Node: /proc/sys/abi/setend
52 Status: Deprecated
53 Default: Emulate (1)*
54 Note: All the cpus on the system must have mixed endian support at EL0
55 for this feature to be enabled. If a new CPU - which doesn't support mixed
56 endian - is hotplugged in after this feature has been enabled, there could
57 be unexpected results in the application.