]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - Documentation/cachetlb.txt
ARM: dts: dra72: enable dss node
[android-sdk/kernel-video.git] / Documentation / cachetlb.txt
1                 Cache and TLB Flushing
2                      Under Linux
4             David S. Miller <davem@redhat.com>
6 This document describes the cache/tlb flushing interfaces called
7 by the Linux VM subsystem.  It enumerates over each interface,
8 describes its intended purpose, and what side effect is expected
9 after the interface is invoked.
11 The side effects described below are stated for a uniprocessor
12 implementation, and what is to happen on that single processor.  The
13 SMP cases are a simple extension, in that you just extend the
14 definition such that the side effect for a particular interface occurs
15 on all processors in the system.  Don't let this scare you into
16 thinking SMP cache/tlb flushing must be so inefficient, this is in
17 fact an area where many optimizations are possible.  For example,
18 if it can be proven that a user address space has never executed
19 on a cpu (see mm_cpumask()), one need not perform a flush
20 for this address space on that cpu.
22 First, the TLB flushing interfaces, since they are the simplest.  The
23 "TLB" is abstracted under Linux as something the cpu uses to cache
24 virtual-->physical address translations obtained from the software
25 page tables.  Meaning that if the software page tables change, it is
26 possible for stale translations to exist in this "TLB" cache.
27 Therefore when software page table changes occur, the kernel will
28 invoke one of the following flush methods _after_ the page table
29 changes occur:
31 1) void flush_tlb_all(void)
33         The most severe flush of all.  After this interface runs,
34         any previous page table modification whatsoever will be
35         visible to the cpu.
37         This is usually invoked when the kernel page tables are
38         changed, since such translations are "global" in nature.
40 2) void flush_tlb_mm(struct mm_struct *mm)
42         This interface flushes an entire user address space from
43         the TLB.  After running, this interface must make sure that
44         any previous page table modifications for the address space
45         'mm' will be visible to the cpu.  That is, after running,
46         there will be no entries in the TLB for 'mm'.
48         This interface is used to handle whole address space
49         page table operations such as what happens during
50         fork, and exec.
52 3) void flush_tlb_range(struct vm_area_struct *vma,
53                         unsigned long start, unsigned long end)
55         Here we are flushing a specific range of (user) virtual
56         address translations from the TLB.  After running, this
57         interface must make sure that any previous page table
58         modifications for the address space 'vma->vm_mm' in the range
59         'start' to 'end-1' will be visible to the cpu.  That is, after
60         running, there will be no entries in the TLB for 'mm' for
61         virtual addresses in the range 'start' to 'end-1'.
63         The "vma" is the backing store being used for the region.
64         Primarily, this is used for munmap() type operations.
66         The interface is provided in hopes that the port can find
67         a suitably efficient method for removing multiple page
68         sized translations from the TLB, instead of having the kernel
69         call flush_tlb_page (see below) for each entry which may be
70         modified.
72 4) void flush_tlb_page(struct vm_area_struct *vma, unsigned long addr)
74         This time we need to remove the PAGE_SIZE sized translation
75         from the TLB.  The 'vma' is the backing structure used by
76         Linux to keep track of mmap'd regions for a process, the
77         address space is available via vma->vm_mm.  Also, one may
78         test (vma->vm_flags & VM_EXEC) to see if this region is
79         executable (and thus could be in the 'instruction TLB' in
80         split-tlb type setups).
82         After running, this interface must make sure that any previous
83         page table modification for address space 'vma->vm_mm' for
84         user virtual address 'addr' will be visible to the cpu.  That
85         is, after running, there will be no entries in the TLB for
86         'vma->vm_mm' for virtual address 'addr'.
88         This is used primarily during fault processing.
90 5) void update_mmu_cache(struct vm_area_struct *vma,
91                          unsigned long address, pte_t *ptep)
93         At the end of every page fault, this routine is invoked to
94         tell the architecture specific code that a translation
95         now exists at virtual address "address" for address space
96         "vma->vm_mm", in the software page tables.
98         A port may use this information in any way it so chooses.
99         For example, it could use this event to pre-load TLB
100         translations for software managed TLB configurations.
101         The sparc64 port currently does this.
103 6) void tlb_migrate_finish(struct mm_struct *mm)
105         This interface is called at the end of an explicit
106         process migration. This interface provides a hook
107         to allow a platform to update TLB or context-specific
108         information for the address space.
110         The ia64 sn2 platform is one example of a platform
111         that uses this interface.
113 Next, we have the cache flushing interfaces.  In general, when Linux
114 is changing an existing virtual-->physical mapping to a new value,
115 the sequence will be in one of the following forms:
117         1) flush_cache_mm(mm);
118            change_all_page_tables_of(mm);
119            flush_tlb_mm(mm);
121         2) flush_cache_range(vma, start, end);
122            change_range_of_page_tables(mm, start, end);
123            flush_tlb_range(vma, start, end);
125         3) flush_cache_page(vma, addr, pfn);
126            set_pte(pte_pointer, new_pte_val);
127            flush_tlb_page(vma, addr);
129 The cache level flush will always be first, because this allows
130 us to properly handle systems whose caches are strict and require
131 a virtual-->physical translation to exist for a virtual address
132 when that virtual address is flushed from the cache.  The HyperSparc
133 cpu is one such cpu with this attribute.
135 The cache flushing routines below need only deal with cache flushing
136 to the extent that it is necessary for a particular cpu.  Mostly,
137 these routines must be implemented for cpus which have virtually
138 indexed caches which must be flushed when virtual-->physical
139 translations are changed or removed.  So, for example, the physically
140 indexed physically tagged caches of IA32 processors have no need to
141 implement these interfaces since the caches are fully synchronized
142 and have no dependency on translation information.
144 Here are the routines, one by one:
146 1) void flush_cache_mm(struct mm_struct *mm)
148         This interface flushes an entire user address space from
149         the caches.  That is, after running, there will be no cache
150         lines associated with 'mm'.
152         This interface is used to handle whole address space
153         page table operations such as what happens during exit and exec.
155 2) void flush_cache_dup_mm(struct mm_struct *mm)
157         This interface flushes an entire user address space from
158         the caches.  That is, after running, there will be no cache
159         lines associated with 'mm'.
161         This interface is used to handle whole address space
162         page table operations such as what happens during fork.
164         This option is separate from flush_cache_mm to allow some
165         optimizations for VIPT caches.
167 3) void flush_cache_range(struct vm_area_struct *vma,
168                           unsigned long start, unsigned long end)
170         Here we are flushing a specific range of (user) virtual
171         addresses from the cache.  After running, there will be no
172         entries in the cache for 'vma->vm_mm' for virtual addresses in
173         the range 'start' to 'end-1'.
175         The "vma" is the backing store being used for the region.
176         Primarily, this is used for munmap() type operations.
178         The interface is provided in hopes that the port can find
179         a suitably efficient method for removing multiple page
180         sized regions from the cache, instead of having the kernel
181         call flush_cache_page (see below) for each entry which may be
182         modified.
184 4) void flush_cache_page(struct vm_area_struct *vma, unsigned long addr, unsigned long pfn)
186         This time we need to remove a PAGE_SIZE sized range
187         from the cache.  The 'vma' is the backing structure used by
188         Linux to keep track of mmap'd regions for a process, the
189         address space is available via vma->vm_mm.  Also, one may
190         test (vma->vm_flags & VM_EXEC) to see if this region is
191         executable (and thus could be in the 'instruction cache' in
192         "Harvard" type cache layouts).
194         The 'pfn' indicates the physical page frame (shift this value
195         left by PAGE_SHIFT to get the physical address) that 'addr'
196         translates to.  It is this mapping which should be removed from
197         the cache.
199         After running, there will be no entries in the cache for
200         'vma->vm_mm' for virtual address 'addr' which translates
201         to 'pfn'.
203         This is used primarily during fault processing.
205 5) void flush_cache_kmaps(void)
207         This routine need only be implemented if the platform utilizes
208         highmem.  It will be called right before all of the kmaps
209         are invalidated.
211         After running, there will be no entries in the cache for
212         the kernel virtual address range PKMAP_ADDR(0) to
213         PKMAP_ADDR(LAST_PKMAP).
215         This routing should be implemented in asm/highmem.h
217 6) void flush_cache_vmap(unsigned long start, unsigned long end)
218    void flush_cache_vunmap(unsigned long start, unsigned long end)
220         Here in these two interfaces we are flushing a specific range
221         of (kernel) virtual addresses from the cache.  After running,
222         there will be no entries in the cache for the kernel address
223         space for virtual addresses in the range 'start' to 'end-1'.
225         The first of these two routines is invoked after map_vm_area()
226         has installed the page table entries.  The second is invoked
227         before unmap_kernel_range() deletes the page table entries.
229 There exists another whole class of cpu cache issues which currently
230 require a whole different set of interfaces to handle properly.
231 The biggest problem is that of virtual aliasing in the data cache
232 of a processor.
234 Is your port susceptible to virtual aliasing in its D-cache?
235 Well, if your D-cache is virtually indexed, is larger in size than
236 PAGE_SIZE, and does not prevent multiple cache lines for the same
237 physical address from existing at once, you have this problem.
239 If your D-cache has this problem, first define asm/shmparam.h SHMLBA
240 properly, it should essentially be the size of your virtually
241 addressed D-cache (or if the size is variable, the largest possible
242 size).  This setting will force the SYSv IPC layer to only allow user
243 processes to mmap shared memory at address which are a multiple of
244 this value.
246 NOTE: This does not fix shared mmaps, check out the sparc64 port for
247 one way to solve this (in particular SPARC_FLAG_MMAPSHARED).
249 Next, you have to solve the D-cache aliasing issue for all
250 other cases.  Please keep in mind that fact that, for a given page
251 mapped into some user address space, there is always at least one more
252 mapping, that of the kernel in its linear mapping starting at
253 PAGE_OFFSET.  So immediately, once the first user maps a given
254 physical page into its address space, by implication the D-cache
255 aliasing problem has the potential to exist since the kernel already
256 maps this page at its virtual address.
258   void copy_user_page(void *to, void *from, unsigned long addr, struct page *page)
259   void clear_user_page(void *to, unsigned long addr, struct page *page)
261         These two routines store data in user anonymous or COW
262         pages.  It allows a port to efficiently avoid D-cache alias
263         issues between userspace and the kernel.
265         For example, a port may temporarily map 'from' and 'to' to
266         kernel virtual addresses during the copy.  The virtual address
267         for these two pages is chosen in such a way that the kernel
268         load/store instructions happen to virtual addresses which are
269         of the same "color" as the user mapping of the page.  Sparc64
270         for example, uses this technique.
272         The 'addr' parameter tells the virtual address where the
273         user will ultimately have this page mapped, and the 'page'
274         parameter gives a pointer to the struct page of the target.
276         If D-cache aliasing is not an issue, these two routines may
277         simply call memcpy/memset directly and do nothing more.
279   void flush_dcache_page(struct page *page)
281         Any time the kernel writes to a page cache page, _OR_
282         the kernel is about to read from a page cache page and
283         user space shared/writable mappings of this page potentially
284         exist, this routine is called.
286         NOTE: This routine need only be called for page cache pages
287               which can potentially ever be mapped into the address
288               space of a user process.  So for example, VFS layer code
289               handling vfs symlinks in the page cache need not call
290               this interface at all.
292         The phrase "kernel writes to a page cache page" means,
293         specifically, that the kernel executes store instructions
294         that dirty data in that page at the page->virtual mapping
295         of that page.  It is important to flush here to handle
296         D-cache aliasing, to make sure these kernel stores are
297         visible to user space mappings of that page.
299         The corollary case is just as important, if there are users
300         which have shared+writable mappings of this file, we must make
301         sure that kernel reads of these pages will see the most recent
302         stores done by the user.
304         If D-cache aliasing is not an issue, this routine may
305         simply be defined as a nop on that architecture.
307         There is a bit set aside in page->flags (PG_arch_1) as
308         "architecture private".  The kernel guarantees that,
309         for pagecache pages, it will clear this bit when such
310         a page first enters the pagecache.
312         This allows these interfaces to be implemented much more
313         efficiently.  It allows one to "defer" (perhaps indefinitely)
314         the actual flush if there are currently no user processes
315         mapping this page.  See sparc64's flush_dcache_page and
316         update_mmu_cache implementations for an example of how to go
317         about doing this.
319         The idea is, first at flush_dcache_page() time, if
320         page->mapping->i_mmap is an empty tree and ->i_mmap_nonlinear
321         an empty list, just mark the architecture private page flag bit.
322         Later, in update_mmu_cache(), a check is made of this flag bit,
323         and if set the flush is done and the flag bit is cleared.
325         IMPORTANT NOTE: It is often important, if you defer the flush,
326                         that the actual flush occurs on the same CPU
327                         as did the cpu stores into the page to make it
328                         dirty.  Again, see sparc64 for examples of how
329                         to deal with this.
331   void copy_to_user_page(struct vm_area_struct *vma, struct page *page,
332                          unsigned long user_vaddr,
333                          void *dst, void *src, int len)
334   void copy_from_user_page(struct vm_area_struct *vma, struct page *page,
335                            unsigned long user_vaddr,
336                            void *dst, void *src, int len)
337         When the kernel needs to copy arbitrary data in and out
338         of arbitrary user pages (f.e. for ptrace()) it will use
339         these two routines.
341         Any necessary cache flushing or other coherency operations
342         that need to occur should happen here.  If the processor's
343         instruction cache does not snoop cpu stores, it is very
344         likely that you will need to flush the instruction cache
345         for copy_to_user_page().
347   void flush_anon_page(struct vm_area_struct *vma, struct page *page,
348                        unsigned long vmaddr)
349         When the kernel needs to access the contents of an anonymous
350         page, it calls this function (currently only
351         get_user_pages()).  Note: flush_dcache_page() deliberately
352         doesn't work for an anonymous page.  The default
353         implementation is a nop (and should remain so for all coherent
354         architectures).  For incoherent architectures, it should flush
355         the cache of the page at vmaddr.
357   void flush_kernel_dcache_page(struct page *page)
358         When the kernel needs to modify a user page is has obtained
359         with kmap, it calls this function after all modifications are
360         complete (but before kunmapping it) to bring the underlying
361         page up to date.  It is assumed here that the user has no
362         incoherent cached copies (i.e. the original page was obtained
363         from a mechanism like get_user_pages()).  The default
364         implementation is a nop and should remain so on all coherent
365         architectures.  On incoherent architectures, this should flush
366         the kernel cache for page (using page_address(page)).
369   void flush_icache_range(unsigned long start, unsigned long end)
370         When the kernel stores into addresses that it will execute
371         out of (eg when loading modules), this function is called.
373         If the icache does not snoop stores then this routine will need
374         to flush it.
376   void flush_icache_page(struct vm_area_struct *vma, struct page *page)
377         All the functionality of flush_icache_page can be implemented in
378         flush_dcache_page and update_mmu_cache. In the future, the hope
379         is to remove this interface completely.
381 The final category of APIs is for I/O to deliberately aliased address
382 ranges inside the kernel.  Such aliases are set up by use of the
383 vmap/vmalloc API.  Since kernel I/O goes via physical pages, the I/O
384 subsystem assumes that the user mapping and kernel offset mapping are
385 the only aliases.  This isn't true for vmap aliases, so anything in
386 the kernel trying to do I/O to vmap areas must manually manage
387 coherency.  It must do this by flushing the vmap range before doing
388 I/O and invalidating it after the I/O returns.
390   void flush_kernel_vmap_range(void *vaddr, int size)
391        flushes the kernel cache for a given virtual address range in
392        the vmap area.  This is to make sure that any data the kernel
393        modified in the vmap range is made visible to the physical
394        page.  The design is to make this area safe to perform I/O on.
395        Note that this API does *not* also flush the offset map alias
396        of the area.
398   void invalidate_kernel_vmap_range(void *vaddr, int size) invalidates
399        the cache for a given virtual address range in the vmap area
400        which prevents the processor from making the cache stale by
401        speculatively reading data while the I/O was occurring to the
402        physical pages.  This is only necessary for data reads into the
403        vmap area.