1 Kernel driver it87
2 ==================
4 Supported chips:
5 * IT8705F
6 Prefix: 'it87'
7 Addresses scanned: from Super I/O config space (8 I/O ports)
8 Datasheet: Once publicly available at the ITE website, but no longer
9 * IT8712F
10 Prefix: 'it8712'
11 Addresses scanned: from Super I/O config space (8 I/O ports)
12 Datasheet: Once publicly available at the ITE website, but no longer
13 * IT8716F/IT8726F
14 Prefix: 'it8716'
15 Addresses scanned: from Super I/O config space (8 I/O ports)
16 Datasheet: Once publicly available at the ITE website, but no longer
17 * IT8718F
18 Prefix: 'it8718'
19 Addresses scanned: from Super I/O config space (8 I/O ports)
20 Datasheet: Once publicly available at the ITE website, but no longer
21 * IT8720F
22 Prefix: 'it8720'
23 Addresses scanned: from Super I/O config space (8 I/O ports)
24 Datasheet: Not publicly available
25 * IT8721F/IT8758E
26 Prefix: 'it8721'
27 Addresses scanned: from Super I/O config space (8 I/O ports)
28 Datasheet: Not publicly available
29 * IT8728F
30 Prefix: 'it8728'
31 Addresses scanned: from Super I/O config space (8 I/O ports)
32 Datasheet: Not publicly available
33 * IT8782F
34 Prefix: 'it8782'
35 Addresses scanned: from Super I/O config space (8 I/O ports)
36 Datasheet: Not publicly available
37 * IT8783E/F
38 Prefix: 'it8783'
39 Addresses scanned: from Super I/O config space (8 I/O ports)
40 Datasheet: Not publicly available
41 * SiS950 [clone of IT8705F]
42 Prefix: 'it87'
43 Addresses scanned: from Super I/O config space (8 I/O ports)
44 Datasheet: No longer be available
46 Authors:
47 Christophe Gauthron
48 Jean Delvare <khali@linux-fr.org>
51 Module Parameters
52 -----------------
54 * update_vbat: int
56 0 if vbat should report power on value, 1 if vbat should be updated after
57 each read. Default is 0. On some boards the battery voltage is provided
58 by either the battery or the onboard power supply. Only the first reading
59 at power on will be the actual battery voltage (which the chip does
60 automatically). On other boards the battery voltage is always fed to
61 the chip so can be read at any time. Excessive reading may decrease
62 battery life but no information is given in the datasheet.
64 * fix_pwm_polarity int
66 Force PWM polarity to active high (DANGEROUS). Some chips are
67 misconfigured by BIOS - PWM values would be inverted. This option tries
68 to fix this. Please contact your BIOS manufacturer and ask him for fix.
71 Hardware Interfaces
72 -------------------
74 All the chips supported by this driver are LPC Super-I/O chips, accessed
75 through the LPC bus (ISA-like I/O ports). The IT8712F additionally has an
76 SMBus interface to the hardware monitoring functions. This driver no
77 longer supports this interface though, as it is slower and less reliable
78 than the ISA access, and was only available on a small number of
79 motherboard models.
82 Description
83 -----------
85 This driver implements support for the IT8705F, IT8712F, IT8716F,
86 IT8718F, IT8720F, IT8721F, IT8726F, IT8728F, IT8758E, IT8781F, IT8782F,
87 IT8783E/F, and SiS950 chips.
89 These chips are 'Super I/O chips', supporting floppy disks, infrared ports,
90 joysticks and other miscellaneous stuff. For hardware monitoring, they
91 include an 'environment controller' with 3 temperature sensors, 3 fan
92 rotation speed sensors, 8 voltage sensors, associated alarms, and chassis
93 intrusion detection.
95 The IT8712F and IT8716F additionally feature VID inputs, used to report
96 the Vcore voltage of the processor. The early IT8712F have 5 VID pins,
97 the IT8716F and late IT8712F have 6. They are shared with other functions
98 though, so the functionality may not be available on a given system.
100 The IT8718F and IT8720F also features VID inputs (up to 8 pins) but the value
101 is stored in the Super-I/O configuration space. Due to technical limitations,
102 this value can currently only be read once at initialization time, so
103 the driver won't notice and report changes in the VID value. The two
104 upper VID bits share their pins with voltage inputs (in5 and in6) so you
105 can't have both on a given board.
107 The IT8716F, IT8718F, IT8720F, IT8721F/IT8758E and later IT8712F revisions
108 have support for 2 additional fans. The additional fans are supported by the
109 driver.
111 The IT8716F, IT8718F, IT8720F, IT8721F/IT8758E, IT8782F, IT8783E/F, and late
112 IT8712F and IT8705F also have optional 16-bit tachometer counters for fans 1 to
113 3. This is better (no more fan clock divider mess) but not compatible with the
114 older chips and revisions. The 16-bit tachometer mode is enabled by the driver
115 when one of the above chips is detected.
117 The IT8726F is just bit enhanced IT8716F with additional hardware
118 for AMD power sequencing. Therefore the chip will appear as IT8716F
119 to userspace applications.
121 The IT8728F is considered compatible with the IT8721F, until a datasheet
122 becomes available (hopefully.)
124 Temperatures are measured in degrees Celsius. An alarm is triggered once
125 when the Overtemperature Shutdown limit is crossed.
127 Fan rotation speeds are reported in RPM (rotations per minute). An alarm is
128 triggered if the rotation speed has dropped below a programmable limit. When
129 16-bit tachometer counters aren't used, fan readings can be divided by
130 a programmable divider (1, 2, 4 or 8) to give the readings more range or
131 accuracy. With a divider of 2, the lowest representable value is around
132 2600 RPM. Not all RPM values can accurately be represented, so some rounding
133 is done.
135 Voltage sensors (also known as IN sensors) report their values in volts. An
136 alarm is triggered if the voltage has crossed a programmable minimum or
137 maximum limit. Note that minimum in this case always means 'closest to
138 zero'; this is important for negative voltage measurements. All voltage
139 inputs can measure voltages between 0 and 4.08 volts, with a resolution of
140 0.016 volt (except IT8721F/IT8758E and IT8728F: 0.012 volt.) The battery
141 voltage in8 does not have limit registers.
143 On the IT8721F/IT8758E, IT8782F, and IT8783E/F, some voltage inputs are
144 internal and scaled inside the chip (in7 (optional for IT8782F and IT8783E/F),
145 in8 and optionally in3). The driver handles this transparently so user-space
146 doesn't have to care.
148 The VID lines (IT8712F/IT8716F/IT8718F/IT8720F) encode the core voltage value:
149 the voltage level your processor should work with. This is hardcoded by
150 the mainboard and/or processor itself. It is a value in volts.
152 If an alarm triggers, it will remain triggered until the hardware register
153 is read at least once. This means that the cause for the alarm may already
154 have disappeared! Note that in the current implementation, all hardware
155 registers are read whenever any data is read (unless it is less than 1.5
156 seconds since the last update). This means that you can easily miss
157 once-only alarms.
159 Out-of-limit readings can also result in beeping, if the chip is properly
160 wired and configured. Beeping can be enabled or disabled per sensor type
161 (temperatures, voltages and fans.)
163 The IT87xx only updates its values each 1.5 seconds; reading it more often
164 will do no harm, but will return 'old' values.
166 To change sensor N to a thermistor, 'echo 4 > tempN_type' where N is 1, 2,
167 or 3. To change sensor N to a thermal diode, 'echo 3 > tempN_type'.
168 Give 0 for unused sensor. Any other value is invalid. To configure this at
169 startup, consult lm_sensors's /etc/sensors.conf. (4 = thermistor;
170 3 = thermal diode)
173 Fan speed control
174 -----------------
176 The fan speed control features are limited to manual PWM mode. Automatic
177 "Smart Guardian" mode control handling is only implemented for older chips
178 (see below.) However if you want to go for "manual mode" just write 1 to
179 pwmN_enable.
181 If you are only able to control the fan speed with very small PWM values,
182 try lowering the PWM base frequency (pwm1_freq). Depending on the fan,
183 it may give you a somewhat greater control range. The same frequency is
184 used to drive all fan outputs, which is why pwm2_freq and pwm3_freq are
185 read-only.
188 Automatic fan speed control (old interface)
189 -------------------------------------------
191 The driver supports the old interface to automatic fan speed control
192 which is implemented by IT8705F chips up to revision F and IT8712F
193 chips up to revision G.
195 This interface implements 4 temperature vs. PWM output trip points.
196 The PWM output of trip point 4 is always the maximum value (fan running
197 at full speed) while the PWM output of the other 3 trip points can be
198 freely chosen. The temperature of all 4 trip points can be freely chosen.
199 Additionally, trip point 1 has an hysteresis temperature attached, to
200 prevent fast switching between fan on and off.
202 The chip automatically computes the PWM output value based on the input
203 temperature, based on this simple rule: if the temperature value is
204 between trip point N and trip point N+1 then the PWM output value is
205 the one of trip point N. The automatic control mode is less flexible
206 than the manual control mode, but it reacts faster, is more robust and
207 doesn't use CPU cycles.
209 Trip points must be set properly before switching to automatic fan speed
210 control mode. The driver will perform basic integrity checks before
211 actually switching to automatic control mode.
214 Temperature offset attributes
215 -----------------------------
217 The driver supports temp[1-3]_offset sysfs attributes to adjust the reported
218 temperature for thermal diodes or diode-connected thermal transistors.
219 If a temperature sensor is configured for thermistors, the attribute values
220 are ignored. If the thermal sensor type is Intel PECI, the temperature offset
221 must be programmed to the critical CPU temperature.