1 Pulse Width Modulation (PWM) interface
3 This provides an overview about the Linux PWM interface
5 PWMs are commonly used for controlling LEDs, fans or vibrators in
6 cell phones. PWMs with a fixed purpose have no need implementing
7 the Linux PWM API (although they could). However, PWMs are often
8 found as discrete devices on SoCs which have no fixed purpose. It's
9 up to the board designer to connect them to LEDs or fans. To provide
10 this kind of flexibility the generic PWM API exists.
12 Identifying PWMs
13 ----------------
15 Users of the legacy PWM API use unique IDs to refer to PWM devices.
17 Instead of referring to a PWM device via its unique ID, board setup code
18 should instead register a static mapping that can be used to match PWM
19 consumers to providers, as given in the following example:
21 static struct pwm_lookup board_pwm_lookup[] = {
22 PWM_LOOKUP("tegra-pwm", 0, "pwm-backlight", NULL),
23 };
25 static void __init board_init(void)
26 {
27 ...
28 pwm_add_table(board_pwm_lookup, ARRAY_SIZE(board_pwm_lookup));
29 ...
30 }
32 Using PWMs
33 ----------
35 Legacy users can request a PWM device using pwm_request() and free it
36 after usage with pwm_free().
38 New users should use the pwm_get() function and pass to it the consumer
39 device or a consumer name. pwm_put() is used to free the PWM device. Managed
40 variants of these functions, devm_pwm_get() and devm_pwm_put(), also exist.
42 After being requested a PWM has to be configured using:
44 int pwm_config(struct pwm_device *pwm, int duty_ns, int period_ns);
46 To start/stop toggling the PWM output use pwm_enable()/pwm_disable().
48 Implementing a PWM driver
49 -------------------------
51 Currently there are two ways to implement pwm drivers. Traditionally
52 there only has been the barebone API meaning that each driver has
53 to implement the pwm_*() functions itself. This means that it's impossible
54 to have multiple PWM drivers in the system. For this reason it's mandatory
55 for new drivers to use the generic PWM framework.
57 A new PWM controller/chip can be added using pwmchip_add() and removed
58 again with pwmchip_remove(). pwmchip_add() takes a filled in struct
59 pwm_chip as argument which provides a description of the PWM chip, the
60 number of PWM devices provider by the chip and the chip-specific
61 implementation of the supported PWM operations to the framework.
63 Locking
64 -------
66 The PWM core list manipulations are protected by a mutex, so pwm_request()
67 and pwm_free() may not be called from an atomic context. Currently the
68 PWM core does not enforce any locking to pwm_enable(), pwm_disable() and
69 pwm_config(), so the calling context is currently driver specific. This
70 is an issue derived from the former barebone API and should be fixed soon.
72 Helpers
73 -------
75 Currently a PWM can only be configured with period_ns and duty_ns. For several
76 use cases freq_hz and duty_percent might be better. Instead of calculating
77 this in your driver please consider adding appropriate helpers to the framework.