2 Real Time Clock (RTC) Drivers for Linux
3 =======================================
5 When Linux developers talk about a "Real Time Clock", they usually mean
6 something that tracks wall clock time and is battery backed so that it
7 works even with system power off. Such clocks will normally not track
8 the local time zone or daylight savings time -- unless they dual boot
9 with MS-Windows -- but will instead be set to Coordinated Universal Time
10 (UTC, formerly "Greenwich Mean Time").
12 The newest non-PC hardware tends to just count seconds, like the time(2)
13 system call reports, but RTCs also very commonly represent time using
14 the Gregorian calendar and 24 hour time, as reported by gmtime(3).
16 Linux has two largely-compatible userspace RTC API families you may
17 need to know about:
19 * /dev/rtc ... is the RTC provided by PC compatible systems,
20 so it's not very portable to non-x86 systems.
22 * /dev/rtc0, /dev/rtc1 ... are part of a framework that's
23 supported by a wide variety of RTC chips on all systems.
25 Programmers need to understand that the PC/AT functionality is not
26 always available, and some systems can do much more. That is, the
27 RTCs use the same API to make requests in both RTC frameworks (using
28 different filenames of course), but the hardware may not offer the
29 same functionality. For example, not every RTC is hooked up to an
30 IRQ, so they can't all issue alarms; and where standard PC RTCs can
31 only issue an alarm up to 24 hours in the future, other hardware may
32 be able to schedule one any time in the upcoming century.
35 Old PC/AT-Compatible driver: /dev/rtc
36 --------------------------------------
38 All PCs (even Alpha machines) have a Real Time Clock built into them.
39 Usually they are built into the chipset of the computer, but some may
40 actually have a Motorola MC146818 (or clone) on the board. This is the
41 clock that keeps the date and time while your computer is turned off.
43 ACPI has standardized that MC146818 functionality, and extended it in
44 a few ways (enabling longer alarm periods, and wake-from-hibernate).
45 That functionality is NOT exposed in the old driver.
47 However it can also be used to generate signals from a slow 2Hz to a
48 relatively fast 8192Hz, in increments of powers of two. These signals
49 are reported by interrupt number 8. (Oh! So *that* is what IRQ 8 is
50 for...) It can also function as a 24hr alarm, raising IRQ 8 when the
51 alarm goes off. The alarm can also be programmed to only check any
52 subset of the three programmable values, meaning that it could be set to
53 ring on the 30th second of the 30th minute of every hour, for example.
54 The clock can also be set to generate an interrupt upon every clock
55 update, thus generating a 1Hz signal.
57 The interrupts are reported via /dev/rtc (major 10, minor 135, read only
58 character device) in the form of an unsigned long. The low byte contains
59 the type of interrupt (update-done, alarm-rang, or periodic) that was
60 raised, and the remaining bytes contain the number of interrupts since
61 the last read. Status information is reported through the pseudo-file
62 /proc/driver/rtc if the /proc filesystem was enabled. The driver has
63 built in locking so that only one process is allowed to have the /dev/rtc
64 interface open at a time.
66 A user process can monitor these interrupts by doing a read(2) or a
67 select(2) on /dev/rtc -- either will block/stop the user process until
68 the next interrupt is received. This is useful for things like
69 reasonably high frequency data acquisition where one doesn't want to
70 burn up 100% CPU by polling gettimeofday etc. etc.
72 At high frequencies, or under high loads, the user process should check
73 the number of interrupts received since the last read to determine if
74 there has been any interrupt "pileup" so to speak. Just for reference, a
75 typical 486-33 running a tight read loop on /dev/rtc will start to suffer
76 occasional interrupt pileup (i.e. > 1 IRQ event since last read) for
77 frequencies above 1024Hz. So you really should check the high bytes
78 of the value you read, especially at frequencies above that of the
79 normal timer interrupt, which is 100Hz.
81 Programming and/or enabling interrupt frequencies greater than 64Hz is
82 only allowed by root. This is perhaps a bit conservative, but we don't want
83 an evil user generating lots of IRQs on a slow 386sx-16, where it might have
84 a negative impact on performance. This 64Hz limit can be changed by writing
85 a different value to /proc/sys/dev/rtc/max-user-freq. Note that the
86 interrupt handler is only a few lines of code to minimize any possibility
87 of this effect.
89 Also, if the kernel time is synchronized with an external source, the
90 kernel will write the time back to the CMOS clock every 11 minutes. In
91 the process of doing this, the kernel briefly turns off RTC periodic
92 interrupts, so be aware of this if you are doing serious work. If you
93 don't synchronize the kernel time with an external source (via ntp or
94 whatever) then the kernel will keep its hands off the RTC, allowing you
95 exclusive access to the device for your applications.
97 The alarm and/or interrupt frequency are programmed into the RTC via
98 various ioctl(2) calls as listed in ./include/linux/rtc.h
99 Rather than write 50 pages describing the ioctl() and so on, it is
100 perhaps more useful to include a small test program that demonstrates
101 how to use them, and demonstrates the features of the driver. This is
102 probably a lot more useful to people interested in writing applications
103 that will be using this driver. See the code at the end of this document.
105 (The original /dev/rtc driver was written by Paul Gortmaker.)
108 New portable "RTC Class" drivers: /dev/rtcN
109 --------------------------------------------
111 Because Linux supports many non-ACPI and non-PC platforms, some of which
112 have more than one RTC style clock, it needed a more portable solution
113 than expecting a single battery-backed MC146818 clone on every system.
114 Accordingly, a new "RTC Class" framework has been defined. It offers
115 three different userspace interfaces:
117 * /dev/rtcN ... much the same as the older /dev/rtc interface
119 * /sys/class/rtc/rtcN ... sysfs attributes support readonly
120 access to some RTC attributes.
122 * /proc/driver/rtc ... the system clock RTC may expose itself
123 using a procfs interface. If there is no RTC for the system clock,
124 rtc0 is used by default. More information is (currently) shown
125 here than through sysfs.
127 The RTC Class framework supports a wide variety of RTCs, ranging from those
128 integrated into embeddable system-on-chip (SOC) processors to discrete chips
129 using I2C, SPI, or some other bus to communicate with the host CPU. There's
130 even support for PC-style RTCs ... including the features exposed on newer PCs
131 through ACPI.
133 The new framework also removes the "one RTC per system" restriction. For
134 example, maybe the low-power battery-backed RTC is a discrete I2C chip, but
135 a high functionality RTC is integrated into the SOC. That system might read
136 the system clock from the discrete RTC, but use the integrated one for all
137 other tasks, because of its greater functionality.
139 SYSFS INTERFACE
140 ---------------
142 The sysfs interface under /sys/class/rtc/rtcN provides access to various
143 rtc attributes without requiring the use of ioctls. All dates and times
144 are in the RTC's timezone, rather than in system time.
146 date: RTC-provided date
147 hctosys: 1 if the RTC provided the system time at boot via the
148 CONFIG_RTC_HCTOSYS kernel option, 0 otherwise
149 max_user_freq: The maximum interrupt rate an unprivileged user may request
150 from this RTC.
151 name: The name of the RTC corresponding to this sysfs directory
152 since_epoch: The number of seconds since the epoch according to the RTC
153 time: RTC-provided time
154 wakealarm: The time at which the clock will generate a system wakeup
155 event. This is a one shot wakeup event, so must be reset
156 after wake if a daily wakeup is required. Format is either
157 seconds since the epoch or, if there's a leading +, seconds
158 in the future.
160 IOCTL INTERFACE
161 ---------------
163 The ioctl() calls supported by /dev/rtc are also supported by the RTC class
164 framework. However, because the chips and systems are not standardized,
165 some PC/AT functionality might not be provided. And in the same way, some
166 newer features -- including those enabled by ACPI -- are exposed by the
167 RTC class framework, but can't be supported by the older driver.
169 * RTC_RD_TIME, RTC_SET_TIME ... every RTC supports at least reading
170 time, returning the result as a Gregorian calendar date and 24 hour
171 wall clock time. To be most useful, this time may also be updated.
173 * RTC_AIE_ON, RTC_AIE_OFF, RTC_ALM_SET, RTC_ALM_READ ... when the RTC
174 is connected to an IRQ line, it can often issue an alarm IRQ up to
175 24 hours in the future. (Use RTC_WKALM_* by preference.)
177 * RTC_WKALM_SET, RTC_WKALM_RD ... RTCs that can issue alarms beyond
178 the next 24 hours use a slightly more powerful API, which supports
179 setting the longer alarm time and enabling its IRQ using a single
180 request (using the same model as EFI firmware).
182 * RTC_UIE_ON, RTC_UIE_OFF ... if the RTC offers IRQs, the RTC framework
183 will emulate this mechanism.
185 * RTC_PIE_ON, RTC_PIE_OFF, RTC_IRQP_SET, RTC_IRQP_READ ... these icotls
186 are emulated via a kernel hrtimer.
188 In many cases, the RTC alarm can be a system wake event, used to force
189 Linux out of a low power sleep state (or hibernation) back to a fully
190 operational state. For example, a system could enter a deep power saving
191 state until it's time to execute some scheduled tasks.
193 Note that many of these ioctls are handled by the common rtc-dev interface.
194 Some common examples:
196 * RTC_RD_TIME, RTC_SET_TIME: the read_time/set_time functions will be
197 called with appropriate values.
199 * RTC_ALM_SET, RTC_ALM_READ, RTC_WKALM_SET, RTC_WKALM_RD: gets or sets
200 the alarm rtc_timer. May call the set_alarm driver function.
202 * RTC_IRQP_SET, RTC_IRQP_READ: These are emulated by the generic code.
204 * RTC_PIE_ON, RTC_PIE_OFF: These are also emulated by the generic code.
206 If all else fails, check out the rtc-test.c driver!
209 -------------------- 8< ---------------- 8< -----------------------------
211 /*
212 * Real Time Clock Driver Test/Example Program
213 *
214 * Compile with:
215 * gcc -s -Wall -Wstrict-prototypes rtctest.c -o rtctest
216 *
217 * Copyright (C) 1996, Paul Gortmaker.
218 *
219 * Released under the GNU General Public License, version 2,
220 * included herein by reference.
221 *
222 */
224 #include <stdio.h>
225 #include <linux/rtc.h>
226 #include <sys/ioctl.h>
227 #include <sys/time.h>
228 #include <sys/types.h>
229 #include <fcntl.h>
230 #include <unistd.h>
231 #include <stdlib.h>
232 #include <errno.h>
235 /*
236 * This expects the new RTC class driver framework, working with
237 * clocks that will often not be clones of what the PC-AT had.
238 * Use the command line to specify another RTC if you need one.
239 */
240 static const char default_rtc[] = "/dev/rtc0";
243 int main(int argc, char **argv)
244 {
245 int i, fd, retval, irqcount = 0;
246 unsigned long tmp, data;
247 struct rtc_time rtc_tm;
248 const char *rtc = default_rtc;
250 switch (argc) {
251 case 2:
252 rtc = argv[1];
253 /* FALLTHROUGH */
254 case 1:
255 break;
256 default:
257 fprintf(stderr, "usage: rtctest [rtcdev]\n");
258 return 1;
259 }
261 fd = open(rtc, O_RDONLY);
263 if (fd == -1) {
264 perror(rtc);
265 exit(errno);
266 }
268 fprintf(stderr, "\n\t\t\tRTC Driver Test Example.\n\n");
270 /* Turn on update interrupts (one per second) */
271 retval = ioctl(fd, RTC_UIE_ON, 0);
272 if (retval == -1) {
273 if (errno == ENOTTY) {
274 fprintf(stderr,
275 "\n...Update IRQs not supported.\n");
276 goto test_READ;
277 }
278 perror("RTC_UIE_ON ioctl");
279 exit(errno);
280 }
282 fprintf(stderr, "Counting 5 update (1/sec) interrupts from reading %s:",
283 rtc);
284 fflush(stderr);
285 for (i=1; i<6; i++) {
286 /* This read will block */
287 retval = read(fd, &data, sizeof(unsigned long));
288 if (retval == -1) {
289 perror("read");
290 exit(errno);
291 }
292 fprintf(stderr, " %d",i);
293 fflush(stderr);
294 irqcount++;
295 }
297 fprintf(stderr, "\nAgain, from using select(2) on /dev/rtc:");
298 fflush(stderr);
299 for (i=1; i<6; i++) {
300 struct timeval tv = {5, 0}; /* 5 second timeout on select */
301 fd_set readfds;
303 FD_ZERO(&readfds);
304 FD_SET(fd, &readfds);
305 /* The select will wait until an RTC interrupt happens. */
306 retval = select(fd+1, &readfds, NULL, NULL, &tv);
307 if (retval == -1) {
308 perror("select");
309 exit(errno);
310 }
311 /* This read won't block unlike the select-less case above. */
312 retval = read(fd, &data, sizeof(unsigned long));
313 if (retval == -1) {
314 perror("read");
315 exit(errno);
316 }
317 fprintf(stderr, " %d",i);
318 fflush(stderr);
319 irqcount++;
320 }
322 /* Turn off update interrupts */
323 retval = ioctl(fd, RTC_UIE_OFF, 0);
324 if (retval == -1) {
325 perror("RTC_UIE_OFF ioctl");
326 exit(errno);
327 }
329 test_READ:
330 /* Read the RTC time/date */
331 retval = ioctl(fd, RTC_RD_TIME, &rtc_tm);
332 if (retval == -1) {
333 perror("RTC_RD_TIME ioctl");
334 exit(errno);
335 }
337 fprintf(stderr, "\n\nCurrent RTC date/time is %d-%d-%d, %02d:%02d:%02d.\n",
338 rtc_tm.tm_mday, rtc_tm.tm_mon + 1, rtc_tm.tm_year + 1900,
339 rtc_tm.tm_hour, rtc_tm.tm_min, rtc_tm.tm_sec);
341 /* Set the alarm to 5 sec in the future, and check for rollover */
342 rtc_tm.tm_sec += 5;
343 if (rtc_tm.tm_sec >= 60) {
344 rtc_tm.tm_sec %= 60;
345 rtc_tm.tm_min++;
346 }
347 if (rtc_tm.tm_min == 60) {
348 rtc_tm.tm_min = 0;
349 rtc_tm.tm_hour++;
350 }
351 if (rtc_tm.tm_hour == 24)
352 rtc_tm.tm_hour = 0;
354 retval = ioctl(fd, RTC_ALM_SET, &rtc_tm);
355 if (retval == -1) {
356 if (errno == ENOTTY) {
357 fprintf(stderr,
358 "\n...Alarm IRQs not supported.\n");
359 goto test_PIE;
360 }
361 perror("RTC_ALM_SET ioctl");
362 exit(errno);
363 }
365 /* Read the current alarm settings */
366 retval = ioctl(fd, RTC_ALM_READ, &rtc_tm);
367 if (retval == -1) {
368 perror("RTC_ALM_READ ioctl");
369 exit(errno);
370 }
372 fprintf(stderr, "Alarm time now set to %02d:%02d:%02d.\n",
373 rtc_tm.tm_hour, rtc_tm.tm_min, rtc_tm.tm_sec);
375 /* Enable alarm interrupts */
376 retval = ioctl(fd, RTC_AIE_ON, 0);
377 if (retval == -1) {
378 perror("RTC_AIE_ON ioctl");
379 exit(errno);
380 }
382 fprintf(stderr, "Waiting 5 seconds for alarm...");
383 fflush(stderr);
384 /* This blocks until the alarm ring causes an interrupt */
385 retval = read(fd, &data, sizeof(unsigned long));
386 if (retval == -1) {
387 perror("read");
388 exit(errno);
389 }
390 irqcount++;
391 fprintf(stderr, " okay. Alarm rang.\n");
393 /* Disable alarm interrupts */
394 retval = ioctl(fd, RTC_AIE_OFF, 0);
395 if (retval == -1) {
396 perror("RTC_AIE_OFF ioctl");
397 exit(errno);
398 }
400 test_PIE:
401 /* Read periodic IRQ rate */
402 retval = ioctl(fd, RTC_IRQP_READ, &tmp);
403 if (retval == -1) {
404 /* not all RTCs support periodic IRQs */
405 if (errno == ENOTTY) {
406 fprintf(stderr, "\nNo periodic IRQ support\n");
407 goto done;
408 }
409 perror("RTC_IRQP_READ ioctl");
410 exit(errno);
411 }
412 fprintf(stderr, "\nPeriodic IRQ rate is %ldHz.\n", tmp);
414 fprintf(stderr, "Counting 20 interrupts at:");
415 fflush(stderr);
417 /* The frequencies 128Hz, 256Hz, ... 8192Hz are only allowed for root. */
418 for (tmp=2; tmp<=64; tmp*=2) {
420 retval = ioctl(fd, RTC_IRQP_SET, tmp);
421 if (retval == -1) {
422 /* not all RTCs can change their periodic IRQ rate */
423 if (errno == ENOTTY) {
424 fprintf(stderr,
425 "\n...Periodic IRQ rate is fixed\n");
426 goto done;
427 }
428 perror("RTC_IRQP_SET ioctl");
429 exit(errno);
430 }
432 fprintf(stderr, "\n%ldHz:\t", tmp);
433 fflush(stderr);
435 /* Enable periodic interrupts */
436 retval = ioctl(fd, RTC_PIE_ON, 0);
437 if (retval == -1) {
438 perror("RTC_PIE_ON ioctl");
439 exit(errno);
440 }
442 for (i=1; i<21; i++) {
443 /* This blocks */
444 retval = read(fd, &data, sizeof(unsigned long));
445 if (retval == -1) {
446 perror("read");
447 exit(errno);
448 }
449 fprintf(stderr, " %d",i);
450 fflush(stderr);
451 irqcount++;
452 }
454 /* Disable periodic interrupts */
455 retval = ioctl(fd, RTC_PIE_OFF, 0);
456 if (retval == -1) {
457 perror("RTC_PIE_OFF ioctl");
458 exit(errno);
459 }
460 }
462 done:
463 fprintf(stderr, "\n\n\t\t\t *** Test complete ***\n");
465 close(fd);
467 return 0;
468 }