]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - Documentation/serial-console.txt
ARM: dts: dra72: enable dss node
[android-sdk/kernel-video.git] / Documentation / serial-console.txt
1                        Linux Serial Console
3 To use a serial port as console you need to compile the support into your
4 kernel - by default it is not compiled in. For PC style serial ports
5 it's the config option next to "Standard/generic (dumb) serial support".
6 You must compile serial support into the kernel and not as a module.
8 It is possible to specify multiple devices for console output. You can
9 define a new kernel command line option to select which device(s) to
10 use for console output.
12 The format of this option is:
14         console=device,options
16         device:         tty0 for the foreground virtual console
17                         ttyX for any other virtual console
18                         ttySx for a serial port
19                         lp0 for the first parallel port
20                         ttyUSB0 for the first USB serial device
22         options:        depend on the driver. For the serial port this
23                         defines the baudrate/parity/bits/flow control of
24                         the port, in the format BBBBPNF, where BBBB is the
25                         speed, P is parity (n/o/e), N is number of bits,
26                         and F is flow control ('r' for RTS). Default is
27                         9600n8. The maximum baudrate is 115200.
29 You can specify multiple console= options on the kernel command line.
30 Output will appear on all of them. The last device will be used when
31 you open /dev/console. So, for example:
33         console=ttyS1,9600 console=tty0
35 defines that opening /dev/console will get you the current foreground
36 virtual console, and kernel messages will appear on both the VGA
37 console and the 2nd serial port (ttyS1 or COM2) at 9600 baud.
39 Note that you can only define one console per device type (serial, video).
41 If no console device is specified, the first device found capable of
42 acting as a system console will be used. At this time, the system
43 first looks for a VGA card and then for a serial port. So if you don't
44 have a VGA card in your system the first serial port will automatically
45 become the console.
47 You will need to create a new device to use /dev/console. The official
48 /dev/console is now character device 5,1.
50 (You can also use a network device as a console.  See
51 Documentation/networking/netconsole.txt for information on that.)
53 Here's an example that will use /dev/ttyS1 (COM2) as the console.
54 Replace the sample values as needed.
56 1. Create /dev/console (real console) and /dev/tty0 (master virtual
57    console):
59    cd /dev
60    rm -f console tty0
61    mknod -m 622 console c 5 1
62    mknod -m 622 tty0 c 4 0
64 2. LILO can also take input from a serial device. This is a very
65    useful option. To tell LILO to use the serial port:
66    In lilo.conf (global section): 
68    serial  = 1,9600n8 (ttyS1, 9600 bd, no parity, 8 bits)
70 3. Adjust to kernel flags for the new kernel,
71    again in lilo.conf (kernel section)
73    append = "console=ttyS1,9600" 
75 4. Make sure a getty runs on the serial port so that you can login to
76    it once the system is done booting. This is done by adding a line
77    like this to /etc/inittab (exact syntax depends on your getty):
79    S1:23:respawn:/sbin/getty -L ttyS1 9600 vt100
81 5. Init and /etc/ioctl.save
83    Sysvinit remembers its stty settings in a file in /etc, called
84    `/etc/ioctl.save'. REMOVE THIS FILE before using the serial
85    console for the first time, because otherwise init will probably
86    set the baudrate to 38400 (baudrate of the virtual console).
88 6. /dev/console and X
89    Programs that want to do something with the virtual console usually
90    open /dev/console. If you have created the new /dev/console device,
91    and your console is NOT the virtual console some programs will fail.
92    Those are programs that want to access the VT interface, and use
93    /dev/console instead of /dev/tty0. Some of those programs are:
95    Xfree86, svgalib, gpm, SVGATextMode
97    It should be fixed in modern versions of these programs though.
99    Note that if you boot without a console= option (or with
100    console=/dev/tty0), /dev/console is the same as /dev/tty0. In that
101    case everything will still work.
103 7. Thanks
105    Thanks to Geert Uytterhoeven <geert@linux-m68k.org>
106    for porting the patches from 2.1.4x to 2.1.6x for taking care of
107    the integration of these patches into m68k, ppc and alpha.
109 Miquel van Smoorenburg <miquels@cistron.nl>, 11-Jun-2000