1 Lesson 1: Spin locks
3 The most basic primitive for locking is spinlock.
5 static DEFINE_SPINLOCK(xxx_lock);
7 unsigned long flags;
9 spin_lock_irqsave(&xxx_lock, flags);
10 ... critical section here ..
11 spin_unlock_irqrestore(&xxx_lock, flags);
13 The above is always safe. It will disable interrupts _locally_, but the
14 spinlock itself will guarantee the global lock, so it will guarantee that
15 there is only one thread-of-control within the region(s) protected by that
16 lock. This works well even under UP also, so the code does _not_ need to
17 worry about UP vs SMP issues: the spinlocks work correctly under both.
19 NOTE! Implications of spin_locks for memory are further described in:
21 Documentation/memory-barriers.txt
22 (5) LOCK operations.
23 (6) UNLOCK operations.
25 The above is usually pretty simple (you usually need and want only one
26 spinlock for most things - using more than one spinlock can make things a
27 lot more complex and even slower and is usually worth it only for
28 sequences that you _know_ need to be split up: avoid it at all cost if you
29 aren't sure).
31 This is really the only really hard part about spinlocks: once you start
32 using spinlocks they tend to expand to areas you might not have noticed
33 before, because you have to make sure the spinlocks correctly protect the
34 shared data structures _everywhere_ they are used. The spinlocks are most
35 easily added to places that are completely independent of other code (for
36 example, internal driver data structures that nobody else ever touches).
38 NOTE! The spin-lock is safe only when you _also_ use the lock itself
39 to do locking across CPU's, which implies that EVERYTHING that
40 touches a shared variable has to agree about the spinlock they want
41 to use.
43 ----
45 Lesson 2: reader-writer spinlocks.
47 If your data accesses have a very natural pattern where you usually tend
48 to mostly read from the shared variables, the reader-writer locks
49 (rw_lock) versions of the spinlocks are sometimes useful. They allow multiple
50 readers to be in the same critical region at once, but if somebody wants
51 to change the variables it has to get an exclusive write lock.
53 NOTE! reader-writer locks require more atomic memory operations than
54 simple spinlocks. Unless the reader critical section is long, you
55 are better off just using spinlocks.
57 The routines look the same as above:
59 rwlock_t xxx_lock = __RW_LOCK_UNLOCKED(xxx_lock);
61 unsigned long flags;
63 read_lock_irqsave(&xxx_lock, flags);
64 .. critical section that only reads the info ...
65 read_unlock_irqrestore(&xxx_lock, flags);
67 write_lock_irqsave(&xxx_lock, flags);
68 .. read and write exclusive access to the info ...
69 write_unlock_irqrestore(&xxx_lock, flags);
71 The above kind of lock may be useful for complex data structures like
72 linked lists, especially searching for entries without changing the list
73 itself. The read lock allows many concurrent readers. Anything that
74 _changes_ the list will have to get the write lock.
76 NOTE! RCU is better for list traversal, but requires careful
77 attention to design detail (see Documentation/RCU/listRCU.txt).
79 Also, you cannot "upgrade" a read-lock to a write-lock, so if you at _any_
80 time need to do any changes (even if you don't do it every time), you have
81 to get the write-lock at the very beginning.
83 NOTE! We are working hard to remove reader-writer spinlocks in most
84 cases, so please don't add a new one without consensus. (Instead, see
85 Documentation/RCU/rcu.txt for complete information.)
87 ----
89 Lesson 3: spinlocks revisited.
91 The single spin-lock primitives above are by no means the only ones. They
92 are the most safe ones, and the ones that work under all circumstances,
93 but partly _because_ they are safe they are also fairly slow. They are slower
94 than they'd need to be, because they do have to disable interrupts
95 (which is just a single instruction on a x86, but it's an expensive one -
96 and on other architectures it can be worse).
98 If you have a case where you have to protect a data structure across
99 several CPU's and you want to use spinlocks you can potentially use
100 cheaper versions of the spinlocks. IFF you know that the spinlocks are
101 never used in interrupt handlers, you can use the non-irq versions:
103 spin_lock(&lock);
104 ...
105 spin_unlock(&lock);
107 (and the equivalent read-write versions too, of course). The spinlock will
108 guarantee the same kind of exclusive access, and it will be much faster.
109 This is useful if you know that the data in question is only ever
110 manipulated from a "process context", ie no interrupts involved.
112 The reasons you mustn't use these versions if you have interrupts that
113 play with the spinlock is that you can get deadlocks:
115 spin_lock(&lock);
116 ...
117 <- interrupt comes in:
118 spin_lock(&lock);
120 where an interrupt tries to lock an already locked variable. This is ok if
121 the other interrupt happens on another CPU, but it is _not_ ok if the
122 interrupt happens on the same CPU that already holds the lock, because the
123 lock will obviously never be released (because the interrupt is waiting
124 for the lock, and the lock-holder is interrupted by the interrupt and will
125 not continue until the interrupt has been processed).
127 (This is also the reason why the irq-versions of the spinlocks only need
128 to disable the _local_ interrupts - it's ok to use spinlocks in interrupts
129 on other CPU's, because an interrupt on another CPU doesn't interrupt the
130 CPU that holds the lock, so the lock-holder can continue and eventually
131 releases the lock).
133 Note that you can be clever with read-write locks and interrupts. For
134 example, if you know that the interrupt only ever gets a read-lock, then
135 you can use a non-irq version of read locks everywhere - because they
136 don't block on each other (and thus there is no dead-lock wrt interrupts.
137 But when you do the write-lock, you have to use the irq-safe version.
139 For an example of being clever with rw-locks, see the "waitqueue_lock"
140 handling in kernel/sched.c - nothing ever _changes_ a wait-queue from
141 within an interrupt, they only read the queue in order to know whom to
142 wake up. So read-locks are safe (which is good: they are very common
143 indeed), while write-locks need to protect themselves against interrupts.
145 Linus
147 ----
149 Reference information:
151 For dynamic initialization, use spin_lock_init() or rwlock_init() as
152 appropriate:
154 spinlock_t xxx_lock;
155 rwlock_t xxx_rw_lock;
157 static int __init xxx_init(void)
158 {
159 spin_lock_init(&xxx_lock);
160 rwlock_init(&xxx_rw_lock);
161 ...
162 }
164 module_init(xxx_init);
166 For static initialization, use DEFINE_SPINLOCK() / DEFINE_RWLOCK() or
167 __SPIN_LOCK_UNLOCKED() / __RW_LOCK_UNLOCKED() as appropriate.