1 Motivation:
3 In complicated DMA pipelines such as graphics (multimedia, camera, gpu, display)
4 a consumer of a buffer needs to know when the producer has finished producing
5 it. Likewise the producer needs to know when the consumer is finished with the
6 buffer so it can reuse it. A particular buffer may be consumed by multiple
7 consumers which will retain the buffer for different amounts of time. In
8 addition, a consumer may consume multiple buffers atomically.
9 The sync framework adds an API which allows synchronization between the
10 producers and consumers in a generic way while also allowing platforms which
11 have shared hardware synchronization primitives to exploit them.
13 Goals:
14 * provide a generic API for expressing synchronization dependencies
15 * allow drivers to exploit hardware synchronization between hardware
16 blocks
17 * provide a userspace API that allows a compositor to manage
18 dependencies.
19 * provide rich telemetry data to allow debugging slowdowns and stalls of
20 the graphics pipeline.
22 Objects:
23 * sync_timeline
24 * sync_pt
25 * sync_fence
27 sync_timeline:
29 A sync_timeline is an abstract monotonically increasing counter. In general,
30 each driver/hardware block context will have one of these. They can be backed
31 by the appropriate hardware or rely on the generic sw_sync implementation.
32 Timelines are only ever created through their specific implementations
33 (i.e. sw_sync.)
35 sync_pt:
37 A sync_pt is an abstract value which marks a point on a sync_timeline. Sync_pts
38 have a single timeline parent. They have 3 states: active, signaled, and error.
39 They start in active state and transition, once, to either signaled (when the
40 timeline counter advances beyond the sync_pt’s value) or error state.
42 sync_fence:
44 Sync_fences are the primary primitives used by drivers to coordinate
45 synchronization of their buffers. They are a collection of sync_pts which may
46 or may not have the same timeline parent. A sync_pt can only exist in one fence
47 and the fence's list of sync_pts is immutable once created. Fences can be
48 waited on synchronously or asynchronously. Two fences can also be merged to
49 create a third fence containing a copy of the two fences’ sync_pts. Fences are
50 backed by file descriptors to allow userspace to coordinate the display pipeline
51 dependencies.
53 Use:
55 A driver implementing sync support should have a work submission function which:
56 * takes a fence argument specifying when to begin work
57 * asynchronously queues that work to kick off when the fence is signaled
58 * returns a fence to indicate when its work will be done.
59 * signals the returned fence once the work is completed.
61 Consider an imaginary display driver that has the following API:
62 /*
63 * assumes buf is ready to be displayed.
64 * blocks until the buffer is on screen.
65 */
66 void display_buffer(struct dma_buf *buf);
68 The new API will become:
69 /*
70 * will display buf when fence is signaled.
71 * returns immediately with a fence that will signal when buf
72 * is no longer displayed.
73 */
74 struct sync_fence* display_buffer(struct dma_buf *buf,
75 struct sync_fence *fence);