1 Documentation for /proc/sys/kernel/* kernel version 2.2.10
2 (c) 1998, 1999, Rik van Riel <riel@nl.linux.org>
3 (c) 2009, Shen Feng<shen@cn.fujitsu.com>
5 For general info and legal blurb, please look in README.
7 ==============================================================
9 This file contains documentation for the sysctl files in
10 /proc/sys/kernel/ and is valid for Linux kernel version 2.2.
12 The files in this directory can be used to tune and monitor
13 miscellaneous and general things in the operation of the Linux
14 kernel. Since some of the files _can_ be used to screw up your
15 system, it is advisable to read both documentation and source
16 before actually making adjustments.
18 Currently, these files might (depending on your configuration)
19 show up in /proc/sys/kernel:
21 - acct
22 - acpi_video_flags
23 - auto_msgmni
24 - bootloader_type [ X86 only ]
25 - bootloader_version [ X86 only ]
26 - callhome [ S390 only ]
27 - cap_last_cap
28 - core_pattern
29 - core_pipe_limit
30 - core_uses_pid
31 - ctrl-alt-del
32 - dmesg_restrict
33 - domainname
34 - hostname
35 - hotplug
36 - kptr_restrict
37 - kstack_depth_to_print [ X86 only ]
38 - l2cr [ PPC only ]
39 - modprobe ==> Documentation/debugging-modules.txt
40 - modules_disabled
41 - msg_next_id [ sysv ipc ]
42 - msgmax
43 - msgmnb
44 - msgmni
45 - nmi_watchdog
46 - osrelease
47 - ostype
48 - overflowgid
49 - overflowuid
50 - panic
51 - panic_on_oops
52 - panic_on_unrecovered_nmi
53 - panic_on_stackoverflow
54 - pid_max
55 - powersave-nap [ PPC only ]
56 - printk
57 - printk_delay
58 - printk_ratelimit
59 - printk_ratelimit_burst
60 - randomize_va_space
61 - real-root-dev ==> Documentation/initrd.txt
62 - reboot-cmd [ SPARC only ]
63 - rtsig-max
64 - rtsig-nr
65 - sem
66 - sem_next_id [ sysv ipc ]
67 - sg-big-buff [ generic SCSI device (sg) ]
68 - shm_next_id [ sysv ipc ]
69 - shm_rmid_forced
70 - shmall
71 - shmmax [ sysv ipc ]
72 - shmmni
73 - softlockup_thresh
74 - stop-a [ SPARC only ]
75 - sysrq ==> Documentation/sysrq.txt
76 - tainted
77 - threads-max
78 - unknown_nmi_panic
79 - version
81 ==============================================================
83 acct:
85 highwater lowwater frequency
87 If BSD-style process accounting is enabled these values control
88 its behaviour. If free space on filesystem where the log lives
89 goes below <lowwater>% accounting suspends. If free space gets
90 above <highwater>% accounting resumes. <Frequency> determines
91 how often do we check the amount of free space (value is in
92 seconds). Default:
93 4 2 30
94 That is, suspend accounting if there left <= 2% free; resume it
95 if we got >=4%; consider information about amount of free space
96 valid for 30 seconds.
98 ==============================================================
100 acpi_video_flags:
102 flags
104 See Doc*/kernel/power/video.txt, it allows mode of video boot to be
105 set during run time.
107 ==============================================================
109 auto_msgmni:
111 Enables/Disables automatic recomputing of msgmni upon memory add/remove
112 or upon ipc namespace creation/removal (see the msgmni description
113 above). Echoing "1" into this file enables msgmni automatic recomputing.
114 Echoing "0" turns it off. auto_msgmni default value is 1.
117 ==============================================================
119 bootloader_type:
121 x86 bootloader identification
123 This gives the bootloader type number as indicated by the bootloader,
124 shifted left by 4, and OR'd with the low four bits of the bootloader
125 version. The reason for this encoding is that this used to match the
126 type_of_loader field in the kernel header; the encoding is kept for
127 backwards compatibility. That is, if the full bootloader type number
128 is 0x15 and the full version number is 0x234, this file will contain
129 the value 340 = 0x154.
131 See the type_of_loader and ext_loader_type fields in
132 Documentation/x86/boot.txt for additional information.
134 ==============================================================
136 bootloader_version:
138 x86 bootloader version
140 The complete bootloader version number. In the example above, this
141 file will contain the value 564 = 0x234.
143 See the type_of_loader and ext_loader_ver fields in
144 Documentation/x86/boot.txt for additional information.
146 ==============================================================
148 callhome:
150 Controls the kernel's callhome behavior in case of a kernel panic.
152 The s390 hardware allows an operating system to send a notification
153 to a service organization (callhome) in case of an operating system panic.
155 When the value in this file is 0 (which is the default behavior)
156 nothing happens in case of a kernel panic. If this value is set to "1"
157 the complete kernel oops message is send to the IBM customer service
158 organization in case the mainframe the Linux operating system is running
159 on has a service contract with IBM.
161 ==============================================================
163 cap_last_cap
165 Highest valid capability of the running kernel. Exports
166 CAP_LAST_CAP from the kernel.
168 ==============================================================
170 core_pattern:
172 core_pattern is used to specify a core dumpfile pattern name.
173 . max length 128 characters; default value is "core"
174 . core_pattern is used as a pattern template for the output filename;
175 certain string patterns (beginning with '%') are substituted with
176 their actual values.
177 . backward compatibility with core_uses_pid:
178 If core_pattern does not include "%p" (default does not)
179 and core_uses_pid is set, then .PID will be appended to
180 the filename.
181 . corename format specifiers:
182 %<NUL> '%' is dropped
183 %% output one '%'
184 %p pid
185 %u uid
186 %g gid
187 %d dump mode, matches PR_SET_DUMPABLE and
188 /proc/sys/fs/suid_dumpable
189 %s signal number
190 %t UNIX time of dump
191 %h hostname
192 %e executable filename (may be shortened)
193 %E executable path
194 %<OTHER> both are dropped
195 . If the first character of the pattern is a '|', the kernel will treat
196 the rest of the pattern as a command to run. The core dump will be
197 written to the standard input of that program instead of to a file.
199 ==============================================================
201 core_pipe_limit:
203 This sysctl is only applicable when core_pattern is configured to pipe
204 core files to a user space helper (when the first character of
205 core_pattern is a '|', see above). When collecting cores via a pipe
206 to an application, it is occasionally useful for the collecting
207 application to gather data about the crashing process from its
208 /proc/pid directory. In order to do this safely, the kernel must wait
209 for the collecting process to exit, so as not to remove the crashing
210 processes proc files prematurely. This in turn creates the
211 possibility that a misbehaving userspace collecting process can block
212 the reaping of a crashed process simply by never exiting. This sysctl
213 defends against that. It defines how many concurrent crashing
214 processes may be piped to user space applications in parallel. If
215 this value is exceeded, then those crashing processes above that value
216 are noted via the kernel log and their cores are skipped. 0 is a
217 special value, indicating that unlimited processes may be captured in
218 parallel, but that no waiting will take place (i.e. the collecting
219 process is not guaranteed access to /proc/<crashing pid>/). This
220 value defaults to 0.
222 ==============================================================
224 core_uses_pid:
226 The default coredump filename is "core". By setting
227 core_uses_pid to 1, the coredump filename becomes core.PID.
228 If core_pattern does not include "%p" (default does not)
229 and core_uses_pid is set, then .PID will be appended to
230 the filename.
232 ==============================================================
234 ctrl-alt-del:
236 When the value in this file is 0, ctrl-alt-del is trapped and
237 sent to the init(1) program to handle a graceful restart.
238 When, however, the value is > 0, Linux's reaction to a Vulcan
239 Nerve Pinch (tm) will be an immediate reboot, without even
240 syncing its dirty buffers.
242 Note: when a program (like dosemu) has the keyboard in 'raw'
243 mode, the ctrl-alt-del is intercepted by the program before it
244 ever reaches the kernel tty layer, and it's up to the program
245 to decide what to do with it.
247 ==============================================================
249 dmesg_restrict:
251 This toggle indicates whether unprivileged users are prevented
252 from using dmesg(8) to view messages from the kernel's log buffer.
253 When dmesg_restrict is set to (0) there are no restrictions. When
254 dmesg_restrict is set set to (1), users must have CAP_SYSLOG to use
255 dmesg(8).
257 The kernel config option CONFIG_SECURITY_DMESG_RESTRICT sets the
258 default value of dmesg_restrict.
260 ==============================================================
262 domainname & hostname:
264 These files can be used to set the NIS/YP domainname and the
265 hostname of your box in exactly the same way as the commands
266 domainname and hostname, i.e.:
267 # echo "darkstar" > /proc/sys/kernel/hostname
268 # echo "mydomain" > /proc/sys/kernel/domainname
269 has the same effect as
270 # hostname "darkstar"
271 # domainname "mydomain"
273 Note, however, that the classic darkstar.frop.org has the
274 hostname "darkstar" and DNS (Internet Domain Name Server)
275 domainname "frop.org", not to be confused with the NIS (Network
276 Information Service) or YP (Yellow Pages) domainname. These two
277 domain names are in general different. For a detailed discussion
278 see the hostname(1) man page.
280 ==============================================================
282 hotplug:
284 Path for the hotplug policy agent.
285 Default value is "/sbin/hotplug".
287 ==============================================================
289 kptr_restrict:
291 This toggle indicates whether restrictions are placed on
292 exposing kernel addresses via /proc and other interfaces. When
293 kptr_restrict is set to (0), there are no restrictions. When
294 kptr_restrict is set to (1), the default, kernel pointers
295 printed using the %pK format specifier will be replaced with 0's
296 unless the user has CAP_SYSLOG. When kptr_restrict is set to
297 (2), kernel pointers printed using %pK will be replaced with 0's
298 regardless of privileges.
300 ==============================================================
302 kstack_depth_to_print: (X86 only)
304 Controls the number of words to print when dumping the raw
305 kernel stack.
307 ==============================================================
309 l2cr: (PPC only)
311 This flag controls the L2 cache of G3 processor boards. If
312 0, the cache is disabled. Enabled if nonzero.
314 ==============================================================
316 modules_disabled:
318 A toggle value indicating if modules are allowed to be loaded
319 in an otherwise modular kernel. This toggle defaults to off
320 (0), but can be set true (1). Once true, modules can be
321 neither loaded nor unloaded, and the toggle cannot be set back
322 to false.
324 ==============================================================
326 msg_next_id, sem_next_id, and shm_next_id:
328 These three toggles allows to specify desired id for next allocated IPC
329 object: message, semaphore or shared memory respectively.
331 By default they are equal to -1, which means generic allocation logic.
332 Possible values to set are in range {0..INT_MAX}.
334 Notes:
335 1) kernel doesn't guarantee, that new object will have desired id. So,
336 it's up to userspace, how to handle an object with "wrong" id.
337 2) Toggle with non-default value will be set back to -1 by kernel after
338 successful IPC object allocation.
340 ==============================================================
342 nmi_watchdog:
344 Enables/Disables the NMI watchdog on x86 systems. When the value is
345 non-zero the NMI watchdog is enabled and will continuously test all
346 online cpus to determine whether or not they are still functioning
347 properly. Currently, passing "nmi_watchdog=" parameter at boot time is
348 required for this function to work.
350 If LAPIC NMI watchdog method is in use (nmi_watchdog=2 kernel
351 parameter), the NMI watchdog shares registers with oprofile. By
352 disabling the NMI watchdog, oprofile may have more registers to
353 utilize.
355 ==============================================================
357 osrelease, ostype & version:
359 # cat osrelease
360 2.1.88
361 # cat ostype
362 Linux
363 # cat version
364 #5 Wed Feb 25 21:49:24 MET 1998
366 The files osrelease and ostype should be clear enough. Version
367 needs a little more clarification however. The '#5' means that
368 this is the fifth kernel built from this source base and the
369 date behind it indicates the time the kernel was built.
370 The only way to tune these values is to rebuild the kernel :-)
372 ==============================================================
374 overflowgid & overflowuid:
376 if your architecture did not always support 32-bit UIDs (i.e. arm,
377 i386, m68k, sh, and sparc32), a fixed UID and GID will be returned to
378 applications that use the old 16-bit UID/GID system calls, if the
379 actual UID or GID would exceed 65535.
381 These sysctls allow you to change the value of the fixed UID and GID.
382 The default is 65534.
384 ==============================================================
386 panic:
388 The value in this file represents the number of seconds the kernel
389 waits before rebooting on a panic. When you use the software watchdog,
390 the recommended setting is 60.
392 ==============================================================
394 panic_on_unrecovered_nmi:
396 The default Linux behaviour on an NMI of either memory or unknown is
397 to continue operation. For many environments such as scientific
398 computing it is preferable that the box is taken out and the error
399 dealt with than an uncorrected parity/ECC error get propagated.
401 A small number of systems do generate NMI's for bizarre random reasons
402 such as power management so the default is off. That sysctl works like
403 the existing panic controls already in that directory.
405 ==============================================================
407 panic_on_oops:
409 Controls the kernel's behaviour when an oops or BUG is encountered.
411 0: try to continue operation
413 1: panic immediately. If the `panic' sysctl is also non-zero then the
414 machine will be rebooted.
416 ==============================================================
418 panic_on_stackoverflow:
420 Controls the kernel's behavior when detecting the overflows of
421 kernel, IRQ and exception stacks except a user stack.
422 This file shows up if CONFIG_DEBUG_STACKOVERFLOW is enabled.
424 0: try to continue operation.
426 1: panic immediately.
428 ==============================================================
431 pid_max:
433 PID allocation wrap value. When the kernel's next PID value
434 reaches this value, it wraps back to a minimum PID value.
435 PIDs of value pid_max or larger are not allocated.
437 ==============================================================
439 ns_last_pid:
441 The last pid allocated in the current (the one task using this sysctl
442 lives in) pid namespace. When selecting a pid for a next task on fork
443 kernel tries to allocate a number starting from this one.
445 ==============================================================
447 powersave-nap: (PPC only)
449 If set, Linux-PPC will use the 'nap' mode of powersaving,
450 otherwise the 'doze' mode will be used.
452 ==============================================================
454 printk:
456 The four values in printk denote: console_loglevel,
457 default_message_loglevel, minimum_console_loglevel and
458 default_console_loglevel respectively.
460 These values influence printk() behavior when printing or
461 logging error messages. See 'man 2 syslog' for more info on
462 the different loglevels.
464 - console_loglevel: messages with a higher priority than
465 this will be printed to the console
466 - default_message_loglevel: messages without an explicit priority
467 will be printed with this priority
468 - minimum_console_loglevel: minimum (highest) value to which
469 console_loglevel can be set
470 - default_console_loglevel: default value for console_loglevel
472 ==============================================================
474 printk_delay:
476 Delay each printk message in printk_delay milliseconds
478 Value from 0 - 10000 is allowed.
480 ==============================================================
482 printk_ratelimit:
484 Some warning messages are rate limited. printk_ratelimit specifies
485 the minimum length of time between these messages (in jiffies), by
486 default we allow one every 5 seconds.
488 A value of 0 will disable rate limiting.
490 ==============================================================
492 printk_ratelimit_burst:
494 While long term we enforce one message per printk_ratelimit
495 seconds, we do allow a burst of messages to pass through.
496 printk_ratelimit_burst specifies the number of messages we can
497 send before ratelimiting kicks in.
499 ==============================================================
501 randomize_va_space:
503 This option can be used to select the type of process address
504 space randomization that is used in the system, for architectures
505 that support this feature.
507 0 - Turn the process address space randomization off. This is the
508 default for architectures that do not support this feature anyways,
509 and kernels that are booted with the "norandmaps" parameter.
511 1 - Make the addresses of mmap base, stack and VDSO page randomized.
512 This, among other things, implies that shared libraries will be
513 loaded to random addresses. Also for PIE-linked binaries, the
514 location of code start is randomized. This is the default if the
515 CONFIG_COMPAT_BRK option is enabled.
517 2 - Additionally enable heap randomization. This is the default if
518 CONFIG_COMPAT_BRK is disabled.
520 There are a few legacy applications out there (such as some ancient
521 versions of libc.so.5 from 1996) that assume that brk area starts
522 just after the end of the code+bss. These applications break when
523 start of the brk area is randomized. There are however no known
524 non-legacy applications that would be broken this way, so for most
525 systems it is safe to choose full randomization.
527 Systems with ancient and/or broken binaries should be configured
528 with CONFIG_COMPAT_BRK enabled, which excludes the heap from process
529 address space randomization.
531 ==============================================================
533 reboot-cmd: (Sparc only)
535 ??? This seems to be a way to give an argument to the Sparc
536 ROM/Flash boot loader. Maybe to tell it what to do after
537 rebooting. ???
539 ==============================================================
541 rtsig-max & rtsig-nr:
543 The file rtsig-max can be used to tune the maximum number
544 of POSIX realtime (queued) signals that can be outstanding
545 in the system.
547 rtsig-nr shows the number of RT signals currently queued.
549 ==============================================================
551 sg-big-buff:
553 This file shows the size of the generic SCSI (sg) buffer.
554 You can't tune it just yet, but you could change it on
555 compile time by editing include/scsi/sg.h and changing
556 the value of SG_BIG_BUFF.
558 There shouldn't be any reason to change this value. If
559 you can come up with one, you probably know what you
560 are doing anyway :)
562 ==============================================================
564 shmall:
566 This parameter sets the total amount of shared memory pages that
567 can be used system wide. Hence, SHMALL should always be at least
568 ceil(shmmax/PAGE_SIZE).
570 If you are not sure what the default PAGE_SIZE is on your Linux
571 system, you can run the following command:
573 # getconf PAGE_SIZE
575 ==============================================================
577 shmmax:
579 This value can be used to query and set the run time limit
580 on the maximum shared memory segment size that can be created.
581 Shared memory segments up to 1Gb are now supported in the
582 kernel. This value defaults to SHMMAX.
584 ==============================================================
586 shm_rmid_forced:
588 Linux lets you set resource limits, including how much memory one
589 process can consume, via setrlimit(2). Unfortunately, shared memory
590 segments are allowed to exist without association with any process, and
591 thus might not be counted against any resource limits. If enabled,
592 shared memory segments are automatically destroyed when their attach
593 count becomes zero after a detach or a process termination. It will
594 also destroy segments that were created, but never attached to, on exit
595 from the process. The only use left for IPC_RMID is to immediately
596 destroy an unattached segment. Of course, this breaks the way things are
597 defined, so some applications might stop working. Note that this
598 feature will do you no good unless you also configure your resource
599 limits (in particular, RLIMIT_AS and RLIMIT_NPROC). Most systems don't
600 need this.
602 Note that if you change this from 0 to 1, already created segments
603 without users and with a dead originative process will be destroyed.
605 ==============================================================
607 softlockup_thresh:
609 This value can be used to lower the softlockup tolerance threshold. The
610 default threshold is 60 seconds. If a cpu is locked up for 60 seconds,
611 the kernel complains. Valid values are 1-60 seconds. Setting this
612 tunable to zero will disable the softlockup detection altogether.
614 ==============================================================
616 tainted:
618 Non-zero if the kernel has been tainted. Numeric values, which
619 can be ORed together:
621 1 - A module with a non-GPL license has been loaded, this
622 includes modules with no license.
623 Set by modutils >= 2.4.9 and module-init-tools.
624 2 - A module was force loaded by insmod -f.
625 Set by modutils >= 2.4.9 and module-init-tools.
626 4 - Unsafe SMP processors: SMP with CPUs not designed for SMP.
627 8 - A module was forcibly unloaded from the system by rmmod -f.
628 16 - A hardware machine check error occurred on the system.
629 32 - A bad page was discovered on the system.
630 64 - The user has asked that the system be marked "tainted". This
631 could be because they are running software that directly modifies
632 the hardware, or for other reasons.
633 128 - The system has died.
634 256 - The ACPI DSDT has been overridden with one supplied by the user
635 instead of using the one provided by the hardware.
636 512 - A kernel warning has occurred.
637 1024 - A module from drivers/staging was loaded.
638 2048 - The system is working around a severe firmware bug.
639 4096 - An out-of-tree module has been loaded.
641 ==============================================================
643 unknown_nmi_panic:
645 The value in this file affects behavior of handling NMI. When the
646 value is non-zero, unknown NMI is trapped and then panic occurs. At
647 that time, kernel debugging information is displayed on console.
649 NMI switch that most IA32 servers have fires unknown NMI up, for
650 example. If a system hangs up, try pressing the NMI switch.