Merge branch 'p-ti-android-3.8.y-video'
[android-sdk/kernel-video.git] / Makefile
1 VERSION = 3
2 PATCHLEVEL = 8
3 SUBLEVEL = 13
4 EXTRAVERSION =
5 NAME = Displaced Humerus Anterior
7 # *DOCUMENTATION*
8 # To see a list of typical targets execute "make help"
9 # More info can be located in ./README
10 # Comments in this file are targeted only to the developer, do not
11 # expect to learn how to build the kernel reading this file.
13 # Do not:
14 # o  use make's built-in rules and variables
15 #    (this increases performance and avoids hard-to-debug behaviour);
16 # o  print "Entering directory ...";
17 MAKEFLAGS += -rR --no-print-directory
19 # Avoid funny character set dependencies
20 unexport LC_ALL
21 LC_COLLATE=C
22 LC_NUMERIC=C
23 export LC_COLLATE LC_NUMERIC
25 # We are using a recursive build, so we need to do a little thinking
26 # to get the ordering right.
27 #
28 # Most importantly: sub-Makefiles should only ever modify files in
29 # their own directory. If in some directory we have a dependency on
30 # a file in another dir (which doesn't happen often, but it's often
31 # unavoidable when linking the built-in.o targets which finally
32 # turn into vmlinux), we will call a sub make in that other dir, and
33 # after that we are sure that everything which is in that other dir
34 # is now up to date.
35 #
36 # The only cases where we need to modify files which have global
37 # effects are thus separated out and done before the recursive
38 # descending is started. They are now explicitly listed as the
39 # prepare rule.
41 # To put more focus on warnings, be less verbose as default
42 # Use 'make V=1' to see the full commands
44 ifeq ("$(origin V)", "command line")
45   KBUILD_VERBOSE = $(V)
46 endif
47 ifndef KBUILD_VERBOSE
48   KBUILD_VERBOSE = 0
49 endif
51 # Call a source code checker (by default, "sparse") as part of the
52 # C compilation.
53 #
54 # Use 'make C=1' to enable checking of only re-compiled files.
55 # Use 'make C=2' to enable checking of *all* source files, regardless
56 # of whether they are re-compiled or not.
57 #
58 # See the file "Documentation/sparse.txt" for more details, including
59 # where to get the "sparse" utility.
61 ifeq ("$(origin C)", "command line")
62   KBUILD_CHECKSRC = $(C)
63 endif
64 ifndef KBUILD_CHECKSRC
65   KBUILD_CHECKSRC = 0
66 endif
68 # Use make M=dir to specify directory of external module to build
69 # Old syntax make ... SUBDIRS=$PWD is still supported
70 # Setting the environment variable KBUILD_EXTMOD take precedence
71 ifdef SUBDIRS
72   KBUILD_EXTMOD ?= $(SUBDIRS)
73 endif
75 ifeq ("$(origin M)", "command line")
76   KBUILD_EXTMOD := $(M)
77 endif
79 # kbuild supports saving output files in a separate directory.
80 # To locate output files in a separate directory two syntaxes are supported.
81 # In both cases the working directory must be the root of the kernel src.
82 # 1) O=
83 # Use "make O=dir/to/store/output/files/"
84 #
85 # 2) Set KBUILD_OUTPUT
86 # Set the environment variable KBUILD_OUTPUT to point to the directory
87 # where the output files shall be placed.
88 # export KBUILD_OUTPUT=dir/to/store/output/files/
89 # make
90 #
91 # The O= assignment takes precedence over the KBUILD_OUTPUT environment
92 # variable.
95 # KBUILD_SRC is set on invocation of make in OBJ directory
96 # KBUILD_SRC is not intended to be used by the regular user (for now)
97 ifeq ($(KBUILD_SRC),)
99 # OK, Make called in directory where kernel src resides
100 # Do we want to locate output files in a separate directory?
101 ifeq ("$(origin O)", "command line")
102   KBUILD_OUTPUT := $(O)
103 endif
105 ifeq ("$(origin W)", "command line")
106   export KBUILD_ENABLE_EXTRA_GCC_CHECKS := $(W)
107 endif
109 # That's our default target when none is given on the command line
110 PHONY := _all
111 _all:
113 # Cancel implicit rules on top Makefile
114 $(CURDIR)/Makefile Makefile: ;
116 ifneq ($(KBUILD_OUTPUT),)
117 # Invoke a second make in the output directory, passing relevant variables
118 # check that the output directory actually exists
119 saved-output := $(KBUILD_OUTPUT)
120 KBUILD_OUTPUT := $(shell cd $(KBUILD_OUTPUT) && /bin/pwd)
121 $(if $(KBUILD_OUTPUT),, \
122      $(error output directory "$(saved-output)" does not exist))
124 PHONY += $(MAKECMDGOALS) sub-make
126 $(filter-out _all sub-make $(CURDIR)/Makefile, $(MAKECMDGOALS)) _all: sub-make
127         @:
129 sub-make: FORCE
130         $(if $(KBUILD_VERBOSE:1=),@)$(MAKE) -C $(KBUILD_OUTPUT) \
131         KBUILD_SRC=$(CURDIR) \
132         KBUILD_EXTMOD="$(KBUILD_EXTMOD)" -f $(CURDIR)/Makefile \
133         $(filter-out _all sub-make,$(MAKECMDGOALS))
135 # Leave processing to above invocation of make
136 skip-makefile := 1
137 endif # ifneq ($(KBUILD_OUTPUT),)
138 endif # ifeq ($(KBUILD_SRC),)
140 # We process the rest of the Makefile if this is the final invocation of make
141 ifeq ($(skip-makefile),)
143 # If building an external module we do not care about the all: rule
144 # but instead _all depend on modules
145 PHONY += all
146 ifeq ($(KBUILD_EXTMOD),)
147 _all: all
148 else
149 _all: modules
150 endif
152 srctree         := $(if $(KBUILD_SRC),$(KBUILD_SRC),$(CURDIR))
153 objtree         := $(CURDIR)
154 src             := $(srctree)
155 obj             := $(objtree)
157 VPATH           := $(srctree)$(if $(KBUILD_EXTMOD),:$(KBUILD_EXTMOD))
159 export srctree objtree VPATH
162 # SUBARCH tells the usermode build what the underlying arch is.  That is set
163 # first, and if a usermode build is happening, the "ARCH=um" on the command
164 # line overrides the setting of ARCH below.  If a native build is happening,
165 # then ARCH is assigned, getting whatever value it gets normally, and 
166 # SUBARCH is subsequently ignored.
168 SUBARCH := $(shell uname -m | sed -e s/i.86/i386/ -e s/sun4u/sparc64/ \
169                                   -e s/arm.*/arm/ -e s/sa110/arm/ \
170                                   -e s/s390x/s390/ -e s/parisc64/parisc/ \
171                                   -e s/ppc.*/powerpc/ -e s/mips.*/mips/ \
172                                   -e s/sh[234].*/sh/ -e s/aarch64.*/arm64/ )
174 # Cross compiling and selecting different set of gcc/bin-utils
175 # ---------------------------------------------------------------------------
177 # When performing cross compilation for other architectures ARCH shall be set
178 # to the target architecture. (See arch/* for the possibilities).
179 # ARCH can be set during invocation of make:
180 # make ARCH=ia64
181 # Another way is to have ARCH set in the environment.
182 # The default ARCH is the host where make is executed.
184 # CROSS_COMPILE specify the prefix used for all executables used
185 # during compilation. Only gcc and related bin-utils executables
186 # are prefixed with $(CROSS_COMPILE).
187 # CROSS_COMPILE can be set on the command line
188 # make CROSS_COMPILE=ia64-linux-
189 # Alternatively CROSS_COMPILE can be set in the environment.
190 # A third alternative is to store a setting in .config so that plain
191 # "make" in the configured kernel build directory always uses that.
192 # Default value for CROSS_COMPILE is not to prefix executables
193 # Note: Some architectures assign CROSS_COMPILE in their arch/*/Makefile
194 export KBUILD_BUILDHOST := $(SUBARCH)
195 ARCH            ?= $(SUBARCH)
196 CROSS_COMPILE   ?= $(CONFIG_CROSS_COMPILE:"%"=%)
198 # Architecture as present in compile.h
199 UTS_MACHINE     := $(ARCH)
200 SRCARCH         := $(ARCH)
202 # Additional ARCH settings for x86
203 ifeq ($(ARCH),i386)
204         SRCARCH := x86
205 endif
206 ifeq ($(ARCH),x86_64)
207         SRCARCH := x86
208 endif
210 # Additional ARCH settings for sparc
211 ifeq ($(ARCH),sparc32)
212        SRCARCH := sparc
213 endif
214 ifeq ($(ARCH),sparc64)
215        SRCARCH := sparc
216 endif
218 # Additional ARCH settings for sh
219 ifeq ($(ARCH),sh64)
220        SRCARCH := sh
221 endif
223 # Additional ARCH settings for tile
224 ifeq ($(ARCH),tilepro)
225        SRCARCH := tile
226 endif
227 ifeq ($(ARCH),tilegx)
228        SRCARCH := tile
229 endif
231 # Where to locate arch specific headers
232 hdr-arch  := $(SRCARCH)
234 KCONFIG_CONFIG  ?= .config
235 export KCONFIG_CONFIG
237 # SHELL used by kbuild
238 CONFIG_SHELL := $(shell if [ -x "$$BASH" ]; then echo $$BASH; \
239           else if [ -x /bin/bash ]; then echo /bin/bash; \
240           else echo sh; fi ; fi)
242 HOSTCC       = gcc
243 HOSTCXX      = g++
244 HOSTCFLAGS   = -Wall -Wmissing-prototypes -Wstrict-prototypes -O2 -fomit-frame-pointer
245 HOSTCXXFLAGS = -O2
247 # Decide whether to build built-in, modular, or both.
248 # Normally, just do built-in.
250 KBUILD_MODULES :=
251 KBUILD_BUILTIN := 1
253 #       If we have only "make modules", don't compile built-in objects.
254 #       When we're building modules with modversions, we need to consider
255 #       the built-in objects during the descend as well, in order to
256 #       make sure the checksums are up to date before we record them.
258 ifeq ($(MAKECMDGOALS),modules)
259   KBUILD_BUILTIN := $(if $(CONFIG_MODVERSIONS),1)
260 endif
262 #       If we have "make <whatever> modules", compile modules
263 #       in addition to whatever we do anyway.
264 #       Just "make" or "make all" shall build modules as well
266 ifneq ($(filter all _all modules,$(MAKECMDGOALS)),)
267   KBUILD_MODULES := 1
268 endif
270 ifeq ($(MAKECMDGOALS),)
271   KBUILD_MODULES := 1
272 endif
274 export KBUILD_MODULES KBUILD_BUILTIN
275 export KBUILD_CHECKSRC KBUILD_SRC KBUILD_EXTMOD
277 # Beautify output
278 # ---------------------------------------------------------------------------
280 # Normally, we echo the whole command before executing it. By making
281 # that echo $($(quiet)$(cmd)), we now have the possibility to set
282 # $(quiet) to choose other forms of output instead, e.g.
284 #         quiet_cmd_cc_o_c = Compiling $(RELDIR)/$@
285 #         cmd_cc_o_c       = $(CC) $(c_flags) -c -o $@ $<
287 # If $(quiet) is empty, the whole command will be printed.
288 # If it is set to "quiet_", only the short version will be printed. 
289 # If it is set to "silent_", nothing will be printed at all, since
290 # the variable $(silent_cmd_cc_o_c) doesn't exist.
292 # A simple variant is to prefix commands with $(Q) - that's useful
293 # for commands that shall be hidden in non-verbose mode.
295 #       $(Q)ln $@ :<
297 # If KBUILD_VERBOSE equals 0 then the above command will be hidden.
298 # If KBUILD_VERBOSE equals 1 then the above command is displayed.
300 ifeq ($(KBUILD_VERBOSE),1)
301   quiet =
302   Q =
303 else
304   quiet=quiet_
305   Q = @
306 endif
308 # If the user is running make -s (silent mode), suppress echoing of
309 # commands
311 ifneq ($(filter s% -s%,$(MAKEFLAGS)),)
312   quiet=silent_
313 endif
315 export quiet Q KBUILD_VERBOSE
318 # Look for make include files relative to root of kernel src
319 MAKEFLAGS += --include-dir=$(srctree)
321 # We need some generic definitions (do not try to remake the file).
322 $(srctree)/scripts/Kbuild.include: ;
323 include $(srctree)/scripts/Kbuild.include
325 # Make variables (CC, etc...)
327 AS              = $(CROSS_COMPILE)as
328 LD              = $(CROSS_COMPILE)ld
329 CC              = $(CROSS_COMPILE)gcc
330 CPP             = $(CC) -E
331 AR              = $(CROSS_COMPILE)ar
332 NM              = $(CROSS_COMPILE)nm
333 STRIP           = $(CROSS_COMPILE)strip
334 OBJCOPY         = $(CROSS_COMPILE)objcopy
335 OBJDUMP         = $(CROSS_COMPILE)objdump
336 AWK             = awk
337 GENKSYMS        = scripts/genksyms/genksyms
338 INSTALLKERNEL  := installkernel
339 DEPMOD          = /sbin/depmod
340 PERL            = perl
341 CHECK           = sparse
343 CHECKFLAGS     := -D__linux__ -Dlinux -D__STDC__ -Dunix -D__unix__ \
344                   -Wbitwise -Wno-return-void $(CF)
345 CFLAGS_MODULE   =
346 AFLAGS_MODULE   =
347 LDFLAGS_MODULE  =
348 CFLAGS_KERNEL   =
349 AFLAGS_KERNEL   =
350 CFLAGS_GCOV     = -fprofile-arcs -ftest-coverage
353 # Use USERINCLUDE when you must reference the UAPI directories only.
354 USERINCLUDE    := \
355                 -I$(srctree)/arch/$(hdr-arch)/include/uapi \
356                 -Iarch/$(hdr-arch)/include/generated/uapi \
357                 -I$(srctree)/include/uapi \
358                 -Iinclude/generated/uapi \
359                 -include $(srctree)/include/linux/kconfig.h
361 # Use LINUXINCLUDE when you must reference the include/ directory.
362 # Needed to be compatible with the O= option
363 LINUXINCLUDE    := \
364                 -I$(srctree)/arch/$(hdr-arch)/include \
365                 -Iarch/$(hdr-arch)/include/generated \
366                 $(if $(KBUILD_SRC), -I$(srctree)/include) \
367                 -Iinclude \
368                 $(USERINCLUDE)
370 KBUILD_CPPFLAGS := -D__KERNEL__
372 KBUILD_CFLAGS   := -Wall -Wundef -Wstrict-prototypes -Wno-trigraphs \
373                    -fno-strict-aliasing -fno-common \
374                    -Werror-implicit-function-declaration \
375                    -Wno-format-security \
376                    -fno-delete-null-pointer-checks
377 KBUILD_AFLAGS_KERNEL :=
378 KBUILD_CFLAGS_KERNEL :=
379 KBUILD_AFLAGS   := -D__ASSEMBLY__
380 KBUILD_AFLAGS_MODULE  := -DMODULE
381 KBUILD_CFLAGS_MODULE  := -DMODULE
382 KBUILD_LDFLAGS_MODULE := -T $(srctree)/scripts/module-common.lds
384 # Read KERNELRELEASE from include/config/kernel.release (if it exists)
385 KERNELRELEASE = $(shell cat include/config/kernel.release 2> /dev/null)
386 KERNELVERSION = $(VERSION)$(if $(PATCHLEVEL),.$(PATCHLEVEL)$(if $(SUBLEVEL),.$(SUBLEVEL)))$(EXTRAVERSION)
388 export VERSION PATCHLEVEL SUBLEVEL KERNELRELEASE KERNELVERSION
389 export ARCH SRCARCH CONFIG_SHELL HOSTCC HOSTCFLAGS CROSS_COMPILE AS LD CC
390 export CPP AR NM STRIP OBJCOPY OBJDUMP
391 export MAKE AWK GENKSYMS INSTALLKERNEL PERL UTS_MACHINE
392 export HOSTCXX HOSTCXXFLAGS LDFLAGS_MODULE CHECK CHECKFLAGS
394 export KBUILD_CPPFLAGS NOSTDINC_FLAGS LINUXINCLUDE OBJCOPYFLAGS LDFLAGS
395 export KBUILD_CFLAGS CFLAGS_KERNEL CFLAGS_MODULE CFLAGS_GCOV
396 export KBUILD_AFLAGS AFLAGS_KERNEL AFLAGS_MODULE
397 export KBUILD_AFLAGS_MODULE KBUILD_CFLAGS_MODULE KBUILD_LDFLAGS_MODULE
398 export KBUILD_AFLAGS_KERNEL KBUILD_CFLAGS_KERNEL
399 export KBUILD_ARFLAGS
401 # When compiling out-of-tree modules, put MODVERDIR in the module
402 # tree rather than in the kernel tree. The kernel tree might
403 # even be read-only.
404 export MODVERDIR := $(if $(KBUILD_EXTMOD),$(firstword $(KBUILD_EXTMOD))/).tmp_versions
406 # Files to ignore in find ... statements
408 RCS_FIND_IGNORE := \( -name SCCS -o -name BitKeeper -o -name .svn -o -name CVS \
409                    -o -name .pc -o -name .hg -o -name .git \) -prune -o
410 export RCS_TAR_IGNORE := --exclude SCCS --exclude BitKeeper --exclude .svn \
411                          --exclude CVS --exclude .pc --exclude .hg --exclude .git
413 # ===========================================================================
414 # Rules shared between *config targets and build targets
416 # Basic helpers built in scripts/
417 PHONY += scripts_basic
418 scripts_basic:
419         $(Q)$(MAKE) $(build)=scripts/basic
420         $(Q)rm -f .tmp_quiet_recordmcount
422 # To avoid any implicit rule to kick in, define an empty command.
423 scripts/basic/%: scripts_basic ;
425 PHONY += outputmakefile
426 # outputmakefile generates a Makefile in the output directory, if using a
427 # separate output directory. This allows convenient use of make in the
428 # output directory.
429 outputmakefile:
430 ifneq ($(KBUILD_SRC),)
431         $(Q)ln -fsn $(srctree) source
432         $(Q)$(CONFIG_SHELL) $(srctree)/scripts/mkmakefile \
433             $(srctree) $(objtree) $(VERSION) $(PATCHLEVEL)
434 endif
436 # Support for using generic headers in asm-generic
437 PHONY += asm-generic
438 asm-generic:
439         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.asm-generic \
440                     src=asm obj=arch/$(SRCARCH)/include/generated/asm
441         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.asm-generic \
442                     src=uapi/asm obj=arch/$(SRCARCH)/include/generated/uapi/asm
444 # To make sure we do not include .config for any of the *config targets
445 # catch them early, and hand them over to scripts/kconfig/Makefile
446 # It is allowed to specify more targets when calling make, including
447 # mixing *config targets and build targets.
448 # For example 'make oldconfig all'.
449 # Detect when mixed targets is specified, and make a second invocation
450 # of make so .config is not included in this case either (for *config).
452 version_h := include/generated/uapi/linux/version.h
454 no-dot-config-targets := clean mrproper distclean \
455                          cscope gtags TAGS tags help %docs check% coccicheck \
456                          $(version_h) headers_% archheaders archscripts \
457                          kernelversion %src-pkg
459 config-targets := 0
460 mixed-targets  := 0
461 dot-config     := 1
463 ifneq ($(filter $(no-dot-config-targets), $(MAKECMDGOALS)),)
464         ifeq ($(filter-out $(no-dot-config-targets), $(MAKECMDGOALS)),)
465                 dot-config := 0
466         endif
467 endif
469 ifeq ($(KBUILD_EXTMOD),)
470         ifneq ($(filter config %config,$(MAKECMDGOALS)),)
471                 config-targets := 1
472                 ifneq ($(filter-out config %config,$(MAKECMDGOALS)),)
473                         mixed-targets := 1
474                 endif
475         endif
476 endif
478 ifeq ($(mixed-targets),1)
479 # ===========================================================================
480 # We're called with mixed targets (*config and build targets).
481 # Handle them one by one.
483 %:: FORCE
484         $(Q)$(MAKE) -C $(srctree) KBUILD_SRC= $@
486 else
487 ifeq ($(config-targets),1)
488 # ===========================================================================
489 # *config targets only - make sure prerequisites are updated, and descend
490 # in scripts/kconfig to make the *config target
492 # Read arch specific Makefile to set KBUILD_DEFCONFIG as needed.
493 # KBUILD_DEFCONFIG may point out an alternative default configuration
494 # used for 'make defconfig'
495 include $(srctree)/arch/$(SRCARCH)/Makefile
496 export KBUILD_DEFCONFIG KBUILD_KCONFIG
498 config: scripts_basic outputmakefile FORCE
499         $(Q)mkdir -p include/linux include/config
500         $(Q)$(MAKE) $(build)=scripts/kconfig $@
502 %config: scripts_basic outputmakefile FORCE
503         $(Q)mkdir -p include/linux include/config
504         $(Q)$(MAKE) $(build)=scripts/kconfig $@
506 else
507 # ===========================================================================
508 # Build targets only - this includes vmlinux, arch specific targets, clean
509 # targets and others. In general all targets except *config targets.
511 ifeq ($(KBUILD_EXTMOD),)
512 # Additional helpers built in scripts/
513 # Carefully list dependencies so we do not try to build scripts twice
514 # in parallel
515 PHONY += scripts
516 scripts: scripts_basic include/config/auto.conf include/config/tristate.conf
517         $(Q)$(MAKE) $(build)=$(@)
519 # Objects we will link into vmlinux / subdirs we need to visit
520 init-y          := init/
521 drivers-y       := drivers/ sound/ firmware/
522 net-y           := net/
523 libs-y          := lib/
524 core-y          := usr/
525 endif # KBUILD_EXTMOD
527 ifeq ($(dot-config),1)
528 # Read in config
529 -include include/config/auto.conf
531 ifeq ($(KBUILD_EXTMOD),)
532 # Read in dependencies to all Kconfig* files, make sure to run
533 # oldconfig if changes are detected.
534 -include include/config/auto.conf.cmd
536 # To avoid any implicit rule to kick in, define an empty command
537 $(KCONFIG_CONFIG) include/config/auto.conf.cmd: ;
539 # If .config is newer than include/config/auto.conf, someone tinkered
540 # with it and forgot to run make oldconfig.
541 # if auto.conf.cmd is missing then we are probably in a cleaned tree so
542 # we execute the config step to be sure to catch updated Kconfig files
543 include/config/%.conf: $(KCONFIG_CONFIG) include/config/auto.conf.cmd
544         $(Q)$(MAKE) -f $(srctree)/Makefile silentoldconfig
545 else
546 # external modules needs include/generated/autoconf.h and include/config/auto.conf
547 # but do not care if they are up-to-date. Use auto.conf to trigger the test
548 PHONY += include/config/auto.conf
550 include/config/auto.conf:
551         $(Q)test -e include/generated/autoconf.h -a -e $@ || (          \
552         echo >&2;                                                       \
553         echo >&2 "  ERROR: Kernel configuration is invalid.";           \
554         echo >&2 "         include/generated/autoconf.h or $@ are missing.";\
555         echo >&2 "         Run 'make oldconfig && make prepare' on kernel src to fix it.";      \
556         echo >&2 ;                                                      \
557         /bin/false)
559 endif # KBUILD_EXTMOD
561 else
562 # Dummy target needed, because used as prerequisite
563 include/config/auto.conf: ;
564 endif # $(dot-config)
566 # The all: target is the default when no target is given on the
567 # command line.
568 # This allow a user to issue only 'make' to build a kernel including modules
569 # Defaults to vmlinux, but the arch makefile usually adds further targets
570 all: vmlinux
572 ifdef CONFIG_CC_OPTIMIZE_FOR_SIZE
573 KBUILD_CFLAGS   += -Os
574 else
575 KBUILD_CFLAGS   += -O2
576 endif
578 include $(srctree)/arch/$(SRCARCH)/Makefile
580 ifdef CONFIG_READABLE_ASM
581 # Disable optimizations that make assembler listings hard to read.
582 # reorder blocks reorders the control in the function
583 # ipa clone creates specialized cloned functions
584 # partial inlining inlines only parts of functions
585 KBUILD_CFLAGS += $(call cc-option,-fno-reorder-blocks,) \
586                  $(call cc-option,-fno-ipa-cp-clone,) \
587                  $(call cc-option,-fno-partial-inlining)
588 endif
590 ifneq ($(CONFIG_FRAME_WARN),0)
591 KBUILD_CFLAGS += $(call cc-option,-Wframe-larger-than=${CONFIG_FRAME_WARN})
592 endif
594 # Force gcc to behave correct even for buggy distributions
595 ifndef CONFIG_CC_STACKPROTECTOR
596 KBUILD_CFLAGS += $(call cc-option, -fno-stack-protector)
597 endif
599 # This warning generated too much noise in a regular build.
600 # Use make W=1 to enable this warning (see scripts/Makefile.build)
601 KBUILD_CFLAGS += $(call cc-disable-warning, unused-but-set-variable)
603 ifdef CONFIG_FRAME_POINTER
604 KBUILD_CFLAGS   += -fno-omit-frame-pointer -fno-optimize-sibling-calls
605 else
606 # Some targets (ARM with Thumb2, for example), can't be built with frame
607 # pointers.  For those, we don't have FUNCTION_TRACER automatically
608 # select FRAME_POINTER.  However, FUNCTION_TRACER adds -pg, and this is
609 # incompatible with -fomit-frame-pointer with current GCC, so we don't use
610 # -fomit-frame-pointer with FUNCTION_TRACER.
611 ifndef CONFIG_FUNCTION_TRACER
612 KBUILD_CFLAGS   += -fomit-frame-pointer
613 endif
614 endif
616 ifdef CONFIG_DEBUG_INFO
617 KBUILD_CFLAGS   += -g
618 KBUILD_AFLAGS   += -gdwarf-2
619 endif
621 ifdef CONFIG_DEBUG_INFO_REDUCED
622 KBUILD_CFLAGS   += $(call cc-option, -femit-struct-debug-baseonly)
623 endif
625 ifdef CONFIG_FUNCTION_TRACER
626 ifdef CONFIG_HAVE_FENTRY
627 CC_USING_FENTRY := $(call cc-option, -mfentry -DCC_USING_FENTRY)
628 endif
629 KBUILD_CFLAGS   += -pg $(CC_USING_FENTRY)
630 KBUILD_AFLAGS   += $(CC_USING_FENTRY)
631 ifdef CONFIG_DYNAMIC_FTRACE
632         ifdef CONFIG_HAVE_C_RECORDMCOUNT
633                 BUILD_C_RECORDMCOUNT := y
634                 export BUILD_C_RECORDMCOUNT
635         endif
636 endif
637 endif
639 # We trigger additional mismatches with less inlining
640 ifdef CONFIG_DEBUG_SECTION_MISMATCH
641 KBUILD_CFLAGS += $(call cc-option, -fno-inline-functions-called-once)
642 endif
644 # arch Makefile may override CC so keep this after arch Makefile is included
645 NOSTDINC_FLAGS += -nostdinc -isystem $(shell $(CC) -print-file-name=include)
646 CHECKFLAGS     += $(NOSTDINC_FLAGS)
648 # warn about C99 declaration after statement
649 KBUILD_CFLAGS += $(call cc-option,-Wdeclaration-after-statement,)
651 # disable pointer signed / unsigned warnings in gcc 4.0
652 KBUILD_CFLAGS += $(call cc-disable-warning, pointer-sign)
654 # disable invalid "can't wrap" optimizations for signed / pointers
655 KBUILD_CFLAGS   += $(call cc-option,-fno-strict-overflow)
657 # conserve stack if available
658 KBUILD_CFLAGS   += $(call cc-option,-fconserve-stack)
660 # use the deterministic mode of AR if available
661 KBUILD_ARFLAGS := $(call ar-option,D)
663 # check for 'asm goto'
664 ifeq ($(shell $(CONFIG_SHELL) $(srctree)/scripts/gcc-goto.sh $(CC)), y)
665         KBUILD_CFLAGS += -DCC_HAVE_ASM_GOTO
666 endif
668 # Add user supplied CPPFLAGS, AFLAGS and CFLAGS as the last assignments
669 KBUILD_CPPFLAGS += $(KCPPFLAGS)
670 KBUILD_AFLAGS += $(KAFLAGS)
671 KBUILD_CFLAGS += $(KCFLAGS)
673 # Use --build-id when available.
674 LDFLAGS_BUILD_ID = $(patsubst -Wl$(comma)%,%,\
675                               $(call cc-ldoption, -Wl$(comma)--build-id,))
676 KBUILD_LDFLAGS_MODULE += $(LDFLAGS_BUILD_ID)
677 LDFLAGS_vmlinux += $(LDFLAGS_BUILD_ID)
679 ifeq ($(CONFIG_STRIP_ASM_SYMS),y)
680 LDFLAGS_vmlinux += $(call ld-option, -X,)
681 endif
683 # Default kernel image to build when no specific target is given.
684 # KBUILD_IMAGE may be overruled on the command line or
685 # set in the environment
686 # Also any assignments in arch/$(ARCH)/Makefile take precedence over
687 # this default value
688 export KBUILD_IMAGE ?= vmlinux
691 # INSTALL_PATH specifies where to place the updated kernel and system map
692 # images. Default is /boot, but you can set it to other values
693 export  INSTALL_PATH ?= /boot
696 # INSTALL_MOD_PATH specifies a prefix to MODLIB for module directory
697 # relocations required by build roots.  This is not defined in the
698 # makefile but the argument can be passed to make if needed.
701 MODLIB  = $(INSTALL_MOD_PATH)/lib/modules/$(KERNELRELEASE)
702 export MODLIB
705 #  INSTALL_MOD_STRIP, if defined, will cause modules to be
706 #  stripped after they are installed.  If INSTALL_MOD_STRIP is '1', then
707 #  the default option --strip-debug will be used.  Otherwise,
708 #  INSTALL_MOD_STRIP value will be used as the options to the strip command.
710 ifdef INSTALL_MOD_STRIP
711 ifeq ($(INSTALL_MOD_STRIP),1)
712 mod_strip_cmd = $(STRIP) --strip-debug
713 else
714 mod_strip_cmd = $(STRIP) $(INSTALL_MOD_STRIP)
715 endif # INSTALL_MOD_STRIP=1
716 else
717 mod_strip_cmd = true
718 endif # INSTALL_MOD_STRIP
719 export mod_strip_cmd
722 ifeq ($(CONFIG_MODULE_SIG),y)
723 MODSECKEY = ./signing_key.priv
724 MODPUBKEY = ./signing_key.x509
725 export MODPUBKEY
726 mod_sign_cmd = perl $(srctree)/scripts/sign-file $(MODSECKEY) $(MODPUBKEY)
727 else
728 mod_sign_cmd = true
729 endif
730 export mod_sign_cmd
733 ifeq ($(KBUILD_EXTMOD),)
734 core-y          += kernel/ mm/ fs/ ipc/ security/ crypto/ block/
736 vmlinux-dirs    := $(patsubst %/,%,$(filter %/, $(init-y) $(init-m) \
737                      $(core-y) $(core-m) $(drivers-y) $(drivers-m) \
738                      $(net-y) $(net-m) $(libs-y) $(libs-m)))
740 vmlinux-alldirs := $(sort $(vmlinux-dirs) $(patsubst %/,%,$(filter %/, \
741                      $(init-n) $(init-) \
742                      $(core-n) $(core-) $(drivers-n) $(drivers-) \
743                      $(net-n)  $(net-)  $(libs-n)    $(libs-))))
745 init-y          := $(patsubst %/, %/built-in.o, $(init-y))
746 core-y          := $(patsubst %/, %/built-in.o, $(core-y))
747 drivers-y       := $(patsubst %/, %/built-in.o, $(drivers-y))
748 net-y           := $(patsubst %/, %/built-in.o, $(net-y))
749 libs-y1         := $(patsubst %/, %/lib.a, $(libs-y))
750 libs-y2         := $(patsubst %/, %/built-in.o, $(libs-y))
751 libs-y          := $(libs-y1) $(libs-y2)
753 # Externally visible symbols (used by link-vmlinux.sh)
754 export KBUILD_VMLINUX_INIT := $(head-y) $(init-y)
755 export KBUILD_VMLINUX_MAIN := $(core-y) $(libs-y) $(drivers-y) $(net-y)
756 export KBUILD_LDS          := arch/$(SRCARCH)/kernel/vmlinux.lds
757 export LDFLAGS_vmlinux
759 vmlinux-deps := $(KBUILD_LDS) $(KBUILD_VMLINUX_INIT) $(KBUILD_VMLINUX_MAIN)
761 # Final link of vmlinux
762       cmd_link-vmlinux = $(CONFIG_SHELL) $< $(LD) $(LDFLAGS) $(LDFLAGS_vmlinux)
763 quiet_cmd_link-vmlinux = LINK    $@
765 # Include targets which we want to
766 # execute if the rest of the kernel build went well.
767 vmlinux: scripts/link-vmlinux.sh $(vmlinux-deps) FORCE
768 ifdef CONFIG_HEADERS_CHECK
769         $(Q)$(MAKE) -f $(srctree)/Makefile headers_check
770 endif
771 ifdef CONFIG_SAMPLES
772         $(Q)$(MAKE) $(build)=samples
773 endif
774 ifdef CONFIG_BUILD_DOCSRC
775         $(Q)$(MAKE) $(build)=Documentation
776 endif
777         +$(call if_changed,link-vmlinux)
779 # The actual objects are generated when descending, 
780 # make sure no implicit rule kicks in
781 $(sort $(vmlinux-deps)): $(vmlinux-dirs) ;
783 # Handle descending into subdirectories listed in $(vmlinux-dirs)
784 # Preset locale variables to speed up the build process. Limit locale
785 # tweaks to this spot to avoid wrong language settings when running
786 # make menuconfig etc.
787 # Error messages still appears in the original language
789 PHONY += $(vmlinux-dirs)
790 $(vmlinux-dirs): prepare scripts
791         $(Q)$(MAKE) $(build)=$@
793 # Store (new) KERNELRELASE string in include/config/kernel.release
794 include/config/kernel.release: include/config/auto.conf FORCE
795         $(Q)rm -f $@
796         $(Q)echo "$(KERNELVERSION)$$($(CONFIG_SHELL) $(srctree)/scripts/setlocalversion $(srctree))" > $@
799 # Things we need to do before we recursively start building the kernel
800 # or the modules are listed in "prepare".
801 # A multi level approach is used. prepareN is processed before prepareN-1.
802 # archprepare is used in arch Makefiles and when processed asm symlink,
803 # version.h and scripts_basic is processed / created.
805 # Listed in dependency order
806 PHONY += prepare archprepare prepare0 prepare1 prepare2 prepare3
808 # prepare3 is used to check if we are building in a separate output directory,
809 # and if so do:
810 # 1) Check that make has not been executed in the kernel src $(srctree)
811 prepare3: include/config/kernel.release
812 ifneq ($(KBUILD_SRC),)
813         @$(kecho) '  Using $(srctree) as source for kernel'
814         $(Q)if [ -f $(srctree)/.config -o -d $(srctree)/include/config ]; then \
815                 echo >&2 "  $(srctree) is not clean, please run 'make mrproper'"; \
816                 echo >&2 "  in the '$(srctree)' directory.";\
817                 /bin/false; \
818         fi;
819 endif
821 # prepare2 creates a makefile if using a separate output directory
822 prepare2: prepare3 outputmakefile asm-generic
824 prepare1: prepare2 $(version_h) include/generated/utsrelease.h \
825                    include/config/auto.conf
826         $(cmd_crmodverdir)
828 archprepare: archheaders archscripts prepare1 scripts_basic
830 prepare0: archprepare FORCE
831         $(Q)$(MAKE) $(build)=.
833 # All the preparing..
834 prepare: prepare0
836 # Generate some files
837 # ---------------------------------------------------------------------------
839 # KERNELRELEASE can change from a few different places, meaning version.h
840 # needs to be updated, so this check is forced on all builds
842 uts_len := 64
843 define filechk_utsrelease.h
844         if [ `echo -n "$(KERNELRELEASE)" | wc -c ` -gt $(uts_len) ]; then \
845           echo '"$(KERNELRELEASE)" exceeds $(uts_len) characters' >&2;    \
846           exit 1;                                                         \
847         fi;                                                               \
848         (echo \#define UTS_RELEASE \"$(KERNELRELEASE)\";)
849 endef
851 define filechk_version.h
852         (echo \#define LINUX_VERSION_CODE $(shell                         \
853         expr $(VERSION) \* 65536 + 0$(PATCHLEVEL) \* 256 + 0$(SUBLEVEL)); \
854         echo '#define KERNEL_VERSION(a,b,c) (((a) << 16) + ((b) << 8) + (c))';)
855 endef
857 $(version_h): $(srctree)/Makefile FORCE
858         $(call filechk,version.h)
860 include/generated/utsrelease.h: include/config/kernel.release FORCE
861         $(call filechk,utsrelease.h)
863 PHONY += headerdep
864 headerdep:
865         $(Q)find $(srctree)/include/ -name '*.h' | xargs --max-args 1 \
866         $(srctree)/scripts/headerdep.pl -I$(srctree)/include
868 # ---------------------------------------------------------------------------
870 PHONY += depend dep
871 depend dep:
872         @echo '*** Warning: make $@ is unnecessary now.'
874 # ---------------------------------------------------------------------------
875 # Firmware install
876 INSTALL_FW_PATH=$(INSTALL_MOD_PATH)/lib/firmware
877 export INSTALL_FW_PATH
879 PHONY += firmware_install
880 firmware_install: FORCE
881         @mkdir -p $(objtree)/firmware
882         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.fwinst obj=firmware __fw_install
884 # ---------------------------------------------------------------------------
885 # Kernel headers
887 #Default location for installed headers
888 export INSTALL_HDR_PATH = $(objtree)/usr
890 hdr-inst := -rR -f $(srctree)/scripts/Makefile.headersinst obj
892 # If we do an all arch process set dst to asm-$(hdr-arch)
893 hdr-dst = $(if $(KBUILD_HEADERS), dst=include/asm-$(hdr-arch), dst=include/asm)
895 PHONY += archheaders
896 archheaders:
898 PHONY += archscripts
899 archscripts:
901 PHONY += __headers
902 __headers: $(version_h) scripts_basic asm-generic archheaders archscripts FORCE
903         $(Q)$(MAKE) $(build)=scripts build_unifdef
905 PHONY += headers_install_all
906 headers_install_all:
907         $(Q)$(CONFIG_SHELL) $(srctree)/scripts/headers.sh install
909 PHONY += headers_install
910 headers_install: __headers
911         $(if $(wildcard $(srctree)/arch/$(hdr-arch)/include/uapi/asm/Kbuild),, \
912           $(error Headers not exportable for the $(SRCARCH) architecture))
913         $(Q)$(MAKE) $(hdr-inst)=include/uapi
914         $(Q)$(MAKE) $(hdr-inst)=arch/$(hdr-arch)/include/uapi/asm $(hdr-dst)
916 PHONY += headers_check_all
917 headers_check_all: headers_install_all
918         $(Q)$(CONFIG_SHELL) $(srctree)/scripts/headers.sh check
920 PHONY += headers_check
921 headers_check: headers_install
922         $(Q)$(MAKE) $(hdr-inst)=include/uapi HDRCHECK=1
923         $(Q)$(MAKE) $(hdr-inst)=arch/$(hdr-arch)/include/uapi/asm $(hdr-dst) HDRCHECK=1
925 # ---------------------------------------------------------------------------
926 # Modules
928 ifdef CONFIG_MODULES
930 # By default, build modules as well
932 all: modules
934 #       Build modules
936 #       A module can be listed more than once in obj-m resulting in
937 #       duplicate lines in modules.order files.  Those are removed
938 #       using awk while concatenating to the final file.
940 PHONY += modules
941 modules: $(vmlinux-dirs) $(if $(KBUILD_BUILTIN),vmlinux) modules.builtin
942         $(Q)$(AWK) '!x[$$0]++' $(vmlinux-dirs:%=$(objtree)/%/modules.order) > $(objtree)/modules.order
943         @$(kecho) '  Building modules, stage 2.';
944         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modpost
945         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.fwinst obj=firmware __fw_modbuild
947 modules.builtin: $(vmlinux-dirs:%=%/modules.builtin)
948         $(Q)$(AWK) '!x[$$0]++' $^ > $(objtree)/modules.builtin
950 %/modules.builtin: include/config/auto.conf
951         $(Q)$(MAKE) $(modbuiltin)=$*
954 # Target to prepare building external modules
955 PHONY += modules_prepare
956 modules_prepare: prepare scripts
958 # Target to install modules
959 PHONY += modules_install
960 modules_install: _modinst_ _modinst_post
962 PHONY += _modinst_
963 _modinst_:
964         @rm -rf $(MODLIB)/kernel
965         @rm -f $(MODLIB)/source
966         @mkdir -p $(MODLIB)/kernel
967         @ln -s $(srctree) $(MODLIB)/source
968         @if [ ! $(objtree) -ef  $(MODLIB)/build ]; then \
969                 rm -f $(MODLIB)/build ; \
970                 ln -s $(objtree) $(MODLIB)/build ; \
971         fi
972         @cp -f $(objtree)/modules.order $(MODLIB)/
973         @cp -f $(objtree)/modules.builtin $(MODLIB)/
974         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modinst
976 # This depmod is only for convenience to give the initial
977 # boot a modules.dep even before / is mounted read-write.  However the
978 # boot script depmod is the master version.
979 PHONY += _modinst_post
980 _modinst_post: _modinst_
981         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.fwinst obj=firmware __fw_modinst
982         $(call cmd,depmod)
984 ifeq ($(CONFIG_MODULE_SIG), y)
985 PHONY += modules_sign
986 modules_sign:
987         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modsign
988 endif
990 else # CONFIG_MODULES
992 # Modules not configured
993 # ---------------------------------------------------------------------------
995 modules modules_install: FORCE
996         @echo >&2
997         @echo >&2 "The present kernel configuration has modules disabled."
998         @echo >&2 "Type 'make config' and enable loadable module support."
999         @echo >&2 "Then build a kernel with module support enabled."
1000         @echo >&2
1001         @exit 1
1003 endif # CONFIG_MODULES
1005 ###
1006 # Cleaning is done on three levels.
1007 # make clean     Delete most generated files
1008 #                Leave enough to build external modules
1009 # make mrproper  Delete the current configuration, and all generated files
1010 # make distclean Remove editor backup files, patch leftover files and the like
1012 # Directories & files removed with 'make clean'
1013 CLEAN_DIRS  += $(MODVERDIR)
1015 # Directories & files removed with 'make mrproper'
1016 MRPROPER_DIRS  += include/config usr/include include/generated          \
1017                   arch/*/include/generated
1018 MRPROPER_FILES += .config .config.old .version .old_version $(version_h) \
1019                   Module.symvers tags TAGS cscope* GPATH GTAGS GRTAGS GSYMS \
1020                   signing_key.priv signing_key.x509 x509.genkey         \
1021                   extra_certificates signing_key.x509.keyid             \
1022                   signing_key.x509.signer
1024 # clean - Delete most, but leave enough to build external modules
1026 clean: rm-dirs  := $(CLEAN_DIRS)
1027 clean: rm-files := $(CLEAN_FILES)
1028 clean-dirs      := $(addprefix _clean_, . $(vmlinux-alldirs) Documentation samples)
1030 PHONY += $(clean-dirs) clean archclean vmlinuxclean
1031 $(clean-dirs):
1032         $(Q)$(MAKE) $(clean)=$(patsubst _clean_%,%,$@)
1034 vmlinuxclean:
1035         $(Q)$(CONFIG_SHELL) $(srctree)/scripts/link-vmlinux.sh clean
1037 clean: archclean vmlinuxclean
1039 # mrproper - Delete all generated files, including .config
1041 mrproper: rm-dirs  := $(wildcard $(MRPROPER_DIRS))
1042 mrproper: rm-files := $(wildcard $(MRPROPER_FILES))
1043 mrproper-dirs      := $(addprefix _mrproper_,Documentation/DocBook scripts)
1045 PHONY += $(mrproper-dirs) mrproper archmrproper
1046 $(mrproper-dirs):
1047         $(Q)$(MAKE) $(clean)=$(patsubst _mrproper_%,%,$@)
1049 mrproper: clean archmrproper $(mrproper-dirs)
1050         $(call cmd,rmdirs)
1051         $(call cmd,rmfiles)
1053 # distclean
1055 PHONY += distclean
1057 distclean: mrproper
1058         @find $(srctree) $(RCS_FIND_IGNORE) \
1059                 \( -name '*.orig' -o -name '*.rej' -o -name '*~' \
1060                 -o -name '*.bak' -o -name '#*#' -o -name '.*.orig' \
1061                 -o -name '.*.rej' \
1062                 -o -name '*%' -o -name '.*.cmd' -o -name 'core' \) \
1063                 -type f -print | xargs rm -f
1066 # Packaging of the kernel to various formats
1067 # ---------------------------------------------------------------------------
1068 # rpm target kept for backward compatibility
1069 package-dir     := $(srctree)/scripts/package
1071 %src-pkg: FORCE
1072         $(Q)$(MAKE) $(build)=$(package-dir) $@
1073 %pkg: include/config/kernel.release FORCE
1074         $(Q)$(MAKE) $(build)=$(package-dir) $@
1075 rpm: include/config/kernel.release FORCE
1076         $(Q)$(MAKE) $(build)=$(package-dir) $@
1079 # Brief documentation of the typical targets used
1080 # ---------------------------------------------------------------------------
1082 boards := $(wildcard $(srctree)/arch/$(SRCARCH)/configs/*_defconfig)
1083 boards := $(notdir $(boards))
1084 board-dirs := $(dir $(wildcard $(srctree)/arch/$(SRCARCH)/configs/*/*_defconfig))
1085 board-dirs := $(sort $(notdir $(board-dirs:/=)))
1087 help:
1088         @echo  'Cleaning targets:'
1089         @echo  '  clean           - Remove most generated files but keep the config and'
1090         @echo  '                    enough build support to build external modules'
1091         @echo  '  mrproper        - Remove all generated files + config + various backup files'
1092         @echo  '  distclean       - mrproper + remove editor backup and patch files'
1093         @echo  ''
1094         @echo  'Configuration targets:'
1095         @$(MAKE) -f $(srctree)/scripts/kconfig/Makefile help
1096         @echo  ''
1097         @echo  'Other generic targets:'
1098         @echo  '  all             - Build all targets marked with [*]'
1099         @echo  '* vmlinux         - Build the bare kernel'
1100         @echo  '* modules         - Build all modules'
1101         @echo  '  modules_install - Install all modules to INSTALL_MOD_PATH (default: /)'
1102         @echo  '  firmware_install- Install all firmware to INSTALL_FW_PATH'
1103         @echo  '                    (default: $$(INSTALL_MOD_PATH)/lib/firmware)'
1104         @echo  '  dir/            - Build all files in dir and below'
1105         @echo  '  dir/file.[oisS] - Build specified target only'
1106         @echo  '  dir/file.lst    - Build specified mixed source/assembly target only'
1107         @echo  '                    (requires a recent binutils and recent build (System.map))'
1108         @echo  '  dir/file.ko     - Build module including final link'
1109         @echo  '  modules_prepare - Set up for building external modules'
1110         @echo  '  tags/TAGS       - Generate tags file for editors'
1111         @echo  '  cscope          - Generate cscope index'
1112         @echo  '  gtags           - Generate GNU GLOBAL index'
1113         @echo  '  kernelrelease   - Output the release version string'
1114         @echo  '  kernelversion   - Output the version stored in Makefile'
1115         @echo  '  headers_install - Install sanitised kernel headers to INSTALL_HDR_PATH'; \
1116          echo  '                    (default: $(INSTALL_HDR_PATH))'; \
1117          echo  ''
1118         @echo  'Static analysers'
1119         @echo  '  checkstack      - Generate a list of stack hogs'
1120         @echo  '  namespacecheck  - Name space analysis on compiled kernel'
1121         @echo  '  versioncheck    - Sanity check on version.h usage'
1122         @echo  '  includecheck    - Check for duplicate included header files'
1123         @echo  '  export_report   - List the usages of all exported symbols'
1124         @echo  '  headers_check   - Sanity check on exported headers'
1125         @echo  '  headerdep       - Detect inclusion cycles in headers'
1126         @$(MAKE) -f $(srctree)/scripts/Makefile.help checker-help
1127         @echo  ''
1128         @echo  'Kernel packaging:'
1129         @$(MAKE) $(build)=$(package-dir) help
1130         @echo  ''
1131         @echo  'Documentation targets:'
1132         @$(MAKE) -f $(srctree)/Documentation/DocBook/Makefile dochelp
1133         @echo  ''
1134         @echo  'Architecture specific targets ($(SRCARCH)):'
1135         @$(if $(archhelp),$(archhelp),\
1136                 echo '  No architecture specific help defined for $(SRCARCH)')
1137         @echo  ''
1138         @$(if $(boards), \
1139                 $(foreach b, $(boards), \
1140                 printf "  %-24s - Build for %s\\n" $(b) $(subst _defconfig,,$(b));) \
1141                 echo '')
1142         @$(if $(board-dirs), \
1143                 $(foreach b, $(board-dirs), \
1144                 printf "  %-16s - Show %s-specific targets\\n" help-$(b) $(b);) \
1145                 printf "  %-16s - Show all of the above\\n" help-boards; \
1146                 echo '')
1148         @echo  '  make V=0|1 [targets] 0 => quiet build (default), 1 => verbose build'
1149         @echo  '  make V=2   [targets] 2 => give reason for rebuild of target'
1150         @echo  '  make O=dir [targets] Locate all output files in "dir", including .config'
1151         @echo  '  make C=1   [targets] Check all c source with $$CHECK (sparse by default)'
1152         @echo  '  make C=2   [targets] Force check of all c source with $$CHECK'
1153         @echo  '  make RECORDMCOUNT_WARN=1 [targets] Warn about ignored mcount sections'
1154         @echo  '  make W=n   [targets] Enable extra gcc checks, n=1,2,3 where'
1155         @echo  '                1: warnings which may be relevant and do not occur too often'
1156         @echo  '                2: warnings which occur quite often but may still be relevant'
1157         @echo  '                3: more obscure warnings, can most likely be ignored'
1158         @echo  '                Multiple levels can be combined with W=12 or W=123'
1159         @echo  ''
1160         @echo  'Execute "make" or "make all" to build all targets marked with [*] '
1161         @echo  'For further info see the ./README file'
1164 help-board-dirs := $(addprefix help-,$(board-dirs))
1166 help-boards: $(help-board-dirs)
1168 boards-per-dir = $(notdir $(wildcard $(srctree)/arch/$(SRCARCH)/configs/$*/*_defconfig))
1170 $(help-board-dirs): help-%:
1171         @echo  'Architecture specific targets ($(SRCARCH) $*):'
1172         @$(if $(boards-per-dir), \
1173                 $(foreach b, $(boards-per-dir), \
1174                 printf "  %-24s - Build for %s\\n" $*/$(b) $(subst _defconfig,,$(b));) \
1175                 echo '')
1178 # Documentation targets
1179 # ---------------------------------------------------------------------------
1180 %docs: scripts_basic FORCE
1181         $(Q)$(MAKE) $(build)=scripts build_docproc
1182         $(Q)$(MAKE) $(build)=Documentation/DocBook $@
1184 else # KBUILD_EXTMOD
1186 ###
1187 # External module support.
1188 # When building external modules the kernel used as basis is considered
1189 # read-only, and no consistency checks are made and the make
1190 # system is not used on the basis kernel. If updates are required
1191 # in the basis kernel ordinary make commands (without M=...) must
1192 # be used.
1194 # The following are the only valid targets when building external
1195 # modules.
1196 # make M=dir clean     Delete all automatically generated files
1197 # make M=dir modules   Make all modules in specified dir
1198 # make M=dir           Same as 'make M=dir modules'
1199 # make M=dir modules_install
1200 #                      Install the modules built in the module directory
1201 #                      Assumes install directory is already created
1203 # We are always building modules
1204 KBUILD_MODULES := 1
1205 PHONY += crmodverdir
1206 crmodverdir:
1207         $(cmd_crmodverdir)
1209 PHONY += $(objtree)/Module.symvers
1210 $(objtree)/Module.symvers:
1211         @test -e $(objtree)/Module.symvers || ( \
1212         echo; \
1213         echo "  WARNING: Symbol version dump $(objtree)/Module.symvers"; \
1214         echo "           is missing; modules will have no dependencies and modversions."; \
1215         echo )
1217 module-dirs := $(addprefix _module_,$(KBUILD_EXTMOD))
1218 PHONY += $(module-dirs) modules
1219 $(module-dirs): crmodverdir $(objtree)/Module.symvers
1220         $(Q)$(MAKE) $(build)=$(patsubst _module_%,%,$@)
1222 modules: $(module-dirs)
1223         @$(kecho) '  Building modules, stage 2.';
1224         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modpost
1226 PHONY += modules_install
1227 modules_install: _emodinst_ _emodinst_post
1229 install-dir := $(if $(INSTALL_MOD_DIR),$(INSTALL_MOD_DIR),extra)
1230 PHONY += _emodinst_
1231 _emodinst_:
1232         $(Q)mkdir -p $(MODLIB)/$(install-dir)
1233         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modinst
1235 PHONY += _emodinst_post
1236 _emodinst_post: _emodinst_
1237         $(call cmd,depmod)
1239 clean-dirs := $(addprefix _clean_,$(KBUILD_EXTMOD))
1241 PHONY += $(clean-dirs) clean
1242 $(clean-dirs):
1243         $(Q)$(MAKE) $(clean)=$(patsubst _clean_%,%,$@)
1245 clean:  rm-dirs := $(MODVERDIR)
1246 clean: rm-files := $(KBUILD_EXTMOD)/Module.symvers
1248 help:
1249         @echo  '  Building external modules.'
1250         @echo  '  Syntax: make -C path/to/kernel/src M=$$PWD target'
1251         @echo  ''
1252         @echo  '  modules         - default target, build the module(s)'
1253         @echo  '  modules_install - install the module'
1254         @echo  '  clean           - remove generated files in module directory only'
1255         @echo  ''
1257 # Dummies...
1258 PHONY += prepare scripts
1259 prepare: ;
1260 scripts: ;
1261 endif # KBUILD_EXTMOD
1263 clean: $(clean-dirs)
1264         $(call cmd,rmdirs)
1265         $(call cmd,rmfiles)
1266         @find $(if $(KBUILD_EXTMOD), $(KBUILD_EXTMOD), .) $(RCS_FIND_IGNORE) \
1267                 \( -name '*.[oas]' -o -name '*.ko' -o -name '.*.cmd' \
1268                 -o -name '*.ko.*' \
1269                 -o -name '.*.d' -o -name '.*.tmp' -o -name '*.mod.c' \
1270                 -o -name '*.symtypes' -o -name 'modules.order' \
1271                 -o -name modules.builtin -o -name '.tmp_*.o.*' \
1272                 -o -name '*.gcno' \) -type f -print | xargs rm -f
1274 # Generate tags for editors
1275 # ---------------------------------------------------------------------------
1276 quiet_cmd_tags = GEN     $@
1277       cmd_tags = $(CONFIG_SHELL) $(srctree)/scripts/tags.sh $@
1279 tags TAGS cscope gtags: FORCE
1280         $(call cmd,tags)
1282 # Scripts to check various things for consistency
1283 # ---------------------------------------------------------------------------
1285 PHONY += includecheck versioncheck coccicheck namespacecheck export_report
1287 includecheck:
1288         find $(srctree)/* $(RCS_FIND_IGNORE) \
1289                 -name '*.[hcS]' -type f -print | sort \
1290                 | xargs $(PERL) -w $(srctree)/scripts/checkincludes.pl
1292 versioncheck:
1293         find $(srctree)/* $(RCS_FIND_IGNORE) \
1294                 -name '*.[hcS]' -type f -print | sort \
1295                 | xargs $(PERL) -w $(srctree)/scripts/checkversion.pl
1297 coccicheck:
1298         $(Q)$(CONFIG_SHELL) $(srctree)/scripts/$@
1300 namespacecheck:
1301         $(PERL) $(srctree)/scripts/namespace.pl
1303 export_report:
1304         $(PERL) $(srctree)/scripts/export_report.pl
1306 endif #ifeq ($(config-targets),1)
1307 endif #ifeq ($(mixed-targets),1)
1309 PHONY += checkstack kernelrelease kernelversion
1311 # UML needs a little special treatment here.  It wants to use the host
1312 # toolchain, so needs $(SUBARCH) passed to checkstack.pl.  Everyone
1313 # else wants $(ARCH), including people doing cross-builds, which means
1314 # that $(SUBARCH) doesn't work here.
1315 ifeq ($(ARCH), um)
1316 CHECKSTACK_ARCH := $(SUBARCH)
1317 else
1318 CHECKSTACK_ARCH := $(ARCH)
1319 endif
1320 checkstack:
1321         $(OBJDUMP) -d vmlinux $$(find . -name '*.ko') | \
1322         $(PERL) $(src)/scripts/checkstack.pl $(CHECKSTACK_ARCH)
1324 kernelrelease:
1325         @echo "$(KERNELVERSION)$$($(CONFIG_SHELL) $(srctree)/scripts/setlocalversion $(srctree))"
1327 kernelversion:
1328         @echo $(KERNELVERSION)
1330 # Clear a bunch of variables before executing the submake
1331 tools/: FORCE
1332         $(Q)mkdir -p $(objtree)/tools
1333         $(Q)$(MAKE) LDFLAGS= MAKEFLAGS= O=$(objtree) subdir=tools -C $(src)/tools/
1335 tools/%: FORCE
1336         $(Q)mkdir -p $(objtree)/tools
1337         $(Q)$(MAKE) LDFLAGS= MAKEFLAGS= O=$(objtree) subdir=tools -C $(src)/tools/ $*
1339 # Single targets
1340 # ---------------------------------------------------------------------------
1341 # Single targets are compatible with:
1342 # - build with mixed source and output
1343 # - build with separate output dir 'make O=...'
1344 # - external modules
1346 #  target-dir => where to store outputfile
1347 #  build-dir  => directory in kernel source tree to use
1349 ifeq ($(KBUILD_EXTMOD),)
1350         build-dir  = $(patsubst %/,%,$(dir $@))
1351         target-dir = $(dir $@)
1352 else
1353         zap-slash=$(filter-out .,$(patsubst %/,%,$(dir $@)))
1354         build-dir  = $(KBUILD_EXTMOD)$(if $(zap-slash),/$(zap-slash))
1355         target-dir = $(if $(KBUILD_EXTMOD),$(dir $<),$(dir $@))
1356 endif
1358 %.s: %.c prepare scripts FORCE
1359         $(Q)$(MAKE) $(build)=$(build-dir) $(target-dir)$(notdir $@)
1360 %.i: %.c prepare scripts FORCE
1361         $(Q)$(MAKE) $(build)=$(build-dir) $(target-dir)$(notdir $@)
1362 %.o: %.c prepare scripts FORCE
1363         $(Q)$(MAKE) $(build)=$(build-dir) $(target-dir)$(notdir $@)
1364 %.lst: %.c prepare scripts FORCE
1365         $(Q)$(MAKE) $(build)=$(build-dir) $(target-dir)$(notdir $@)
1366 %.s: %.S prepare scripts FORCE
1367         $(Q)$(MAKE) $(build)=$(build-dir) $(target-dir)$(notdir $@)
1368 %.o: %.S prepare scripts FORCE
1369         $(Q)$(MAKE) $(build)=$(build-dir) $(target-dir)$(notdir $@)
1370 %.symtypes: %.c prepare scripts FORCE
1371         $(Q)$(MAKE) $(build)=$(build-dir) $(target-dir)$(notdir $@)
1373 # Modules
1374 /: prepare scripts FORCE
1375         $(cmd_crmodverdir)
1376         $(Q)$(MAKE) KBUILD_MODULES=$(if $(CONFIG_MODULES),1) \
1377         $(build)=$(build-dir)
1378 %/: prepare scripts FORCE
1379         $(cmd_crmodverdir)
1380         $(Q)$(MAKE) KBUILD_MODULES=$(if $(CONFIG_MODULES),1) \
1381         $(build)=$(build-dir)
1382 %.ko: prepare scripts FORCE
1383         $(cmd_crmodverdir)
1384         $(Q)$(MAKE) KBUILD_MODULES=$(if $(CONFIG_MODULES),1)   \
1385         $(build)=$(build-dir) $(@:.ko=.o)
1386         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modpost
1388 # FIXME Should go into a make.lib or something 
1389 # ===========================================================================
1391 quiet_cmd_rmdirs = $(if $(wildcard $(rm-dirs)),CLEAN   $(wildcard $(rm-dirs)))
1392       cmd_rmdirs = rm -rf $(rm-dirs)
1394 quiet_cmd_rmfiles = $(if $(wildcard $(rm-files)),CLEAN   $(wildcard $(rm-files)))
1395       cmd_rmfiles = rm -f $(rm-files)
1397 # Run depmod only if we have System.map and depmod is executable
1398 quiet_cmd_depmod = DEPMOD  $(KERNELRELEASE)
1399       cmd_depmod = $(CONFIG_SHELL) $(srctree)/scripts/depmod.sh $(DEPMOD) \
1400                    $(KERNELRELEASE)
1402 # Create temporary dir for module support files
1403 # clean it up only when building all modules
1404 cmd_crmodverdir = $(Q)mkdir -p $(MODVERDIR) \
1405                   $(if $(KBUILD_MODULES),; rm -f $(MODVERDIR)/*)
1407 # read all saved command lines
1409 targets := $(wildcard $(sort $(targets)))
1410 cmd_files := $(wildcard .*.cmd $(foreach f,$(targets),$(dir $(f)).$(notdir $(f)).cmd))
1412 ifneq ($(cmd_files),)
1413   $(cmd_files): ;       # Do not try to update included dependency files
1414   include $(cmd_files)
1415 endif
1417 # Shorthand for $(Q)$(MAKE) -f scripts/Makefile.clean obj=dir
1418 # Usage:
1419 # $(Q)$(MAKE) $(clean)=dir
1420 clean := -f $(if $(KBUILD_SRC),$(srctree)/)scripts/Makefile.clean obj
1422 endif   # skip-makefile
1424 PHONY += FORCE
1425 FORCE:
1427 # Declare the contents of the .PHONY variable as phony.  We keep that
1428 # information in a variable so we can use it in if_changed and friends.
1429 .PHONY: $(PHONY)