1 #ifndef _ALPHA_FCNTL_H
2 #define _ALPHA_FCNTL_H
4 #define O_CREAT 01000 /* not fcntl */
5 #define O_TRUNC 02000 /* not fcntl */
6 #define O_EXCL 04000 /* not fcntl */
7 #define O_NOCTTY 010000 /* not fcntl */
9 #define O_NONBLOCK 00004
10 #define O_APPEND 00010
11 #define O_DSYNC 040000 /* used to be O_SYNC, see below */
12 #define O_DIRECTORY 0100000 /* must be a directory */
13 #define O_NOFOLLOW 0200000 /* don't follow links */
14 #define O_LARGEFILE 0400000 /* will be set by the kernel on every open */
15 #define O_DIRECT 02000000 /* direct disk access - should check with OSF/1 */
16 #define O_NOATIME 04000000
17 #define O_CLOEXEC 010000000 /* set close_on_exec */
18 /*
19 * Before Linux 2.6.33 only O_DSYNC semantics were implemented, but using
20 * the O_SYNC flag. We continue to use the existing numerical value
21 * for O_DSYNC semantics now, but using the correct symbolic name for it.
22 * This new value is used to request true Posix O_SYNC semantics. It is
23 * defined in this strange way to make sure applications compiled against
24 * new headers get at least O_DSYNC semantics on older kernels.
25 *
26 * This has the nice side-effect that we can simply test for O_DSYNC
27 * wherever we do not care if O_DSYNC or O_SYNC is used.
28 *
29 * Note: __O_SYNC must never be used directly.
30 */
31 #define __O_SYNC 020000000
32 #define O_SYNC (__O_SYNC|O_DSYNC)
34 #define O_PATH 040000000
36 #define F_GETLK 7
37 #define F_SETLK 8
38 #define F_SETLKW 9
40 #define F_SETOWN 5 /* for sockets. */
41 #define F_GETOWN 6 /* for sockets. */
42 #define F_SETSIG 10 /* for sockets. */
43 #define F_GETSIG 11 /* for sockets. */
45 /* for posix fcntl() and lockf() */
46 #define F_RDLCK 1
47 #define F_WRLCK 2
48 #define F_UNLCK 8
50 /* for old implementation of bsd flock () */
51 #define F_EXLCK 16 /* or 3 */
52 #define F_SHLCK 32 /* or 4 */
54 #include <asm-generic/fcntl.h>
56 #endif