1 config ARM
2 bool
3 default y
4 select ARCH_BINFMT_ELF_RANDOMIZE_PIE
5 select ARCH_HAS_ATOMIC64_DEC_IF_POSITIVE
6 select ARCH_HAVE_CUSTOM_GPIO_H
7 select ARCH_WANT_IPC_PARSE_VERSION
8 select BUILDTIME_EXTABLE_SORT if MMU
9 select CPU_PM if (SUSPEND || CPU_IDLE)
10 select DCACHE_WORD_ACCESS if (CPU_V6 || CPU_V6K || CPU_V7) && !CPU_BIG_ENDIAN && MMU
11 select GENERIC_ATOMIC64 if (CPU_V6 || !CPU_32v6K || !AEABI)
12 select GENERIC_CLOCKEVENTS_BROADCAST if SMP
13 select GENERIC_IRQ_PROBE
14 select GENERIC_IRQ_SHOW
15 select GENERIC_PCI_IOMAP
16 select GENERIC_SMP_IDLE_THREAD
17 select GENERIC_STRNCPY_FROM_USER
18 select GENERIC_STRNLEN_USER
19 select HARDIRQS_SW_RESEND
20 select HAVE_AOUT
21 select HAVE_ARCH_JUMP_LABEL if !XIP_KERNEL
22 select HAVE_ARCH_KGDB
23 select HAVE_ARCH_SECCOMP_FILTER
24 select HAVE_ARCH_TRACEHOOK
25 select HAVE_BPF_JIT
26 select HAVE_C_RECORDMCOUNT
27 select HAVE_DEBUG_KMEMLEAK
28 select HAVE_DMA_API_DEBUG
29 select HAVE_DMA_ATTRS
30 select HAVE_DMA_CONTIGUOUS if MMU
31 select HAVE_DYNAMIC_FTRACE if (!XIP_KERNEL)
32 select HAVE_FTRACE_MCOUNT_RECORD if (!XIP_KERNEL)
33 select HAVE_FUNCTION_GRAPH_TRACER if (!THUMB2_KERNEL)
34 select HAVE_FUNCTION_TRACER if (!XIP_KERNEL)
35 select HAVE_GENERIC_DMA_COHERENT
36 select HAVE_GENERIC_HARDIRQS
37 select HAVE_HW_BREAKPOINT if (PERF_EVENTS && (CPU_V6 || CPU_V6K || CPU_V7))
38 select HAVE_IDE if PCI || ISA || PCMCIA
39 select HAVE_IRQ_WORK
40 select HAVE_KERNEL_GZIP
41 select HAVE_KERNEL_LZMA
42 select HAVE_KERNEL_LZO
43 select HAVE_KERNEL_XZ
44 select HAVE_KPROBES if !XIP_KERNEL
45 select HAVE_KRETPROBES if (HAVE_KPROBES)
46 select HAVE_MEMBLOCK
47 select HAVE_OPROFILE if (HAVE_PERF_EVENTS)
48 select HAVE_PERF_EVENTS
49 select HAVE_REGS_AND_STACK_ACCESS_API
50 select HAVE_SYSCALL_TRACEPOINTS
51 select HAVE_UID16
52 select KTIME_SCALAR
53 select PERF_USE_VMALLOC
54 select RTC_LIB
55 select SYS_SUPPORTS_APM_EMULATION
56 select HAVE_MOD_ARCH_SPECIFIC if ARM_UNWIND
57 select MODULES_USE_ELF_REL
58 select CLONE_BACKWARDS
59 help
60 The ARM series is a line of low-power-consumption RISC chip designs
61 licensed by ARM Ltd and targeted at embedded applications and
62 handhelds such as the Compaq IPAQ. ARM-based PCs are no longer
63 manufactured, but legacy ARM-based PC hardware remains popular in
64 Europe. There is an ARM Linux project with a web page at
65 <http://www.arm.linux.org.uk/>.
67 config ARM_HAS_SG_CHAIN
68 bool
70 config NEED_SG_DMA_LENGTH
71 bool
73 config ARM_DMA_USE_IOMMU
74 bool
75 select ARM_HAS_SG_CHAIN
76 select NEED_SG_DMA_LENGTH
78 config HAVE_PWM
79 bool
81 config MIGHT_HAVE_PCI
82 bool
84 config SYS_SUPPORTS_APM_EMULATION
85 bool
87 config GENERIC_GPIO
88 bool
90 config HAVE_TCM
91 bool
92 select GENERIC_ALLOCATOR
94 config HAVE_PROC_CPU
95 bool
97 config NO_IOPORT
98 bool
100 config EISA
101 bool
102 ---help---
103 The Extended Industry Standard Architecture (EISA) bus was
104 developed as an open alternative to the IBM MicroChannel bus.
106 The EISA bus provided some of the features of the IBM MicroChannel
107 bus while maintaining backward compatibility with cards made for
108 the older ISA bus. The EISA bus saw limited use between 1988 and
109 1995 when it was made obsolete by the PCI bus.
111 Say Y here if you are building a kernel for an EISA-based machine.
113 Otherwise, say N.
115 config SBUS
116 bool
118 config STACKTRACE_SUPPORT
119 bool
120 default y
122 config HAVE_LATENCYTOP_SUPPORT
123 bool
124 depends on !SMP
125 default y
127 config LOCKDEP_SUPPORT
128 bool
129 default y
131 config TRACE_IRQFLAGS_SUPPORT
132 bool
133 default y
135 config RWSEM_GENERIC_SPINLOCK
136 bool
137 default y
139 config RWSEM_XCHGADD_ALGORITHM
140 bool
142 config ARCH_HAS_ILOG2_U32
143 bool
145 config ARCH_HAS_ILOG2_U64
146 bool
148 config ARCH_HAS_CPUFREQ
149 bool
150 help
151 Internal node to signify that the ARCH has CPUFREQ support
152 and that the relevant menu configurations are displayed for
153 it.
155 config GENERIC_HWEIGHT
156 bool
157 default y
159 config GENERIC_CALIBRATE_DELAY
160 bool
161 default y
163 config ARCH_MAY_HAVE_PC_FDC
164 bool
166 config ZONE_DMA
167 bool
169 config NEED_DMA_MAP_STATE
170 def_bool y
172 config ARCH_HAS_DMA_SET_COHERENT_MASK
173 bool
175 config GENERIC_ISA_DMA
176 bool
178 config FIQ
179 bool
181 config NEED_RET_TO_USER
182 bool
184 config ARCH_MTD_XIP
185 bool
187 config VECTORS_BASE
188 hex
189 default 0xffff0000 if MMU || CPU_HIGH_VECTOR
190 default DRAM_BASE if REMAP_VECTORS_TO_RAM
191 default 0x00000000
192 help
193 The base address of exception vectors.
195 config ARM_PATCH_PHYS_VIRT
196 bool "Patch physical to virtual translations at runtime" if EMBEDDED
197 default y
198 depends on !XIP_KERNEL && MMU
199 depends on !ARCH_REALVIEW || !SPARSEMEM
200 help
201 Patch phys-to-virt and virt-to-phys translation functions at
202 boot and module load time according to the position of the
203 kernel in system memory.
205 This can only be used with non-XIP MMU kernels where the base
206 of physical memory is at a 16MB boundary.
208 Only disable this option if you know that you do not require
209 this feature (eg, building a kernel for a single machine) and
210 you need to shrink the kernel to the minimal size.
212 config NEED_MACH_GPIO_H
213 bool
214 help
215 Select this when mach/gpio.h is required to provide special
216 definitions for this platform. The need for mach/gpio.h should
217 be avoided when possible.
219 config NEED_MACH_IO_H
220 bool
221 help
222 Select this when mach/io.h is required to provide special
223 definitions for this platform. The need for mach/io.h should
224 be avoided when possible.
226 config NEED_MACH_MEMORY_H
227 bool
228 help
229 Select this when mach/memory.h is required to provide special
230 definitions for this platform. The need for mach/memory.h should
231 be avoided when possible.
233 config PHYS_OFFSET
234 hex "Physical address of main memory" if MMU
235 depends on !ARM_PATCH_PHYS_VIRT && !NEED_MACH_MEMORY_H
236 default DRAM_BASE if !MMU
237 help
238 Please provide the physical address corresponding to the
239 location of main memory in your system.
241 config GENERIC_BUG
242 def_bool y
243 depends on BUG
245 source "init/Kconfig"
247 source "kernel/Kconfig.freezer"
249 menu "System Type"
251 config MMU
252 bool "MMU-based Paged Memory Management Support"
253 default y
254 help
255 Select if you want MMU-based virtualised addressing space
256 support by paged memory management. If unsure, say 'Y'.
258 #
259 # The "ARM system type" choice list is ordered alphabetically by option
260 # text. Please add new entries in the option alphabetic order.
261 #
262 choice
263 prompt "ARM system type"
264 default ARCH_MULTIPLATFORM
266 config ARCH_MULTIPLATFORM
267 bool "Allow multiple platforms to be selected"
268 depends on MMU
269 select ARM_PATCH_PHYS_VIRT
270 select AUTO_ZRELADDR
271 select COMMON_CLK
272 select MULTI_IRQ_HANDLER
273 select SPARSE_IRQ
274 select USE_OF
276 config ARCH_INTEGRATOR
277 bool "ARM Ltd. Integrator family"
278 select ARCH_HAS_CPUFREQ
279 select ARM_AMBA
280 select COMMON_CLK
281 select COMMON_CLK_VERSATILE
282 select GENERIC_CLOCKEVENTS
283 select HAVE_TCM
284 select ICST
285 select MULTI_IRQ_HANDLER
286 select NEED_MACH_MEMORY_H
287 select PLAT_VERSATILE
288 select SPARSE_IRQ
289 select VERSATILE_FPGA_IRQ
290 help
291 Support for ARM's Integrator platform.
293 config ARCH_REALVIEW
294 bool "ARM Ltd. RealView family"
295 select ARCH_WANT_OPTIONAL_GPIOLIB
296 select ARM_AMBA
297 select ARM_TIMER_SP804
298 select COMMON_CLK
299 select COMMON_CLK_VERSATILE
300 select GENERIC_CLOCKEVENTS
301 select GPIO_PL061 if GPIOLIB
302 select ICST
303 select NEED_MACH_MEMORY_H
304 select PLAT_VERSATILE
305 select PLAT_VERSATILE_CLCD
306 help
307 This enables support for ARM Ltd RealView boards.
309 config ARCH_VERSATILE
310 bool "ARM Ltd. Versatile family"
311 select ARCH_WANT_OPTIONAL_GPIOLIB
312 select ARM_AMBA
313 select ARM_TIMER_SP804
314 select ARM_VIC
315 select CLKDEV_LOOKUP
316 select GENERIC_CLOCKEVENTS
317 select HAVE_MACH_CLKDEV
318 select ICST
319 select PLAT_VERSATILE
320 select PLAT_VERSATILE_CLCD
321 select PLAT_VERSATILE_CLOCK
322 select VERSATILE_FPGA_IRQ
323 help
324 This enables support for ARM Ltd Versatile board.
326 config ARCH_AT91
327 bool "Atmel AT91"
328 select ARCH_REQUIRE_GPIOLIB
329 select CLKDEV_LOOKUP
330 select HAVE_CLK
331 select IRQ_DOMAIN
332 select NEED_MACH_GPIO_H
333 select NEED_MACH_IO_H if PCCARD
334 select PINCTRL
335 select PINCTRL_AT91 if USE_OF
336 help
337 This enables support for systems based on Atmel
338 AT91RM9200 and AT91SAM9* processors.
340 config ARCH_BCM2835
341 bool "Broadcom BCM2835 family"
342 select ARCH_REQUIRE_GPIOLIB
343 select ARM_AMBA
344 select ARM_ERRATA_411920
345 select ARM_TIMER_SP804
346 select CLKDEV_LOOKUP
347 select COMMON_CLK
348 select CPU_V6
349 select GENERIC_CLOCKEVENTS
350 select GENERIC_GPIO
351 select MULTI_IRQ_HANDLER
352 select PINCTRL
353 select PINCTRL_BCM2835
354 select SPARSE_IRQ
355 select USE_OF
356 help
357 This enables support for the Broadcom BCM2835 SoC. This SoC is
358 use in the Raspberry Pi, and Roku 2 devices.
360 config ARCH_CNS3XXX
361 bool "Cavium Networks CNS3XXX family"
362 select ARM_GIC
363 select CPU_V6K
364 select GENERIC_CLOCKEVENTS
365 select MIGHT_HAVE_CACHE_L2X0
366 select MIGHT_HAVE_PCI
367 select PCI_DOMAINS if PCI
368 help
369 Support for Cavium Networks CNS3XXX platform.
371 config ARCH_CLPS711X
372 bool "Cirrus Logic CLPS711x/EP721x/EP731x-based"
373 select ARCH_REQUIRE_GPIOLIB
374 select AUTO_ZRELADDR
375 select CLKDEV_LOOKUP
376 select COMMON_CLK
377 select CPU_ARM720T
378 select GENERIC_CLOCKEVENTS
379 select MULTI_IRQ_HANDLER
380 select NEED_MACH_MEMORY_H
381 select SPARSE_IRQ
382 help
383 Support for Cirrus Logic 711x/721x/731x based boards.
385 config ARCH_GEMINI
386 bool "Cortina Systems Gemini"
387 select ARCH_REQUIRE_GPIOLIB
388 select ARCH_USES_GETTIMEOFFSET
389 select CPU_FA526
390 help
391 Support for the Cortina Systems Gemini family SoCs
393 config ARCH_SIRF
394 bool "CSR SiRF"
395 select ARCH_REQUIRE_GPIOLIB
396 select COMMON_CLK
397 select GENERIC_CLOCKEVENTS
398 select GENERIC_IRQ_CHIP
399 select MIGHT_HAVE_CACHE_L2X0
400 select NO_IOPORT
401 select PINCTRL
402 select PINCTRL_SIRF
403 select USE_OF
404 help
405 Support for CSR SiRFprimaII/Marco/Polo platforms
407 config ARCH_EBSA110
408 bool "EBSA-110"
409 select ARCH_USES_GETTIMEOFFSET
410 select CPU_SA110
411 select ISA
412 select NEED_MACH_IO_H
413 select NEED_MACH_MEMORY_H
414 select NO_IOPORT
415 help
416 This is an evaluation board for the StrongARM processor available
417 from Digital. It has limited hardware on-board, including an
418 Ethernet interface, two PCMCIA sockets, two serial ports and a
419 parallel port.
421 config ARCH_EP93XX
422 bool "EP93xx-based"
423 select ARCH_HAS_HOLES_MEMORYMODEL
424 select ARCH_REQUIRE_GPIOLIB
425 select ARCH_USES_GETTIMEOFFSET
426 select ARM_AMBA
427 select ARM_VIC
428 select CLKDEV_LOOKUP
429 select CPU_ARM920T
430 select NEED_MACH_MEMORY_H
431 help
432 This enables support for the Cirrus EP93xx series of CPUs.
434 config ARCH_FOOTBRIDGE
435 bool "FootBridge"
436 select CPU_SA110
437 select FOOTBRIDGE
438 select GENERIC_CLOCKEVENTS
439 select HAVE_IDE
440 select NEED_MACH_IO_H if !MMU
441 select NEED_MACH_MEMORY_H
442 help
443 Support for systems based on the DC21285 companion chip
444 ("FootBridge"), such as the Simtec CATS and the Rebel NetWinder.
446 config ARCH_MXS
447 bool "Freescale MXS-based"
448 select ARCH_REQUIRE_GPIOLIB
449 select CLKDEV_LOOKUP
450 select CLKSRC_MMIO
451 select COMMON_CLK
452 select GENERIC_CLOCKEVENTS
453 select HAVE_CLK_PREPARE
454 select MULTI_IRQ_HANDLER
455 select PINCTRL
456 select SPARSE_IRQ
457 select USE_OF
458 help
459 Support for Freescale MXS-based family of processors
461 config ARCH_NETX
462 bool "Hilscher NetX based"
463 select ARM_VIC
464 select CLKSRC_MMIO
465 select CPU_ARM926T
466 select GENERIC_CLOCKEVENTS
467 help
468 This enables support for systems based on the Hilscher NetX Soc
470 config ARCH_H720X
471 bool "Hynix HMS720x-based"
472 select ARCH_USES_GETTIMEOFFSET
473 select CPU_ARM720T
474 select ISA_DMA_API
475 help
476 This enables support for systems based on the Hynix HMS720x
478 config ARCH_IOP13XX
479 bool "IOP13xx-based"
480 depends on MMU
481 select ARCH_SUPPORTS_MSI
482 select CPU_XSC3
483 select NEED_MACH_MEMORY_H
484 select NEED_RET_TO_USER
485 select PCI
486 select PLAT_IOP
487 select VMSPLIT_1G
488 help
489 Support for Intel's IOP13XX (XScale) family of processors.
491 config ARCH_IOP32X
492 bool "IOP32x-based"
493 depends on MMU
494 select ARCH_REQUIRE_GPIOLIB
495 select CPU_XSCALE
496 select NEED_MACH_GPIO_H
497 select NEED_RET_TO_USER
498 select PCI
499 select PLAT_IOP
500 help
501 Support for Intel's 80219 and IOP32X (XScale) family of
502 processors.
504 config ARCH_IOP33X
505 bool "IOP33x-based"
506 depends on MMU
507 select ARCH_REQUIRE_GPIOLIB
508 select CPU_XSCALE
509 select NEED_MACH_GPIO_H
510 select NEED_RET_TO_USER
511 select PCI
512 select PLAT_IOP
513 help
514 Support for Intel's IOP33X (XScale) family of processors.
516 config ARCH_IXP4XX
517 bool "IXP4xx-based"
518 depends on MMU
519 select ARCH_HAS_DMA_SET_COHERENT_MASK
520 select ARCH_REQUIRE_GPIOLIB
521 select CLKSRC_MMIO
522 select CPU_XSCALE
523 select DMABOUNCE if PCI
524 select GENERIC_CLOCKEVENTS
525 select MIGHT_HAVE_PCI
526 select NEED_MACH_IO_H
527 help
528 Support for Intel's IXP4XX (XScale) family of processors.
530 config ARCH_DOVE
531 bool "Marvell Dove"
532 select ARCH_REQUIRE_GPIOLIB
533 select COMMON_CLK_DOVE
534 select CPU_V7
535 select GENERIC_CLOCKEVENTS
536 select MIGHT_HAVE_PCI
537 select PINCTRL
538 select PINCTRL_DOVE
539 select PLAT_ORION_LEGACY
540 select USB_ARCH_HAS_EHCI
541 help
542 Support for the Marvell Dove SoC 88AP510
544 config ARCH_KIRKWOOD
545 bool "Marvell Kirkwood"
546 select ARCH_REQUIRE_GPIOLIB
547 select CPU_FEROCEON
548 select GENERIC_CLOCKEVENTS
549 select PCI
550 select PCI_QUIRKS
551 select PINCTRL
552 select PINCTRL_KIRKWOOD
553 select PLAT_ORION_LEGACY
554 help
555 Support for the following Marvell Kirkwood series SoCs:
556 88F6180, 88F6192 and 88F6281.
558 config ARCH_MV78XX0
559 bool "Marvell MV78xx0"
560 select ARCH_REQUIRE_GPIOLIB
561 select CPU_FEROCEON
562 select GENERIC_CLOCKEVENTS
563 select PCI
564 select PLAT_ORION_LEGACY
565 help
566 Support for the following Marvell MV78xx0 series SoCs:
567 MV781x0, MV782x0.
569 config ARCH_ORION5X
570 bool "Marvell Orion"
571 depends on MMU
572 select ARCH_REQUIRE_GPIOLIB
573 select CPU_FEROCEON
574 select GENERIC_CLOCKEVENTS
575 select PCI
576 select PLAT_ORION_LEGACY
577 help
578 Support for the following Marvell Orion 5x series SoCs:
579 Orion-1 (5181), Orion-VoIP (5181L), Orion-NAS (5182),
580 Orion-2 (5281), Orion-1-90 (6183).
582 config ARCH_MMP
583 bool "Marvell PXA168/910/MMP2"
584 depends on MMU
585 select ARCH_REQUIRE_GPIOLIB
586 select CLKDEV_LOOKUP
587 select GENERIC_ALLOCATOR
588 select GENERIC_CLOCKEVENTS
589 select GPIO_PXA
590 select IRQ_DOMAIN
591 select NEED_MACH_GPIO_H
592 select PINCTRL
593 select PLAT_PXA
594 select SPARSE_IRQ
595 help
596 Support for Marvell's PXA168/PXA910(MMP) and MMP2 processor line.
598 config ARCH_KS8695
599 bool "Micrel/Kendin KS8695"
600 select ARCH_REQUIRE_GPIOLIB
601 select CLKSRC_MMIO
602 select CPU_ARM922T
603 select GENERIC_CLOCKEVENTS
604 select NEED_MACH_MEMORY_H
605 help
606 Support for Micrel/Kendin KS8695 "Centaur" (ARM922T) based
607 System-on-Chip devices.
609 config ARCH_W90X900
610 bool "Nuvoton W90X900 CPU"
611 select ARCH_REQUIRE_GPIOLIB
612 select CLKDEV_LOOKUP
613 select CLKSRC_MMIO
614 select CPU_ARM926T
615 select GENERIC_CLOCKEVENTS
616 help
617 Support for Nuvoton (Winbond logic dept.) ARM9 processor,
618 At present, the w90x900 has been renamed nuc900, regarding
619 the ARM series product line, you can login the following
620 link address to know more.
622 <http://www.nuvoton.com/hq/enu/ProductAndSales/ProductLines/
623 ConsumerElectronicsIC/ARMMicrocontroller/ARMMicrocontroller>
625 config ARCH_LPC32XX
626 bool "NXP LPC32XX"
627 select ARCH_REQUIRE_GPIOLIB
628 select ARM_AMBA
629 select CLKDEV_LOOKUP
630 select CLKSRC_MMIO
631 select CPU_ARM926T
632 select GENERIC_CLOCKEVENTS
633 select HAVE_IDE
634 select HAVE_PWM
635 select USB_ARCH_HAS_OHCI
636 select USE_OF
637 help
638 Support for the NXP LPC32XX family of processors
640 config ARCH_TEGRA
641 bool "NVIDIA Tegra"
642 select ARCH_HAS_CPUFREQ
643 select CLKDEV_LOOKUP
644 select CLKSRC_MMIO
645 select COMMON_CLK
646 select GENERIC_CLOCKEVENTS
647 select GENERIC_GPIO
648 select HAVE_CLK
649 select HAVE_SMP
650 select MIGHT_HAVE_CACHE_L2X0
651 select SPARSE_IRQ
652 select USE_OF
653 help
654 This enables support for NVIDIA Tegra based systems (Tegra APX,
655 Tegra 6xx and Tegra 2 series).
657 config ARCH_PXA
658 bool "PXA2xx/PXA3xx-based"
659 depends on MMU
660 select ARCH_HAS_CPUFREQ
661 select ARCH_MTD_XIP
662 select ARCH_REQUIRE_GPIOLIB
663 select ARM_CPU_SUSPEND if PM
664 select AUTO_ZRELADDR
665 select CLKDEV_LOOKUP
666 select CLKSRC_MMIO
667 select GENERIC_CLOCKEVENTS
668 select GPIO_PXA
669 select HAVE_IDE
670 select MULTI_IRQ_HANDLER
671 select NEED_MACH_GPIO_H
672 select PLAT_PXA
673 select SPARSE_IRQ
674 help
675 Support for Intel/Marvell's PXA2xx/PXA3xx processor line.
677 config ARCH_MSM
678 bool "Qualcomm MSM"
679 select ARCH_REQUIRE_GPIOLIB
680 select CLKDEV_LOOKUP
681 select GENERIC_CLOCKEVENTS
682 select HAVE_CLK
683 help
684 Support for Qualcomm MSM/QSD based systems. This runs on the
685 apps processor of the MSM/QSD and depends on a shared memory
686 interface to the modem processor which runs the baseband
687 stack and controls some vital subsystems
688 (clock and power control, etc).
690 config ARCH_SHMOBILE
691 bool "Renesas SH-Mobile / R-Mobile"
692 select CLKDEV_LOOKUP
693 select GENERIC_CLOCKEVENTS
694 select HAVE_CLK
695 select HAVE_MACH_CLKDEV
696 select HAVE_SMP
697 select MIGHT_HAVE_CACHE_L2X0
698 select MULTI_IRQ_HANDLER
699 select NEED_MACH_MEMORY_H
700 select NO_IOPORT
701 select PM_GENERIC_DOMAINS if PM
702 select SPARSE_IRQ
703 help
704 Support for Renesas's SH-Mobile and R-Mobile ARM platforms.
706 config ARCH_RPC
707 bool "RiscPC"
708 select ARCH_ACORN
709 select ARCH_MAY_HAVE_PC_FDC
710 select ARCH_SPARSEMEM_ENABLE
711 select ARCH_USES_GETTIMEOFFSET
712 select FIQ
713 select HAVE_IDE
714 select HAVE_PATA_PLATFORM
715 select ISA_DMA_API
716 select NEED_MACH_IO_H
717 select NEED_MACH_MEMORY_H
718 select NO_IOPORT
719 help
720 On the Acorn Risc-PC, Linux can support the internal IDE disk and
721 CD-ROM interface, serial and parallel port, and the floppy drive.
723 config ARCH_SA1100
724 bool "SA1100-based"
725 select ARCH_HAS_CPUFREQ
726 select ARCH_MTD_XIP
727 select ARCH_REQUIRE_GPIOLIB
728 select ARCH_SPARSEMEM_ENABLE
729 select CLKDEV_LOOKUP
730 select CLKSRC_MMIO
731 select CPU_FREQ
732 select CPU_SA1100
733 select GENERIC_CLOCKEVENTS
734 select HAVE_IDE
735 select ISA
736 select NEED_MACH_GPIO_H
737 select NEED_MACH_MEMORY_H
738 select SPARSE_IRQ
739 help
740 Support for StrongARM 11x0 based boards.
742 config ARCH_S3C24XX
743 bool "Samsung S3C24XX SoCs"
744 select ARCH_HAS_CPUFREQ
745 select ARCH_USES_GETTIMEOFFSET
746 select CLKDEV_LOOKUP
747 select GENERIC_GPIO
748 select HAVE_CLK
749 select HAVE_S3C2410_I2C if I2C
750 select HAVE_S3C2410_WATCHDOG if WATCHDOG
751 select HAVE_S3C_RTC if RTC_CLASS
752 select NEED_MACH_GPIO_H
753 select NEED_MACH_IO_H
754 help
755 Samsung S3C2410, S3C2412, S3C2413, S3C2416, S3C2440, S3C2442, S3C2443
756 and S3C2450 SoCs based systems, such as the Simtec Electronics BAST
757 (<http://www.simtec.co.uk/products/EB110ITX/>), the IPAQ 1940 or the
758 Samsung SMDK2410 development board (and derivatives).
760 config ARCH_S3C64XX
761 bool "Samsung S3C64XX"
762 select ARCH_HAS_CPUFREQ
763 select ARCH_REQUIRE_GPIOLIB
764 select ARCH_USES_GETTIMEOFFSET
765 select ARM_VIC
766 select CLKDEV_LOOKUP
767 select CPU_V6
768 select HAVE_CLK
769 select HAVE_S3C2410_I2C if I2C
770 select HAVE_S3C2410_WATCHDOG if WATCHDOG
771 select HAVE_TCM
772 select NEED_MACH_GPIO_H
773 select NO_IOPORT
774 select PLAT_SAMSUNG
775 select S3C_DEV_NAND
776 select S3C_GPIO_TRACK
777 select SAMSUNG_CLKSRC
778 select SAMSUNG_GPIOLIB_4BIT
779 select SAMSUNG_IRQ_VIC_TIMER
780 select USB_ARCH_HAS_OHCI
781 help
782 Samsung S3C64XX series based systems
784 config ARCH_S5P64X0
785 bool "Samsung S5P6440 S5P6450"
786 select CLKDEV_LOOKUP
787 select CLKSRC_MMIO
788 select CPU_V6
789 select GENERIC_CLOCKEVENTS
790 select GENERIC_GPIO
791 select HAVE_CLK
792 select HAVE_S3C2410_I2C if I2C
793 select HAVE_S3C2410_WATCHDOG if WATCHDOG
794 select HAVE_S3C_RTC if RTC_CLASS
795 select NEED_MACH_GPIO_H
796 help
797 Samsung S5P64X0 CPU based systems, such as the Samsung SMDK6440,
798 SMDK6450.
800 config ARCH_S5PC100
801 bool "Samsung S5PC100"
802 select ARCH_USES_GETTIMEOFFSET
803 select CLKDEV_LOOKUP
804 select CPU_V7
805 select GENERIC_GPIO
806 select HAVE_CLK
807 select HAVE_S3C2410_I2C if I2C
808 select HAVE_S3C2410_WATCHDOG if WATCHDOG
809 select HAVE_S3C_RTC if RTC_CLASS
810 select NEED_MACH_GPIO_H
811 help
812 Samsung S5PC100 series based systems
814 config ARCH_S5PV210
815 bool "Samsung S5PV210/S5PC110"
816 select ARCH_HAS_CPUFREQ
817 select ARCH_HAS_HOLES_MEMORYMODEL
818 select ARCH_SPARSEMEM_ENABLE
819 select CLKDEV_LOOKUP
820 select CLKSRC_MMIO
821 select CPU_V7
822 select GENERIC_CLOCKEVENTS
823 select GENERIC_GPIO
824 select HAVE_CLK
825 select HAVE_S3C2410_I2C if I2C
826 select HAVE_S3C2410_WATCHDOG if WATCHDOG
827 select HAVE_S3C_RTC if RTC_CLASS
828 select NEED_MACH_GPIO_H
829 select NEED_MACH_MEMORY_H
830 help
831 Samsung S5PV210/S5PC110 series based systems
833 config ARCH_EXYNOS
834 bool "Samsung EXYNOS"
835 select ARCH_HAS_CPUFREQ
836 select ARCH_HAS_HOLES_MEMORYMODEL
837 select ARCH_SPARSEMEM_ENABLE
838 select CLKDEV_LOOKUP
839 select CPU_V7
840 select GENERIC_CLOCKEVENTS
841 select GENERIC_GPIO
842 select HAVE_CLK
843 select HAVE_S3C2410_I2C if I2C
844 select HAVE_S3C2410_WATCHDOG if WATCHDOG
845 select HAVE_S3C_RTC if RTC_CLASS
846 select NEED_MACH_GPIO_H
847 select NEED_MACH_MEMORY_H
848 help
849 Support for SAMSUNG's EXYNOS SoCs (EXYNOS4/5)
851 config ARCH_SHARK
852 bool "Shark"
853 select ARCH_USES_GETTIMEOFFSET
854 select CPU_SA110
855 select ISA
856 select ISA_DMA
857 select NEED_MACH_MEMORY_H
858 select PCI
859 select ZONE_DMA
860 help
861 Support for the StrongARM based Digital DNARD machine, also known
862 as "Shark" (<http://www.shark-linux.de/shark.html>).
864 config ARCH_U300
865 bool "ST-Ericsson U300 Series"
866 depends on MMU
867 select ARCH_REQUIRE_GPIOLIB
868 select ARM_AMBA
869 select ARM_PATCH_PHYS_VIRT
870 select ARM_VIC
871 select CLKDEV_LOOKUP
872 select CLKSRC_MMIO
873 select COMMON_CLK
874 select CPU_ARM926T
875 select GENERIC_CLOCKEVENTS
876 select GENERIC_GPIO
877 select HAVE_TCM
878 select SPARSE_IRQ
879 help
880 Support for ST-Ericsson U300 series mobile platforms.
882 config ARCH_U8500
883 bool "ST-Ericsson U8500 Series"
884 depends on MMU
885 select ARCH_HAS_CPUFREQ
886 select ARCH_REQUIRE_GPIOLIB
887 select ARM_AMBA
888 select CLKDEV_LOOKUP
889 select CPU_V7
890 select GENERIC_CLOCKEVENTS
891 select HAVE_SMP
892 select MIGHT_HAVE_CACHE_L2X0
893 select SPARSE_IRQ
894 help
895 Support for ST-Ericsson's Ux500 architecture
897 config ARCH_NOMADIK
898 bool "STMicroelectronics Nomadik"
899 select ARCH_REQUIRE_GPIOLIB
900 select ARM_AMBA
901 select ARM_VIC
902 select COMMON_CLK
903 select CPU_ARM926T
904 select GENERIC_CLOCKEVENTS
905 select MIGHT_HAVE_CACHE_L2X0
906 select PINCTRL
907 select PINCTRL_STN8815
908 select SPARSE_IRQ
909 help
910 Support for the Nomadik platform by ST-Ericsson
912 config PLAT_SPEAR
913 bool "ST SPEAr"
914 select ARCH_HAS_CPUFREQ
915 select ARCH_REQUIRE_GPIOLIB
916 select ARM_AMBA
917 select CLKDEV_LOOKUP
918 select CLKSRC_MMIO
919 select COMMON_CLK
920 select GENERIC_CLOCKEVENTS
921 select HAVE_CLK
922 help
923 Support for ST's SPEAr platform (SPEAr3xx, SPEAr6xx and SPEAr13xx).
925 config ARCH_DAVINCI
926 bool "TI DaVinci"
927 select ARCH_HAS_HOLES_MEMORYMODEL
928 select ARCH_REQUIRE_GPIOLIB
929 select CLKDEV_LOOKUP
930 select GENERIC_ALLOCATOR
931 select GENERIC_CLOCKEVENTS
932 select GENERIC_IRQ_CHIP
933 select HAVE_IDE
934 select NEED_MACH_GPIO_H
935 select TI_PRIV_EDMA
936 select USE_OF
937 select ZONE_DMA
938 help
939 Support for TI's DaVinci platform.
941 config ARCH_OMAP
942 bool "TI OMAP"
943 depends on MMU
944 select ARCH_HAS_CPUFREQ
945 select ARCH_HAS_HOLES_MEMORYMODEL
946 select ARCH_REQUIRE_GPIOLIB
947 select CLKSRC_MMIO
948 select GENERIC_CLOCKEVENTS
949 select HAVE_CLK
950 help
951 Support for TI's OMAP platform (OMAP1/2/3/4).
953 config ARCH_VT8500_SINGLE
954 bool "VIA/WonderMedia 85xx"
955 select ARCH_HAS_CPUFREQ
956 select ARCH_REQUIRE_GPIOLIB
957 select CLKDEV_LOOKUP
958 select COMMON_CLK
959 select CPU_ARM926T
960 select GENERIC_CLOCKEVENTS
961 select GENERIC_GPIO
962 select HAVE_CLK
963 select MULTI_IRQ_HANDLER
964 select SPARSE_IRQ
965 select USE_OF
966 help
967 Support for VIA/WonderMedia VT8500/WM85xx System-on-Chip.
969 endchoice
971 menu "Multiple platform selection"
972 depends on ARCH_MULTIPLATFORM
974 comment "CPU Core family selection"
976 config ARCH_MULTI_V4
977 bool "ARMv4 based platforms (FA526, StrongARM)"
978 depends on !ARCH_MULTI_V6_V7
979 select ARCH_MULTI_V4_V5
981 config ARCH_MULTI_V4T
982 bool "ARMv4T based platforms (ARM720T, ARM920T, ...)"
983 depends on !ARCH_MULTI_V6_V7
984 select ARCH_MULTI_V4_V5
986 config ARCH_MULTI_V5
987 bool "ARMv5 based platforms (ARM926T, XSCALE, PJ1, ...)"
988 depends on !ARCH_MULTI_V6_V7
989 select ARCH_MULTI_V4_V5
991 config ARCH_MULTI_V4_V5
992 bool
994 config ARCH_MULTI_V6
995 bool "ARMv6 based platforms (ARM11, Scorpion, ...)"
996 select ARCH_MULTI_V6_V7
997 select CPU_V6
999 config ARCH_MULTI_V7
1000 bool "ARMv7 based platforms (Cortex-A, PJ4, Krait)"
1001 default y
1002 select ARCH_MULTI_V6_V7
1003 select ARCH_VEXPRESS
1004 select CPU_V7
1006 config ARCH_MULTI_V6_V7
1007 bool
1009 config ARCH_MULTI_CPU_AUTO
1010 def_bool !(ARCH_MULTI_V4 || ARCH_MULTI_V4T || ARCH_MULTI_V6_V7)
1011 select ARCH_MULTI_V5
1013 endmenu
1015 #
1016 # This is sorted alphabetically by mach-* pathname. However, plat-*
1017 # Kconfigs may be included either alphabetically (according to the
1018 # plat- suffix) or along side the corresponding mach-* source.
1019 #
1020 source "arch/arm/mach-mvebu/Kconfig"
1022 source "arch/arm/mach-at91/Kconfig"
1024 source "arch/arm/mach-bcm/Kconfig"
1026 source "arch/arm/mach-clps711x/Kconfig"
1028 source "arch/arm/mach-cns3xxx/Kconfig"
1030 source "arch/arm/mach-davinci/Kconfig"
1032 source "arch/arm/mach-dove/Kconfig"
1034 source "arch/arm/mach-ep93xx/Kconfig"
1036 source "arch/arm/mach-footbridge/Kconfig"
1038 source "arch/arm/mach-gemini/Kconfig"
1040 source "arch/arm/mach-h720x/Kconfig"
1042 source "arch/arm/mach-highbank/Kconfig"
1044 source "arch/arm/mach-integrator/Kconfig"
1046 source "arch/arm/mach-iop32x/Kconfig"
1048 source "arch/arm/mach-iop33x/Kconfig"
1050 source "arch/arm/mach-iop13xx/Kconfig"
1052 source "arch/arm/mach-ixp4xx/Kconfig"
1054 source "arch/arm/mach-kirkwood/Kconfig"
1056 source "arch/arm/mach-ks8695/Kconfig"
1058 source "arch/arm/mach-msm/Kconfig"
1060 source "arch/arm/mach-mv78xx0/Kconfig"
1062 source "arch/arm/mach-imx/Kconfig"
1064 source "arch/arm/mach-mxs/Kconfig"
1066 source "arch/arm/mach-netx/Kconfig"
1068 source "arch/arm/mach-nomadik/Kconfig"
1070 source "arch/arm/plat-omap/Kconfig"
1072 source "arch/arm/mach-omap1/Kconfig"
1074 source "arch/arm/mach-omap2/Kconfig"
1076 source "arch/arm/mach-orion5x/Kconfig"
1078 source "arch/arm/mach-picoxcell/Kconfig"
1080 source "arch/arm/mach-pxa/Kconfig"
1081 source "arch/arm/plat-pxa/Kconfig"
1083 source "arch/arm/mach-mmp/Kconfig"
1085 source "arch/arm/mach-realview/Kconfig"
1087 source "arch/arm/mach-sa1100/Kconfig"
1089 source "arch/arm/plat-samsung/Kconfig"
1090 source "arch/arm/plat-s3c24xx/Kconfig"
1092 source "arch/arm/mach-socfpga/Kconfig"
1094 source "arch/arm/plat-spear/Kconfig"
1096 source "arch/arm/mach-s3c24xx/Kconfig"
1097 if ARCH_S3C24XX
1098 source "arch/arm/mach-s3c2412/Kconfig"
1099 source "arch/arm/mach-s3c2440/Kconfig"
1100 endif
1102 if ARCH_S3C64XX
1103 source "arch/arm/mach-s3c64xx/Kconfig"
1104 endif
1106 source "arch/arm/mach-s5p64x0/Kconfig"
1108 source "arch/arm/mach-s5pc100/Kconfig"
1110 source "arch/arm/mach-s5pv210/Kconfig"
1112 source "arch/arm/mach-exynos/Kconfig"
1114 source "arch/arm/mach-shmobile/Kconfig"
1116 source "arch/arm/mach-sunxi/Kconfig"
1118 source "arch/arm/mach-prima2/Kconfig"
1120 source "arch/arm/mach-tegra/Kconfig"
1122 source "arch/arm/mach-u300/Kconfig"
1124 source "arch/arm/mach-ux500/Kconfig"
1126 source "arch/arm/mach-versatile/Kconfig"
1128 source "arch/arm/mach-vexpress/Kconfig"
1129 source "arch/arm/plat-versatile/Kconfig"
1131 source "arch/arm/mach-vt8500/Kconfig"
1133 source "arch/arm/mach-w90x900/Kconfig"
1135 source "arch/arm/mach-zynq/Kconfig"
1137 # Definitions to make life easier
1138 config ARCH_ACORN
1139 bool
1141 config PLAT_IOP
1142 bool
1143 select GENERIC_CLOCKEVENTS
1145 config PLAT_ORION
1146 bool
1147 select CLKSRC_MMIO
1148 select COMMON_CLK
1149 select GENERIC_IRQ_CHIP
1150 select IRQ_DOMAIN
1152 config PLAT_ORION_LEGACY
1153 bool
1154 select PLAT_ORION
1156 config PLAT_PXA
1157 bool
1159 config PLAT_VERSATILE
1160 bool
1162 config ARM_TIMER_SP804
1163 bool
1164 select CLKSRC_MMIO
1165 select HAVE_SCHED_CLOCK
1167 source arch/arm/mm/Kconfig
1169 config ARM_NR_BANKS
1170 int
1171 default 16 if ARCH_EP93XX
1172 default 8
1174 config IWMMXT
1175 bool "Enable iWMMXt support"
1176 depends on CPU_XSCALE || CPU_XSC3 || CPU_MOHAWK || CPU_PJ4
1177 default y if PXA27x || PXA3xx || ARCH_MMP
1178 help
1179 Enable support for iWMMXt context switching at run time if
1180 running on a CPU that supports it.
1182 config XSCALE_PMU
1183 bool
1184 depends on CPU_XSCALE
1185 default y
1187 config MULTI_IRQ_HANDLER
1188 bool
1189 help
1190 Allow each machine to specify it's own IRQ handler at run time.
1192 if !MMU
1193 source "arch/arm/Kconfig-nommu"
1194 endif
1196 config ARM_ERRATA_326103
1197 bool "ARM errata: FSR write bit incorrect on a SWP to read-only memory"
1198 depends on CPU_V6
1199 help
1200 Executing a SWP instruction to read-only memory does not set bit 11
1201 of the FSR on the ARM 1136 prior to r1p0. This causes the kernel to
1202 treat the access as a read, preventing a COW from occurring and
1203 causing the faulting task to livelock.
1205 config ARM_ERRATA_411920
1206 bool "ARM errata: Invalidation of the Instruction Cache operation can fail"
1207 depends on CPU_V6 || CPU_V6K
1208 help
1209 Invalidation of the Instruction Cache operation can
1210 fail. This erratum is present in 1136 (before r1p4), 1156 and 1176.
1211 It does not affect the MPCore. This option enables the ARM Ltd.
1212 recommended workaround.
1214 config ARM_ERRATA_430973
1215 bool "ARM errata: Stale prediction on replaced interworking branch"
1216 depends on CPU_V7
1217 help
1218 This option enables the workaround for the 430973 Cortex-A8
1219 (r1p0..r1p2) erratum. If a code sequence containing an ARM/Thumb
1220 interworking branch is replaced with another code sequence at the
1221 same virtual address, whether due to self-modifying code or virtual
1222 to physical address re-mapping, Cortex-A8 does not recover from the
1223 stale interworking branch prediction. This results in Cortex-A8
1224 executing the new code sequence in the incorrect ARM or Thumb state.
1225 The workaround enables the BTB/BTAC operations by setting ACTLR.IBE
1226 and also flushes the branch target cache at every context switch.
1227 Note that setting specific bits in the ACTLR register may not be
1228 available in non-secure mode.
1230 config ARM_ERRATA_458693
1231 bool "ARM errata: Processor deadlock when a false hazard is created"
1232 depends on CPU_V7
1233 depends on !ARCH_MULTIPLATFORM
1234 help
1235 This option enables the workaround for the 458693 Cortex-A8 (r2p0)
1236 erratum. For very specific sequences of memory operations, it is
1237 possible for a hazard condition intended for a cache line to instead
1238 be incorrectly associated with a different cache line. This false
1239 hazard might then cause a processor deadlock. The workaround enables
1240 the L1 caching of the NEON accesses and disables the PLD instruction
1241 in the ACTLR register. Note that setting specific bits in the ACTLR
1242 register may not be available in non-secure mode.
1244 config ARM_ERRATA_460075
1245 bool "ARM errata: Data written to the L2 cache can be overwritten with stale data"
1246 depends on CPU_V7
1247 depends on !ARCH_MULTIPLATFORM
1248 help
1249 This option enables the workaround for the 460075 Cortex-A8 (r2p0)
1250 erratum. Any asynchronous access to the L2 cache may encounter a
1251 situation in which recent store transactions to the L2 cache are lost
1252 and overwritten with stale memory contents from external memory. The
1253 workaround disables the write-allocate mode for the L2 cache via the
1254 ACTLR register. Note that setting specific bits in the ACTLR register
1255 may not be available in non-secure mode.
1257 config ARM_ERRATA_742230
1258 bool "ARM errata: DMB operation may be faulty"
1259 depends on CPU_V7 && SMP
1260 depends on !ARCH_MULTIPLATFORM
1261 help
1262 This option enables the workaround for the 742230 Cortex-A9
1263 (r1p0..r2p2) erratum. Under rare circumstances, a DMB instruction
1264 between two write operations may not ensure the correct visibility
1265 ordering of the two writes. This workaround sets a specific bit in
1266 the diagnostic register of the Cortex-A9 which causes the DMB
1267 instruction to behave as a DSB, ensuring the correct behaviour of
1268 the two writes.
1270 config ARM_ERRATA_742231
1271 bool "ARM errata: Incorrect hazard handling in the SCU may lead to data corruption"
1272 depends on CPU_V7 && SMP
1273 depends on !ARCH_MULTIPLATFORM
1274 help
1275 This option enables the workaround for the 742231 Cortex-A9
1276 (r2p0..r2p2) erratum. Under certain conditions, specific to the
1277 Cortex-A9 MPCore micro-architecture, two CPUs working in SMP mode,
1278 accessing some data located in the same cache line, may get corrupted
1279 data due to bad handling of the address hazard when the line gets
1280 replaced from one of the CPUs at the same time as another CPU is
1281 accessing it. This workaround sets specific bits in the diagnostic
1282 register of the Cortex-A9 which reduces the linefill issuing
1283 capabilities of the processor.
1285 config PL310_ERRATA_588369
1286 bool "PL310 errata: Clean & Invalidate maintenance operations do not invalidate clean lines"
1287 depends on CACHE_L2X0
1288 help
1289 The PL310 L2 cache controller implements three types of Clean &
1290 Invalidate maintenance operations: by Physical Address
1291 (offset 0x7F0), by Index/Way (0x7F8) and by Way (0x7FC).
1292 They are architecturally defined to behave as the execution of a
1293 clean operation followed immediately by an invalidate operation,
1294 both performing to the same memory location. This functionality
1295 is not correctly implemented in PL310 as clean lines are not
1296 invalidated as a result of these operations.
1298 config ARM_ERRATA_720789
1299 bool "ARM errata: TLBIASIDIS and TLBIMVAIS operations can broadcast a faulty ASID"
1300 depends on CPU_V7
1301 help
1302 This option enables the workaround for the 720789 Cortex-A9 (prior to
1303 r2p0) erratum. A faulty ASID can be sent to the other CPUs for the
1304 broadcasted CP15 TLB maintenance operations TLBIASIDIS and TLBIMVAIS.
1305 As a consequence of this erratum, some TLB entries which should be
1306 invalidated are not, resulting in an incoherency in the system page
1307 tables. The workaround changes the TLB flushing routines to invalidate
1308 entries regardless of the ASID.
1310 config PL310_ERRATA_727915
1311 bool "PL310 errata: Background Clean & Invalidate by Way operation can cause data corruption"
1312 depends on CACHE_L2X0
1313 help
1314 PL310 implements the Clean & Invalidate by Way L2 cache maintenance
1315 operation (offset 0x7FC). This operation runs in background so that
1316 PL310 can handle normal accesses while it is in progress. Under very
1317 rare circumstances, due to this erratum, write data can be lost when
1318 PL310 treats a cacheable write transaction during a Clean &
1319 Invalidate by Way operation.
1321 config ARM_ERRATA_743622
1322 bool "ARM errata: Faulty hazard checking in the Store Buffer may lead to data corruption"
1323 depends on CPU_V7
1324 depends on !ARCH_MULTIPLATFORM
1325 help
1326 This option enables the workaround for the 743622 Cortex-A9
1327 (r2p*) erratum. Under very rare conditions, a faulty
1328 optimisation in the Cortex-A9 Store Buffer may lead to data
1329 corruption. This workaround sets a specific bit in the diagnostic
1330 register of the Cortex-A9 which disables the Store Buffer
1331 optimisation, preventing the defect from occurring. This has no
1332 visible impact on the overall performance or power consumption of the
1333 processor.
1335 config ARM_ERRATA_751472
1336 bool "ARM errata: Interrupted ICIALLUIS may prevent completion of broadcasted operation"
1337 depends on CPU_V7
1338 depends on !ARCH_MULTIPLATFORM
1339 help
1340 This option enables the workaround for the 751472 Cortex-A9 (prior
1341 to r3p0) erratum. An interrupted ICIALLUIS operation may prevent the
1342 completion of a following broadcasted operation if the second
1343 operation is received by a CPU before the ICIALLUIS has completed,
1344 potentially leading to corrupted entries in the cache or TLB.
1346 config PL310_ERRATA_753970
1347 bool "PL310 errata: cache sync operation may be faulty"
1348 depends on CACHE_PL310
1349 help
1350 This option enables the workaround for the 753970 PL310 (r3p0) erratum.
1352 Under some condition the effect of cache sync operation on
1353 the store buffer still remains when the operation completes.
1354 This means that the store buffer is always asked to drain and
1355 this prevents it from merging any further writes. The workaround
1356 is to replace the normal offset of cache sync operation (0x730)
1357 by another offset targeting an unmapped PL310 register 0x740.
1358 This has the same effect as the cache sync operation: store buffer
1359 drain and waiting for all buffers empty.
1361 config ARM_ERRATA_754322
1362 bool "ARM errata: possible faulty MMU translations following an ASID switch"
1363 depends on CPU_V7
1364 help
1365 This option enables the workaround for the 754322 Cortex-A9 (r2p*,
1366 r3p*) erratum. A speculative memory access may cause a page table walk
1367 which starts prior to an ASID switch but completes afterwards. This
1368 can populate the micro-TLB with a stale entry which may be hit with
1369 the new ASID. This workaround places two dsb instructions in the mm
1370 switching code so that no page table walks can cross the ASID switch.
1372 config ARM_ERRATA_754327
1373 bool "ARM errata: no automatic Store Buffer drain"
1374 depends on CPU_V7 && SMP
1375 help
1376 This option enables the workaround for the 754327 Cortex-A9 (prior to
1377 r2p0) erratum. The Store Buffer does not have any automatic draining
1378 mechanism and therefore a livelock may occur if an external agent
1379 continuously polls a memory location waiting to observe an update.
1380 This workaround defines cpu_relax() as smp_mb(), preventing correctly
1381 written polling loops from denying visibility of updates to memory.
1383 config ARM_ERRATA_364296
1384 bool "ARM errata: Possible cache data corruption with hit-under-miss enabled"
1385 depends on CPU_V6 && !SMP
1386 help
1387 This options enables the workaround for the 364296 ARM1136
1388 r0p2 erratum (possible cache data corruption with
1389 hit-under-miss enabled). It sets the undocumented bit 31 in
1390 the auxiliary control register and the FI bit in the control
1391 register, thus disabling hit-under-miss without putting the
1392 processor into full low interrupt latency mode. ARM11MPCore
1393 is not affected.
1395 config ARM_ERRATA_764369
1396 bool "ARM errata: Data cache line maintenance operation by MVA may not succeed"
1397 depends on CPU_V7 && SMP
1398 help
1399 This option enables the workaround for erratum 764369
1400 affecting Cortex-A9 MPCore with two or more processors (all
1401 current revisions). Under certain timing circumstances, a data
1402 cache line maintenance operation by MVA targeting an Inner
1403 Shareable memory region may fail to proceed up to either the
1404 Point of Coherency or to the Point of Unification of the
1405 system. This workaround adds a DSB instruction before the
1406 relevant cache maintenance functions and sets a specific bit
1407 in the diagnostic control register of the SCU.
1409 config PL310_ERRATA_769419
1410 bool "PL310 errata: no automatic Store Buffer drain"
1411 depends on CACHE_L2X0
1412 help
1413 On revisions of the PL310 prior to r3p2, the Store Buffer does
1414 not automatically drain. This can cause normal, non-cacheable
1415 writes to be retained when the memory system is idle, leading
1416 to suboptimal I/O performance for drivers using coherent DMA.
1417 This option adds a write barrier to the cpu_idle loop so that,
1418 on systems with an outer cache, the store buffer is drained
1419 explicitly.
1421 config ARM_ERRATA_775420
1422 bool "ARM errata: A data cache maintenance operation which aborts, might lead to deadlock"
1423 depends on CPU_V7
1424 help
1425 This option enables the workaround for the 775420 Cortex-A9 (r2p2,
1426 r2p6,r2p8,r2p10,r3p0) erratum. In case a date cache maintenance
1427 operation aborts with MMU exception, it might cause the processor
1428 to deadlock. This workaround puts DSB before executing ISB if
1429 an abort may occur on cache maintenance.
1431 config ARM_ERRATA_798181
1432 bool "ARM errata: TLBI/DSB failure on Cortex-A15"
1433 depends on CPU_V7 && SMP
1434 help
1435 On Cortex-A15 (r0p0..r3p2) the TLBI*IS/DSB operations are not
1436 adequately shooting down all use of the old entries. This
1437 option enables the Linux kernel workaround for this erratum
1438 which sends an IPI to the CPUs that are running the same ASID
1439 as the one being invalidated.
1441 endmenu
1443 source "arch/arm/common/Kconfig"
1445 menu "Bus support"
1447 config ARM_AMBA
1448 bool
1450 config ISA
1451 bool
1452 help
1453 Find out whether you have ISA slots on your motherboard. ISA is the
1454 name of a bus system, i.e. the way the CPU talks to the other stuff
1455 inside your box. Other bus systems are PCI, EISA, MicroChannel
1456 (MCA) or VESA. ISA is an older system, now being displaced by PCI;
1457 newer boards don't support it. If you have ISA, say Y, otherwise N.
1459 # Select ISA DMA controller support
1460 config ISA_DMA
1461 bool
1462 select ISA_DMA_API
1464 # Select ISA DMA interface
1465 config ISA_DMA_API
1466 bool
1468 config PCI
1469 bool "PCI support" if MIGHT_HAVE_PCI
1470 help
1471 Find out whether you have a PCI motherboard. PCI is the name of a
1472 bus system, i.e. the way the CPU talks to the other stuff inside
1473 your box. Other bus systems are ISA, EISA, MicroChannel (MCA) or
1474 VESA. If you have PCI, say Y, otherwise N.
1476 config PCI_DOMAINS
1477 bool
1478 depends on PCI
1480 config PCI_NANOENGINE
1481 bool "BSE nanoEngine PCI support"
1482 depends on SA1100_NANOENGINE
1483 help
1484 Enable PCI on the BSE nanoEngine board.
1486 config PCI_SYSCALL
1487 def_bool PCI
1489 # Select the host bridge type
1490 config PCI_HOST_VIA82C505
1491 bool
1492 depends on PCI && ARCH_SHARK
1493 default y
1495 config PCI_HOST_ITE8152
1496 bool
1497 depends on PCI && MACH_ARMCORE
1498 default y
1499 select DMABOUNCE
1501 source "drivers/pci/Kconfig"
1503 source "drivers/pcmcia/Kconfig"
1505 endmenu
1507 menu "Kernel Features"
1509 config HAVE_SMP
1510 bool
1511 help
1512 This option should be selected by machines which have an SMP-
1513 capable CPU.
1515 The only effect of this option is to make the SMP-related
1516 options available to the user for configuration.
1518 config SMP
1519 bool "Symmetric Multi-Processing"
1520 depends on CPU_V6K || CPU_V7
1521 depends on GENERIC_CLOCKEVENTS
1522 depends on HAVE_SMP
1523 depends on MMU
1524 select HAVE_ARM_SCU if !ARCH_MSM_SCORPIONMP
1525 select USE_GENERIC_SMP_HELPERS
1526 help
1527 This enables support for systems with more than one CPU. If you have
1528 a system with only one CPU, like most personal computers, say N. If
1529 you have a system with more than one CPU, say Y.
1531 If you say N here, the kernel will run on single and multiprocessor
1532 machines, but will use only one CPU of a multiprocessor machine. If
1533 you say Y here, the kernel will run on many, but not all, single
1534 processor machines. On a single processor machine, the kernel will
1535 run faster if you say N here.
1537 See also <file:Documentation/x86/i386/IO-APIC.txt>,
1538 <file:Documentation/nmi_watchdog.txt> and the SMP-HOWTO available at
1539 <http://tldp.org/HOWTO/SMP-HOWTO.html>.
1541 If you don't know what to do here, say N.
1543 config SMP_ON_UP
1544 bool "Allow booting SMP kernel on uniprocessor systems (EXPERIMENTAL)"
1545 depends on EXPERIMENTAL
1546 depends on SMP && !XIP_KERNEL
1547 default y
1548 help
1549 SMP kernels contain instructions which fail on non-SMP processors.
1550 Enabling this option allows the kernel to modify itself to make
1551 these instructions safe. Disabling it allows about 1K of space
1552 savings.
1554 If you don't know what to do here, say Y.
1556 config ARM_CPU_TOPOLOGY
1557 bool "Support cpu topology definition"
1558 depends on SMP && CPU_V7
1559 default y
1560 help
1561 Support ARM cpu topology definition. The MPIDR register defines
1562 affinity between processors which is then used to describe the cpu
1563 topology of an ARM System.
1565 config SCHED_MC
1566 bool "Multi-core scheduler support"
1567 depends on ARM_CPU_TOPOLOGY
1568 help
1569 Multi-core scheduler support improves the CPU scheduler's decision
1570 making when dealing with multi-core CPU chips at a cost of slightly
1571 increased overhead in some places. If unsure say N here.
1573 config SCHED_SMT
1574 bool "SMT scheduler support"
1575 depends on ARM_CPU_TOPOLOGY
1576 help
1577 Improves the CPU scheduler's decision making when dealing with
1578 MultiThreading at a cost of slightly increased overhead in some
1579 places. If unsure say N here.
1581 config HAVE_ARM_SCU
1582 bool
1583 help
1584 This option enables support for the ARM system coherency unit
1586 config ARM_ARCH_TIMER
1587 bool "Architected timer support"
1588 depends on CPU_V7
1589 help
1590 This option enables support for the ARM architected timer
1592 config HAVE_ARM_TWD
1593 bool
1594 depends on SMP
1595 help
1596 This options enables support for the ARM timer and watchdog unit
1598 choice
1599 prompt "Memory split"
1600 default VMSPLIT_3G
1601 help
1602 Select the desired split between kernel and user memory.
1604 If you are not absolutely sure what you are doing, leave this
1605 option alone!
1607 config VMSPLIT_3G
1608 bool "3G/1G user/kernel split"
1609 config VMSPLIT_2G
1610 bool "2G/2G user/kernel split"
1611 config VMSPLIT_1G
1612 bool "1G/3G user/kernel split"
1613 endchoice
1615 config PAGE_OFFSET
1616 hex
1617 default 0x40000000 if VMSPLIT_1G
1618 default 0x80000000 if VMSPLIT_2G
1619 default 0xC0000000
1621 config NR_CPUS
1622 int "Maximum number of CPUs (2-32)"
1623 range 2 32
1624 depends on SMP
1625 default "4"
1627 config HOTPLUG_CPU
1628 bool "Support for hot-pluggable CPUs"
1629 depends on SMP && HOTPLUG
1630 help
1631 Say Y here to experiment with turning CPUs off and on. CPUs
1632 can be controlled through /sys/devices/system/cpu.
1634 config LOCAL_TIMERS
1635 bool "Use local timer interrupts"
1636 depends on SMP
1637 default y
1638 select HAVE_ARM_TWD if (!ARCH_MSM_SCORPIONMP && !EXYNOS4_MCT)
1639 help
1640 Enable support for local timers on SMP platforms, rather then the
1641 legacy IPI broadcast method. Local timers allows the system
1642 accounting to be spread across the timer interval, preventing a
1643 "thundering herd" at every timer tick.
1645 config ARCH_NR_GPIO
1646 int
1647 default 1024 if ARCH_SHMOBILE || ARCH_TEGRA
1648 default 355 if ARCH_U8500
1649 default 264 if MACH_H4700
1650 default 512 if SOC_OMAP5 || SOC_DRA7XX
1651 default 288 if ARCH_VT8500
1652 default 0
1653 help
1654 Maximum number of GPIOs in the system.
1656 If unsure, leave the default value.
1658 source kernel/Kconfig.preempt
1660 config HZ
1661 int
1662 default 200 if ARCH_EBSA110 || ARCH_S3C24XX || ARCH_S5P64X0 || \
1663 ARCH_S5PV210 || ARCH_EXYNOS4
1664 default OMAP_32K_TIMER_HZ if ARCH_OMAP && OMAP_32K_TIMER
1665 default AT91_TIMER_HZ if ARCH_AT91
1666 default SHMOBILE_TIMER_HZ if ARCH_SHMOBILE
1667 default 100
1669 config THUMB2_KERNEL
1670 bool "Compile the kernel in Thumb-2 mode"
1671 depends on CPU_V7 && !CPU_V6 && !CPU_V6K
1672 select AEABI
1673 select ARM_ASM_UNIFIED
1674 select ARM_UNWIND
1675 help
1676 By enabling this option, the kernel will be compiled in
1677 Thumb-2 mode. A compiler/assembler that understand the unified
1678 ARM-Thumb syntax is needed.
1680 If unsure, say N.
1682 config THUMB2_AVOID_R_ARM_THM_JUMP11
1683 bool "Work around buggy Thumb-2 short branch relocations in gas"
1684 depends on THUMB2_KERNEL && MODULES
1685 default y
1686 help
1687 Various binutils versions can resolve Thumb-2 branches to
1688 locally-defined, preemptible global symbols as short-range "b.n"
1689 branch instructions.
1691 This is a problem, because there's no guarantee the final
1692 destination of the symbol, or any candidate locations for a
1693 trampoline, are within range of the branch. For this reason, the
1694 kernel does not support fixing up the R_ARM_THM_JUMP11 (102)
1695 relocation in modules at all, and it makes little sense to add
1696 support.
1698 The symptom is that the kernel fails with an "unsupported
1699 relocation" error when loading some modules.
1701 Until fixed tools are available, passing
1702 -fno-optimize-sibling-calls to gcc should prevent gcc generating
1703 code which hits this problem, at the cost of a bit of extra runtime
1704 stack usage in some cases.
1706 The problem is described in more detail at:
1707 https://bugs.launchpad.net/binutils-linaro/+bug/725126
1709 Only Thumb-2 kernels are affected.
1711 Unless you are sure your tools don't have this problem, say Y.
1713 config ARM_ASM_UNIFIED
1714 bool
1716 config AEABI
1717 bool "Use the ARM EABI to compile the kernel"
1718 help
1719 This option allows for the kernel to be compiled using the latest
1720 ARM ABI (aka EABI). This is only useful if you are using a user
1721 space environment that is also compiled with EABI.
1723 Since there are major incompatibilities between the legacy ABI and
1724 EABI, especially with regard to structure member alignment, this
1725 option also changes the kernel syscall calling convention to
1726 disambiguate both ABIs and allow for backward compatibility support
1727 (selected with CONFIG_OABI_COMPAT).
1729 To use this you need GCC version 4.0.0 or later.
1731 config OABI_COMPAT
1732 bool "Allow old ABI binaries to run with this kernel (EXPERIMENTAL)"
1733 depends on AEABI && EXPERIMENTAL && !THUMB2_KERNEL
1734 default y
1735 help
1736 This option preserves the old syscall interface along with the
1737 new (ARM EABI) one. It also provides a compatibility layer to
1738 intercept syscalls that have structure arguments which layout
1739 in memory differs between the legacy ABI and the new ARM EABI
1740 (only for non "thumb" binaries). This option adds a tiny
1741 overhead to all syscalls and produces a slightly larger kernel.
1742 If you know you'll be using only pure EABI user space then you
1743 can say N here. If this option is not selected and you attempt
1744 to execute a legacy ABI binary then the result will be
1745 UNPREDICTABLE (in fact it can be predicted that it won't work
1746 at all). If in doubt say Y.
1748 config ARCH_HAS_HOLES_MEMORYMODEL
1749 bool
1751 config ARCH_SPARSEMEM_ENABLE
1752 bool
1754 config ARCH_SPARSEMEM_DEFAULT
1755 def_bool ARCH_SPARSEMEM_ENABLE
1757 config ARCH_SELECT_MEMORY_MODEL
1758 def_bool ARCH_SPARSEMEM_ENABLE
1760 config HAVE_ARCH_PFN_VALID
1761 def_bool ARCH_HAS_HOLES_MEMORYMODEL || !SPARSEMEM
1763 config HIGHMEM
1764 bool "High Memory Support"
1765 depends on MMU
1766 help
1767 The address space of ARM processors is only 4 Gigabytes large
1768 and it has to accommodate user address space, kernel address
1769 space as well as some memory mapped IO. That means that, if you
1770 have a large amount of physical memory and/or IO, not all of the
1771 memory can be "permanently mapped" by the kernel. The physical
1772 memory that is not permanently mapped is called "high memory".
1774 Depending on the selected kernel/user memory split, minimum
1775 vmalloc space and actual amount of RAM, you may not need this
1776 option which should result in a slightly faster kernel.
1778 If unsure, say n.
1780 config HIGHPTE
1781 bool "Allocate 2nd-level pagetables from highmem"
1782 depends on HIGHMEM
1784 config HW_PERF_EVENTS
1785 bool "Enable hardware performance counter support for perf events"
1786 depends on PERF_EVENTS
1787 default y
1788 help
1789 Enable hardware performance counter support for perf events. If
1790 disabled, perf events will use software events only.
1792 source "mm/Kconfig"
1794 config FORCE_MAX_ZONEORDER
1795 int "Maximum zone order" if ARCH_SHMOBILE
1796 range 11 64 if ARCH_SHMOBILE
1797 default "12" if SOC_AM33XX
1798 default "9" if SA1111
1799 default "11"
1800 help
1801 The kernel memory allocator divides physically contiguous memory
1802 blocks into "zones", where each zone is a power of two number of
1803 pages. This option selects the largest power of two that the kernel
1804 keeps in the memory allocator. If you need to allocate very large
1805 blocks of physically contiguous memory, then you may need to
1806 increase this value.
1808 This config option is actually maximum order plus one. For example,
1809 a value of 11 means that the largest free memory block is 2^10 pages.
1811 config ALIGNMENT_TRAP
1812 bool
1813 depends on CPU_CP15_MMU
1814 default y if !ARCH_EBSA110
1815 select HAVE_PROC_CPU if PROC_FS
1816 help
1817 ARM processors cannot fetch/store information which is not
1818 naturally aligned on the bus, i.e., a 4 byte fetch must start at an
1819 address divisible by 4. On 32-bit ARM processors, these non-aligned
1820 fetch/store instructions will be emulated in software if you say
1821 here, which has a severe performance impact. This is necessary for
1822 correct operation of some network protocols. With an IP-only
1823 configuration it is safe to say N, otherwise say Y.
1825 config UACCESS_WITH_MEMCPY
1826 bool "Use kernel mem{cpy,set}() for {copy_to,clear}_user()"
1827 depends on MMU
1828 default y if CPU_FEROCEON
1829 help
1830 Implement faster copy_to_user and clear_user methods for CPU
1831 cores where a 8-word STM instruction give significantly higher
1832 memory write throughput than a sequence of individual 32bit stores.
1834 A possible side effect is a slight increase in scheduling latency
1835 between threads sharing the same address space if they invoke
1836 such copy operations with large buffers.
1838 However, if the CPU data cache is using a write-allocate mode,
1839 this option is unlikely to provide any performance gain.
1841 config SECCOMP
1842 bool
1843 prompt "Enable seccomp to safely compute untrusted bytecode"
1844 ---help---
1845 This kernel feature is useful for number crunching applications
1846 that may need to compute untrusted bytecode during their
1847 execution. By using pipes or other transports made available to
1848 the process as file descriptors supporting the read/write
1849 syscalls, it's possible to isolate those applications in
1850 their own address space using seccomp. Once seccomp is
1851 enabled via prctl(PR_SET_SECCOMP), it cannot be disabled
1852 and the task is only allowed to execute a few safe syscalls
1853 defined by each seccomp mode.
1855 config CC_STACKPROTECTOR
1856 bool "Enable -fstack-protector buffer overflow detection (EXPERIMENTAL)"
1857 depends on EXPERIMENTAL
1858 help
1859 This option turns on the -fstack-protector GCC feature. This
1860 feature puts, at the beginning of functions, a canary value on
1861 the stack just before the return address, and validates
1862 the value just before actually returning. Stack based buffer
1863 overflows (that need to overwrite this return address) now also
1864 overwrite the canary, which gets detected and the attack is then
1865 neutralized via a kernel panic.
1866 This feature requires gcc version 4.2 or above.
1868 config XEN_DOM0
1869 def_bool y
1870 depends on XEN
1872 config XEN
1873 bool "Xen guest support on ARM (EXPERIMENTAL)"
1874 depends on EXPERIMENTAL && ARM && OF
1875 depends on CPU_V7 && !CPU_V6
1876 help
1877 Say Y if you want to run Linux in a Virtual Machine on Xen on ARM.
1879 endmenu
1881 menu "Boot options"
1883 config USE_OF
1884 bool "Flattened Device Tree support"
1885 select IRQ_DOMAIN
1886 select OF
1887 select OF_EARLY_FLATTREE
1888 help
1889 Include support for flattened device tree machine descriptions.
1891 config ATAGS
1892 bool "Support for the traditional ATAGS boot data passing" if USE_OF
1893 default y
1894 help
1895 This is the traditional way of passing data to the kernel at boot
1896 time. If you are solely relying on the flattened device tree (or
1897 the ARM_ATAG_DTB_COMPAT option) then you may unselect this option
1898 to remove ATAGS support from your kernel binary. If unsure,
1899 leave this to y.
1901 config DEPRECATED_PARAM_STRUCT
1902 bool "Provide old way to pass kernel parameters"
1903 depends on ATAGS
1904 help
1905 This was deprecated in 2001 and announced to live on for 5 years.
1906 Some old boot loaders still use this way.
1908 # Compressed boot loader in ROM. Yes, we really want to ask about
1909 # TEXT and BSS so we preserve their values in the config files.
1910 config ZBOOT_ROM_TEXT
1911 hex "Compressed ROM boot loader base address"
1912 default "0"
1913 help
1914 The physical address at which the ROM-able zImage is to be
1915 placed in the target. Platforms which normally make use of
1916 ROM-able zImage formats normally set this to a suitable
1917 value in their defconfig file.
1919 If ZBOOT_ROM is not enabled, this has no effect.
1921 config ZBOOT_ROM_BSS
1922 hex "Compressed ROM boot loader BSS address"
1923 default "0"
1924 help
1925 The base address of an area of read/write memory in the target
1926 for the ROM-able zImage which must be available while the
1927 decompressor is running. It must be large enough to hold the
1928 entire decompressed kernel plus an additional 128 KiB.
1929 Platforms which normally make use of ROM-able zImage formats
1930 normally set this to a suitable value in their defconfig file.
1932 If ZBOOT_ROM is not enabled, this has no effect.
1934 config ZBOOT_ROM
1935 bool "Compressed boot loader in ROM/flash"
1936 depends on ZBOOT_ROM_TEXT != ZBOOT_ROM_BSS
1937 help
1938 Say Y here if you intend to execute your compressed kernel image
1939 (zImage) directly from ROM or flash. If unsure, say N.
1941 choice
1942 prompt "Include SD/MMC loader in zImage (EXPERIMENTAL)"
1943 depends on ZBOOT_ROM && ARCH_SH7372 && EXPERIMENTAL
1944 default ZBOOT_ROM_NONE
1945 help
1946 Include experimental SD/MMC loading code in the ROM-able zImage.
1947 With this enabled it is possible to write the ROM-able zImage
1948 kernel image to an MMC or SD card and boot the kernel straight
1949 from the reset vector. At reset the processor Mask ROM will load
1950 the first part of the ROM-able zImage which in turn loads the
1951 rest the kernel image to RAM.
1953 config ZBOOT_ROM_NONE
1954 bool "No SD/MMC loader in zImage (EXPERIMENTAL)"
1955 help
1956 Do not load image from SD or MMC
1958 config ZBOOT_ROM_MMCIF
1959 bool "Include MMCIF loader in zImage (EXPERIMENTAL)"
1960 help
1961 Load image from MMCIF hardware block.
1963 config ZBOOT_ROM_SH_MOBILE_SDHI
1964 bool "Include SuperH Mobile SDHI loader in zImage (EXPERIMENTAL)"
1965 help
1966 Load image from SDHI hardware block
1968 endchoice
1970 config ARM_APPENDED_DTB
1971 bool "Use appended device tree blob to zImage (EXPERIMENTAL)"
1972 depends on OF && !ZBOOT_ROM && EXPERIMENTAL
1973 help
1974 With this option, the boot code will look for a device tree binary
1975 (DTB) appended to zImage
1976 (e.g. cat zImage <filename>.dtb > zImage_w_dtb).
1978 This is meant as a backward compatibility convenience for those
1979 systems with a bootloader that can't be upgraded to accommodate
1980 the documented boot protocol using a device tree.
1982 Beware that there is very little in terms of protection against
1983 this option being confused by leftover garbage in memory that might
1984 look like a DTB header after a reboot if no actual DTB is appended
1985 to zImage. Do not leave this option active in a production kernel
1986 if you don't intend to always append a DTB. Proper passing of the
1987 location into r2 of a bootloader provided DTB is always preferable
1988 to this option.
1990 config ARM_ATAG_DTB_COMPAT
1991 bool "Supplement the appended DTB with traditional ATAG information"
1992 depends on ARM_APPENDED_DTB
1993 help
1994 Some old bootloaders can't be updated to a DTB capable one, yet
1995 they provide ATAGs with memory configuration, the ramdisk address,
1996 the kernel cmdline string, etc. Such information is dynamically
1997 provided by the bootloader and can't always be stored in a static
1998 DTB. To allow a device tree enabled kernel to be used with such
1999 bootloaders, this option allows zImage to extract the information
2000 from the ATAG list and store it at run time into the appended DTB.
2002 choice
2003 prompt "Kernel command line type" if ARM_ATAG_DTB_COMPAT
2004 default ARM_ATAG_DTB_COMPAT_CMDLINE_FROM_BOOTLOADER
2006 config ARM_ATAG_DTB_COMPAT_CMDLINE_FROM_BOOTLOADER
2007 bool "Use bootloader kernel arguments if available"
2008 help
2009 Uses the command-line options passed by the boot loader instead of
2010 the device tree bootargs property. If the boot loader doesn't provide
2011 any, the device tree bootargs property will be used.
2013 config ARM_ATAG_DTB_COMPAT_CMDLINE_EXTEND
2014 bool "Extend with bootloader kernel arguments"
2015 help
2016 The command-line arguments provided by the boot loader will be
2017 appended to the the device tree bootargs property.
2019 endchoice
2021 config CMDLINE
2022 string "Default kernel command string"
2023 default ""
2024 help
2025 On some architectures (EBSA110 and CATS), there is currently no way
2026 for the boot loader to pass arguments to the kernel. For these
2027 architectures, you should supply some command-line options at build
2028 time by entering them here. As a minimum, you should specify the
2029 memory size and the root device (e.g., mem=64M root=/dev/nfs).
2031 choice
2032 prompt "Kernel command line type" if CMDLINE != ""
2033 default CMDLINE_FROM_BOOTLOADER
2034 depends on ATAGS
2036 config CMDLINE_FROM_BOOTLOADER
2037 bool "Use bootloader kernel arguments if available"
2038 help
2039 Uses the command-line options passed by the boot loader. If
2040 the boot loader doesn't provide any, the default kernel command
2041 string provided in CMDLINE will be used.
2043 config CMDLINE_EXTEND
2044 bool "Extend bootloader kernel arguments"
2045 help
2046 The command-line arguments provided by the boot loader will be
2047 appended to the default kernel command string.
2049 config CMDLINE_FORCE
2050 bool "Always use the default kernel command string"
2051 help
2052 Always use the default kernel command string, even if the boot
2053 loader passes other arguments to the kernel.
2054 This is useful if you cannot or don't want to change the
2055 command-line options your boot loader passes to the kernel.
2056 endchoice
2058 config XIP_KERNEL
2059 bool "Kernel Execute-In-Place from ROM"
2060 depends on !ZBOOT_ROM && !ARM_LPAE && !ARCH_MULTIPLATFORM
2061 help
2062 Execute-In-Place allows the kernel to run from non-volatile storage
2063 directly addressable by the CPU, such as NOR flash. This saves RAM
2064 space since the text section of the kernel is not loaded from flash
2065 to RAM. Read-write sections, such as the data section and stack,
2066 are still copied to RAM. The XIP kernel is not compressed since
2067 it has to run directly from flash, so it will take more space to
2068 store it. The flash address used to link the kernel object files,
2069 and for storing it, is configuration dependent. Therefore, if you
2070 say Y here, you must know the proper physical address where to
2071 store the kernel image depending on your own flash memory usage.
2073 Also note that the make target becomes "make xipImage" rather than
2074 "make zImage" or "make Image". The final kernel binary to put in
2075 ROM memory will be arch/arm/boot/xipImage.
2077 If unsure, say N.
2079 config XIP_PHYS_ADDR
2080 hex "XIP Kernel Physical Location"
2081 depends on XIP_KERNEL
2082 default "0x00080000"
2083 help
2084 This is the physical address in your flash memory the kernel will
2085 be linked for and stored to. This address is dependent on your
2086 own flash usage.
2088 config KEXEC
2089 bool "Kexec system call (EXPERIMENTAL)"
2090 depends on EXPERIMENTAL && (!SMP || HOTPLUG_CPU)
2091 help
2092 kexec is a system call that implements the ability to shutdown your
2093 current kernel, and to start another kernel. It is like a reboot
2094 but it is independent of the system firmware. And like a reboot
2095 you can start any kernel with it, not just Linux.
2097 It is an ongoing process to be certain the hardware in a machine
2098 is properly shutdown, so do not be surprised if this code does not
2099 initially work for you. It may help to enable device hotplugging
2100 support.
2102 config ATAGS_PROC
2103 bool "Export atags in procfs"
2104 depends on ATAGS && KEXEC
2105 default y
2106 help
2107 Should the atags used to boot the kernel be exported in an "atags"
2108 file in procfs. Useful with kexec.
2110 config CRASH_DUMP
2111 bool "Build kdump crash kernel (EXPERIMENTAL)"
2112 depends on EXPERIMENTAL
2113 help
2114 Generate crash dump after being started by kexec. This should
2115 be normally only set in special crash dump kernels which are
2116 loaded in the main kernel with kexec-tools into a specially
2117 reserved region and then later executed after a crash by
2118 kdump/kexec. The crash dump kernel must be compiled to a
2119 memory address not used by the main kernel
2121 For more details see Documentation/kdump/kdump.txt
2123 config AUTO_ZRELADDR
2124 bool "Auto calculation of the decompressed kernel image address"
2125 depends on !ZBOOT_ROM && !ARCH_U300
2126 help
2127 ZRELADDR is the physical address where the decompressed kernel
2128 image will be placed. If AUTO_ZRELADDR is selected, the address
2129 will be determined at run-time by masking the current IP with
2130 0xf8000000. This assumes the zImage being placed in the first 128MB
2131 from start of memory.
2133 endmenu
2135 menu "CPU Power Management"
2137 if ARCH_HAS_CPUFREQ
2139 source "drivers/cpufreq/Kconfig"
2141 config CPU_FREQ_IMX
2142 tristate "CPUfreq driver for i.MX CPUs"
2143 depends on ARCH_MXC && CPU_FREQ
2144 select CPU_FREQ_TABLE
2145 help
2146 This enables the CPUfreq driver for i.MX CPUs.
2148 config CPU_FREQ_SA1100
2149 bool
2151 config CPU_FREQ_SA1110
2152 bool
2154 config CPU_FREQ_INTEGRATOR
2155 tristate "CPUfreq driver for ARM Integrator CPUs"
2156 depends on ARCH_INTEGRATOR && CPU_FREQ
2157 default y
2158 help
2159 This enables the CPUfreq driver for ARM Integrator CPUs.
2161 For details, take a look at <file:Documentation/cpu-freq>.
2163 If in doubt, say Y.
2165 config CPU_FREQ_PXA
2166 bool
2167 depends on CPU_FREQ && ARCH_PXA && PXA25x
2168 default y
2169 select CPU_FREQ_DEFAULT_GOV_USERSPACE
2170 select CPU_FREQ_TABLE
2172 config CPU_FREQ_S3C
2173 bool
2174 help
2175 Internal configuration node for common cpufreq on Samsung SoC
2177 config CPU_FREQ_S3C24XX
2178 bool "CPUfreq driver for Samsung S3C24XX series CPUs (EXPERIMENTAL)"
2179 depends on ARCH_S3C24XX && CPU_FREQ && EXPERIMENTAL
2180 select CPU_FREQ_S3C
2181 help
2182 This enables the CPUfreq driver for the Samsung S3C24XX family
2183 of CPUs.
2185 For details, take a look at <file:Documentation/cpu-freq>.
2187 If in doubt, say N.
2189 config CPU_FREQ_S3C24XX_PLL
2190 bool "Support CPUfreq changing of PLL frequency (EXPERIMENTAL)"
2191 depends on CPU_FREQ_S3C24XX && EXPERIMENTAL
2192 help
2193 Compile in support for changing the PLL frequency from the
2194 S3C24XX series CPUfreq driver. The PLL takes time to settle
2195 after a frequency change, so by default it is not enabled.
2197 This also means that the PLL tables for the selected CPU(s) will
2198 be built which may increase the size of the kernel image.
2200 config CPU_FREQ_S3C24XX_DEBUG
2201 bool "Debug CPUfreq Samsung driver core"
2202 depends on CPU_FREQ_S3C24XX
2203 help
2204 Enable s3c_freq_dbg for the Samsung S3C CPUfreq core
2206 config CPU_FREQ_S3C24XX_IODEBUG
2207 bool "Debug CPUfreq Samsung driver IO timing"
2208 depends on CPU_FREQ_S3C24XX
2209 help
2210 Enable s3c_freq_iodbg for the Samsung S3C CPUfreq core
2212 config CPU_FREQ_S3C24XX_DEBUGFS
2213 bool "Export debugfs for CPUFreq"
2214 depends on CPU_FREQ_S3C24XX && DEBUG_FS
2215 help
2216 Export status information via debugfs.
2218 endif
2220 source "drivers/cpuidle/Kconfig"
2222 endmenu
2224 menu "Floating point emulation"
2226 comment "At least one emulation must be selected"
2228 config FPE_NWFPE
2229 bool "NWFPE math emulation"
2230 depends on (!AEABI || OABI_COMPAT) && !THUMB2_KERNEL
2231 ---help---
2232 Say Y to include the NWFPE floating point emulator in the kernel.
2233 This is necessary to run most binaries. Linux does not currently
2234 support floating point hardware so you need to say Y here even if
2235 your machine has an FPA or floating point co-processor podule.
2237 You may say N here if you are going to load the Acorn FPEmulator
2238 early in the bootup.
2240 config FPE_NWFPE_XP
2241 bool "Support extended precision"
2242 depends on FPE_NWFPE
2243 help
2244 Say Y to include 80-bit support in the kernel floating-point
2245 emulator. Otherwise, only 32 and 64-bit support is compiled in.
2246 Note that gcc does not generate 80-bit operations by default,
2247 so in most cases this option only enlarges the size of the
2248 floating point emulator without any good reason.
2250 You almost surely want to say N here.
2252 config FPE_FASTFPE
2253 bool "FastFPE math emulation (EXPERIMENTAL)"
2254 depends on (!AEABI || OABI_COMPAT) && !CPU_32v3 && EXPERIMENTAL
2255 ---help---
2256 Say Y here to include the FAST floating point emulator in the kernel.
2257 This is an experimental much faster emulator which now also has full
2258 precision for the mantissa. It does not support any exceptions.
2259 It is very simple, and approximately 3-6 times faster than NWFPE.
2261 It should be sufficient for most programs. It may be not suitable
2262 for scientific calculations, but you have to check this for yourself.
2263 If you do not feel you need a faster FP emulation you should better
2264 choose NWFPE.
2266 config VFP
2267 bool "VFP-format floating point maths"
2268 depends on CPU_V6 || CPU_V6K || CPU_ARM926T || CPU_V7 || CPU_FEROCEON
2269 help
2270 Say Y to include VFP support code in the kernel. This is needed
2271 if your hardware includes a VFP unit.
2273 Please see <file:Documentation/arm/VFP/release-notes.txt> for
2274 release notes and additional status information.
2276 Say N if your target does not have VFP hardware.
2278 config VFPv3
2279 bool
2280 depends on VFP
2281 default y if CPU_V7
2283 config NEON
2284 bool "Advanced SIMD (NEON) Extension support"
2285 depends on VFPv3 && CPU_V7
2286 help
2287 Say Y to include support code for NEON, the ARMv7 Advanced SIMD
2288 Extension.
2290 endmenu
2292 menu "Userspace binary formats"
2294 source "fs/Kconfig.binfmt"
2296 config ARTHUR
2297 tristate "RISC OS personality"
2298 depends on !AEABI
2299 help
2300 Say Y here to include the kernel code necessary if you want to run
2301 Acorn RISC OS/Arthur binaries under Linux. This code is still very
2302 experimental; if this sounds frightening, say N and sleep in peace.
2303 You can also say M here to compile this support as a module (which
2304 will be called arthur).
2306 endmenu
2308 menu "Power management options"
2310 source "kernel/power/Kconfig"
2312 config ARCH_SUSPEND_POSSIBLE
2313 depends on !ARCH_S5PC100
2314 depends on CPU_ARM920T || CPU_ARM926T || CPU_SA1100 || \
2315 CPU_V6 || CPU_V6K || CPU_V7 || CPU_XSC3 || CPU_XSCALE || CPU_MOHAWK
2316 def_bool y
2318 config ARM_CPU_SUSPEND
2319 def_bool PM_SLEEP
2321 endmenu
2323 source "net/Kconfig"
2325 source "drivers/Kconfig"
2327 source "fs/Kconfig"
2329 source "arch/arm/Kconfig.debug"
2331 source "security/Kconfig"
2333 source "crypto/Kconfig"
2335 source "lib/Kconfig"