]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - arch/arm/include/asm/memory.h
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/dtor/input
[android-sdk/kernel-video.git] / arch / arm / include / asm / memory.h
1 /*
2  *  arch/arm/include/asm/memory.h
3  *
4  *  Copyright (C) 2000-2002 Russell King
5  *  modification for nommu, Hyok S. Choi, 2004
6  *
7  * This program is free software; you can redistribute it and/or modify
8  * it under the terms of the GNU General Public License version 2 as
9  * published by the Free Software Foundation.
10  *
11  *  Note: this file should not be included by non-asm/.h files
12  */
13 #ifndef __ASM_ARM_MEMORY_H
14 #define __ASM_ARM_MEMORY_H
16 #include <linux/compiler.h>
17 #include <linux/const.h>
18 #include <linux/types.h>
19 #include <linux/sizes.h>
21 #ifdef CONFIG_NEED_MACH_MEMORY_H
22 #include <mach/memory.h>
23 #endif
25 /*
26  * Allow for constants defined here to be used from assembly code
27  * by prepending the UL suffix only with actual C code compilation.
28  */
29 #define UL(x) _AC(x, UL)
31 #ifdef CONFIG_MMU
33 /*
34  * PAGE_OFFSET - the virtual address of the start of the kernel image
35  * TASK_SIZE - the maximum size of a user space task.
36  * TASK_UNMAPPED_BASE - the lower boundary of the mmap VM area
37  */
38 #define PAGE_OFFSET             UL(CONFIG_PAGE_OFFSET)
39 #define TASK_SIZE               (UL(CONFIG_PAGE_OFFSET) - UL(0x01000000))
40 #define TASK_UNMAPPED_BASE      ALIGN(TASK_SIZE / 3, SZ_16M)
42 /*
43  * The maximum size of a 26-bit user space task.
44  */
45 #define TASK_SIZE_26            UL(0x04000000)
47 /*
48  * The module space lives between the addresses given by TASK_SIZE
49  * and PAGE_OFFSET - it must be within 32MB of the kernel text.
50  */
51 #ifndef CONFIG_THUMB2_KERNEL
52 #define MODULES_VADDR           (PAGE_OFFSET - 16*1024*1024)
53 #else
54 /* smaller range for Thumb-2 symbols relocation (2^24)*/
55 #define MODULES_VADDR           (PAGE_OFFSET - 8*1024*1024)
56 #endif
58 #if TASK_SIZE > MODULES_VADDR
59 #error Top of user space clashes with start of module space
60 #endif
62 /*
63  * The highmem pkmap virtual space shares the end of the module area.
64  */
65 #ifdef CONFIG_HIGHMEM
66 #define MODULES_END             (PAGE_OFFSET - PMD_SIZE)
67 #else
68 #define MODULES_END             (PAGE_OFFSET)
69 #endif
71 /*
72  * The XIP kernel gets mapped at the bottom of the module vm area.
73  * Since we use sections to map it, this macro replaces the physical address
74  * with its virtual address while keeping offset from the base section.
75  */
76 #define XIP_VIRT_ADDR(physaddr)  (MODULES_VADDR + ((physaddr) & 0x000fffff))
78 /*
79  * Allow 16MB-aligned ioremap pages
80  */
81 #define IOREMAP_MAX_ORDER       24
83 #define CONSISTENT_END          (0xffe00000UL)
85 #else /* CONFIG_MMU */
87 /*
88  * The limitation of user task size can grow up to the end of free ram region.
89  * It is difficult to define and perhaps will never meet the original meaning
90  * of this define that was meant to.
91  * Fortunately, there is no reference for this in noMMU mode, for now.
92  */
93 #ifndef TASK_SIZE
94 #define TASK_SIZE               (CONFIG_DRAM_SIZE)
95 #endif
97 #ifndef TASK_UNMAPPED_BASE
98 #define TASK_UNMAPPED_BASE      UL(0x00000000)
99 #endif
101 #ifndef PHYS_OFFSET
102 #define PHYS_OFFSET             UL(CONFIG_DRAM_BASE)
103 #endif
105 #ifndef END_MEM
106 #define END_MEM                 (UL(CONFIG_DRAM_BASE) + CONFIG_DRAM_SIZE)
107 #endif
109 #ifndef PAGE_OFFSET
110 #define PAGE_OFFSET             (PHYS_OFFSET)
111 #endif
113 /*
114  * The module can be at any place in ram in nommu mode.
115  */
116 #define MODULES_END             (END_MEM)
117 #define MODULES_VADDR           (PHYS_OFFSET)
119 #define XIP_VIRT_ADDR(physaddr)  (physaddr)
121 #endif /* !CONFIG_MMU */
123 /*
124  * We fix the TCM memories max 32 KiB ITCM resp DTCM at these
125  * locations
126  */
127 #ifdef CONFIG_HAVE_TCM
128 #define ITCM_OFFSET     UL(0xfffe0000)
129 #define DTCM_OFFSET     UL(0xfffe8000)
130 #endif
132 /*
133  * Convert a physical address to a Page Frame Number and back
134  */
135 #define __phys_to_pfn(paddr)    ((unsigned long)((paddr) >> PAGE_SHIFT))
136 #define __pfn_to_phys(pfn)      ((phys_addr_t)(pfn) << PAGE_SHIFT)
138 /*
139  * Convert a page to/from a physical address
140  */
141 #define page_to_phys(page)      (__pfn_to_phys(page_to_pfn(page)))
142 #define phys_to_page(phys)      (pfn_to_page(__phys_to_pfn(phys)))
144 #ifndef __ASSEMBLY__
146 /*
147  * Physical vs virtual RAM address space conversion.  These are
148  * private definitions which should NOT be used outside memory.h
149  * files.  Use virt_to_phys/phys_to_virt/__pa/__va instead.
150  */
151 #ifndef __virt_to_phys
152 #ifdef CONFIG_ARM_PATCH_PHYS_VIRT
154 /*
155  * Constants used to force the right instruction encodings and shifts
156  * so that all we need to do is modify the 8-bit constant field.
157  */
158 #define __PV_BITS_31_24 0x81000000
160 extern unsigned long __pv_phys_offset;
161 #define PHYS_OFFSET __pv_phys_offset
163 #define __pv_stub(from,to,instr,type)                   \
164         __asm__("@ __pv_stub\n"                         \
165         "1:     " instr "       %0, %1, %2\n"           \
166         "       .pushsection .pv_table,\"a\"\n"         \
167         "       .long   1b\n"                           \
168         "       .popsection\n"                          \
169         : "=r" (to)                                     \
170         : "r" (from), "I" (type))
172 static inline unsigned long __virt_to_phys(unsigned long x)
174         unsigned long t;
175         __pv_stub(x, t, "add", __PV_BITS_31_24);
176         return t;
179 static inline unsigned long __phys_to_virt(unsigned long x)
181         unsigned long t;
182         __pv_stub(x, t, "sub", __PV_BITS_31_24);
183         return t;
185 #else
186 #define __virt_to_phys(x)       ((x) - PAGE_OFFSET + PHYS_OFFSET)
187 #define __phys_to_virt(x)       ((x) - PHYS_OFFSET + PAGE_OFFSET)
188 #endif
189 #endif
190 #endif /* __ASSEMBLY__ */
192 #ifndef PHYS_OFFSET
193 #ifdef PLAT_PHYS_OFFSET
194 #define PHYS_OFFSET     PLAT_PHYS_OFFSET
195 #else
196 #define PHYS_OFFSET     UL(CONFIG_PHYS_OFFSET)
197 #endif
198 #endif
200 #ifndef __ASSEMBLY__
202 /*
203  * PFNs are used to describe any physical page; this means
204  * PFN 0 == physical address 0.
205  *
206  * This is the PFN of the first RAM page in the kernel
207  * direct-mapped view.  We assume this is the first page
208  * of RAM in the mem_map as well.
209  */
210 #define PHYS_PFN_OFFSET (PHYS_OFFSET >> PAGE_SHIFT)
212 /*
213  * These are *only* valid on the kernel direct mapped RAM memory.
214  * Note: Drivers should NOT use these.  They are the wrong
215  * translation for translating DMA addresses.  Use the driver
216  * DMA support - see dma-mapping.h.
217  */
218 static inline phys_addr_t virt_to_phys(const volatile void *x)
220         return __virt_to_phys((unsigned long)(x));
223 static inline void *phys_to_virt(phys_addr_t x)
225         return (void *)(__phys_to_virt((unsigned long)(x)));
228 /*
229  * Drivers should NOT use these either.
230  */
231 #define __pa(x)                 __virt_to_phys((unsigned long)(x))
232 #define __va(x)                 ((void *)__phys_to_virt((unsigned long)(x)))
233 #define pfn_to_kaddr(pfn)       __va((pfn) << PAGE_SHIFT)
235 /*
236  * Virtual <-> DMA view memory address translations
237  * Again, these are *only* valid on the kernel direct mapped RAM
238  * memory.  Use of these is *deprecated* (and that doesn't mean
239  * use the __ prefixed forms instead.)  See dma-mapping.h.
240  */
241 #ifndef __virt_to_bus
242 #define __virt_to_bus   __virt_to_phys
243 #define __bus_to_virt   __phys_to_virt
244 #define __pfn_to_bus(x) __pfn_to_phys(x)
245 #define __bus_to_pfn(x) __phys_to_pfn(x)
246 #endif
248 static inline __deprecated unsigned long virt_to_bus(void *x)
250         return __virt_to_bus((unsigned long)x);
253 static inline __deprecated void *bus_to_virt(unsigned long x)
255         return (void *)__bus_to_virt(x);
258 /*
259  * Conversion between a struct page and a physical address.
260  *
261  * Note: when converting an unknown physical address to a
262  * struct page, the resulting pointer must be validated
263  * using VALID_PAGE().  It must return an invalid struct page
264  * for any physical address not corresponding to a system
265  * RAM address.
266  *
267  *  page_to_pfn(page)   convert a struct page * to a PFN number
268  *  pfn_to_page(pfn)    convert a _valid_ PFN number to struct page *
269  *
270  *  virt_to_page(k)     convert a _valid_ virtual address to struct page *
271  *  virt_addr_valid(k)  indicates whether a virtual address is valid
272  */
273 #define ARCH_PFN_OFFSET         PHYS_PFN_OFFSET
275 #define virt_to_page(kaddr)     pfn_to_page(__pa(kaddr) >> PAGE_SHIFT)
276 #define virt_addr_valid(kaddr)  ((unsigned long)(kaddr) >= PAGE_OFFSET && (unsigned long)(kaddr) < (unsigned long)high_memory)
278 #endif
280 #include <asm-generic/memory_model.h>
282 #endif