1 /******************************************************************************
2 * Guest OS interface to ARM Xen.
3 *
4 * Stefano Stabellini <stefano.stabellini@eu.citrix.com>, Citrix, 2012
5 */
7 #ifndef _ASM_ARM_XEN_INTERFACE_H
8 #define _ASM_ARM_XEN_INTERFACE_H
10 #include <linux/types.h>
12 #define uint64_aligned_t uint64_t __attribute__((aligned(8)))
14 #define __DEFINE_GUEST_HANDLE(name, type) \
15 typedef struct { union { type *p; uint64_aligned_t q; }; } \
16 __guest_handle_ ## name
18 #define DEFINE_GUEST_HANDLE_STRUCT(name) \
19 __DEFINE_GUEST_HANDLE(name, struct name)
20 #define DEFINE_GUEST_HANDLE(name) __DEFINE_GUEST_HANDLE(name, name)
21 #define GUEST_HANDLE(name) __guest_handle_ ## name
23 #define set_xen_guest_handle(hnd, val) \
24 do { \
25 if (sizeof(hnd) == 8) \
26 *(uint64_t *)&(hnd) = 0; \
27 (hnd).p = val; \
28 } while (0)
30 #ifndef __ASSEMBLY__
31 /* Explicitly size integers that represent pfns in the interface with
32 * Xen so that we can have one ABI that works for 32 and 64 bit guests.
33 * Note that this means that the xen_pfn_t type may be capable of
34 * representing pfn's which the guest cannot represent in its own pfn
35 * type. However since pfn space is controlled by the guest this is
36 * fine since it simply wouldn't be able to create any sure pfns in
37 * the first place.
38 */
39 typedef uint64_t xen_pfn_t;
40 #define PRI_xen_pfn "llx"
41 typedef uint64_t xen_ulong_t;
42 #define PRI_xen_ulong "llx"
43 /* Guest handles for primitive C types. */
44 __DEFINE_GUEST_HANDLE(uchar, unsigned char);
45 __DEFINE_GUEST_HANDLE(uint, unsigned int);
46 DEFINE_GUEST_HANDLE(char);
47 DEFINE_GUEST_HANDLE(int);
48 DEFINE_GUEST_HANDLE(void);
49 DEFINE_GUEST_HANDLE(uint64_t);
50 DEFINE_GUEST_HANDLE(uint32_t);
51 DEFINE_GUEST_HANDLE(xen_pfn_t);
52 DEFINE_GUEST_HANDLE(xen_ulong_t);
54 /* Maximum number of virtual CPUs in multi-processor guests. */
55 #define MAX_VIRT_CPUS 1
57 struct arch_vcpu_info { };
58 struct arch_shared_info { };
60 /* TODO: Move pvclock definitions some place arch independent */
61 struct pvclock_vcpu_time_info {
62 u32 version;
63 u32 pad0;
64 u64 tsc_timestamp;
65 u64 system_time;
66 u32 tsc_to_system_mul;
67 s8 tsc_shift;
68 u8 flags;
69 u8 pad[2];
70 } __attribute__((__packed__)); /* 32 bytes */
72 /* It is OK to have a 12 bytes struct with no padding because it is packed */
73 struct pvclock_wall_clock {
74 u32 version;
75 u32 sec;
76 u32 nsec;
77 } __attribute__((__packed__));
78 #endif
80 #endif /* _ASM_ARM_XEN_INTERFACE_H */