1 /*
2 * Copyright (c) 2012 Linaro Limited.
3 *
4 * This program is free software; you can redistribute it and/or modify
5 * it under the terms of the GNU General Public License as published by
6 * the Free Software Foundation; either version 2 of the License, or
7 * (at your option) any later version.
8 *
9 * This program is distributed in the hope that it will be useful,
10 * but WITHOUT ANY WARRANTY; without even the implied warranty of
11 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
12 * GNU General Public License for more details.
13 *
14 * You should have received a copy of the GNU General Public License along
15 * with this program; if not, write to the Free Software Foundation, Inc.,
16 * 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
17 */
19 #include <linux/init.h>
20 #include <linux/linkage.h>
21 #include <asm/assembler.h>
22 #include <asm/virt.h>
24 #ifndef ZIMAGE
25 /*
26 * For the kernel proper, we need to find out the CPU boot mode long after
27 * boot, so we need to store it in a writable variable.
28 *
29 * This is not in .bss, because we set it sufficiently early that the boot-time
30 * zeroing of .bss would clobber it.
31 */
32 .data
33 ENTRY(__boot_cpu_mode)
34 .long 0
35 .text
37 /*
38 * Save the primary CPU boot mode. Requires 3 scratch registers.
39 */
40 .macro store_primary_cpu_mode reg1, reg2, reg3
41 mrs \reg1, cpsr
42 and \reg1, \reg1, #MODE_MASK
43 adr \reg2, .L__boot_cpu_mode_offset
44 ldr \reg3, [\reg2]
45 str \reg1, [\reg2, \reg3]
46 .endm
48 /*
49 * Compare the current mode with the one saved on the primary CPU.
50 * If they don't match, record that fact. The Z bit indicates
51 * if there's a match or not.
52 * Requires 3 additionnal scratch registers.
53 */
54 .macro compare_cpu_mode_with_primary mode, reg1, reg2, reg3
55 adr \reg2, .L__boot_cpu_mode_offset
56 ldr \reg3, [\reg2]
57 ldr \reg1, [\reg2, \reg3]
58 cmp \mode, \reg1 @ matches primary CPU boot mode?
59 orrne r7, r7, #BOOT_CPU_MODE_MISMATCH
60 strne r7, [r5, r6] @ record what happened and give up
61 .endm
63 #else /* ZIMAGE */
65 .macro store_primary_cpu_mode reg1:req, reg2:req, reg3:req
66 .endm
68 /*
69 * The zImage loader only runs on one CPU, so we don't bother with mult-CPU
70 * consistency checking:
71 */
72 .macro compare_cpu_mode_with_primary mode, reg1, reg2, reg3
73 cmp \mode, \mode
74 .endm
76 #endif /* ZIMAGE */
78 /*
79 * Hypervisor stub installation functions.
80 *
81 * These must be called with the MMU and D-cache off.
82 * They are not ABI compliant and are only intended to be called from the kernel
83 * entry points in head.S.
84 */
85 @ Call this from the primary CPU
86 ENTRY(__hyp_stub_install)
87 store_primary_cpu_mode r4, r5, r6
88 ENDPROC(__hyp_stub_install)
90 @ fall through...
92 @ Secondary CPUs should call here
93 ENTRY(__hyp_stub_install_secondary)
94 mrs r4, cpsr
95 and r4, r4, #MODE_MASK
97 /*
98 * If the secondary has booted with a different mode, give up
99 * immediately.
100 */
101 compare_cpu_mode_with_primary r4, r5, r6, r7
102 movne pc, lr
104 /*
105 * Once we have given up on one CPU, we do not try to install the
106 * stub hypervisor on the remaining ones: because the saved boot mode
107 * is modified, it can't compare equal to the CPSR mode field any
108 * more.
109 *
110 * Otherwise...
111 */
113 cmp r4, #HYP_MODE
114 movne pc, lr @ give up if the CPU is not in HYP mode
116 /*
117 * Configure HSCTLR to set correct exception endianness/instruction set
118 * state etc.
119 * Turn off all traps
120 * Eventually, CPU-specific code might be needed -- assume not for now
121 *
122 * This code relies on the "eret" instruction to synchronize the
123 * various coprocessor accesses. This is done when we switch to SVC
124 * (see safe_svcmode_maskall).
125 */
126 @ Now install the hypervisor stub:
127 adr r7, __hyp_stub_vectors
128 mcr p15, 4, r7, c12, c0, 0 @ set hypervisor vector base (HVBAR)
130 @ Disable all traps, so we don't get any nasty surprise
131 mov r7, #0
132 mcr p15, 4, r7, c1, c1, 0 @ HCR
133 mcr p15, 4, r7, c1, c1, 2 @ HCPTR
134 mcr p15, 4, r7, c1, c1, 3 @ HSTR
136 THUMB( orr r7, #(1 << 30) ) @ HSCTLR.TE
137 #ifdef CONFIG_CPU_BIG_ENDIAN
138 orr r7, #(1 << 9) @ HSCTLR.EE
139 #endif
140 mcr p15, 4, r7, c1, c0, 0 @ HSCTLR
142 mrc p15, 4, r7, c1, c1, 1 @ HDCR
143 and r7, #0x1f @ Preserve HPMN
144 mcr p15, 4, r7, c1, c1, 1 @ HDCR
146 #if !defined(ZIMAGE) && defined(CONFIG_ARM_ARCH_TIMER)
147 @ make CNTP_* and CNTPCT accessible from PL1
148 mrc p15, 0, r7, c0, c1, 1 @ ID_PFR1
149 lsr r7, #16
150 and r7, #0xf
151 cmp r7, #1
152 bne 1f
153 mrc p15, 4, r7, c14, c1, 0 @ CNTHCTL
154 orr r7, r7, #3 @ PL1PCEN | PL1PCTEN
155 mcr p15, 4, r7, c14, c1, 0 @ CNTHCTL
156 1:
157 #endif
159 bx lr @ The boot CPU mode is left in r4.
160 ENDPROC(__hyp_stub_install_secondary)
162 __hyp_stub_do_trap:
163 cmp r0, #-1
164 mrceq p15, 4, r0, c12, c0, 0 @ get HVBAR
165 mcrne p15, 4, r0, c12, c0, 0 @ set HVBAR
166 __ERET
167 ENDPROC(__hyp_stub_do_trap)
169 /*
170 * __hyp_set_vectors: Call this after boot to set the initial hypervisor
171 * vectors as part of hypervisor installation. On an SMP system, this should
172 * be called on each CPU.
173 *
174 * r0 must be the physical address of the new vector table (which must lie in
175 * the bottom 4GB of physical address space.
176 *
177 * r0 must be 32-byte aligned.
178 *
179 * Before calling this, you must check that the stub hypervisor is installed
180 * everywhere, by waiting for any secondary CPUs to be brought up and then
181 * checking that BOOT_CPU_MODE_HAVE_HYP(__boot_cpu_mode) is true.
182 *
183 * If not, there is a pre-existing hypervisor, some CPUs failed to boot, or
184 * something else went wrong... in such cases, trying to install a new
185 * hypervisor is unlikely to work as desired.
186 *
187 * When you call into your shiny new hypervisor, sp_hyp will contain junk,
188 * so you will need to set that to something sensible at the new hypervisor's
189 * initialisation entry point.
190 */
191 ENTRY(__hyp_get_vectors)
192 mov r0, #-1
193 ENDPROC(__hyp_get_vectors)
194 @ fall through
195 ENTRY(__hyp_set_vectors)
196 __HVC(0)
197 mov pc, lr
198 ENDPROC(__hyp_set_vectors)
200 #ifndef ZIMAGE
201 .align 2
202 .L__boot_cpu_mode_offset:
203 .long __boot_cpu_mode - .
204 #endif
206 .align 5
207 __hyp_stub_vectors:
208 __hyp_stub_reset: W(b) .
209 __hyp_stub_und: W(b) .
210 __hyp_stub_svc: W(b) .
211 __hyp_stub_pabort: W(b) .
212 __hyp_stub_dabort: W(b) .
213 __hyp_stub_trap: W(b) __hyp_stub_do_trap
214 __hyp_stub_irq: W(b) .
215 __hyp_stub_fiq: W(b) .
216 ENDPROC(__hyp_stub_vectors)