]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - arch/arm/mach-at91/irq.c
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/dtor/input
[android-sdk/kernel-video.git] / arch / arm / mach-at91 / irq.c
1 /*
2  * linux/arch/arm/mach-at91/irq.c
3  *
4  *  Copyright (C) 2004 SAN People
5  *  Copyright (C) 2004 ATMEL
6  *  Copyright (C) Rick Bronson
7  *
8  * This program is free software; you can redistribute it and/or modify
9  * it under the terms of the GNU General Public License as published by
10  * the Free Software Foundation; either version 2 of the License, or
11  * (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
21  */
23 #include <linux/init.h>
24 #include <linux/module.h>
25 #include <linux/mm.h>
26 #include <linux/bitmap.h>
27 #include <linux/types.h>
28 #include <linux/irq.h>
29 #include <linux/of.h>
30 #include <linux/of_address.h>
31 #include <linux/of_irq.h>
32 #include <linux/irqdomain.h>
33 #include <linux/err.h>
34 #include <linux/slab.h>
36 #include <mach/hardware.h>
37 #include <asm/irq.h>
38 #include <asm/setup.h>
40 #include <asm/exception.h>
41 #include <asm/mach/arch.h>
42 #include <asm/mach/irq.h>
43 #include <asm/mach/map.h>
45 #include "at91_aic.h"
47 void __iomem *at91_aic_base;
48 static struct irq_domain *at91_aic_domain;
49 static struct device_node *at91_aic_np;
50 static unsigned int n_irqs = NR_AIC_IRQS;
51 static unsigned long at91_aic_caps = 0;
53 /* AIC5 introduces a Source Select Register */
54 #define AT91_AIC_CAP_AIC5       (1 << 0)
55 #define has_aic5()              (at91_aic_caps & AT91_AIC_CAP_AIC5)
57 #ifdef CONFIG_PM
59 static unsigned long *wakeups;
60 static unsigned long *backups;
62 #define set_backup(bit) set_bit(bit, backups)
63 #define clear_backup(bit) clear_bit(bit, backups)
65 static int at91_aic_pm_init(void)
66 {
67         backups = kzalloc(BITS_TO_LONGS(n_irqs) * sizeof(*backups), GFP_KERNEL);
68         if (!backups)
69                 return -ENOMEM;
71         wakeups = kzalloc(BITS_TO_LONGS(n_irqs) * sizeof(*backups), GFP_KERNEL);
72         if (!wakeups) {
73                 kfree(backups);
74                 return -ENOMEM;
75         }
77         return 0;
78 }
80 static int at91_aic_set_wake(struct irq_data *d, unsigned value)
81 {
82         if (unlikely(d->hwirq >= n_irqs))
83                 return -EINVAL;
85         if (value)
86                 set_bit(d->hwirq, wakeups);
87         else
88                 clear_bit(d->hwirq, wakeups);
90         return 0;
91 }
93 void at91_irq_suspend(void)
94 {
95         int i = 0, bit;
97         if (has_aic5()) {
98                 /* disable enabled irqs */
99                 while ((bit = find_next_bit(backups, n_irqs, i)) < n_irqs) {
100                         at91_aic_write(AT91_AIC5_SSR,
101                                        bit & AT91_AIC5_INTSEL_MSK);
102                         at91_aic_write(AT91_AIC5_IDCR, 1);
103                         i = bit;
104                 }
105                 /* enable wakeup irqs */
106                 i = 0;
107                 while ((bit = find_next_bit(wakeups, n_irqs, i)) < n_irqs) {
108                         at91_aic_write(AT91_AIC5_SSR,
109                                        bit & AT91_AIC5_INTSEL_MSK);
110                         at91_aic_write(AT91_AIC5_IECR, 1);
111                         i = bit;
112                 }
113         } else {
114                 at91_aic_write(AT91_AIC_IDCR, *backups);
115                 at91_aic_write(AT91_AIC_IECR, *wakeups);
116         }
119 void at91_irq_resume(void)
121         int i = 0, bit;
123         if (has_aic5()) {
124                 /* disable wakeup irqs */
125                 while ((bit = find_next_bit(wakeups, n_irqs, i)) < n_irqs) {
126                         at91_aic_write(AT91_AIC5_SSR,
127                                        bit & AT91_AIC5_INTSEL_MSK);
128                         at91_aic_write(AT91_AIC5_IDCR, 1);
129                         i = bit;
130                 }
131                 /* enable irqs disabled for suspend */
132                 i = 0;
133                 while ((bit = find_next_bit(backups, n_irqs, i)) < n_irqs) {
134                         at91_aic_write(AT91_AIC5_SSR,
135                                        bit & AT91_AIC5_INTSEL_MSK);
136                         at91_aic_write(AT91_AIC5_IECR, 1);
137                         i = bit;
138                 }
139         } else {
140                 at91_aic_write(AT91_AIC_IDCR, *wakeups);
141                 at91_aic_write(AT91_AIC_IECR, *backups);
142         }
145 #else
146 static inline int at91_aic_pm_init(void)
148         return 0;
151 #define set_backup(bit)
152 #define clear_backup(bit)
153 #define at91_aic_set_wake       NULL
155 #endif /* CONFIG_PM */
157 asmlinkage void __exception_irq_entry
158 at91_aic_handle_irq(struct pt_regs *regs)
160         u32 irqnr;
161         u32 irqstat;
163         irqnr = at91_aic_read(AT91_AIC_IVR);
164         irqstat = at91_aic_read(AT91_AIC_ISR);
166         /*
167          * ISR value is 0 when there is no current interrupt or when there is
168          * a spurious interrupt
169          */
170         if (!irqstat)
171                 at91_aic_write(AT91_AIC_EOICR, 0);
172         else
173                 handle_IRQ(irqnr, regs);
176 asmlinkage void __exception_irq_entry
177 at91_aic5_handle_irq(struct pt_regs *regs)
179         u32 irqnr;
180         u32 irqstat;
182         irqnr = at91_aic_read(AT91_AIC5_IVR);
183         irqstat = at91_aic_read(AT91_AIC5_ISR);
185         if (!irqstat)
186                 at91_aic_write(AT91_AIC5_EOICR, 0);
187         else
188                 handle_IRQ(irqnr, regs);
191 static void at91_aic_mask_irq(struct irq_data *d)
193         /* Disable interrupt on AIC */
194         at91_aic_write(AT91_AIC_IDCR, 1 << d->hwirq);
195         /* Update ISR cache */
196         clear_backup(d->hwirq);
199 static void __maybe_unused at91_aic5_mask_irq(struct irq_data *d)
201         /* Disable interrupt on AIC5 */
202         at91_aic_write(AT91_AIC5_SSR, d->hwirq & AT91_AIC5_INTSEL_MSK);
203         at91_aic_write(AT91_AIC5_IDCR, 1);
204         /* Update ISR cache */
205         clear_backup(d->hwirq);
208 static void at91_aic_unmask_irq(struct irq_data *d)
210         /* Enable interrupt on AIC */
211         at91_aic_write(AT91_AIC_IECR, 1 << d->hwirq);
212         /* Update ISR cache */
213         set_backup(d->hwirq);
216 static void __maybe_unused at91_aic5_unmask_irq(struct irq_data *d)
218         /* Enable interrupt on AIC5 */
219         at91_aic_write(AT91_AIC5_SSR, d->hwirq & AT91_AIC5_INTSEL_MSK);
220         at91_aic_write(AT91_AIC5_IECR, 1);
221         /* Update ISR cache */
222         set_backup(d->hwirq);
225 static void at91_aic_eoi(struct irq_data *d)
227         /*
228          * Mark end-of-interrupt on AIC, the controller doesn't care about
229          * the value written. Moreover it's a write-only register.
230          */
231         at91_aic_write(AT91_AIC_EOICR, 0);
234 static void __maybe_unused at91_aic5_eoi(struct irq_data *d)
236         at91_aic_write(AT91_AIC5_EOICR, 0);
239 unsigned long *at91_extern_irq;
241 #define is_extern_irq(hwirq) test_bit(hwirq, at91_extern_irq)
243 static int at91_aic_compute_srctype(struct irq_data *d, unsigned type)
245         int srctype;
247         switch (type) {
248         case IRQ_TYPE_LEVEL_HIGH:
249                 srctype = AT91_AIC_SRCTYPE_HIGH;
250                 break;
251         case IRQ_TYPE_EDGE_RISING:
252                 srctype = AT91_AIC_SRCTYPE_RISING;
253                 break;
254         case IRQ_TYPE_LEVEL_LOW:
255                 if ((d->hwirq == AT91_ID_FIQ) || is_extern_irq(d->hwirq))               /* only supported on external interrupts */
256                         srctype = AT91_AIC_SRCTYPE_LOW;
257                 else
258                         srctype = -EINVAL;
259                 break;
260         case IRQ_TYPE_EDGE_FALLING:
261                 if ((d->hwirq == AT91_ID_FIQ) || is_extern_irq(d->hwirq))               /* only supported on external interrupts */
262                         srctype = AT91_AIC_SRCTYPE_FALLING;
263                 else
264                         srctype = -EINVAL;
265                 break;
266         default:
267                 srctype = -EINVAL;
268         }
270         return srctype;
273 static int at91_aic_set_type(struct irq_data *d, unsigned type)
275         unsigned int smr;
276         int srctype;
278         srctype = at91_aic_compute_srctype(d, type);
279         if (srctype < 0)
280                 return srctype;
282         if (has_aic5()) {
283                 at91_aic_write(AT91_AIC5_SSR,
284                                d->hwirq & AT91_AIC5_INTSEL_MSK);
285                 smr = at91_aic_read(AT91_AIC5_SMR) & ~AT91_AIC_SRCTYPE;
286                 at91_aic_write(AT91_AIC5_SMR, smr | srctype);
287         } else {
288                 smr = at91_aic_read(AT91_AIC_SMR(d->hwirq))
289                       & ~AT91_AIC_SRCTYPE;
290                 at91_aic_write(AT91_AIC_SMR(d->hwirq), smr | srctype);
291         }
293         return 0;
296 static struct irq_chip at91_aic_chip = {
297         .name           = "AIC",
298         .irq_mask       = at91_aic_mask_irq,
299         .irq_unmask     = at91_aic_unmask_irq,
300         .irq_set_type   = at91_aic_set_type,
301         .irq_set_wake   = at91_aic_set_wake,
302         .irq_eoi        = at91_aic_eoi,
303 };
305 static void __init at91_aic_hw_init(unsigned int spu_vector)
307         int i;
309         /*
310          * Perform 8 End Of Interrupt Command to make sure AIC
311          * will not Lock out nIRQ
312          */
313         for (i = 0; i < 8; i++)
314                 at91_aic_write(AT91_AIC_EOICR, 0);
316         /*
317          * Spurious Interrupt ID in Spurious Vector Register.
318          * When there is no current interrupt, the IRQ Vector Register
319          * reads the value stored in AIC_SPU
320          */
321         at91_aic_write(AT91_AIC_SPU, spu_vector);
323         /* No debugging in AIC: Debug (Protect) Control Register */
324         at91_aic_write(AT91_AIC_DCR, 0);
326         /* Disable and clear all interrupts initially */
327         at91_aic_write(AT91_AIC_IDCR, 0xFFFFFFFF);
328         at91_aic_write(AT91_AIC_ICCR, 0xFFFFFFFF);
331 static void __init __maybe_unused at91_aic5_hw_init(unsigned int spu_vector)
333         int i;
335         /*
336          * Perform 8 End Of Interrupt Command to make sure AIC
337          * will not Lock out nIRQ
338          */
339         for (i = 0; i < 8; i++)
340                 at91_aic_write(AT91_AIC5_EOICR, 0);
342         /*
343          * Spurious Interrupt ID in Spurious Vector Register.
344          * When there is no current interrupt, the IRQ Vector Register
345          * reads the value stored in AIC_SPU
346          */
347         at91_aic_write(AT91_AIC5_SPU, spu_vector);
349         /* No debugging in AIC: Debug (Protect) Control Register */
350         at91_aic_write(AT91_AIC5_DCR, 0);
352         /* Disable and clear all interrupts initially */
353         for (i = 0; i < n_irqs; i++) {
354                 at91_aic_write(AT91_AIC5_SSR, i & AT91_AIC5_INTSEL_MSK);
355                 at91_aic_write(AT91_AIC5_IDCR, 1);
356                 at91_aic_write(AT91_AIC5_ICCR, 1);
357         }
360 #if defined(CONFIG_OF)
361 static unsigned int *at91_aic_irq_priorities;
363 static int at91_aic_irq_map(struct irq_domain *h, unsigned int virq,
364                                                         irq_hw_number_t hw)
366         /* Put virq number in Source Vector Register */
367         at91_aic_write(AT91_AIC_SVR(hw), virq);
369         /* Active Low interrupt, with priority */
370         at91_aic_write(AT91_AIC_SMR(hw),
371                        AT91_AIC_SRCTYPE_LOW | at91_aic_irq_priorities[hw]);
373         irq_set_chip_and_handler(virq, &at91_aic_chip, handle_fasteoi_irq);
374         set_irq_flags(virq, IRQF_VALID | IRQF_PROBE);
376         return 0;
379 static int at91_aic5_irq_map(struct irq_domain *h, unsigned int virq,
380                 irq_hw_number_t hw)
382         at91_aic_write(AT91_AIC5_SSR, hw & AT91_AIC5_INTSEL_MSK);
384         /* Put virq number in Source Vector Register */
385         at91_aic_write(AT91_AIC5_SVR, virq);
387         /* Active Low interrupt, with priority */
388         at91_aic_write(AT91_AIC5_SMR,
389                        AT91_AIC_SRCTYPE_LOW | at91_aic_irq_priorities[hw]);
391         irq_set_chip_and_handler(virq, &at91_aic_chip, handle_fasteoi_irq);
392         set_irq_flags(virq, IRQF_VALID | IRQF_PROBE);
394         return 0;
397 static int at91_aic_irq_domain_xlate(struct irq_domain *d, struct device_node *ctrlr,
398                                 const u32 *intspec, unsigned int intsize,
399                                 irq_hw_number_t *out_hwirq, unsigned int *out_type)
401         if (WARN_ON(intsize < 3))
402                 return -EINVAL;
403         if (WARN_ON(intspec[0] >= n_irqs))
404                 return -EINVAL;
405         if (WARN_ON((intspec[2] < AT91_AIC_IRQ_MIN_PRIORITY)
406                     || (intspec[2] > AT91_AIC_IRQ_MAX_PRIORITY)))
407                 return -EINVAL;
409         *out_hwirq = intspec[0];
410         *out_type = intspec[1] & IRQ_TYPE_SENSE_MASK;
411         at91_aic_irq_priorities[*out_hwirq] = intspec[2];
413         return 0;
416 static struct irq_domain_ops at91_aic_irq_ops = {
417         .map    = at91_aic_irq_map,
418         .xlate  = at91_aic_irq_domain_xlate,
419 };
421 int __init at91_aic_of_common_init(struct device_node *node,
422                                     struct device_node *parent)
424         struct property *prop;
425         const __be32 *p;
426         u32 val;
428         at91_extern_irq = kzalloc(BITS_TO_LONGS(n_irqs)
429                                   * sizeof(*at91_extern_irq), GFP_KERNEL);
430         if (!at91_extern_irq)
431                 return -ENOMEM;
433         if (at91_aic_pm_init()) {
434                 kfree(at91_extern_irq);
435                 return -ENOMEM;
436         }
438         at91_aic_irq_priorities = kzalloc(n_irqs
439                                           * sizeof(*at91_aic_irq_priorities),
440                                           GFP_KERNEL);
441         if (!at91_aic_irq_priorities)
442                 return -ENOMEM;
444         at91_aic_base = of_iomap(node, 0);
445         at91_aic_np = node;
447         at91_aic_domain = irq_domain_add_linear(at91_aic_np, n_irqs,
448                                                 &at91_aic_irq_ops, NULL);
449         if (!at91_aic_domain)
450                 panic("Unable to add AIC irq domain (DT)\n");
452         of_property_for_each_u32(node, "atmel,external-irqs", prop, p, val) {
453                 if (val >= n_irqs)
454                         pr_warn("AIC: external irq %d >= %d skip it\n",
455                                 val, n_irqs);
456                 else
457                         set_bit(val, at91_extern_irq);
458         }
460         irq_set_default_host(at91_aic_domain);
462         return 0;
465 int __init at91_aic_of_init(struct device_node *node,
466                                      struct device_node *parent)
468         int err;
470         err = at91_aic_of_common_init(node, parent);
471         if (err)
472                 return err;
474         at91_aic_hw_init(n_irqs);
476         return 0;
479 int __init at91_aic5_of_init(struct device_node *node,
480                                      struct device_node *parent)
482         int err;
484         at91_aic_caps |= AT91_AIC_CAP_AIC5;
485         n_irqs = NR_AIC5_IRQS;
486         at91_aic_chip.irq_ack           = at91_aic5_mask_irq;
487         at91_aic_chip.irq_mask          = at91_aic5_mask_irq;
488         at91_aic_chip.irq_unmask        = at91_aic5_unmask_irq;
489         at91_aic_chip.irq_eoi           = at91_aic5_eoi;
490         at91_aic_irq_ops.map            = at91_aic5_irq_map;
492         err = at91_aic_of_common_init(node, parent);
493         if (err)
494                 return err;
496         at91_aic5_hw_init(n_irqs);
498         return 0;
500 #endif
502 /*
503  * Initialize the AIC interrupt controller.
504  */
505 void __init at91_aic_init(unsigned int *priority, unsigned int ext_irq_mask)
507         unsigned int i;
508         int irq_base;
510         at91_extern_irq = kzalloc(BITS_TO_LONGS(n_irqs)
511                                   * sizeof(*at91_extern_irq), GFP_KERNEL);
513         if (at91_aic_pm_init() || at91_extern_irq == NULL)
514                 panic("Unable to allocate bit maps\n");
516         *at91_extern_irq = ext_irq_mask;
518         at91_aic_base = ioremap(AT91_AIC, 512);
519         if (!at91_aic_base)
520                 panic("Unable to ioremap AIC registers\n");
522         /* Add irq domain for AIC */
523         irq_base = irq_alloc_descs(-1, 0, n_irqs, 0);
524         if (irq_base < 0) {
525                 WARN(1, "Cannot allocate irq_descs, assuming pre-allocated\n");
526                 irq_base = 0;
527         }
528         at91_aic_domain = irq_domain_add_legacy(at91_aic_np, n_irqs,
529                                                 irq_base, 0,
530                                                 &irq_domain_simple_ops, NULL);
532         if (!at91_aic_domain)
533                 panic("Unable to add AIC irq domain\n");
535         irq_set_default_host(at91_aic_domain);
537         /*
538          * The IVR is used by macro get_irqnr_and_base to read and verify.
539          * The irq number is NR_AIC_IRQS when a spurious interrupt has occurred.
540          */
541         for (i = 0; i < n_irqs; i++) {
542                 /* Put hardware irq number in Source Vector Register: */
543                 at91_aic_write(AT91_AIC_SVR(i), NR_IRQS_LEGACY + i);
544                 /* Active Low interrupt, with the specified priority */
545                 at91_aic_write(AT91_AIC_SMR(i), AT91_AIC_SRCTYPE_LOW | priority[i]);
546                 irq_set_chip_and_handler(NR_IRQS_LEGACY + i, &at91_aic_chip, handle_fasteoi_irq);
547                 set_irq_flags(i, IRQF_VALID | IRQF_PROBE);
548         }
550         at91_aic_hw_init(n_irqs);