1 /*
2 * linux/arch/arm/mach-omap1/clock.h
3 *
4 * Copyright (C) 2004 - 2005, 2009 Nokia corporation
5 * Written by Tuukka Tikkanen <tuukka.tikkanen@elektrobit.com>
6 * Based on clocks.h by Tony Lindgren, Gordon McNutt and RidgeRun, Inc
7 *
8 * This program is free software; you can redistribute it and/or modify
9 * it under the terms of the GNU General Public License version 2 as
10 * published by the Free Software Foundation.
11 */
13 #ifndef __ARCH_ARM_MACH_OMAP1_CLOCK_H
14 #define __ARCH_ARM_MACH_OMAP1_CLOCK_H
16 #include <linux/clk.h>
17 #include <linux/list.h>
19 #include <linux/clkdev.h>
21 struct module;
22 struct clk;
24 struct omap_clk {
25 u16 cpu;
26 struct clk_lookup lk;
27 };
29 #define CLK(dev, con, ck, cp) \
30 { \
31 .cpu = cp, \
32 .lk = { \
33 .dev_id = dev, \
34 .con_id = con, \
35 .clk = ck, \
36 }, \
37 }
39 /* Platform flags for the clkdev-OMAP integration code */
40 #define CK_310 (1 << 0)
41 #define CK_7XX (1 << 1) /* 7xx, 850 */
42 #define CK_1510 (1 << 2)
43 #define CK_16XX (1 << 3) /* 16xx, 17xx, 5912 */
44 #define CK_1710 (1 << 4) /* 1710 extra for rate selection */
47 /* Temporary, needed during the common clock framework conversion */
48 #define __clk_get_name(clk) (clk->name)
49 #define __clk_get_parent(clk) (clk->parent)
50 #define __clk_get_rate(clk) (clk->rate)
52 /**
53 * struct clkops - some clock function pointers
54 * @enable: fn ptr that enables the current clock in hardware
55 * @disable: fn ptr that enables the current clock in hardware
56 * @find_idlest: function returning the IDLEST register for the clock's IP blk
57 * @find_companion: function returning the "companion" clk reg for the clock
58 * @allow_idle: fn ptr that enables autoidle for the current clock in hardware
59 * @deny_idle: fn ptr that disables autoidle for the current clock in hardware
60 *
61 * A "companion" clk is an accompanying clock to the one being queried
62 * that must be enabled for the IP module connected to the clock to
63 * become accessible by the hardware. Neither @find_idlest nor
64 * @find_companion should be needed; that information is IP
65 * block-specific; the hwmod code has been created to handle this, but
66 * until hwmod data is ready and drivers have been converted to use PM
67 * runtime calls in place of clk_enable()/clk_disable(), @find_idlest and
68 * @find_companion must, unfortunately, remain.
69 */
70 struct clkops {
71 int (*enable)(struct clk *);
72 void (*disable)(struct clk *);
73 void (*find_idlest)(struct clk *, void __iomem **,
74 u8 *, u8 *);
75 void (*find_companion)(struct clk *, void __iomem **,
76 u8 *);
77 void (*allow_idle)(struct clk *);
78 void (*deny_idle)(struct clk *);
79 };
81 /*
82 * struct clk.flags possibilities
83 *
84 * XXX document the rest of the clock flags here
85 *
86 * CLOCK_CLKOUTX2: (OMAP4 only) DPLL CLKOUT and CLKOUTX2 GATE_CTRL
87 * bits share the same register. This flag allows the
88 * omap4_dpllmx*() code to determine which GATE_CTRL bit field
89 * should be used. This is a temporary solution - a better approach
90 * would be to associate clock type-specific data with the clock,
91 * similar to the struct dpll_data approach.
92 */
93 #define ENABLE_REG_32BIT (1 << 0) /* Use 32-bit access */
94 #define CLOCK_IDLE_CONTROL (1 << 1)
95 #define CLOCK_NO_IDLE_PARENT (1 << 2)
96 #define ENABLE_ON_INIT (1 << 3) /* Enable upon framework init */
97 #define INVERT_ENABLE (1 << 4) /* 0 enables, 1 disables */
98 #define CLOCK_CLKOUTX2 (1 << 5)
100 /**
101 * struct clk - OMAP struct clk
102 * @node: list_head connecting this clock into the full clock list
103 * @ops: struct clkops * for this clock
104 * @name: the name of the clock in the hardware (used in hwmod data and debug)
105 * @parent: pointer to this clock's parent struct clk
106 * @children: list_head connecting to the child clks' @sibling list_heads
107 * @sibling: list_head connecting this clk to its parent clk's @children
108 * @rate: current clock rate
109 * @enable_reg: register to write to enable the clock (see @enable_bit)
110 * @recalc: fn ptr that returns the clock's current rate
111 * @set_rate: fn ptr that can change the clock's current rate
112 * @round_rate: fn ptr that can round the clock's current rate
113 * @init: fn ptr to do clock-specific initialization
114 * @enable_bit: bitshift to write to enable/disable the clock (see @enable_reg)
115 * @usecount: number of users that have requested this clock to be enabled
116 * @fixed_div: when > 0, this clock's rate is its parent's rate / @fixed_div
117 * @flags: see "struct clk.flags possibilities" above
118 * @rate_offset: bitshift for rate selection bitfield (OMAP1 only)
119 * @src_offset: bitshift for source selection bitfield (OMAP1 only)
120 *
121 * XXX @rate_offset, @src_offset should probably be removed and OMAP1
122 * clock code converted to use clksel.
123 *
124 * XXX @usecount is poorly named. It should be "enable_count" or
125 * something similar. "users" in the description refers to kernel
126 * code (core code or drivers) that have called clk_enable() and not
127 * yet called clk_disable(); the usecount of parent clocks is also
128 * incremented by the clock code when clk_enable() is called on child
129 * clocks and decremented by the clock code when clk_disable() is
130 * called on child clocks.
131 *
132 * XXX @clkdm, @usecount, @children, @sibling should be marked for
133 * internal use only.
134 *
135 * @children and @sibling are used to optimize parent-to-child clock
136 * tree traversals. (child-to-parent traversals use @parent.)
137 *
138 * XXX The notion of the clock's current rate probably needs to be
139 * separated from the clock's target rate.
140 */
141 struct clk {
142 struct list_head node;
143 const struct clkops *ops;
144 const char *name;
145 struct clk *parent;
146 struct list_head children;
147 struct list_head sibling; /* node for children */
148 unsigned long rate;
149 void __iomem *enable_reg;
150 unsigned long (*recalc)(struct clk *);
151 int (*set_rate)(struct clk *, unsigned long);
152 long (*round_rate)(struct clk *, unsigned long);
153 void (*init)(struct clk *);
154 u8 enable_bit;
155 s8 usecount;
156 u8 fixed_div;
157 u8 flags;
158 u8 rate_offset;
159 u8 src_offset;
160 #if defined(CONFIG_PM_DEBUG) && defined(CONFIG_DEBUG_FS)
161 struct dentry *dent; /* For visible tree hierarchy */
162 #endif
163 };
165 struct clk_functions {
166 int (*clk_enable)(struct clk *clk);
167 void (*clk_disable)(struct clk *clk);
168 long (*clk_round_rate)(struct clk *clk, unsigned long rate);
169 int (*clk_set_rate)(struct clk *clk, unsigned long rate);
170 int (*clk_set_parent)(struct clk *clk, struct clk *parent);
171 void (*clk_allow_idle)(struct clk *clk);
172 void (*clk_deny_idle)(struct clk *clk);
173 void (*clk_disable_unused)(struct clk *clk);
174 };
176 extern int mpurate;
178 extern int clk_init(struct clk_functions *custom_clocks);
179 extern void clk_preinit(struct clk *clk);
180 extern int clk_register(struct clk *clk);
181 extern void clk_reparent(struct clk *child, struct clk *parent);
182 extern void clk_unregister(struct clk *clk);
183 extern void propagate_rate(struct clk *clk);
184 extern void recalculate_root_clocks(void);
185 extern unsigned long followparent_recalc(struct clk *clk);
186 extern void clk_enable_init_clocks(void);
187 unsigned long omap_fixed_divisor_recalc(struct clk *clk);
188 extern struct clk *omap_clk_get_by_name(const char *name);
189 extern int omap_clk_enable_autoidle_all(void);
190 extern int omap_clk_disable_autoidle_all(void);
192 extern const struct clkops clkops_null;
194 extern struct clk dummy_ck;
196 int omap1_clk_init(void);
197 void omap1_clk_late_init(void);
198 extern int omap1_clk_enable(struct clk *clk);
199 extern void omap1_clk_disable(struct clk *clk);
200 extern long omap1_clk_round_rate(struct clk *clk, unsigned long rate);
201 extern int omap1_clk_set_rate(struct clk *clk, unsigned long rate);
202 extern unsigned long omap1_ckctl_recalc(struct clk *clk);
203 extern int omap1_set_sossi_rate(struct clk *clk, unsigned long rate);
204 extern unsigned long omap1_sossi_recalc(struct clk *clk);
205 extern unsigned long omap1_ckctl_recalc_dsp_domain(struct clk *clk);
206 extern int omap1_clk_set_rate_dsp_domain(struct clk *clk, unsigned long rate);
207 extern int omap1_set_uart_rate(struct clk *clk, unsigned long rate);
208 extern unsigned long omap1_uart_recalc(struct clk *clk);
209 extern int omap1_set_ext_clk_rate(struct clk *clk, unsigned long rate);
210 extern long omap1_round_ext_clk_rate(struct clk *clk, unsigned long rate);
211 extern void omap1_init_ext_clk(struct clk *clk);
212 extern int omap1_select_table_rate(struct clk *clk, unsigned long rate);
213 extern long omap1_round_to_table_rate(struct clk *clk, unsigned long rate);
214 extern int omap1_clk_set_rate_ckctl_arm(struct clk *clk, unsigned long rate);
215 extern long omap1_clk_round_rate_ckctl_arm(struct clk *clk, unsigned long rate);
216 extern unsigned long omap1_watchdog_recalc(struct clk *clk);
218 #ifdef CONFIG_OMAP_RESET_CLOCKS
219 extern void omap1_clk_disable_unused(struct clk *clk);
220 #else
221 #define omap1_clk_disable_unused NULL
222 #endif
224 struct uart_clk {
225 struct clk clk;
226 unsigned long sysc_addr;
227 };
229 /* Provide a method for preventing idling some ARM IDLECT clocks */
230 struct arm_idlect1_clk {
231 struct clk clk;
232 unsigned long no_idle_count;
233 __u8 idlect_shift;
234 };
236 /* ARM_CKCTL bit shifts */
237 #define CKCTL_PERDIV_OFFSET 0
238 #define CKCTL_LCDDIV_OFFSET 2
239 #define CKCTL_ARMDIV_OFFSET 4
240 #define CKCTL_DSPDIV_OFFSET 6
241 #define CKCTL_TCDIV_OFFSET 8
242 #define CKCTL_DSPMMUDIV_OFFSET 10
243 /*#define ARM_TIMXO 12*/
244 #define EN_DSPCK 13
245 /*#define ARM_INTHCK_SEL 14*/ /* Divide-by-2 for mpu inth_ck */
246 /* DSP_CKCTL bit shifts */
247 #define CKCTL_DSPPERDIV_OFFSET 0
249 /* ARM_IDLECT2 bit shifts */
250 #define EN_WDTCK 0
251 #define EN_XORPCK 1
252 #define EN_PERCK 2
253 #define EN_LCDCK 3
254 #define EN_LBCK 4 /* Not on 1610/1710 */
255 /*#define EN_HSABCK 5*/
256 #define EN_APICK 6
257 #define EN_TIMCK 7
258 #define DMACK_REQ 8
259 #define EN_GPIOCK 9 /* Not on 1610/1710 */
260 /*#define EN_LBFREECK 10*/
261 #define EN_CKOUT_ARM 11
263 /* ARM_IDLECT3 bit shifts */
264 #define EN_OCPI_CK 0
265 #define EN_TC1_CK 2
266 #define EN_TC2_CK 4
268 /* DSP_IDLECT2 bit shifts (0,1,2 are same as for ARM_IDLECT2) */
269 #define EN_DSPTIMCK 5
271 /* Various register defines for clock controls scattered around OMAP chip */
272 #define SDW_MCLK_INV_BIT 2 /* In ULPD_CLKC_CTRL */
273 #define USB_MCLK_EN_BIT 4 /* In ULPD_CLKC_CTRL */
274 #define USB_HOST_HHC_UHOST_EN 9 /* In MOD_CONF_CTRL_0 */
275 #define SWD_ULPD_PLL_CLK_REQ 1 /* In SWD_CLK_DIV_CTRL_SEL */
276 #define COM_ULPD_PLL_CLK_REQ 1 /* In COM_CLK_DIV_CTRL_SEL */
277 #define SWD_CLK_DIV_CTRL_SEL 0xfffe0874
278 #define COM_CLK_DIV_CTRL_SEL 0xfffe0878
279 #define SOFT_REQ_REG 0xfffe0834
280 #define SOFT_REQ_REG2 0xfffe0880
282 extern __u32 arm_idlect1_mask;
283 extern struct clk *api_ck_p, *ck_dpll1_p, *ck_ref_p;
285 extern const struct clkops clkops_dspck;
286 extern const struct clkops clkops_dummy;
287 extern const struct clkops clkops_uart_16xx;
288 extern const struct clkops clkops_generic;
290 /* used for passing SoC type to omap1_{select,round_to}_table_rate() */
291 extern u32 cpu_mask;
293 #endif