1 /*
2 * DPLL + CORE_CLK composite clock functions
3 *
4 * Copyright (C) 2005-2008 Texas Instruments, Inc.
5 * Copyright (C) 2004-2010 Nokia Corporation
6 *
7 * Contacts:
8 * Richard Woodruff <r-woodruff2@ti.com>
9 * Paul Walmsley
10 *
11 * Based on earlier work by Tuukka Tikkanen, Tony Lindgren,
12 * Gordon McNutt and RidgeRun, Inc.
13 *
14 * This program is free software; you can redistribute it and/or modify
15 * it under the terms of the GNU General Public License version 2 as
16 * published by the Free Software Foundation.
17 *
18 * XXX The DPLL and CORE clocks should be split into two separate clock
19 * types.
20 */
21 #undef DEBUG
23 #include <linux/kernel.h>
24 #include <linux/errno.h>
25 #include <linux/clk.h>
26 #include <linux/io.h>
28 #include "clock.h"
29 #include "clock2xxx.h"
30 #include "opp2xxx.h"
31 #include "cm2xxx.h"
32 #include "cm-regbits-24xx.h"
33 #include "sdrc.h"
34 #include "sram.h"
36 /* #define DOWN_VARIABLE_DPLL 1 */ /* Experimental */
38 /*
39 * dpll_core_ck: pointer to the combined dpll_ck + core_ck on OMAP2xxx
40 * (currently defined as "dpll_ck" in the OMAP2xxx clock tree). Set
41 * during dpll_ck init and used later by omap2xxx_clk_get_core_rate().
42 */
43 static struct clk_hw_omap *dpll_core_ck;
45 /**
46 * omap2xxx_clk_get_core_rate - return the CORE_CLK rate
47 *
48 * Returns the CORE_CLK rate. CORE_CLK can have one of three rate
49 * sources on OMAP2xxx: the DPLL CLKOUT rate, DPLL CLKOUTX2, or 32KHz
50 * (the latter is unusual). This currently should be called with
51 * struct clk *dpll_ck, which is a composite clock of dpll_ck and
52 * core_ck.
53 */
54 unsigned long omap2xxx_clk_get_core_rate(void)
55 {
56 long long core_clk;
57 u32 v;
59 WARN_ON(!dpll_core_ck);
61 core_clk = omap2_get_dpll_rate(dpll_core_ck);
63 v = omap2_cm_read_mod_reg(PLL_MOD, CM_CLKSEL2);
64 v &= OMAP24XX_CORE_CLK_SRC_MASK;
66 if (v == CORE_CLK_SRC_32K)
67 core_clk = 32768;
68 else
69 core_clk *= v;
71 return core_clk;
72 }
74 /*
75 * Uses the current prcm set to tell if a rate is valid.
76 * You can go slower, but not faster within a given rate set.
77 */
78 static long omap2_dpllcore_round_rate(unsigned long target_rate)
79 {
80 u32 high, low, core_clk_src;
82 core_clk_src = omap2_cm_read_mod_reg(PLL_MOD, CM_CLKSEL2);
83 core_clk_src &= OMAP24XX_CORE_CLK_SRC_MASK;
85 if (core_clk_src == CORE_CLK_SRC_DPLL) { /* DPLL clockout */
86 high = curr_prcm_set->dpll_speed * 2;
87 low = curr_prcm_set->dpll_speed;
88 } else { /* DPLL clockout x 2 */
89 high = curr_prcm_set->dpll_speed;
90 low = curr_prcm_set->dpll_speed / 2;
91 }
93 #ifdef DOWN_VARIABLE_DPLL
94 if (target_rate > high)
95 return high;
96 else
97 return target_rate;
98 #else
99 if (target_rate > low)
100 return high;
101 else
102 return low;
103 #endif
105 }
107 unsigned long omap2_dpllcore_recalc(struct clk_hw *hw,
108 unsigned long parent_rate)
109 {
110 return omap2xxx_clk_get_core_rate();
111 }
113 int omap2_reprogram_dpllcore(struct clk_hw *hw, unsigned long rate,
114 unsigned long parent_rate)
115 {
116 struct clk_hw_omap *clk = to_clk_hw_omap(hw);
117 u32 cur_rate, low, mult, div, valid_rate, done_rate;
118 u32 bypass = 0;
119 struct prcm_config tmpset;
120 const struct dpll_data *dd;
122 cur_rate = omap2xxx_clk_get_core_rate();
123 mult = omap2_cm_read_mod_reg(PLL_MOD, CM_CLKSEL2);
124 mult &= OMAP24XX_CORE_CLK_SRC_MASK;
126 if ((rate == (cur_rate / 2)) && (mult == 2)) {
127 omap2xxx_sdrc_reprogram(CORE_CLK_SRC_DPLL, 1);
128 } else if ((rate == (cur_rate * 2)) && (mult == 1)) {
129 omap2xxx_sdrc_reprogram(CORE_CLK_SRC_DPLL_X2, 1);
130 } else if (rate != cur_rate) {
131 valid_rate = omap2_dpllcore_round_rate(rate);
132 if (valid_rate != rate)
133 return -EINVAL;
135 if (mult == 1)
136 low = curr_prcm_set->dpll_speed;
137 else
138 low = curr_prcm_set->dpll_speed / 2;
140 dd = clk->dpll_data;
141 if (!dd)
142 return -EINVAL;
144 tmpset.cm_clksel1_pll = __raw_readl(dd->mult_div1_reg);
145 tmpset.cm_clksel1_pll &= ~(dd->mult_mask |
146 dd->div1_mask);
147 div = ((curr_prcm_set->xtal_speed / 1000000) - 1);
148 tmpset.cm_clksel2_pll = omap2_cm_read_mod_reg(PLL_MOD, CM_CLKSEL2);
149 tmpset.cm_clksel2_pll &= ~OMAP24XX_CORE_CLK_SRC_MASK;
150 if (rate > low) {
151 tmpset.cm_clksel2_pll |= CORE_CLK_SRC_DPLL_X2;
152 mult = ((rate / 2) / 1000000);
153 done_rate = CORE_CLK_SRC_DPLL_X2;
154 } else {
155 tmpset.cm_clksel2_pll |= CORE_CLK_SRC_DPLL;
156 mult = (rate / 1000000);
157 done_rate = CORE_CLK_SRC_DPLL;
158 }
159 tmpset.cm_clksel1_pll |= (div << __ffs(dd->mult_mask));
160 tmpset.cm_clksel1_pll |= (mult << __ffs(dd->div1_mask));
162 /* Worst case */
163 tmpset.base_sdrc_rfr = SDRC_RFR_CTRL_BYPASS;
165 if (rate == curr_prcm_set->xtal_speed) /* If asking for 1-1 */
166 bypass = 1;
168 /* For omap2xxx_sdrc_init_params() */
169 omap2xxx_sdrc_reprogram(CORE_CLK_SRC_DPLL_X2, 1);
171 /* Force dll lock mode */
172 omap2_set_prcm(tmpset.cm_clksel1_pll, tmpset.base_sdrc_rfr,
173 bypass);
175 /* Errata: ret dll entry state */
176 omap2xxx_sdrc_init_params(omap2xxx_sdrc_dll_is_unlocked());
177 omap2xxx_sdrc_reprogram(done_rate, 0);
178 }
180 return 0;
181 }
183 /**
184 * omap2xxx_clkt_dpllcore_init - clk init function for dpll_ck
185 * @clk: struct clk *dpll_ck
186 *
187 * Store a local copy of @clk in dpll_core_ck so other code can query
188 * the core rate without having to clk_get(), which can sleep. Must
189 * only be called once. No return value. XXX If the clock
190 * registration process is ever changed such that dpll_ck is no longer
191 * statically defined, this code may need to change to increment some
192 * kind of use count on dpll_ck.
193 */
194 void omap2xxx_clkt_dpllcore_init(struct clk_hw *hw)
195 {
196 WARN(dpll_core_ck, "dpll_core_ck already set - should never happen");
197 dpll_core_ck = to_clk_hw_omap(hw);
198 }