]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - arch/arm/mach-omap2/omap_device.c
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
[android-sdk/kernel-video.git] / arch / arm / mach-omap2 / omap_device.c
1 /*
2  * omap_device implementation
3  *
4  * Copyright (C) 2009-2010 Nokia Corporation
5  * Paul Walmsley, Kevin Hilman
6  *
7  * Developed in collaboration with (alphabetical order): Benoit
8  * Cousson, Thara Gopinath, Tony Lindgren, Rajendra Nayak, Vikram
9  * Pandita, Sakari Poussa, Anand Sawant, Santosh Shilimkar, Richard
10  * Woodruff
11  *
12  * This program is free software; you can redistribute it and/or modify
13  * it under the terms of the GNU General Public License version 2 as
14  * published by the Free Software Foundation.
15  *
16  * This code provides a consistent interface for OMAP device drivers
17  * to control power management and interconnect properties of their
18  * devices.
19  *
20  * In the medium- to long-term, this code should either be
21  * a) implemented via arch-specific pointers in platform_data
22  * or
23  * b) implemented as a proper omap_bus/omap_device in Linux, no more
24  *    platform_data func pointers
25  *
26  *
27  * Guidelines for usage by driver authors:
28  *
29  * 1. These functions are intended to be used by device drivers via
30  * function pointers in struct platform_data.  As an example,
31  * omap_device_enable() should be passed to the driver as
32  *
33  * struct foo_driver_platform_data {
34  * ...
35  *      int (*device_enable)(struct platform_device *pdev);
36  * ...
37  * }
38  *
39  * Note that the generic "device_enable" name is used, rather than
40  * "omap_device_enable".  This is so other architectures can pass in their
41  * own enable/disable functions here.
42  *
43  * This should be populated during device setup:
44  *
45  * ...
46  * pdata->device_enable = omap_device_enable;
47  * ...
48  *
49  * 2. Drivers should first check to ensure the function pointer is not null
50  * before calling it, as in:
51  *
52  * if (pdata->device_enable)
53  *     pdata->device_enable(pdev);
54  *
55  * This allows other architectures that don't use similar device_enable()/
56  * device_shutdown() functions to execute normally.
57  *
58  * ...
59  *
60  * Suggested usage by device drivers:
61  *
62  * During device initialization:
63  * device_enable()
64  *
65  * During device idle:
66  * (save remaining device context if necessary)
67  * device_idle();
68  *
69  * During device resume:
70  * device_enable();
71  * (restore context if necessary)
72  *
73  * During device shutdown:
74  * device_shutdown()
75  * (device must be reinitialized at this point to use it again)
76  *
77  */
78 #undef DEBUG
80 #include <linux/kernel.h>
81 #include <linux/export.h>
82 #include <linux/platform_device.h>
83 #include <linux/slab.h>
84 #include <linux/err.h>
85 #include <linux/io.h>
86 #include <linux/clk.h>
87 #include <linux/clkdev.h>
88 #include <linux/pm_runtime.h>
89 #include <linux/of.h>
90 #include <linux/notifier.h>
92 #include "omap_device.h"
93 #include "omap_hwmod.h"
95 /* These parameters are passed to _omap_device_{de,}activate() */
96 #define USE_WAKEUP_LAT                  0
97 #define IGNORE_WAKEUP_LAT               1
99 static int omap_early_device_register(struct platform_device *pdev);
101 static struct omap_device_pm_latency omap_default_latency[] = {
102         {
103                 .deactivate_func = omap_device_idle_hwmods,
104                 .activate_func   = omap_device_enable_hwmods,
105                 .flags = OMAP_DEVICE_LATENCY_AUTO_ADJUST,
106         }
107 };
109 /* Private functions */
111 /**
112  * _omap_device_activate - increase device readiness
113  * @od: struct omap_device *
114  * @ignore_lat: increase to latency target (0) or full readiness (1)?
115  *
116  * Increase readiness of omap_device @od (thus decreasing device
117  * wakeup latency, but consuming more power).  If @ignore_lat is
118  * IGNORE_WAKEUP_LAT, make the omap_device fully active.  Otherwise,
119  * if @ignore_lat is USE_WAKEUP_LAT, and the device's maximum wakeup
120  * latency is greater than the requested maximum wakeup latency, step
121  * backwards in the omap_device_pm_latency table to ensure the
122  * device's maximum wakeup latency is less than or equal to the
123  * requested maximum wakeup latency.  Returns 0.
124  */
125 static int _omap_device_activate(struct omap_device *od, u8 ignore_lat)
127         struct timespec a, b, c;
129         dev_dbg(&od->pdev->dev, "omap_device: activating\n");
131         while (od->pm_lat_level > 0) {
132                 struct omap_device_pm_latency *odpl;
133                 unsigned long long act_lat = 0;
135                 od->pm_lat_level--;
137                 odpl = od->pm_lats + od->pm_lat_level;
139                 if (!ignore_lat &&
140                     (od->dev_wakeup_lat <= od->_dev_wakeup_lat_limit))
141                         break;
143                 read_persistent_clock(&a);
145                 /* XXX check return code */
146                 odpl->activate_func(od);
148                 read_persistent_clock(&b);
150                 c = timespec_sub(b, a);
151                 act_lat = timespec_to_ns(&c);
153                 dev_dbg(&od->pdev->dev,
154                         "omap_device: pm_lat %d: activate: elapsed time %llu nsec\n",
155                         od->pm_lat_level, act_lat);
157                 if (act_lat > odpl->activate_lat) {
158                         odpl->activate_lat_worst = act_lat;
159                         if (odpl->flags & OMAP_DEVICE_LATENCY_AUTO_ADJUST) {
160                                 odpl->activate_lat = act_lat;
161                                 dev_dbg(&od->pdev->dev,
162                                         "new worst case activate latency %d: %llu\n",
163                                         od->pm_lat_level, act_lat);
164                         } else
165                                 dev_warn(&od->pdev->dev,
166                                          "activate latency %d higher than expected. (%llu > %d)\n",
167                                          od->pm_lat_level, act_lat,
168                                          odpl->activate_lat);
169                 }
171                 od->dev_wakeup_lat -= odpl->activate_lat;
172         }
174         return 0;
177 /**
178  * _omap_device_deactivate - decrease device readiness
179  * @od: struct omap_device *
180  * @ignore_lat: decrease to latency target (0) or full inactivity (1)?
181  *
182  * Decrease readiness of omap_device @od (thus increasing device
183  * wakeup latency, but conserving power).  If @ignore_lat is
184  * IGNORE_WAKEUP_LAT, make the omap_device fully inactive.  Otherwise,
185  * if @ignore_lat is USE_WAKEUP_LAT, and the device's maximum wakeup
186  * latency is less than the requested maximum wakeup latency, step
187  * forwards in the omap_device_pm_latency table to ensure the device's
188  * maximum wakeup latency is less than or equal to the requested
189  * maximum wakeup latency.  Returns 0.
190  */
191 static int _omap_device_deactivate(struct omap_device *od, u8 ignore_lat)
193         struct timespec a, b, c;
195         dev_dbg(&od->pdev->dev, "omap_device: deactivating\n");
197         while (od->pm_lat_level < od->pm_lats_cnt) {
198                 struct omap_device_pm_latency *odpl;
199                 unsigned long long deact_lat = 0;
201                 odpl = od->pm_lats + od->pm_lat_level;
203                 if (!ignore_lat &&
204                     ((od->dev_wakeup_lat + odpl->activate_lat) >
205                      od->_dev_wakeup_lat_limit))
206                         break;
208                 read_persistent_clock(&a);
210                 /* XXX check return code */
211                 odpl->deactivate_func(od);
213                 read_persistent_clock(&b);
215                 c = timespec_sub(b, a);
216                 deact_lat = timespec_to_ns(&c);
218                 dev_dbg(&od->pdev->dev,
219                         "omap_device: pm_lat %d: deactivate: elapsed time %llu nsec\n",
220                         od->pm_lat_level, deact_lat);
222                 if (deact_lat > odpl->deactivate_lat) {
223                         odpl->deactivate_lat_worst = deact_lat;
224                         if (odpl->flags & OMAP_DEVICE_LATENCY_AUTO_ADJUST) {
225                                 odpl->deactivate_lat = deact_lat;
226                                 dev_dbg(&od->pdev->dev,
227                                         "new worst case deactivate latency %d: %llu\n",
228                                         od->pm_lat_level, deact_lat);
229                         } else
230                                 dev_warn(&od->pdev->dev,
231                                          "deactivate latency %d higher than expected. (%llu > %d)\n",
232                                          od->pm_lat_level, deact_lat,
233                                          odpl->deactivate_lat);
234                 }
236                 od->dev_wakeup_lat += odpl->activate_lat;
238                 od->pm_lat_level++;
239         }
241         return 0;
244 static void _add_clkdev(struct omap_device *od, const char *clk_alias,
245                        const char *clk_name)
247         struct clk *r;
248         struct clk_lookup *l;
250         if (!clk_alias || !clk_name)
251                 return;
253         dev_dbg(&od->pdev->dev, "Creating %s -> %s\n", clk_alias, clk_name);
255         r = clk_get_sys(dev_name(&od->pdev->dev), clk_alias);
256         if (!IS_ERR(r)) {
257                 dev_warn(&od->pdev->dev,
258                          "alias %s already exists\n", clk_alias);
259                 clk_put(r);
260                 return;
261         }
263         r = clk_get(NULL, clk_name);
264         if (IS_ERR(r)) {
265                 dev_err(&od->pdev->dev,
266                         "clk_get for %s failed\n", clk_name);
267                 return;
268         }
270         l = clkdev_alloc(r, clk_alias, dev_name(&od->pdev->dev));
271         if (!l) {
272                 dev_err(&od->pdev->dev,
273                         "clkdev_alloc for %s failed\n", clk_alias);
274                 return;
275         }
277         clkdev_add(l);
280 /**
281  * _add_hwmod_clocks_clkdev - Add clkdev entry for hwmod optional clocks
282  * and main clock
283  * @od: struct omap_device *od
284  * @oh: struct omap_hwmod *oh
285  *
286  * For the main clock and every optional clock present per hwmod per
287  * omap_device, this function adds an entry in the clkdev table of the
288  * form <dev-id=dev_name, con-id=role> if it does not exist already.
289  *
290  * The function is called from inside omap_device_build_ss(), after
291  * omap_device_register.
292  *
293  * This allows drivers to get a pointer to its optional clocks based on its role
294  * by calling clk_get(<dev*>, <role>).
295  * In the case of the main clock, a "fck" alias is used.
296  *
297  * No return value.
298  */
299 static void _add_hwmod_clocks_clkdev(struct omap_device *od,
300                                      struct omap_hwmod *oh)
302         int i;
304         _add_clkdev(od, "fck", oh->main_clk);
306         for (i = 0; i < oh->opt_clks_cnt; i++)
307                 _add_clkdev(od, oh->opt_clks[i].role, oh->opt_clks[i].clk);
311 /**
312  * omap_device_build_from_dt - build an omap_device with multiple hwmods
313  * @pdev_name: name of the platform_device driver to use
314  * @pdev_id: this platform_device's connection ID
315  * @oh: ptr to the single omap_hwmod that backs this omap_device
316  * @pdata: platform_data ptr to associate with the platform_device
317  * @pdata_len: amount of memory pointed to by @pdata
318  * @pm_lats: pointer to a omap_device_pm_latency array for this device
319  * @pm_lats_cnt: ARRAY_SIZE() of @pm_lats
320  * @is_early_device: should the device be registered as an early device or not
321  *
322  * Function for building an omap_device already registered from device-tree
323  *
324  * Returns 0 or PTR_ERR() on error.
325  */
326 static int omap_device_build_from_dt(struct platform_device *pdev)
328         struct omap_hwmod **hwmods;
329         struct omap_device *od;
330         struct omap_hwmod *oh;
331         struct device_node *node = pdev->dev.of_node;
332         const char *oh_name;
333         int oh_cnt, i, ret = 0;
335         oh_cnt = of_property_count_strings(node, "ti,hwmods");
336         if (!oh_cnt || IS_ERR_VALUE(oh_cnt)) {
337                 dev_dbg(&pdev->dev, "No 'hwmods' to build omap_device\n");
338                 return -ENODEV;
339         }
341         hwmods = kzalloc(sizeof(struct omap_hwmod *) * oh_cnt, GFP_KERNEL);
342         if (!hwmods) {
343                 ret = -ENOMEM;
344                 goto odbfd_exit;
345         }
347         for (i = 0; i < oh_cnt; i++) {
348                 of_property_read_string_index(node, "ti,hwmods", i, &oh_name);
349                 oh = omap_hwmod_lookup(oh_name);
350                 if (!oh) {
351                         dev_err(&pdev->dev, "Cannot lookup hwmod '%s'\n",
352                                 oh_name);
353                         ret = -EINVAL;
354                         goto odbfd_exit1;
355                 }
356                 hwmods[i] = oh;
357         }
359         od = omap_device_alloc(pdev, hwmods, oh_cnt, NULL, 0);
360         if (!od) {
361                 dev_err(&pdev->dev, "Cannot allocate omap_device for :%s\n",
362                         oh_name);
363                 ret = PTR_ERR(od);
364                 goto odbfd_exit1;
365         }
367         /* Fix up missing resource names */
368         for (i = 0; i < pdev->num_resources; i++) {
369                 struct resource *r = &pdev->resource[i];
371                 if (r->name == NULL)
372                         r->name = dev_name(&pdev->dev);
373         }
375         pdev->dev.pm_domain = &omap_device_pm_domain;
377 odbfd_exit1:
378         kfree(hwmods);
379 odbfd_exit:
380         return ret;
383 static int _omap_device_notifier_call(struct notifier_block *nb,
384                                       unsigned long event, void *dev)
386         struct platform_device *pdev = to_platform_device(dev);
387         struct omap_device *od;
389         switch (event) {
390         case BUS_NOTIFY_DEL_DEVICE:
391                 if (pdev->archdata.od)
392                         omap_device_delete(pdev->archdata.od);
393                 break;
394         case BUS_NOTIFY_ADD_DEVICE:
395                 if (pdev->dev.of_node)
396                         omap_device_build_from_dt(pdev);
397                 /* fall through */
398         default:
399                 od = to_omap_device(pdev);
400                 if (od)
401                         od->_driver_status = event;
402         }
404         return NOTIFY_DONE;
408 /* Public functions for use by core code */
410 /**
411  * omap_device_get_context_loss_count - get lost context count
412  * @od: struct omap_device *
413  *
414  * Using the primary hwmod, query the context loss count for this
415  * device.
416  *
417  * Callers should consider context for this device lost any time this
418  * function returns a value different than the value the caller got
419  * the last time it called this function.
420  *
421  * If any hwmods exist for the omap_device assoiated with @pdev,
422  * return the context loss counter for that hwmod, otherwise return
423  * zero.
424  */
425 int omap_device_get_context_loss_count(struct platform_device *pdev)
427         struct omap_device *od;
428         u32 ret = 0;
430         od = to_omap_device(pdev);
432         if (od->hwmods_cnt)
433                 ret = omap_hwmod_get_context_loss_count(od->hwmods[0]);
435         return ret;
438 /**
439  * omap_device_count_resources - count number of struct resource entries needed
440  * @od: struct omap_device *
441  * @flags: Type of resources to include when counting (IRQ/DMA/MEM)
442  *
443  * Count the number of struct resource entries needed for this
444  * omap_device @od.  Used by omap_device_build_ss() to determine how
445  * much memory to allocate before calling
446  * omap_device_fill_resources().  Returns the count.
447  */
448 static int omap_device_count_resources(struct omap_device *od,
449                                        unsigned long flags)
451         int c = 0;
452         int i;
454         for (i = 0; i < od->hwmods_cnt; i++)
455                 c += omap_hwmod_count_resources(od->hwmods[i], flags);
457         pr_debug("omap_device: %s: counted %d total resources across %d hwmods\n",
458                  od->pdev->name, c, od->hwmods_cnt);
460         return c;
463 /**
464  * omap_device_fill_resources - fill in array of struct resource
465  * @od: struct omap_device *
466  * @res: pointer to an array of struct resource to be filled in
467  *
468  * Populate one or more empty struct resource pointed to by @res with
469  * the resource data for this omap_device @od.  Used by
470  * omap_device_build_ss() after calling omap_device_count_resources().
471  * Ideally this function would not be needed at all.  If omap_device
472  * replaces platform_device, then we can specify our own
473  * get_resource()/ get_irq()/etc functions that use the underlying
474  * omap_hwmod information.  Or if platform_device is extended to use
475  * subarchitecture-specific function pointers, the various
476  * platform_device functions can simply call omap_device internal
477  * functions to get device resources.  Hacking around the existing
478  * platform_device code wastes memory.  Returns 0.
479  */
480 static int omap_device_fill_resources(struct omap_device *od,
481                                       struct resource *res)
483         int i, r;
485         for (i = 0; i < od->hwmods_cnt; i++) {
486                 r = omap_hwmod_fill_resources(od->hwmods[i], res);
487                 res += r;
488         }
490         return 0;
493 /**
494  * _od_fill_dma_resources - fill in array of struct resource with dma resources
495  * @od: struct omap_device *
496  * @res: pointer to an array of struct resource to be filled in
497  *
498  * Populate one or more empty struct resource pointed to by @res with
499  * the dma resource data for this omap_device @od.  Used by
500  * omap_device_alloc() after calling omap_device_count_resources().
501  *
502  * Ideally this function would not be needed at all.  If we have
503  * mechanism to get dma resources from DT.
504  *
505  * Returns 0.
506  */
507 static int _od_fill_dma_resources(struct omap_device *od,
508                                       struct resource *res)
510         int i, r;
512         for (i = 0; i < od->hwmods_cnt; i++) {
513                 r = omap_hwmod_fill_dma_resources(od->hwmods[i], res);
514                 res += r;
515         }
517         return 0;
520 /**
521  * omap_device_alloc - allocate an omap_device
522  * @pdev: platform_device that will be included in this omap_device
523  * @oh: ptr to the single omap_hwmod that backs this omap_device
524  * @pdata: platform_data ptr to associate with the platform_device
525  * @pdata_len: amount of memory pointed to by @pdata
526  * @pm_lats: pointer to a omap_device_pm_latency array for this device
527  * @pm_lats_cnt: ARRAY_SIZE() of @pm_lats
528  *
529  * Convenience function for allocating an omap_device structure and filling
530  * hwmods, resources and pm_latency attributes.
531  *
532  * Returns an struct omap_device pointer or ERR_PTR() on error;
533  */
534 struct omap_device *omap_device_alloc(struct platform_device *pdev,
535                                         struct omap_hwmod **ohs, int oh_cnt,
536                                         struct omap_device_pm_latency *pm_lats,
537                                         int pm_lats_cnt)
539         int ret = -ENOMEM;
540         struct omap_device *od;
541         struct resource *res = NULL;
542         int i, res_count;
543         struct omap_hwmod **hwmods;
545         od = kzalloc(sizeof(struct omap_device), GFP_KERNEL);
546         if (!od) {
547                 ret = -ENOMEM;
548                 goto oda_exit1;
549         }
550         od->hwmods_cnt = oh_cnt;
552         hwmods = kmemdup(ohs, sizeof(struct omap_hwmod *) * oh_cnt, GFP_KERNEL);
553         if (!hwmods)
554                 goto oda_exit2;
556         od->hwmods = hwmods;
557         od->pdev = pdev;
559         /*
560          * Non-DT Boot:
561          *   Here, pdev->num_resources = 0, and we should get all the
562          *   resources from hwmod.
563          *
564          * DT Boot:
565          *   OF framework will construct the resource structure (currently
566          *   does for MEM & IRQ resource) and we should respect/use these
567          *   resources, killing hwmod dependency.
568          *   If pdev->num_resources > 0, we assume that MEM & IRQ resources
569          *   have been allocated by OF layer already (through DTB).
570          *   As preparation for the future we examine the OF provided resources
571          *   to see if we have DMA resources provided already. In this case
572          *   there is no need to update the resources for the device, we use the
573          *   OF provided ones.
574          *
575          * TODO: Once DMA resource is available from OF layer, we should
576          *   kill filling any resources from hwmod.
577          */
578         if (!pdev->num_resources) {
579                 /* Count all resources for the device */
580                 res_count = omap_device_count_resources(od, IORESOURCE_IRQ |
581                                                             IORESOURCE_DMA |
582                                                             IORESOURCE_MEM);
583         } else {
584                 /* Take a look if we already have DMA resource via DT */
585                 for (i = 0; i < pdev->num_resources; i++) {
586                         struct resource *r = &pdev->resource[i];
588                         /* We have it, no need to touch the resources */
589                         if (r->flags == IORESOURCE_DMA)
590                                 goto have_everything;
591                 }
592                 /* Count only DMA resources for the device */
593                 res_count = omap_device_count_resources(od, IORESOURCE_DMA);
594                 /* The device has no DMA resource, no need for update */
595                 if (!res_count)
596                         goto have_everything;
598                 res_count += pdev->num_resources;
599         }
601         /* Allocate resources memory to account for new resources */
602         res = kzalloc(sizeof(struct resource) * res_count, GFP_KERNEL);
603         if (!res)
604                 goto oda_exit3;
606         if (!pdev->num_resources) {
607                 dev_dbg(&pdev->dev, "%s: using %d resources from hwmod\n",
608                         __func__, res_count);
609                 omap_device_fill_resources(od, res);
610         } else {
611                 dev_dbg(&pdev->dev,
612                         "%s: appending %d DMA resources from hwmod\n",
613                         __func__, res_count - pdev->num_resources);
614                 memcpy(res, pdev->resource,
615                        sizeof(struct resource) * pdev->num_resources);
616                 _od_fill_dma_resources(od, &res[pdev->num_resources]);
617         }
619         ret = platform_device_add_resources(pdev, res, res_count);
620         kfree(res);
622         if (ret)
623                 goto oda_exit3;
625 have_everything:
626         if (!pm_lats) {
627                 pm_lats = omap_default_latency;
628                 pm_lats_cnt = ARRAY_SIZE(omap_default_latency);
629         }
631         od->pm_lats_cnt = pm_lats_cnt;
632         od->pm_lats = kmemdup(pm_lats,
633                         sizeof(struct omap_device_pm_latency) * pm_lats_cnt,
634                         GFP_KERNEL);
635         if (!od->pm_lats)
636                 goto oda_exit3;
638         pdev->archdata.od = od;
640         for (i = 0; i < oh_cnt; i++) {
641                 hwmods[i]->od = od;
642                 _add_hwmod_clocks_clkdev(od, hwmods[i]);
643         }
645         return od;
647 oda_exit3:
648         kfree(hwmods);
649 oda_exit2:
650         kfree(od);
651 oda_exit1:
652         dev_err(&pdev->dev, "omap_device: build failed (%d)\n", ret);
654         return ERR_PTR(ret);
657 void omap_device_delete(struct omap_device *od)
659         if (!od)
660                 return;
662         od->pdev->archdata.od = NULL;
663         kfree(od->pm_lats);
664         kfree(od->hwmods);
665         kfree(od);
668 /**
669  * omap_device_build - build and register an omap_device with one omap_hwmod
670  * @pdev_name: name of the platform_device driver to use
671  * @pdev_id: this platform_device's connection ID
672  * @oh: ptr to the single omap_hwmod that backs this omap_device
673  * @pdata: platform_data ptr to associate with the platform_device
674  * @pdata_len: amount of memory pointed to by @pdata
675  * @pm_lats: pointer to a omap_device_pm_latency array for this device
676  * @pm_lats_cnt: ARRAY_SIZE() of @pm_lats
677  * @is_early_device: should the device be registered as an early device or not
678  *
679  * Convenience function for building and registering a single
680  * omap_device record, which in turn builds and registers a
681  * platform_device record.  See omap_device_build_ss() for more
682  * information.  Returns ERR_PTR(-EINVAL) if @oh is NULL; otherwise,
683  * passes along the return value of omap_device_build_ss().
684  */
685 struct platform_device __init *omap_device_build(const char *pdev_name, int pdev_id,
686                                       struct omap_hwmod *oh, void *pdata,
687                                       int pdata_len,
688                                       struct omap_device_pm_latency *pm_lats,
689                                       int pm_lats_cnt, int is_early_device)
691         struct omap_hwmod *ohs[] = { oh };
693         if (!oh)
694                 return ERR_PTR(-EINVAL);
696         return omap_device_build_ss(pdev_name, pdev_id, ohs, 1, pdata,
697                                     pdata_len, pm_lats, pm_lats_cnt,
698                                     is_early_device);
701 /**
702  * omap_device_build_ss - build and register an omap_device with multiple hwmods
703  * @pdev_name: name of the platform_device driver to use
704  * @pdev_id: this platform_device's connection ID
705  * @oh: ptr to the single omap_hwmod that backs this omap_device
706  * @pdata: platform_data ptr to associate with the platform_device
707  * @pdata_len: amount of memory pointed to by @pdata
708  * @pm_lats: pointer to a omap_device_pm_latency array for this device
709  * @pm_lats_cnt: ARRAY_SIZE() of @pm_lats
710  * @is_early_device: should the device be registered as an early device or not
711  *
712  * Convenience function for building and registering an omap_device
713  * subsystem record.  Subsystem records consist of multiple
714  * omap_hwmods.  This function in turn builds and registers a
715  * platform_device record.  Returns an ERR_PTR() on error, or passes
716  * along the return value of omap_device_register().
717  */
718 struct platform_device __init *omap_device_build_ss(const char *pdev_name, int pdev_id,
719                                          struct omap_hwmod **ohs, int oh_cnt,
720                                          void *pdata, int pdata_len,
721                                          struct omap_device_pm_latency *pm_lats,
722                                          int pm_lats_cnt, int is_early_device)
724         int ret = -ENOMEM;
725         struct platform_device *pdev;
726         struct omap_device *od;
728         if (!ohs || oh_cnt == 0 || !pdev_name)
729                 return ERR_PTR(-EINVAL);
731         if (!pdata && pdata_len > 0)
732                 return ERR_PTR(-EINVAL);
734         pdev = platform_device_alloc(pdev_name, pdev_id);
735         if (!pdev) {
736                 ret = -ENOMEM;
737                 goto odbs_exit;
738         }
740         /* Set the dev_name early to allow dev_xxx in omap_device_alloc */
741         if (pdev->id != -1)
742                 dev_set_name(&pdev->dev, "%s.%d", pdev->name,  pdev->id);
743         else
744                 dev_set_name(&pdev->dev, "%s", pdev->name);
746         od = omap_device_alloc(pdev, ohs, oh_cnt, pm_lats, pm_lats_cnt);
747         if (IS_ERR(od))
748                 goto odbs_exit1;
750         ret = platform_device_add_data(pdev, pdata, pdata_len);
751         if (ret)
752                 goto odbs_exit2;
754         if (is_early_device)
755                 ret = omap_early_device_register(pdev);
756         else
757                 ret = omap_device_register(pdev);
758         if (ret)
759                 goto odbs_exit2;
761         return pdev;
763 odbs_exit2:
764         omap_device_delete(od);
765 odbs_exit1:
766         platform_device_put(pdev);
767 odbs_exit:
769         pr_err("omap_device: %s: build failed (%d)\n", pdev_name, ret);
771         return ERR_PTR(ret);
774 /**
775  * omap_early_device_register - register an omap_device as an early platform
776  * device.
777  * @od: struct omap_device * to register
778  *
779  * Register the omap_device structure.  This currently just calls
780  * platform_early_add_device() on the underlying platform_device.
781  * Returns 0 by default.
782  */
783 static int __init omap_early_device_register(struct platform_device *pdev)
785         struct platform_device *devices[1];
787         devices[0] = pdev;
788         early_platform_add_devices(devices, 1);
789         return 0;
792 #ifdef CONFIG_PM_RUNTIME
793 static int _od_runtime_suspend(struct device *dev)
795         struct platform_device *pdev = to_platform_device(dev);
796         int ret;
798         ret = pm_generic_runtime_suspend(dev);
800         if (!ret)
801                 omap_device_idle(pdev);
803         return ret;
806 static int _od_runtime_idle(struct device *dev)
808         return pm_generic_runtime_idle(dev);
811 static int _od_runtime_resume(struct device *dev)
813         struct platform_device *pdev = to_platform_device(dev);
815         omap_device_enable(pdev);
817         return pm_generic_runtime_resume(dev);
819 #endif
821 #ifdef CONFIG_SUSPEND
822 static int _od_suspend_noirq(struct device *dev)
824         struct platform_device *pdev = to_platform_device(dev);
825         struct omap_device *od = to_omap_device(pdev);
826         int ret;
828         /* Don't attempt late suspend on a driver that is not bound */
829         if (od->_driver_status != BUS_NOTIFY_BOUND_DRIVER)
830                 return 0;
832         ret = pm_generic_suspend_noirq(dev);
834         if (!ret && !pm_runtime_status_suspended(dev)) {
835                 if (pm_generic_runtime_suspend(dev) == 0) {
836                         omap_device_idle(pdev);
837                         od->flags |= OMAP_DEVICE_SUSPENDED;
838                 }
839         }
841         return ret;
844 static int _od_resume_noirq(struct device *dev)
846         struct platform_device *pdev = to_platform_device(dev);
847         struct omap_device *od = to_omap_device(pdev);
849         if ((od->flags & OMAP_DEVICE_SUSPENDED) &&
850             !pm_runtime_status_suspended(dev)) {
851                 od->flags &= ~OMAP_DEVICE_SUSPENDED;
852                 omap_device_enable(pdev);
853                 pm_generic_runtime_resume(dev);
854         }
856         return pm_generic_resume_noirq(dev);
858 #else
859 #define _od_suspend_noirq NULL
860 #define _od_resume_noirq NULL
861 #endif
863 struct dev_pm_domain omap_device_pm_domain = {
864         .ops = {
865                 SET_RUNTIME_PM_OPS(_od_runtime_suspend, _od_runtime_resume,
866                                    _od_runtime_idle)
867                 USE_PLATFORM_PM_SLEEP_OPS
868                 .suspend_noirq = _od_suspend_noirq,
869                 .resume_noirq = _od_resume_noirq,
870         }
871 };
873 /**
874  * omap_device_register - register an omap_device with one omap_hwmod
875  * @od: struct omap_device * to register
876  *
877  * Register the omap_device structure.  This currently just calls
878  * platform_device_register() on the underlying platform_device.
879  * Returns the return value of platform_device_register().
880  */
881 int omap_device_register(struct platform_device *pdev)
883         pr_debug("omap_device: %s: registering\n", pdev->name);
885         pdev->dev.pm_domain = &omap_device_pm_domain;
886         return platform_device_add(pdev);
890 /* Public functions for use by device drivers through struct platform_data */
892 /**
893  * omap_device_enable - fully activate an omap_device
894  * @od: struct omap_device * to activate
895  *
896  * Do whatever is necessary for the hwmods underlying omap_device @od
897  * to be accessible and ready to operate.  This generally involves
898  * enabling clocks, setting SYSCONFIG registers; and in the future may
899  * involve remuxing pins.  Device drivers should call this function
900  * (through platform_data function pointers) where they would normally
901  * enable clocks, etc.  Returns -EINVAL if called when the omap_device
902  * is already enabled, or passes along the return value of
903  * _omap_device_activate().
904  */
905 int omap_device_enable(struct platform_device *pdev)
907         int ret;
908         struct omap_device *od;
910         od = to_omap_device(pdev);
912         if (od->_state == OMAP_DEVICE_STATE_ENABLED) {
913                 dev_warn(&pdev->dev,
914                          "omap_device: %s() called from invalid state %d\n",
915                          __func__, od->_state);
916                 return -EINVAL;
917         }
919         /* Enable everything if we're enabling this device from scratch */
920         if (od->_state == OMAP_DEVICE_STATE_UNKNOWN)
921                 od->pm_lat_level = od->pm_lats_cnt;
923         ret = _omap_device_activate(od, IGNORE_WAKEUP_LAT);
925         od->dev_wakeup_lat = 0;
926         od->_dev_wakeup_lat_limit = UINT_MAX;
927         od->_state = OMAP_DEVICE_STATE_ENABLED;
929         return ret;
932 /**
933  * omap_device_idle - idle an omap_device
934  * @od: struct omap_device * to idle
935  *
936  * Idle omap_device @od by calling as many .deactivate_func() entries
937  * in the omap_device's pm_lats table as is possible without exceeding
938  * the device's maximum wakeup latency limit, pm_lat_limit.  Device
939  * drivers should call this function (through platform_data function
940  * pointers) where they would normally disable clocks after operations
941  * complete, etc..  Returns -EINVAL if the omap_device is not
942  * currently enabled, or passes along the return value of
943  * _omap_device_deactivate().
944  */
945 int omap_device_idle(struct platform_device *pdev)
947         int ret;
948         struct omap_device *od;
950         od = to_omap_device(pdev);
952         if (od->_state != OMAP_DEVICE_STATE_ENABLED) {
953                 dev_warn(&pdev->dev,
954                          "omap_device: %s() called from invalid state %d\n",
955                          __func__, od->_state);
956                 return -EINVAL;
957         }
959         ret = _omap_device_deactivate(od, USE_WAKEUP_LAT);
961         od->_state = OMAP_DEVICE_STATE_IDLE;
963         return ret;
966 /**
967  * omap_device_shutdown - shut down an omap_device
968  * @od: struct omap_device * to shut down
969  *
970  * Shut down omap_device @od by calling all .deactivate_func() entries
971  * in the omap_device's pm_lats table and then shutting down all of
972  * the underlying omap_hwmods.  Used when a device is being "removed"
973  * or a device driver is being unloaded.  Returns -EINVAL if the
974  * omap_device is not currently enabled or idle, or passes along the
975  * return value of _omap_device_deactivate().
976  */
977 int omap_device_shutdown(struct platform_device *pdev)
979         int ret, i;
980         struct omap_device *od;
982         od = to_omap_device(pdev);
984         if (od->_state != OMAP_DEVICE_STATE_ENABLED &&
985             od->_state != OMAP_DEVICE_STATE_IDLE) {
986                 dev_warn(&pdev->dev,
987                          "omap_device: %s() called from invalid state %d\n",
988                          __func__, od->_state);
989                 return -EINVAL;
990         }
992         ret = _omap_device_deactivate(od, IGNORE_WAKEUP_LAT);
994         for (i = 0; i < od->hwmods_cnt; i++)
995                 omap_hwmod_shutdown(od->hwmods[i]);
997         od->_state = OMAP_DEVICE_STATE_SHUTDOWN;
999         return ret;
1002 /**
1003  * omap_device_assert_hardreset - set a device's hardreset line
1004  * @pdev: struct platform_device * to reset
1005  * @name: const char * name of the reset line
1006  *
1007  * Set the hardreset line identified by @name on the IP blocks
1008  * associated with the hwmods backing the platform_device @pdev.  All
1009  * of the hwmods associated with @pdev must have the same hardreset
1010  * line linked to them for this to work.  Passes along the return value
1011  * of omap_hwmod_assert_hardreset() in the event of any failure, or
1012  * returns 0 upon success.
1013  */
1014 int omap_device_assert_hardreset(struct platform_device *pdev, const char *name)
1016         struct omap_device *od = to_omap_device(pdev);
1017         int ret = 0;
1018         int i;
1020         for (i = 0; i < od->hwmods_cnt; i++) {
1021                 ret = omap_hwmod_assert_hardreset(od->hwmods[i], name);
1022                 if (ret)
1023                         break;
1024         }
1026         return ret;
1029 /**
1030  * omap_device_deassert_hardreset - release a device's hardreset line
1031  * @pdev: struct platform_device * to reset
1032  * @name: const char * name of the reset line
1033  *
1034  * Release the hardreset line identified by @name on the IP blocks
1035  * associated with the hwmods backing the platform_device @pdev.  All
1036  * of the hwmods associated with @pdev must have the same hardreset
1037  * line linked to them for this to work.  Passes along the return
1038  * value of omap_hwmod_deassert_hardreset() in the event of any
1039  * failure, or returns 0 upon success.
1040  */
1041 int omap_device_deassert_hardreset(struct platform_device *pdev,
1042                                    const char *name)
1044         struct omap_device *od = to_omap_device(pdev);
1045         int ret = 0;
1046         int i;
1048         for (i = 0; i < od->hwmods_cnt; i++) {
1049                 ret = omap_hwmod_deassert_hardreset(od->hwmods[i], name);
1050                 if (ret)
1051                         break;
1052         }
1054         return ret;
1057 /**
1058  * omap_device_align_pm_lat - activate/deactivate device to match wakeup lat lim
1059  * @od: struct omap_device *
1060  *
1061  * When a device's maximum wakeup latency limit changes, call some of
1062  * the .activate_func or .deactivate_func function pointers in the
1063  * omap_device's pm_lats array to ensure that the device's maximum
1064  * wakeup latency is less than or equal to the new latency limit.
1065  * Intended to be called by OMAP PM code whenever a device's maximum
1066  * wakeup latency limit changes (e.g., via
1067  * omap_pm_set_dev_wakeup_lat()).  Returns 0 if nothing needs to be
1068  * done (e.g., if the omap_device is not currently idle, or if the
1069  * wakeup latency is already current with the new limit) or passes
1070  * along the return value of _omap_device_deactivate() or
1071  * _omap_device_activate().
1072  */
1073 int omap_device_align_pm_lat(struct platform_device *pdev,
1074                              u32 new_wakeup_lat_limit)
1076         int ret = -EINVAL;
1077         struct omap_device *od;
1079         od = to_omap_device(pdev);
1081         if (new_wakeup_lat_limit == od->dev_wakeup_lat)
1082                 return 0;
1084         od->_dev_wakeup_lat_limit = new_wakeup_lat_limit;
1086         if (od->_state != OMAP_DEVICE_STATE_IDLE)
1087                 return 0;
1088         else if (new_wakeup_lat_limit > od->dev_wakeup_lat)
1089                 ret = _omap_device_deactivate(od, USE_WAKEUP_LAT);
1090         else if (new_wakeup_lat_limit < od->dev_wakeup_lat)
1091                 ret = _omap_device_activate(od, USE_WAKEUP_LAT);
1093         return ret;
1096 /**
1097  * omap_device_get_pwrdm - return the powerdomain * associated with @od
1098  * @od: struct omap_device *
1099  *
1100  * Return the powerdomain associated with the first underlying
1101  * omap_hwmod for this omap_device.  Intended for use by core OMAP PM
1102  * code.  Returns NULL on error or a struct powerdomain * upon
1103  * success.
1104  */
1105 struct powerdomain *omap_device_get_pwrdm(struct omap_device *od)
1107         /*
1108          * XXX Assumes that all omap_hwmod powerdomains are identical.
1109          * This may not necessarily be true.  There should be a sanity
1110          * check in here to WARN() if any difference appears.
1111          */
1112         if (!od->hwmods_cnt)
1113                 return NULL;
1115         return omap_hwmod_get_pwrdm(od->hwmods[0]);
1118 /**
1119  * omap_device_get_mpu_rt_va - return the MPU's virtual addr for the hwmod base
1120  * @od: struct omap_device *
1121  *
1122  * Return the MPU's virtual address for the base of the hwmod, from
1123  * the ioremap() that the hwmod code does.  Only valid if there is one
1124  * hwmod associated with this device.  Returns NULL if there are zero
1125  * or more than one hwmods associated with this omap_device;
1126  * otherwise, passes along the return value from
1127  * omap_hwmod_get_mpu_rt_va().
1128  */
1129 void __iomem *omap_device_get_rt_va(struct omap_device *od)
1131         if (od->hwmods_cnt != 1)
1132                 return NULL;
1134         return omap_hwmod_get_mpu_rt_va(od->hwmods[0]);
1137 /**
1138  * omap_device_get_by_hwmod_name() - convert a hwmod name to
1139  * device pointer.
1140  * @oh_name: name of the hwmod device
1141  *
1142  * Returns back a struct device * pointer associated with a hwmod
1143  * device represented by a hwmod_name
1144  */
1145 struct device *omap_device_get_by_hwmod_name(const char *oh_name)
1147         struct omap_hwmod *oh;
1149         if (!oh_name) {
1150                 WARN(1, "%s: no hwmod name!\n", __func__);
1151                 return ERR_PTR(-EINVAL);
1152         }
1154         oh = omap_hwmod_lookup(oh_name);
1155         if (IS_ERR_OR_NULL(oh)) {
1156                 WARN(1, "%s: no hwmod for %s\n", __func__,
1157                         oh_name);
1158                 return ERR_PTR(oh ? PTR_ERR(oh) : -ENODEV);
1159         }
1160         if (IS_ERR_OR_NULL(oh->od)) {
1161                 WARN(1, "%s: no omap_device for %s\n", __func__,
1162                         oh_name);
1163                 return ERR_PTR(oh->od ? PTR_ERR(oh->od) : -ENODEV);
1164         }
1166         if (IS_ERR_OR_NULL(oh->od->pdev))
1167                 return ERR_PTR(oh->od->pdev ? PTR_ERR(oh->od->pdev) : -ENODEV);
1169         return &oh->od->pdev->dev;
1171 EXPORT_SYMBOL(omap_device_get_by_hwmod_name);
1173 /*
1174  * Public functions intended for use in omap_device_pm_latency
1175  * .activate_func and .deactivate_func function pointers
1176  */
1178 /**
1179  * omap_device_enable_hwmods - call omap_hwmod_enable() on all hwmods
1180  * @od: struct omap_device *od
1181  *
1182  * Enable all underlying hwmods.  Returns 0.
1183  */
1184 int omap_device_enable_hwmods(struct omap_device *od)
1186         int i;
1188         for (i = 0; i < od->hwmods_cnt; i++)
1189                 omap_hwmod_enable(od->hwmods[i]);
1191         /* XXX pass along return value here? */
1192         return 0;
1195 /**
1196  * omap_device_idle_hwmods - call omap_hwmod_idle() on all hwmods
1197  * @od: struct omap_device *od
1198  *
1199  * Idle all underlying hwmods.  Returns 0.
1200  */
1201 int omap_device_idle_hwmods(struct omap_device *od)
1203         int i;
1205         for (i = 0; i < od->hwmods_cnt; i++)
1206                 omap_hwmod_idle(od->hwmods[i]);
1208         /* XXX pass along return value here? */
1209         return 0;
1212 /**
1213  * omap_device_disable_clocks - disable all main and interface clocks
1214  * @od: struct omap_device *od
1215  *
1216  * Disable the main functional clock and interface clock for all of the
1217  * omap_hwmods associated with the omap_device.  Returns 0.
1218  */
1219 int omap_device_disable_clocks(struct omap_device *od)
1221         int i;
1223         for (i = 0; i < od->hwmods_cnt; i++)
1224                 omap_hwmod_disable_clocks(od->hwmods[i]);
1226         /* XXX pass along return value here? */
1227         return 0;
1230 /**
1231  * omap_device_enable_clocks - enable all main and interface clocks
1232  * @od: struct omap_device *od
1233  *
1234  * Enable the main functional clock and interface clock for all of the
1235  * omap_hwmods associated with the omap_device.  Returns 0.
1236  */
1237 int omap_device_enable_clocks(struct omap_device *od)
1239         int i;
1241         for (i = 0; i < od->hwmods_cnt; i++)
1242                 omap_hwmod_enable_clocks(od->hwmods[i]);
1244         /* XXX pass along return value here? */
1245         return 0;
1248 static struct notifier_block platform_nb = {
1249         .notifier_call = _omap_device_notifier_call,
1250 };
1252 static int __init omap_device_init(void)
1254         bus_register_notifier(&platform_bus_type, &platform_nb);
1255         return 0;
1257 core_initcall(omap_device_init);
1259 /**
1260  * omap_device_late_idle - idle devices without drivers
1261  * @dev: struct device * associated with omap_device
1262  * @data: unused
1263  *
1264  * Check the driver bound status of this device, and idle it
1265  * if there is no driver attached.
1266  */
1267 static int __init omap_device_late_idle(struct device *dev, void *data)
1269         struct platform_device *pdev = to_platform_device(dev);
1270         struct omap_device *od = to_omap_device(pdev);
1272         if (!od)
1273                 return 0;
1275         /*
1276          * If omap_device state is enabled, but has no driver bound,
1277          * idle it.
1278          */
1279         if (od->_driver_status != BUS_NOTIFY_BOUND_DRIVER) {
1280                 if (od->_state == OMAP_DEVICE_STATE_ENABLED) {
1281                         dev_warn(dev, "%s: enabled but no driver.  Idling\n",
1282                                  __func__);
1283                         omap_device_idle(pdev);
1284                 }
1285         }
1287         return 0;
1290 static int __init omap_device_late_init(void)
1292         bus_for_each_dev(&platform_bus_type, NULL, NULL, omap_device_late_idle);
1293         return 0;
1295 late_initcall(omap_device_late_init);