1 /*
2 * OMAP2/3 common powerdomain definitions
3 *
4 * Copyright (C) 2007-2008, 2011 Texas Instruments, Inc.
5 * Copyright (C) 2007-2011 Nokia Corporation
6 *
7 * Paul Walmsley, Jouni Högander
8 *
9 * This program is free software; you can redistribute it and/or modify
10 * it under the terms of the GNU General Public License version 2 as
11 * published by the Free Software Foundation.
12 */
14 /*
15 * The names for the DSP/IVA2 powerdomains are confusing.
16 *
17 * Most OMAP chips have an on-board DSP.
18 *
19 * On the 2420, this is a 'C55 DSP called, simply, the DSP. Its
20 * powerdomain is called the "DSP power domain." On the 2430, the
21 * on-board DSP is a 'C64 DSP, now called (along with its hardware
22 * accelerators) the IVA2 or IVA2.1. Its powerdomain is still called
23 * the "DSP power domain." On the 3430, the DSP is a 'C64 DSP like the
24 * 2430, also known as the IVA2; but its powerdomain is now called the
25 * "IVA2 power domain."
26 *
27 * The 2420 also has something called the IVA, which is a separate ARM
28 * core, and has nothing to do with the DSP/IVA2.
29 *
30 * Ideally the DSP/IVA2 could just be the same powerdomain, but the PRCM
31 * address offset is different between the C55 and C64 DSPs.
32 */
34 #include "powerdomain.h"
36 #include "prcm-common.h"
37 #include "prm.h"
39 /* OMAP2/3-common powerdomains */
41 /*
42 * The GFX powerdomain is not present on 3430ES2, but currently we do not
43 * have a macro to filter it out at compile-time.
44 */
45 struct powerdomain gfx_omap2_pwrdm = {
46 .name = "gfx_pwrdm",
47 .prcm_offs = GFX_MOD,
48 .pwrsts = PWRSTS_OFF_RET_ON,
49 .pwrsts_logic_ret = PWRSTS_RET,
50 .banks = 1,
51 .pwrsts_mem_ret = {
52 [0] = PWRSTS_RET, /* MEMRETSTATE */
53 },
54 .pwrsts_mem_on = {
55 [0] = PWRSTS_ON, /* MEMONSTATE */
56 },
57 .voltdm = { .name = "core" },
58 };
60 struct powerdomain wkup_omap2_pwrdm = {
61 .name = "wkup_pwrdm",
62 .prcm_offs = WKUP_MOD,
63 .pwrsts = PWRSTS_ON,
64 .voltdm = { .name = "wakeup" },
65 };