1 /*
2 * OMAP2+ common Power & Reset Management (PRM) IP block functions
3 *
4 * Copyright (C) 2011 Texas Instruments, Inc.
5 * Tero Kristo <t-kristo@ti.com>
6 *
7 * This program is free software; you can redistribute it and/or modify
8 * it under the terms of the GNU General Public License version 2 as
9 * published by the Free Software Foundation.
10 *
11 *
12 * For historical purposes, the API used to configure the PRM
13 * interrupt handler refers to it as the "PRCM interrupt." The
14 * underlying registers are located in the PRM on OMAP3/4.
15 *
16 * XXX This code should eventually be moved to a PRM driver.
17 */
19 #include <linux/kernel.h>
20 #include <linux/module.h>
21 #include <linux/init.h>
22 #include <linux/io.h>
23 #include <linux/irq.h>
24 #include <linux/interrupt.h>
25 #include <linux/slab.h>
27 #include "prm2xxx_3xxx.h"
28 #include "prm2xxx.h"
29 #include "prm3xxx.h"
30 #include "prm44xx.h"
31 #include "common.h"
33 /*
34 * OMAP_PRCM_MAX_NR_PENDING_REG: maximum number of PRM_IRQ*_MPU regs
35 * XXX this is technically not needed, since
36 * omap_prcm_register_chain_handler() could allocate this based on the
37 * actual amount of memory needed for the SoC
38 */
39 #define OMAP_PRCM_MAX_NR_PENDING_REG 2
41 /*
42 * prcm_irq_chips: an array of all of the "generic IRQ chips" in use
43 * by the PRCM interrupt handler code. There will be one 'chip' per
44 * PRM_{IRQSTATUS,IRQENABLE}_MPU register pair. (So OMAP3 will have
45 * one "chip" and OMAP4 will have two.)
46 */
47 static struct irq_chip_generic **prcm_irq_chips;
49 /*
50 * prcm_irq_setup: the PRCM IRQ parameters for the hardware the code
51 * is currently running on. Defined and passed by initialization code
52 * that calls omap_prcm_register_chain_handler().
53 */
54 static struct omap_prcm_irq_setup *prcm_irq_setup;
56 /* prm_base: base virtual address of the PRM IP block */
57 void __iomem *prm_base;
59 /*
60 * prm_ll_data: function pointers to SoC-specific implementations of
61 * common PRM functions
62 */
63 static struct prm_ll_data null_prm_ll_data;
64 static struct prm_ll_data *prm_ll_data = &null_prm_ll_data;
66 /* Private functions */
68 /*
69 * Move priority events from events to priority_events array
70 */
71 static void omap_prcm_events_filter_priority(unsigned long *events,
72 unsigned long *priority_events)
73 {
74 int i;
76 for (i = 0; i < prcm_irq_setup->nr_regs; i++) {
77 priority_events[i] =
78 events[i] & prcm_irq_setup->priority_mask[i];
79 events[i] ^= priority_events[i];
80 }
81 }
83 /*
84 * PRCM Interrupt Handler
85 *
86 * This is a common handler for the OMAP PRCM interrupts. Pending
87 * interrupts are detected by a call to prcm_pending_events and
88 * dispatched accordingly. Clearing of the wakeup events should be
89 * done by the SoC specific individual handlers.
90 */
91 static void omap_prcm_irq_handler(unsigned int irq, struct irq_desc *desc)
92 {
93 unsigned long pending[OMAP_PRCM_MAX_NR_PENDING_REG];
94 unsigned long priority_pending[OMAP_PRCM_MAX_NR_PENDING_REG];
95 struct irq_chip *chip = irq_desc_get_chip(desc);
96 unsigned int virtirq;
97 int nr_irq = prcm_irq_setup->nr_regs * 32;
99 /*
100 * If we are suspended, mask all interrupts from PRCM level,
101 * this does not ack them, and they will be pending until we
102 * re-enable the interrupts, at which point the
103 * omap_prcm_irq_handler will be executed again. The
104 * _save_and_clear_irqen() function must ensure that the PRM
105 * write to disable all IRQs has reached the PRM before
106 * returning, or spurious PRCM interrupts may occur during
107 * suspend.
108 */
109 if (prcm_irq_setup->suspended) {
110 prcm_irq_setup->save_and_clear_irqen(prcm_irq_setup->saved_mask);
111 prcm_irq_setup->suspend_save_flag = true;
112 }
114 /*
115 * Loop until all pending irqs are handled, since
116 * generic_handle_irq() can cause new irqs to come
117 */
118 while (!prcm_irq_setup->suspended) {
119 prcm_irq_setup->read_pending_irqs(pending);
121 /* No bit set, then all IRQs are handled */
122 if (find_first_bit(pending, nr_irq) >= nr_irq)
123 break;
125 omap_prcm_events_filter_priority(pending, priority_pending);
127 /*
128 * Loop on all currently pending irqs so that new irqs
129 * cannot starve previously pending irqs
130 */
132 /* Serve priority events first */
133 for_each_set_bit(virtirq, priority_pending, nr_irq)
134 generic_handle_irq(prcm_irq_setup->base_irq + virtirq);
136 /* Serve normal events next */
137 for_each_set_bit(virtirq, pending, nr_irq)
138 generic_handle_irq(prcm_irq_setup->base_irq + virtirq);
139 }
140 if (chip->irq_ack)
141 chip->irq_ack(&desc->irq_data);
142 if (chip->irq_eoi)
143 chip->irq_eoi(&desc->irq_data);
144 chip->irq_unmask(&desc->irq_data);
146 prcm_irq_setup->ocp_barrier(); /* avoid spurious IRQs */
147 }
149 /* Public functions */
151 /**
152 * omap_prcm_event_to_irq - given a PRCM event name, returns the
153 * corresponding IRQ on which the handler should be registered
154 * @name: name of the PRCM interrupt bit to look up - see struct omap_prcm_irq
155 *
156 * Returns the Linux internal IRQ ID corresponding to @name upon success,
157 * or -ENOENT upon failure.
158 */
159 int omap_prcm_event_to_irq(const char *name)
160 {
161 int i;
163 if (!prcm_irq_setup || !name)
164 return -ENOENT;
166 for (i = 0; i < prcm_irq_setup->nr_irqs; i++)
167 if (!strcmp(prcm_irq_setup->irqs[i].name, name))
168 return prcm_irq_setup->base_irq +
169 prcm_irq_setup->irqs[i].offset;
171 return -ENOENT;
172 }
174 /**
175 * omap_prcm_irq_cleanup - reverses memory allocated and other steps
176 * done by omap_prcm_register_chain_handler()
177 *
178 * No return value.
179 */
180 void omap_prcm_irq_cleanup(void)
181 {
182 int i;
184 if (!prcm_irq_setup) {
185 pr_err("PRCM: IRQ handler not initialized; cannot cleanup\n");
186 return;
187 }
189 if (prcm_irq_chips) {
190 for (i = 0; i < prcm_irq_setup->nr_regs; i++) {
191 if (prcm_irq_chips[i])
192 irq_remove_generic_chip(prcm_irq_chips[i],
193 0xffffffff, 0, 0);
194 prcm_irq_chips[i] = NULL;
195 }
196 kfree(prcm_irq_chips);
197 prcm_irq_chips = NULL;
198 }
200 kfree(prcm_irq_setup->saved_mask);
201 prcm_irq_setup->saved_mask = NULL;
203 kfree(prcm_irq_setup->priority_mask);
204 prcm_irq_setup->priority_mask = NULL;
206 irq_set_chained_handler(prcm_irq_setup->irq, NULL);
208 if (prcm_irq_setup->base_irq > 0)
209 irq_free_descs(prcm_irq_setup->base_irq,
210 prcm_irq_setup->nr_regs * 32);
211 prcm_irq_setup->base_irq = 0;
212 }
214 void omap_prcm_irq_prepare(void)
215 {
216 prcm_irq_setup->suspended = true;
217 }
219 void omap_prcm_irq_complete(void)
220 {
221 prcm_irq_setup->suspended = false;
223 /* If we have not saved the masks, do not attempt to restore */
224 if (!prcm_irq_setup->suspend_save_flag)
225 return;
227 prcm_irq_setup->suspend_save_flag = false;
229 /*
230 * Re-enable all masked PRCM irq sources, this causes the PRCM
231 * interrupt to fire immediately if the events were masked
232 * previously in the chain handler
233 */
234 prcm_irq_setup->restore_irqen(prcm_irq_setup->saved_mask);
235 }
237 /**
238 * omap_prcm_register_chain_handler - initializes the prcm chained interrupt
239 * handler based on provided parameters
240 * @irq_setup: hardware data about the underlying PRM/PRCM
241 *
242 * Set up the PRCM chained interrupt handler on the PRCM IRQ. Sets up
243 * one generic IRQ chip per PRM interrupt status/enable register pair.
244 * Returns 0 upon success, -EINVAL if called twice or if invalid
245 * arguments are passed, or -ENOMEM on any other error.
246 */
247 int omap_prcm_register_chain_handler(struct omap_prcm_irq_setup *irq_setup)
248 {
249 int nr_regs;
250 u32 mask[OMAP_PRCM_MAX_NR_PENDING_REG];
251 int offset, i;
252 struct irq_chip_generic *gc;
253 struct irq_chip_type *ct;
255 if (!irq_setup)
256 return -EINVAL;
258 nr_regs = irq_setup->nr_regs;
260 if (prcm_irq_setup) {
261 pr_err("PRCM: already initialized; won't reinitialize\n");
262 return -EINVAL;
263 }
265 if (nr_regs > OMAP_PRCM_MAX_NR_PENDING_REG) {
266 pr_err("PRCM: nr_regs too large\n");
267 return -EINVAL;
268 }
270 prcm_irq_setup = irq_setup;
272 prcm_irq_chips = kzalloc(sizeof(void *) * nr_regs, GFP_KERNEL);
273 prcm_irq_setup->saved_mask = kzalloc(sizeof(u32) * nr_regs, GFP_KERNEL);
274 prcm_irq_setup->priority_mask = kzalloc(sizeof(u32) * nr_regs,
275 GFP_KERNEL);
277 if (!prcm_irq_chips || !prcm_irq_setup->saved_mask ||
278 !prcm_irq_setup->priority_mask) {
279 pr_err("PRCM: kzalloc failed\n");
280 goto err;
281 }
283 memset(mask, 0, sizeof(mask));
285 for (i = 0; i < irq_setup->nr_irqs; i++) {
286 offset = irq_setup->irqs[i].offset;
287 mask[offset >> 5] |= 1 << (offset & 0x1f);
288 if (irq_setup->irqs[i].priority)
289 irq_setup->priority_mask[offset >> 5] |=
290 1 << (offset & 0x1f);
291 }
293 irq_set_chained_handler(irq_setup->irq, omap_prcm_irq_handler);
295 irq_setup->base_irq = irq_alloc_descs(-1, 0, irq_setup->nr_regs * 32,
296 0);
298 if (irq_setup->base_irq < 0) {
299 pr_err("PRCM: failed to allocate irq descs: %d\n",
300 irq_setup->base_irq);
301 goto err;
302 }
304 for (i = 0; i < irq_setup->nr_regs; i++) {
305 gc = irq_alloc_generic_chip("PRCM", 1,
306 irq_setup->base_irq + i * 32, prm_base,
307 handle_level_irq);
309 if (!gc) {
310 pr_err("PRCM: failed to allocate generic chip\n");
311 goto err;
312 }
313 ct = gc->chip_types;
314 ct->chip.irq_ack = irq_gc_ack_set_bit;
315 ct->chip.irq_mask = irq_gc_mask_clr_bit;
316 ct->chip.irq_unmask = irq_gc_mask_set_bit;
318 ct->regs.ack = irq_setup->ack + i * 4;
319 ct->regs.mask = irq_setup->mask + i * 4;
321 irq_setup_generic_chip(gc, mask[i], 0, IRQ_NOREQUEST, 0);
322 prcm_irq_chips[i] = gc;
323 }
325 return 0;
327 err:
328 omap_prcm_irq_cleanup();
329 return -ENOMEM;
330 }
332 /**
333 * omap2_set_globals_prm - set the PRM base address (for early use)
334 * @prm: PRM base virtual address
335 *
336 * XXX Will be replaced when the PRM/CM drivers are completed.
337 */
338 void __init omap2_set_globals_prm(void __iomem *prm)
339 {
340 prm_base = prm;
341 }
343 /**
344 * prm_read_reset_sources - return the sources of the SoC's last reset
345 *
346 * Return a u32 bitmask representing the reset sources that caused the
347 * SoC to reset. The low-level per-SoC functions called by this
348 * function remap the SoC-specific reset source bits into an
349 * OMAP-common set of reset source bits, defined in
350 * arch/arm/mach-omap2/prm.h. Returns the standardized reset source
351 * u32 bitmask from the hardware upon success, or returns (1 <<
352 * OMAP_UNKNOWN_RST_SRC_ID_SHIFT) if no low-level read_reset_sources()
353 * function was registered.
354 */
355 u32 prm_read_reset_sources(void)
356 {
357 u32 ret = 1 << OMAP_UNKNOWN_RST_SRC_ID_SHIFT;
359 if (prm_ll_data->read_reset_sources)
360 ret = prm_ll_data->read_reset_sources();
361 else
362 WARN_ONCE(1, "prm: %s: no mapping function defined for reset sources\n", __func__);
364 return ret;
365 }
367 /**
368 * prm_was_any_context_lost_old - was device context lost? (old API)
369 * @part: PRM partition ID (e.g., OMAP4430_PRM_PARTITION)
370 * @inst: PRM instance offset (e.g., OMAP4430_PRM_MPU_INST)
371 * @idx: CONTEXT register offset
372 *
373 * Return 1 if any bits were set in the *_CONTEXT_* register
374 * identified by (@part, @inst, @idx), which means that some context
375 * was lost for that module; otherwise, return 0. XXX Deprecated;
376 * callers need to use a less-SoC-dependent way to identify hardware
377 * IP blocks.
378 */
379 bool prm_was_any_context_lost_old(u8 part, s16 inst, u16 idx)
380 {
381 bool ret = true;
383 if (prm_ll_data->was_any_context_lost_old)
384 ret = prm_ll_data->was_any_context_lost_old(part, inst, idx);
385 else
386 WARN_ONCE(1, "prm: %s: no mapping function defined\n",
387 __func__);
389 return ret;
390 }
392 /**
393 * prm_clear_context_lost_flags_old - clear context loss flags (old API)
394 * @part: PRM partition ID (e.g., OMAP4430_PRM_PARTITION)
395 * @inst: PRM instance offset (e.g., OMAP4430_PRM_MPU_INST)
396 * @idx: CONTEXT register offset
397 *
398 * Clear hardware context loss bits for the module identified by
399 * (@part, @inst, @idx). No return value. XXX Deprecated; callers
400 * need to use a less-SoC-dependent way to identify hardware IP
401 * blocks.
402 */
403 void prm_clear_context_loss_flags_old(u8 part, s16 inst, u16 idx)
404 {
405 if (prm_ll_data->clear_context_loss_flags_old)
406 prm_ll_data->clear_context_loss_flags_old(part, inst, idx);
407 else
408 WARN_ONCE(1, "prm: %s: no mapping function defined\n",
409 __func__);
410 }
412 /**
413 * prm_register - register per-SoC low-level data with the PRM
414 * @pld: low-level per-SoC OMAP PRM data & function pointers to register
415 *
416 * Register per-SoC low-level OMAP PRM data and function pointers with
417 * the OMAP PRM common interface. The caller must keep the data
418 * pointed to by @pld valid until it calls prm_unregister() and
419 * it returns successfully. Returns 0 upon success, -EINVAL if @pld
420 * is NULL, or -EEXIST if prm_register() has already been called
421 * without an intervening prm_unregister().
422 */
423 int prm_register(struct prm_ll_data *pld)
424 {
425 if (!pld)
426 return -EINVAL;
428 if (prm_ll_data != &null_prm_ll_data)
429 return -EEXIST;
431 prm_ll_data = pld;
433 return 0;
434 }
436 /**
437 * prm_unregister - unregister per-SoC low-level data & function pointers
438 * @pld: low-level per-SoC OMAP PRM data & function pointers to unregister
439 *
440 * Unregister per-SoC low-level OMAP PRM data and function pointers
441 * that were previously registered with prm_register(). The
442 * caller may not destroy any of the data pointed to by @pld until
443 * this function returns successfully. Returns 0 upon success, or
444 * -EINVAL if @pld is NULL or if @pld does not match the struct
445 * prm_ll_data * previously registered by prm_register().
446 */
447 int prm_unregister(struct prm_ll_data *pld)
448 {
449 if (!pld || prm_ll_data != pld)
450 return -EINVAL;
452 prm_ll_data = &null_prm_ll_data;
454 return 0;
455 }