]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - arch/powerpc/include/asm/io-workarounds.h
Merge branch 'drm-nouveau-fixes-3.8' of git://anongit.freedesktop.org/git/nouveau...
[android-sdk/kernel-video.git] / arch / powerpc / include / asm / io-workarounds.h
1 /*
2  * Support PCI IO workaround
3  *
4  * (C) Copyright 2007-2008 TOSHIBA CORPORATION
5  *
6  * This program is free software; you can redistribute it and/or modify
7  * it under the terms of the GNU General Public License as published by
8  * the Free Software Foundation; either version 2 of the License, or
9  * (at your option) any later version.
10  *
11  * This program is distributed in the hope that it will be useful,
12  * but WITHOUT ANY WARRANTY; without even the implied warranty of
13  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
14  * GNU General Public License for more details.
15  *
16  * You should have received a copy of the GNU General Public License along
17  * with this program; if not, write to the Free Software Foundation, Inc.,
18  * 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
19  */
21 #ifndef _IO_WORKAROUNDS_H
22 #define _IO_WORKAROUNDS_H
24 #include <linux/io.h>
25 #include <asm/pci-bridge.h>
27 /* Bus info */
28 struct iowa_bus {
29         struct pci_controller *phb;
30         struct ppc_pci_io *ops;
31         void   *private;
32 };
34 void iowa_register_bus(struct pci_controller *, struct ppc_pci_io *,
35                        int (*)(struct iowa_bus *, void *), void *);
36 struct iowa_bus *iowa_mem_find_bus(const PCI_IO_ADDR);
37 struct iowa_bus *iowa_pio_find_bus(unsigned long);
39 extern struct ppc_pci_io spiderpci_ops;
40 extern int spiderpci_iowa_init(struct iowa_bus *, void *);
42 #define SPIDER_PCI_REG_BASE             0xd000
43 #define SPIDER_PCI_REG_SIZE             0x1000
44 #define SPIDER_PCI_VCI_CNTL_STAT        0x0110
45 #define SPIDER_PCI_DUMMY_READ           0x0810
46 #define SPIDER_PCI_DUMMY_READ_BASE      0x0814
48 #endif /* _IO_WORKAROUNDS_H */