]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - arch/sparc/kernel/leon_pci.c
Merge branch 'drm-nouveau-fixes-3.8' of git://anongit.freedesktop.org/git/nouveau...
[android-sdk/kernel-video.git] / arch / sparc / kernel / leon_pci.c
1 /*
2  * leon_pci.c: LEON Host PCI support
3  *
4  * Copyright (C) 2011 Aeroflex Gaisler AB, Daniel Hellstrom
5  *
6  * Code is partially derived from pcic.c
7  */
9 #include <linux/of_device.h>
10 #include <linux/kernel.h>
11 #include <linux/pci.h>
12 #include <linux/export.h>
13 #include <asm/leon.h>
14 #include <asm/leon_pci.h>
16 /* The LEON architecture does not rely on a BIOS or bootloader to setup
17  * PCI for us. The Linux generic routines are used to setup resources,
18  * reset values of configuration-space register settings are preserved.
19  *
20  * PCI Memory and Prefetchable Memory is direct-mapped. However I/O Space is
21  * accessed through a Window which is translated to low 64KB in PCI space, the
22  * first 4KB is not used so 60KB is available.
23  */
24 void leon_pci_init(struct platform_device *ofdev, struct leon_pci_info *info)
25 {
26         LIST_HEAD(resources);
27         struct pci_bus *root_bus;
29         pci_add_resource_offset(&resources, &info->io_space,
30                                 info->io_space.start - 0x1000);
31         pci_add_resource(&resources, &info->mem_space);
33         root_bus = pci_scan_root_bus(&ofdev->dev, 0, info->ops, info,
34                                      &resources);
35         if (root_bus) {
36                 /* Setup IRQs of all devices using custom routines */
37                 pci_fixup_irqs(pci_common_swizzle, info->map_irq);
39                 /* Assign devices with resources */
40                 pci_assign_unassigned_resources();
41         } else {
42                 pci_free_resource_list(&resources);
43         }
44 }
46 void pcibios_fixup_bus(struct pci_bus *pbus)
47 {
48         struct pci_dev *dev;
49         int i, has_io, has_mem;
50         u16 cmd;
52         list_for_each_entry(dev, &pbus->devices, bus_list) {
53                 /*
54                  * We can not rely on that the bootloader has enabled I/O
55                  * or memory access to PCI devices. Instead we enable it here
56                  * if the device has BARs of respective type.
57                  */
58                 has_io = has_mem = 0;
59                 for (i = 0; i < PCI_ROM_RESOURCE; i++) {
60                         unsigned long f = dev->resource[i].flags;
61                         if (f & IORESOURCE_IO)
62                                 has_io = 1;
63                         else if (f & IORESOURCE_MEM)
64                                 has_mem = 1;
65                 }
66                 /* ROM BARs are mapped into 32-bit memory space */
67                 if (dev->resource[PCI_ROM_RESOURCE].end != 0) {
68                         dev->resource[PCI_ROM_RESOURCE].flags |=
69                                                         IORESOURCE_ROM_ENABLE;
70                         has_mem = 1;
71                 }
72                 pci_bus_read_config_word(pbus, dev->devfn, PCI_COMMAND, &cmd);
73                 if (has_io && !(cmd & PCI_COMMAND_IO)) {
74 #ifdef CONFIG_PCI_DEBUG
75                         printk(KERN_INFO "LEONPCI: Enabling I/O for dev %s\n",
76                                          pci_name(dev));
77 #endif
78                         cmd |= PCI_COMMAND_IO;
79                         pci_bus_write_config_word(pbus, dev->devfn, PCI_COMMAND,
80                                                                         cmd);
81                 }
82                 if (has_mem && !(cmd & PCI_COMMAND_MEMORY)) {
83 #ifdef CONFIG_PCI_DEBUG
84                         printk(KERN_INFO "LEONPCI: Enabling MEMORY for dev"
85                                          "%s\n", pci_name(dev));
86 #endif
87                         cmd |= PCI_COMMAND_MEMORY;
88                         pci_bus_write_config_word(pbus, dev->devfn, PCI_COMMAND,
89                                                                         cmd);
90                 }
91         }
92 }
94 resource_size_t pcibios_align_resource(void *data, const struct resource *res,
95                                 resource_size_t size, resource_size_t align)
96 {
97         return res->start;
98 }
100 int pcibios_enable_device(struct pci_dev *dev, int mask)
102         return pci_enable_resources(dev, mask);
105 /* in/out routines taken from pcic.c
106  *
107  * This probably belongs here rather than ioport.c because
108  * we do not want this crud linked into SBus kernels.
109  * Also, think for a moment about likes of floppy.c that
110  * include architecture specific parts. They may want to redefine ins/outs.
111  *
112  * We do not use horrible macros here because we want to
113  * advance pointer by sizeof(size).
114  */
115 void outsb(unsigned long addr, const void *src, unsigned long count)
117         while (count) {
118                 count -= 1;
119                 outb(*(const char *)src, addr);
120                 src += 1;
121                 /* addr += 1; */
122         }
124 EXPORT_SYMBOL(outsb);
126 void outsw(unsigned long addr, const void *src, unsigned long count)
128         while (count) {
129                 count -= 2;
130                 outw(*(const short *)src, addr);
131                 src += 2;
132                 /* addr += 2; */
133         }
135 EXPORT_SYMBOL(outsw);
137 void outsl(unsigned long addr, const void *src, unsigned long count)
139         while (count) {
140                 count -= 4;
141                 outl(*(const long *)src, addr);
142                 src += 4;
143                 /* addr += 4; */
144         }
146 EXPORT_SYMBOL(outsl);
148 void insb(unsigned long addr, void *dst, unsigned long count)
150         while (count) {
151                 count -= 1;
152                 *(unsigned char *)dst = inb(addr);
153                 dst += 1;
154                 /* addr += 1; */
155         }
157 EXPORT_SYMBOL(insb);
159 void insw(unsigned long addr, void *dst, unsigned long count)
161         while (count) {
162                 count -= 2;
163                 *(unsigned short *)dst = inw(addr);
164                 dst += 2;
165                 /* addr += 2; */
166         }
168 EXPORT_SYMBOL(insw);
170 void insl(unsigned long addr, void *dst, unsigned long count)
172         while (count) {
173                 count -= 4;
174                 /*
175                  * XXX I am sure we are in for an unaligned trap here.
176                  */
177                 *(unsigned long *)dst = inl(addr);
178                 dst += 4;
179                 /* addr += 4; */
180         }
182 EXPORT_SYMBOL(insl);