]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - arch/x86/boot/header.S
Merge branch 'drm-nouveau-fixes-3.8' of git://anongit.freedesktop.org/git/nouveau...
[android-sdk/kernel-video.git] / arch / x86 / boot / header.S
1 /*
2  *      header.S
3  *
4  *      Copyright (C) 1991, 1992 Linus Torvalds
5  *
6  *      Based on bootsect.S and setup.S
7  *      modified by more people than can be counted
8  *
9  *      Rewritten as a common file by H. Peter Anvin (Apr 2007)
10  *
11  * BIG FAT NOTE: We're in real mode using 64k segments.  Therefore segment
12  * addresses must be multiplied by 16 to obtain their respective linear
13  * addresses. To avoid confusion, linear addresses are written using leading
14  * hex while segment addresses are written as segment:offset.
15  *
16  */
18 #include <asm/segment.h>
19 #include <generated/utsrelease.h>
20 #include <asm/boot.h>
21 #include <asm/e820.h>
22 #include <asm/page_types.h>
23 #include <asm/setup.h>
24 #include <asm/bootparam.h>
25 #include "boot.h"
26 #include "voffset.h"
27 #include "zoffset.h"
29 BOOTSEG         = 0x07C0                /* original address of boot-sector */
30 SYSSEG          = 0x1000                /* historical load address >> 4 */
32 #ifndef SVGA_MODE
33 #define SVGA_MODE ASK_VGA
34 #endif
36 #ifndef ROOT_RDONLY
37 #define ROOT_RDONLY 1
38 #endif
40         .code16
41         .section ".bstext", "ax"
43         .global bootsect_start
44 bootsect_start:
45 #ifdef CONFIG_EFI_STUB
46         # "MZ", MS-DOS header
47         .byte 0x4d
48         .byte 0x5a
49 #endif
51         # Normalize the start address
52         ljmp    $BOOTSEG, $start2
54 start2:
55         movw    %cs, %ax
56         movw    %ax, %ds
57         movw    %ax, %es
58         movw    %ax, %ss
59         xorw    %sp, %sp
60         sti
61         cld
63         movw    $bugger_off_msg, %si
65 msg_loop:
66         lodsb
67         andb    %al, %al
68         jz      bs_die
69         movb    $0xe, %ah
70         movw    $7, %bx
71         int     $0x10
72         jmp     msg_loop
74 bs_die:
75         # Allow the user to press a key, then reboot
76         xorw    %ax, %ax
77         int     $0x16
78         int     $0x19
80         # int 0x19 should never return.  In case it does anyway,
81         # invoke the BIOS reset code...
82         ljmp    $0xf000,$0xfff0
84 #ifdef CONFIG_EFI_STUB
85         .org    0x3c
86         #
87         # Offset to the PE header.
88         #
89         .long   pe_header
90 #endif /* CONFIG_EFI_STUB */
92         .section ".bsdata", "a"
93 bugger_off_msg:
94         .ascii  "Direct floppy boot is not supported. "
95         .ascii  "Use a boot loader program instead.\r\n"
96         .ascii  "\n"
97         .ascii  "Remove disk and press any key to reboot ...\r\n"
98         .byte   0
100 #ifdef CONFIG_EFI_STUB
101 pe_header:
102         .ascii  "PE"
103         .word   0
105 coff_header:
106 #ifdef CONFIG_X86_32
107         .word   0x14c                           # i386
108 #else
109         .word   0x8664                          # x86-64
110 #endif
111         .word   3                               # nr_sections
112         .long   0                               # TimeDateStamp
113         .long   0                               # PointerToSymbolTable
114         .long   1                               # NumberOfSymbols
115         .word   section_table - optional_header # SizeOfOptionalHeader
116 #ifdef CONFIG_X86_32
117         .word   0x306                           # Characteristics.
118                                                 # IMAGE_FILE_32BIT_MACHINE |
119                                                 # IMAGE_FILE_DEBUG_STRIPPED |
120                                                 # IMAGE_FILE_EXECUTABLE_IMAGE |
121                                                 # IMAGE_FILE_LINE_NUMS_STRIPPED
122 #else
123         .word   0x206                           # Characteristics
124                                                 # IMAGE_FILE_DEBUG_STRIPPED |
125                                                 # IMAGE_FILE_EXECUTABLE_IMAGE |
126                                                 # IMAGE_FILE_LINE_NUMS_STRIPPED
127 #endif
129 optional_header:
130 #ifdef CONFIG_X86_32
131         .word   0x10b                           # PE32 format
132 #else
133         .word   0x20b                           # PE32+ format
134 #endif
135         .byte   0x02                            # MajorLinkerVersion
136         .byte   0x14                            # MinorLinkerVersion
138         # Filled in by build.c
139         .long   0                               # SizeOfCode
141         .long   0                               # SizeOfInitializedData
142         .long   0                               # SizeOfUninitializedData
144         # Filled in by build.c
145         .long   0x0000                          # AddressOfEntryPoint
147         .long   0x0200                          # BaseOfCode
148 #ifdef CONFIG_X86_32
149         .long   0                               # data
150 #endif
152 extra_header_fields:
153 #ifdef CONFIG_X86_32
154         .long   0                               # ImageBase
155 #else
156         .quad   0                               # ImageBase
157 #endif
158         .long   0x20                            # SectionAlignment
159         .long   0x20                            # FileAlignment
160         .word   0                               # MajorOperatingSystemVersion
161         .word   0                               # MinorOperatingSystemVersion
162         .word   0                               # MajorImageVersion
163         .word   0                               # MinorImageVersion
164         .word   0                               # MajorSubsystemVersion
165         .word   0                               # MinorSubsystemVersion
166         .long   0                               # Win32VersionValue
168         #
169         # The size of the bzImage is written in tools/build.c
170         #
171         .long   0                               # SizeOfImage
173         .long   0x200                           # SizeOfHeaders
174         .long   0                               # CheckSum
175         .word   0xa                             # Subsystem (EFI application)
176         .word   0                               # DllCharacteristics
177 #ifdef CONFIG_X86_32
178         .long   0                               # SizeOfStackReserve
179         .long   0                               # SizeOfStackCommit
180         .long   0                               # SizeOfHeapReserve
181         .long   0                               # SizeOfHeapCommit
182 #else
183         .quad   0                               # SizeOfStackReserve
184         .quad   0                               # SizeOfStackCommit
185         .quad   0                               # SizeOfHeapReserve
186         .quad   0                               # SizeOfHeapCommit
187 #endif
188         .long   0                               # LoaderFlags
189         .long   0x6                             # NumberOfRvaAndSizes
191         .quad   0                               # ExportTable
192         .quad   0                               # ImportTable
193         .quad   0                               # ResourceTable
194         .quad   0                               # ExceptionTable
195         .quad   0                               # CertificationTable
196         .quad   0                               # BaseRelocationTable
198         # Section table
199 section_table:
200         #
201         # The offset & size fields are filled in by build.c.
202         #
203         .ascii  ".setup"
204         .byte   0
205         .byte   0
206         .long   0
207         .long   0x0                             # startup_{32,64}
208         .long   0                               # Size of initialized data
209                                                 # on disk
210         .long   0x0                             # startup_{32,64}
211         .long   0                               # PointerToRelocations
212         .long   0                               # PointerToLineNumbers
213         .word   0                               # NumberOfRelocations
214         .word   0                               # NumberOfLineNumbers
215         .long   0x60500020                      # Characteristics (section flags)
217         #
218         # The EFI application loader requires a relocation section
219         # because EFI applications must be relocatable. The .reloc
220         # offset & size fields are filled in by build.c.
221         #
222         .ascii  ".reloc"
223         .byte   0
224         .byte   0
225         .long   0
226         .long   0
227         .long   0                               # SizeOfRawData
228         .long   0                               # PointerToRawData
229         .long   0                               # PointerToRelocations
230         .long   0                               # PointerToLineNumbers
231         .word   0                               # NumberOfRelocations
232         .word   0                               # NumberOfLineNumbers
233         .long   0x42100040                      # Characteristics (section flags)
235         #
236         # The offset & size fields are filled in by build.c.
237         #
238         .ascii  ".text"
239         .byte   0
240         .byte   0
241         .byte   0
242         .long   0
243         .long   0x0                             # startup_{32,64}
244         .long   0                               # Size of initialized data
245                                                 # on disk
246         .long   0x0                             # startup_{32,64}
247         .long   0                               # PointerToRelocations
248         .long   0                               # PointerToLineNumbers
249         .word   0                               # NumberOfRelocations
250         .word   0                               # NumberOfLineNumbers
251         .long   0x60500020                      # Characteristics (section flags)
253 #endif /* CONFIG_EFI_STUB */
255         # Kernel attributes; used by setup.  This is part 1 of the
256         # header, from the old boot sector.
258         .section ".header", "a"
259         .globl  sentinel
260 sentinel:       .byte 0xff, 0xff        /* Used to detect broken loaders */
262         .globl  hdr
263 hdr:
264 setup_sects:    .byte 0                 /* Filled in by build.c */
265 root_flags:     .word ROOT_RDONLY
266 syssize:        .long 0                 /* Filled in by build.c */
267 ram_size:       .word 0                 /* Obsolete */
268 vid_mode:       .word SVGA_MODE
269 root_dev:       .word 0                 /* Filled in by build.c */
270 boot_flag:      .word 0xAA55
272         # offset 512, entry point
274         .globl  _start
275 _start:
276                 # Explicitly enter this as bytes, or the assembler
277                 # tries to generate a 3-byte jump here, which causes
278                 # everything else to push off to the wrong offset.
279                 .byte   0xeb            # short (2-byte) jump
280                 .byte   start_of_setup-1f
281 1:
283         # Part 2 of the header, from the old setup.S
285                 .ascii  "HdrS"          # header signature
286                 .word   0x020c          # header version number (>= 0x0105)
287                                         # or else old loadlin-1.5 will fail)
288                 .globl realmode_swtch
289 realmode_swtch: .word   0, 0            # default_switch, SETUPSEG
290 start_sys_seg:  .word   SYSSEG          # obsolete and meaningless, but just
291                                         # in case something decided to "use" it
292                 .word   kernel_version-512 # pointing to kernel version string
293                                         # above section of header is compatible
294                                         # with loadlin-1.5 (header v1.5). Don't
295                                         # change it.
297 type_of_loader: .byte   0               # 0 means ancient bootloader, newer
298                                         # bootloaders know to change this.
299                                         # See Documentation/x86/boot.txt for
300                                         # assigned ids
302 # flags, unused bits must be zero (RFU) bit within loadflags
303 loadflags:
304                 .byte   LOADED_HIGH     # The kernel is to be loaded high
306 setup_move_size: .word  0x8000          # size to move, when setup is not
307                                         # loaded at 0x90000. We will move setup
308                                         # to 0x90000 then just before jumping
309                                         # into the kernel. However, only the
310                                         # loader knows how much data behind
311                                         # us also needs to be loaded.
313 code32_start:                           # here loaders can put a different
314                                         # start address for 32-bit code.
315                 .long   0x100000        # 0x100000 = default for big kernel
317 ramdisk_image:  .long   0               # address of loaded ramdisk image
318                                         # Here the loader puts the 32-bit
319                                         # address where it loaded the image.
320                                         # This only will be read by the kernel.
322 ramdisk_size:   .long   0               # its size in bytes
324 bootsect_kludge:
325                 .long   0               # obsolete
327 heap_end_ptr:   .word   _end+STACK_SIZE-512
328                                         # (Header version 0x0201 or later)
329                                         # space from here (exclusive) down to
330                                         # end of setup code can be used by setup
331                                         # for local heap purposes.
333 ext_loader_ver:
334                 .byte   0               # Extended boot loader version
335 ext_loader_type:
336                 .byte   0               # Extended boot loader type
338 cmd_line_ptr:   .long   0               # (Header version 0x0202 or later)
339                                         # If nonzero, a 32-bit pointer
340                                         # to the kernel command line.
341                                         # The command line should be
342                                         # located between the start of
343                                         # setup and the end of low
344                                         # memory (0xa0000), or it may
345                                         # get overwritten before it
346                                         # gets read.  If this field is
347                                         # used, there is no longer
348                                         # anything magical about the
349                                         # 0x90000 segment; the setup
350                                         # can be located anywhere in
351                                         # low memory 0x10000 or higher.
353 ramdisk_max:    .long 0x7fffffff
354                                         # (Header version 0x0203 or later)
355                                         # The highest safe address for
356                                         # the contents of an initrd
357                                         # The current kernel allows up to 4 GB,
358                                         # but leave it at 2 GB to avoid
359                                         # possible bootloader bugs.
361 kernel_alignment:  .long CONFIG_PHYSICAL_ALIGN  #physical addr alignment
362                                                 #required for protected mode
363                                                 #kernel
364 #ifdef CONFIG_RELOCATABLE
365 relocatable_kernel:    .byte 1
366 #else
367 relocatable_kernel:    .byte 0
368 #endif
369 min_alignment:          .byte MIN_KERNEL_ALIGN_LG2      # minimum alignment
371 xloadflags:
372 #ifdef CONFIG_X86_64
373 # define XLF0 XLF_KERNEL_64                     /* 64-bit kernel */
374 #else
375 # define XLF0 0
376 #endif
377 #ifdef CONFIG_EFI_STUB
378 # ifdef CONFIG_X86_64
379 #  define XLF23 XLF_EFI_HANDOVER_64             /* 64-bit EFI handover ok */
380 # else
381 #  define XLF23 XLF_EFI_HANDOVER_32             /* 32-bit EFI handover ok */
382 # endif
383 #else
384 # define XLF23 0
385 #endif
386                         .word XLF0 | XLF23
388 cmdline_size:   .long   COMMAND_LINE_SIZE-1     #length of the command line,
389                                                 #added with boot protocol
390                                                 #version 2.06
392 hardware_subarch:       .long 0                 # subarchitecture, added with 2.07
393                                                 # default to 0 for normal x86 PC
395 hardware_subarch_data:  .quad 0
397 payload_offset:         .long ZO_input_data
398 payload_length:         .long ZO_z_input_len
400 setup_data:             .quad 0                 # 64-bit physical pointer to
401                                                 # single linked list of
402                                                 # struct setup_data
404 pref_address:           .quad LOAD_PHYSICAL_ADDR        # preferred load addr
406 #define ZO_INIT_SIZE    (ZO__end - ZO_startup_32 + ZO_z_extract_offset)
407 #define VO_INIT_SIZE    (VO__end - VO__text)
408 #if ZO_INIT_SIZE > VO_INIT_SIZE
409 #define INIT_SIZE ZO_INIT_SIZE
410 #else
411 #define INIT_SIZE VO_INIT_SIZE
412 #endif
413 init_size:              .long INIT_SIZE         # kernel initialization size
414 handover_offset:
415 #ifdef CONFIG_EFI_STUB
416                         .long 0x30              # offset to the handover
417                                                 # protocol entry point
418 #else
419                         .long 0
420 #endif
422 # End of setup header #####################################################
424         .section ".entrytext", "ax"
425 start_of_setup:
426 # Force %es = %ds
427         movw    %ds, %ax
428         movw    %ax, %es
429         cld
431 # Apparently some ancient versions of LILO invoked the kernel with %ss != %ds,
432 # which happened to work by accident for the old code.  Recalculate the stack
433 # pointer if %ss is invalid.  Otherwise leave it alone, LOADLIN sets up the
434 # stack behind its own code, so we can't blindly put it directly past the heap.
436         movw    %ss, %dx
437         cmpw    %ax, %dx        # %ds == %ss?
438         movw    %sp, %dx
439         je      2f              # -> assume %sp is reasonably set
441         # Invalid %ss, make up a new stack
442         movw    $_end, %dx
443         testb   $CAN_USE_HEAP, loadflags
444         jz      1f
445         movw    heap_end_ptr, %dx
446 1:      addw    $STACK_SIZE, %dx
447         jnc     2f
448         xorw    %dx, %dx        # Prevent wraparound
450 2:      # Now %dx should point to the end of our stack space
451         andw    $~3, %dx        # dword align (might as well...)
452         jnz     3f
453         movw    $0xfffc, %dx    # Make sure we're not zero
454 3:      movw    %ax, %ss
455         movzwl  %dx, %esp       # Clear upper half of %esp
456         sti                     # Now we should have a working stack
458 # We will have entered with %cs = %ds+0x20, normalize %cs so
459 # it is on par with the other segments.
460         pushw   %ds
461         pushw   $6f
462         lretw
463 6:
465 # Check signature at end of setup
466         cmpl    $0x5a5aaa55, setup_sig
467         jne     setup_bad
469 # Zero the bss
470         movw    $__bss_start, %di
471         movw    $_end+3, %cx
472         xorl    %eax, %eax
473         subw    %di, %cx
474         shrw    $2, %cx
475         rep; stosl
477 # Jump to C code (should not return)
478         calll   main
480 # Setup corrupt somehow...
481 setup_bad:
482         movl    $setup_corrupt, %eax
483         calll   puts
484         # Fall through...
486         .globl  die
487         .type   die, @function
488 die:
489         hlt
490         jmp     die
492         .size   die, .-die
494         .section ".initdata", "a"
495 setup_corrupt:
496         .byte   7
497         .string "No setup signature found...\n"