1 #
2 # Makefile for the Linux kernel device drivers.
3 #
4 # 15 Sep 2000, Christoph Hellwig <hch@infradead.org>
5 # Rewritten to use lists instead of if-statements.
6 #
8 obj-y += irqchip/
9 obj-y += bus/
11 obj-$(CONFIG_GENERIC_PHY) += phy/
13 # GPIO must come after pinctrl as gpios may need to mux pins etc
14 obj-y += pinctrl/
15 obj-y += gpio/
16 obj-y += pwm/
17 obj-$(CONFIG_PCI) += pci/
18 obj-$(CONFIG_PARISC) += parisc/
19 obj-$(CONFIG_RAPIDIO) += rapidio/
20 obj-y += video/
21 obj-y += idle/
23 # IPMI must come before ACPI in order to provide IPMI opregion support
24 obj-$(CONFIG_IPMI_HANDLER) += char/ipmi/
26 obj-$(CONFIG_ACPI) += acpi/
27 obj-$(CONFIG_SFI) += sfi/
28 # PnP must come after ACPI since it will eventually need to check if acpi
29 # was used and do nothing if so
30 obj-$(CONFIG_PNP) += pnp/
31 obj-y += amba/
32 # Many drivers will want to use DMA so this has to be made available
33 # really early.
34 obj-$(CONFIG_DMADEVICES) += dma/
36 obj-$(CONFIG_VIRTIO) += virtio/
37 obj-$(CONFIG_XEN) += xen/
39 # regulators early, since some subsystems rely on them to initialize
40 obj-$(CONFIG_REGULATOR) += regulator/
42 # reset controllers early, since gpu drivers might rely on them to initialize
43 obj-$(CONFIG_RESET_CONTROLLER) += reset/
45 # tty/ comes before char/ so that the VT console is the boot-time
46 # default.
47 obj-y += tty/
48 obj-y += char/
50 # gpu/ comes after char for AGP vs DRM startup
51 obj-y += gpu/
53 obj-$(CONFIG_CONNECTOR) += connector/
55 # i810fb and intelfb depend on char/agp/
56 obj-$(CONFIG_FB_I810) += video/fbdev/i810/
57 obj-$(CONFIG_FB_INTEL) += video/fbdev/intelfb/
59 obj-$(CONFIG_PARPORT) += parport/
60 obj-y += base/ block/ misc/ mfd/ nfc/
61 obj-$(CONFIG_NUBUS) += nubus/
62 obj-y += macintosh/
63 obj-$(CONFIG_IDE) += ide/
64 obj-$(CONFIG_SCSI) += scsi/
65 obj-$(CONFIG_ATA) += ata/
66 obj-$(CONFIG_TARGET_CORE) += target/
67 obj-$(CONFIG_MTD) += mtd/
68 obj-$(CONFIG_SPI) += spi/
69 obj-y += hsi/
70 obj-y += net/
71 obj-$(CONFIG_ATM) += atm/
72 obj-$(CONFIG_FUSION) += message/
73 obj-y += firewire/
74 obj-$(CONFIG_UIO) += uio/
75 obj-$(CONFIG_VFIO) += vfio/
76 obj-y += cdrom/
77 obj-y += auxdisplay/
78 obj-$(CONFIG_PCCARD) += pcmcia/
79 obj-$(CONFIG_DIO) += dio/
80 obj-$(CONFIG_SBUS) += sbus/
81 obj-$(CONFIG_ZORRO) += zorro/
82 obj-$(CONFIG_MAC) += macintosh/
83 obj-$(CONFIG_ATA_OVER_ETH) += block/aoe/
84 obj-$(CONFIG_PARIDE) += block/paride/
85 obj-$(CONFIG_TC) += tc/
86 obj-$(CONFIG_UWB) += uwb/
87 obj-$(CONFIG_USB_PHY) += usb/
88 obj-$(CONFIG_USB) += usb/
89 obj-$(CONFIG_PCI) += usb/
90 obj-$(CONFIG_USB_GADGET) += usb/
91 obj-$(CONFIG_SERIO) += input/serio/
92 obj-$(CONFIG_GAMEPORT) += input/gameport/
93 obj-$(CONFIG_INPUT) += input/
94 obj-$(CONFIG_I2O) += message/
95 obj-$(CONFIG_RTC_LIB) += rtc/
96 obj-y += i2c/ media/
97 obj-$(CONFIG_PPS) += pps/
98 obj-$(CONFIG_PTP_1588_CLOCK) += ptp/
99 obj-$(CONFIG_W1) += w1/
100 obj-$(CONFIG_POWER_SUPPLY) += power/
101 obj-$(CONFIG_HWMON) += hwmon/
102 obj-$(CONFIG_THERMAL) += thermal/
103 obj-$(CONFIG_WATCHDOG) += watchdog/
104 obj-$(CONFIG_MD) += md/
105 obj-$(CONFIG_BT) += bluetooth/
106 obj-$(CONFIG_ACCESSIBILITY) += accessibility/
107 obj-$(CONFIG_ISDN) += isdn/
108 obj-$(CONFIG_EDAC) += edac/
109 obj-$(CONFIG_EISA) += eisa/
110 obj-y += lguest/
111 obj-$(CONFIG_CPU_FREQ) += cpufreq/
112 obj-$(CONFIG_CPU_IDLE) += cpuidle/
113 obj-y += mmc/
114 obj-$(CONFIG_MEMSTICK) += memstick/
115 obj-y += leds/
116 obj-$(CONFIG_SWITCH) += switch/
117 obj-$(CONFIG_INFINIBAND) += infiniband/
118 obj-$(CONFIG_SGI_SN) += sn/
119 obj-y += firmware/
120 obj-$(CONFIG_CRYPTO) += crypto/
121 obj-$(CONFIG_SUPERH) += sh/
122 obj-$(CONFIG_ARCH_SHMOBILE_LEGACY) += sh/
123 ifndef CONFIG_ARCH_USES_GETTIMEOFFSET
124 obj-y += clocksource/
125 endif
126 obj-$(CONFIG_DCA) += dca/
127 obj-$(CONFIG_HID) += hid/
128 obj-$(CONFIG_PPC_PS3) += ps3/
129 obj-$(CONFIG_OF) += of/
130 obj-$(CONFIG_SSB) += ssb/
131 obj-$(CONFIG_BCMA) += bcma/
132 obj-$(CONFIG_VHOST_RING) += vhost/
133 obj-$(CONFIG_VLYNQ) += vlynq/
134 obj-$(CONFIG_STAGING) += staging/
135 obj-y += platform/
136 #common clk code
137 obj-y += clk/
139 obj-$(CONFIG_MAILBOX) += mailbox/
140 obj-$(CONFIG_HWSPINLOCK) += hwspinlock/
141 obj-$(CONFIG_NFC) += nfc/
142 obj-$(CONFIG_IOMMU_SUPPORT) += iommu/
143 obj-$(CONFIG_REMOTEPROC) += remoteproc/
144 obj-$(CONFIG_RPMSG) += rpmsg/
146 # Virtualization drivers
147 obj-$(CONFIG_VIRT_DRIVERS) += virt/
148 obj-$(CONFIG_HYPERV) += hv/
150 obj-$(CONFIG_PM_DEVFREQ) += devfreq/
151 obj-$(CONFIG_EXTCON) += extcon/
152 obj-$(CONFIG_MEMORY) += memory/
153 obj-$(CONFIG_IIO) += iio/
154 obj-$(CONFIG_VME_BUS) += vme/
155 obj-$(CONFIG_IPACK_BUS) += ipack/
156 obj-$(CONFIG_NTB) += ntb/
157 obj-$(CONFIG_FMC) += fmc/
158 obj-$(CONFIG_POWERCAP) += powercap/