1 /*
2 * processor_idle - idle state submodule to the ACPI processor driver
3 *
4 * Copyright (C) 2001, 2002 Andy Grover <andrew.grover@intel.com>
5 * Copyright (C) 2001, 2002 Paul Diefenbaugh <paul.s.diefenbaugh@intel.com>
6 * Copyright (C) 2004, 2005 Dominik Brodowski <linux@brodo.de>
7 * Copyright (C) 2004 Anil S Keshavamurthy <anil.s.keshavamurthy@intel.com>
8 * - Added processor hotplug support
9 * Copyright (C) 2005 Venkatesh Pallipadi <venkatesh.pallipadi@intel.com>
10 * - Added support for C3 on SMP
11 *
12 * ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
13 *
14 * This program is free software; you can redistribute it and/or modify
15 * it under the terms of the GNU General Public License as published by
16 * the Free Software Foundation; either version 2 of the License, or (at
17 * your option) any later version.
18 *
19 * This program is distributed in the hope that it will be useful, but
20 * WITHOUT ANY WARRANTY; without even the implied warranty of
21 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
22 * General Public License for more details.
23 *
24 * You should have received a copy of the GNU General Public License along
25 * with this program; if not, write to the Free Software Foundation, Inc.,
26 * 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA.
27 *
28 * ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
29 */
31 #include <linux/kernel.h>
32 #include <linux/module.h>
33 #include <linux/init.h>
34 #include <linux/cpufreq.h>
35 #include <linux/slab.h>
36 #include <linux/acpi.h>
37 #include <linux/dmi.h>
38 #include <linux/moduleparam.h>
39 #include <linux/sched.h> /* need_resched() */
40 #include <linux/pm_qos.h>
41 #include <linux/clockchips.h>
42 #include <linux/cpuidle.h>
43 #include <linux/irqflags.h>
45 /*
46 * Include the apic definitions for x86 to have the APIC timer related defines
47 * available also for UP (on SMP it gets magically included via linux/smp.h).
48 * asm/acpi.h is not an option, as it would require more include magic. Also
49 * creating an empty asm-ia64/apic.h would just trade pest vs. cholera.
50 */
51 #ifdef CONFIG_X86
52 #include <asm/apic.h>
53 #endif
55 #include <asm/io.h>
56 #include <asm/uaccess.h>
58 #include <acpi/acpi_bus.h>
59 #include <acpi/processor.h>
60 #include <asm/processor.h>
62 #define PREFIX "ACPI: "
64 #define ACPI_PROCESSOR_CLASS "processor"
65 #define _COMPONENT ACPI_PROCESSOR_COMPONENT
66 ACPI_MODULE_NAME("processor_idle");
67 #define PM_TIMER_TICK_NS (1000000000ULL/PM_TIMER_FREQUENCY)
68 #define C2_OVERHEAD 1 /* 1us */
69 #define C3_OVERHEAD 1 /* 1us */
70 #define PM_TIMER_TICKS_TO_US(p) (((p) * 1000)/(PM_TIMER_FREQUENCY/1000))
72 static unsigned int max_cstate __read_mostly = ACPI_PROCESSOR_MAX_POWER;
73 module_param(max_cstate, uint, 0000);
74 static unsigned int nocst __read_mostly;
75 module_param(nocst, uint, 0000);
76 static int bm_check_disable __read_mostly;
77 module_param(bm_check_disable, uint, 0000);
79 static unsigned int latency_factor __read_mostly = 2;
80 module_param(latency_factor, uint, 0644);
82 static DEFINE_PER_CPU(struct cpuidle_device *, acpi_cpuidle_device);
84 static int disabled_by_idle_boot_param(void)
85 {
86 return boot_option_idle_override == IDLE_POLL ||
87 boot_option_idle_override == IDLE_FORCE_MWAIT ||
88 boot_option_idle_override == IDLE_HALT;
89 }
91 /*
92 * IBM ThinkPad R40e crashes mysteriously when going into C2 or C3.
93 * For now disable this. Probably a bug somewhere else.
94 *
95 * To skip this limit, boot/load with a large max_cstate limit.
96 */
97 static int set_max_cstate(const struct dmi_system_id *id)
98 {
99 if (max_cstate > ACPI_PROCESSOR_MAX_POWER)
100 return 0;
102 printk(KERN_NOTICE PREFIX "%s detected - limiting to C%ld max_cstate."
103 " Override with \"processor.max_cstate=%d\"\n", id->ident,
104 (long)id->driver_data, ACPI_PROCESSOR_MAX_POWER + 1);
106 max_cstate = (long)id->driver_data;
108 return 0;
109 }
111 /* Actually this shouldn't be __cpuinitdata, would be better to fix the
112 callers to only run once -AK */
113 static struct dmi_system_id __cpuinitdata processor_power_dmi_table[] = {
114 { set_max_cstate, "Clevo 5600D", {
115 DMI_MATCH(DMI_BIOS_VENDOR,"Phoenix Technologies LTD"),
116 DMI_MATCH(DMI_BIOS_VERSION,"SHE845M0.86C.0013.D.0302131307")},
117 (void *)2},
118 { set_max_cstate, "Pavilion zv5000", {
119 DMI_MATCH(DMI_SYS_VENDOR, "Hewlett-Packard"),
120 DMI_MATCH(DMI_PRODUCT_NAME,"Pavilion zv5000 (DS502A#ABA)")},
121 (void *)1},
122 { set_max_cstate, "Asus L8400B", {
123 DMI_MATCH(DMI_SYS_VENDOR, "ASUSTeK Computer Inc."),
124 DMI_MATCH(DMI_PRODUCT_NAME,"L8400B series Notebook PC")},
125 (void *)1},
126 {},
127 };
130 /*
131 * Callers should disable interrupts before the call and enable
132 * interrupts after return.
133 */
134 static void acpi_safe_halt(void)
135 {
136 current_thread_info()->status &= ~TS_POLLING;
137 /*
138 * TS_POLLING-cleared state must be visible before we
139 * test NEED_RESCHED:
140 */
141 smp_mb();
142 if (!need_resched()) {
143 safe_halt();
144 local_irq_disable();
145 }
146 current_thread_info()->status |= TS_POLLING;
147 }
149 #ifdef ARCH_APICTIMER_STOPS_ON_C3
151 /*
152 * Some BIOS implementations switch to C3 in the published C2 state.
153 * This seems to be a common problem on AMD boxen, but other vendors
154 * are affected too. We pick the most conservative approach: we assume
155 * that the local APIC stops in both C2 and C3.
156 */
157 static void lapic_timer_check_state(int state, struct acpi_processor *pr,
158 struct acpi_processor_cx *cx)
159 {
160 struct acpi_processor_power *pwr = &pr->power;
161 u8 type = local_apic_timer_c2_ok ? ACPI_STATE_C3 : ACPI_STATE_C2;
163 if (cpu_has(&cpu_data(pr->id), X86_FEATURE_ARAT))
164 return;
166 if (amd_e400_c1e_detected)
167 type = ACPI_STATE_C1;
169 /*
170 * Check, if one of the previous states already marked the lapic
171 * unstable
172 */
173 if (pwr->timer_broadcast_on_state < state)
174 return;
176 if (cx->type >= type)
177 pr->power.timer_broadcast_on_state = state;
178 }
180 static void __lapic_timer_propagate_broadcast(void *arg)
181 {
182 struct acpi_processor *pr = (struct acpi_processor *) arg;
183 unsigned long reason;
185 reason = pr->power.timer_broadcast_on_state < INT_MAX ?
186 CLOCK_EVT_NOTIFY_BROADCAST_ON : CLOCK_EVT_NOTIFY_BROADCAST_OFF;
188 clockevents_notify(reason, &pr->id);
189 }
191 static void lapic_timer_propagate_broadcast(struct acpi_processor *pr)
192 {
193 smp_call_function_single(pr->id, __lapic_timer_propagate_broadcast,
194 (void *)pr, 1);
195 }
197 /* Power(C) State timer broadcast control */
198 static void lapic_timer_state_broadcast(struct acpi_processor *pr,
199 struct acpi_processor_cx *cx,
200 int broadcast)
201 {
202 int state = cx - pr->power.states;
204 if (state >= pr->power.timer_broadcast_on_state) {
205 unsigned long reason;
207 reason = broadcast ? CLOCK_EVT_NOTIFY_BROADCAST_ENTER :
208 CLOCK_EVT_NOTIFY_BROADCAST_EXIT;
209 clockevents_notify(reason, &pr->id);
210 }
211 }
213 #else
215 static void lapic_timer_check_state(int state, struct acpi_processor *pr,
216 struct acpi_processor_cx *cstate) { }
217 static void lapic_timer_propagate_broadcast(struct acpi_processor *pr) { }
218 static void lapic_timer_state_broadcast(struct acpi_processor *pr,
219 struct acpi_processor_cx *cx,
220 int broadcast)
221 {
222 }
224 #endif
226 static u32 saved_bm_rld;
228 static void acpi_idle_bm_rld_save(void)
229 {
230 acpi_read_bit_register(ACPI_BITREG_BUS_MASTER_RLD, &saved_bm_rld);
231 }
232 static void acpi_idle_bm_rld_restore(void)
233 {
234 u32 resumed_bm_rld;
236 acpi_read_bit_register(ACPI_BITREG_BUS_MASTER_RLD, &resumed_bm_rld);
238 if (resumed_bm_rld != saved_bm_rld)
239 acpi_write_bit_register(ACPI_BITREG_BUS_MASTER_RLD, saved_bm_rld);
240 }
242 int acpi_processor_suspend(struct device *dev)
243 {
244 acpi_idle_bm_rld_save();
245 return 0;
246 }
248 int acpi_processor_resume(struct device *dev)
249 {
250 acpi_idle_bm_rld_restore();
251 return 0;
252 }
254 #if defined(CONFIG_X86)
255 static void tsc_check_state(int state)
256 {
257 switch (boot_cpu_data.x86_vendor) {
258 case X86_VENDOR_AMD:
259 case X86_VENDOR_INTEL:
260 /*
261 * AMD Fam10h TSC will tick in all
262 * C/P/S0/S1 states when this bit is set.
263 */
264 if (boot_cpu_has(X86_FEATURE_NONSTOP_TSC))
265 return;
267 /*FALL THROUGH*/
268 default:
269 /* TSC could halt in idle, so notify users */
270 if (state > ACPI_STATE_C1)
271 mark_tsc_unstable("TSC halts in idle");
272 }
273 }
274 #else
275 static void tsc_check_state(int state) { return; }
276 #endif
278 static int acpi_processor_get_power_info_fadt(struct acpi_processor *pr)
279 {
281 if (!pr)
282 return -EINVAL;
284 if (!pr->pblk)
285 return -ENODEV;
287 /* if info is obtained from pblk/fadt, type equals state */
288 pr->power.states[ACPI_STATE_C2].type = ACPI_STATE_C2;
289 pr->power.states[ACPI_STATE_C3].type = ACPI_STATE_C3;
291 #ifndef CONFIG_HOTPLUG_CPU
292 /*
293 * Check for P_LVL2_UP flag before entering C2 and above on
294 * an SMP system.
295 */
296 if ((num_online_cpus() > 1) &&
297 !(acpi_gbl_FADT.flags & ACPI_FADT_C2_MP_SUPPORTED))
298 return -ENODEV;
299 #endif
301 /* determine C2 and C3 address from pblk */
302 pr->power.states[ACPI_STATE_C2].address = pr->pblk + 4;
303 pr->power.states[ACPI_STATE_C3].address = pr->pblk + 5;
305 /* determine latencies from FADT */
306 pr->power.states[ACPI_STATE_C2].latency = acpi_gbl_FADT.c2_latency;
307 pr->power.states[ACPI_STATE_C3].latency = acpi_gbl_FADT.c3_latency;
309 /*
310 * FADT specified C2 latency must be less than or equal to
311 * 100 microseconds.
312 */
313 if (acpi_gbl_FADT.c2_latency > ACPI_PROCESSOR_MAX_C2_LATENCY) {
314 ACPI_DEBUG_PRINT((ACPI_DB_INFO,
315 "C2 latency too large [%d]\n", acpi_gbl_FADT.c2_latency));
316 /* invalidate C2 */
317 pr->power.states[ACPI_STATE_C2].address = 0;
318 }
320 /*
321 * FADT supplied C3 latency must be less than or equal to
322 * 1000 microseconds.
323 */
324 if (acpi_gbl_FADT.c3_latency > ACPI_PROCESSOR_MAX_C3_LATENCY) {
325 ACPI_DEBUG_PRINT((ACPI_DB_INFO,
326 "C3 latency too large [%d]\n", acpi_gbl_FADT.c3_latency));
327 /* invalidate C3 */
328 pr->power.states[ACPI_STATE_C3].address = 0;
329 }
331 ACPI_DEBUG_PRINT((ACPI_DB_INFO,
332 "lvl2[0x%08x] lvl3[0x%08x]\n",
333 pr->power.states[ACPI_STATE_C2].address,
334 pr->power.states[ACPI_STATE_C3].address));
336 return 0;
337 }
339 static int acpi_processor_get_power_info_default(struct acpi_processor *pr)
340 {
341 if (!pr->power.states[ACPI_STATE_C1].valid) {
342 /* set the first C-State to C1 */
343 /* all processors need to support C1 */
344 pr->power.states[ACPI_STATE_C1].type = ACPI_STATE_C1;
345 pr->power.states[ACPI_STATE_C1].valid = 1;
346 pr->power.states[ACPI_STATE_C1].entry_method = ACPI_CSTATE_HALT;
347 }
348 /* the C0 state only exists as a filler in our array */
349 pr->power.states[ACPI_STATE_C0].valid = 1;
350 return 0;
351 }
353 static int acpi_processor_get_power_info_cst(struct acpi_processor *pr)
354 {
355 acpi_status status = 0;
356 u64 count;
357 int current_count;
358 int i;
359 struct acpi_buffer buffer = { ACPI_ALLOCATE_BUFFER, NULL };
360 union acpi_object *cst;
363 if (nocst)
364 return -ENODEV;
366 current_count = 0;
368 status = acpi_evaluate_object(pr->handle, "_CST", NULL, &buffer);
369 if (ACPI_FAILURE(status)) {
370 ACPI_DEBUG_PRINT((ACPI_DB_INFO, "No _CST, giving up\n"));
371 return -ENODEV;
372 }
374 cst = buffer.pointer;
376 /* There must be at least 2 elements */
377 if (!cst || (cst->type != ACPI_TYPE_PACKAGE) || cst->package.count < 2) {
378 printk(KERN_ERR PREFIX "not enough elements in _CST\n");
379 status = -EFAULT;
380 goto end;
381 }
383 count = cst->package.elements[0].integer.value;
385 /* Validate number of power states. */
386 if (count < 1 || count != cst->package.count - 1) {
387 printk(KERN_ERR PREFIX "count given by _CST is not valid\n");
388 status = -EFAULT;
389 goto end;
390 }
392 /* Tell driver that at least _CST is supported. */
393 pr->flags.has_cst = 1;
395 for (i = 1; i <= count; i++) {
396 union acpi_object *element;
397 union acpi_object *obj;
398 struct acpi_power_register *reg;
399 struct acpi_processor_cx cx;
401 memset(&cx, 0, sizeof(cx));
403 element = &(cst->package.elements[i]);
404 if (element->type != ACPI_TYPE_PACKAGE)
405 continue;
407 if (element->package.count != 4)
408 continue;
410 obj = &(element->package.elements[0]);
412 if (obj->type != ACPI_TYPE_BUFFER)
413 continue;
415 reg = (struct acpi_power_register *)obj->buffer.pointer;
417 if (reg->space_id != ACPI_ADR_SPACE_SYSTEM_IO &&
418 (reg->space_id != ACPI_ADR_SPACE_FIXED_HARDWARE))
419 continue;
421 /* There should be an easy way to extract an integer... */
422 obj = &(element->package.elements[1]);
423 if (obj->type != ACPI_TYPE_INTEGER)
424 continue;
426 cx.type = obj->integer.value;
427 /*
428 * Some buggy BIOSes won't list C1 in _CST -
429 * Let acpi_processor_get_power_info_default() handle them later
430 */
431 if (i == 1 && cx.type != ACPI_STATE_C1)
432 current_count++;
434 cx.address = reg->address;
435 cx.index = current_count + 1;
437 cx.entry_method = ACPI_CSTATE_SYSTEMIO;
438 if (reg->space_id == ACPI_ADR_SPACE_FIXED_HARDWARE) {
439 if (acpi_processor_ffh_cstate_probe
440 (pr->id, &cx, reg) == 0) {
441 cx.entry_method = ACPI_CSTATE_FFH;
442 } else if (cx.type == ACPI_STATE_C1) {
443 /*
444 * C1 is a special case where FIXED_HARDWARE
445 * can be handled in non-MWAIT way as well.
446 * In that case, save this _CST entry info.
447 * Otherwise, ignore this info and continue.
448 */
449 cx.entry_method = ACPI_CSTATE_HALT;
450 snprintf(cx.desc, ACPI_CX_DESC_LEN, "ACPI HLT");
451 } else {
452 continue;
453 }
454 if (cx.type == ACPI_STATE_C1 &&
455 (boot_option_idle_override == IDLE_NOMWAIT)) {
456 /*
457 * In most cases the C1 space_id obtained from
458 * _CST object is FIXED_HARDWARE access mode.
459 * But when the option of idle=halt is added,
460 * the entry_method type should be changed from
461 * CSTATE_FFH to CSTATE_HALT.
462 * When the option of idle=nomwait is added,
463 * the C1 entry_method type should be
464 * CSTATE_HALT.
465 */
466 cx.entry_method = ACPI_CSTATE_HALT;
467 snprintf(cx.desc, ACPI_CX_DESC_LEN, "ACPI HLT");
468 }
469 } else {
470 snprintf(cx.desc, ACPI_CX_DESC_LEN, "ACPI IOPORT 0x%x",
471 cx.address);
472 }
474 if (cx.type == ACPI_STATE_C1) {
475 cx.valid = 1;
476 }
478 obj = &(element->package.elements[2]);
479 if (obj->type != ACPI_TYPE_INTEGER)
480 continue;
482 cx.latency = obj->integer.value;
484 obj = &(element->package.elements[3]);
485 if (obj->type != ACPI_TYPE_INTEGER)
486 continue;
488 current_count++;
489 memcpy(&(pr->power.states[current_count]), &cx, sizeof(cx));
491 /*
492 * We support total ACPI_PROCESSOR_MAX_POWER - 1
493 * (From 1 through ACPI_PROCESSOR_MAX_POWER - 1)
494 */
495 if (current_count >= (ACPI_PROCESSOR_MAX_POWER - 1)) {
496 printk(KERN_WARNING
497 "Limiting number of power states to max (%d)\n",
498 ACPI_PROCESSOR_MAX_POWER);
499 printk(KERN_WARNING
500 "Please increase ACPI_PROCESSOR_MAX_POWER if needed.\n");
501 break;
502 }
503 }
505 ACPI_DEBUG_PRINT((ACPI_DB_INFO, "Found %d power states\n",
506 current_count));
508 /* Validate number of power states discovered */
509 if (current_count < 2)
510 status = -EFAULT;
512 end:
513 kfree(buffer.pointer);
515 return status;
516 }
518 static void acpi_processor_power_verify_c3(struct acpi_processor *pr,
519 struct acpi_processor_cx *cx)
520 {
521 static int bm_check_flag = -1;
522 static int bm_control_flag = -1;
525 if (!cx->address)
526 return;
528 /*
529 * PIIX4 Erratum #18: We don't support C3 when Type-F (fast)
530 * DMA transfers are used by any ISA device to avoid livelock.
531 * Note that we could disable Type-F DMA (as recommended by
532 * the erratum), but this is known to disrupt certain ISA
533 * devices thus we take the conservative approach.
534 */
535 else if (errata.piix4.fdma) {
536 ACPI_DEBUG_PRINT((ACPI_DB_INFO,
537 "C3 not supported on PIIX4 with Type-F DMA\n"));
538 return;
539 }
541 /* All the logic here assumes flags.bm_check is same across all CPUs */
542 if (bm_check_flag == -1) {
543 /* Determine whether bm_check is needed based on CPU */
544 acpi_processor_power_init_bm_check(&(pr->flags), pr->id);
545 bm_check_flag = pr->flags.bm_check;
546 bm_control_flag = pr->flags.bm_control;
547 } else {
548 pr->flags.bm_check = bm_check_flag;
549 pr->flags.bm_control = bm_control_flag;
550 }
552 if (pr->flags.bm_check) {
553 if (!pr->flags.bm_control) {
554 if (pr->flags.has_cst != 1) {
555 /* bus mastering control is necessary */
556 ACPI_DEBUG_PRINT((ACPI_DB_INFO,
557 "C3 support requires BM control\n"));
558 return;
559 } else {
560 /* Here we enter C3 without bus mastering */
561 ACPI_DEBUG_PRINT((ACPI_DB_INFO,
562 "C3 support without BM control\n"));
563 }
564 }
565 } else {
566 /*
567 * WBINVD should be set in fadt, for C3 state to be
568 * supported on when bm_check is not required.
569 */
570 if (!(acpi_gbl_FADT.flags & ACPI_FADT_WBINVD)) {
571 ACPI_DEBUG_PRINT((ACPI_DB_INFO,
572 "Cache invalidation should work properly"
573 " for C3 to be enabled on SMP systems\n"));
574 return;
575 }
576 }
578 /*
579 * Otherwise we've met all of our C3 requirements.
580 * Normalize the C3 latency to expidite policy. Enable
581 * checking of bus mastering status (bm_check) so we can
582 * use this in our C3 policy
583 */
584 cx->valid = 1;
586 /*
587 * On older chipsets, BM_RLD needs to be set
588 * in order for Bus Master activity to wake the
589 * system from C3. Newer chipsets handle DMA
590 * during C3 automatically and BM_RLD is a NOP.
591 * In either case, the proper way to
592 * handle BM_RLD is to set it and leave it set.
593 */
594 acpi_write_bit_register(ACPI_BITREG_BUS_MASTER_RLD, 1);
596 return;
597 }
599 static int acpi_processor_power_verify(struct acpi_processor *pr)
600 {
601 unsigned int i;
602 unsigned int working = 0;
604 pr->power.timer_broadcast_on_state = INT_MAX;
606 for (i = 1; i < ACPI_PROCESSOR_MAX_POWER && i <= max_cstate; i++) {
607 struct acpi_processor_cx *cx = &pr->power.states[i];
609 switch (cx->type) {
610 case ACPI_STATE_C1:
611 cx->valid = 1;
612 break;
614 case ACPI_STATE_C2:
615 if (!cx->address)
616 break;
617 cx->valid = 1;
618 break;
620 case ACPI_STATE_C3:
621 acpi_processor_power_verify_c3(pr, cx);
622 break;
623 }
624 if (!cx->valid)
625 continue;
627 lapic_timer_check_state(i, pr, cx);
628 tsc_check_state(cx->type);
629 working++;
630 }
632 lapic_timer_propagate_broadcast(pr);
634 return (working);
635 }
637 static int acpi_processor_get_power_info(struct acpi_processor *pr)
638 {
639 unsigned int i;
640 int result;
643 /* NOTE: the idle thread may not be running while calling
644 * this function */
646 /* Zero initialize all the C-states info. */
647 memset(pr->power.states, 0, sizeof(pr->power.states));
649 result = acpi_processor_get_power_info_cst(pr);
650 if (result == -ENODEV)
651 result = acpi_processor_get_power_info_fadt(pr);
653 if (result)
654 return result;
656 acpi_processor_get_power_info_default(pr);
658 pr->power.count = acpi_processor_power_verify(pr);
660 /*
661 * if one state of type C2 or C3 is available, mark this
662 * CPU as being "idle manageable"
663 */
664 for (i = 1; i < ACPI_PROCESSOR_MAX_POWER; i++) {
665 if (pr->power.states[i].valid) {
666 pr->power.count = i;
667 if (pr->power.states[i].type >= ACPI_STATE_C2)
668 pr->flags.power = 1;
669 }
670 }
672 return 0;
673 }
675 /**
676 * acpi_idle_bm_check - checks if bus master activity was detected
677 */
678 static int acpi_idle_bm_check(void)
679 {
680 u32 bm_status = 0;
682 if (bm_check_disable)
683 return 0;
685 acpi_read_bit_register(ACPI_BITREG_BUS_MASTER_STATUS, &bm_status);
686 if (bm_status)
687 acpi_write_bit_register(ACPI_BITREG_BUS_MASTER_STATUS, 1);
688 /*
689 * PIIX4 Erratum #18: Note that BM_STS doesn't always reflect
690 * the true state of bus mastering activity; forcing us to
691 * manually check the BMIDEA bit of each IDE channel.
692 */
693 else if (errata.piix4.bmisx) {
694 if ((inb_p(errata.piix4.bmisx + 0x02) & 0x01)
695 || (inb_p(errata.piix4.bmisx + 0x0A) & 0x01))
696 bm_status = 1;
697 }
698 return bm_status;
699 }
701 /**
702 * acpi_idle_do_entry - a helper function that does C2 and C3 type entry
703 * @cx: cstate data
704 *
705 * Caller disables interrupt before call and enables interrupt after return.
706 */
707 static inline void acpi_idle_do_entry(struct acpi_processor_cx *cx)
708 {
709 /* Don't trace irqs off for idle */
710 stop_critical_timings();
711 if (cx->entry_method == ACPI_CSTATE_FFH) {
712 /* Call into architectural FFH based C-state */
713 acpi_processor_ffh_cstate_enter(cx);
714 } else if (cx->entry_method == ACPI_CSTATE_HALT) {
715 acpi_safe_halt();
716 } else {
717 /* IO port based C-state */
718 inb(cx->address);
719 /* Dummy wait op - must do something useless after P_LVL2 read
720 because chipsets cannot guarantee that STPCLK# signal
721 gets asserted in time to freeze execution properly. */
722 inl(acpi_gbl_FADT.xpm_timer_block.address);
723 }
724 start_critical_timings();
725 }
727 /**
728 * acpi_idle_enter_c1 - enters an ACPI C1 state-type
729 * @dev: the target CPU
730 * @drv: cpuidle driver containing cpuidle state info
731 * @index: index of target state
732 *
733 * This is equivalent to the HALT instruction.
734 */
735 static int acpi_idle_enter_c1(struct cpuidle_device *dev,
736 struct cpuidle_driver *drv, int index)
737 {
738 struct acpi_processor *pr;
739 struct cpuidle_state_usage *state_usage = &dev->states_usage[index];
740 struct acpi_processor_cx *cx = cpuidle_get_statedata(state_usage);
742 pr = __this_cpu_read(processors);
744 if (unlikely(!pr))
745 return -EINVAL;
747 lapic_timer_state_broadcast(pr, cx, 1);
748 acpi_idle_do_entry(cx);
750 lapic_timer_state_broadcast(pr, cx, 0);
752 return index;
753 }
756 /**
757 * acpi_idle_play_dead - enters an ACPI state for long-term idle (i.e. off-lining)
758 * @dev: the target CPU
759 * @index: the index of suggested state
760 */
761 static int acpi_idle_play_dead(struct cpuidle_device *dev, int index)
762 {
763 struct cpuidle_state_usage *state_usage = &dev->states_usage[index];
764 struct acpi_processor_cx *cx = cpuidle_get_statedata(state_usage);
766 ACPI_FLUSH_CPU_CACHE();
768 while (1) {
770 if (cx->entry_method == ACPI_CSTATE_HALT)
771 safe_halt();
772 else if (cx->entry_method == ACPI_CSTATE_SYSTEMIO) {
773 inb(cx->address);
774 /* See comment in acpi_idle_do_entry() */
775 inl(acpi_gbl_FADT.xpm_timer_block.address);
776 } else
777 return -ENODEV;
778 }
780 /* Never reached */
781 return 0;
782 }
784 /**
785 * acpi_idle_enter_simple - enters an ACPI state without BM handling
786 * @dev: the target CPU
787 * @drv: cpuidle driver with cpuidle state information
788 * @index: the index of suggested state
789 */
790 static int acpi_idle_enter_simple(struct cpuidle_device *dev,
791 struct cpuidle_driver *drv, int index)
792 {
793 struct acpi_processor *pr;
794 struct cpuidle_state_usage *state_usage = &dev->states_usage[index];
795 struct acpi_processor_cx *cx = cpuidle_get_statedata(state_usage);
797 pr = __this_cpu_read(processors);
799 if (unlikely(!pr))
800 return -EINVAL;
802 if (cx->entry_method != ACPI_CSTATE_FFH) {
803 current_thread_info()->status &= ~TS_POLLING;
804 /*
805 * TS_POLLING-cleared state must be visible before we test
806 * NEED_RESCHED:
807 */
808 smp_mb();
810 if (unlikely(need_resched())) {
811 current_thread_info()->status |= TS_POLLING;
812 return -EINVAL;
813 }
814 }
816 /*
817 * Must be done before busmaster disable as we might need to
818 * access HPET !
819 */
820 lapic_timer_state_broadcast(pr, cx, 1);
822 if (cx->type == ACPI_STATE_C3)
823 ACPI_FLUSH_CPU_CACHE();
825 /* Tell the scheduler that we are going deep-idle: */
826 sched_clock_idle_sleep_event();
827 acpi_idle_do_entry(cx);
829 sched_clock_idle_wakeup_event(0);
831 if (cx->entry_method != ACPI_CSTATE_FFH)
832 current_thread_info()->status |= TS_POLLING;
834 lapic_timer_state_broadcast(pr, cx, 0);
835 return index;
836 }
838 static int c3_cpu_count;
839 static DEFINE_RAW_SPINLOCK(c3_lock);
841 /**
842 * acpi_idle_enter_bm - enters C3 with proper BM handling
843 * @dev: the target CPU
844 * @drv: cpuidle driver containing state data
845 * @index: the index of suggested state
846 *
847 * If BM is detected, the deepest non-C3 idle state is entered instead.
848 */
849 static int acpi_idle_enter_bm(struct cpuidle_device *dev,
850 struct cpuidle_driver *drv, int index)
851 {
852 struct acpi_processor *pr;
853 struct cpuidle_state_usage *state_usage = &dev->states_usage[index];
854 struct acpi_processor_cx *cx = cpuidle_get_statedata(state_usage);
856 pr = __this_cpu_read(processors);
858 if (unlikely(!pr))
859 return -EINVAL;
861 if (!cx->bm_sts_skip && acpi_idle_bm_check()) {
862 if (drv->safe_state_index >= 0) {
863 return drv->states[drv->safe_state_index].enter(dev,
864 drv, drv->safe_state_index);
865 } else {
866 acpi_safe_halt();
867 return -EBUSY;
868 }
869 }
871 if (cx->entry_method != ACPI_CSTATE_FFH) {
872 current_thread_info()->status &= ~TS_POLLING;
873 /*
874 * TS_POLLING-cleared state must be visible before we test
875 * NEED_RESCHED:
876 */
877 smp_mb();
879 if (unlikely(need_resched())) {
880 current_thread_info()->status |= TS_POLLING;
881 return -EINVAL;
882 }
883 }
885 acpi_unlazy_tlb(smp_processor_id());
887 /* Tell the scheduler that we are going deep-idle: */
888 sched_clock_idle_sleep_event();
889 /*
890 * Must be done before busmaster disable as we might need to
891 * access HPET !
892 */
893 lapic_timer_state_broadcast(pr, cx, 1);
895 /*
896 * disable bus master
897 * bm_check implies we need ARB_DIS
898 * !bm_check implies we need cache flush
899 * bm_control implies whether we can do ARB_DIS
900 *
901 * That leaves a case where bm_check is set and bm_control is
902 * not set. In that case we cannot do much, we enter C3
903 * without doing anything.
904 */
905 if (pr->flags.bm_check && pr->flags.bm_control) {
906 raw_spin_lock(&c3_lock);
907 c3_cpu_count++;
908 /* Disable bus master arbitration when all CPUs are in C3 */
909 if (c3_cpu_count == num_online_cpus())
910 acpi_write_bit_register(ACPI_BITREG_ARB_DISABLE, 1);
911 raw_spin_unlock(&c3_lock);
912 } else if (!pr->flags.bm_check) {
913 ACPI_FLUSH_CPU_CACHE();
914 }
916 acpi_idle_do_entry(cx);
918 /* Re-enable bus master arbitration */
919 if (pr->flags.bm_check && pr->flags.bm_control) {
920 raw_spin_lock(&c3_lock);
921 acpi_write_bit_register(ACPI_BITREG_ARB_DISABLE, 0);
922 c3_cpu_count--;
923 raw_spin_unlock(&c3_lock);
924 }
926 sched_clock_idle_wakeup_event(0);
928 if (cx->entry_method != ACPI_CSTATE_FFH)
929 current_thread_info()->status |= TS_POLLING;
931 lapic_timer_state_broadcast(pr, cx, 0);
932 return index;
933 }
935 struct cpuidle_driver acpi_idle_driver = {
936 .name = "acpi_idle",
937 .owner = THIS_MODULE,
938 .en_core_tk_irqen = 1,
939 };
941 /**
942 * acpi_processor_setup_cpuidle_cx - prepares and configures CPUIDLE
943 * device i.e. per-cpu data
944 *
945 * @pr: the ACPI processor
946 */
947 static int acpi_processor_setup_cpuidle_cx(struct acpi_processor *pr)
948 {
949 int i, count = CPUIDLE_DRIVER_STATE_START;
950 struct acpi_processor_cx *cx;
951 struct cpuidle_state_usage *state_usage;
952 struct cpuidle_device *dev = per_cpu(acpi_cpuidle_device, pr->id);
954 if (!pr->flags.power_setup_done)
955 return -EINVAL;
957 if (pr->flags.power == 0) {
958 return -EINVAL;
959 }
961 if (!dev)
962 return -EINVAL;
964 dev->cpu = pr->id;
966 if (max_cstate == 0)
967 max_cstate = 1;
969 for (i = 1; i < ACPI_PROCESSOR_MAX_POWER && i <= max_cstate; i++) {
970 cx = &pr->power.states[i];
971 state_usage = &dev->states_usage[count];
973 if (!cx->valid)
974 continue;
976 #ifdef CONFIG_HOTPLUG_CPU
977 if ((cx->type != ACPI_STATE_C1) && (num_online_cpus() > 1) &&
978 !pr->flags.has_cst &&
979 !(acpi_gbl_FADT.flags & ACPI_FADT_C2_MP_SUPPORTED))
980 continue;
981 #endif
983 cpuidle_set_statedata(state_usage, cx);
985 count++;
986 if (count == CPUIDLE_STATE_MAX)
987 break;
988 }
990 dev->state_count = count;
992 if (!count)
993 return -EINVAL;
995 return 0;
996 }
998 /**
999 * acpi_processor_setup_cpuidle states- prepares and configures cpuidle
1000 * global state data i.e. idle routines
1001 *
1002 * @pr: the ACPI processor
1003 */
1004 static int acpi_processor_setup_cpuidle_states(struct acpi_processor *pr)
1005 {
1006 int i, count = CPUIDLE_DRIVER_STATE_START;
1007 struct acpi_processor_cx *cx;
1008 struct cpuidle_state *state;
1009 struct cpuidle_driver *drv = &acpi_idle_driver;
1011 if (!pr->flags.power_setup_done)
1012 return -EINVAL;
1014 if (pr->flags.power == 0)
1015 return -EINVAL;
1017 drv->safe_state_index = -1;
1018 for (i = 0; i < CPUIDLE_STATE_MAX; i++) {
1019 drv->states[i].name[0] = '\0';
1020 drv->states[i].desc[0] = '\0';
1021 }
1023 if (max_cstate == 0)
1024 max_cstate = 1;
1026 for (i = 1; i < ACPI_PROCESSOR_MAX_POWER && i <= max_cstate; i++) {
1027 cx = &pr->power.states[i];
1029 if (!cx->valid)
1030 continue;
1032 #ifdef CONFIG_HOTPLUG_CPU
1033 if ((cx->type != ACPI_STATE_C1) && (num_online_cpus() > 1) &&
1034 !pr->flags.has_cst &&
1035 !(acpi_gbl_FADT.flags & ACPI_FADT_C2_MP_SUPPORTED))
1036 continue;
1037 #endif
1039 state = &drv->states[count];
1040 snprintf(state->name, CPUIDLE_NAME_LEN, "C%d", i);
1041 strncpy(state->desc, cx->desc, CPUIDLE_DESC_LEN);
1042 state->exit_latency = cx->latency;
1043 state->target_residency = cx->latency * latency_factor;
1045 state->flags = 0;
1046 switch (cx->type) {
1047 case ACPI_STATE_C1:
1048 if (cx->entry_method == ACPI_CSTATE_FFH)
1049 state->flags |= CPUIDLE_FLAG_TIME_VALID;
1051 state->enter = acpi_idle_enter_c1;
1052 state->enter_dead = acpi_idle_play_dead;
1053 drv->safe_state_index = count;
1054 break;
1056 case ACPI_STATE_C2:
1057 state->flags |= CPUIDLE_FLAG_TIME_VALID;
1058 state->enter = acpi_idle_enter_simple;
1059 state->enter_dead = acpi_idle_play_dead;
1060 drv->safe_state_index = count;
1061 break;
1063 case ACPI_STATE_C3:
1064 state->flags |= CPUIDLE_FLAG_TIME_VALID;
1065 state->enter = pr->flags.bm_check ?
1066 acpi_idle_enter_bm :
1067 acpi_idle_enter_simple;
1068 break;
1069 }
1071 count++;
1072 if (count == CPUIDLE_STATE_MAX)
1073 break;
1074 }
1076 drv->state_count = count;
1078 if (!count)
1079 return -EINVAL;
1081 return 0;
1082 }
1084 int acpi_processor_hotplug(struct acpi_processor *pr)
1085 {
1086 int ret = 0;
1087 struct cpuidle_device *dev;
1089 if (disabled_by_idle_boot_param())
1090 return 0;
1092 if (!pr)
1093 return -EINVAL;
1095 if (nocst) {
1096 return -ENODEV;
1097 }
1099 if (!pr->flags.power_setup_done)
1100 return -ENODEV;
1102 dev = per_cpu(acpi_cpuidle_device, pr->id);
1103 cpuidle_pause_and_lock();
1104 cpuidle_disable_device(dev);
1105 acpi_processor_get_power_info(pr);
1106 if (pr->flags.power) {
1107 acpi_processor_setup_cpuidle_cx(pr);
1108 ret = cpuidle_enable_device(dev);
1109 }
1110 cpuidle_resume_and_unlock();
1112 return ret;
1113 }
1115 int acpi_processor_cst_has_changed(struct acpi_processor *pr)
1116 {
1117 int cpu;
1118 struct acpi_processor *_pr;
1119 struct cpuidle_device *dev;
1121 if (disabled_by_idle_boot_param())
1122 return 0;
1124 if (!pr)
1125 return -EINVAL;
1127 if (nocst)
1128 return -ENODEV;
1130 if (!pr->flags.power_setup_done)
1131 return -ENODEV;
1133 /*
1134 * FIXME: Design the ACPI notification to make it once per
1135 * system instead of once per-cpu. This condition is a hack
1136 * to make the code that updates C-States be called once.
1137 */
1139 if (pr->id == 0 && cpuidle_get_driver() == &acpi_idle_driver) {
1141 cpuidle_pause_and_lock();
1142 /* Protect against cpu-hotplug */
1143 get_online_cpus();
1145 /* Disable all cpuidle devices */
1146 for_each_online_cpu(cpu) {
1147 _pr = per_cpu(processors, cpu);
1148 if (!_pr || !_pr->flags.power_setup_done)
1149 continue;
1150 dev = per_cpu(acpi_cpuidle_device, cpu);
1151 cpuidle_disable_device(dev);
1152 }
1154 /* Populate Updated C-state information */
1155 acpi_processor_get_power_info(pr);
1156 acpi_processor_setup_cpuidle_states(pr);
1158 /* Enable all cpuidle devices */
1159 for_each_online_cpu(cpu) {
1160 _pr = per_cpu(processors, cpu);
1161 if (!_pr || !_pr->flags.power_setup_done)
1162 continue;
1163 acpi_processor_get_power_info(_pr);
1164 if (_pr->flags.power) {
1165 acpi_processor_setup_cpuidle_cx(_pr);
1166 dev = per_cpu(acpi_cpuidle_device, cpu);
1167 cpuidle_enable_device(dev);
1168 }
1169 }
1170 put_online_cpus();
1171 cpuidle_resume_and_unlock();
1172 }
1174 return 0;
1175 }
1177 static int acpi_processor_registered;
1179 int __cpuinit acpi_processor_power_init(struct acpi_processor *pr)
1180 {
1181 acpi_status status = 0;
1182 int retval;
1183 struct cpuidle_device *dev;
1184 static int first_run;
1186 if (disabled_by_idle_boot_param())
1187 return 0;
1189 if (!first_run) {
1190 dmi_check_system(processor_power_dmi_table);
1191 max_cstate = acpi_processor_cstate_check(max_cstate);
1192 if (max_cstate < ACPI_C_STATES_MAX)
1193 printk(KERN_NOTICE
1194 "ACPI: processor limited to max C-state %d\n",
1195 max_cstate);
1196 first_run++;
1197 }
1199 if (!pr)
1200 return -EINVAL;
1202 if (acpi_gbl_FADT.cst_control && !nocst) {
1203 status =
1204 acpi_os_write_port(acpi_gbl_FADT.smi_command, acpi_gbl_FADT.cst_control, 8);
1205 if (ACPI_FAILURE(status)) {
1206 ACPI_EXCEPTION((AE_INFO, status,
1207 "Notifying BIOS of _CST ability failed"));
1208 }
1209 }
1211 acpi_processor_get_power_info(pr);
1212 pr->flags.power_setup_done = 1;
1214 /*
1215 * Install the idle handler if processor power management is supported.
1216 * Note that we use previously set idle handler will be used on
1217 * platforms that only support C1.
1218 */
1219 if (pr->flags.power) {
1220 /* Register acpi_idle_driver if not already registered */
1221 if (!acpi_processor_registered) {
1222 acpi_processor_setup_cpuidle_states(pr);
1223 retval = cpuidle_register_driver(&acpi_idle_driver);
1224 if (retval)
1225 return retval;
1226 printk(KERN_DEBUG "ACPI: %s registered with cpuidle\n",
1227 acpi_idle_driver.name);
1228 }
1230 dev = kzalloc(sizeof(*dev), GFP_KERNEL);
1231 if (!dev)
1232 return -ENOMEM;
1233 per_cpu(acpi_cpuidle_device, pr->id) = dev;
1235 acpi_processor_setup_cpuidle_cx(pr);
1237 /* Register per-cpu cpuidle_device. Cpuidle driver
1238 * must already be registered before registering device
1239 */
1240 retval = cpuidle_register_device(dev);
1241 if (retval) {
1242 if (acpi_processor_registered == 0)
1243 cpuidle_unregister_driver(&acpi_idle_driver);
1244 return retval;
1245 }
1246 acpi_processor_registered++;
1247 }
1248 return 0;
1249 }
1251 int acpi_processor_power_exit(struct acpi_processor *pr)
1252 {
1253 struct cpuidle_device *dev = per_cpu(acpi_cpuidle_device, pr->id);
1255 if (disabled_by_idle_boot_param())
1256 return 0;
1258 if (pr->flags.power) {
1259 cpuidle_unregister_device(dev);
1260 acpi_processor_registered--;
1261 if (acpi_processor_registered == 0)
1262 cpuidle_unregister_driver(&acpi_idle_driver);
1263 }
1265 pr->flags.power_setup_done = 0;
1266 return 0;
1267 }