]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - drivers/char/agp/efficeon-agp.c
Merge branch 'drm-nouveau-fixes-3.8' of git://anongit.freedesktop.org/git/nouveau...
[android-sdk/kernel-video.git] / drivers / char / agp / efficeon-agp.c
1 /*
2  * Transmeta's Efficeon AGPGART driver.
3  *
4  * Based upon a diff by Linus around November '02.
5  *
6  * Ported to the 2.6 kernel by Carlos Puchol <cpglinux@puchol.com>
7  * and H. Peter Anvin <hpa@transmeta.com>.
8  */
10 /*
11  * NOTE-cpg-040217:
12  *
13  *   - when compiled as a module, after loading the module,
14  *     it will refuse to unload, indicating it is in use,
15  *     when it is not.
16  *   - no s3 (suspend to ram) testing.
17  *   - tested on the efficeon integrated nothbridge for tens
18  *     of iterations of starting x and glxgears.
19  *   - tested with radeon 9000 and radeon mobility m9 cards
20  *   - tested with c3/c4 enabled (with the mobility m9 card)
21  */
23 #include <linux/module.h>
24 #include <linux/pci.h>
25 #include <linux/init.h>
26 #include <linux/agp_backend.h>
27 #include <linux/gfp.h>
28 #include <linux/page-flags.h>
29 #include <linux/mm.h>
30 #include "agp.h"
31 #include "intel-agp.h"
33 /*
34  * The real differences to the generic AGP code is
35  * in the GART mappings - a two-level setup with the
36  * first level being an on-chip 64-entry table.
37  *
38  * The page array is filled through the ATTPAGE register
39  * (Aperture Translation Table Page Register) at 0xB8. Bits:
40  *  31:20: physical page address
41  *   11:9: Page Attribute Table Index (PATI)
42  *         must match the PAT index for the
43  *         mapped pages (the 2nd level page table pages
44  *         themselves should be just regular WB-cacheable,
45  *         so this is normally zero.)
46  *      8: Present
47  *    7:6: reserved, write as zero
48  *    5:0: GATT directory index: which 1st-level entry
49  *
50  * The Efficeon AGP spec requires pages to be WB-cacheable
51  * but to be explicitly CLFLUSH'd after any changes.
52  */
53 #define EFFICEON_ATTPAGE        0xb8
54 #define EFFICEON_L1_SIZE        64      /* Number of PDE pages */
56 #define EFFICEON_PATI           (0 << 9)
57 #define EFFICEON_PRESENT        (1 << 8)
59 static struct _efficeon_private {
60         unsigned long l1_table[EFFICEON_L1_SIZE];
61 } efficeon_private;
63 static const struct gatt_mask efficeon_generic_masks[] =
64 {
65         {.mask = 0x00000001, .type = 0}
66 };
68 /* This function does the same thing as mask_memory() for this chipset... */
69 static inline unsigned long efficeon_mask_memory(struct page *page)
70 {
71         unsigned long addr = page_to_phys(page);
72         return addr | 0x00000001;
73 }
75 static const struct aper_size_info_lvl2 efficeon_generic_sizes[4] =
76 {
77         {256, 65536, 0},
78         {128, 32768, 32},
79         {64, 16384, 48},
80         {32, 8192, 56}
81 };
83 /*
84  * Control interfaces are largely identical to
85  * the legacy Intel 440BX..
86  */
88 static int efficeon_fetch_size(void)
89 {
90         int i;
91         u16 temp;
92         struct aper_size_info_lvl2 *values;
94         pci_read_config_word(agp_bridge->dev, INTEL_APSIZE, &temp);
95         values = A_SIZE_LVL2(agp_bridge->driver->aperture_sizes);
97         for (i = 0; i < agp_bridge->driver->num_aperture_sizes; i++) {
98                 if (temp == values[i].size_value) {
99                         agp_bridge->previous_size =
100                             agp_bridge->current_size = (void *) (values + i);
101                         agp_bridge->aperture_size_idx = i;
102                         return values[i].size;
103                 }
104         }
106         return 0;
109 static void efficeon_tlbflush(struct agp_memory * mem)
111         printk(KERN_DEBUG PFX "efficeon_tlbflush()\n");
112         pci_write_config_dword(agp_bridge->dev, INTEL_AGPCTRL, 0x2200);
113         pci_write_config_dword(agp_bridge->dev, INTEL_AGPCTRL, 0x2280);
116 static void efficeon_cleanup(void)
118         u16 temp;
119         struct aper_size_info_lvl2 *previous_size;
121         printk(KERN_DEBUG PFX "efficeon_cleanup()\n");
122         previous_size = A_SIZE_LVL2(agp_bridge->previous_size);
123         pci_read_config_word(agp_bridge->dev, INTEL_NBXCFG, &temp);
124         pci_write_config_word(agp_bridge->dev, INTEL_NBXCFG, temp & ~(1 << 9));
125         pci_write_config_word(agp_bridge->dev, INTEL_APSIZE,
126                               previous_size->size_value);
129 static int efficeon_configure(void)
131         u32 temp;
132         u16 temp2;
133         struct aper_size_info_lvl2 *current_size;
135         printk(KERN_DEBUG PFX "efficeon_configure()\n");
137         current_size = A_SIZE_LVL2(agp_bridge->current_size);
139         /* aperture size */
140         pci_write_config_word(agp_bridge->dev, INTEL_APSIZE,
141                               current_size->size_value);
143         /* address to map to */
144         pci_read_config_dword(agp_bridge->dev, AGP_APBASE, &temp);
145         agp_bridge->gart_bus_addr = (temp & PCI_BASE_ADDRESS_MEM_MASK);
147         /* agpctrl */
148         pci_write_config_dword(agp_bridge->dev, INTEL_AGPCTRL, 0x2280);
150         /* paccfg/nbxcfg */
151         pci_read_config_word(agp_bridge->dev, INTEL_NBXCFG, &temp2);
152         pci_write_config_word(agp_bridge->dev, INTEL_NBXCFG,
153                               (temp2 & ~(1 << 10)) | (1 << 9) | (1 << 11));
154         /* clear any possible error conditions */
155         pci_write_config_byte(agp_bridge->dev, INTEL_ERRSTS + 1, 7);
156         return 0;
159 static int efficeon_free_gatt_table(struct agp_bridge_data *bridge)
161         int index, freed = 0;
163         for (index = 0; index < EFFICEON_L1_SIZE; index++) {
164                 unsigned long page = efficeon_private.l1_table[index];
165                 if (page) {
166                         efficeon_private.l1_table[index] = 0;
167                         ClearPageReserved(virt_to_page((char *)page));
168                         free_page(page);
169                         freed++;
170                 }
171                 printk(KERN_DEBUG PFX "efficeon_free_gatt_table(%p, %02x, %08x)\n",
172                         agp_bridge->dev, EFFICEON_ATTPAGE, index);
173                 pci_write_config_dword(agp_bridge->dev,
174                         EFFICEON_ATTPAGE, index);
175         }
176         printk(KERN_DEBUG PFX "efficeon_free_gatt_table() freed %d pages\n", freed);
177         return 0;
181 /*
182  * Since we don't need contiguous memory we just try
183  * to get the gatt table once
184  */
186 #define GET_PAGE_DIR_OFF(addr) (addr >> 22)
187 #define GET_PAGE_DIR_IDX(addr) (GET_PAGE_DIR_OFF(addr) - \
188         GET_PAGE_DIR_OFF(agp_bridge->gart_bus_addr))
189 #define GET_GATT_OFF(addr) ((addr & 0x003ff000) >> 12)
190 #undef  GET_GATT
191 #define GET_GATT(addr) (efficeon_private.gatt_pages[\
192         GET_PAGE_DIR_IDX(addr)]->remapped)
194 static int efficeon_create_gatt_table(struct agp_bridge_data *bridge)
196         int index;
197         const int pati    = EFFICEON_PATI;
198         const int present = EFFICEON_PRESENT;
199         const int clflush_chunk = ((cpuid_ebx(1) >> 8) & 0xff) << 3;
200         int num_entries, l1_pages;
202         num_entries = A_SIZE_LVL2(agp_bridge->current_size)->num_entries;
204         printk(KERN_DEBUG PFX "efficeon_create_gatt_table(%d)\n", num_entries);
206         /* There are 2^10 PTE pages per PDE page */
207         BUG_ON(num_entries & 0x3ff);
208         l1_pages = num_entries >> 10;
210         for (index = 0 ; index < l1_pages ; index++) {
211                 int offset;
212                 unsigned long page;
213                 unsigned long value;
215                 page = efficeon_private.l1_table[index];
216                 BUG_ON(page);
218                 page = get_zeroed_page(GFP_KERNEL);
219                 if (!page) {
220                         efficeon_free_gatt_table(agp_bridge);
221                         return -ENOMEM;
222                 }
223                 SetPageReserved(virt_to_page((char *)page));
225                 for (offset = 0; offset < PAGE_SIZE; offset += clflush_chunk)
226                         clflush((char *)page+offset);
228                 efficeon_private.l1_table[index] = page;
230                 value = virt_to_phys((unsigned long *)page) | pati | present | index;
232                 pci_write_config_dword(agp_bridge->dev,
233                         EFFICEON_ATTPAGE, value);
234         }
236         return 0;
239 static int efficeon_insert_memory(struct agp_memory * mem, off_t pg_start, int type)
241         int i, count = mem->page_count, num_entries;
242         unsigned int *page, *last_page;
243         const int clflush_chunk = ((cpuid_ebx(1) >> 8) & 0xff) << 3;
244         const unsigned long clflush_mask = ~(clflush_chunk-1);
246         printk(KERN_DEBUG PFX "efficeon_insert_memory(%lx, %d)\n", pg_start, count);
248         num_entries = A_SIZE_LVL2(agp_bridge->current_size)->num_entries;
249         if ((pg_start + mem->page_count) > num_entries)
250                 return -EINVAL;
251         if (type != 0 || mem->type != 0)
252                 return -EINVAL;
254         if (!mem->is_flushed) {
255                 global_cache_flush();
256                 mem->is_flushed = true;
257         }
259         last_page = NULL;
260         for (i = 0; i < count; i++) {
261                 int index = pg_start + i;
262                 unsigned long insert = efficeon_mask_memory(mem->pages[i]);
264                 page = (unsigned int *) efficeon_private.l1_table[index >> 10];
266                 if (!page)
267                         continue;
269                 page += (index & 0x3ff);
270                 *page = insert;
272                 /* clflush is slow, so don't clflush until we have to */
273                 if (last_page &&
274                     (((unsigned long)page^(unsigned long)last_page) &
275                      clflush_mask))
276                         clflush(last_page);
278                 last_page = page;
279         }
281         if ( last_page )
282                 clflush(last_page);
284         agp_bridge->driver->tlb_flush(mem);
285         return 0;
288 static int efficeon_remove_memory(struct agp_memory * mem, off_t pg_start, int type)
290         int i, count = mem->page_count, num_entries;
292         printk(KERN_DEBUG PFX "efficeon_remove_memory(%lx, %d)\n", pg_start, count);
294         num_entries = A_SIZE_LVL2(agp_bridge->current_size)->num_entries;
296         if ((pg_start + mem->page_count) > num_entries)
297                 return -EINVAL;
298         if (type != 0 || mem->type != 0)
299                 return -EINVAL;
301         for (i = 0; i < count; i++) {
302                 int index = pg_start + i;
303                 unsigned int *page = (unsigned int *) efficeon_private.l1_table[index >> 10];
305                 if (!page)
306                         continue;
307                 page += (index & 0x3ff);
308                 *page = 0;
309         }
310         agp_bridge->driver->tlb_flush(mem);
311         return 0;
315 static const struct agp_bridge_driver efficeon_driver = {
316         .owner                  = THIS_MODULE,
317         .aperture_sizes         = efficeon_generic_sizes,
318         .size_type              = LVL2_APER_SIZE,
319         .num_aperture_sizes     = 4,
320         .configure              = efficeon_configure,
321         .fetch_size             = efficeon_fetch_size,
322         .cleanup                = efficeon_cleanup,
323         .tlb_flush              = efficeon_tlbflush,
324         .mask_memory            = agp_generic_mask_memory,
325         .masks                  = efficeon_generic_masks,
326         .agp_enable             = agp_generic_enable,
327         .cache_flush            = global_cache_flush,
329         // Efficeon-specific GATT table setup / populate / teardown
330         .create_gatt_table      = efficeon_create_gatt_table,
331         .free_gatt_table        = efficeon_free_gatt_table,
332         .insert_memory          = efficeon_insert_memory,
333         .remove_memory          = efficeon_remove_memory,
334         .cant_use_aperture      = false,        // true might be faster?
336         // Generic
337         .alloc_by_type          = agp_generic_alloc_by_type,
338         .free_by_type           = agp_generic_free_by_type,
339         .agp_alloc_page         = agp_generic_alloc_page,
340         .agp_alloc_pages        = agp_generic_alloc_pages,
341         .agp_destroy_page       = agp_generic_destroy_page,
342         .agp_destroy_pages      = agp_generic_destroy_pages,
343         .agp_type_to_mask_type  = agp_generic_type_to_mask_type,
344 };
346 static int agp_efficeon_probe(struct pci_dev *pdev,
347                               const struct pci_device_id *ent)
349         struct agp_bridge_data *bridge;
350         u8 cap_ptr;
351         struct resource *r;
353         cap_ptr = pci_find_capability(pdev, PCI_CAP_ID_AGP);
354         if (!cap_ptr)
355                 return -ENODEV;
357         /* Probe for Efficeon controller */
358         if (pdev->device != PCI_DEVICE_ID_EFFICEON) {
359                 printk(KERN_ERR PFX "Unsupported Efficeon chipset (device id: %04x)\n",
360                     pdev->device);
361                 return -ENODEV;
362         }
364         printk(KERN_INFO PFX "Detected Transmeta Efficeon TM8000 series chipset\n");
366         bridge = agp_alloc_bridge();
367         if (!bridge)
368                 return -ENOMEM;
370         bridge->driver = &efficeon_driver;
371         bridge->dev = pdev;
372         bridge->capndx = cap_ptr;
374         /*
375         * If the device has not been properly setup, the following will catch
376         * the problem and should stop the system from crashing.
377         * 20030610 - hamish@zot.org
378         */
379         if (pci_enable_device(pdev)) {
380                 printk(KERN_ERR PFX "Unable to Enable PCI device\n");
381                 agp_put_bridge(bridge);
382                 return -ENODEV;
383         }
385         /*
386         * The following fixes the case where the BIOS has "forgotten" to
387         * provide an address range for the GART.
388         * 20030610 - hamish@zot.org
389         */
390         r = &pdev->resource[0];
391         if (!r->start && r->end) {
392                 if (pci_assign_resource(pdev, 0)) {
393                         printk(KERN_ERR PFX "could not assign resource 0\n");
394                         agp_put_bridge(bridge);
395                         return -ENODEV;
396                 }
397         }
399         /* Fill in the mode register */
400         if (cap_ptr) {
401                 pci_read_config_dword(pdev,
402                                 bridge->capndx+PCI_AGP_STATUS,
403                                 &bridge->mode);
404         }
406         pci_set_drvdata(pdev, bridge);
407         return agp_add_bridge(bridge);
410 static void agp_efficeon_remove(struct pci_dev *pdev)
412         struct agp_bridge_data *bridge = pci_get_drvdata(pdev);
414         agp_remove_bridge(bridge);
415         agp_put_bridge(bridge);
418 #ifdef CONFIG_PM
419 static int agp_efficeon_suspend(struct pci_dev *dev, pm_message_t state)
421         return 0;
424 static int agp_efficeon_resume(struct pci_dev *pdev)
426         printk(KERN_DEBUG PFX "agp_efficeon_resume()\n");
427         return efficeon_configure();
429 #endif
431 static struct pci_device_id agp_efficeon_pci_table[] = {
432         {
433         .class          = (PCI_CLASS_BRIDGE_HOST << 8),
434         .class_mask     = ~0,
435         .vendor         = PCI_VENDOR_ID_TRANSMETA,
436         .device         = PCI_ANY_ID,
437         .subvendor      = PCI_ANY_ID,
438         .subdevice      = PCI_ANY_ID,
439         },
440         { }
441 };
443 MODULE_DEVICE_TABLE(pci, agp_efficeon_pci_table);
445 static struct pci_driver agp_efficeon_pci_driver = {
446         .name           = "agpgart-efficeon",
447         .id_table       = agp_efficeon_pci_table,
448         .probe          = agp_efficeon_probe,
449         .remove         = agp_efficeon_remove,
450 #ifdef CONFIG_PM
451         .suspend        = agp_efficeon_suspend,
452         .resume         = agp_efficeon_resume,
453 #endif
454 };
456 static int __init agp_efficeon_init(void)
458         static int agp_initialised=0;
460         if (agp_off)
461                 return -EINVAL;
463         if (agp_initialised == 1)
464                 return 0;
465         agp_initialised=1;
467         return pci_register_driver(&agp_efficeon_pci_driver);
470 static void __exit agp_efficeon_cleanup(void)
472         pci_unregister_driver(&agp_efficeon_pci_driver);
475 module_init(agp_efficeon_init);
476 module_exit(agp_efficeon_cleanup);
478 MODULE_AUTHOR("Carlos Puchol <cpglinux@puchol.com>");
479 MODULE_LICENSE("GPL and additional rights");