1 /*
2 * Copyright (C) 2006, 2007, 2009 Rusty Russell, IBM Corporation
3 * Copyright (C) 2009, 2010, 2011 Red Hat, Inc.
4 * Copyright (C) 2009, 2010, 2011 Amit Shah <amit.shah@redhat.com>
5 *
6 * This program is free software; you can redistribute it and/or modify
7 * it under the terms of the GNU General Public License as published by
8 * the Free Software Foundation; either version 2 of the License, or
9 * (at your option) any later version.
10 *
11 * This program is distributed in the hope that it will be useful,
12 * but WITHOUT ANY WARRANTY; without even the implied warranty of
13 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
14 * GNU General Public License for more details.
15 *
16 * You should have received a copy of the GNU General Public License
17 * along with this program; if not, write to the Free Software
18 * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA
19 */
20 #include <linux/cdev.h>
21 #include <linux/debugfs.h>
22 #include <linux/completion.h>
23 #include <linux/device.h>
24 #include <linux/err.h>
25 #include <linux/freezer.h>
26 #include <linux/fs.h>
27 #include <linux/splice.h>
28 #include <linux/pagemap.h>
29 #include <linux/init.h>
30 #include <linux/list.h>
31 #include <linux/poll.h>
32 #include <linux/sched.h>
33 #include <linux/slab.h>
34 #include <linux/spinlock.h>
35 #include <linux/virtio.h>
36 #include <linux/virtio_console.h>
37 #include <linux/wait.h>
38 #include <linux/workqueue.h>
39 #include <linux/module.h>
40 #include <linux/dma-mapping.h>
41 #include <linux/kconfig.h>
42 #include "../tty/hvc/hvc_console.h"
44 #define is_rproc_enabled IS_ENABLED(CONFIG_REMOTEPROC)
46 /*
47 * This is a global struct for storing common data for all the devices
48 * this driver handles.
49 *
50 * Mainly, it has a linked list for all the consoles in one place so
51 * that callbacks from hvc for get_chars(), put_chars() work properly
52 * across multiple devices and multiple ports per device.
53 */
54 struct ports_driver_data {
55 /* Used for registering chardevs */
56 struct class *class;
58 /* Used for exporting per-port information to debugfs */
59 struct dentry *debugfs_dir;
61 /* List of all the devices we're handling */
62 struct list_head portdevs;
64 /* Number of devices this driver is handling */
65 unsigned int index;
67 /*
68 * This is used to keep track of the number of hvc consoles
69 * spawned by this driver. This number is given as the first
70 * argument to hvc_alloc(). To correctly map an initial
71 * console spawned via hvc_instantiate to the console being
72 * hooked up via hvc_alloc, we need to pass the same vtermno.
73 *
74 * We also just assume the first console being initialised was
75 * the first one that got used as the initial console.
76 */
77 unsigned int next_vtermno;
79 /* All the console devices handled by this driver */
80 struct list_head consoles;
81 };
82 static struct ports_driver_data pdrvdata;
84 DEFINE_SPINLOCK(pdrvdata_lock);
85 DECLARE_COMPLETION(early_console_added);
87 /* This struct holds information that's relevant only for console ports */
88 struct console {
89 /* We'll place all consoles in a list in the pdrvdata struct */
90 struct list_head list;
92 /* The hvc device associated with this console port */
93 struct hvc_struct *hvc;
95 /* The size of the console */
96 struct winsize ws;
98 /*
99 * This number identifies the number that we used to register
100 * with hvc in hvc_instantiate() and hvc_alloc(); this is the
101 * number passed on by the hvc callbacks to us to
102 * differentiate between the other console ports handled by
103 * this driver
104 */
105 u32 vtermno;
106 };
108 struct port_buffer {
109 char *buf;
111 /* size of the buffer in *buf above */
112 size_t size;
114 /* used length of the buffer */
115 size_t len;
116 /* offset in the buf from which to consume data */
117 size_t offset;
119 /* DMA address of buffer */
120 dma_addr_t dma;
122 /* Device we got DMA memory from */
123 struct device *dev;
125 /* List of pending dma buffers to free */
126 struct list_head list;
128 /* If sgpages == 0 then buf is used */
129 unsigned int sgpages;
131 /* sg is used if spages > 0. sg must be the last in is struct */
132 struct scatterlist sg[0];
133 };
135 /*
136 * This is a per-device struct that stores data common to all the
137 * ports for that device (vdev->priv).
138 */
139 struct ports_device {
140 /* Next portdev in the list, head is in the pdrvdata struct */
141 struct list_head list;
143 /*
144 * Workqueue handlers where we process deferred work after
145 * notification
146 */
147 struct work_struct control_work;
149 struct list_head ports;
151 /* To protect the list of ports */
152 spinlock_t ports_lock;
154 /* To protect the vq operations for the control channel */
155 spinlock_t cvq_lock;
157 /* The current config space is stored here */
158 struct virtio_console_config config;
160 /* The virtio device we're associated with */
161 struct virtio_device *vdev;
163 /*
164 * A couple of virtqueues for the control channel: one for
165 * guest->host transfers, one for host->guest transfers
166 */
167 struct virtqueue *c_ivq, *c_ovq;
169 /* Array of per-port IO virtqueues */
170 struct virtqueue **in_vqs, **out_vqs;
172 /* Used for numbering devices for sysfs and debugfs */
173 unsigned int drv_index;
175 /* Major number for this device. Ports will be created as minors. */
176 int chr_major;
177 };
179 struct port_stats {
180 unsigned long bytes_sent, bytes_received, bytes_discarded;
181 };
183 /* This struct holds the per-port data */
184 struct port {
185 /* Next port in the list, head is in the ports_device */
186 struct list_head list;
188 /* Pointer to the parent virtio_console device */
189 struct ports_device *portdev;
191 /* The current buffer from which data has to be fed to readers */
192 struct port_buffer *inbuf;
194 /*
195 * To protect the operations on the in_vq associated with this
196 * port. Has to be a spinlock because it can be called from
197 * interrupt context (get_char()).
198 */
199 spinlock_t inbuf_lock;
201 /* Protect the operations on the out_vq. */
202 spinlock_t outvq_lock;
204 /* The IO vqs for this port */
205 struct virtqueue *in_vq, *out_vq;
207 /* File in the debugfs directory that exposes this port's information */
208 struct dentry *debugfs_file;
210 /*
211 * Keep count of the bytes sent, received and discarded for
212 * this port for accounting and debugging purposes. These
213 * counts are not reset across port open / close events.
214 */
215 struct port_stats stats;
217 /*
218 * The entries in this struct will be valid if this port is
219 * hooked up to an hvc console
220 */
221 struct console cons;
223 /* Each port associates with a separate char device */
224 struct cdev *cdev;
225 struct device *dev;
227 /* Reference-counting to handle port hot-unplugs and file operations */
228 struct kref kref;
230 /* A waitqueue for poll() or blocking read operations */
231 wait_queue_head_t waitqueue;
233 /* The 'name' of the port that we expose via sysfs properties */
234 char *name;
236 /* We can notify apps of host connect / disconnect events via SIGIO */
237 struct fasync_struct *async_queue;
239 /* The 'id' to identify the port with the Host */
240 u32 id;
242 bool outvq_full;
244 /* Is the host device open */
245 bool host_connected;
247 /* We should allow only one process to open a port */
248 bool guest_connected;
249 };
251 /* This is the very early arch-specified put chars function. */
252 static int (*early_put_chars)(u32, const char *, int);
254 static struct port *find_port_by_vtermno(u32 vtermno)
255 {
256 struct port *port;
257 struct console *cons;
258 unsigned long flags;
260 spin_lock_irqsave(&pdrvdata_lock, flags);
261 list_for_each_entry(cons, &pdrvdata.consoles, list) {
262 if (cons->vtermno == vtermno) {
263 port = container_of(cons, struct port, cons);
264 goto out;
265 }
266 }
267 port = NULL;
268 out:
269 spin_unlock_irqrestore(&pdrvdata_lock, flags);
270 return port;
271 }
273 static struct port *find_port_by_devt_in_portdev(struct ports_device *portdev,
274 dev_t dev)
275 {
276 struct port *port;
277 unsigned long flags;
279 spin_lock_irqsave(&portdev->ports_lock, flags);
280 list_for_each_entry(port, &portdev->ports, list)
281 if (port->cdev->dev == dev)
282 goto out;
283 port = NULL;
284 out:
285 spin_unlock_irqrestore(&portdev->ports_lock, flags);
287 return port;
288 }
290 static struct port *find_port_by_devt(dev_t dev)
291 {
292 struct ports_device *portdev;
293 struct port *port;
294 unsigned long flags;
296 spin_lock_irqsave(&pdrvdata_lock, flags);
297 list_for_each_entry(portdev, &pdrvdata.portdevs, list) {
298 port = find_port_by_devt_in_portdev(portdev, dev);
299 if (port)
300 goto out;
301 }
302 port = NULL;
303 out:
304 spin_unlock_irqrestore(&pdrvdata_lock, flags);
305 return port;
306 }
308 static struct port *find_port_by_id(struct ports_device *portdev, u32 id)
309 {
310 struct port *port;
311 unsigned long flags;
313 spin_lock_irqsave(&portdev->ports_lock, flags);
314 list_for_each_entry(port, &portdev->ports, list)
315 if (port->id == id)
316 goto out;
317 port = NULL;
318 out:
319 spin_unlock_irqrestore(&portdev->ports_lock, flags);
321 return port;
322 }
324 static struct port *find_port_by_vq(struct ports_device *portdev,
325 struct virtqueue *vq)
326 {
327 struct port *port;
328 unsigned long flags;
330 spin_lock_irqsave(&portdev->ports_lock, flags);
331 list_for_each_entry(port, &portdev->ports, list)
332 if (port->in_vq == vq || port->out_vq == vq)
333 goto out;
334 port = NULL;
335 out:
336 spin_unlock_irqrestore(&portdev->ports_lock, flags);
337 return port;
338 }
340 static bool is_console_port(struct port *port)
341 {
342 if (port->cons.hvc)
343 return true;
344 return false;
345 }
347 static bool is_rproc_serial(const struct virtio_device *vdev)
348 {
349 return is_rproc_enabled && vdev->id.device == VIRTIO_ID_RPROC_SERIAL;
350 }
352 static inline bool use_multiport(struct ports_device *portdev)
353 {
354 /*
355 * This condition can be true when put_chars is called from
356 * early_init
357 */
358 if (!portdev->vdev)
359 return 0;
360 return portdev->vdev->features[0] & (1 << VIRTIO_CONSOLE_F_MULTIPORT);
361 }
363 static DEFINE_SPINLOCK(dma_bufs_lock);
364 static LIST_HEAD(pending_free_dma_bufs);
366 static void free_buf(struct port_buffer *buf, bool can_sleep)
367 {
368 unsigned int i;
370 for (i = 0; i < buf->sgpages; i++) {
371 struct page *page = sg_page(&buf->sg[i]);
372 if (!page)
373 break;
374 put_page(page);
375 }
377 if (!buf->dev) {
378 kfree(buf->buf);
379 } else if (is_rproc_enabled) {
380 unsigned long flags;
382 /* dma_free_coherent requires interrupts to be enabled. */
383 if (!can_sleep) {
384 /* queue up dma-buffers to be freed later */
385 spin_lock_irqsave(&dma_bufs_lock, flags);
386 list_add_tail(&buf->list, &pending_free_dma_bufs);
387 spin_unlock_irqrestore(&dma_bufs_lock, flags);
388 return;
389 }
390 dma_free_coherent(buf->dev, buf->size, buf->buf, buf->dma);
392 /* Release device refcnt and allow it to be freed */
393 put_device(buf->dev);
394 }
396 kfree(buf);
397 }
399 static void reclaim_dma_bufs(void)
400 {
401 unsigned long flags;
402 struct port_buffer *buf, *tmp;
403 LIST_HEAD(tmp_list);
405 if (list_empty(&pending_free_dma_bufs))
406 return;
408 /* Create a copy of the pending_free_dma_bufs while holding the lock */
409 spin_lock_irqsave(&dma_bufs_lock, flags);
410 list_cut_position(&tmp_list, &pending_free_dma_bufs,
411 pending_free_dma_bufs.prev);
412 spin_unlock_irqrestore(&dma_bufs_lock, flags);
414 /* Release the dma buffers, without irqs enabled */
415 list_for_each_entry_safe(buf, tmp, &tmp_list, list) {
416 list_del(&buf->list);
417 free_buf(buf, true);
418 }
419 }
421 static struct port_buffer *alloc_buf(struct virtqueue *vq, size_t buf_size,
422 int pages)
423 {
424 struct port_buffer *buf;
426 reclaim_dma_bufs();
428 /*
429 * Allocate buffer and the sg list. The sg list array is allocated
430 * directly after the port_buffer struct.
431 */
432 buf = kmalloc(sizeof(*buf) + sizeof(struct scatterlist) * pages,
433 GFP_KERNEL);
434 if (!buf)
435 goto fail;
437 buf->sgpages = pages;
438 if (pages > 0) {
439 buf->dev = NULL;
440 buf->buf = NULL;
441 return buf;
442 }
444 if (is_rproc_serial(vq->vdev)) {
445 /*
446 * Allocate DMA memory from ancestor. When a virtio
447 * device is created by remoteproc, the DMA memory is
448 * associated with the grandparent device:
449 * vdev => rproc => platform-dev.
450 * The code here would have been less quirky if
451 * DMA_MEMORY_INCLUDES_CHILDREN had been supported
452 * in dma-coherent.c
453 */
454 if (!vq->vdev->dev.parent || !vq->vdev->dev.parent->parent)
455 goto free_buf;
456 buf->dev = vq->vdev->dev.parent->parent;
458 /* Increase device refcnt to avoid freeing it */
459 get_device(buf->dev);
460 buf->buf = dma_alloc_coherent(buf->dev, buf_size, &buf->dma,
461 GFP_KERNEL);
462 } else {
463 buf->dev = NULL;
464 buf->buf = kmalloc(buf_size, GFP_KERNEL);
465 }
467 if (!buf->buf)
468 goto free_buf;
469 buf->len = 0;
470 buf->offset = 0;
471 buf->size = buf_size;
472 return buf;
474 free_buf:
475 kfree(buf);
476 fail:
477 return NULL;
478 }
480 /* Callers should take appropriate locks */
481 static struct port_buffer *get_inbuf(struct port *port)
482 {
483 struct port_buffer *buf;
484 unsigned int len;
486 if (port->inbuf)
487 return port->inbuf;
489 buf = virtqueue_get_buf(port->in_vq, &len);
490 if (buf) {
491 buf->len = len;
492 buf->offset = 0;
493 port->stats.bytes_received += len;
494 }
495 return buf;
496 }
498 /*
499 * Create a scatter-gather list representing our input buffer and put
500 * it in the queue.
501 *
502 * Callers should take appropriate locks.
503 */
504 static int add_inbuf(struct virtqueue *vq, struct port_buffer *buf)
505 {
506 struct scatterlist sg[1];
507 int ret;
509 sg_init_one(sg, buf->buf, buf->size);
511 ret = virtqueue_add_buf(vq, sg, 0, 1, buf, GFP_ATOMIC);
512 virtqueue_kick(vq);
513 if (!ret)
514 ret = vq->num_free;
515 return ret;
516 }
518 /* Discard any unread data this port has. Callers lockers. */
519 static void discard_port_data(struct port *port)
520 {
521 struct port_buffer *buf;
522 unsigned int err;
524 if (!port->portdev) {
525 /* Device has been unplugged. vqs are already gone. */
526 return;
527 }
528 buf = get_inbuf(port);
530 err = 0;
531 while (buf) {
532 port->stats.bytes_discarded += buf->len - buf->offset;
533 if (add_inbuf(port->in_vq, buf) < 0) {
534 err++;
535 free_buf(buf, false);
536 }
537 port->inbuf = NULL;
538 buf = get_inbuf(port);
539 }
540 if (err)
541 dev_warn(port->dev, "Errors adding %d buffers back to vq\n",
542 err);
543 }
545 static bool port_has_data(struct port *port)
546 {
547 unsigned long flags;
548 bool ret;
550 ret = false;
551 spin_lock_irqsave(&port->inbuf_lock, flags);
552 port->inbuf = get_inbuf(port);
553 if (port->inbuf)
554 ret = true;
556 spin_unlock_irqrestore(&port->inbuf_lock, flags);
557 return ret;
558 }
560 static ssize_t __send_control_msg(struct ports_device *portdev, u32 port_id,
561 unsigned int event, unsigned int value)
562 {
563 struct scatterlist sg[1];
564 struct virtio_console_control cpkt;
565 struct virtqueue *vq;
566 unsigned int len;
568 if (!use_multiport(portdev))
569 return 0;
571 cpkt.id = port_id;
572 cpkt.event = event;
573 cpkt.value = value;
575 vq = portdev->c_ovq;
577 sg_init_one(sg, &cpkt, sizeof(cpkt));
578 if (virtqueue_add_buf(vq, sg, 1, 0, &cpkt, GFP_ATOMIC) == 0) {
579 virtqueue_kick(vq);
580 while (!virtqueue_get_buf(vq, &len))
581 cpu_relax();
582 }
583 return 0;
584 }
586 static ssize_t send_control_msg(struct port *port, unsigned int event,
587 unsigned int value)
588 {
589 /* Did the port get unplugged before userspace closed it? */
590 if (port->portdev)
591 return __send_control_msg(port->portdev, port->id, event, value);
592 return 0;
593 }
596 /* Callers must take the port->outvq_lock */
597 static void reclaim_consumed_buffers(struct port *port)
598 {
599 struct port_buffer *buf;
600 unsigned int len;
602 if (!port->portdev) {
603 /* Device has been unplugged. vqs are already gone. */
604 return;
605 }
606 while ((buf = virtqueue_get_buf(port->out_vq, &len))) {
607 free_buf(buf, false);
608 port->outvq_full = false;
609 }
610 }
612 static ssize_t __send_to_port(struct port *port, struct scatterlist *sg,
613 int nents, size_t in_count,
614 void *data, bool nonblock)
615 {
616 struct virtqueue *out_vq;
617 int err;
618 unsigned long flags;
619 unsigned int len;
621 out_vq = port->out_vq;
623 spin_lock_irqsave(&port->outvq_lock, flags);
625 reclaim_consumed_buffers(port);
627 err = virtqueue_add_buf(out_vq, sg, nents, 0, data, GFP_ATOMIC);
629 /* Tell Host to go! */
630 virtqueue_kick(out_vq);
632 if (err) {
633 in_count = 0;
634 goto done;
635 }
637 if (out_vq->num_free == 0)
638 port->outvq_full = true;
640 if (nonblock)
641 goto done;
643 /*
644 * Wait till the host acknowledges it pushed out the data we
645 * sent. This is done for data from the hvc_console; the tty
646 * operations are performed with spinlocks held so we can't
647 * sleep here. An alternative would be to copy the data to a
648 * buffer and relax the spinning requirement. The downside is
649 * we need to kmalloc a GFP_ATOMIC buffer each time the
650 * console driver writes something out.
651 */
652 while (!virtqueue_get_buf(out_vq, &len))
653 cpu_relax();
654 done:
655 spin_unlock_irqrestore(&port->outvq_lock, flags);
657 port->stats.bytes_sent += in_count;
658 /*
659 * We're expected to return the amount of data we wrote -- all
660 * of it
661 */
662 return in_count;
663 }
665 /*
666 * Give out the data that's requested from the buffer that we have
667 * queued up.
668 */
669 static ssize_t fill_readbuf(struct port *port, char *out_buf, size_t out_count,
670 bool to_user)
671 {
672 struct port_buffer *buf;
673 unsigned long flags;
675 if (!out_count || !port_has_data(port))
676 return 0;
678 buf = port->inbuf;
679 out_count = min(out_count, buf->len - buf->offset);
681 if (to_user) {
682 ssize_t ret;
684 ret = copy_to_user(out_buf, buf->buf + buf->offset, out_count);
685 if (ret)
686 return -EFAULT;
687 } else {
688 memcpy(out_buf, buf->buf + buf->offset, out_count);
689 }
691 buf->offset += out_count;
693 if (buf->offset == buf->len) {
694 /*
695 * We're done using all the data in this buffer.
696 * Re-queue so that the Host can send us more data.
697 */
698 spin_lock_irqsave(&port->inbuf_lock, flags);
699 port->inbuf = NULL;
701 if (add_inbuf(port->in_vq, buf) < 0)
702 dev_warn(port->dev, "failed add_buf\n");
704 spin_unlock_irqrestore(&port->inbuf_lock, flags);
705 }
706 /* Return the number of bytes actually copied */
707 return out_count;
708 }
710 /* The condition that must be true for polling to end */
711 static bool will_read_block(struct port *port)
712 {
713 if (!port->guest_connected) {
714 /* Port got hot-unplugged. Let's exit. */
715 return false;
716 }
717 return !port_has_data(port) && port->host_connected;
718 }
720 static bool will_write_block(struct port *port)
721 {
722 bool ret;
724 if (!port->guest_connected) {
725 /* Port got hot-unplugged. Let's exit. */
726 return false;
727 }
728 if (!port->host_connected)
729 return true;
731 spin_lock_irq(&port->outvq_lock);
732 /*
733 * Check if the Host has consumed any buffers since we last
734 * sent data (this is only applicable for nonblocking ports).
735 */
736 reclaim_consumed_buffers(port);
737 ret = port->outvq_full;
738 spin_unlock_irq(&port->outvq_lock);
740 return ret;
741 }
743 static ssize_t port_fops_read(struct file *filp, char __user *ubuf,
744 size_t count, loff_t *offp)
745 {
746 struct port *port;
747 ssize_t ret;
749 port = filp->private_data;
751 if (!port_has_data(port)) {
752 /*
753 * If nothing's connected on the host just return 0 in
754 * case of list_empty; this tells the userspace app
755 * that there's no connection
756 */
757 if (!port->host_connected)
758 return 0;
759 if (filp->f_flags & O_NONBLOCK)
760 return -EAGAIN;
762 ret = wait_event_freezable(port->waitqueue,
763 !will_read_block(port));
764 if (ret < 0)
765 return ret;
766 }
767 /* Port got hot-unplugged. */
768 if (!port->guest_connected)
769 return -ENODEV;
770 /*
771 * We could've received a disconnection message while we were
772 * waiting for more data.
773 *
774 * This check is not clubbed in the if() statement above as we
775 * might receive some data as well as the host could get
776 * disconnected after we got woken up from our wait. So we
777 * really want to give off whatever data we have and only then
778 * check for host_connected.
779 */
780 if (!port_has_data(port) && !port->host_connected)
781 return 0;
783 return fill_readbuf(port, ubuf, count, true);
784 }
786 static int wait_port_writable(struct port *port, bool nonblock)
787 {
788 int ret;
790 if (will_write_block(port)) {
791 if (nonblock)
792 return -EAGAIN;
794 ret = wait_event_freezable(port->waitqueue,
795 !will_write_block(port));
796 if (ret < 0)
797 return ret;
798 }
799 /* Port got hot-unplugged. */
800 if (!port->guest_connected)
801 return -ENODEV;
803 return 0;
804 }
806 static ssize_t port_fops_write(struct file *filp, const char __user *ubuf,
807 size_t count, loff_t *offp)
808 {
809 struct port *port;
810 struct port_buffer *buf;
811 ssize_t ret;
812 bool nonblock;
813 struct scatterlist sg[1];
815 /* Userspace could be out to fool us */
816 if (!count)
817 return 0;
819 port = filp->private_data;
821 nonblock = filp->f_flags & O_NONBLOCK;
823 ret = wait_port_writable(port, nonblock);
824 if (ret < 0)
825 return ret;
827 count = min((size_t)(32 * 1024), count);
829 buf = alloc_buf(port->out_vq, count, 0);
830 if (!buf)
831 return -ENOMEM;
833 ret = copy_from_user(buf->buf, ubuf, count);
834 if (ret) {
835 ret = -EFAULT;
836 goto free_buf;
837 }
839 /*
840 * We now ask send_buf() to not spin for generic ports -- we
841 * can re-use the same code path that non-blocking file
842 * descriptors take for blocking file descriptors since the
843 * wait is already done and we're certain the write will go
844 * through to the host.
845 */
846 nonblock = true;
847 sg_init_one(sg, buf->buf, count);
848 ret = __send_to_port(port, sg, 1, count, buf, nonblock);
850 if (nonblock && ret > 0)
851 goto out;
853 free_buf:
854 free_buf(buf, true);
855 out:
856 return ret;
857 }
859 struct sg_list {
860 unsigned int n;
861 unsigned int size;
862 size_t len;
863 struct scatterlist *sg;
864 };
866 static int pipe_to_sg(struct pipe_inode_info *pipe, struct pipe_buffer *buf,
867 struct splice_desc *sd)
868 {
869 struct sg_list *sgl = sd->u.data;
870 unsigned int offset, len;
872 if (sgl->n == sgl->size)
873 return 0;
875 /* Try lock this page */
876 if (buf->ops->steal(pipe, buf) == 0) {
877 /* Get reference and unlock page for moving */
878 get_page(buf->page);
879 unlock_page(buf->page);
881 len = min(buf->len, sd->len);
882 sg_set_page(&(sgl->sg[sgl->n]), buf->page, len, buf->offset);
883 } else {
884 /* Failback to copying a page */
885 struct page *page = alloc_page(GFP_KERNEL);
886 char *src = buf->ops->map(pipe, buf, 1);
887 char *dst;
889 if (!page)
890 return -ENOMEM;
891 dst = kmap(page);
893 offset = sd->pos & ~PAGE_MASK;
895 len = sd->len;
896 if (len + offset > PAGE_SIZE)
897 len = PAGE_SIZE - offset;
899 memcpy(dst + offset, src + buf->offset, len);
901 kunmap(page);
902 buf->ops->unmap(pipe, buf, src);
904 sg_set_page(&(sgl->sg[sgl->n]), page, len, offset);
905 }
906 sgl->n++;
907 sgl->len += len;
909 return len;
910 }
912 /* Faster zero-copy write by splicing */
913 static ssize_t port_fops_splice_write(struct pipe_inode_info *pipe,
914 struct file *filp, loff_t *ppos,
915 size_t len, unsigned int flags)
916 {
917 struct port *port = filp->private_data;
918 struct sg_list sgl;
919 ssize_t ret;
920 struct port_buffer *buf;
921 struct splice_desc sd = {
922 .total_len = len,
923 .flags = flags,
924 .pos = *ppos,
925 .u.data = &sgl,
926 };
928 /*
929 * Rproc_serial does not yet support splice. To support splice
930 * pipe_to_sg() must allocate dma-buffers and copy content from
931 * regular pages to dma pages. And alloc_buf and free_buf must
932 * support allocating and freeing such a list of dma-buffers.
933 */
934 if (is_rproc_serial(port->out_vq->vdev))
935 return -EINVAL;
937 ret = wait_port_writable(port, filp->f_flags & O_NONBLOCK);
938 if (ret < 0)
939 return ret;
941 buf = alloc_buf(port->out_vq, 0, pipe->nrbufs);
942 if (!buf)
943 return -ENOMEM;
945 sgl.n = 0;
946 sgl.len = 0;
947 sgl.size = pipe->nrbufs;
948 sgl.sg = buf->sg;
949 sg_init_table(sgl.sg, sgl.size);
950 ret = __splice_from_pipe(pipe, &sd, pipe_to_sg);
951 if (likely(ret > 0))
952 ret = __send_to_port(port, buf->sg, sgl.n, sgl.len, buf, true);
954 if (unlikely(ret <= 0))
955 free_buf(buf, true);
956 return ret;
957 }
959 static unsigned int port_fops_poll(struct file *filp, poll_table *wait)
960 {
961 struct port *port;
962 unsigned int ret;
964 port = filp->private_data;
965 poll_wait(filp, &port->waitqueue, wait);
967 if (!port->guest_connected) {
968 /* Port got unplugged */
969 return POLLHUP;
970 }
971 ret = 0;
972 if (!will_read_block(port))
973 ret |= POLLIN | POLLRDNORM;
974 if (!will_write_block(port))
975 ret |= POLLOUT;
976 if (!port->host_connected)
977 ret |= POLLHUP;
979 return ret;
980 }
982 static void remove_port(struct kref *kref);
984 static int port_fops_release(struct inode *inode, struct file *filp)
985 {
986 struct port *port;
988 port = filp->private_data;
990 /* Notify host of port being closed */
991 send_control_msg(port, VIRTIO_CONSOLE_PORT_OPEN, 0);
993 spin_lock_irq(&port->inbuf_lock);
994 port->guest_connected = false;
996 discard_port_data(port);
998 spin_unlock_irq(&port->inbuf_lock);
1000 spin_lock_irq(&port->outvq_lock);
1001 reclaim_consumed_buffers(port);
1002 spin_unlock_irq(&port->outvq_lock);
1004 reclaim_dma_bufs();
1005 /*
1006 * Locks aren't necessary here as a port can't be opened after
1007 * unplug, and if a port isn't unplugged, a kref would already
1008 * exist for the port. Plus, taking ports_lock here would
1009 * create a dependency on other locks taken by functions
1010 * inside remove_port if we're the last holder of the port,
1011 * creating many problems.
1012 */
1013 kref_put(&port->kref, remove_port);
1015 return 0;
1016 }
1018 static int port_fops_open(struct inode *inode, struct file *filp)
1019 {
1020 struct cdev *cdev = inode->i_cdev;
1021 struct port *port;
1022 int ret;
1024 port = find_port_by_devt(cdev->dev);
1025 filp->private_data = port;
1027 /* Prevent against a port getting hot-unplugged at the same time */
1028 spin_lock_irq(&port->portdev->ports_lock);
1029 kref_get(&port->kref);
1030 spin_unlock_irq(&port->portdev->ports_lock);
1032 /*
1033 * Don't allow opening of console port devices -- that's done
1034 * via /dev/hvc
1035 */
1036 if (is_console_port(port)) {
1037 ret = -ENXIO;
1038 goto out;
1039 }
1041 /* Allow only one process to open a particular port at a time */
1042 spin_lock_irq(&port->inbuf_lock);
1043 if (port->guest_connected) {
1044 spin_unlock_irq(&port->inbuf_lock);
1045 ret = -EMFILE;
1046 goto out;
1047 }
1049 port->guest_connected = true;
1050 spin_unlock_irq(&port->inbuf_lock);
1052 spin_lock_irq(&port->outvq_lock);
1053 /*
1054 * There might be a chance that we missed reclaiming a few
1055 * buffers in the window of the port getting previously closed
1056 * and opening now.
1057 */
1058 reclaim_consumed_buffers(port);
1059 spin_unlock_irq(&port->outvq_lock);
1061 nonseekable_open(inode, filp);
1063 /* Notify host of port being opened */
1064 send_control_msg(filp->private_data, VIRTIO_CONSOLE_PORT_OPEN, 1);
1066 return 0;
1067 out:
1068 kref_put(&port->kref, remove_port);
1069 return ret;
1070 }
1072 static int port_fops_fasync(int fd, struct file *filp, int mode)
1073 {
1074 struct port *port;
1076 port = filp->private_data;
1077 return fasync_helper(fd, filp, mode, &port->async_queue);
1078 }
1080 /*
1081 * The file operations that we support: programs in the guest can open
1082 * a console device, read from it, write to it, poll for data and
1083 * close it. The devices are at
1084 * /dev/vport<device number>p<port number>
1085 */
1086 static const struct file_operations port_fops = {
1087 .owner = THIS_MODULE,
1088 .open = port_fops_open,
1089 .read = port_fops_read,
1090 .write = port_fops_write,
1091 .splice_write = port_fops_splice_write,
1092 .poll = port_fops_poll,
1093 .release = port_fops_release,
1094 .fasync = port_fops_fasync,
1095 .llseek = no_llseek,
1096 };
1098 /*
1099 * The put_chars() callback is pretty straightforward.
1100 *
1101 * We turn the characters into a scatter-gather list, add it to the
1102 * output queue and then kick the Host. Then we sit here waiting for
1103 * it to finish: inefficient in theory, but in practice
1104 * implementations will do it immediately (lguest's Launcher does).
1105 */
1106 static int put_chars(u32 vtermno, const char *buf, int count)
1107 {
1108 struct port *port;
1109 struct scatterlist sg[1];
1111 if (unlikely(early_put_chars))
1112 return early_put_chars(vtermno, buf, count);
1114 port = find_port_by_vtermno(vtermno);
1115 if (!port)
1116 return -EPIPE;
1118 sg_init_one(sg, buf, count);
1119 return __send_to_port(port, sg, 1, count, (void *)buf, false);
1120 }
1122 /*
1123 * get_chars() is the callback from the hvc_console infrastructure
1124 * when an interrupt is received.
1125 *
1126 * We call out to fill_readbuf that gets us the required data from the
1127 * buffers that are queued up.
1128 */
1129 static int get_chars(u32 vtermno, char *buf, int count)
1130 {
1131 struct port *port;
1133 /* If we've not set up the port yet, we have no input to give. */
1134 if (unlikely(early_put_chars))
1135 return 0;
1137 port = find_port_by_vtermno(vtermno);
1138 if (!port)
1139 return -EPIPE;
1141 /* If we don't have an input queue yet, we can't get input. */
1142 BUG_ON(!port->in_vq);
1144 return fill_readbuf(port, buf, count, false);
1145 }
1147 static void resize_console(struct port *port)
1148 {
1149 struct virtio_device *vdev;
1151 /* The port could have been hot-unplugged */
1152 if (!port || !is_console_port(port))
1153 return;
1155 vdev = port->portdev->vdev;
1157 /* Don't test F_SIZE at all if we're rproc: not a valid feature! */
1158 if (!is_rproc_serial(vdev) &&
1159 virtio_has_feature(vdev, VIRTIO_CONSOLE_F_SIZE))
1160 hvc_resize(port->cons.hvc, port->cons.ws);
1161 }
1163 /* We set the configuration at this point, since we now have a tty */
1164 static int notifier_add_vio(struct hvc_struct *hp, int data)
1165 {
1166 struct port *port;
1168 port = find_port_by_vtermno(hp->vtermno);
1169 if (!port)
1170 return -EINVAL;
1172 hp->irq_requested = 1;
1173 resize_console(port);
1175 return 0;
1176 }
1178 static void notifier_del_vio(struct hvc_struct *hp, int data)
1179 {
1180 hp->irq_requested = 0;
1181 }
1183 /* The operations for console ports. */
1184 static const struct hv_ops hv_ops = {
1185 .get_chars = get_chars,
1186 .put_chars = put_chars,
1187 .notifier_add = notifier_add_vio,
1188 .notifier_del = notifier_del_vio,
1189 .notifier_hangup = notifier_del_vio,
1190 };
1192 /*
1193 * Console drivers are initialized very early so boot messages can go
1194 * out, so we do things slightly differently from the generic virtio
1195 * initialization of the net and block drivers.
1196 *
1197 * At this stage, the console is output-only. It's too early to set
1198 * up a virtqueue, so we let the drivers do some boutique early-output
1199 * thing.
1200 */
1201 int __init virtio_cons_early_init(int (*put_chars)(u32, const char *, int))
1202 {
1203 early_put_chars = put_chars;
1204 return hvc_instantiate(0, 0, &hv_ops);
1205 }
1207 int init_port_console(struct port *port)
1208 {
1209 int ret;
1211 /*
1212 * The Host's telling us this port is a console port. Hook it
1213 * up with an hvc console.
1214 *
1215 * To set up and manage our virtual console, we call
1216 * hvc_alloc().
1217 *
1218 * The first argument of hvc_alloc() is the virtual console
1219 * number. The second argument is the parameter for the
1220 * notification mechanism (like irq number). We currently
1221 * leave this as zero, virtqueues have implicit notifications.
1222 *
1223 * The third argument is a "struct hv_ops" containing the
1224 * put_chars() get_chars(), notifier_add() and notifier_del()
1225 * pointers. The final argument is the output buffer size: we
1226 * can do any size, so we put PAGE_SIZE here.
1227 */
1228 port->cons.vtermno = pdrvdata.next_vtermno;
1230 port->cons.hvc = hvc_alloc(port->cons.vtermno, 0, &hv_ops, PAGE_SIZE);
1231 if (IS_ERR(port->cons.hvc)) {
1232 ret = PTR_ERR(port->cons.hvc);
1233 dev_err(port->dev,
1234 "error %d allocating hvc for port\n", ret);
1235 port->cons.hvc = NULL;
1236 return ret;
1237 }
1238 spin_lock_irq(&pdrvdata_lock);
1239 pdrvdata.next_vtermno++;
1240 list_add_tail(&port->cons.list, &pdrvdata.consoles);
1241 spin_unlock_irq(&pdrvdata_lock);
1242 port->guest_connected = true;
1244 /*
1245 * Start using the new console output if this is the first
1246 * console to come up.
1247 */
1248 if (early_put_chars)
1249 early_put_chars = NULL;
1251 /* Notify host of port being opened */
1252 send_control_msg(port, VIRTIO_CONSOLE_PORT_OPEN, 1);
1254 return 0;
1255 }
1257 static ssize_t show_port_name(struct device *dev,
1258 struct device_attribute *attr, char *buffer)
1259 {
1260 struct port *port;
1262 port = dev_get_drvdata(dev);
1264 return sprintf(buffer, "%s\n", port->name);
1265 }
1267 static DEVICE_ATTR(name, S_IRUGO, show_port_name, NULL);
1269 static struct attribute *port_sysfs_entries[] = {
1270 &dev_attr_name.attr,
1271 NULL
1272 };
1274 static struct attribute_group port_attribute_group = {
1275 .name = NULL, /* put in device directory */
1276 .attrs = port_sysfs_entries,
1277 };
1279 static ssize_t debugfs_read(struct file *filp, char __user *ubuf,
1280 size_t count, loff_t *offp)
1281 {
1282 struct port *port;
1283 char *buf;
1284 ssize_t ret, out_offset, out_count;
1286 out_count = 1024;
1287 buf = kmalloc(out_count, GFP_KERNEL);
1288 if (!buf)
1289 return -ENOMEM;
1291 port = filp->private_data;
1292 out_offset = 0;
1293 out_offset += snprintf(buf + out_offset, out_count,
1294 "name: %s\n", port->name ? port->name : "");
1295 out_offset += snprintf(buf + out_offset, out_count - out_offset,
1296 "guest_connected: %d\n", port->guest_connected);
1297 out_offset += snprintf(buf + out_offset, out_count - out_offset,
1298 "host_connected: %d\n", port->host_connected);
1299 out_offset += snprintf(buf + out_offset, out_count - out_offset,
1300 "outvq_full: %d\n", port->outvq_full);
1301 out_offset += snprintf(buf + out_offset, out_count - out_offset,
1302 "bytes_sent: %lu\n", port->stats.bytes_sent);
1303 out_offset += snprintf(buf + out_offset, out_count - out_offset,
1304 "bytes_received: %lu\n",
1305 port->stats.bytes_received);
1306 out_offset += snprintf(buf + out_offset, out_count - out_offset,
1307 "bytes_discarded: %lu\n",
1308 port->stats.bytes_discarded);
1309 out_offset += snprintf(buf + out_offset, out_count - out_offset,
1310 "is_console: %s\n",
1311 is_console_port(port) ? "yes" : "no");
1312 out_offset += snprintf(buf + out_offset, out_count - out_offset,
1313 "console_vtermno: %u\n", port->cons.vtermno);
1315 ret = simple_read_from_buffer(ubuf, count, offp, buf, out_offset);
1316 kfree(buf);
1317 return ret;
1318 }
1320 static const struct file_operations port_debugfs_ops = {
1321 .owner = THIS_MODULE,
1322 .open = simple_open,
1323 .read = debugfs_read,
1324 };
1326 static void set_console_size(struct port *port, u16 rows, u16 cols)
1327 {
1328 if (!port || !is_console_port(port))
1329 return;
1331 port->cons.ws.ws_row = rows;
1332 port->cons.ws.ws_col = cols;
1333 }
1335 static unsigned int fill_queue(struct virtqueue *vq, spinlock_t *lock)
1336 {
1337 struct port_buffer *buf;
1338 unsigned int nr_added_bufs;
1339 int ret;
1341 nr_added_bufs = 0;
1342 do {
1343 buf = alloc_buf(vq, PAGE_SIZE, 0);
1344 if (!buf)
1345 break;
1347 spin_lock_irq(lock);
1348 ret = add_inbuf(vq, buf);
1349 if (ret < 0) {
1350 spin_unlock_irq(lock);
1351 free_buf(buf, true);
1352 break;
1353 }
1354 nr_added_bufs++;
1355 spin_unlock_irq(lock);
1356 } while (ret > 0);
1358 return nr_added_bufs;
1359 }
1361 static void send_sigio_to_port(struct port *port)
1362 {
1363 if (port->async_queue && port->guest_connected)
1364 kill_fasync(&port->async_queue, SIGIO, POLL_OUT);
1365 }
1367 static int add_port(struct ports_device *portdev, u32 id)
1368 {
1369 char debugfs_name[16];
1370 struct port *port;
1371 struct port_buffer *buf;
1372 dev_t devt;
1373 unsigned int nr_added_bufs;
1374 int err;
1376 port = kmalloc(sizeof(*port), GFP_KERNEL);
1377 if (!port) {
1378 err = -ENOMEM;
1379 goto fail;
1380 }
1381 kref_init(&port->kref);
1383 port->portdev = portdev;
1384 port->id = id;
1386 port->name = NULL;
1387 port->inbuf = NULL;
1388 port->cons.hvc = NULL;
1389 port->async_queue = NULL;
1391 port->cons.ws.ws_row = port->cons.ws.ws_col = 0;
1393 port->host_connected = port->guest_connected = false;
1394 port->stats = (struct port_stats) { 0 };
1396 port->outvq_full = false;
1398 port->in_vq = portdev->in_vqs[port->id];
1399 port->out_vq = portdev->out_vqs[port->id];
1401 port->cdev = cdev_alloc();
1402 if (!port->cdev) {
1403 dev_err(&port->portdev->vdev->dev, "Error allocating cdev\n");
1404 err = -ENOMEM;
1405 goto free_port;
1406 }
1407 port->cdev->ops = &port_fops;
1409 devt = MKDEV(portdev->chr_major, id);
1410 err = cdev_add(port->cdev, devt, 1);
1411 if (err < 0) {
1412 dev_err(&port->portdev->vdev->dev,
1413 "Error %d adding cdev for port %u\n", err, id);
1414 goto free_cdev;
1415 }
1416 port->dev = device_create(pdrvdata.class, &port->portdev->vdev->dev,
1417 devt, port, "vport%up%u",
1418 port->portdev->drv_index, id);
1419 if (IS_ERR(port->dev)) {
1420 err = PTR_ERR(port->dev);
1421 dev_err(&port->portdev->vdev->dev,
1422 "Error %d creating device for port %u\n",
1423 err, id);
1424 goto free_cdev;
1425 }
1427 spin_lock_init(&port->inbuf_lock);
1428 spin_lock_init(&port->outvq_lock);
1429 init_waitqueue_head(&port->waitqueue);
1431 /* Fill the in_vq with buffers so the host can send us data. */
1432 nr_added_bufs = fill_queue(port->in_vq, &port->inbuf_lock);
1433 if (!nr_added_bufs) {
1434 dev_err(port->dev, "Error allocating inbufs\n");
1435 err = -ENOMEM;
1436 goto free_device;
1437 }
1439 if (is_rproc_serial(port->portdev->vdev))
1440 /*
1441 * For rproc_serial assume remote processor is connected.
1442 * rproc_serial does not want the console port, only
1443 * the generic port implementation.
1444 */
1445 port->host_connected = true;
1446 else if (!use_multiport(port->portdev)) {
1447 /*
1448 * If we're not using multiport support,
1449 * this has to be a console port.
1450 */
1451 err = init_port_console(port);
1452 if (err)
1453 goto free_inbufs;
1454 }
1456 spin_lock_irq(&portdev->ports_lock);
1457 list_add_tail(&port->list, &port->portdev->ports);
1458 spin_unlock_irq(&portdev->ports_lock);
1460 /*
1461 * Tell the Host we're set so that it can send us various
1462 * configuration parameters for this port (eg, port name,
1463 * caching, whether this is a console port, etc.)
1464 */
1465 send_control_msg(port, VIRTIO_CONSOLE_PORT_READY, 1);
1467 if (pdrvdata.debugfs_dir) {
1468 /*
1469 * Finally, create the debugfs file that we can use to
1470 * inspect a port's state at any time
1471 */
1472 sprintf(debugfs_name, "vport%up%u",
1473 port->portdev->drv_index, id);
1474 port->debugfs_file = debugfs_create_file(debugfs_name, 0444,
1475 pdrvdata.debugfs_dir,
1476 port,
1477 &port_debugfs_ops);
1478 }
1479 return 0;
1481 free_inbufs:
1482 while ((buf = virtqueue_detach_unused_buf(port->in_vq)))
1483 free_buf(buf, true);
1484 free_device:
1485 device_destroy(pdrvdata.class, port->dev->devt);
1486 free_cdev:
1487 cdev_del(port->cdev);
1488 free_port:
1489 kfree(port);
1490 fail:
1491 /* The host might want to notify management sw about port add failure */
1492 __send_control_msg(portdev, id, VIRTIO_CONSOLE_PORT_READY, 0);
1493 return err;
1494 }
1496 /* No users remain, remove all port-specific data. */
1497 static void remove_port(struct kref *kref)
1498 {
1499 struct port *port;
1501 port = container_of(kref, struct port, kref);
1503 sysfs_remove_group(&port->dev->kobj, &port_attribute_group);
1504 device_destroy(pdrvdata.class, port->dev->devt);
1505 cdev_del(port->cdev);
1507 kfree(port->name);
1509 debugfs_remove(port->debugfs_file);
1511 kfree(port);
1512 }
1514 static void remove_port_data(struct port *port)
1515 {
1516 struct port_buffer *buf;
1518 /* Remove unused data this port might have received. */
1519 discard_port_data(port);
1521 reclaim_consumed_buffers(port);
1523 /* Remove buffers we queued up for the Host to send us data in. */
1524 while ((buf = virtqueue_detach_unused_buf(port->in_vq)))
1525 free_buf(buf, true);
1527 /* Free pending buffers from the out-queue. */
1528 while ((buf = virtqueue_detach_unused_buf(port->out_vq)))
1529 free_buf(buf, true);
1530 }
1532 /*
1533 * Port got unplugged. Remove port from portdev's list and drop the
1534 * kref reference. If no userspace has this port opened, it will
1535 * result in immediate removal the port.
1536 */
1537 static void unplug_port(struct port *port)
1538 {
1539 spin_lock_irq(&port->portdev->ports_lock);
1540 list_del(&port->list);
1541 spin_unlock_irq(&port->portdev->ports_lock);
1543 if (port->guest_connected) {
1544 port->guest_connected = false;
1545 port->host_connected = false;
1546 wake_up_interruptible(&port->waitqueue);
1548 /* Let the app know the port is going down. */
1549 send_sigio_to_port(port);
1550 }
1552 if (is_console_port(port)) {
1553 spin_lock_irq(&pdrvdata_lock);
1554 list_del(&port->cons.list);
1555 spin_unlock_irq(&pdrvdata_lock);
1556 hvc_remove(port->cons.hvc);
1557 }
1559 remove_port_data(port);
1561 /*
1562 * We should just assume the device itself has gone off --
1563 * else a close on an open port later will try to send out a
1564 * control message.
1565 */
1566 port->portdev = NULL;
1568 /*
1569 * Locks around here are not necessary - a port can't be
1570 * opened after we removed the port struct from ports_list
1571 * above.
1572 */
1573 kref_put(&port->kref, remove_port);
1574 }
1576 /* Any private messages that the Host and Guest want to share */
1577 static void handle_control_message(struct ports_device *portdev,
1578 struct port_buffer *buf)
1579 {
1580 struct virtio_console_control *cpkt;
1581 struct port *port;
1582 size_t name_size;
1583 int err;
1585 cpkt = (struct virtio_console_control *)(buf->buf + buf->offset);
1587 port = find_port_by_id(portdev, cpkt->id);
1588 if (!port && cpkt->event != VIRTIO_CONSOLE_PORT_ADD) {
1589 /* No valid header at start of buffer. Drop it. */
1590 dev_dbg(&portdev->vdev->dev,
1591 "Invalid index %u in control packet\n", cpkt->id);
1592 return;
1593 }
1595 switch (cpkt->event) {
1596 case VIRTIO_CONSOLE_PORT_ADD:
1597 if (port) {
1598 dev_dbg(&portdev->vdev->dev,
1599 "Port %u already added\n", port->id);
1600 send_control_msg(port, VIRTIO_CONSOLE_PORT_READY, 1);
1601 break;
1602 }
1603 if (cpkt->id >= portdev->config.max_nr_ports) {
1604 dev_warn(&portdev->vdev->dev,
1605 "Request for adding port with out-of-bound id %u, max. supported id: %u\n",
1606 cpkt->id, portdev->config.max_nr_ports - 1);
1607 break;
1608 }
1609 add_port(portdev, cpkt->id);
1610 break;
1611 case VIRTIO_CONSOLE_PORT_REMOVE:
1612 unplug_port(port);
1613 break;
1614 case VIRTIO_CONSOLE_CONSOLE_PORT:
1615 if (!cpkt->value)
1616 break;
1617 if (is_console_port(port))
1618 break;
1620 init_port_console(port);
1621 complete(&early_console_added);
1622 /*
1623 * Could remove the port here in case init fails - but
1624 * have to notify the host first.
1625 */
1626 break;
1627 case VIRTIO_CONSOLE_RESIZE: {
1628 struct {
1629 __u16 rows;
1630 __u16 cols;
1631 } size;
1633 if (!is_console_port(port))
1634 break;
1636 memcpy(&size, buf->buf + buf->offset + sizeof(*cpkt),
1637 sizeof(size));
1638 set_console_size(port, size.rows, size.cols);
1640 port->cons.hvc->irq_requested = 1;
1641 resize_console(port);
1642 break;
1643 }
1644 case VIRTIO_CONSOLE_PORT_OPEN:
1645 port->host_connected = cpkt->value;
1646 wake_up_interruptible(&port->waitqueue);
1647 /*
1648 * If the host port got closed and the host had any
1649 * unconsumed buffers, we'll be able to reclaim them
1650 * now.
1651 */
1652 spin_lock_irq(&port->outvq_lock);
1653 reclaim_consumed_buffers(port);
1654 spin_unlock_irq(&port->outvq_lock);
1656 /*
1657 * If the guest is connected, it'll be interested in
1658 * knowing the host connection state changed.
1659 */
1660 send_sigio_to_port(port);
1661 break;
1662 case VIRTIO_CONSOLE_PORT_NAME:
1663 /*
1664 * If we woke up after hibernation, we can get this
1665 * again. Skip it in that case.
1666 */
1667 if (port->name)
1668 break;
1670 /*
1671 * Skip the size of the header and the cpkt to get the size
1672 * of the name that was sent
1673 */
1674 name_size = buf->len - buf->offset - sizeof(*cpkt) + 1;
1676 port->name = kmalloc(name_size, GFP_KERNEL);
1677 if (!port->name) {
1678 dev_err(port->dev,
1679 "Not enough space to store port name\n");
1680 break;
1681 }
1682 strncpy(port->name, buf->buf + buf->offset + sizeof(*cpkt),
1683 name_size - 1);
1684 port->name[name_size - 1] = 0;
1686 /*
1687 * Since we only have one sysfs attribute, 'name',
1688 * create it only if we have a name for the port.
1689 */
1690 err = sysfs_create_group(&port->dev->kobj,
1691 &port_attribute_group);
1692 if (err) {
1693 dev_err(port->dev,
1694 "Error %d creating sysfs device attributes\n",
1695 err);
1696 } else {
1697 /*
1698 * Generate a udev event so that appropriate
1699 * symlinks can be created based on udev
1700 * rules.
1701 */
1702 kobject_uevent(&port->dev->kobj, KOBJ_CHANGE);
1703 }
1704 break;
1705 }
1706 }
1708 static void control_work_handler(struct work_struct *work)
1709 {
1710 struct ports_device *portdev;
1711 struct virtqueue *vq;
1712 struct port_buffer *buf;
1713 unsigned int len;
1715 portdev = container_of(work, struct ports_device, control_work);
1716 vq = portdev->c_ivq;
1718 spin_lock(&portdev->cvq_lock);
1719 while ((buf = virtqueue_get_buf(vq, &len))) {
1720 spin_unlock(&portdev->cvq_lock);
1722 buf->len = len;
1723 buf->offset = 0;
1725 handle_control_message(portdev, buf);
1727 spin_lock(&portdev->cvq_lock);
1728 if (add_inbuf(portdev->c_ivq, buf) < 0) {
1729 dev_warn(&portdev->vdev->dev,
1730 "Error adding buffer to queue\n");
1731 free_buf(buf, false);
1732 }
1733 }
1734 spin_unlock(&portdev->cvq_lock);
1735 }
1737 static void out_intr(struct virtqueue *vq)
1738 {
1739 struct port *port;
1741 port = find_port_by_vq(vq->vdev->priv, vq);
1742 if (!port)
1743 return;
1745 wake_up_interruptible(&port->waitqueue);
1746 }
1748 static void in_intr(struct virtqueue *vq)
1749 {
1750 struct port *port;
1751 unsigned long flags;
1753 port = find_port_by_vq(vq->vdev->priv, vq);
1754 if (!port)
1755 return;
1757 spin_lock_irqsave(&port->inbuf_lock, flags);
1758 port->inbuf = get_inbuf(port);
1760 /*
1761 * Don't queue up data when port is closed. This condition
1762 * can be reached when a console port is not yet connected (no
1763 * tty is spawned) and the host sends out data to console
1764 * ports. For generic serial ports, the host won't
1765 * (shouldn't) send data till the guest is connected.
1766 */
1767 if (!port->guest_connected)
1768 discard_port_data(port);
1770 spin_unlock_irqrestore(&port->inbuf_lock, flags);
1772 wake_up_interruptible(&port->waitqueue);
1774 /* Send a SIGIO indicating new data in case the process asked for it */
1775 send_sigio_to_port(port);
1777 if (is_console_port(port) && hvc_poll(port->cons.hvc))
1778 hvc_kick();
1779 }
1781 static void control_intr(struct virtqueue *vq)
1782 {
1783 struct ports_device *portdev;
1785 portdev = vq->vdev->priv;
1786 schedule_work(&portdev->control_work);
1787 }
1789 static void config_intr(struct virtio_device *vdev)
1790 {
1791 struct ports_device *portdev;
1793 portdev = vdev->priv;
1795 if (!use_multiport(portdev)) {
1796 struct port *port;
1797 u16 rows, cols;
1799 vdev->config->get(vdev,
1800 offsetof(struct virtio_console_config, cols),
1801 &cols, sizeof(u16));
1802 vdev->config->get(vdev,
1803 offsetof(struct virtio_console_config, rows),
1804 &rows, sizeof(u16));
1806 port = find_port_by_id(portdev, 0);
1807 set_console_size(port, rows, cols);
1809 /*
1810 * We'll use this way of resizing only for legacy
1811 * support. For newer userspace
1812 * (VIRTIO_CONSOLE_F_MULTPORT+), use control messages
1813 * to indicate console size changes so that it can be
1814 * done per-port.
1815 */
1816 resize_console(port);
1817 }
1818 }
1820 static int init_vqs(struct ports_device *portdev)
1821 {
1822 vq_callback_t **io_callbacks;
1823 char **io_names;
1824 struct virtqueue **vqs;
1825 u32 i, j, nr_ports, nr_queues;
1826 int err;
1828 nr_ports = portdev->config.max_nr_ports;
1829 nr_queues = use_multiport(portdev) ? (nr_ports + 1) * 2 : 2;
1831 vqs = kmalloc(nr_queues * sizeof(struct virtqueue *), GFP_KERNEL);
1832 io_callbacks = kmalloc(nr_queues * sizeof(vq_callback_t *), GFP_KERNEL);
1833 io_names = kmalloc(nr_queues * sizeof(char *), GFP_KERNEL);
1834 portdev->in_vqs = kmalloc(nr_ports * sizeof(struct virtqueue *),
1835 GFP_KERNEL);
1836 portdev->out_vqs = kmalloc(nr_ports * sizeof(struct virtqueue *),
1837 GFP_KERNEL);
1838 if (!vqs || !io_callbacks || !io_names || !portdev->in_vqs ||
1839 !portdev->out_vqs) {
1840 err = -ENOMEM;
1841 goto free;
1842 }
1844 /*
1845 * For backward compat (newer host but older guest), the host
1846 * spawns a console port first and also inits the vqs for port
1847 * 0 before others.
1848 */
1849 j = 0;
1850 io_callbacks[j] = in_intr;
1851 io_callbacks[j + 1] = out_intr;
1852 io_names[j] = "input";
1853 io_names[j + 1] = "output";
1854 j += 2;
1856 if (use_multiport(portdev)) {
1857 io_callbacks[j] = control_intr;
1858 io_callbacks[j + 1] = NULL;
1859 io_names[j] = "control-i";
1860 io_names[j + 1] = "control-o";
1862 for (i = 1; i < nr_ports; i++) {
1863 j += 2;
1864 io_callbacks[j] = in_intr;
1865 io_callbacks[j + 1] = out_intr;
1866 io_names[j] = "input";
1867 io_names[j + 1] = "output";
1868 }
1869 }
1870 /* Find the queues. */
1871 err = portdev->vdev->config->find_vqs(portdev->vdev, nr_queues, vqs,
1872 io_callbacks,
1873 (const char **)io_names);
1874 if (err)
1875 goto free;
1877 j = 0;
1878 portdev->in_vqs[0] = vqs[0];
1879 portdev->out_vqs[0] = vqs[1];
1880 j += 2;
1881 if (use_multiport(portdev)) {
1882 portdev->c_ivq = vqs[j];
1883 portdev->c_ovq = vqs[j + 1];
1885 for (i = 1; i < nr_ports; i++) {
1886 j += 2;
1887 portdev->in_vqs[i] = vqs[j];
1888 portdev->out_vqs[i] = vqs[j + 1];
1889 }
1890 }
1891 kfree(io_names);
1892 kfree(io_callbacks);
1893 kfree(vqs);
1895 return 0;
1897 free:
1898 kfree(portdev->out_vqs);
1899 kfree(portdev->in_vqs);
1900 kfree(io_names);
1901 kfree(io_callbacks);
1902 kfree(vqs);
1904 return err;
1905 }
1907 static const struct file_operations portdev_fops = {
1908 .owner = THIS_MODULE,
1909 };
1911 static void remove_vqs(struct ports_device *portdev)
1912 {
1913 portdev->vdev->config->del_vqs(portdev->vdev);
1914 kfree(portdev->in_vqs);
1915 kfree(portdev->out_vqs);
1916 }
1918 static void remove_controlq_data(struct ports_device *portdev)
1919 {
1920 struct port_buffer *buf;
1921 unsigned int len;
1923 if (!use_multiport(portdev))
1924 return;
1926 while ((buf = virtqueue_get_buf(portdev->c_ivq, &len)))
1927 free_buf(buf, true);
1929 while ((buf = virtqueue_detach_unused_buf(portdev->c_ivq)))
1930 free_buf(buf, true);
1931 }
1933 /*
1934 * Once we're further in boot, we get probed like any other virtio
1935 * device.
1936 *
1937 * If the host also supports multiple console ports, we check the
1938 * config space to see how many ports the host has spawned. We
1939 * initialize each port found.
1940 */
1941 static int virtcons_probe(struct virtio_device *vdev)
1942 {
1943 struct ports_device *portdev;
1944 int err;
1945 bool multiport;
1946 bool early = early_put_chars != NULL;
1948 /* Ensure to read early_put_chars now */
1949 barrier();
1951 portdev = kmalloc(sizeof(*portdev), GFP_KERNEL);
1952 if (!portdev) {
1953 err = -ENOMEM;
1954 goto fail;
1955 }
1957 /* Attach this portdev to this virtio_device, and vice-versa. */
1958 portdev->vdev = vdev;
1959 vdev->priv = portdev;
1961 spin_lock_irq(&pdrvdata_lock);
1962 portdev->drv_index = pdrvdata.index++;
1963 spin_unlock_irq(&pdrvdata_lock);
1965 portdev->chr_major = register_chrdev(0, "virtio-portsdev",
1966 &portdev_fops);
1967 if (portdev->chr_major < 0) {
1968 dev_err(&vdev->dev,
1969 "Error %d registering chrdev for device %u\n",
1970 portdev->chr_major, portdev->drv_index);
1971 err = portdev->chr_major;
1972 goto free;
1973 }
1975 multiport = false;
1976 portdev->config.max_nr_ports = 1;
1978 /* Don't test MULTIPORT at all if we're rproc: not a valid feature! */
1979 if (!is_rproc_serial(vdev) &&
1980 virtio_config_val(vdev, VIRTIO_CONSOLE_F_MULTIPORT,
1981 offsetof(struct virtio_console_config,
1982 max_nr_ports),
1983 &portdev->config.max_nr_ports) == 0) {
1984 multiport = true;
1985 }
1987 err = init_vqs(portdev);
1988 if (err < 0) {
1989 dev_err(&vdev->dev, "Error %d initializing vqs\n", err);
1990 goto free_chrdev;
1991 }
1993 spin_lock_init(&portdev->ports_lock);
1994 INIT_LIST_HEAD(&portdev->ports);
1996 if (multiport) {
1997 unsigned int nr_added_bufs;
1999 spin_lock_init(&portdev->cvq_lock);
2000 INIT_WORK(&portdev->control_work, &control_work_handler);
2002 nr_added_bufs = fill_queue(portdev->c_ivq, &portdev->cvq_lock);
2003 if (!nr_added_bufs) {
2004 dev_err(&vdev->dev,
2005 "Error allocating buffers for control queue\n");
2006 err = -ENOMEM;
2007 goto free_vqs;
2008 }
2009 } else {
2010 /*
2011 * For backward compatibility: Create a console port
2012 * if we're running on older host.
2013 */
2014 add_port(portdev, 0);
2015 }
2017 spin_lock_irq(&pdrvdata_lock);
2018 list_add_tail(&portdev->list, &pdrvdata.portdevs);
2019 spin_unlock_irq(&pdrvdata_lock);
2021 __send_control_msg(portdev, VIRTIO_CONSOLE_BAD_ID,
2022 VIRTIO_CONSOLE_DEVICE_READY, 1);
2024 /*
2025 * If there was an early virtio console, assume that there are no
2026 * other consoles. We need to wait until the hvc_alloc matches the
2027 * hvc_instantiate, otherwise tty_open will complain, resulting in
2028 * a "Warning: unable to open an initial console" boot failure.
2029 * Without multiport this is done in add_port above. With multiport
2030 * this might take some host<->guest communication - thus we have to
2031 * wait.
2032 */
2033 if (multiport && early)
2034 wait_for_completion(&early_console_added);
2036 return 0;
2038 free_vqs:
2039 /* The host might want to notify mgmt sw about device add failure */
2040 __send_control_msg(portdev, VIRTIO_CONSOLE_BAD_ID,
2041 VIRTIO_CONSOLE_DEVICE_READY, 0);
2042 remove_vqs(portdev);
2043 free_chrdev:
2044 unregister_chrdev(portdev->chr_major, "virtio-portsdev");
2045 free:
2046 kfree(portdev);
2047 fail:
2048 return err;
2049 }
2051 static void virtcons_remove(struct virtio_device *vdev)
2052 {
2053 struct ports_device *portdev;
2054 struct port *port, *port2;
2056 portdev = vdev->priv;
2058 spin_lock_irq(&pdrvdata_lock);
2059 list_del(&portdev->list);
2060 spin_unlock_irq(&pdrvdata_lock);
2062 /* Disable interrupts for vqs */
2063 vdev->config->reset(vdev);
2064 /* Finish up work that's lined up */
2065 cancel_work_sync(&portdev->control_work);
2067 list_for_each_entry_safe(port, port2, &portdev->ports, list)
2068 unplug_port(port);
2070 unregister_chrdev(portdev->chr_major, "virtio-portsdev");
2072 /*
2073 * When yanking out a device, we immediately lose the
2074 * (device-side) queues. So there's no point in keeping the
2075 * guest side around till we drop our final reference. This
2076 * also means that any ports which are in an open state will
2077 * have to just stop using the port, as the vqs are going
2078 * away.
2079 */
2080 remove_controlq_data(portdev);
2081 remove_vqs(portdev);
2082 kfree(portdev);
2083 }
2085 static struct virtio_device_id id_table[] = {
2086 { VIRTIO_ID_CONSOLE, VIRTIO_DEV_ANY_ID },
2087 { 0 },
2088 };
2090 static unsigned int features[] = {
2091 VIRTIO_CONSOLE_F_SIZE,
2092 VIRTIO_CONSOLE_F_MULTIPORT,
2093 };
2095 static struct virtio_device_id rproc_serial_id_table[] = {
2096 #if IS_ENABLED(CONFIG_REMOTEPROC)
2097 { VIRTIO_ID_RPROC_SERIAL, VIRTIO_DEV_ANY_ID },
2098 #endif
2099 { 0 },
2100 };
2102 static unsigned int rproc_serial_features[] = {
2103 };
2105 #ifdef CONFIG_PM
2106 static int virtcons_freeze(struct virtio_device *vdev)
2107 {
2108 struct ports_device *portdev;
2109 struct port *port;
2111 portdev = vdev->priv;
2113 vdev->config->reset(vdev);
2115 virtqueue_disable_cb(portdev->c_ivq);
2116 cancel_work_sync(&portdev->control_work);
2117 /*
2118 * Once more: if control_work_handler() was running, it would
2119 * enable the cb as the last step.
2120 */
2121 virtqueue_disable_cb(portdev->c_ivq);
2122 remove_controlq_data(portdev);
2124 list_for_each_entry(port, &portdev->ports, list) {
2125 virtqueue_disable_cb(port->in_vq);
2126 virtqueue_disable_cb(port->out_vq);
2127 /*
2128 * We'll ask the host later if the new invocation has
2129 * the port opened or closed.
2130 */
2131 port->host_connected = false;
2132 remove_port_data(port);
2133 }
2134 remove_vqs(portdev);
2136 return 0;
2137 }
2139 static int virtcons_restore(struct virtio_device *vdev)
2140 {
2141 struct ports_device *portdev;
2142 struct port *port;
2143 int ret;
2145 portdev = vdev->priv;
2147 ret = init_vqs(portdev);
2148 if (ret)
2149 return ret;
2151 if (use_multiport(portdev))
2152 fill_queue(portdev->c_ivq, &portdev->cvq_lock);
2154 list_for_each_entry(port, &portdev->ports, list) {
2155 port->in_vq = portdev->in_vqs[port->id];
2156 port->out_vq = portdev->out_vqs[port->id];
2158 fill_queue(port->in_vq, &port->inbuf_lock);
2160 /* Get port open/close status on the host */
2161 send_control_msg(port, VIRTIO_CONSOLE_PORT_READY, 1);
2163 /*
2164 * If a port was open at the time of suspending, we
2165 * have to let the host know that it's still open.
2166 */
2167 if (port->guest_connected)
2168 send_control_msg(port, VIRTIO_CONSOLE_PORT_OPEN, 1);
2169 }
2170 return 0;
2171 }
2172 #endif
2174 static struct virtio_driver virtio_console = {
2175 .feature_table = features,
2176 .feature_table_size = ARRAY_SIZE(features),
2177 .driver.name = KBUILD_MODNAME,
2178 .driver.owner = THIS_MODULE,
2179 .id_table = id_table,
2180 .probe = virtcons_probe,
2181 .remove = virtcons_remove,
2182 .config_changed = config_intr,
2183 #ifdef CONFIG_PM
2184 .freeze = virtcons_freeze,
2185 .restore = virtcons_restore,
2186 #endif
2187 };
2189 static struct virtio_driver virtio_rproc_serial = {
2190 .feature_table = rproc_serial_features,
2191 .feature_table_size = ARRAY_SIZE(rproc_serial_features),
2192 .driver.name = "virtio_rproc_serial",
2193 .driver.owner = THIS_MODULE,
2194 .id_table = rproc_serial_id_table,
2195 .probe = virtcons_probe,
2196 .remove = virtcons_remove,
2197 };
2199 static int __init init(void)
2200 {
2201 int err;
2203 pdrvdata.class = class_create(THIS_MODULE, "virtio-ports");
2204 if (IS_ERR(pdrvdata.class)) {
2205 err = PTR_ERR(pdrvdata.class);
2206 pr_err("Error %d creating virtio-ports class\n", err);
2207 return err;
2208 }
2210 pdrvdata.debugfs_dir = debugfs_create_dir("virtio-ports", NULL);
2211 if (!pdrvdata.debugfs_dir) {
2212 pr_warning("Error %ld creating debugfs dir for virtio-ports\n",
2213 PTR_ERR(pdrvdata.debugfs_dir));
2214 }
2215 INIT_LIST_HEAD(&pdrvdata.consoles);
2216 INIT_LIST_HEAD(&pdrvdata.portdevs);
2218 err = register_virtio_driver(&virtio_console);
2219 if (err < 0) {
2220 pr_err("Error %d registering virtio driver\n", err);
2221 goto free;
2222 }
2223 err = register_virtio_driver(&virtio_rproc_serial);
2224 if (err < 0) {
2225 pr_err("Error %d registering virtio rproc serial driver\n",
2226 err);
2227 goto unregister;
2228 }
2229 return 0;
2230 unregister:
2231 unregister_virtio_driver(&virtio_console);
2232 free:
2233 if (pdrvdata.debugfs_dir)
2234 debugfs_remove_recursive(pdrvdata.debugfs_dir);
2235 class_destroy(pdrvdata.class);
2236 return err;
2237 }
2239 static void __exit fini(void)
2240 {
2241 reclaim_dma_bufs();
2243 unregister_virtio_driver(&virtio_console);
2244 unregister_virtio_driver(&virtio_rproc_serial);
2246 class_destroy(pdrvdata.class);
2247 if (pdrvdata.debugfs_dir)
2248 debugfs_remove_recursive(pdrvdata.debugfs_dir);
2249 }
2250 module_init(init);
2251 module_exit(fini);
2253 MODULE_DEVICE_TABLE(virtio, id_table);
2254 MODULE_DESCRIPTION("Virtio console driver");
2255 MODULE_LICENSE("GPL");