Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
[android-sdk/kernel-video.git] / drivers / cpufreq / Kconfig
1 menu "CPU Frequency scaling"
3 config CPU_FREQ
4         bool "CPU Frequency scaling"
5         help
6           CPU Frequency scaling allows you to change the clock speed of 
7           CPUs on the fly. This is a nice method to save power, because 
8           the lower the CPU clock speed, the less power the CPU consumes.
10           Note that this driver doesn't automatically change the CPU
11           clock speed, you need to either enable a dynamic cpufreq governor
12           (see below) after boot, or use a userspace tool.
14           For details, take a look at <file:Documentation/cpu-freq>.
16           If in doubt, say N.
18 if CPU_FREQ
20 config CPU_FREQ_TABLE
21         tristate
23 config CPU_FREQ_GOV_COMMON
24         bool
26 config CPU_FREQ_STAT
27         tristate "CPU frequency translation statistics"
28         select CPU_FREQ_TABLE
29         default y
30         help
31           This driver exports CPU frequency statistics information through sysfs
32           file system.
34           To compile this driver as a module, choose M here: the
35           module will be called cpufreq_stats.
37           If in doubt, say N.
39 config CPU_FREQ_STAT_DETAILS
40         bool "CPU frequency translation statistics details"
41         depends on CPU_FREQ_STAT
42         help
43           This will show detail CPU frequency translation table in sysfs file
44           system.
46           If in doubt, say N.
48 choice
49         prompt "Default CPUFreq governor"
50         default CPU_FREQ_DEFAULT_GOV_USERSPACE if CPU_FREQ_SA1100 || CPU_FREQ_SA1110
51         default CPU_FREQ_DEFAULT_GOV_PERFORMANCE
52         help
53           This option sets which CPUFreq governor shall be loaded at
54           startup. If in doubt, select 'performance'.
56 config CPU_FREQ_DEFAULT_GOV_PERFORMANCE
57         bool "performance"
58         select CPU_FREQ_GOV_PERFORMANCE
59         help
60           Use the CPUFreq governor 'performance' as default. This sets
61           the frequency statically to the highest frequency supported by
62           the CPU.
64 config CPU_FREQ_DEFAULT_GOV_POWERSAVE
65         bool "powersave"
66         depends on EXPERT
67         select CPU_FREQ_GOV_POWERSAVE
68         help
69           Use the CPUFreq governor 'powersave' as default. This sets
70           the frequency statically to the lowest frequency supported by
71           the CPU.
73 config CPU_FREQ_DEFAULT_GOV_USERSPACE
74         bool "userspace"
75         select CPU_FREQ_GOV_USERSPACE
76         help
77           Use the CPUFreq governor 'userspace' as default. This allows
78           you to set the CPU frequency manually or when a userspace 
79           program shall be able to set the CPU dynamically without having
80           to enable the userspace governor manually.
82 config CPU_FREQ_DEFAULT_GOV_ONDEMAND
83         bool "ondemand"
84         select CPU_FREQ_GOV_ONDEMAND
85         select CPU_FREQ_GOV_PERFORMANCE
86         help
87           Use the CPUFreq governor 'ondemand' as default. This allows
88           you to get a full dynamic frequency capable system by simply
89           loading your cpufreq low-level hardware driver.
90           Be aware that not all cpufreq drivers support the ondemand
91           governor. If unsure have a look at the help section of the
92           driver. Fallback governor will be the performance governor.
94 config CPU_FREQ_DEFAULT_GOV_CONSERVATIVE
95         bool "conservative"
96         select CPU_FREQ_GOV_CONSERVATIVE
97         select CPU_FREQ_GOV_PERFORMANCE
98         help
99           Use the CPUFreq governor 'conservative' as default. This allows
100           you to get a full dynamic frequency capable system by simply
101           loading your cpufreq low-level hardware driver.
102           Be aware that not all cpufreq drivers support the conservative
103           governor. If unsure have a look at the help section of the
104           driver. Fallback governor will be the performance governor.
106 config CPU_FREQ_DEFAULT_GOV_INTERACTIVE
107         bool "interactive"
108         select CPU_FREQ_GOV_INTERACTIVE
109         help
110           Use the CPUFreq governor 'interactive' as default. This allows
111           you to get a full dynamic cpu frequency capable system by simply
112           loading your cpufreq low-level hardware driver, using the
113           'interactive' governor for latency-sensitive workloads.
115 endchoice
117 config CPU_FREQ_GOV_PERFORMANCE
118         tristate "'performance' governor"
119         help
120           This cpufreq governor sets the frequency statically to the
121           highest available CPU frequency.
123           To compile this driver as a module, choose M here: the
124           module will be called cpufreq_performance.
126           If in doubt, say Y.
128 config CPU_FREQ_GOV_POWERSAVE
129         tristate "'powersave' governor"
130         help
131           This cpufreq governor sets the frequency statically to the
132           lowest available CPU frequency.
134           To compile this driver as a module, choose M here: the
135           module will be called cpufreq_powersave.
137           If in doubt, say Y.
139 config CPU_FREQ_GOV_USERSPACE
140         tristate "'userspace' governor for userspace frequency scaling"
141         help
142           Enable this cpufreq governor when you either want to set the
143           CPU frequency manually or when a userspace program shall
144           be able to set the CPU dynamically, like on LART 
145           <http://www.lartmaker.nl/>.
147           To compile this driver as a module, choose M here: the
148           module will be called cpufreq_userspace.
150           For details, take a look at <file:Documentation/cpu-freq/>.
152           If in doubt, say Y.
154 config CPU_FREQ_GOV_ONDEMAND
155         tristate "'ondemand' cpufreq policy governor"
156         select CPU_FREQ_TABLE
157         select CPU_FREQ_GOV_COMMON
158         help
159           'ondemand' - This driver adds a dynamic cpufreq policy governor.
160           The governor does a periodic polling and 
161           changes frequency based on the CPU utilization.
162           The support for this governor depends on CPU capability to
163           do fast frequency switching (i.e, very low latency frequency
164           transitions). 
166           To compile this driver as a module, choose M here: the
167           module will be called cpufreq_ondemand.
169           For details, take a look at linux/Documentation/cpu-freq.
171           If in doubt, say N.
173 config CPU_FREQ_GOV_INTERACTIVE
174         tristate "'interactive' cpufreq policy governor"
175         help
176           'interactive' - This driver adds a dynamic cpufreq policy governor
177           designed for latency-sensitive workloads.
179           This governor attempts to reduce the latency of clock
180           increases so that the system is more responsive to
181           interactive workloads.
183           To compile this driver as a module, choose M here: the
184           module will be called cpufreq_interactive.
186           For details, take a look at linux/Documentation/cpu-freq.
188           If in doubt, say N.
190 config CPU_FREQ_GOV_CONSERVATIVE
191         tristate "'conservative' cpufreq governor"
192         depends on CPU_FREQ
193         select CPU_FREQ_GOV_COMMON
194         help
195           'conservative' - this driver is rather similar to the 'ondemand'
196           governor both in its source code and its purpose, the difference is
197           its optimisation for better suitability in a battery powered
198           environment.  The frequency is gracefully increased and decreased
199           rather than jumping to 100% when speed is required.
201           If you have a desktop machine then you should really be considering
202           the 'ondemand' governor instead, however if you are using a laptop,
203           PDA or even an AMD64 based computer (due to the unacceptable
204           step-by-step latency issues between the minimum and maximum frequency
205           transitions in the CPU) you will probably want to use this governor.
207           To compile this driver as a module, choose M here: the
208           module will be called cpufreq_conservative.
210           For details, take a look at linux/Documentation/cpu-freq.
212           If in doubt, say N.
214 config GENERIC_CPUFREQ_CPU0
215         tristate "Generic CPU0 cpufreq driver"
216         depends on HAVE_CLK && REGULATOR && PM_OPP && OF
217         select CPU_FREQ_TABLE
218         help
219           This adds a generic cpufreq driver for CPU0 frequency management.
220           It supports both uniprocessor (UP) and symmetric multiprocessor (SMP)
221           systems which share clock and voltage across all CPUs.
223           If in doubt, say N.
225 menu "x86 CPU frequency scaling drivers"
226 depends on X86
227 source "drivers/cpufreq/Kconfig.x86"
228 endmenu
230 menu "ARM CPU frequency scaling drivers"
231 depends on ARM
232 source "drivers/cpufreq/Kconfig.arm"
233 endmenu
235 menu "PowerPC CPU frequency scaling drivers"
236 depends on PPC32 || PPC64
237 source "drivers/cpufreq/Kconfig.powerpc"
238 endmenu
240 endif
241 endmenu