]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - drivers/cpufreq/Kconfig
Merge remote-tracking branch 'asoc/fix/sta529' into tmp
[android-sdk/kernel-video.git] / drivers / cpufreq / Kconfig
1 menu "CPU Frequency scaling"
3 config CPU_FREQ
4         bool "CPU Frequency scaling"
5         help
6           CPU Frequency scaling allows you to change the clock speed of 
7           CPUs on the fly. This is a nice method to save power, because 
8           the lower the CPU clock speed, the less power the CPU consumes.
10           Note that this driver doesn't automatically change the CPU
11           clock speed, you need to either enable a dynamic cpufreq governor
12           (see below) after boot, or use a userspace tool.
14           For details, take a look at <file:Documentation/cpu-freq>.
16           If in doubt, say N.
18 if CPU_FREQ
20 config CPU_FREQ_TABLE
21         tristate
23 config CPU_FREQ_GOV_COMMON
24         bool
26 config CPU_FREQ_STAT
27         tristate "CPU frequency translation statistics"
28         select CPU_FREQ_TABLE
29         default y
30         help
31           This driver exports CPU frequency statistics information through sysfs
32           file system.
34           To compile this driver as a module, choose M here: the
35           module will be called cpufreq_stats.
37           If in doubt, say N.
39 config CPU_FREQ_STAT_DETAILS
40         bool "CPU frequency translation statistics details"
41         depends on CPU_FREQ_STAT
42         help
43           This will show detail CPU frequency translation table in sysfs file
44           system.
46           If in doubt, say N.
48 choice
49         prompt "Default CPUFreq governor"
50         default CPU_FREQ_DEFAULT_GOV_USERSPACE if CPU_FREQ_SA1100 || CPU_FREQ_SA1110
51         default CPU_FREQ_DEFAULT_GOV_PERFORMANCE
52         help
53           This option sets which CPUFreq governor shall be loaded at
54           startup. If in doubt, select 'performance'.
56 config CPU_FREQ_DEFAULT_GOV_PERFORMANCE
57         bool "performance"
58         select CPU_FREQ_GOV_PERFORMANCE
59         help
60           Use the CPUFreq governor 'performance' as default. This sets
61           the frequency statically to the highest frequency supported by
62           the CPU.
64 config CPU_FREQ_DEFAULT_GOV_POWERSAVE
65         bool "powersave"
66         depends on EXPERT
67         select CPU_FREQ_GOV_POWERSAVE
68         help
69           Use the CPUFreq governor 'powersave' as default. This sets
70           the frequency statically to the lowest frequency supported by
71           the CPU.
73 config CPU_FREQ_DEFAULT_GOV_USERSPACE
74         bool "userspace"
75         select CPU_FREQ_GOV_USERSPACE
76         help
77           Use the CPUFreq governor 'userspace' as default. This allows
78           you to set the CPU frequency manually or when a userspace 
79           program shall be able to set the CPU dynamically without having
80           to enable the userspace governor manually.
82 config CPU_FREQ_DEFAULT_GOV_ONDEMAND
83         bool "ondemand"
84         select CPU_FREQ_GOV_ONDEMAND
85         select CPU_FREQ_GOV_PERFORMANCE
86         help
87           Use the CPUFreq governor 'ondemand' as default. This allows
88           you to get a full dynamic frequency capable system by simply
89           loading your cpufreq low-level hardware driver.
90           Be aware that not all cpufreq drivers support the ondemand
91           governor. If unsure have a look at the help section of the
92           driver. Fallback governor will be the performance governor.
94 config CPU_FREQ_DEFAULT_GOV_CONSERVATIVE
95         bool "conservative"
96         select CPU_FREQ_GOV_CONSERVATIVE
97         select CPU_FREQ_GOV_PERFORMANCE
98         help
99           Use the CPUFreq governor 'conservative' as default. This allows
100           you to get a full dynamic frequency capable system by simply
101           loading your cpufreq low-level hardware driver.
102           Be aware that not all cpufreq drivers support the conservative
103           governor. If unsure have a look at the help section of the
104           driver. Fallback governor will be the performance governor.
105 endchoice
107 config CPU_FREQ_GOV_PERFORMANCE
108         tristate "'performance' governor"
109         help
110           This cpufreq governor sets the frequency statically to the
111           highest available CPU frequency.
113           To compile this driver as a module, choose M here: the
114           module will be called cpufreq_performance.
116           If in doubt, say Y.
118 config CPU_FREQ_GOV_POWERSAVE
119         tristate "'powersave' governor"
120         help
121           This cpufreq governor sets the frequency statically to the
122           lowest available CPU frequency.
124           To compile this driver as a module, choose M here: the
125           module will be called cpufreq_powersave.
127           If in doubt, say Y.
129 config CPU_FREQ_GOV_USERSPACE
130         tristate "'userspace' governor for userspace frequency scaling"
131         help
132           Enable this cpufreq governor when you either want to set the
133           CPU frequency manually or when a userspace program shall
134           be able to set the CPU dynamically, like on LART 
135           <http://www.lartmaker.nl/>.
137           To compile this driver as a module, choose M here: the
138           module will be called cpufreq_userspace.
140           For details, take a look at <file:Documentation/cpu-freq/>.
142           If in doubt, say Y.
144 config CPU_FREQ_GOV_ONDEMAND
145         tristate "'ondemand' cpufreq policy governor"
146         select CPU_FREQ_TABLE
147         select CPU_FREQ_GOV_COMMON
148         help
149           'ondemand' - This driver adds a dynamic cpufreq policy governor.
150           The governor does a periodic polling and 
151           changes frequency based on the CPU utilization.
152           The support for this governor depends on CPU capability to
153           do fast frequency switching (i.e, very low latency frequency
154           transitions). 
156           To compile this driver as a module, choose M here: the
157           module will be called cpufreq_ondemand.
159           For details, take a look at linux/Documentation/cpu-freq.
161           If in doubt, say N.
163 config CPU_FREQ_GOV_CONSERVATIVE
164         tristate "'conservative' cpufreq governor"
165         depends on CPU_FREQ
166         select CPU_FREQ_GOV_COMMON
167         help
168           'conservative' - this driver is rather similar to the 'ondemand'
169           governor both in its source code and its purpose, the difference is
170           its optimisation for better suitability in a battery powered
171           environment.  The frequency is gracefully increased and decreased
172           rather than jumping to 100% when speed is required.
174           If you have a desktop machine then you should really be considering
175           the 'ondemand' governor instead, however if you are using a laptop,
176           PDA or even an AMD64 based computer (due to the unacceptable
177           step-by-step latency issues between the minimum and maximum frequency
178           transitions in the CPU) you will probably want to use this governor.
180           To compile this driver as a module, choose M here: the
181           module will be called cpufreq_conservative.
183           For details, take a look at linux/Documentation/cpu-freq.
185           If in doubt, say N.
187 config GENERIC_CPUFREQ_CPU0
188         bool "Generic CPU0 cpufreq driver"
189         depends on HAVE_CLK && REGULATOR && PM_OPP && OF
190         select CPU_FREQ_TABLE
191         help
192           This adds a generic cpufreq driver for CPU0 frequency management.
193           It supports both uniprocessor (UP) and symmetric multiprocessor (SMP)
194           systems which share clock and voltage across all CPUs.
196           If in doubt, say N.
198 menu "x86 CPU frequency scaling drivers"
199 depends on X86
200 source "drivers/cpufreq/Kconfig.x86"
201 endmenu
203 menu "ARM CPU frequency scaling drivers"
204 depends on ARM
205 source "drivers/cpufreq/Kconfig.arm"
206 endmenu
208 menu "PowerPC CPU frequency scaling drivers"
209 depends on PPC32 || PPC64
210 source "drivers/cpufreq/Kconfig.powerpc"
211 endmenu
213 endif
214 endmenu