]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - drivers/edac/i5000_edac.c
Merge branch 'drm-nouveau-fixes-3.8' of git://anongit.freedesktop.org/git/nouveau...
[android-sdk/kernel-video.git] / drivers / edac / i5000_edac.c
1 /*
2  * Intel 5000(P/V/X) class Memory Controllers kernel module
3  *
4  * This file may be distributed under the terms of the
5  * GNU General Public License.
6  *
7  * Written by Douglas Thompson Linux Networx (http://lnxi.com)
8  *      norsk5@xmission.com
9  *
10  * This module is based on the following document:
11  *
12  * Intel 5000X Chipset Memory Controller Hub (MCH) - Datasheet
13  *      http://developer.intel.com/design/chipsets/datashts/313070.htm
14  *
15  */
17 #include <linux/module.h>
18 #include <linux/init.h>
19 #include <linux/pci.h>
20 #include <linux/pci_ids.h>
21 #include <linux/slab.h>
22 #include <linux/edac.h>
23 #include <asm/mmzone.h>
25 #include "edac_core.h"
27 /*
28  * Alter this version for the I5000 module when modifications are made
29  */
30 #define I5000_REVISION    " Ver: 2.0.12"
31 #define EDAC_MOD_STR      "i5000_edac"
33 #define i5000_printk(level, fmt, arg...) \
34         edac_printk(level, "i5000", fmt, ##arg)
36 #define i5000_mc_printk(mci, level, fmt, arg...) \
37         edac_mc_chipset_printk(mci, level, "i5000", fmt, ##arg)
39 #ifndef PCI_DEVICE_ID_INTEL_FBD_0
40 #define PCI_DEVICE_ID_INTEL_FBD_0       0x25F5
41 #endif
42 #ifndef PCI_DEVICE_ID_INTEL_FBD_1
43 #define PCI_DEVICE_ID_INTEL_FBD_1       0x25F6
44 #endif
46 /* Device 16,
47  * Function 0: System Address
48  * Function 1: Memory Branch Map, Control, Errors Register
49  * Function 2: FSB Error Registers
50  *
51  * All 3 functions of Device 16 (0,1,2) share the SAME DID
52  */
53 #define PCI_DEVICE_ID_INTEL_I5000_DEV16 0x25F0
55 /* OFFSETS for Function 0 */
57 /* OFFSETS for Function 1 */
58 #define         AMBASE                  0x48
59 #define         MAXCH                   0x56
60 #define         MAXDIMMPERCH            0x57
61 #define         TOLM                    0x6C
62 #define         REDMEMB                 0x7C
63 #define                 RED_ECC_LOCATOR(x)      ((x) & 0x3FFFF)
64 #define                 REC_ECC_LOCATOR_EVEN(x) ((x) & 0x001FF)
65 #define                 REC_ECC_LOCATOR_ODD(x)  ((x) & 0x3FE00)
66 #define         MIR0                    0x80
67 #define         MIR1                    0x84
68 #define         MIR2                    0x88
69 #define         AMIR0                   0x8C
70 #define         AMIR1                   0x90
71 #define         AMIR2                   0x94
73 #define         FERR_FAT_FBD            0x98
74 #define         NERR_FAT_FBD            0x9C
75 #define                 EXTRACT_FBDCHAN_INDX(x) (((x)>>28) & 0x3)
76 #define                 FERR_FAT_FBDCHAN 0x30000000
77 #define                 FERR_FAT_M3ERR  0x00000004
78 #define                 FERR_FAT_M2ERR  0x00000002
79 #define                 FERR_FAT_M1ERR  0x00000001
80 #define                 FERR_FAT_MASK   (FERR_FAT_M1ERR | \
81                                                 FERR_FAT_M2ERR | \
82                                                 FERR_FAT_M3ERR)
84 #define         FERR_NF_FBD             0xA0
86 /* Thermal and SPD or BFD errors */
87 #define                 FERR_NF_M28ERR  0x01000000
88 #define                 FERR_NF_M27ERR  0x00800000
89 #define                 FERR_NF_M26ERR  0x00400000
90 #define                 FERR_NF_M25ERR  0x00200000
91 #define                 FERR_NF_M24ERR  0x00100000
92 #define                 FERR_NF_M23ERR  0x00080000
93 #define                 FERR_NF_M22ERR  0x00040000
94 #define                 FERR_NF_M21ERR  0x00020000
96 /* Correctable errors */
97 #define                 FERR_NF_M20ERR  0x00010000
98 #define                 FERR_NF_M19ERR  0x00008000
99 #define                 FERR_NF_M18ERR  0x00004000
100 #define                 FERR_NF_M17ERR  0x00002000
102 /* Non-Retry or redundant Retry errors */
103 #define                 FERR_NF_M16ERR  0x00001000
104 #define                 FERR_NF_M15ERR  0x00000800
105 #define                 FERR_NF_M14ERR  0x00000400
106 #define                 FERR_NF_M13ERR  0x00000200
108 /* Uncorrectable errors */
109 #define                 FERR_NF_M12ERR  0x00000100
110 #define                 FERR_NF_M11ERR  0x00000080
111 #define                 FERR_NF_M10ERR  0x00000040
112 #define                 FERR_NF_M9ERR   0x00000020
113 #define                 FERR_NF_M8ERR   0x00000010
114 #define                 FERR_NF_M7ERR   0x00000008
115 #define                 FERR_NF_M6ERR   0x00000004
116 #define                 FERR_NF_M5ERR   0x00000002
117 #define                 FERR_NF_M4ERR   0x00000001
119 #define                 FERR_NF_UNCORRECTABLE   (FERR_NF_M12ERR | \
120                                                         FERR_NF_M11ERR | \
121                                                         FERR_NF_M10ERR | \
122                                                         FERR_NF_M9ERR | \
123                                                         FERR_NF_M8ERR | \
124                                                         FERR_NF_M7ERR | \
125                                                         FERR_NF_M6ERR | \
126                                                         FERR_NF_M5ERR | \
127                                                         FERR_NF_M4ERR)
128 #define                 FERR_NF_CORRECTABLE     (FERR_NF_M20ERR | \
129                                                         FERR_NF_M19ERR | \
130                                                         FERR_NF_M18ERR | \
131                                                         FERR_NF_M17ERR)
132 #define                 FERR_NF_DIMM_SPARE      (FERR_NF_M27ERR | \
133                                                         FERR_NF_M28ERR)
134 #define                 FERR_NF_THERMAL         (FERR_NF_M26ERR | \
135                                                         FERR_NF_M25ERR | \
136                                                         FERR_NF_M24ERR | \
137                                                         FERR_NF_M23ERR)
138 #define                 FERR_NF_SPD_PROTOCOL    (FERR_NF_M22ERR)
139 #define                 FERR_NF_NORTH_CRC       (FERR_NF_M21ERR)
140 #define                 FERR_NF_NON_RETRY       (FERR_NF_M13ERR | \
141                                                         FERR_NF_M14ERR | \
142                                                         FERR_NF_M15ERR)
144 #define         NERR_NF_FBD             0xA4
145 #define                 FERR_NF_MASK            (FERR_NF_UNCORRECTABLE | \
146                                                         FERR_NF_CORRECTABLE | \
147                                                         FERR_NF_DIMM_SPARE | \
148                                                         FERR_NF_THERMAL | \
149                                                         FERR_NF_SPD_PROTOCOL | \
150                                                         FERR_NF_NORTH_CRC | \
151                                                         FERR_NF_NON_RETRY)
153 #define         EMASK_FBD               0xA8
154 #define                 EMASK_FBD_M28ERR        0x08000000
155 #define                 EMASK_FBD_M27ERR        0x04000000
156 #define                 EMASK_FBD_M26ERR        0x02000000
157 #define                 EMASK_FBD_M25ERR        0x01000000
158 #define                 EMASK_FBD_M24ERR        0x00800000
159 #define                 EMASK_FBD_M23ERR        0x00400000
160 #define                 EMASK_FBD_M22ERR        0x00200000
161 #define                 EMASK_FBD_M21ERR        0x00100000
162 #define                 EMASK_FBD_M20ERR        0x00080000
163 #define                 EMASK_FBD_M19ERR        0x00040000
164 #define                 EMASK_FBD_M18ERR        0x00020000
165 #define                 EMASK_FBD_M17ERR        0x00010000
167 #define                 EMASK_FBD_M15ERR        0x00004000
168 #define                 EMASK_FBD_M14ERR        0x00002000
169 #define                 EMASK_FBD_M13ERR        0x00001000
170 #define                 EMASK_FBD_M12ERR        0x00000800
171 #define                 EMASK_FBD_M11ERR        0x00000400
172 #define                 EMASK_FBD_M10ERR        0x00000200
173 #define                 EMASK_FBD_M9ERR         0x00000100
174 #define                 EMASK_FBD_M8ERR         0x00000080
175 #define                 EMASK_FBD_M7ERR         0x00000040
176 #define                 EMASK_FBD_M6ERR         0x00000020
177 #define                 EMASK_FBD_M5ERR         0x00000010
178 #define                 EMASK_FBD_M4ERR         0x00000008
179 #define                 EMASK_FBD_M3ERR         0x00000004
180 #define                 EMASK_FBD_M2ERR         0x00000002
181 #define                 EMASK_FBD_M1ERR         0x00000001
183 #define                 ENABLE_EMASK_FBD_FATAL_ERRORS   (EMASK_FBD_M1ERR | \
184                                                         EMASK_FBD_M2ERR | \
185                                                         EMASK_FBD_M3ERR)
187 #define                 ENABLE_EMASK_FBD_UNCORRECTABLE  (EMASK_FBD_M4ERR | \
188                                                         EMASK_FBD_M5ERR | \
189                                                         EMASK_FBD_M6ERR | \
190                                                         EMASK_FBD_M7ERR | \
191                                                         EMASK_FBD_M8ERR | \
192                                                         EMASK_FBD_M9ERR | \
193                                                         EMASK_FBD_M10ERR | \
194                                                         EMASK_FBD_M11ERR | \
195                                                         EMASK_FBD_M12ERR)
196 #define                 ENABLE_EMASK_FBD_CORRECTABLE    (EMASK_FBD_M17ERR | \
197                                                         EMASK_FBD_M18ERR | \
198                                                         EMASK_FBD_M19ERR | \
199                                                         EMASK_FBD_M20ERR)
200 #define                 ENABLE_EMASK_FBD_DIMM_SPARE     (EMASK_FBD_M27ERR | \
201                                                         EMASK_FBD_M28ERR)
202 #define                 ENABLE_EMASK_FBD_THERMALS       (EMASK_FBD_M26ERR | \
203                                                         EMASK_FBD_M25ERR | \
204                                                         EMASK_FBD_M24ERR | \
205                                                         EMASK_FBD_M23ERR)
206 #define                 ENABLE_EMASK_FBD_SPD_PROTOCOL   (EMASK_FBD_M22ERR)
207 #define                 ENABLE_EMASK_FBD_NORTH_CRC      (EMASK_FBD_M21ERR)
208 #define                 ENABLE_EMASK_FBD_NON_RETRY      (EMASK_FBD_M15ERR | \
209                                                         EMASK_FBD_M14ERR | \
210                                                         EMASK_FBD_M13ERR)
212 #define         ENABLE_EMASK_ALL        (ENABLE_EMASK_FBD_NON_RETRY | \
213                                         ENABLE_EMASK_FBD_NORTH_CRC | \
214                                         ENABLE_EMASK_FBD_SPD_PROTOCOL | \
215                                         ENABLE_EMASK_FBD_THERMALS | \
216                                         ENABLE_EMASK_FBD_DIMM_SPARE | \
217                                         ENABLE_EMASK_FBD_FATAL_ERRORS | \
218                                         ENABLE_EMASK_FBD_CORRECTABLE | \
219                                         ENABLE_EMASK_FBD_UNCORRECTABLE)
221 #define         ERR0_FBD                0xAC
222 #define         ERR1_FBD                0xB0
223 #define         ERR2_FBD                0xB4
224 #define         MCERR_FBD               0xB8
225 #define         NRECMEMA                0xBE
226 #define                 NREC_BANK(x)            (((x)>>12) & 0x7)
227 #define                 NREC_RDWR(x)            (((x)>>11) & 1)
228 #define                 NREC_RANK(x)            (((x)>>8) & 0x7)
229 #define         NRECMEMB                0xC0
230 #define                 NREC_CAS(x)             (((x)>>16) & 0xFFFFFF)
231 #define                 NREC_RAS(x)             ((x) & 0x7FFF)
232 #define         NRECFGLOG               0xC4
233 #define         NREEECFBDA              0xC8
234 #define         NREEECFBDB              0xCC
235 #define         NREEECFBDC              0xD0
236 #define         NREEECFBDD              0xD4
237 #define         NREEECFBDE              0xD8
238 #define         REDMEMA                 0xDC
239 #define         RECMEMA                 0xE2
240 #define                 REC_BANK(x)             (((x)>>12) & 0x7)
241 #define                 REC_RDWR(x)             (((x)>>11) & 1)
242 #define                 REC_RANK(x)             (((x)>>8) & 0x7)
243 #define         RECMEMB                 0xE4
244 #define                 REC_CAS(x)              (((x)>>16) & 0xFFFFFF)
245 #define                 REC_RAS(x)              ((x) & 0x7FFF)
246 #define         RECFGLOG                0xE8
247 #define         RECFBDA                 0xEC
248 #define         RECFBDB                 0xF0
249 #define         RECFBDC                 0xF4
250 #define         RECFBDD                 0xF8
251 #define         RECFBDE                 0xFC
253 /* OFFSETS for Function 2 */
255 /*
256  * Device 21,
257  * Function 0: Memory Map Branch 0
258  *
259  * Device 22,
260  * Function 0: Memory Map Branch 1
261  */
262 #define PCI_DEVICE_ID_I5000_BRANCH_0    0x25F5
263 #define PCI_DEVICE_ID_I5000_BRANCH_1    0x25F6
265 #define AMB_PRESENT_0   0x64
266 #define AMB_PRESENT_1   0x66
267 #define MTR0            0x80
268 #define MTR1            0x84
269 #define MTR2            0x88
270 #define MTR3            0x8C
272 #define NUM_MTRS                4
273 #define CHANNELS_PER_BRANCH     2
274 #define MAX_BRANCHES            2
276 /* Defines to extract the various fields from the
277  *      MTRx - Memory Technology Registers
278  */
279 #define MTR_DIMMS_PRESENT(mtr)          ((mtr) & (0x1 << 8))
280 #define MTR_DRAM_WIDTH(mtr)             ((((mtr) >> 6) & 0x1) ? 8 : 4)
281 #define MTR_DRAM_BANKS(mtr)             ((((mtr) >> 5) & 0x1) ? 8 : 4)
282 #define MTR_DRAM_BANKS_ADDR_BITS(mtr)   ((MTR_DRAM_BANKS(mtr) == 8) ? 3 : 2)
283 #define MTR_DIMM_RANK(mtr)              (((mtr) >> 4) & 0x1)
284 #define MTR_DIMM_RANK_ADDR_BITS(mtr)    (MTR_DIMM_RANK(mtr) ? 2 : 1)
285 #define MTR_DIMM_ROWS(mtr)              (((mtr) >> 2) & 0x3)
286 #define MTR_DIMM_ROWS_ADDR_BITS(mtr)    (MTR_DIMM_ROWS(mtr) + 13)
287 #define MTR_DIMM_COLS(mtr)              ((mtr) & 0x3)
288 #define MTR_DIMM_COLS_ADDR_BITS(mtr)    (MTR_DIMM_COLS(mtr) + 10)
290 /* enables the report of miscellaneous messages as CE errors - default off */
291 static int misc_messages;
293 /* Enumeration of supported devices */
294 enum i5000_chips {
295         I5000P = 0,
296         I5000V = 1,             /* future */
297         I5000X = 2              /* future */
298 };
300 /* Device name and register DID (Device ID) */
301 struct i5000_dev_info {
302         const char *ctl_name;   /* name for this device */
303         u16 fsb_mapping_errors; /* DID for the branchmap,control */
304 };
306 /* Table of devices attributes supported by this driver */
307 static const struct i5000_dev_info i5000_devs[] = {
308         [I5000P] = {
309                 .ctl_name = "I5000",
310                 .fsb_mapping_errors = PCI_DEVICE_ID_INTEL_I5000_DEV16,
311         },
312 };
314 struct i5000_dimm_info {
315         int megabytes;          /* size, 0 means not present  */
316         int dual_rank;
317 };
319 #define MAX_CHANNELS    6       /* max possible channels */
320 #define MAX_CSROWS      (8*2)   /* max possible csrows per channel */
322 /* driver private data structure */
323 struct i5000_pvt {
324         struct pci_dev *system_address; /* 16.0 */
325         struct pci_dev *branchmap_werrors;      /* 16.1 */
326         struct pci_dev *fsb_error_regs; /* 16.2 */
327         struct pci_dev *branch_0;       /* 21.0 */
328         struct pci_dev *branch_1;       /* 22.0 */
330         u16 tolm;               /* top of low memory */
331         union {
332                 u64 ambase;             /* AMB BAR */
333                 struct {
334                         u32 ambase_bottom;
335                         u32 ambase_top;
336                 } u __packed;
337         };
339         u16 mir0, mir1, mir2;
341         u16 b0_mtr[NUM_MTRS];   /* Memory Technlogy Reg */
342         u16 b0_ambpresent0;     /* Branch 0, Channel 0 */
343         u16 b0_ambpresent1;     /* Brnach 0, Channel 1 */
345         u16 b1_mtr[NUM_MTRS];   /* Memory Technlogy Reg */
346         u16 b1_ambpresent0;     /* Branch 1, Channel 8 */
347         u16 b1_ambpresent1;     /* Branch 1, Channel 1 */
349         /* DIMM information matrix, allocating architecture maximums */
350         struct i5000_dimm_info dimm_info[MAX_CSROWS][MAX_CHANNELS];
352         /* Actual values for this controller */
353         int maxch;              /* Max channels */
354         int maxdimmperch;       /* Max DIMMs per channel */
355 };
357 /* I5000 MCH error information retrieved from Hardware */
358 struct i5000_error_info {
360         /* These registers are always read from the MC */
361         u32 ferr_fat_fbd;       /* First Errors Fatal */
362         u32 nerr_fat_fbd;       /* Next Errors Fatal */
363         u32 ferr_nf_fbd;        /* First Errors Non-Fatal */
364         u32 nerr_nf_fbd;        /* Next Errors Non-Fatal */
366         /* These registers are input ONLY if there was a Recoverable  Error */
367         u32 redmemb;            /* Recoverable Mem Data Error log B */
368         u16 recmema;            /* Recoverable Mem Error log A */
369         u32 recmemb;            /* Recoverable Mem Error log B */
371         /* These registers are input ONLY if there was a
372          * Non-Recoverable Error */
373         u16 nrecmema;           /* Non-Recoverable Mem log A */
374         u16 nrecmemb;           /* Non-Recoverable Mem log B */
376 };
378 static struct edac_pci_ctl_info *i5000_pci;
380 /*
381  *      i5000_get_error_info    Retrieve the hardware error information from
382  *                              the hardware and cache it in the 'info'
383  *                              structure
384  */
385 static void i5000_get_error_info(struct mem_ctl_info *mci,
386                                  struct i5000_error_info *info)
388         struct i5000_pvt *pvt;
389         u32 value;
391         pvt = mci->pvt_info;
393         /* read in the 1st FATAL error register */
394         pci_read_config_dword(pvt->branchmap_werrors, FERR_FAT_FBD, &value);
396         /* Mask only the bits that the doc says are valid
397          */
398         value &= (FERR_FAT_FBDCHAN | FERR_FAT_MASK);
400         /* If there is an error, then read in the */
401         /* NEXT FATAL error register and the Memory Error Log Register A */
402         if (value & FERR_FAT_MASK) {
403                 info->ferr_fat_fbd = value;
405                 /* harvest the various error data we need */
406                 pci_read_config_dword(pvt->branchmap_werrors,
407                                 NERR_FAT_FBD, &info->nerr_fat_fbd);
408                 pci_read_config_word(pvt->branchmap_werrors,
409                                 NRECMEMA, &info->nrecmema);
410                 pci_read_config_word(pvt->branchmap_werrors,
411                                 NRECMEMB, &info->nrecmemb);
413                 /* Clear the error bits, by writing them back */
414                 pci_write_config_dword(pvt->branchmap_werrors,
415                                 FERR_FAT_FBD, value);
416         } else {
417                 info->ferr_fat_fbd = 0;
418                 info->nerr_fat_fbd = 0;
419                 info->nrecmema = 0;
420                 info->nrecmemb = 0;
421         }
423         /* read in the 1st NON-FATAL error register */
424         pci_read_config_dword(pvt->branchmap_werrors, FERR_NF_FBD, &value);
426         /* If there is an error, then read in the 1st NON-FATAL error
427          * register as well */
428         if (value & FERR_NF_MASK) {
429                 info->ferr_nf_fbd = value;
431                 /* harvest the various error data we need */
432                 pci_read_config_dword(pvt->branchmap_werrors,
433                                 NERR_NF_FBD, &info->nerr_nf_fbd);
434                 pci_read_config_word(pvt->branchmap_werrors,
435                                 RECMEMA, &info->recmema);
436                 pci_read_config_dword(pvt->branchmap_werrors,
437                                 RECMEMB, &info->recmemb);
438                 pci_read_config_dword(pvt->branchmap_werrors,
439                                 REDMEMB, &info->redmemb);
441                 /* Clear the error bits, by writing them back */
442                 pci_write_config_dword(pvt->branchmap_werrors,
443                                 FERR_NF_FBD, value);
444         } else {
445                 info->ferr_nf_fbd = 0;
446                 info->nerr_nf_fbd = 0;
447                 info->recmema = 0;
448                 info->recmemb = 0;
449                 info->redmemb = 0;
450         }
453 /*
454  * i5000_process_fatal_error_info(struct mem_ctl_info *mci,
455  *                                      struct i5000_error_info *info,
456  *                                      int handle_errors);
457  *
458  *      handle the Intel FATAL errors, if any
459  */
460 static void i5000_process_fatal_error_info(struct mem_ctl_info *mci,
461                                         struct i5000_error_info *info,
462                                         int handle_errors)
464         char msg[EDAC_MC_LABEL_LEN + 1 + 160];
465         char *specific = NULL;
466         u32 allErrors;
467         int channel;
468         int bank;
469         int rank;
470         int rdwr;
471         int ras, cas;
473         /* mask off the Error bits that are possible */
474         allErrors = (info->ferr_fat_fbd & FERR_FAT_MASK);
475         if (!allErrors)
476                 return;         /* if no error, return now */
478         channel = EXTRACT_FBDCHAN_INDX(info->ferr_fat_fbd);
480         /* Use the NON-Recoverable macros to extract data */
481         bank = NREC_BANK(info->nrecmema);
482         rank = NREC_RANK(info->nrecmema);
483         rdwr = NREC_RDWR(info->nrecmema);
484         ras = NREC_RAS(info->nrecmemb);
485         cas = NREC_CAS(info->nrecmemb);
487         edac_dbg(0, "\t\tCSROW= %d  Channel= %d (DRAM Bank= %d rdwr= %s ras= %d cas= %d)\n",
488                  rank, channel, bank,
489                  rdwr ? "Write" : "Read", ras, cas);
491         /* Only 1 bit will be on */
492         switch (allErrors) {
493         case FERR_FAT_M1ERR:
494                 specific = "Alert on non-redundant retry or fast "
495                                 "reset timeout";
496                 break;
497         case FERR_FAT_M2ERR:
498                 specific = "Northbound CRC error on non-redundant "
499                                 "retry";
500                 break;
501         case FERR_FAT_M3ERR:
502                 {
503                 static int done;
505                 /*
506                  * This error is generated to inform that the intelligent
507                  * throttling is disabled and the temperature passed the
508                  * specified middle point. Since this is something the BIOS
509                  * should take care of, we'll warn only once to avoid
510                  * worthlessly flooding the log.
511                  */
512                 if (done)
513                         return;
514                 done++;
516                 specific = ">Tmid Thermal event with intelligent "
517                            "throttling disabled";
518                 }
519                 break;
520         }
522         /* Form out message */
523         snprintf(msg, sizeof(msg),
524                  "Bank=%d RAS=%d CAS=%d FATAL Err=0x%x (%s)",
525                  bank, ras, cas, allErrors, specific);
527         /* Call the helper to output message */
528         edac_mc_handle_error(HW_EVENT_ERR_FATAL, mci, 1, 0, 0, 0,
529                              channel >> 1, channel & 1, rank,
530                              rdwr ? "Write error" : "Read error",
531                              msg);
534 /*
535  * i5000_process_fatal_error_info(struct mem_ctl_info *mci,
536  *                              struct i5000_error_info *info,
537  *                              int handle_errors);
538  *
539  *      handle the Intel NON-FATAL errors, if any
540  */
541 static void i5000_process_nonfatal_error_info(struct mem_ctl_info *mci,
542                                         struct i5000_error_info *info,
543                                         int handle_errors)
545         char msg[EDAC_MC_LABEL_LEN + 1 + 170];
546         char *specific = NULL;
547         u32 allErrors;
548         u32 ue_errors;
549         u32 ce_errors;
550         u32 misc_errors;
551         int branch;
552         int channel;
553         int bank;
554         int rank;
555         int rdwr;
556         int ras, cas;
558         /* mask off the Error bits that are possible */
559         allErrors = (info->ferr_nf_fbd & FERR_NF_MASK);
560         if (!allErrors)
561                 return;         /* if no error, return now */
563         /* ONLY ONE of the possible error bits will be set, as per the docs */
564         ue_errors = allErrors & FERR_NF_UNCORRECTABLE;
565         if (ue_errors) {
566                 edac_dbg(0, "\tUncorrected bits= 0x%x\n", ue_errors);
568                 branch = EXTRACT_FBDCHAN_INDX(info->ferr_nf_fbd);
570                 /*
571                  * According with i5000 datasheet, bit 28 has no significance
572                  * for errors M4Err-M12Err and M17Err-M21Err, on FERR_NF_FBD
573                  */
574                 channel = branch & 2;
576                 bank = NREC_BANK(info->nrecmema);
577                 rank = NREC_RANK(info->nrecmema);
578                 rdwr = NREC_RDWR(info->nrecmema);
579                 ras = NREC_RAS(info->nrecmemb);
580                 cas = NREC_CAS(info->nrecmemb);
582                 edac_dbg(0, "\t\tCSROW= %d  Channels= %d,%d  (Branch= %d DRAM Bank= %d rdwr= %s ras= %d cas= %d)\n",
583                          rank, channel, channel + 1, branch >> 1, bank,
584                          rdwr ? "Write" : "Read", ras, cas);
586                 switch (ue_errors) {
587                 case FERR_NF_M12ERR:
588                         specific = "Non-Aliased Uncorrectable Patrol Data ECC";
589                         break;
590                 case FERR_NF_M11ERR:
591                         specific = "Non-Aliased Uncorrectable Spare-Copy "
592                                         "Data ECC";
593                         break;
594                 case FERR_NF_M10ERR:
595                         specific = "Non-Aliased Uncorrectable Mirrored Demand "
596                                         "Data ECC";
597                         break;
598                 case FERR_NF_M9ERR:
599                         specific = "Non-Aliased Uncorrectable Non-Mirrored "
600                                         "Demand Data ECC";
601                         break;
602                 case FERR_NF_M8ERR:
603                         specific = "Aliased Uncorrectable Patrol Data ECC";
604                         break;
605                 case FERR_NF_M7ERR:
606                         specific = "Aliased Uncorrectable Spare-Copy Data ECC";
607                         break;
608                 case FERR_NF_M6ERR:
609                         specific = "Aliased Uncorrectable Mirrored Demand "
610                                         "Data ECC";
611                         break;
612                 case FERR_NF_M5ERR:
613                         specific = "Aliased Uncorrectable Non-Mirrored Demand "
614                                         "Data ECC";
615                         break;
616                 case FERR_NF_M4ERR:
617                         specific = "Uncorrectable Data ECC on Replay";
618                         break;
619                 }
621                 /* Form out message */
622                 snprintf(msg, sizeof(msg),
623                          "Rank=%d Bank=%d RAS=%d CAS=%d, UE Err=0x%x (%s)",
624                          rank, bank, ras, cas, ue_errors, specific);
626                 /* Call the helper to output message */
627                 edac_mc_handle_error(HW_EVENT_ERR_UNCORRECTED, mci, 1, 0, 0, 0,
628                                 channel >> 1, -1, rank,
629                                 rdwr ? "Write error" : "Read error",
630                                 msg);
631         }
633         /* Check correctable errors */
634         ce_errors = allErrors & FERR_NF_CORRECTABLE;
635         if (ce_errors) {
636                 edac_dbg(0, "\tCorrected bits= 0x%x\n", ce_errors);
638                 branch = EXTRACT_FBDCHAN_INDX(info->ferr_nf_fbd);
640                 channel = 0;
641                 if (REC_ECC_LOCATOR_ODD(info->redmemb))
642                         channel = 1;
644                 /* Convert channel to be based from zero, instead of
645                  * from branch base of 0 */
646                 channel += branch;
648                 bank = REC_BANK(info->recmema);
649                 rank = REC_RANK(info->recmema);
650                 rdwr = REC_RDWR(info->recmema);
651                 ras = REC_RAS(info->recmemb);
652                 cas = REC_CAS(info->recmemb);
654                 edac_dbg(0, "\t\tCSROW= %d Channel= %d  (Branch %d DRAM Bank= %d rdwr= %s ras= %d cas= %d)\n",
655                          rank, channel, branch >> 1, bank,
656                          rdwr ? "Write" : "Read", ras, cas);
658                 switch (ce_errors) {
659                 case FERR_NF_M17ERR:
660                         specific = "Correctable Non-Mirrored Demand Data ECC";
661                         break;
662                 case FERR_NF_M18ERR:
663                         specific = "Correctable Mirrored Demand Data ECC";
664                         break;
665                 case FERR_NF_M19ERR:
666                         specific = "Correctable Spare-Copy Data ECC";
667                         break;
668                 case FERR_NF_M20ERR:
669                         specific = "Correctable Patrol Data ECC";
670                         break;
671                 }
673                 /* Form out message */
674                 snprintf(msg, sizeof(msg),
675                          "Rank=%d Bank=%d RDWR=%s RAS=%d "
676                          "CAS=%d, CE Err=0x%x (%s))", branch >> 1, bank,
677                          rdwr ? "Write" : "Read", ras, cas, ce_errors,
678                          specific);
680                 /* Call the helper to output message */
681                 edac_mc_handle_error(HW_EVENT_ERR_CORRECTED, mci, 1, 0, 0, 0,
682                                 channel >> 1, channel % 2, rank,
683                                 rdwr ? "Write error" : "Read error",
684                                 msg);
685         }
687         if (!misc_messages)
688                 return;
690         misc_errors = allErrors & (FERR_NF_NON_RETRY | FERR_NF_NORTH_CRC |
691                                    FERR_NF_SPD_PROTOCOL | FERR_NF_DIMM_SPARE);
692         if (misc_errors) {
693                 switch (misc_errors) {
694                 case FERR_NF_M13ERR:
695                         specific = "Non-Retry or Redundant Retry FBD Memory "
696                                         "Alert or Redundant Fast Reset Timeout";
697                         break;
698                 case FERR_NF_M14ERR:
699                         specific = "Non-Retry or Redundant Retry FBD "
700                                         "Configuration Alert";
701                         break;
702                 case FERR_NF_M15ERR:
703                         specific = "Non-Retry or Redundant Retry FBD "
704                                         "Northbound CRC error on read data";
705                         break;
706                 case FERR_NF_M21ERR:
707                         specific = "FBD Northbound CRC error on "
708                                         "FBD Sync Status";
709                         break;
710                 case FERR_NF_M22ERR:
711                         specific = "SPD protocol error";
712                         break;
713                 case FERR_NF_M27ERR:
714                         specific = "DIMM-spare copy started";
715                         break;
716                 case FERR_NF_M28ERR:
717                         specific = "DIMM-spare copy completed";
718                         break;
719                 }
720                 branch = EXTRACT_FBDCHAN_INDX(info->ferr_nf_fbd);
722                 /* Form out message */
723                 snprintf(msg, sizeof(msg),
724                          "Err=%#x (%s)", misc_errors, specific);
726                 /* Call the helper to output message */
727                 edac_mc_handle_error(HW_EVENT_ERR_CORRECTED, mci, 1, 0, 0, 0,
728                                 branch >> 1, -1, -1,
729                                 "Misc error", msg);
730         }
733 /*
734  *      i5000_process_error_info        Process the error info that is
735  *      in the 'info' structure, previously retrieved from hardware
736  */
737 static void i5000_process_error_info(struct mem_ctl_info *mci,
738                                 struct i5000_error_info *info,
739                                 int handle_errors)
741         /* First handle any fatal errors that occurred */
742         i5000_process_fatal_error_info(mci, info, handle_errors);
744         /* now handle any non-fatal errors that occurred */
745         i5000_process_nonfatal_error_info(mci, info, handle_errors);
748 /*
749  *      i5000_clear_error       Retrieve any error from the hardware
750  *                              but do NOT process that error.
751  *                              Used for 'clearing' out of previous errors
752  *                              Called by the Core module.
753  */
754 static void i5000_clear_error(struct mem_ctl_info *mci)
756         struct i5000_error_info info;
758         i5000_get_error_info(mci, &info);
761 /*
762  *      i5000_check_error       Retrieve and process errors reported by the
763  *                              hardware. Called by the Core module.
764  */
765 static void i5000_check_error(struct mem_ctl_info *mci)
767         struct i5000_error_info info;
768         edac_dbg(4, "MC%d\n", mci->mc_idx);
769         i5000_get_error_info(mci, &info);
770         i5000_process_error_info(mci, &info, 1);
773 /*
774  *      i5000_get_devices       Find and perform 'get' operation on the MCH's
775  *                      device/functions we want to reference for this driver
776  *
777  *                      Need to 'get' device 16 func 1 and func 2
778  */
779 static int i5000_get_devices(struct mem_ctl_info *mci, int dev_idx)
781         //const struct i5000_dev_info *i5000_dev = &i5000_devs[dev_idx];
782         struct i5000_pvt *pvt;
783         struct pci_dev *pdev;
785         pvt = mci->pvt_info;
787         /* Attempt to 'get' the MCH register we want */
788         pdev = NULL;
789         while (1) {
790                 pdev = pci_get_device(PCI_VENDOR_ID_INTEL,
791                                 PCI_DEVICE_ID_INTEL_I5000_DEV16, pdev);
793                 /* End of list, leave */
794                 if (pdev == NULL) {
795                         i5000_printk(KERN_ERR,
796                                 "'system address,Process Bus' "
797                                 "device not found:"
798                                 "vendor 0x%x device 0x%x FUNC 1 "
799                                 "(broken BIOS?)\n",
800                                 PCI_VENDOR_ID_INTEL,
801                                 PCI_DEVICE_ID_INTEL_I5000_DEV16);
803                         return 1;
804                 }
806                 /* Scan for device 16 func 1 */
807                 if (PCI_FUNC(pdev->devfn) == 1)
808                         break;
809         }
811         pvt->branchmap_werrors = pdev;
813         /* Attempt to 'get' the MCH register we want */
814         pdev = NULL;
815         while (1) {
816                 pdev = pci_get_device(PCI_VENDOR_ID_INTEL,
817                                 PCI_DEVICE_ID_INTEL_I5000_DEV16, pdev);
819                 if (pdev == NULL) {
820                         i5000_printk(KERN_ERR,
821                                 "MC: 'branchmap,control,errors' "
822                                 "device not found:"
823                                 "vendor 0x%x device 0x%x Func 2 "
824                                 "(broken BIOS?)\n",
825                                 PCI_VENDOR_ID_INTEL,
826                                 PCI_DEVICE_ID_INTEL_I5000_DEV16);
828                         pci_dev_put(pvt->branchmap_werrors);
829                         return 1;
830                 }
832                 /* Scan for device 16 func 1 */
833                 if (PCI_FUNC(pdev->devfn) == 2)
834                         break;
835         }
837         pvt->fsb_error_regs = pdev;
839         edac_dbg(1, "System Address, processor bus- PCI Bus ID: %s  %x:%x\n",
840                  pci_name(pvt->system_address),
841                  pvt->system_address->vendor, pvt->system_address->device);
842         edac_dbg(1, "Branchmap, control and errors - PCI Bus ID: %s  %x:%x\n",
843                  pci_name(pvt->branchmap_werrors),
844                  pvt->branchmap_werrors->vendor,
845                  pvt->branchmap_werrors->device);
846         edac_dbg(1, "FSB Error Regs - PCI Bus ID: %s  %x:%x\n",
847                  pci_name(pvt->fsb_error_regs),
848                  pvt->fsb_error_regs->vendor, pvt->fsb_error_regs->device);
850         pdev = NULL;
851         pdev = pci_get_device(PCI_VENDOR_ID_INTEL,
852                         PCI_DEVICE_ID_I5000_BRANCH_0, pdev);
854         if (pdev == NULL) {
855                 i5000_printk(KERN_ERR,
856                         "MC: 'BRANCH 0' device not found:"
857                         "vendor 0x%x device 0x%x Func 0 (broken BIOS?)\n",
858                         PCI_VENDOR_ID_INTEL, PCI_DEVICE_ID_I5000_BRANCH_0);
860                 pci_dev_put(pvt->branchmap_werrors);
861                 pci_dev_put(pvt->fsb_error_regs);
862                 return 1;
863         }
865         pvt->branch_0 = pdev;
867         /* If this device claims to have more than 2 channels then
868          * fetch Branch 1's information
869          */
870         if (pvt->maxch >= CHANNELS_PER_BRANCH) {
871                 pdev = NULL;
872                 pdev = pci_get_device(PCI_VENDOR_ID_INTEL,
873                                 PCI_DEVICE_ID_I5000_BRANCH_1, pdev);
875                 if (pdev == NULL) {
876                         i5000_printk(KERN_ERR,
877                                 "MC: 'BRANCH 1' device not found:"
878                                 "vendor 0x%x device 0x%x Func 0 "
879                                 "(broken BIOS?)\n",
880                                 PCI_VENDOR_ID_INTEL,
881                                 PCI_DEVICE_ID_I5000_BRANCH_1);
883                         pci_dev_put(pvt->branchmap_werrors);
884                         pci_dev_put(pvt->fsb_error_regs);
885                         pci_dev_put(pvt->branch_0);
886                         return 1;
887                 }
889                 pvt->branch_1 = pdev;
890         }
892         return 0;
895 /*
896  *      i5000_put_devices       'put' all the devices that we have
897  *                              reserved via 'get'
898  */
899 static void i5000_put_devices(struct mem_ctl_info *mci)
901         struct i5000_pvt *pvt;
903         pvt = mci->pvt_info;
905         pci_dev_put(pvt->branchmap_werrors);    /* FUNC 1 */
906         pci_dev_put(pvt->fsb_error_regs);       /* FUNC 2 */
907         pci_dev_put(pvt->branch_0);     /* DEV 21 */
909         /* Only if more than 2 channels do we release the second branch */
910         if (pvt->maxch >= CHANNELS_PER_BRANCH)
911                 pci_dev_put(pvt->branch_1);     /* DEV 22 */
914 /*
915  *      determine_amb_resent
916  *
917  *              the information is contained in NUM_MTRS different registers
918  *              determineing which of the NUM_MTRS requires knowing
919  *              which channel is in question
920  *
921  *      2 branches, each with 2 channels
922  *              b0_ambpresent0 for channel '0'
923  *              b0_ambpresent1 for channel '1'
924  *              b1_ambpresent0 for channel '2'
925  *              b1_ambpresent1 for channel '3'
926  */
927 static int determine_amb_present_reg(struct i5000_pvt *pvt, int channel)
929         int amb_present;
931         if (channel < CHANNELS_PER_BRANCH) {
932                 if (channel & 0x1)
933                         amb_present = pvt->b0_ambpresent1;
934                 else
935                         amb_present = pvt->b0_ambpresent0;
936         } else {
937                 if (channel & 0x1)
938                         amb_present = pvt->b1_ambpresent1;
939                 else
940                         amb_present = pvt->b1_ambpresent0;
941         }
943         return amb_present;
946 /*
947  * determine_mtr(pvt, csrow, channel)
948  *
949  *      return the proper MTR register as determine by the csrow and channel desired
950  */
951 static int determine_mtr(struct i5000_pvt *pvt, int slot, int channel)
953         int mtr;
955         if (channel < CHANNELS_PER_BRANCH)
956                 mtr = pvt->b0_mtr[slot];
957         else
958                 mtr = pvt->b1_mtr[slot];
960         return mtr;
963 /*
964  */
965 static void decode_mtr(int slot_row, u16 mtr)
967         int ans;
969         ans = MTR_DIMMS_PRESENT(mtr);
971         edac_dbg(2, "\tMTR%d=0x%x:  DIMMs are %sPresent\n",
972                  slot_row, mtr, ans ? "" : "NOT ");
973         if (!ans)
974                 return;
976         edac_dbg(2, "\t\tWIDTH: x%d\n", MTR_DRAM_WIDTH(mtr));
977         edac_dbg(2, "\t\tNUMBANK: %d bank(s)\n", MTR_DRAM_BANKS(mtr));
978         edac_dbg(2, "\t\tNUMRANK: %s\n",
979                  MTR_DIMM_RANK(mtr) ? "double" : "single");
980         edac_dbg(2, "\t\tNUMROW: %s\n",
981                  MTR_DIMM_ROWS(mtr) == 0 ? "8,192 - 13 rows" :
982                  MTR_DIMM_ROWS(mtr) == 1 ? "16,384 - 14 rows" :
983                  MTR_DIMM_ROWS(mtr) == 2 ? "32,768 - 15 rows" :
984                  "reserved");
985         edac_dbg(2, "\t\tNUMCOL: %s\n",
986                  MTR_DIMM_COLS(mtr) == 0 ? "1,024 - 10 columns" :
987                  MTR_DIMM_COLS(mtr) == 1 ? "2,048 - 11 columns" :
988                  MTR_DIMM_COLS(mtr) == 2 ? "4,096 - 12 columns" :
989                  "reserved");
992 static void handle_channel(struct i5000_pvt *pvt, int slot, int channel,
993                         struct i5000_dimm_info *dinfo)
995         int mtr;
996         int amb_present_reg;
997         int addrBits;
999         mtr = determine_mtr(pvt, slot, channel);
1000         if (MTR_DIMMS_PRESENT(mtr)) {
1001                 amb_present_reg = determine_amb_present_reg(pvt, channel);
1003                 /* Determine if there is a DIMM present in this DIMM slot */
1004                 if (amb_present_reg) {
1005                         dinfo->dual_rank = MTR_DIMM_RANK(mtr);
1007                         /* Start with the number of bits for a Bank
1008                                 * on the DRAM */
1009                         addrBits = MTR_DRAM_BANKS_ADDR_BITS(mtr);
1010                         /* Add the number of ROW bits */
1011                         addrBits += MTR_DIMM_ROWS_ADDR_BITS(mtr);
1012                         /* add the number of COLUMN bits */
1013                         addrBits += MTR_DIMM_COLS_ADDR_BITS(mtr);
1015                         /* Dual-rank memories have twice the size */
1016                         if (dinfo->dual_rank)
1017                                 addrBits++;
1019                         addrBits += 6;  /* add 64 bits per DIMM */
1020                         addrBits -= 20; /* divide by 2^^20 */
1021                         addrBits -= 3;  /* 8 bits per bytes */
1023                         dinfo->megabytes = 1 << addrBits;
1024                 }
1025         }
1028 /*
1029  *      calculate_dimm_size
1030  *
1031  *      also will output a DIMM matrix map, if debug is enabled, for viewing
1032  *      how the DIMMs are populated
1033  */
1034 static void calculate_dimm_size(struct i5000_pvt *pvt)
1036         struct i5000_dimm_info *dinfo;
1037         int slot, channel, branch;
1038         char *p, *mem_buffer;
1039         int space, n;
1041         /* ================= Generate some debug output ================= */
1042         space = PAGE_SIZE;
1043         mem_buffer = p = kmalloc(space, GFP_KERNEL);
1044         if (p == NULL) {
1045                 i5000_printk(KERN_ERR, "MC: %s:%s() kmalloc() failed\n",
1046                         __FILE__, __func__);
1047                 return;
1048         }
1050         /* Scan all the actual slots
1051          * and calculate the information for each DIMM
1052          * Start with the highest slot first, to display it first
1053          * and work toward the 0th slot
1054          */
1055         for (slot = pvt->maxdimmperch - 1; slot >= 0; slot--) {
1057                 /* on an odd slot, first output a 'boundary' marker,
1058                  * then reset the message buffer  */
1059                 if (slot & 0x1) {
1060                         n = snprintf(p, space, "--------------------------"
1061                                 "--------------------------------");
1062                         p += n;
1063                         space -= n;
1064                         edac_dbg(2, "%s\n", mem_buffer);
1065                         p = mem_buffer;
1066                         space = PAGE_SIZE;
1067                 }
1068                 n = snprintf(p, space, "slot %2d    ", slot);
1069                 p += n;
1070                 space -= n;
1072                 for (channel = 0; channel < pvt->maxch; channel++) {
1073                         dinfo = &pvt->dimm_info[slot][channel];
1074                         handle_channel(pvt, slot, channel, dinfo);
1075                         if (dinfo->megabytes)
1076                                 n = snprintf(p, space, "%4d MB %dR| ",
1077                                              dinfo->megabytes, dinfo->dual_rank + 1);
1078                         else
1079                                 n = snprintf(p, space, "%4d MB   | ", 0);
1080                         p += n;
1081                         space -= n;
1082                 }
1083                 p += n;
1084                 space -= n;
1085                 edac_dbg(2, "%s\n", mem_buffer);
1086                 p = mem_buffer;
1087                 space = PAGE_SIZE;
1088         }
1090         /* Output the last bottom 'boundary' marker */
1091         n = snprintf(p, space, "--------------------------"
1092                 "--------------------------------");
1093         p += n;
1094         space -= n;
1095         edac_dbg(2, "%s\n", mem_buffer);
1096         p = mem_buffer;
1097         space = PAGE_SIZE;
1099         /* now output the 'channel' labels */
1100         n = snprintf(p, space, "           ");
1101         p += n;
1102         space -= n;
1103         for (channel = 0; channel < pvt->maxch; channel++) {
1104                 n = snprintf(p, space, "channel %d | ", channel);
1105                 p += n;
1106                 space -= n;
1107         }
1108         edac_dbg(2, "%s\n", mem_buffer);
1109         p = mem_buffer;
1110         space = PAGE_SIZE;
1112         n = snprintf(p, space, "           ");
1113         p += n;
1114         for (branch = 0; branch < MAX_BRANCHES; branch++) {
1115                 n = snprintf(p, space, "       branch %d       | ", branch);
1116                 p += n;
1117                 space -= n;
1118         }
1120         /* output the last message and free buffer */
1121         edac_dbg(2, "%s\n", mem_buffer);
1122         kfree(mem_buffer);
1125 /*
1126  *      i5000_get_mc_regs       read in the necessary registers and
1127  *                              cache locally
1128  *
1129  *                      Fills in the private data members
1130  */
1131 static void i5000_get_mc_regs(struct mem_ctl_info *mci)
1133         struct i5000_pvt *pvt;
1134         u32 actual_tolm;
1135         u16 limit;
1136         int slot_row;
1137         int maxch;
1138         int maxdimmperch;
1139         int way0, way1;
1141         pvt = mci->pvt_info;
1143         pci_read_config_dword(pvt->system_address, AMBASE,
1144                         &pvt->u.ambase_bottom);
1145         pci_read_config_dword(pvt->system_address, AMBASE + sizeof(u32),
1146                         &pvt->u.ambase_top);
1148         maxdimmperch = pvt->maxdimmperch;
1149         maxch = pvt->maxch;
1151         edac_dbg(2, "AMBASE= 0x%lx  MAXCH= %d  MAX-DIMM-Per-CH= %d\n",
1152                  (long unsigned int)pvt->ambase, pvt->maxch, pvt->maxdimmperch);
1154         /* Get the Branch Map regs */
1155         pci_read_config_word(pvt->branchmap_werrors, TOLM, &pvt->tolm);
1156         pvt->tolm >>= 12;
1157         edac_dbg(2, "TOLM (number of 256M regions) =%u (0x%x)\n",
1158                  pvt->tolm, pvt->tolm);
1160         actual_tolm = pvt->tolm << 28;
1161         edac_dbg(2, "Actual TOLM byte addr=%u (0x%x)\n",
1162                  actual_tolm, actual_tolm);
1164         pci_read_config_word(pvt->branchmap_werrors, MIR0, &pvt->mir0);
1165         pci_read_config_word(pvt->branchmap_werrors, MIR1, &pvt->mir1);
1166         pci_read_config_word(pvt->branchmap_werrors, MIR2, &pvt->mir2);
1168         /* Get the MIR[0-2] regs */
1169         limit = (pvt->mir0 >> 4) & 0x0FFF;
1170         way0 = pvt->mir0 & 0x1;
1171         way1 = pvt->mir0 & 0x2;
1172         edac_dbg(2, "MIR0: limit= 0x%x  WAY1= %u  WAY0= %x\n",
1173                  limit, way1, way0);
1174         limit = (pvt->mir1 >> 4) & 0x0FFF;
1175         way0 = pvt->mir1 & 0x1;
1176         way1 = pvt->mir1 & 0x2;
1177         edac_dbg(2, "MIR1: limit= 0x%x  WAY1= %u  WAY0= %x\n",
1178                  limit, way1, way0);
1179         limit = (pvt->mir2 >> 4) & 0x0FFF;
1180         way0 = pvt->mir2 & 0x1;
1181         way1 = pvt->mir2 & 0x2;
1182         edac_dbg(2, "MIR2: limit= 0x%x  WAY1= %u  WAY0= %x\n",
1183                  limit, way1, way0);
1185         /* Get the MTR[0-3] regs */
1186         for (slot_row = 0; slot_row < NUM_MTRS; slot_row++) {
1187                 int where = MTR0 + (slot_row * sizeof(u32));
1189                 pci_read_config_word(pvt->branch_0, where,
1190                                 &pvt->b0_mtr[slot_row]);
1192                 edac_dbg(2, "MTR%d where=0x%x B0 value=0x%x\n",
1193                          slot_row, where, pvt->b0_mtr[slot_row]);
1195                 if (pvt->maxch >= CHANNELS_PER_BRANCH) {
1196                         pci_read_config_word(pvt->branch_1, where,
1197                                         &pvt->b1_mtr[slot_row]);
1198                         edac_dbg(2, "MTR%d where=0x%x B1 value=0x%x\n",
1199                                  slot_row, where, pvt->b1_mtr[slot_row]);
1200                 } else {
1201                         pvt->b1_mtr[slot_row] = 0;
1202                 }
1203         }
1205         /* Read and dump branch 0's MTRs */
1206         edac_dbg(2, "Memory Technology Registers:\n");
1207         edac_dbg(2, "   Branch 0:\n");
1208         for (slot_row = 0; slot_row < NUM_MTRS; slot_row++) {
1209                 decode_mtr(slot_row, pvt->b0_mtr[slot_row]);
1210         }
1211         pci_read_config_word(pvt->branch_0, AMB_PRESENT_0,
1212                         &pvt->b0_ambpresent0);
1213         edac_dbg(2, "\t\tAMB-Branch 0-present0 0x%x:\n", pvt->b0_ambpresent0);
1214         pci_read_config_word(pvt->branch_0, AMB_PRESENT_1,
1215                         &pvt->b0_ambpresent1);
1216         edac_dbg(2, "\t\tAMB-Branch 0-present1 0x%x:\n", pvt->b0_ambpresent1);
1218         /* Only if we have 2 branchs (4 channels) */
1219         if (pvt->maxch < CHANNELS_PER_BRANCH) {
1220                 pvt->b1_ambpresent0 = 0;
1221                 pvt->b1_ambpresent1 = 0;
1222         } else {
1223                 /* Read and dump  branch 1's MTRs */
1224                 edac_dbg(2, "   Branch 1:\n");
1225                 for (slot_row = 0; slot_row < NUM_MTRS; slot_row++) {
1226                         decode_mtr(slot_row, pvt->b1_mtr[slot_row]);
1227                 }
1228                 pci_read_config_word(pvt->branch_1, AMB_PRESENT_0,
1229                                 &pvt->b1_ambpresent0);
1230                 edac_dbg(2, "\t\tAMB-Branch 1-present0 0x%x:\n",
1231                          pvt->b1_ambpresent0);
1232                 pci_read_config_word(pvt->branch_1, AMB_PRESENT_1,
1233                                 &pvt->b1_ambpresent1);
1234                 edac_dbg(2, "\t\tAMB-Branch 1-present1 0x%x:\n",
1235                          pvt->b1_ambpresent1);
1236         }
1238         /* Go and determine the size of each DIMM and place in an
1239          * orderly matrix */
1240         calculate_dimm_size(pvt);
1243 /*
1244  *      i5000_init_csrows       Initialize the 'csrows' table within
1245  *                              the mci control structure with the
1246  *                              addressing of memory.
1247  *
1248  *      return:
1249  *              0       success
1250  *              1       no actual memory found on this MC
1251  */
1252 static int i5000_init_csrows(struct mem_ctl_info *mci)
1254         struct i5000_pvt *pvt;
1255         struct dimm_info *dimm;
1256         int empty, channel_count;
1257         int max_csrows;
1258         int mtr;
1259         int csrow_megs;
1260         int channel;
1261         int slot;
1263         pvt = mci->pvt_info;
1265         channel_count = pvt->maxch;
1266         max_csrows = pvt->maxdimmperch * 2;
1268         empty = 1;              /* Assume NO memory */
1270         /*
1271          * FIXME: The memory layout used to map slot/channel into the
1272          * real memory architecture is weird: branch+slot are "csrows"
1273          * and channel is channel. That required an extra array (dimm_info)
1274          * to map the dimms. A good cleanup would be to remove this array,
1275          * and do a loop here with branch, channel, slot
1276          */
1277         for (slot = 0; slot < max_csrows; slot++) {
1278                 for (channel = 0; channel < pvt->maxch; channel++) {
1280                         mtr = determine_mtr(pvt, slot, channel);
1282                         if (!MTR_DIMMS_PRESENT(mtr))
1283                                 continue;
1285                         dimm = EDAC_DIMM_PTR(mci->layers, mci->dimms, mci->n_layers,
1286                                        channel / MAX_BRANCHES,
1287                                        channel % MAX_BRANCHES, slot);
1289                         csrow_megs = pvt->dimm_info[slot][channel].megabytes;
1290                         dimm->grain = 8;
1292                         /* Assume DDR2 for now */
1293                         dimm->mtype = MEM_FB_DDR2;
1295                         /* ask what device type on this row */
1296                         if (MTR_DRAM_WIDTH(mtr))
1297                                 dimm->dtype = DEV_X8;
1298                         else
1299                                 dimm->dtype = DEV_X4;
1301                         dimm->edac_mode = EDAC_S8ECD8ED;
1302                         dimm->nr_pages = csrow_megs << 8;
1303                 }
1305                 empty = 0;
1306         }
1308         return empty;
1311 /*
1312  *      i5000_enable_error_reporting
1313  *                      Turn on the memory reporting features of the hardware
1314  */
1315 static void i5000_enable_error_reporting(struct mem_ctl_info *mci)
1317         struct i5000_pvt *pvt;
1318         u32 fbd_error_mask;
1320         pvt = mci->pvt_info;
1322         /* Read the FBD Error Mask Register */
1323         pci_read_config_dword(pvt->branchmap_werrors, EMASK_FBD,
1324                         &fbd_error_mask);
1326         /* Enable with a '0' */
1327         fbd_error_mask &= ~(ENABLE_EMASK_ALL);
1329         pci_write_config_dword(pvt->branchmap_werrors, EMASK_FBD,
1330                         fbd_error_mask);
1333 /*
1334  * i5000_get_dimm_and_channel_counts(pdev, &nr_csrows, &num_channels)
1335  *
1336  *      ask the device how many channels are present and how many CSROWS
1337  *       as well
1338  */
1339 static void i5000_get_dimm_and_channel_counts(struct pci_dev *pdev,
1340                                         int *num_dimms_per_channel,
1341                                         int *num_channels)
1343         u8 value;
1345         /* Need to retrieve just how many channels and dimms per channel are
1346          * supported on this memory controller
1347          */
1348         pci_read_config_byte(pdev, MAXDIMMPERCH, &value);
1349         *num_dimms_per_channel = (int)value;
1351         pci_read_config_byte(pdev, MAXCH, &value);
1352         *num_channels = (int)value;
1355 /*
1356  *      i5000_probe1    Probe for ONE instance of device to see if it is
1357  *                      present.
1358  *      return:
1359  *              0 for FOUND a device
1360  *              < 0 for error code
1361  */
1362 static int i5000_probe1(struct pci_dev *pdev, int dev_idx)
1364         struct mem_ctl_info *mci;
1365         struct edac_mc_layer layers[3];
1366         struct i5000_pvt *pvt;
1367         int num_channels;
1368         int num_dimms_per_channel;
1370         edac_dbg(0, "MC: pdev bus %u dev=0x%x fn=0x%x\n",
1371                  pdev->bus->number,
1372                  PCI_SLOT(pdev->devfn), PCI_FUNC(pdev->devfn));
1374         /* We only are looking for func 0 of the set */
1375         if (PCI_FUNC(pdev->devfn) != 0)
1376                 return -ENODEV;
1378         /* Ask the devices for the number of CSROWS and CHANNELS so
1379          * that we can calculate the memory resources, etc
1380          *
1381          * The Chipset will report what it can handle which will be greater
1382          * or equal to what the motherboard manufacturer will implement.
1383          *
1384          * As we don't have a motherboard identification routine to determine
1385          * actual number of slots/dimms per channel, we thus utilize the
1386          * resource as specified by the chipset. Thus, we might have
1387          * have more DIMMs per channel than actually on the mobo, but this
1388          * allows the driver to support up to the chipset max, without
1389          * some fancy mobo determination.
1390          */
1391         i5000_get_dimm_and_channel_counts(pdev, &num_dimms_per_channel,
1392                                         &num_channels);
1394         edac_dbg(0, "MC: Number of Branches=2 Channels= %d  DIMMS= %d\n",
1395                  num_channels, num_dimms_per_channel);
1397         /* allocate a new MC control structure */
1399         layers[0].type = EDAC_MC_LAYER_BRANCH;
1400         layers[0].size = MAX_BRANCHES;
1401         layers[0].is_virt_csrow = false;
1402         layers[1].type = EDAC_MC_LAYER_CHANNEL;
1403         layers[1].size = num_channels / MAX_BRANCHES;
1404         layers[1].is_virt_csrow = false;
1405         layers[2].type = EDAC_MC_LAYER_SLOT;
1406         layers[2].size = num_dimms_per_channel;
1407         layers[2].is_virt_csrow = true;
1408         mci = edac_mc_alloc(0, ARRAY_SIZE(layers), layers, sizeof(*pvt));
1409         if (mci == NULL)
1410                 return -ENOMEM;
1412         edac_dbg(0, "MC: mci = %p\n", mci);
1414         mci->pdev = &pdev->dev; /* record ptr  to the generic device */
1416         pvt = mci->pvt_info;
1417         pvt->system_address = pdev;     /* Record this device in our private */
1418         pvt->maxch = num_channels;
1419         pvt->maxdimmperch = num_dimms_per_channel;
1421         /* 'get' the pci devices we want to reserve for our use */
1422         if (i5000_get_devices(mci, dev_idx))
1423                 goto fail0;
1425         /* Time to get serious */
1426         i5000_get_mc_regs(mci); /* retrieve the hardware registers */
1428         mci->mc_idx = 0;
1429         mci->mtype_cap = MEM_FLAG_FB_DDR2;
1430         mci->edac_ctl_cap = EDAC_FLAG_NONE;
1431         mci->edac_cap = EDAC_FLAG_NONE;
1432         mci->mod_name = "i5000_edac.c";
1433         mci->mod_ver = I5000_REVISION;
1434         mci->ctl_name = i5000_devs[dev_idx].ctl_name;
1435         mci->dev_name = pci_name(pdev);
1436         mci->ctl_page_to_phys = NULL;
1438         /* Set the function pointer to an actual operation function */
1439         mci->edac_check = i5000_check_error;
1441         /* initialize the MC control structure 'csrows' table
1442          * with the mapping and control information */
1443         if (i5000_init_csrows(mci)) {
1444                 edac_dbg(0, "MC: Setting mci->edac_cap to EDAC_FLAG_NONE because i5000_init_csrows() returned nonzero value\n");
1445                 mci->edac_cap = EDAC_FLAG_NONE; /* no csrows found */
1446         } else {
1447                 edac_dbg(1, "MC: Enable error reporting now\n");
1448                 i5000_enable_error_reporting(mci);
1449         }
1451         /* add this new MC control structure to EDAC's list of MCs */
1452         if (edac_mc_add_mc(mci)) {
1453                 edac_dbg(0, "MC: failed edac_mc_add_mc()\n");
1454                 /* FIXME: perhaps some code should go here that disables error
1455                  * reporting if we just enabled it
1456                  */
1457                 goto fail1;
1458         }
1460         i5000_clear_error(mci);
1462         /* allocating generic PCI control info */
1463         i5000_pci = edac_pci_create_generic_ctl(&pdev->dev, EDAC_MOD_STR);
1464         if (!i5000_pci) {
1465                 printk(KERN_WARNING
1466                         "%s(): Unable to create PCI control\n",
1467                         __func__);
1468                 printk(KERN_WARNING
1469                         "%s(): PCI error report via EDAC not setup\n",
1470                         __func__);
1471         }
1473         return 0;
1475         /* Error exit unwinding stack */
1476 fail1:
1478         i5000_put_devices(mci);
1480 fail0:
1481         edac_mc_free(mci);
1482         return -ENODEV;
1485 /*
1486  *      i5000_init_one  constructor for one instance of device
1487  *
1488  *      returns:
1489  *              negative on error
1490  *              count (>= 0)
1491  */
1492 static int i5000_init_one(struct pci_dev *pdev, const struct pci_device_id *id)
1494         int rc;
1496         edac_dbg(0, "MC:\n");
1498         /* wake up device */
1499         rc = pci_enable_device(pdev);
1500         if (rc)
1501                 return rc;
1503         /* now probe and enable the device */
1504         return i5000_probe1(pdev, id->driver_data);
1507 /*
1508  *      i5000_remove_one        destructor for one instance of device
1509  *
1510  */
1511 static void i5000_remove_one(struct pci_dev *pdev)
1513         struct mem_ctl_info *mci;
1515         edac_dbg(0, "\n");
1517         if (i5000_pci)
1518                 edac_pci_release_generic_ctl(i5000_pci);
1520         if ((mci = edac_mc_del_mc(&pdev->dev)) == NULL)
1521                 return;
1523         /* retrieve references to resources, and free those resources */
1524         i5000_put_devices(mci);
1525         edac_mc_free(mci);
1528 /*
1529  *      pci_device_id   table for which devices we are looking for
1530  *
1531  *      The "E500P" device is the first device supported.
1532  */
1533 static DEFINE_PCI_DEVICE_TABLE(i5000_pci_tbl) = {
1534         {PCI_DEVICE(PCI_VENDOR_ID_INTEL, PCI_DEVICE_ID_INTEL_I5000_DEV16),
1535          .driver_data = I5000P},
1537         {0,}                    /* 0 terminated list. */
1538 };
1540 MODULE_DEVICE_TABLE(pci, i5000_pci_tbl);
1542 /*
1543  *      i5000_driver    pci_driver structure for this module
1544  *
1545  */
1546 static struct pci_driver i5000_driver = {
1547         .name = KBUILD_BASENAME,
1548         .probe = i5000_init_one,
1549         .remove = i5000_remove_one,
1550         .id_table = i5000_pci_tbl,
1551 };
1553 /*
1554  *      i5000_init              Module entry function
1555  *                      Try to initialize this module for its devices
1556  */
1557 static int __init i5000_init(void)
1559         int pci_rc;
1561         edac_dbg(2, "MC:\n");
1563        /* Ensure that the OPSTATE is set correctly for POLL or NMI */
1564        opstate_init();
1566         pci_rc = pci_register_driver(&i5000_driver);
1568         return (pci_rc < 0) ? pci_rc : 0;
1571 /*
1572  *      i5000_exit()    Module exit function
1573  *                      Unregister the driver
1574  */
1575 static void __exit i5000_exit(void)
1577         edac_dbg(2, "MC:\n");
1578         pci_unregister_driver(&i5000_driver);
1581 module_init(i5000_init);
1582 module_exit(i5000_exit);
1584 MODULE_LICENSE("GPL");
1585 MODULE_AUTHOR
1586     ("Linux Networx (http://lnxi.com) Doug Thompson <norsk5@xmission.com>");
1587 MODULE_DESCRIPTION("MC Driver for Intel I5000 memory controllers - "
1588                 I5000_REVISION);
1590 module_param(edac_op_state, int, 0444);
1591 MODULE_PARM_DESC(edac_op_state, "EDAC Error Reporting state: 0=Poll,1=NMI");
1592 module_param(misc_messages, int, 0444);
1593 MODULE_PARM_DESC(misc_messages, "Log miscellaneous non fatal messages");