1 #
2 # Drm device configuration
3 #
4 # This driver provides support for the
5 # Direct Rendering Infrastructure (DRI) in XFree86 4.1.0 and higher.
6 #
7 menuconfig DRM
8 tristate "Direct Rendering Manager (XFree86 4.1.0 and higher DRI support)"
9 depends on (AGP || AGP=n) && !EMULATED_CMPXCHG && MMU
10 select I2C
11 select I2C_ALGOBIT
12 select DMA_SHARED_BUFFER
13 help
14 Kernel-level support for the Direct Rendering Infrastructure (DRI)
15 introduced in XFree86 4.0. If you say Y here, you need to select
16 the module that's right for your graphics card from the list below.
17 These modules provide support for synchronization, security, and
18 DMA transfers. Please see <http://dri.sourceforge.net/> for more
19 details. You should also select and configure AGP
20 (/dev/agpgart) support if it is available for your platform.
22 config DRM_USB
23 tristate
24 depends on DRM
25 depends on USB_SUPPORT && USB_ARCH_HAS_HCD
26 select USB
28 config DRM_KMS_HELPER
29 tristate
30 depends on DRM
31 select FB
32 select FRAMEBUFFER_CONSOLE if !EXPERT
33 select FRAMEBUFFER_CONSOLE_DETECT_PRIMARY if FRAMEBUFFER_CONSOLE
34 help
35 FB and CRTC helpers for KMS drivers.
37 config DRM_LOAD_EDID_FIRMWARE
38 bool "Allow to specify an EDID data set instead of probing for it"
39 depends on DRM_KMS_HELPER
40 help
41 Say Y here, if you want to use EDID data to be loaded from the
42 /lib/firmware directory or one of the provided built-in
43 data sets. This may be necessary, if the graphics adapter or
44 monitor are unable to provide appropriate EDID data. Since this
45 feature is provided as a workaround for broken hardware, the
46 default case is N. Details and instructions how to build your own
47 EDID data are given in Documentation/EDID/HOWTO.txt.
49 config DRM_TTM
50 tristate
51 depends on DRM
52 help
53 GPU memory management subsystem for devices with multiple
54 GPU memory types. Will be enabled automatically if a device driver
55 uses it.
57 config DRM_GEM_CMA_HELPER
58 bool
59 depends on DRM
60 help
61 Choose this if you need the GEM CMA helper functions
63 config DRM_KMS_CMA_HELPER
64 bool
65 select DRM_GEM_CMA_HELPER
66 select FB_SYS_FILLRECT
67 select FB_SYS_COPYAREA
68 select FB_SYS_IMAGEBLIT
69 help
70 Choose this if you need the KMS CMA helper functions
72 config DRM_TDFX
73 tristate "3dfx Banshee/Voodoo3+"
74 depends on DRM && PCI
75 help
76 Choose this option if you have a 3dfx Banshee or Voodoo3 (or later),
77 graphics card. If M is selected, the module will be called tdfx.
79 config DRM_R128
80 tristate "ATI Rage 128"
81 depends on DRM && PCI
82 select FW_LOADER
83 help
84 Choose this option if you have an ATI Rage 128 graphics card. If M
85 is selected, the module will be called r128. AGP support for
86 this card is strongly suggested (unless you have a PCI version).
88 config DRM_RADEON
89 tristate "ATI Radeon"
90 depends on DRM && PCI
91 select FB_CFB_FILLRECT
92 select FB_CFB_COPYAREA
93 select FB_CFB_IMAGEBLIT
94 select FW_LOADER
95 select DRM_KMS_HELPER
96 select DRM_TTM
97 select POWER_SUPPLY
98 select HWMON
99 help
100 Choose this option if you have an ATI Radeon graphics card. There
101 are both PCI and AGP versions. You don't need to choose this to
102 run the Radeon in plain VGA mode.
104 If M is selected, the module will be called radeon.
106 source "drivers/gpu/drm/radeon/Kconfig"
108 source "drivers/gpu/drm/nouveau/Kconfig"
110 config DRM_I810
111 tristate "Intel I810"
112 # !PREEMPT because of missing ioctl locking
113 depends on DRM && AGP && AGP_INTEL && (!PREEMPT || BROKEN)
114 help
115 Choose this option if you have an Intel I810 graphics card. If M is
116 selected, the module will be called i810. AGP support is required
117 for this driver to work.
119 config DRM_I915
120 tristate "Intel 8xx/9xx/G3x/G4x/HD Graphics"
121 depends on DRM
122 depends on AGP
123 depends on AGP_INTEL
124 # we need shmfs for the swappable backing store, and in particular
125 # the shmem_readpage() which depends upon tmpfs
126 select SHMEM
127 select TMPFS
128 select DRM_KMS_HELPER
129 select FB_CFB_FILLRECT
130 select FB_CFB_COPYAREA
131 select FB_CFB_IMAGEBLIT
132 # i915 depends on ACPI_VIDEO when ACPI is enabled
133 # but for select to work, need to select ACPI_VIDEO's dependencies, ick
134 select BACKLIGHT_LCD_SUPPORT if ACPI
135 select BACKLIGHT_CLASS_DEVICE if ACPI
136 select VIDEO_OUTPUT_CONTROL if ACPI
137 select INPUT if ACPI
138 select ACPI_VIDEO if ACPI
139 select ACPI_BUTTON if ACPI
140 help
141 Choose this option if you have a system that has "Intel Graphics
142 Media Accelerator" or "HD Graphics" integrated graphics,
143 including 830M, 845G, 852GM, 855GM, 865G, 915G, 945G, 965G,
144 G35, G41, G43, G45 chipsets and Celeron, Pentium, Core i3,
145 Core i5, Core i7 as well as Atom CPUs with integrated graphics.
146 If M is selected, the module will be called i915. AGP support
147 is required for this driver to work. This driver is used by
148 the Intel driver in X.org 6.8 and XFree86 4.4 and above. It
149 replaces the older i830 module that supported a subset of the
150 hardware in older X.org releases.
152 Note that the older i810/i815 chipsets require the use of the
153 i810 driver instead, and the Atom z5xx series has an entirely
154 different implementation.
156 config DRM_I915_KMS
157 bool "Enable modesetting on intel by default"
158 depends on DRM_I915
159 help
160 Choose this option if you want kernel modesetting enabled by default,
161 and you have a new enough userspace to support this. Running old
162 userspaces with this enabled will cause pain. Note that this causes
163 the driver to bind to PCI devices, which precludes loading things
164 like intelfb.
166 config DRM_MGA
167 tristate "Matrox g200/g400"
168 depends on DRM && PCI
169 select FW_LOADER
170 help
171 Choose this option if you have a Matrox G200, G400 or G450 graphics
172 card. If M is selected, the module will be called mga. AGP
173 support is required for this driver to work.
175 config DRM_SIS
176 tristate "SiS video cards"
177 depends on DRM && AGP
178 depends on FB_SIS || FB_SIS=n
179 help
180 Choose this option if you have a SiS 630 or compatible video
181 chipset. If M is selected the module will be called sis. AGP
182 support is required for this driver to work.
184 config DRM_VIA
185 tristate "Via unichrome video cards"
186 depends on DRM && PCI
187 help
188 Choose this option if you have a Via unichrome or compatible video
189 chipset. If M is selected the module will be called via.
191 config DRM_SAVAGE
192 tristate "Savage video cards"
193 depends on DRM && PCI
194 help
195 Choose this option if you have a Savage3D/4/SuperSavage/Pro/Twister
196 chipset. If M is selected the module will be called savage.
198 source "drivers/gpu/drm/exynos/Kconfig"
200 source "drivers/gpu/drm/vmwgfx/Kconfig"
202 source "drivers/gpu/drm/gma500/Kconfig"
204 source "drivers/gpu/drm/udl/Kconfig"
206 source "drivers/gpu/drm/ast/Kconfig"
208 source "drivers/gpu/drm/mgag200/Kconfig"
210 source "drivers/gpu/drm/cirrus/Kconfig"
212 source "drivers/gpu/drm/shmobile/Kconfig"
214 source "drivers/gpu/drm/tegra/Kconfig"
216 source "drivers/gpu/drm/omapdrm/Kconfig"