1 /*
2 * drivers/gpu/drm/omapdrm/omap_crtc.c
3 *
4 * Copyright (C) 2011 Texas Instruments
5 * Author: Rob Clark <rob@ti.com>
6 *
7 * This program is free software; you can redistribute it and/or modify it
8 * under the terms of the GNU General Public License version 2 as published by
9 * the Free Software Foundation.
10 *
11 * This program is distributed in the hope that it will be useful, but WITHOUT
12 * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
13 * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for
14 * more details.
15 *
16 * You should have received a copy of the GNU General Public License along with
17 * this program. If not, see <http://www.gnu.org/licenses/>.
18 */
20 #include "omap_drv.h"
22 #include <drm/drm_mode.h>
23 #include "drm_crtc.h"
24 #include "drm_crtc_helper.h"
26 #define to_omap_crtc(x) container_of(x, struct omap_crtc, base)
28 struct omap_crtc {
29 struct drm_crtc base;
30 struct drm_plane *plane;
32 const char *name;
33 int pipe;
34 enum omap_channel channel;
35 struct omap_overlay_manager_info info;
37 /*
38 * Temporary: eventually this will go away, but it is needed
39 * for now to keep the output's happy. (They only need
40 * mgr->id.) Eventually this will be replaced w/ something
41 * more common-panel-framework-y
42 */
43 struct omap_overlay_manager mgr;
45 struct omap_video_timings timings;
46 bool enabled;
47 bool full_update;
49 struct omap_drm_apply apply;
51 struct omap_drm_irq apply_irq;
52 struct omap_drm_irq error_irq;
54 /* list of in-progress apply's: */
55 struct list_head pending_applies;
57 /* list of queued apply's: */
58 struct list_head queued_applies;
60 /* for handling queued and in-progress applies: */
61 struct work_struct apply_work;
63 /* if there is a pending flip, these will be non-null: */
64 struct drm_pending_vblank_event *event;
65 struct drm_framebuffer *old_fb;
67 /* for handling page flips without caring about what
68 * the callback is called from. Possibly we should just
69 * make omap_gem always call the cb from the worker so
70 * we don't have to care about this..
71 *
72 * XXX maybe fold into apply_work??
73 */
74 struct work_struct page_flip_work;
75 };
77 /*
78 * Manager-ops, callbacks from output when they need to configure
79 * the upstream part of the video pipe.
80 *
81 * Most of these we can ignore until we add support for command-mode
82 * panels.. for video-mode the crtc-helpers already do an adequate
83 * job of sequencing the setup of the video pipe in the proper order
84 */
86 /* we can probably ignore these until we support command-mode panels: */
87 static void omap_crtc_start_update(struct omap_overlay_manager *mgr)
88 {
89 }
91 static int omap_crtc_enable(struct omap_overlay_manager *mgr)
92 {
93 return 0;
94 }
96 static void omap_crtc_disable(struct omap_overlay_manager *mgr)
97 {
98 }
100 static void omap_crtc_set_timings(struct omap_overlay_manager *mgr,
101 const struct omap_video_timings *timings)
102 {
103 struct omap_crtc *omap_crtc = container_of(mgr, struct omap_crtc, mgr);
104 DBG("%s", omap_crtc->name);
105 omap_crtc->timings = *timings;
106 omap_crtc->full_update = true;
107 }
109 static void omap_crtc_set_lcd_config(struct omap_overlay_manager *mgr,
110 const struct dss_lcd_mgr_config *config)
111 {
112 struct omap_crtc *omap_crtc = container_of(mgr, struct omap_crtc, mgr);
113 DBG("%s", omap_crtc->name);
114 dispc_mgr_set_lcd_config(omap_crtc->channel, config);
115 }
117 static int omap_crtc_register_framedone_handler(
118 struct omap_overlay_manager *mgr,
119 void (*handler)(void *), void *data)
120 {
121 return 0;
122 }
124 static void omap_crtc_unregister_framedone_handler(
125 struct omap_overlay_manager *mgr,
126 void (*handler)(void *), void *data)
127 {
128 }
130 static const struct dss_mgr_ops mgr_ops = {
131 .start_update = omap_crtc_start_update,
132 .enable = omap_crtc_enable,
133 .disable = omap_crtc_disable,
134 .set_timings = omap_crtc_set_timings,
135 .set_lcd_config = omap_crtc_set_lcd_config,
136 .register_framedone_handler = omap_crtc_register_framedone_handler,
137 .unregister_framedone_handler = omap_crtc_unregister_framedone_handler,
138 };
140 /*
141 * CRTC funcs:
142 */
144 static void omap_crtc_destroy(struct drm_crtc *crtc)
145 {
146 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
148 DBG("%s", omap_crtc->name);
150 WARN_ON(omap_crtc->apply_irq.registered);
151 omap_irq_unregister(crtc->dev, &omap_crtc->error_irq);
153 omap_crtc->plane->funcs->destroy(omap_crtc->plane);
154 drm_crtc_cleanup(crtc);
156 kfree(omap_crtc);
157 }
159 static void omap_crtc_dpms(struct drm_crtc *crtc, int mode)
160 {
161 struct omap_drm_private *priv = crtc->dev->dev_private;
162 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
163 bool enabled = (mode == DRM_MODE_DPMS_ON);
164 int i;
166 DBG("%s: %d", omap_crtc->name, mode);
168 if (enabled != omap_crtc->enabled) {
169 omap_crtc->enabled = enabled;
170 omap_crtc->full_update = true;
171 omap_crtc_apply(crtc, &omap_crtc->apply);
173 /* also enable our private plane: */
174 WARN_ON(omap_plane_dpms(omap_crtc->plane, mode));
176 /* and any attached overlay planes: */
177 for (i = 0; i < priv->num_planes; i++) {
178 struct drm_plane *plane = priv->planes[i];
179 if (plane->crtc == crtc)
180 WARN_ON(omap_plane_dpms(plane, mode));
181 }
182 }
183 }
185 static bool omap_crtc_mode_fixup(struct drm_crtc *crtc,
186 const struct drm_display_mode *mode,
187 struct drm_display_mode *adjusted_mode)
188 {
189 return true;
190 }
192 static int omap_crtc_mode_set(struct drm_crtc *crtc,
193 struct drm_display_mode *mode,
194 struct drm_display_mode *adjusted_mode,
195 int x, int y,
196 struct drm_framebuffer *old_fb)
197 {
198 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
200 mode = adjusted_mode;
202 DBG("%s: set mode: %d:\"%s\" %d %d %d %d %d %d %d %d %d %d 0x%x 0x%x",
203 omap_crtc->name, mode->base.id, mode->name,
204 mode->vrefresh, mode->clock,
205 mode->hdisplay, mode->hsync_start,
206 mode->hsync_end, mode->htotal,
207 mode->vdisplay, mode->vsync_start,
208 mode->vsync_end, mode->vtotal,
209 mode->type, mode->flags);
211 copy_timings_drm_to_omap(&omap_crtc->timings, mode);
212 omap_crtc->full_update = true;
214 return omap_plane_mode_set(omap_crtc->plane, crtc, crtc->fb,
215 0, 0, mode->hdisplay, mode->vdisplay,
216 x << 16, y << 16,
217 mode->hdisplay << 16, mode->vdisplay << 16,
218 NULL, NULL);
219 }
221 static void omap_crtc_prepare(struct drm_crtc *crtc)
222 {
223 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
224 DBG("%s", omap_crtc->name);
225 omap_crtc_dpms(crtc, DRM_MODE_DPMS_OFF);
226 }
228 static void omap_crtc_commit(struct drm_crtc *crtc)
229 {
230 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
231 DBG("%s", omap_crtc->name);
232 omap_crtc_dpms(crtc, DRM_MODE_DPMS_ON);
233 }
235 static int omap_crtc_mode_set_base(struct drm_crtc *crtc, int x, int y,
236 struct drm_framebuffer *old_fb)
237 {
238 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
239 struct drm_plane *plane = omap_crtc->plane;
240 struct drm_display_mode *mode = &crtc->mode;
242 return omap_plane_mode_set(plane, crtc, crtc->fb,
243 0, 0, mode->hdisplay, mode->vdisplay,
244 x << 16, y << 16,
245 mode->hdisplay << 16, mode->vdisplay << 16,
246 NULL, NULL);
247 }
249 static void omap_crtc_load_lut(struct drm_crtc *crtc)
250 {
251 }
253 static void vblank_cb(void *arg)
254 {
255 struct drm_crtc *crtc = arg;
256 struct drm_device *dev = crtc->dev;
257 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
258 unsigned long flags;
260 spin_lock_irqsave(&dev->event_lock, flags);
262 /* wakeup userspace */
263 if (omap_crtc->event)
264 drm_send_vblank_event(dev, omap_crtc->pipe, omap_crtc->event);
266 omap_crtc->event = NULL;
267 omap_crtc->old_fb = NULL;
269 spin_unlock_irqrestore(&dev->event_lock, flags);
270 }
272 static void page_flip_worker(struct work_struct *work)
273 {
274 struct omap_crtc *omap_crtc =
275 container_of(work, struct omap_crtc, page_flip_work);
276 struct drm_crtc *crtc = &omap_crtc->base;
277 struct drm_device *dev = crtc->dev;
278 struct drm_display_mode *mode = &crtc->mode;
279 struct drm_gem_object *bo;
281 mutex_lock(&dev->mode_config.mutex);
282 omap_plane_mode_set(omap_crtc->plane, crtc, crtc->fb,
283 0, 0, mode->hdisplay, mode->vdisplay,
284 crtc->x << 16, crtc->y << 16,
285 mode->hdisplay << 16, mode->vdisplay << 16,
286 vblank_cb, crtc);
287 mutex_unlock(&dev->mode_config.mutex);
289 bo = omap_framebuffer_bo(crtc->fb, 0);
290 drm_gem_object_unreference_unlocked(bo);
291 }
293 static void page_flip_cb(void *arg)
294 {
295 struct drm_crtc *crtc = arg;
296 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
297 struct omap_drm_private *priv = crtc->dev->dev_private;
299 /* avoid assumptions about what ctxt we are called from: */
300 queue_work(priv->wq, &omap_crtc->page_flip_work);
301 }
303 static int omap_crtc_page_flip_locked(struct drm_crtc *crtc,
304 struct drm_framebuffer *fb,
305 struct drm_pending_vblank_event *event)
306 {
307 struct drm_device *dev = crtc->dev;
308 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
309 struct drm_gem_object *bo;
311 DBG("%d -> %d (event=%p)", crtc->fb ? crtc->fb->base.id : -1,
312 fb->base.id, event);
314 if (omap_crtc->old_fb) {
315 dev_err(dev->dev, "already a pending flip\n");
316 return -EINVAL;
317 }
319 omap_crtc->event = event;
320 crtc->fb = fb;
322 /*
323 * Hold a reference temporarily until the crtc is updated
324 * and takes the reference to the bo. This avoids it
325 * getting freed from under us:
326 */
327 bo = omap_framebuffer_bo(fb, 0);
328 drm_gem_object_reference(bo);
330 omap_gem_op_async(bo, OMAP_GEM_READ, page_flip_cb, crtc);
332 return 0;
333 }
335 static int omap_crtc_set_property(struct drm_crtc *crtc,
336 struct drm_property *property, uint64_t val)
337 {
338 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
339 struct omap_drm_private *priv = crtc->dev->dev_private;
341 if (property == priv->rotation_prop) {
342 crtc->invert_dimensions =
343 !!(val & ((1LL << DRM_ROTATE_90) | (1LL << DRM_ROTATE_270)));
344 }
346 return omap_plane_set_property(omap_crtc->plane, property, val);
347 }
349 static const struct drm_crtc_funcs omap_crtc_funcs = {
350 .set_config = drm_crtc_helper_set_config,
351 .destroy = omap_crtc_destroy,
352 .page_flip = omap_crtc_page_flip_locked,
353 .set_property = omap_crtc_set_property,
354 };
356 static const struct drm_crtc_helper_funcs omap_crtc_helper_funcs = {
357 .dpms = omap_crtc_dpms,
358 .mode_fixup = omap_crtc_mode_fixup,
359 .mode_set = omap_crtc_mode_set,
360 .prepare = omap_crtc_prepare,
361 .commit = omap_crtc_commit,
362 .mode_set_base = omap_crtc_mode_set_base,
363 .load_lut = omap_crtc_load_lut,
364 };
366 const struct omap_video_timings *omap_crtc_timings(struct drm_crtc *crtc)
367 {
368 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
369 return &omap_crtc->timings;
370 }
372 enum omap_channel omap_crtc_channel(struct drm_crtc *crtc)
373 {
374 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
375 return omap_crtc->channel;
376 }
378 static void omap_crtc_error_irq(struct omap_drm_irq *irq, uint32_t irqstatus)
379 {
380 struct omap_crtc *omap_crtc =
381 container_of(irq, struct omap_crtc, error_irq);
382 struct drm_crtc *crtc = &omap_crtc->base;
383 DRM_ERROR("%s: errors: %08x\n", omap_crtc->name, irqstatus);
384 /* avoid getting in a flood, unregister the irq until next vblank */
385 omap_irq_unregister(crtc->dev, &omap_crtc->error_irq);
386 }
388 static void omap_crtc_apply_irq(struct omap_drm_irq *irq, uint32_t irqstatus)
389 {
390 struct omap_crtc *omap_crtc =
391 container_of(irq, struct omap_crtc, apply_irq);
392 struct drm_crtc *crtc = &omap_crtc->base;
394 if (!omap_crtc->error_irq.registered)
395 omap_irq_register(crtc->dev, &omap_crtc->error_irq);
397 if (!dispc_mgr_go_busy(omap_crtc->channel)) {
398 struct omap_drm_private *priv =
399 crtc->dev->dev_private;
400 DBG("%s: apply done", omap_crtc->name);
401 omap_irq_unregister(crtc->dev, &omap_crtc->apply_irq);
402 queue_work(priv->wq, &omap_crtc->apply_work);
403 }
404 }
406 static void apply_worker(struct work_struct *work)
407 {
408 struct omap_crtc *omap_crtc =
409 container_of(work, struct omap_crtc, apply_work);
410 struct drm_crtc *crtc = &omap_crtc->base;
411 struct drm_device *dev = crtc->dev;
412 struct omap_drm_apply *apply, *n;
413 bool need_apply;
415 /*
416 * Synchronize everything on mode_config.mutex, to keep
417 * the callbacks and list modification all serialized
418 * with respect to modesetting ioctls from userspace.
419 */
420 mutex_lock(&dev->mode_config.mutex);
421 dispc_runtime_get();
423 /*
424 * If we are still pending a previous update, wait.. when the
425 * pending update completes, we get kicked again.
426 */
427 if (omap_crtc->apply_irq.registered)
428 goto out;
430 /* finish up previous apply's: */
431 list_for_each_entry_safe(apply, n,
432 &omap_crtc->pending_applies, pending_node) {
433 apply->post_apply(apply);
434 list_del(&apply->pending_node);
435 }
437 need_apply = !list_empty(&omap_crtc->queued_applies);
439 /* then handle the next round of of queued apply's: */
440 list_for_each_entry_safe(apply, n,
441 &omap_crtc->queued_applies, queued_node) {
442 apply->pre_apply(apply);
443 list_del(&apply->queued_node);
444 apply->queued = false;
445 list_add_tail(&apply->pending_node,
446 &omap_crtc->pending_applies);
447 }
449 if (need_apply) {
450 enum omap_channel channel = omap_crtc->channel;
452 DBG("%s: GO", omap_crtc->name);
454 if (dispc_mgr_is_enabled(channel)) {
455 omap_irq_register(dev, &omap_crtc->apply_irq);
456 dispc_mgr_go(channel);
457 } else {
458 struct omap_drm_private *priv = dev->dev_private;
459 queue_work(priv->wq, &omap_crtc->apply_work);
460 }
461 }
463 out:
464 dispc_runtime_put();
465 mutex_unlock(&dev->mode_config.mutex);
466 }
468 int omap_crtc_apply(struct drm_crtc *crtc,
469 struct omap_drm_apply *apply)
470 {
471 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
472 struct drm_device *dev = crtc->dev;
474 WARN_ON(!mutex_is_locked(&dev->mode_config.mutex));
476 /* no need to queue it again if it is already queued: */
477 if (apply->queued)
478 return 0;
480 apply->queued = true;
481 list_add_tail(&apply->queued_node, &omap_crtc->queued_applies);
483 /*
484 * If there are no currently pending updates, then go ahead and
485 * kick the worker immediately, otherwise it will run again when
486 * the current update finishes.
487 */
488 if (list_empty(&omap_crtc->pending_applies)) {
489 struct omap_drm_private *priv = crtc->dev->dev_private;
490 queue_work(priv->wq, &omap_crtc->apply_work);
491 }
493 return 0;
494 }
496 /* called only from apply */
497 static void set_enabled(struct drm_crtc *crtc, bool enable)
498 {
499 struct drm_device *dev = crtc->dev;
500 struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
501 enum omap_channel channel = omap_crtc->channel;
502 struct omap_irq_wait *wait = NULL;
504 if (dispc_mgr_is_enabled(channel) == enable)
505 return;
507 /* ignore sync-lost irqs during enable/disable */
508 omap_irq_unregister(crtc->dev, &omap_crtc->error_irq);
510 if (dispc_mgr_get_framedone_irq(channel)) {
511 if (!enable) {
512 wait = omap_irq_wait_init(dev,
513 dispc_mgr_get_framedone_irq(channel), 1);
514 }
515 } else {
516 /*
517 * When we disable digit output, we need to wait until fields
518 * are done. Otherwise the DSS is still working, and turning
519 * off the clocks prevents DSS from going to OFF mode. And when
520 * enabling, we need to wait for the extra sync losts
521 */
522 wait = omap_irq_wait_init(dev,
523 dispc_mgr_get_vsync_irq(channel), 2);
524 }
526 dispc_mgr_enable(channel, enable);
528 if (wait) {
529 int ret = omap_irq_wait(dev, wait, msecs_to_jiffies(100));
530 if (ret) {
531 dev_err(dev->dev, "%s: timeout waiting for %s\n",
532 omap_crtc->name, enable ? "enable" : "disable");
533 }
534 }
536 omap_irq_register(crtc->dev, &omap_crtc->error_irq);
537 }
539 static void omap_crtc_pre_apply(struct omap_drm_apply *apply)
540 {
541 struct omap_crtc *omap_crtc =
542 container_of(apply, struct omap_crtc, apply);
543 struct drm_crtc *crtc = &omap_crtc->base;
544 struct drm_encoder *encoder = NULL;
546 DBG("%s: enabled=%d, full=%d", omap_crtc->name,
547 omap_crtc->enabled, omap_crtc->full_update);
549 if (omap_crtc->full_update) {
550 struct omap_drm_private *priv = crtc->dev->dev_private;
551 int i;
552 for (i = 0; i < priv->num_encoders; i++) {
553 if (priv->encoders[i]->crtc == crtc) {
554 encoder = priv->encoders[i];
555 break;
556 }
557 }
558 }
560 if (!omap_crtc->enabled) {
561 set_enabled(&omap_crtc->base, false);
562 if (encoder)
563 omap_encoder_set_enabled(encoder, false);
564 } else {
565 if (encoder) {
566 omap_encoder_set_enabled(encoder, false);
567 omap_encoder_update(encoder, &omap_crtc->mgr,
568 &omap_crtc->timings);
569 omap_encoder_set_enabled(encoder, true);
570 omap_crtc->full_update = false;
571 }
573 dispc_mgr_setup(omap_crtc->channel, &omap_crtc->info);
574 dispc_mgr_set_timings(omap_crtc->channel,
575 &omap_crtc->timings);
576 set_enabled(&omap_crtc->base, true);
577 }
579 omap_crtc->full_update = false;
580 }
582 static void omap_crtc_post_apply(struct omap_drm_apply *apply)
583 {
584 /* nothing needed for post-apply */
585 }
587 static const char *channel_names[] = {
588 [OMAP_DSS_CHANNEL_LCD] = "lcd",
589 [OMAP_DSS_CHANNEL_DIGIT] = "tv",
590 [OMAP_DSS_CHANNEL_LCD2] = "lcd2",
591 };
593 /* initialize crtc */
594 struct drm_crtc *omap_crtc_init(struct drm_device *dev,
595 struct drm_plane *plane, enum omap_channel channel, int id)
596 {
597 struct drm_crtc *crtc = NULL;
598 struct omap_crtc *omap_crtc;
599 struct omap_overlay_manager_info *info;
601 DBG("%s", channel_names[channel]);
603 omap_crtc = kzalloc(sizeof(*omap_crtc), GFP_KERNEL);
605 if (!omap_crtc) {
606 dev_err(dev->dev, "could not allocate CRTC\n");
607 goto fail;
608 }
610 crtc = &omap_crtc->base;
612 INIT_WORK(&omap_crtc->page_flip_work, page_flip_worker);
613 INIT_WORK(&omap_crtc->apply_work, apply_worker);
615 INIT_LIST_HEAD(&omap_crtc->pending_applies);
616 INIT_LIST_HEAD(&omap_crtc->queued_applies);
618 omap_crtc->apply.pre_apply = omap_crtc_pre_apply;
619 omap_crtc->apply.post_apply = omap_crtc_post_apply;
621 omap_crtc->apply_irq.irqmask = pipe2vbl(id);
622 omap_crtc->apply_irq.irq = omap_crtc_apply_irq;
624 omap_crtc->error_irq.irqmask =
625 dispc_mgr_get_sync_lost_irq(channel);
626 omap_crtc->error_irq.irq = omap_crtc_error_irq;
627 omap_irq_register(dev, &omap_crtc->error_irq);
629 omap_crtc->channel = channel;
630 omap_crtc->plane = plane;
631 omap_crtc->plane->crtc = crtc;
632 omap_crtc->name = channel_names[channel];
633 omap_crtc->pipe = id;
635 /* temporary: */
636 omap_crtc->mgr.id = channel;
638 dss_install_mgr_ops(&mgr_ops);
640 /* TODO: fix hard-coded setup.. add properties! */
641 info = &omap_crtc->info;
642 info->default_color = 0x00000000;
643 info->trans_key = 0x00000000;
644 info->trans_key_type = OMAP_DSS_COLOR_KEY_GFX_DST;
645 info->trans_enabled = false;
647 drm_crtc_init(dev, crtc, &omap_crtc_funcs);
648 drm_crtc_helper_add(crtc, &omap_crtc_helper_funcs);
650 omap_plane_install_properties(omap_crtc->plane, &crtc->base);
652 return crtc;
654 fail:
655 if (crtc)
656 omap_crtc_destroy(crtc);
658 return NULL;
659 }