c196c75c9d2b80d6ca81980e0933edf187f9ceee
[android-sdk/kernel-video.git] / drivers / gpu / drm / omapdrm / omap_gem.c
1 /*
2  * drivers/gpu/drm/omapdrm/omap_gem.c
3  *
4  * Copyright (C) 2011 Texas Instruments
5  * Author: Rob Clark <rob.clark@linaro.org>
6  *
7  * This program is free software; you can redistribute it and/or modify it
8  * under the terms of the GNU General Public License version 2 as published by
9  * the Free Software Foundation.
10  *
11  * This program is distributed in the hope that it will be useful, but WITHOUT
12  * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
13  * FITNESS FOR A PARTICULAR PURPOSE.  See the GNU General Public License for
14  * more details.
15  *
16  * You should have received a copy of the GNU General Public License along with
17  * this program.  If not, see <http://www.gnu.org/licenses/>.
18  */
21 #include <linux/spinlock.h>
22 #include <linux/shmem_fs.h>
23 #include <drm/drm_vma_manager.h>
25 #include "omap_drv.h"
26 #include "omap_dmm_tiler.h"
28 /* remove these once drm core helpers are merged */
29 struct page **_drm_gem_get_pages(struct drm_gem_object *obj, gfp_t gfpmask);
30 void _drm_gem_put_pages(struct drm_gem_object *obj, struct page **pages,
31                 bool dirty, bool accessed);
32 int _drm_gem_create_mmap_offset_size(struct drm_gem_object *obj, size_t size);
34 /*
35  * GEM buffer object implementation.
36  */
38 #define to_omap_bo(x) container_of(x, struct omap_gem_object, base)
40 /* note: we use upper 8 bits of flags for driver-internal flags: */
41 #define OMAP_BO_DMA                     0x01000000      /* actually is physically contiguous */
42 #define OMAP_BO_EXT_SYNC        0x02000000      /* externally allocated sync object */
43 #define OMAP_BO_EXT_MEM         0x04000000      /* externally allocated memory */
46 struct omap_gem_object {
47         struct drm_gem_object base;
49         struct list_head mm_list;
51         uint32_t flags;
53         /** width/height for tiled formats (rounded up to slot boundaries) */
54         uint16_t width, height;
56         /** roll applied when mapping to DMM */
57         uint32_t roll;
59         /**
60          * If buffer is allocated physically contiguous, the OMAP_BO_DMA flag
61          * is set and the paddr is valid.  Also if the buffer is remapped in
62          * TILER and paddr_cnt > 0, then paddr is valid.  But if you are using
63          * the physical address and OMAP_BO_DMA is not set, then you should
64          * be going thru omap_gem_{get,put}_paddr() to ensure the mapping is
65          * not removed from under your feet.
66          *
67          * Note that OMAP_BO_SCANOUT is a hint from userspace that DMA capable
68          * buffer is requested, but doesn't mean that it is.  Use the
69          * OMAP_BO_DMA flag to determine if the buffer has a DMA capable
70          * physical address.
71          */
72         dma_addr_t paddr;
74         /**
75          * # of users of paddr
76          */
77         uint32_t paddr_cnt;
79         /**
80          * tiler block used when buffer is remapped in DMM/TILER.
81          */
82         struct tiler_block *block;
84         /**
85          * Array of backing pages, if allocated.  Note that pages are never
86          * allocated for buffers originally allocated from contiguous memory
87          */
88         struct page **pages;
90         /** addresses corresponding to pages in above array */
91         dma_addr_t *addrs;
93         /**
94          * Virtual address, if mapped.
95          */
96         void *vaddr;
98         /**
99          * sync-object allocated on demand (if needed)
100          *
101          * Per-buffer sync-object for tracking pending and completed hw/dma
102          * read and write operations.  The layout in memory is dictated by
103          * the SGX firmware, which uses this information to stall the command
104          * stream if a surface is not ready yet.
105          *
106          * Note that when buffer is used by SGX, the sync-object needs to be
107          * allocated from a special heap of sync-objects.  This way many sync
108          * objects can be packed in a page, and not waste GPU virtual address
109          * space.  Because of this we have to have a omap_gem_set_sync_object()
110          * API to allow replacement of the syncobj after it has (potentially)
111          * already been allocated.  A bit ugly but I haven't thought of a
112          * better alternative.
113          */
114         struct {
115                 uint32_t write_pending;
116                 uint32_t write_complete;
117                 uint32_t read_pending;
118                 uint32_t read_complete;
119         } *sync;
121         struct omap_gem_vm_ops *ops;
123         /**
124          * per-mapper private data..
125          *
126          * TODO maybe there can be a more flexible way to store per-mapper
127          * data.. for now I just keep it simple, and since this is only
128          * accessible externally via omap_gem_priv()/omap_get_set_priv()
129          */
130         void *priv[MAX_MAPPERS];
132 };
134 static int get_pages(struct drm_gem_object *obj, struct page ***pages);
135 static uint64_t mmap_offset(struct drm_gem_object *obj);
137 /* To deal with userspace mmap'ings of 2d tiled buffers, which (a) are
138  * not necessarily pinned in TILER all the time, and (b) when they are
139  * they are not necessarily page aligned, we reserve one or more small
140  * regions in each of the 2d containers to use as a user-GART where we
141  * can create a second page-aligned mapping of parts of the buffer
142  * being accessed from userspace.
143  *
144  * Note that we could optimize slightly when we know that multiple
145  * tiler containers are backed by the same PAT.. but I'll leave that
146  * for later..
147  */
148 #define NUM_USERGART_ENTRIES 2
149 struct usergart_entry {
150         struct tiler_block *block;      /* the reserved tiler block */
151         dma_addr_t paddr;
152         struct drm_gem_object *obj;     /* the current pinned obj */
153         pgoff_t obj_pgoff;              /* page offset of obj currently
154                                            mapped in */
155 };
156 static struct {
157         struct usergart_entry entry[NUM_USERGART_ENTRIES];
158         int height;                             /* height in rows */
159         int height_shift;               /* ilog2(height in rows) */
160         int slot_shift;                 /* ilog2(width per slot) */
161         int stride_pfn;                 /* stride in pages */
162         int last;                               /* index of last used entry */
163 } *usergart;
165 static void evict_entry(struct drm_gem_object *obj,
166                 enum tiler_fmt fmt, struct usergart_entry *entry)
168         struct omap_gem_object *omap_obj = to_omap_bo(obj);
169         int n = usergart[fmt].height;
170         size_t size = PAGE_SIZE * n;
171         loff_t off = mmap_offset(obj) +
172                         (entry->obj_pgoff << PAGE_SHIFT);
173         const int m = 1 + ((omap_obj->width << fmt) / PAGE_SIZE);
175         if (m > 1) {
176                 int i;
177                 /* if stride > than PAGE_SIZE then sparse mapping: */
178                 for (i = n; i > 0; i--) {
179                         unmap_mapping_range(obj->dev->anon_inode->i_mapping,
180                                             off, PAGE_SIZE, 1);
181                         off += PAGE_SIZE * m;
182                 }
183         } else {
184                 unmap_mapping_range(obj->dev->anon_inode->i_mapping,
185                                     off, size, 1);
186         }
188         entry->obj = NULL;
191 /* Evict a buffer from usergart, if it is mapped there */
192 static void evict(struct drm_gem_object *obj)
194         struct omap_gem_object *omap_obj = to_omap_bo(obj);
196         if (omap_obj->flags & OMAP_BO_TILED) {
197                 enum tiler_fmt fmt = gem2fmt(omap_obj->flags);
198                 int i;
200                 if (!usergart)
201                         return;
203                 for (i = 0; i < NUM_USERGART_ENTRIES; i++) {
204                         struct usergart_entry *entry = &usergart[fmt].entry[i];
205                         if (entry->obj == obj)
206                                 evict_entry(obj, fmt, entry);
207                 }
208         }
211 /* GEM objects can either be allocated from contiguous memory (in which
212  * case obj->filp==NULL), or w/ shmem backing (obj->filp!=NULL).  But non
213  * contiguous buffers can be remapped in TILER/DMM if they need to be
214  * contiguous... but we don't do this all the time to reduce pressure
215  * on TILER/DMM space when we know at allocation time that the buffer
216  * will need to be scanned out.
217  */
218 static inline bool is_shmem(struct drm_gem_object *obj)
220         return obj->filp != NULL;
223 /**
224  * shmem buffers that are mapped cached can simulate coherency via using
225  * page faulting to keep track of dirty pages
226  */
227 static inline bool is_cached_coherent(struct drm_gem_object *obj)
229         struct omap_gem_object *omap_obj = to_omap_bo(obj);
230         return is_shmem(obj) &&
231                 ((omap_obj->flags & OMAP_BO_CACHE_MASK) == OMAP_BO_CACHED);
234 static DEFINE_SPINLOCK(sync_lock);
236 /** ensure backing pages are allocated */
237 static int omap_gem_attach_pages(struct drm_gem_object *obj)
239         struct drm_device *dev = obj->dev;
240         struct omap_gem_object *omap_obj = to_omap_bo(obj);
241         struct page **pages;
242         int npages = obj->size >> PAGE_SHIFT;
243         int i, ret;
244         dma_addr_t *addrs;
246         WARN_ON(omap_obj->pages);
248         /* TODO: __GFP_DMA32 .. but somehow GFP_HIGHMEM is coming from the
249          * mapping_gfp_mask(mapping) which conflicts w/ GFP_DMA32.. probably
250          * we actually want CMA memory for it all anyways..
251          */
252         pages = drm_gem_get_pages(obj, GFP_KERNEL);
253         if (IS_ERR(pages)) {
254                 dev_err(obj->dev->dev, "could not get pages: %ld\n", PTR_ERR(pages));
255                 return PTR_ERR(pages);
256         }
258         /* for non-cached buffers, ensure the new pages are clean because
259          * DSS, GPU, etc. are not cache coherent:
260          */
261         if (omap_obj->flags & (OMAP_BO_WC|OMAP_BO_UNCACHED)) {
262                 addrs = kmalloc(npages * sizeof(*addrs), GFP_KERNEL);
263                 if (!addrs) {
264                         ret = -ENOMEM;
265                         goto free_pages;
266                 }
268                 for (i = 0; i < npages; i++) {
269                         addrs[i] = dma_map_page(dev->dev, pages[i],
270                                         0, PAGE_SIZE, DMA_BIDIRECTIONAL);
271                 }
272         } else {
273                 addrs = kzalloc(npages * sizeof(*addrs), GFP_KERNEL);
274                 if (!addrs) {
275                         ret = -ENOMEM;
276                         goto free_pages;
277                 }
278         }
280         omap_obj->addrs = addrs;
281         omap_obj->pages = pages;
283         return 0;
285 free_pages:
286         drm_gem_put_pages(obj, pages, true, false);
288         return ret;
291 /** release backing pages */
292 static void omap_gem_detach_pages(struct drm_gem_object *obj)
294         struct omap_gem_object *omap_obj = to_omap_bo(obj);
296         /* for non-cached buffers, ensure the new pages are clean because
297          * DSS, GPU, etc. are not cache coherent:
298          */
299         if (omap_obj->flags & (OMAP_BO_WC|OMAP_BO_UNCACHED)) {
300                 int i, npages = obj->size >> PAGE_SHIFT;
301                 for (i = 0; i < npages; i++) {
302                         dma_unmap_page(obj->dev->dev, omap_obj->addrs[i],
303                                         PAGE_SIZE, DMA_BIDIRECTIONAL);
304                 }
305         }
307         kfree(omap_obj->addrs);
308         omap_obj->addrs = NULL;
310         drm_gem_put_pages(obj, omap_obj->pages, true, false);
311         omap_obj->pages = NULL;
314 /* get buffer flags */
315 uint32_t omap_gem_flags(struct drm_gem_object *obj)
317         return to_omap_bo(obj)->flags;
319 EXPORT_SYMBOL(omap_gem_flags);
321 /** get mmap offset */
322 static uint64_t mmap_offset(struct drm_gem_object *obj)
324         struct drm_device *dev = obj->dev;
325         int ret;
326         size_t size;
328         WARN_ON(!mutex_is_locked(&dev->struct_mutex));
330         /* Make it mmapable */
331         size = omap_gem_mmap_size(obj);
332         ret = drm_gem_create_mmap_offset_size(obj, size);
333         if (ret) {
334                 dev_err(dev->dev, "could not allocate mmap offset\n");
335                 return 0;
336         }
338         return drm_vma_node_offset_addr(&obj->vma_node);
341 uint64_t omap_gem_mmap_offset(struct drm_gem_object *obj)
343         uint64_t offset;
344         mutex_lock(&obj->dev->struct_mutex);
345         offset = mmap_offset(obj);
346         mutex_unlock(&obj->dev->struct_mutex);
347         return offset;
349 EXPORT_SYMBOL(omap_gem_mmap_offset);
351 /** get mmap size */
352 size_t omap_gem_mmap_size(struct drm_gem_object *obj)
354         struct omap_gem_object *omap_obj = to_omap_bo(obj);
355         size_t size = obj->size;
357         if (omap_obj->flags & OMAP_BO_TILED) {
358                 /* for tiled buffers, the virtual size has stride rounded up
359                  * to 4kb.. (to hide the fact that row n+1 might start 16kb or
360                  * 32kb later!).  But we don't back the entire buffer with
361                  * pages, only the valid picture part.. so need to adjust for
362                  * this in the size used to mmap and generate mmap offset
363                  */
364                 size = tiler_vsize(gem2fmt(omap_obj->flags),
365                                 omap_obj->width, omap_obj->height);
366         }
368         return size;
371 /* get tiled size, returns -EINVAL if not tiled buffer */
372 int omap_gem_tiled_size(struct drm_gem_object *obj, uint16_t *w, uint16_t *h)
374         struct omap_gem_object *omap_obj = to_omap_bo(obj);
375         if (omap_obj->flags & OMAP_BO_TILED) {
376                 *w = omap_obj->width;
377                 *h = omap_obj->height;
378                 return 0;
379         }
380         return -EINVAL;
382 EXPORT_SYMBOL(omap_gem_tiled_size);
384 /* Normal handling for the case of faulting in non-tiled buffers */
385 static int fault_1d(struct drm_gem_object *obj,
386                 struct vm_area_struct *vma, struct vm_fault *vmf)
388         struct omap_gem_object *omap_obj = to_omap_bo(obj);
389         unsigned long pfn;
390         pgoff_t pgoff;
392         /* We don't use vmf->pgoff since that has the fake offset: */
393         pgoff = ((unsigned long)vmf->virtual_address -
394                         vma->vm_start) >> PAGE_SHIFT;
396         if (omap_obj->pages) {
397                 omap_gem_cpu_sync(obj, pgoff);
398                 pfn = page_to_pfn(omap_obj->pages[pgoff]);
399         } else {
400                 BUG_ON(!(omap_obj->flags & OMAP_BO_DMA));
401                 pfn = (omap_obj->paddr >> PAGE_SHIFT) + pgoff;
402         }
404         VERB("Inserting %p pfn %lx, pa %lx", vmf->virtual_address,
405                         pfn, pfn << PAGE_SHIFT);
407         return vm_insert_mixed(vma, (unsigned long)vmf->virtual_address, pfn);
410 /* Special handling for the case of faulting in 2d tiled buffers */
411 static int fault_2d(struct drm_gem_object *obj,
412                 struct vm_area_struct *vma, struct vm_fault *vmf)
414         struct omap_gem_object *omap_obj = to_omap_bo(obj);
415         struct usergart_entry *entry;
416         enum tiler_fmt fmt = gem2fmt(omap_obj->flags);
417         struct page *pages[64];  /* XXX is this too much to have on stack? */
418         unsigned long pfn;
419         pgoff_t pgoff, base_pgoff;
420         void __user *vaddr;
421         int i, ret, slots;
423         /*
424          * Note the height of the slot is also equal to the number of pages
425          * that need to be mapped in to fill 4kb wide CPU page.  If the slot
426          * height is 64, then 64 pages fill a 4kb wide by 64 row region.
427          */
428         const int n = usergart[fmt].height;
429         const int n_shift = usergart[fmt].height_shift;
431         /*
432          * If buffer width in bytes > PAGE_SIZE then the virtual stride is
433          * rounded up to next multiple of PAGE_SIZE.. this need to be taken
434          * into account in some of the math, so figure out virtual stride
435          * in pages
436          */
437         const int m = 1 + ((omap_obj->width << fmt) / PAGE_SIZE);
439         /* We don't use vmf->pgoff since that has the fake offset: */
440         pgoff = ((unsigned long)vmf->virtual_address -
441                         vma->vm_start) >> PAGE_SHIFT;
443         /*
444          * Actual address we start mapping at is rounded down to previous slot
445          * boundary in the y direction:
446          */
447         base_pgoff = round_down(pgoff, m << n_shift);
449         /* figure out buffer width in slots */
450         slots = omap_obj->width >> usergart[fmt].slot_shift;
452         vaddr = vmf->virtual_address - ((pgoff - base_pgoff) << PAGE_SHIFT);
454         entry = &usergart[fmt].entry[usergart[fmt].last];
456         /* evict previous buffer using this usergart entry, if any: */
457         if (entry->obj)
458                 evict_entry(entry->obj, fmt, entry);
460         entry->obj = obj;
461         entry->obj_pgoff = base_pgoff;
463         /* now convert base_pgoff to phys offset from virt offset: */
464         base_pgoff = (base_pgoff >> n_shift) * slots;
466         /* for wider-than 4k.. figure out which part of the slot-row we want: */
467         if (m > 1) {
468                 int off = pgoff % m;
469                 entry->obj_pgoff += off;
470                 base_pgoff /= m;
471                 slots = min(slots - (off << n_shift), n);
472                 base_pgoff += off << n_shift;
473                 vaddr += off << PAGE_SHIFT;
474         }
476         /*
477          * Map in pages. Beyond the valid pixel part of the buffer, we set
478          * pages[i] to NULL to get a dummy page mapped in.. if someone
479          * reads/writes it they will get random/undefined content, but at
480          * least it won't be corrupting whatever other random page used to
481          * be mapped in, or other undefined behavior.
482          */
483         memcpy(pages, &omap_obj->pages[base_pgoff],
484                         sizeof(struct page *) * slots);
485         memset(pages + slots, 0,
486                         sizeof(struct page *) * (n - slots));
488         ret = tiler_pin(entry->block, pages, ARRAY_SIZE(pages), 0, true);
489         if (ret) {
490                 dev_err(obj->dev->dev, "failed to pin: %d\n", ret);
491                 return ret;
492         }
494         pfn = entry->paddr >> PAGE_SHIFT;
496         VERB("Inserting %p pfn %lx, pa %lx", vmf->virtual_address,
497                         pfn, pfn << PAGE_SHIFT);
499         for (i = n; i > 0; i--) {
500                 vm_insert_mixed(vma, (unsigned long)vaddr, pfn);
501                 pfn += usergart[fmt].stride_pfn;
502                 vaddr += PAGE_SIZE * m;
503         }
505         /* simple round-robin: */
506         usergart[fmt].last = (usergart[fmt].last + 1) % NUM_USERGART_ENTRIES;
508         return 0;
511 /**
512  * omap_gem_fault               -       pagefault handler for GEM objects
513  * @vma: the VMA of the GEM object
514  * @vmf: fault detail
515  *
516  * Invoked when a fault occurs on an mmap of a GEM managed area. GEM
517  * does most of the work for us including the actual map/unmap calls
518  * but we need to do the actual page work.
519  *
520  * The VMA was set up by GEM. In doing so it also ensured that the
521  * vma->vm_private_data points to the GEM object that is backing this
522  * mapping.
523  */
524 int omap_gem_fault(struct vm_area_struct *vma, struct vm_fault *vmf)
526         struct drm_gem_object *obj = vma->vm_private_data;
527         struct omap_gem_object *omap_obj = to_omap_bo(obj);
528         struct drm_device *dev = obj->dev;
529         struct page **pages;
530         int ret;
532         /* Make sure we don't parallel update on a fault, nor move or remove
533          * something from beneath our feet
534          */
535         mutex_lock(&dev->struct_mutex);
537         /* if a shmem backed object, make sure we have pages attached now */
538         ret = get_pages(obj, &pages);
539         if (ret)
540                 goto fail;
542         /* where should we do corresponding put_pages().. we are mapping
543          * the original page, rather than thru a GART, so we can't rely
544          * on eviction to trigger this.  But munmap() or all mappings should
545          * probably trigger put_pages()?
546          */
548         if (omap_obj->flags & OMAP_BO_TILED)
549                 ret = fault_2d(obj, vma, vmf);
550         else
551                 ret = fault_1d(obj, vma, vmf);
554 fail:
555         mutex_unlock(&dev->struct_mutex);
556         switch (ret) {
557         case 0:
558         case -ERESTARTSYS:
559         case -EINTR:
560                 return VM_FAULT_NOPAGE;
561         case -ENOMEM:
562                 return VM_FAULT_OOM;
563         default:
564                 return VM_FAULT_SIGBUS;
565         }
568 /** We override mainly to fix up some of the vm mapping flags.. */
569 int omap_gem_mmap(struct file *filp, struct vm_area_struct *vma)
571         int ret;
573         ret = drm_gem_mmap(filp, vma);
574         if (ret) {
575                 DBG("mmap failed: %d", ret);
576                 return ret;
577         }
579         return omap_gem_mmap_obj(vma->vm_private_data, vma);
582 int omap_gem_mmap_obj(struct drm_gem_object *obj,
583                 struct vm_area_struct *vma)
585         struct omap_gem_object *omap_obj = to_omap_bo(obj);
587         vma->vm_flags &= ~VM_PFNMAP;
588         vma->vm_flags |= VM_MIXEDMAP;
590         if (omap_obj->flags & OMAP_BO_WC) {
591                 vma->vm_page_prot = pgprot_writecombine(vm_get_page_prot(vma->vm_flags));
592         } else if (omap_obj->flags & OMAP_BO_UNCACHED) {
593                 vma->vm_page_prot = pgprot_noncached(vm_get_page_prot(vma->vm_flags));
594         } else {
595                 /*
596                  * We do have some private objects, at least for scanout buffers
597                  * on hardware without DMM/TILER.  But these are allocated write-
598                  * combine
599                  */
600                 if (WARN_ON(!obj->filp))
601                         return -EINVAL;
603                 /*
604                  * Shunt off cached objs to shmem file so they have their own
605                  * address_space (so unmap_mapping_range does what we want,
606                  * in particular in the case of mmap'd dmabufs)
607                  */
608                 fput(vma->vm_file);
609                 vma->vm_pgoff = 0;
610                 vma->vm_file  = get_file(obj->filp);
612                 vma->vm_page_prot = vm_get_page_prot(vma->vm_flags);
613         }
615         if (omap_obj->ops && omap_obj->ops->mmap)
616                 omap_obj->ops->mmap(obj->filp, vma);
618         return 0;
622 /**
623  * omap_gem_dumb_create -       create a dumb buffer
624  * @drm_file: our client file
625  * @dev: our device
626  * @args: the requested arguments copied from userspace
627  *
628  * Allocate a buffer suitable for use for a frame buffer of the
629  * form described by user space. Give userspace a handle by which
630  * to reference it.
631  */
632 int omap_gem_dumb_create(struct drm_file *file, struct drm_device *dev,
633                 struct drm_mode_create_dumb *args)
635         union omap_gem_size gsize;
637         /* in case someone tries to feed us a completely bogus stride: */
638         args->pitch = align_pitch(args->pitch, args->width, args->bpp);
639         args->size = PAGE_ALIGN(args->pitch * args->height);
641         gsize = (union omap_gem_size){
642                 .bytes = args->size,
643         };
645         return omap_gem_new_handle(dev, file, gsize,
646                         OMAP_BO_SCANOUT | OMAP_BO_WC, &args->handle);
649 /**
650  * omap_gem_dumb_map    -       buffer mapping for dumb interface
651  * @file: our drm client file
652  * @dev: drm device
653  * @handle: GEM handle to the object (from dumb_create)
654  *
655  * Do the necessary setup to allow the mapping of the frame buffer
656  * into user memory. We don't have to do much here at the moment.
657  */
658 int omap_gem_dumb_map_offset(struct drm_file *file, struct drm_device *dev,
659                 uint32_t handle, uint64_t *offset)
661         struct drm_gem_object *obj;
662         int ret = 0;
664         /* GEM does all our handle to object mapping */
665         obj = drm_gem_object_lookup(dev, file, handle);
666         if (obj == NULL) {
667                 ret = -ENOENT;
668                 goto fail;
669         }
671         *offset = omap_gem_mmap_offset(obj);
673         drm_gem_object_unreference_unlocked(obj);
675 fail:
676         return ret;
679 /* Set scrolling position.  This allows us to implement fast scrolling
680  * for console.
681  *
682  * Call only from non-atomic contexts.
683  */
684 int omap_gem_roll(struct drm_gem_object *obj, uint32_t roll)
686         struct omap_gem_object *omap_obj = to_omap_bo(obj);
687         uint32_t npages = obj->size >> PAGE_SHIFT;
688         int ret = 0;
690         if (roll > npages) {
691                 dev_err(obj->dev->dev, "invalid roll: %d\n", roll);
692                 return -EINVAL;
693         }
695         omap_obj->roll = roll;
697         mutex_lock(&obj->dev->struct_mutex);
699         /* if we aren't mapped yet, we don't need to do anything */
700         if (omap_obj->block) {
701                 struct page **pages;
702                 ret = get_pages(obj, &pages);
703                 if (ret)
704                         goto fail;
705                 ret = tiler_pin(omap_obj->block, pages, npages, roll, true);
706                 if (ret)
707                         dev_err(obj->dev->dev, "could not repin: %d\n", ret);
708         }
710 fail:
711         mutex_unlock(&obj->dev->struct_mutex);
713         return ret;
716 /* Sync the buffer for CPU access.. note pages should already be
717  * attached, ie. omap_gem_get_pages()
718  */
719 void omap_gem_cpu_sync(struct drm_gem_object *obj, int pgoff)
721         struct drm_device *dev = obj->dev;
722         struct omap_gem_object *omap_obj = to_omap_bo(obj);
724         if (is_cached_coherent(obj) && omap_obj->addrs[pgoff]) {
725                 dma_unmap_page(dev->dev, omap_obj->addrs[pgoff],
726                                 PAGE_SIZE, DMA_BIDIRECTIONAL);
727                 omap_obj->addrs[pgoff] = 0;
728         }
731 /* sync the buffer for DMA access */
732 void omap_gem_dma_sync(struct drm_gem_object *obj,
733                 enum dma_data_direction dir)
735         struct drm_device *dev = obj->dev;
736         struct omap_gem_object *omap_obj = to_omap_bo(obj);
738         if (is_cached_coherent(obj)) {
739                 int i, npages = obj->size >> PAGE_SHIFT;
740                 struct page **pages = omap_obj->pages;
741                 bool dirty = false;
743                 for (i = 0; i < npages; i++) {
744                         if (!omap_obj->addrs[i]) {
745                                 omap_obj->addrs[i] = dma_map_page(dev->dev, pages[i], 0,
746                                                 PAGE_SIZE, DMA_BIDIRECTIONAL);
747                                 dirty = true;
748                         }
749                 }
751                 if (dirty) {
752                         unmap_mapping_range(obj->filp->f_mapping, 0,
753                                         omap_gem_mmap_size(obj), 1);
754                 }
755         }
758 /* Get physical address for DMA.. if 'remap' is true, and the buffer is not
759  * already contiguous, remap it to pin in physically contiguous memory.. (ie.
760  * map in TILER)
761  */
762 int omap_gem_get_paddr(struct drm_gem_object *obj,
763                 dma_addr_t *paddr, bool remap)
765         struct omap_drm_private *priv = obj->dev->dev_private;
766         struct omap_gem_object *omap_obj = to_omap_bo(obj);
767         int ret = 0;
769         mutex_lock(&obj->dev->struct_mutex);
771         if (remap && is_shmem(obj) && priv->has_dmm) {
772                 if (omap_obj->paddr_cnt == 0) {
773                         struct page **pages;
774                         uint32_t npages = obj->size >> PAGE_SHIFT;
775                         enum tiler_fmt fmt = gem2fmt(omap_obj->flags);
776                         struct tiler_block *block;
778                         BUG_ON(omap_obj->block);
780                         ret = get_pages(obj, &pages);
781                         if (ret)
782                                 goto fail;
784                         if (omap_obj->flags & OMAP_BO_TILED) {
785                                 block = tiler_reserve_2d(fmt,
786                                                 omap_obj->width,
787                                                 omap_obj->height, 0);
788                         } else {
789                                 block = tiler_reserve_1d(obj->size);
790                         }
792                         if (IS_ERR(block)) {
793                                 ret = PTR_ERR(block);
794                                 dev_err(obj->dev->dev,
795                                         "could not remap: %d (%d)\n", ret, fmt);
796                                 goto fail;
797                         }
799                         /* TODO: enable async refill.. */
800                         ret = tiler_pin(block, pages, npages,
801                                         omap_obj->roll, true);
802                         if (ret) {
803                                 tiler_release(block);
804                                 dev_err(obj->dev->dev,
805                                                 "could not pin: %d\n", ret);
806                                 goto fail;
807                         }
809                         omap_obj->paddr = tiler_ssptr(block);
810                         omap_obj->block = block;
812                         DBG("got paddr: %pad", &omap_obj->paddr);
813                 }
815                 omap_obj->paddr_cnt++;
817                 *paddr = omap_obj->paddr;
818         } else if (omap_obj->flags & OMAP_BO_DMA) {
819                 *paddr = omap_obj->paddr;
820         } else {
821                 ret = -EINVAL;
822                 goto fail;
823         }
825 fail:
826         mutex_unlock(&obj->dev->struct_mutex);
828         return ret;
830 EXPORT_SYMBOL(omap_gem_get_paddr);
832 /* Release physical address, when DMA is no longer being performed.. this
833  * could potentially unpin and unmap buffers from TILER
834  */
835 void omap_gem_put_paddr(struct drm_gem_object *obj)
837         struct omap_gem_object *omap_obj = to_omap_bo(obj);
838         int ret;
840         mutex_lock(&obj->dev->struct_mutex);
841         if (omap_obj->paddr_cnt > 0) {
842                 omap_obj->paddr_cnt--;
843                 if (omap_obj->paddr_cnt == 0) {
844                         ret = tiler_unpin(omap_obj->block);
845                         if (ret) {
846                                 dev_err(obj->dev->dev,
847                                         "could not unpin pages: %d\n", ret);
848                         }
849                         ret = tiler_release(omap_obj->block);
850                         if (ret) {
851                                 dev_err(obj->dev->dev,
852                                         "could not release unmap: %d\n", ret);
853                         }
854                         omap_obj->paddr = 0;
855                         omap_obj->block = NULL;
856                 }
857         }
859         mutex_unlock(&obj->dev->struct_mutex);
861 EXPORT_SYMBOL(omap_gem_put_paddr);
863 /* Get rotated scanout address (only valid if already pinned), at the
864  * specified orientation and x,y offset from top-left corner of buffer
865  * (only valid for tiled 2d buffers)
866  */
867 int omap_gem_rotated_paddr(struct drm_gem_object *obj, uint32_t orient,
868                 int x, int y, dma_addr_t *paddr)
870         struct omap_gem_object *omap_obj = to_omap_bo(obj);
871         int ret = -EINVAL;
873         mutex_lock(&obj->dev->struct_mutex);
874         if ((omap_obj->paddr_cnt > 0) && omap_obj->block &&
875                         (omap_obj->flags & OMAP_BO_TILED)) {
876                 *paddr = tiler_tsptr(omap_obj->block, orient, x, y);
877                 ret = 0;
878         }
879         mutex_unlock(&obj->dev->struct_mutex);
880         return ret;
883 /* Get tiler stride for the buffer (only valid for 2d tiled buffers) */
884 int omap_gem_tiled_stride(struct drm_gem_object *obj, uint32_t orient)
886         struct omap_gem_object *omap_obj = to_omap_bo(obj);
887         int ret = -EINVAL;
888         if (omap_obj->flags & OMAP_BO_TILED)
889                 ret = tiler_stride(gem2fmt(omap_obj->flags), orient);
890         return ret;
892 EXPORT_SYMBOL(omap_gem_tiled_stride);
894 /* acquire pages when needed (for example, for DMA where physically
895  * contiguous buffer is not required
896  */
897 static int get_pages(struct drm_gem_object *obj, struct page ***pages)
899         struct omap_gem_object *omap_obj = to_omap_bo(obj);
900         int ret = 0;
902         if (is_shmem(obj) && !omap_obj->pages) {
903                 ret = omap_gem_attach_pages(obj);
904                 if (ret) {
905                         dev_err(obj->dev->dev, "could not attach pages\n");
906                         return ret;
907                 }
908         }
910         /* TODO: even phys-contig.. we should have a list of pages? */
911         *pages = omap_obj->pages;
913         return 0;
916 /* if !remap, and we don't have pages backing, then fail, rather than
917  * increasing the pin count (which we don't really do yet anyways,
918  * because we don't support swapping pages back out).  And 'remap'
919  * might not be quite the right name, but I wanted to keep it working
920  * similarly to omap_gem_get_paddr().  Note though that mutex is not
921  * aquired if !remap (because this can be called in atomic ctxt),
922  * but probably omap_gem_get_paddr() should be changed to work in the
923  * same way.  If !remap, a matching omap_gem_put_pages() call is not
924  * required (and should not be made).
925  */
926 int omap_gem_get_pages(struct drm_gem_object *obj, struct page ***pages,
927                 bool remap)
929         int ret;
930         if (!remap) {
931                 struct omap_gem_object *omap_obj = to_omap_bo(obj);
932                 if (!omap_obj->pages)
933                         return -ENOMEM;
934                 *pages = omap_obj->pages;
935                 return 0;
936         }
937         mutex_lock(&obj->dev->struct_mutex);
938         ret = get_pages(obj, pages);
939         mutex_unlock(&obj->dev->struct_mutex);
940         return ret;
942 EXPORT_SYMBOL(omap_gem_get_pages);
944 /* release pages when DMA no longer being performed */
945 int omap_gem_put_pages(struct drm_gem_object *obj)
947         /* do something here if we dynamically attach/detach pages.. at
948          * least they would no longer need to be pinned if everyone has
949          * released the pages..
950          */
951         return 0;
953 EXPORT_SYMBOL(omap_gem_put_pages);
955 /* Get kernel virtual address for CPU access.. this more or less only
956  * exists for omap_fbdev.  This should be called with struct_mutex
957  * held.
958  */
959 void *omap_gem_vaddr(struct drm_gem_object *obj)
961         struct omap_gem_object *omap_obj = to_omap_bo(obj);
962         WARN_ON(!mutex_is_locked(&obj->dev->struct_mutex));
963         if (!omap_obj->vaddr) {
964                 struct page **pages;
965                 int ret = get_pages(obj, &pages);
966                 if (ret)
967                         return ERR_PTR(ret);
968                 omap_obj->vaddr = vmap(pages, obj->size >> PAGE_SHIFT,
969                                 VM_MAP, pgprot_writecombine(PAGE_KERNEL));
970         }
971         return omap_obj->vaddr;
974 #ifdef CONFIG_PM
975 /* re-pin objects in DMM in resume path: */
976 int omap_gem_resume(struct device *dev)
978         struct drm_device *drm_dev = dev_get_drvdata(dev);
979         struct omap_drm_private *priv = drm_dev->dev_private;
980         struct omap_gem_object *omap_obj;
981         int ret = 0;
983         list_for_each_entry(omap_obj, &priv->obj_list, mm_list) {
984                 if (omap_obj->block) {
985                         struct drm_gem_object *obj = &omap_obj->base;
986                         uint32_t npages = obj->size >> PAGE_SHIFT;
987                         WARN_ON(!omap_obj->pages);  /* this can't happen */
988                         ret = tiler_pin(omap_obj->block,
989                                         omap_obj->pages, npages,
990                                         omap_obj->roll, true);
991                         if (ret) {
992                                 dev_err(dev, "could not repin: %d\n", ret);
993                                 return ret;
994                         }
995                 }
996         }
998         return 0;
1000 #endif
1002 #ifdef CONFIG_DEBUG_FS
1003 void omap_gem_describe(struct drm_gem_object *obj, struct seq_file *m)
1005         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1006         uint64_t off;
1008         off = drm_vma_node_start(&obj->vma_node);
1010         seq_printf(m, "%08x: %2d (%2d) %08llx %pad (%2d) %p %4d",
1011                         omap_obj->flags, obj->name, obj->refcount.refcount.counter,
1012                         off, &omap_obj->paddr, omap_obj->paddr_cnt,
1013                         omap_obj->vaddr, omap_obj->roll);
1015         if (omap_obj->flags & OMAP_BO_TILED) {
1016                 seq_printf(m, " %dx%d", omap_obj->width, omap_obj->height);
1017                 if (omap_obj->block) {
1018                         struct tcm_area *area = &omap_obj->block->area;
1019                         seq_printf(m, " (%dx%d, %dx%d)",
1020                                         area->p0.x, area->p0.y,
1021                                         area->p1.x, area->p1.y);
1022                 }
1023         } else {
1024                 seq_printf(m, " %d", obj->size);
1025         }
1027         seq_printf(m, "\n");
1030 void omap_gem_describe_objects(struct list_head *list, struct seq_file *m)
1032         struct omap_gem_object *omap_obj;
1033         int count = 0;
1034         size_t size = 0;
1036         list_for_each_entry(omap_obj, list, mm_list) {
1037                 struct drm_gem_object *obj = &omap_obj->base;
1038                 seq_printf(m, "   ");
1039                 omap_gem_describe(obj, m);
1040                 count++;
1041                 size += obj->size;
1042         }
1044         seq_printf(m, "Total %d objects, %zu bytes\n", count, size);
1046 #endif
1048 /* Buffer Synchronization:
1049  */
1051 struct omap_gem_sync_waiter {
1052         struct list_head list;
1053         struct omap_gem_object *omap_obj;
1054         enum omap_gem_op op;
1055         uint32_t read_target, write_target;
1056         /* notify called w/ sync_lock held */
1057         void (*notify)(void *arg);
1058         void *arg;
1059 };
1061 /* list of omap_gem_sync_waiter.. the notify fxn gets called back when
1062  * the read and/or write target count is achieved which can call a user
1063  * callback (ex. to kick 3d and/or 2d), wakeup blocked task (prep for
1064  * cpu access), etc.
1065  */
1066 static LIST_HEAD(waiters);
1068 static inline bool is_waiting(struct omap_gem_sync_waiter *waiter)
1070         struct omap_gem_object *omap_obj = waiter->omap_obj;
1071         if ((waiter->op & OMAP_GEM_READ) &&
1072                         (omap_obj->sync->write_complete < waiter->write_target))
1073                 return true;
1074         if ((waiter->op & OMAP_GEM_WRITE) &&
1075                         (omap_obj->sync->read_complete < waiter->read_target))
1076                 return true;
1077         return false;
1080 /* macro for sync debug.. */
1081 #define SYNCDBG 0
1082 #define SYNC(fmt, ...) do { if (SYNCDBG) \
1083                 printk(KERN_ERR "%s:%d: "fmt"\n", \
1084                                 __func__, __LINE__, ##__VA_ARGS__); \
1085         } while (0)
1088 static void sync_op_update(void)
1090         LIST_HEAD(call_list);
1092         struct omap_gem_sync_waiter *waiter, *n;
1093         list_for_each_entry_safe(waiter, n, &waiters, list) {
1094                 if (!is_waiting(waiter)) {
1095                         list_del(&waiter->list);
1096                         list_add(&waiter->list, &call_list);
1097                 }
1098         }
1100         spin_unlock(&sync_lock);
1102         list_for_each_entry_safe(waiter, n, &call_list, list) {
1103                 SYNC("notify: %p", waiter);
1104                 list_del(&waiter->list);
1105                 waiter->notify(waiter->arg);
1106                 kfree(waiter);
1107         }
1109         spin_lock(&sync_lock);
1112 static inline int sync_op(struct drm_gem_object *obj,
1113                 enum omap_gem_op op, bool start)
1115         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1116         int ret = 0;
1118         spin_lock(&sync_lock);
1120         if (!omap_obj->sync) {
1121                 omap_obj->sync = kzalloc(sizeof(*omap_obj->sync), GFP_ATOMIC);
1122                 if (!omap_obj->sync) {
1123                         ret = -ENOMEM;
1124                         goto unlock;
1125                 }
1126         }
1128         if (start) {
1129                 if (op & OMAP_GEM_READ)
1130                         omap_obj->sync->read_pending++;
1131                 if (op & OMAP_GEM_WRITE)
1132                         omap_obj->sync->write_pending++;
1133         } else {
1134                 if (op & OMAP_GEM_READ)
1135                         omap_obj->sync->read_complete++;
1136                 if (op & OMAP_GEM_WRITE)
1137                         omap_obj->sync->write_complete++;
1138                 sync_op_update();
1139         }
1141 unlock:
1142         spin_unlock(&sync_lock);
1144         return ret;
1147 /* it is a bit lame to handle updates in this sort of polling way, but
1148  * in case of PVR, the GPU can directly update read/write complete
1149  * values, and not really tell us which ones it updated.. this also
1150  * means that sync_lock is not quite sufficient.  So we'll need to
1151  * do something a bit better when it comes time to add support for
1152  * separate 2d hw..
1153  */
1154 void omap_gem_op_update(void)
1156         spin_lock(&sync_lock);
1157         sync_op_update();
1158         spin_unlock(&sync_lock);
1160 EXPORT_SYMBOL(omap_gem_op_update);
1162 /* mark the start of read and/or write operation */
1163 int omap_gem_op_start(struct drm_gem_object *obj, enum omap_gem_op op)
1165         return sync_op(obj, op, true);
1167 EXPORT_SYMBOL(omap_gem_op_start);
1169 int omap_gem_op_finish(struct drm_gem_object *obj, enum omap_gem_op op)
1171         return sync_op(obj, op, false);
1173 EXPORT_SYMBOL(omap_gem_op_finish);
1175 static DECLARE_WAIT_QUEUE_HEAD(sync_event);
1177 static void sync_notify(void *arg)
1179         struct task_struct **waiter_task = arg;
1180         *waiter_task = NULL;
1181         wake_up_all(&sync_event);
1184 int omap_gem_op_sync(struct drm_gem_object *obj, enum omap_gem_op op)
1186         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1187         int ret = 0;
1188         if (omap_obj->sync) {
1189                 struct task_struct *waiter_task = current;
1190                 struct omap_gem_sync_waiter *waiter =
1191                                 kzalloc(sizeof(*waiter), GFP_KERNEL);
1193                 if (!waiter)
1194                         return -ENOMEM;
1196                 waiter->omap_obj = omap_obj;
1197                 waiter->op = op;
1198                 waiter->read_target = omap_obj->sync->read_pending;
1199                 waiter->write_target = omap_obj->sync->write_pending;
1200                 waiter->notify = sync_notify;
1201                 waiter->arg = &waiter_task;
1203                 spin_lock(&sync_lock);
1204                 if (is_waiting(waiter)) {
1205                         SYNC("waited: %p", waiter);
1206                         list_add_tail(&waiter->list, &waiters);
1207                         spin_unlock(&sync_lock);
1208                         ret = wait_event_interruptible(sync_event,
1209                                         (waiter_task == NULL));
1210                         spin_lock(&sync_lock);
1211                         if (waiter_task) {
1212                                 SYNC("interrupted: %p", waiter);
1213                                 /* we were interrupted */
1214                                 list_del(&waiter->list);
1215                                 waiter_task = NULL;
1216                         } else {
1217                                 /* freed in sync_op_update() */
1218                                 waiter = NULL;
1219                         }
1220                 }
1221                 spin_unlock(&sync_lock);
1223                 if (waiter)
1224                         kfree(waiter);
1225         }
1226         return ret;
1228 EXPORT_SYMBOL(omap_gem_op_sync);
1230 /* call fxn(arg), either synchronously or asynchronously if the op
1231  * is currently blocked..  fxn() can be called from any context
1232  *
1233  * (TODO for now fxn is called back from whichever context calls
1234  * omap_gem_op_update().. but this could be better defined later
1235  * if needed)
1236  *
1237  * TODO more code in common w/ _sync()..
1238  */
1239 int omap_gem_op_async(struct drm_gem_object *obj, enum omap_gem_op op,
1240                 void (*fxn)(void *arg), void *arg)
1242         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1243         if (omap_obj->sync) {
1244                 struct omap_gem_sync_waiter *waiter =
1245                                 kzalloc(sizeof(*waiter), GFP_ATOMIC);
1247                 if (!waiter)
1248                         return -ENOMEM;
1250                 waiter->omap_obj = omap_obj;
1251                 waiter->op = op;
1252                 waiter->read_target = omap_obj->sync->read_pending;
1253                 waiter->write_target = omap_obj->sync->write_pending;
1254                 waiter->notify = fxn;
1255                 waiter->arg = arg;
1257                 spin_lock(&sync_lock);
1258                 if (is_waiting(waiter)) {
1259                         SYNC("waited: %p", waiter);
1260                         list_add_tail(&waiter->list, &waiters);
1261                         spin_unlock(&sync_lock);
1262                         return 0;
1263                 }
1265                 spin_unlock(&sync_lock);
1267                 kfree(waiter);
1268         }
1270         /* no waiting.. */
1271         fxn(arg);
1273         return 0;
1275 EXPORT_SYMBOL(omap_gem_op_async);
1277 /* special API so PVR can update the buffer to use a sync-object allocated
1278  * from it's sync-obj heap.  Only used for a newly allocated (from PVR's
1279  * perspective) sync-object, so we overwrite the new syncobj w/ values
1280  * from the already allocated syncobj (if there is one)
1281  */
1282 int omap_gem_set_sync_object(struct drm_gem_object *obj, void *syncobj)
1284         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1285         int ret = 0;
1287         spin_lock(&sync_lock);
1289         if ((omap_obj->flags & OMAP_BO_EXT_SYNC) && !syncobj) {
1290                 /* clearing a previously set syncobj */
1291                 syncobj = kmemdup(omap_obj->sync, sizeof(*omap_obj->sync),
1292                                   GFP_ATOMIC);
1293                 if (!syncobj) {
1294                         ret = -ENOMEM;
1295                         goto unlock;
1296                 }
1297                 omap_obj->flags &= ~OMAP_BO_EXT_SYNC;
1298                 omap_obj->sync = syncobj;
1299         } else if (syncobj && !(omap_obj->flags & OMAP_BO_EXT_SYNC)) {
1300                 /* replacing an existing syncobj */
1301                 if (omap_obj->sync) {
1302                         memcpy(syncobj, omap_obj->sync, sizeof(*omap_obj->sync));
1303                         kfree(omap_obj->sync);
1304                 }
1305                 omap_obj->flags |= OMAP_BO_EXT_SYNC;
1306                 omap_obj->sync = syncobj;
1307         }
1309 unlock:
1310         spin_unlock(&sync_lock);
1311         return ret;
1313 EXPORT_SYMBOL(omap_gem_set_sync_object);
1315 /* don't call directly.. called from GEM core when it is time to actually
1316  * free the object..
1317  */
1318 void omap_gem_free_object(struct drm_gem_object *obj)
1320         struct drm_device *dev = obj->dev;
1321         struct omap_drm_private *priv = dev->dev_private;
1322         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1324         evict(obj);
1326         WARN_ON(!mutex_is_locked(&dev->struct_mutex));
1328         spin_lock(&priv->list_lock);
1329         list_del(&omap_obj->mm_list);
1330         spin_unlock(&priv->list_lock);
1332         drm_gem_free_mmap_offset(obj);
1334         /* this means the object is still pinned.. which really should
1335          * not happen.  I think..
1336          */
1337         WARN_ON(omap_obj->paddr_cnt > 0);
1339         /* don't free externally allocated backing memory */
1340         if (!(omap_obj->flags & OMAP_BO_EXT_MEM)) {
1341                 if (omap_obj->pages)
1342                         omap_gem_detach_pages(obj);
1344                 if (!is_shmem(obj)) {
1345                         dma_free_writecombine(dev->dev, obj->size,
1346                                         omap_obj->vaddr, omap_obj->paddr);
1347                 } else if (omap_obj->vaddr) {
1348                         vunmap(omap_obj->vaddr);
1349                 }
1350         }
1352         /* don't free externally allocated syncobj */
1353         if (!(omap_obj->flags & OMAP_BO_EXT_SYNC))
1354                 kfree(omap_obj->sync);
1356         drm_gem_object_release(obj);
1358         kfree(omap_obj);
1361 /* convenience method to construct a GEM buffer object, and userspace handle */
1362 int omap_gem_new_handle(struct drm_device *dev, struct drm_file *file,
1363                 union omap_gem_size gsize, uint32_t flags, uint32_t *handle)
1365         struct drm_gem_object *obj;
1366         int ret;
1368         obj = omap_gem_new(dev, gsize, flags);
1369         if (!obj)
1370                 return -ENOMEM;
1372         ret = drm_gem_handle_create(file, obj, handle);
1373         if (ret) {
1374                 struct omap_gem_object *omap_obj = to_omap_bo(obj);
1375                 drm_gem_object_release(obj);
1376                 kfree(omap_obj); /* TODO isn't there a dtor to call? just copying i915 */
1377                 return ret;
1378         }
1380         /* drop reference from allocate - handle holds it now */
1381         drm_gem_object_unreference_unlocked(obj);
1383         return 0;
1386 /* GEM buffer object constructor */
1387 struct drm_gem_object *omap_gem_new(struct drm_device *dev,
1388                 union omap_gem_size gsize, uint32_t flags)
1390         struct omap_drm_private *priv = dev->dev_private;
1391         struct omap_gem_object *omap_obj;
1392         struct drm_gem_object *obj = NULL;
1393         size_t size;
1394         int ret;
1396         if (flags & OMAP_BO_TILED) {
1397                 if (!usergart) {
1398                         dev_err(dev->dev, "Tiled buffers require DMM\n");
1399                         goto fail;
1400                 }
1402                 /* tiled buffers are always shmem paged backed.. when they are
1403                  * scanned out, they are remapped into DMM/TILER
1404                  */
1405                 flags &= ~OMAP_BO_SCANOUT;
1407                 /* currently don't allow cached buffers.. there is some caching
1408                  * stuff that needs to be handled better
1409                  */
1410                 flags &= ~(OMAP_BO_CACHED|OMAP_BO_WC|OMAP_BO_UNCACHED);
1411                 flags |= tiler_get_cpu_cache_flags();
1413                 /* align dimensions to slot boundaries... */
1414                 tiler_align(gem2fmt(flags),
1415                                 &gsize.tiled.width, &gsize.tiled.height);
1417                 /* ...and calculate size based on aligned dimensions */
1418                 size = tiler_size(gem2fmt(flags),
1419                                 gsize.tiled.width, gsize.tiled.height);
1420         } else {
1421                 size = PAGE_ALIGN(gsize.bytes);
1422         }
1424         omap_obj = kzalloc(sizeof(*omap_obj), GFP_KERNEL);
1425         if (!omap_obj)
1426                 goto fail;
1428         spin_lock(&priv->list_lock);
1429         list_add(&omap_obj->mm_list, &priv->obj_list);
1430         spin_unlock(&priv->list_lock);
1432         obj = &omap_obj->base;
1434         if ((flags & OMAP_BO_SCANOUT) && !priv->has_dmm) {
1435                 /* attempt to allocate contiguous memory if we don't
1436                  * have DMM for remappign discontiguous buffers
1437                  */
1438                 omap_obj->vaddr =  dma_alloc_writecombine(dev->dev, size,
1439                                 &omap_obj->paddr, GFP_KERNEL);
1440                 if (!omap_obj->vaddr) {
1441                         spin_lock(&priv->list_lock);
1442                         list_del(&omap_obj->mm_list);
1443                         spin_unlock(&priv->list_lock);
1445                         kfree(omap_obj);
1447                         return NULL;
1448                 }
1450                 flags |= OMAP_BO_DMA;
1451         }
1453         omap_obj->flags = flags;
1455         if (flags & OMAP_BO_TILED) {
1456                 omap_obj->width = gsize.tiled.width;
1457                 omap_obj->height = gsize.tiled.height;
1458         }
1460         ret = 0;
1461         if (flags & (OMAP_BO_DMA|OMAP_BO_EXT_MEM))
1462                 drm_gem_private_object_init(dev, obj, size);
1463         else
1464                 ret = drm_gem_object_init(dev, obj, size);
1466         if (ret)
1467                 goto fail;
1469         return obj;
1471 fail:
1472         if (obj)
1473                 omap_gem_free_object(obj);
1475         return NULL;
1478 /* init/cleanup.. if DMM is used, we need to set some stuff up.. */
1479 void omap_gem_init(struct drm_device *dev)
1481         struct omap_drm_private *priv = dev->dev_private;
1482         const enum tiler_fmt fmts[] = {
1483                         TILFMT_8BIT, TILFMT_16BIT, TILFMT_32BIT
1484         };
1485         int i, j;
1487         if (!dmm_is_available()) {
1488                 /* DMM only supported on OMAP4 and later, so this isn't fatal */
1489                 dev_warn(dev->dev, "DMM not available, disable DMM support\n");
1490                 return;
1491         }
1493         usergart = kcalloc(3, sizeof(*usergart), GFP_KERNEL);
1494         if (!usergart)
1495                 return;
1497         /* reserve 4k aligned/wide regions for userspace mappings: */
1498         for (i = 0; i < ARRAY_SIZE(fmts); i++) {
1499                 uint16_t h = 1, w = PAGE_SIZE >> i;
1500                 tiler_align(fmts[i], &w, &h);
1501                 /* note: since each region is 1 4kb page wide, and minimum
1502                  * number of rows, the height ends up being the same as the
1503                  * # of pages in the region
1504                  */
1505                 usergart[i].height = h;
1506                 usergart[i].height_shift = ilog2(h);
1507                 usergart[i].stride_pfn = tiler_stride(fmts[i], 0) >> PAGE_SHIFT;
1508                 usergart[i].slot_shift = ilog2((PAGE_SIZE / h) >> i);
1509                 for (j = 0; j < NUM_USERGART_ENTRIES; j++) {
1510                         struct usergart_entry *entry = &usergart[i].entry[j];
1511                         struct tiler_block *block =
1512                                         tiler_reserve_2d(fmts[i], w, h,
1513                                                         PAGE_SIZE);
1514                         if (IS_ERR(block)) {
1515                                 dev_err(dev->dev,
1516                                                 "reserve failed: %d, %d, %ld\n",
1517                                                 i, j, PTR_ERR(block));
1518                                 return;
1519                         }
1520                         entry->paddr = tiler_ssptr(block);
1521                         entry->block = block;
1523                         DBG("%d:%d: %dx%d: paddr=%pad stride=%d", i, j, w, h,
1524                                         &entry->paddr,
1525                                         usergart[i].stride_pfn << PAGE_SHIFT);
1526                 }
1527         }
1529         priv->has_dmm = true;
1532 void omap_gem_deinit(struct drm_device *dev)
1534         /* I believe we can rely on there being no more outstanding GEM
1535          * objects which could depend on usergart/dmm at this point.
1536          */
1537         kfree(usergart);
1540 /****** PLUGIN API specific ******/
1542 /* This constructor is mainly to give plugins a way to wrap their
1543  * own allocations
1544  */
1545 struct drm_gem_object *omap_gem_new_ext(struct drm_device *dev,
1546                 union omap_gem_size gsize, uint32_t flags,
1547                 dma_addr_t paddr, struct page **pages,
1548                 struct omap_gem_vm_ops *ops)
1550         struct drm_gem_object *obj;
1552         BUG_ON((flags & OMAP_BO_TILED) && !pages);
1554         if (paddr)
1555                 flags |= OMAP_BO_DMA;
1557         obj = omap_gem_new(dev, gsize, flags | OMAP_BO_EXT_MEM);
1558         if (obj) {
1559                 struct omap_gem_object *omap_obj = to_omap_bo(obj);
1560                 omap_obj->paddr = paddr;
1561                 omap_obj->pages = pages;
1562                 omap_obj->ops = ops;
1563         }
1564         return obj;
1566 EXPORT_SYMBOL(omap_gem_new_ext);
1568 void omap_gem_vm_open(struct vm_area_struct *vma)
1570         struct drm_gem_object *obj = vma->vm_private_data;
1571         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1573         if (omap_obj->ops && omap_obj->ops->open)
1574                 omap_obj->ops->open(vma);
1575         else
1576                 drm_gem_vm_open(vma);
1580 void omap_gem_vm_close(struct vm_area_struct *vma)
1582         struct drm_gem_object *obj = vma->vm_private_data;
1583         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1585         if (omap_obj->ops && omap_obj->ops->close)
1586                 omap_obj->ops->close(vma);
1587         else
1588                 drm_gem_vm_close(vma);
1592 void *omap_gem_priv(struct drm_gem_object *obj, int mapper_id)
1594         BUG_ON((mapper_id >= MAX_MAPPERS) || (mapper_id < 0));
1595         return to_omap_bo(obj)->priv[mapper_id];
1597 EXPORT_SYMBOL(omap_gem_priv);
1599 void omap_gem_set_priv(struct drm_gem_object *obj, int mapper_id, void *priv)
1601         BUG_ON((mapper_id >= MAX_MAPPERS) || (mapper_id < 0));
1602         to_omap_bo(obj)->priv[mapper_id] = priv;
1604 EXPORT_SYMBOL(omap_gem_set_priv);