]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - drivers/gpu/drm/omapdrm/omap_gem.c
Merge branch 'pm-ti-linux-3.14.y' of git://git.ti.com/~kristo/ti-linux-kernel/pm...
[android-sdk/kernel-video.git] / drivers / gpu / drm / omapdrm / omap_gem.c
1 /*
2  * drivers/gpu/drm/omapdrm/omap_gem.c
3  *
4  * Copyright (C) 2011 Texas Instruments
5  * Author: Rob Clark <rob.clark@linaro.org>
6  *
7  * This program is free software; you can redistribute it and/or modify it
8  * under the terms of the GNU General Public License version 2 as published by
9  * the Free Software Foundation.
10  *
11  * This program is distributed in the hope that it will be useful, but WITHOUT
12  * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
13  * FITNESS FOR A PARTICULAR PURPOSE.  See the GNU General Public License for
14  * more details.
15  *
16  * You should have received a copy of the GNU General Public License along with
17  * this program.  If not, see <http://www.gnu.org/licenses/>.
18  */
21 #include <linux/spinlock.h>
22 #include <linux/shmem_fs.h>
23 #include <drm/drm_vma_manager.h>
25 #include "omap_drv.h"
26 #include "omap_dmm_tiler.h"
28 /* remove these once drm core helpers are merged */
29 struct page **_drm_gem_get_pages(struct drm_gem_object *obj, gfp_t gfpmask);
30 void _drm_gem_put_pages(struct drm_gem_object *obj, struct page **pages,
31                 bool dirty, bool accessed);
32 int _drm_gem_create_mmap_offset_size(struct drm_gem_object *obj, size_t size);
34 /*
35  * GEM buffer object implementation.
36  */
38 #define to_omap_bo(x) container_of(x, struct omap_gem_object, base)
40 /* note: we use upper 8 bits of flags for driver-internal flags: */
41 #define OMAP_BO_DMA                     0x01000000      /* actually is physically contiguous */
42 #define OMAP_BO_EXT_SYNC        0x02000000      /* externally allocated sync object */
43 #define OMAP_BO_EXT_MEM         0x04000000      /* externally allocated memory */
46 struct omap_gem_object {
47         struct drm_gem_object base;
49         struct list_head mm_list;
51         uint32_t flags;
53         /** width/height for tiled formats (rounded up to slot boundaries) */
54         uint16_t width, height;
56         /** roll applied when mapping to DMM */
57         uint32_t roll;
59         /**
60          * If buffer is allocated physically contiguous, the OMAP_BO_DMA flag
61          * is set and the paddr is valid.  Also if the buffer is remapped in
62          * TILER and paddr_cnt > 0, then paddr is valid.  But if you are using
63          * the physical address and OMAP_BO_DMA is not set, then you should
64          * be going thru omap_gem_{get,put}_paddr() to ensure the mapping is
65          * not removed from under your feet.
66          *
67          * Note that OMAP_BO_SCANOUT is a hint from userspace that DMA capable
68          * buffer is requested, but doesn't mean that it is.  Use the
69          * OMAP_BO_DMA flag to determine if the buffer has a DMA capable
70          * physical address.
71          */
72         dma_addr_t paddr;
74         /**
75          * # of users of paddr
76          */
77         uint32_t paddr_cnt;
79         /**
80          * tiler block used when buffer is remapped in DMM/TILER.
81          */
82         struct tiler_block *block;
84         /**
85          * Array of backing pages, if allocated.  Note that pages are never
86          * allocated for buffers originally allocated from contiguous memory
87          */
88         struct page **pages;
90         /** addresses corresponding to pages in above array */
91         dma_addr_t *addrs;
93         /**
94          * Virtual address, if mapped.
95          */
96         void *vaddr;
98         /**
99          * sync-object allocated on demand (if needed)
100          *
101          * Per-buffer sync-object for tracking pending and completed hw/dma
102          * read and write operations.  The layout in memory is dictated by
103          * the SGX firmware, which uses this information to stall the command
104          * stream if a surface is not ready yet.
105          *
106          * Note that when buffer is used by SGX, the sync-object needs to be
107          * allocated from a special heap of sync-objects.  This way many sync
108          * objects can be packed in a page, and not waste GPU virtual address
109          * space.  Because of this we have to have a omap_gem_set_sync_object()
110          * API to allow replacement of the syncobj after it has (potentially)
111          * already been allocated.  A bit ugly but I haven't thought of a
112          * better alternative.
113          */
114         struct {
115                 uint32_t write_pending;
116                 uint32_t write_complete;
117                 uint32_t read_pending;
118                 uint32_t read_complete;
119         } *sync;
120 };
122 static int get_pages(struct drm_gem_object *obj, struct page ***pages);
123 static uint64_t mmap_offset(struct drm_gem_object *obj);
125 /* To deal with userspace mmap'ings of 2d tiled buffers, which (a) are
126  * not necessarily pinned in TILER all the time, and (b) when they are
127  * they are not necessarily page aligned, we reserve one or more small
128  * regions in each of the 2d containers to use as a user-GART where we
129  * can create a second page-aligned mapping of parts of the buffer
130  * being accessed from userspace.
131  *
132  * Note that we could optimize slightly when we know that multiple
133  * tiler containers are backed by the same PAT.. but I'll leave that
134  * for later..
135  */
136 #define NUM_USERGART_ENTRIES 2
137 struct usergart_entry {
138         struct tiler_block *block;      /* the reserved tiler block */
139         dma_addr_t paddr;
140         struct drm_gem_object *obj;     /* the current pinned obj */
141         pgoff_t obj_pgoff;              /* page offset of obj currently
142                                            mapped in */
143 };
144 static struct {
145         struct usergart_entry entry[NUM_USERGART_ENTRIES];
146         int height;                             /* height in rows */
147         int height_shift;               /* ilog2(height in rows) */
148         int slot_shift;                 /* ilog2(width per slot) */
149         int stride_pfn;                 /* stride in pages */
150         int last;                               /* index of last used entry */
151 } *usergart;
153 static void evict_entry(struct drm_gem_object *obj,
154                 enum tiler_fmt fmt, struct usergart_entry *entry)
156         struct omap_gem_object *omap_obj = to_omap_bo(obj);
157         int n = usergart[fmt].height;
158         size_t size = PAGE_SIZE * n;
159         loff_t off = mmap_offset(obj) +
160                         (entry->obj_pgoff << PAGE_SHIFT);
161         const int m = 1 + ((omap_obj->width << fmt) / PAGE_SIZE);
163         if (m > 1) {
164                 int i;
165                 /* if stride > than PAGE_SIZE then sparse mapping: */
166                 for (i = n; i > 0; i--) {
167                         unmap_mapping_range(obj->dev->anon_inode->i_mapping,
168                                             off, PAGE_SIZE, 1);
169                         off += PAGE_SIZE * m;
170                 }
171         } else {
172                 unmap_mapping_range(obj->dev->anon_inode->i_mapping,
173                                     off, size, 1);
174         }
176         entry->obj = NULL;
179 /* Evict a buffer from usergart, if it is mapped there */
180 static void evict(struct drm_gem_object *obj)
182         struct omap_gem_object *omap_obj = to_omap_bo(obj);
184         if (omap_obj->flags & OMAP_BO_TILED) {
185                 enum tiler_fmt fmt = gem2fmt(omap_obj->flags);
186                 int i;
188                 if (!usergart)
189                         return;
191                 for (i = 0; i < NUM_USERGART_ENTRIES; i++) {
192                         struct usergart_entry *entry = &usergart[fmt].entry[i];
193                         if (entry->obj == obj)
194                                 evict_entry(obj, fmt, entry);
195                 }
196         }
199 /* GEM objects can either be allocated from contiguous memory (in which
200  * case obj->filp==NULL), or w/ shmem backing (obj->filp!=NULL).  But non
201  * contiguous buffers can be remapped in TILER/DMM if they need to be
202  * contiguous... but we don't do this all the time to reduce pressure
203  * on TILER/DMM space when we know at allocation time that the buffer
204  * will need to be scanned out.
205  */
206 static inline bool is_shmem(struct drm_gem_object *obj)
208         return obj->filp != NULL;
211 /**
212  * shmem buffers that are mapped cached can simulate coherency via using
213  * page faulting to keep track of dirty pages
214  */
215 static inline bool is_cached_coherent(struct drm_gem_object *obj)
217         struct omap_gem_object *omap_obj = to_omap_bo(obj);
218         return is_shmem(obj) &&
219                 ((omap_obj->flags & OMAP_BO_CACHE_MASK) == OMAP_BO_CACHED);
222 static DEFINE_SPINLOCK(sync_lock);
224 /** ensure backing pages are allocated */
225 static int omap_gem_attach_pages(struct drm_gem_object *obj)
227         struct drm_device *dev = obj->dev;
228         struct omap_gem_object *omap_obj = to_omap_bo(obj);
229         struct page **pages;
230         int npages = obj->size >> PAGE_SHIFT;
231         int i, ret;
232         dma_addr_t *addrs;
234         WARN_ON(omap_obj->pages);
236         /* TODO: __GFP_DMA32 .. but somehow GFP_HIGHMEM is coming from the
237          * mapping_gfp_mask(mapping) which conflicts w/ GFP_DMA32.. probably
238          * we actually want CMA memory for it all anyways..
239          */
240         pages = drm_gem_get_pages(obj, GFP_KERNEL);
241         if (IS_ERR(pages)) {
242                 dev_err(obj->dev->dev, "could not get pages: %ld\n", PTR_ERR(pages));
243                 return PTR_ERR(pages);
244         }
246         /* for non-cached buffers, ensure the new pages are clean because
247          * DSS, GPU, etc. are not cache coherent:
248          */
249         if (omap_obj->flags & (OMAP_BO_WC|OMAP_BO_UNCACHED)) {
250                 addrs = kmalloc(npages * sizeof(*addrs), GFP_KERNEL);
251                 if (!addrs) {
252                         ret = -ENOMEM;
253                         goto free_pages;
254                 }
256                 for (i = 0; i < npages; i++) {
257                         addrs[i] = dma_map_page(dev->dev, pages[i],
258                                         0, PAGE_SIZE, DMA_BIDIRECTIONAL);
259                 }
260         } else {
261                 addrs = kzalloc(npages * sizeof(*addrs), GFP_KERNEL);
262                 if (!addrs) {
263                         ret = -ENOMEM;
264                         goto free_pages;
265                 }
266         }
268         omap_obj->addrs = addrs;
269         omap_obj->pages = pages;
271         return 0;
273 free_pages:
274         drm_gem_put_pages(obj, pages, true, false);
276         return ret;
279 /** release backing pages */
280 static void omap_gem_detach_pages(struct drm_gem_object *obj)
282         struct omap_gem_object *omap_obj = to_omap_bo(obj);
284         /* for non-cached buffers, ensure the new pages are clean because
285          * DSS, GPU, etc. are not cache coherent:
286          */
287         if (omap_obj->flags & (OMAP_BO_WC|OMAP_BO_UNCACHED)) {
288                 int i, npages = obj->size >> PAGE_SHIFT;
289                 for (i = 0; i < npages; i++) {
290                         dma_unmap_page(obj->dev->dev, omap_obj->addrs[i],
291                                         PAGE_SIZE, DMA_BIDIRECTIONAL);
292                 }
293         }
295         kfree(omap_obj->addrs);
296         omap_obj->addrs = NULL;
298         drm_gem_put_pages(obj, omap_obj->pages, true, false);
299         omap_obj->pages = NULL;
302 /* get buffer flags */
303 uint32_t omap_gem_flags(struct drm_gem_object *obj)
305         return to_omap_bo(obj)->flags;
308 /** get mmap offset */
309 static uint64_t mmap_offset(struct drm_gem_object *obj)
311         struct drm_device *dev = obj->dev;
312         int ret;
313         size_t size;
315         WARN_ON(!mutex_is_locked(&dev->struct_mutex));
317         /* Make it mmapable */
318         size = omap_gem_mmap_size(obj);
319         ret = drm_gem_create_mmap_offset_size(obj, size);
320         if (ret) {
321                 dev_err(dev->dev, "could not allocate mmap offset\n");
322                 return 0;
323         }
325         return drm_vma_node_offset_addr(&obj->vma_node);
328 uint64_t omap_gem_mmap_offset(struct drm_gem_object *obj)
330         uint64_t offset;
331         mutex_lock(&obj->dev->struct_mutex);
332         offset = mmap_offset(obj);
333         mutex_unlock(&obj->dev->struct_mutex);
334         return offset;
337 /** get mmap size */
338 size_t omap_gem_mmap_size(struct drm_gem_object *obj)
340         struct omap_gem_object *omap_obj = to_omap_bo(obj);
341         size_t size = obj->size;
343         if (omap_obj->flags & OMAP_BO_TILED) {
344                 /* for tiled buffers, the virtual size has stride rounded up
345                  * to 4kb.. (to hide the fact that row n+1 might start 16kb or
346                  * 32kb later!).  But we don't back the entire buffer with
347                  * pages, only the valid picture part.. so need to adjust for
348                  * this in the size used to mmap and generate mmap offset
349                  */
350                 size = tiler_vsize(gem2fmt(omap_obj->flags),
351                                 omap_obj->width, omap_obj->height);
352         }
354         return size;
357 /* get tiled size, returns -EINVAL if not tiled buffer */
358 int omap_gem_tiled_size(struct drm_gem_object *obj, uint16_t *w, uint16_t *h)
360         struct omap_gem_object *omap_obj = to_omap_bo(obj);
361         if (omap_obj->flags & OMAP_BO_TILED) {
362                 *w = omap_obj->width;
363                 *h = omap_obj->height;
364                 return 0;
365         }
366         return -EINVAL;
369 /* Normal handling for the case of faulting in non-tiled buffers */
370 static int fault_1d(struct drm_gem_object *obj,
371                 struct vm_area_struct *vma, struct vm_fault *vmf)
373         struct omap_gem_object *omap_obj = to_omap_bo(obj);
374         unsigned long pfn;
375         pgoff_t pgoff;
377         /* We don't use vmf->pgoff since that has the fake offset: */
378         pgoff = ((unsigned long)vmf->virtual_address -
379                         vma->vm_start) >> PAGE_SHIFT;
381         if (omap_obj->pages) {
382                 omap_gem_cpu_sync(obj, pgoff);
383                 pfn = page_to_pfn(omap_obj->pages[pgoff]);
384         } else {
385                 BUG_ON(!(omap_obj->flags & OMAP_BO_DMA));
386                 pfn = (omap_obj->paddr >> PAGE_SHIFT) + pgoff;
387         }
389         VERB("Inserting %p pfn %lx, pa %lx", vmf->virtual_address,
390                         pfn, pfn << PAGE_SHIFT);
392         return vm_insert_mixed(vma, (unsigned long)vmf->virtual_address, pfn);
395 /* Special handling for the case of faulting in 2d tiled buffers */
396 static int fault_2d(struct drm_gem_object *obj,
397                 struct vm_area_struct *vma, struct vm_fault *vmf)
399         struct omap_gem_object *omap_obj = to_omap_bo(obj);
400         struct usergart_entry *entry;
401         enum tiler_fmt fmt = gem2fmt(omap_obj->flags);
402         struct page *pages[64];  /* XXX is this too much to have on stack? */
403         unsigned long pfn;
404         pgoff_t pgoff, base_pgoff;
405         void __user *vaddr;
406         int i, ret, slots;
408         /*
409          * Note the height of the slot is also equal to the number of pages
410          * that need to be mapped in to fill 4kb wide CPU page.  If the slot
411          * height is 64, then 64 pages fill a 4kb wide by 64 row region.
412          */
413         const int n = usergart[fmt].height;
414         const int n_shift = usergart[fmt].height_shift;
416         /*
417          * If buffer width in bytes > PAGE_SIZE then the virtual stride is
418          * rounded up to next multiple of PAGE_SIZE.. this need to be taken
419          * into account in some of the math, so figure out virtual stride
420          * in pages
421          */
422         const int m = 1 + ((omap_obj->width << fmt) / PAGE_SIZE);
424         /* We don't use vmf->pgoff since that has the fake offset: */
425         pgoff = ((unsigned long)vmf->virtual_address -
426                         vma->vm_start) >> PAGE_SHIFT;
428         /*
429          * Actual address we start mapping at is rounded down to previous slot
430          * boundary in the y direction:
431          */
432         base_pgoff = round_down(pgoff, m << n_shift);
434         /* figure out buffer width in slots */
435         slots = omap_obj->width >> usergart[fmt].slot_shift;
437         vaddr = vmf->virtual_address - ((pgoff - base_pgoff) << PAGE_SHIFT);
439         entry = &usergart[fmt].entry[usergart[fmt].last];
441         /* evict previous buffer using this usergart entry, if any: */
442         if (entry->obj)
443                 evict_entry(entry->obj, fmt, entry);
445         entry->obj = obj;
446         entry->obj_pgoff = base_pgoff;
448         /* now convert base_pgoff to phys offset from virt offset: */
449         base_pgoff = (base_pgoff >> n_shift) * slots;
451         /* for wider-than 4k.. figure out which part of the slot-row we want: */
452         if (m > 1) {
453                 int off = pgoff % m;
454                 entry->obj_pgoff += off;
455                 base_pgoff /= m;
456                 slots = min(slots - (off << n_shift), n);
457                 base_pgoff += off << n_shift;
458                 vaddr += off << PAGE_SHIFT;
459         }
461         /*
462          * Map in pages. Beyond the valid pixel part of the buffer, we set
463          * pages[i] to NULL to get a dummy page mapped in.. if someone
464          * reads/writes it they will get random/undefined content, but at
465          * least it won't be corrupting whatever other random page used to
466          * be mapped in, or other undefined behavior.
467          */
468         memcpy(pages, &omap_obj->pages[base_pgoff],
469                         sizeof(struct page *) * slots);
470         memset(pages + slots, 0,
471                         sizeof(struct page *) * (n - slots));
473         ret = tiler_pin(entry->block, pages, ARRAY_SIZE(pages), 0, true);
474         if (ret) {
475                 dev_err(obj->dev->dev, "failed to pin: %d\n", ret);
476                 return ret;
477         }
479         pfn = entry->paddr >> PAGE_SHIFT;
481         VERB("Inserting %p pfn %lx, pa %lx", vmf->virtual_address,
482                         pfn, pfn << PAGE_SHIFT);
484         for (i = n; i > 0; i--) {
485                 vm_insert_mixed(vma, (unsigned long)vaddr, pfn);
486                 pfn += usergart[fmt].stride_pfn;
487                 vaddr += PAGE_SIZE * m;
488         }
490         /* simple round-robin: */
491         usergart[fmt].last = (usergart[fmt].last + 1) % NUM_USERGART_ENTRIES;
493         return 0;
496 /**
497  * omap_gem_fault               -       pagefault handler for GEM objects
498  * @vma: the VMA of the GEM object
499  * @vmf: fault detail
500  *
501  * Invoked when a fault occurs on an mmap of a GEM managed area. GEM
502  * does most of the work for us including the actual map/unmap calls
503  * but we need to do the actual page work.
504  *
505  * The VMA was set up by GEM. In doing so it also ensured that the
506  * vma->vm_private_data points to the GEM object that is backing this
507  * mapping.
508  */
509 int omap_gem_fault(struct vm_area_struct *vma, struct vm_fault *vmf)
511         struct drm_gem_object *obj = vma->vm_private_data;
512         struct omap_gem_object *omap_obj = to_omap_bo(obj);
513         struct drm_device *dev = obj->dev;
514         struct page **pages;
515         int ret;
517         /* Make sure we don't parallel update on a fault, nor move or remove
518          * something from beneath our feet
519          */
520         mutex_lock(&dev->struct_mutex);
522         /* if a shmem backed object, make sure we have pages attached now */
523         ret = get_pages(obj, &pages);
524         if (ret)
525                 goto fail;
527         /* where should we do corresponding put_pages().. we are mapping
528          * the original page, rather than thru a GART, so we can't rely
529          * on eviction to trigger this.  But munmap() or all mappings should
530          * probably trigger put_pages()?
531          */
533         if (omap_obj->flags & OMAP_BO_TILED)
534                 ret = fault_2d(obj, vma, vmf);
535         else
536                 ret = fault_1d(obj, vma, vmf);
539 fail:
540         mutex_unlock(&dev->struct_mutex);
541         switch (ret) {
542         case 0:
543         case -ERESTARTSYS:
544         case -EINTR:
545                 return VM_FAULT_NOPAGE;
546         case -ENOMEM:
547                 return VM_FAULT_OOM;
548         default:
549                 return VM_FAULT_SIGBUS;
550         }
553 /** We override mainly to fix up some of the vm mapping flags.. */
554 int omap_gem_mmap(struct file *filp, struct vm_area_struct *vma)
556         int ret;
558         ret = drm_gem_mmap(filp, vma);
559         if (ret) {
560                 DBG("mmap failed: %d", ret);
561                 return ret;
562         }
564         return omap_gem_mmap_obj(vma->vm_private_data, vma);
567 int omap_gem_mmap_obj(struct drm_gem_object *obj,
568                 struct vm_area_struct *vma)
570         struct omap_gem_object *omap_obj = to_omap_bo(obj);
572         vma->vm_flags &= ~VM_PFNMAP;
573         vma->vm_flags |= VM_MIXEDMAP;
575         if (omap_obj->flags & OMAP_BO_WC) {
576                 vma->vm_page_prot = pgprot_writecombine(vm_get_page_prot(vma->vm_flags));
577         } else if (omap_obj->flags & OMAP_BO_UNCACHED) {
578                 vma->vm_page_prot = pgprot_noncached(vm_get_page_prot(vma->vm_flags));
579         } else {
580                 /*
581                  * We do have some private objects, at least for scanout buffers
582                  * on hardware without DMM/TILER.  But these are allocated write-
583                  * combine
584                  */
585                 if (WARN_ON(!obj->filp))
586                         return -EINVAL;
588                 /*
589                  * Shunt off cached objs to shmem file so they have their own
590                  * address_space (so unmap_mapping_range does what we want,
591                  * in particular in the case of mmap'd dmabufs)
592                  */
593                 fput(vma->vm_file);
594                 vma->vm_pgoff = 0;
595                 vma->vm_file  = get_file(obj->filp);
597                 vma->vm_page_prot = vm_get_page_prot(vma->vm_flags);
598         }
600         return 0;
604 /**
605  * omap_gem_dumb_create -       create a dumb buffer
606  * @drm_file: our client file
607  * @dev: our device
608  * @args: the requested arguments copied from userspace
609  *
610  * Allocate a buffer suitable for use for a frame buffer of the
611  * form described by user space. Give userspace a handle by which
612  * to reference it.
613  */
614 int omap_gem_dumb_create(struct drm_file *file, struct drm_device *dev,
615                 struct drm_mode_create_dumb *args)
617         union omap_gem_size gsize;
619         /* in case someone tries to feed us a completely bogus stride: */
620         args->pitch = align_pitch(args->pitch, args->width, args->bpp);
621         args->size = PAGE_ALIGN(args->pitch * args->height);
623         gsize = (union omap_gem_size){
624                 .bytes = args->size,
625         };
627         return omap_gem_new_handle(dev, file, gsize,
628                         OMAP_BO_SCANOUT | OMAP_BO_WC, &args->handle);
631 /**
632  * omap_gem_dumb_map    -       buffer mapping for dumb interface
633  * @file: our drm client file
634  * @dev: drm device
635  * @handle: GEM handle to the object (from dumb_create)
636  *
637  * Do the necessary setup to allow the mapping of the frame buffer
638  * into user memory. We don't have to do much here at the moment.
639  */
640 int omap_gem_dumb_map_offset(struct drm_file *file, struct drm_device *dev,
641                 uint32_t handle, uint64_t *offset)
643         struct drm_gem_object *obj;
644         int ret = 0;
646         /* GEM does all our handle to object mapping */
647         obj = drm_gem_object_lookup(dev, file, handle);
648         if (obj == NULL) {
649                 ret = -ENOENT;
650                 goto fail;
651         }
653         *offset = omap_gem_mmap_offset(obj);
655         drm_gem_object_unreference_unlocked(obj);
657 fail:
658         return ret;
661 /* Set scrolling position.  This allows us to implement fast scrolling
662  * for console.
663  *
664  * Call only from non-atomic contexts.
665  */
666 int omap_gem_roll(struct drm_gem_object *obj, uint32_t roll)
668         struct omap_gem_object *omap_obj = to_omap_bo(obj);
669         uint32_t npages = obj->size >> PAGE_SHIFT;
670         int ret = 0;
672         if (roll > npages) {
673                 dev_err(obj->dev->dev, "invalid roll: %d\n", roll);
674                 return -EINVAL;
675         }
677         omap_obj->roll = roll;
679         mutex_lock(&obj->dev->struct_mutex);
681         /* if we aren't mapped yet, we don't need to do anything */
682         if (omap_obj->block) {
683                 struct page **pages;
684                 ret = get_pages(obj, &pages);
685                 if (ret)
686                         goto fail;
687                 ret = tiler_pin(omap_obj->block, pages, npages, roll, true);
688                 if (ret)
689                         dev_err(obj->dev->dev, "could not repin: %d\n", ret);
690         }
692 fail:
693         mutex_unlock(&obj->dev->struct_mutex);
695         return ret;
698 /* Sync the buffer for CPU access.. note pages should already be
699  * attached, ie. omap_gem_get_pages()
700  */
701 void omap_gem_cpu_sync(struct drm_gem_object *obj, int pgoff)
703         struct drm_device *dev = obj->dev;
704         struct omap_gem_object *omap_obj = to_omap_bo(obj);
706         if (is_cached_coherent(obj) && omap_obj->addrs[pgoff]) {
707                 dma_unmap_page(dev->dev, omap_obj->addrs[pgoff],
708                                 PAGE_SIZE, DMA_BIDIRECTIONAL);
709                 omap_obj->addrs[pgoff] = 0;
710         }
713 /* sync the buffer for DMA access */
714 void omap_gem_dma_sync(struct drm_gem_object *obj,
715                 enum dma_data_direction dir)
717         struct drm_device *dev = obj->dev;
718         struct omap_gem_object *omap_obj = to_omap_bo(obj);
720         if (is_cached_coherent(obj)) {
721                 int i, npages = obj->size >> PAGE_SHIFT;
722                 struct page **pages = omap_obj->pages;
723                 bool dirty = false;
725                 for (i = 0; i < npages; i++) {
726                         if (!omap_obj->addrs[i]) {
727                                 omap_obj->addrs[i] = dma_map_page(dev->dev, pages[i], 0,
728                                                 PAGE_SIZE, DMA_BIDIRECTIONAL);
729                                 dirty = true;
730                         }
731                 }
733                 if (dirty) {
734                         unmap_mapping_range(obj->filp->f_mapping, 0,
735                                         omap_gem_mmap_size(obj), 1);
736                 }
737         }
740 /* Get physical address for DMA.. if 'remap' is true, and the buffer is not
741  * already contiguous, remap it to pin in physically contiguous memory.. (ie.
742  * map in TILER)
743  */
744 int omap_gem_get_paddr(struct drm_gem_object *obj,
745                 dma_addr_t *paddr, bool remap)
747         struct omap_drm_private *priv = obj->dev->dev_private;
748         struct omap_gem_object *omap_obj = to_omap_bo(obj);
749         int ret = 0;
751         mutex_lock(&obj->dev->struct_mutex);
753         if (remap && is_shmem(obj) && priv->has_dmm) {
754                 if (omap_obj->paddr_cnt == 0) {
755                         struct page **pages;
756                         uint32_t npages = obj->size >> PAGE_SHIFT;
757                         enum tiler_fmt fmt = gem2fmt(omap_obj->flags);
758                         struct tiler_block *block;
760                         BUG_ON(omap_obj->block);
762                         ret = get_pages(obj, &pages);
763                         if (ret)
764                                 goto fail;
766                         if (omap_obj->flags & OMAP_BO_TILED) {
767                                 block = tiler_reserve_2d(fmt,
768                                                 omap_obj->width,
769                                                 omap_obj->height, 0);
770                         } else {
771                                 block = tiler_reserve_1d(obj->size);
772                         }
774                         if (IS_ERR(block)) {
775                                 ret = PTR_ERR(block);
776                                 dev_err(obj->dev->dev,
777                                         "could not remap: %d (%d)\n", ret, fmt);
778                                 goto fail;
779                         }
781                         /* TODO: enable async refill.. */
782                         ret = tiler_pin(block, pages, npages,
783                                         omap_obj->roll, true);
784                         if (ret) {
785                                 tiler_release(block);
786                                 dev_err(obj->dev->dev,
787                                                 "could not pin: %d\n", ret);
788                                 goto fail;
789                         }
791                         omap_obj->paddr = tiler_ssptr(block);
792                         omap_obj->block = block;
794                         DBG("got paddr: %pad", &omap_obj->paddr);
795                 }
797                 omap_obj->paddr_cnt++;
799                 *paddr = omap_obj->paddr;
800         } else if (omap_obj->flags & OMAP_BO_DMA) {
801                 *paddr = omap_obj->paddr;
802         } else {
803                 ret = -EINVAL;
804                 goto fail;
805         }
807 fail:
808         mutex_unlock(&obj->dev->struct_mutex);
810         return ret;
813 /* Release physical address, when DMA is no longer being performed.. this
814  * could potentially unpin and unmap buffers from TILER
815  */
816 int omap_gem_put_paddr(struct drm_gem_object *obj)
818         struct omap_gem_object *omap_obj = to_omap_bo(obj);
819         int ret = 0;
821         mutex_lock(&obj->dev->struct_mutex);
822         if (omap_obj->paddr_cnt > 0) {
823                 omap_obj->paddr_cnt--;
824                 if (omap_obj->paddr_cnt == 0) {
825                         ret = tiler_unpin(omap_obj->block);
826                         if (ret) {
827                                 dev_err(obj->dev->dev,
828                                         "could not unpin pages: %d\n", ret);
829                                 goto fail;
830                         }
831                         ret = tiler_release(omap_obj->block);
832                         if (ret) {
833                                 dev_err(obj->dev->dev,
834                                         "could not release unmap: %d\n", ret);
835                         }
836                         omap_obj->paddr = 0;
837                         omap_obj->block = NULL;
838                 }
839         }
840 fail:
841         mutex_unlock(&obj->dev->struct_mutex);
842         return ret;
845 /* Get rotated scanout address (only valid if already pinned), at the
846  * specified orientation and x,y offset from top-left corner of buffer
847  * (only valid for tiled 2d buffers)
848  */
849 int omap_gem_rotated_paddr(struct drm_gem_object *obj, uint32_t orient,
850                 int x, int y, dma_addr_t *paddr)
852         struct omap_gem_object *omap_obj = to_omap_bo(obj);
853         int ret = -EINVAL;
855         mutex_lock(&obj->dev->struct_mutex);
856         if ((omap_obj->paddr_cnt > 0) && omap_obj->block &&
857                         (omap_obj->flags & OMAP_BO_TILED)) {
858                 *paddr = tiler_tsptr(omap_obj->block, orient, x, y);
859                 ret = 0;
860         }
861         mutex_unlock(&obj->dev->struct_mutex);
862         return ret;
865 /* Get tiler stride for the buffer (only valid for 2d tiled buffers) */
866 int omap_gem_tiled_stride(struct drm_gem_object *obj, uint32_t orient)
868         struct omap_gem_object *omap_obj = to_omap_bo(obj);
869         int ret = -EINVAL;
870         if (omap_obj->flags & OMAP_BO_TILED)
871                 ret = tiler_stride(gem2fmt(omap_obj->flags), orient);
872         return ret;
875 /* acquire pages when needed (for example, for DMA where physically
876  * contiguous buffer is not required
877  */
878 static int get_pages(struct drm_gem_object *obj, struct page ***pages)
880         struct omap_gem_object *omap_obj = to_omap_bo(obj);
881         int ret = 0;
883         if (is_shmem(obj) && !omap_obj->pages) {
884                 ret = omap_gem_attach_pages(obj);
885                 if (ret) {
886                         dev_err(obj->dev->dev, "could not attach pages\n");
887                         return ret;
888                 }
889         }
891         /* TODO: even phys-contig.. we should have a list of pages? */
892         *pages = omap_obj->pages;
894         return 0;
897 /* if !remap, and we don't have pages backing, then fail, rather than
898  * increasing the pin count (which we don't really do yet anyways,
899  * because we don't support swapping pages back out).  And 'remap'
900  * might not be quite the right name, but I wanted to keep it working
901  * similarly to omap_gem_get_paddr().  Note though that mutex is not
902  * aquired if !remap (because this can be called in atomic ctxt),
903  * but probably omap_gem_get_paddr() should be changed to work in the
904  * same way.  If !remap, a matching omap_gem_put_pages() call is not
905  * required (and should not be made).
906  */
907 int omap_gem_get_pages(struct drm_gem_object *obj, struct page ***pages,
908                 bool remap)
910         int ret;
911         if (!remap) {
912                 struct omap_gem_object *omap_obj = to_omap_bo(obj);
913                 if (!omap_obj->pages)
914                         return -ENOMEM;
915                 *pages = omap_obj->pages;
916                 return 0;
917         }
918         mutex_lock(&obj->dev->struct_mutex);
919         ret = get_pages(obj, pages);
920         mutex_unlock(&obj->dev->struct_mutex);
921         return ret;
924 /* release pages when DMA no longer being performed */
925 int omap_gem_put_pages(struct drm_gem_object *obj)
927         /* do something here if we dynamically attach/detach pages.. at
928          * least they would no longer need to be pinned if everyone has
929          * released the pages..
930          */
931         return 0;
934 /* Get kernel virtual address for CPU access.. this more or less only
935  * exists for omap_fbdev.  This should be called with struct_mutex
936  * held.
937  */
938 void *omap_gem_vaddr(struct drm_gem_object *obj)
940         struct omap_gem_object *omap_obj = to_omap_bo(obj);
941         WARN_ON(!mutex_is_locked(&obj->dev->struct_mutex));
942         if (!omap_obj->vaddr) {
943                 struct page **pages;
944                 int ret = get_pages(obj, &pages);
945                 if (ret)
946                         return ERR_PTR(ret);
947                 omap_obj->vaddr = vmap(pages, obj->size >> PAGE_SHIFT,
948                                 VM_MAP, pgprot_writecombine(PAGE_KERNEL));
949         }
950         return omap_obj->vaddr;
953 #ifdef CONFIG_PM
954 /* re-pin objects in DMM in resume path: */
955 int omap_gem_resume(struct device *dev)
957         struct drm_device *drm_dev = dev_get_drvdata(dev);
958         struct omap_drm_private *priv = drm_dev->dev_private;
959         struct omap_gem_object *omap_obj;
960         int ret = 0;
962         list_for_each_entry(omap_obj, &priv->obj_list, mm_list) {
963                 if (omap_obj->block) {
964                         struct drm_gem_object *obj = &omap_obj->base;
965                         uint32_t npages = obj->size >> PAGE_SHIFT;
966                         WARN_ON(!omap_obj->pages);  /* this can't happen */
967                         ret = tiler_pin(omap_obj->block,
968                                         omap_obj->pages, npages,
969                                         omap_obj->roll, true);
970                         if (ret) {
971                                 dev_err(dev, "could not repin: %d\n", ret);
972                                 return ret;
973                         }
974                 }
975         }
977         return 0;
979 #endif
981 #ifdef CONFIG_DEBUG_FS
982 void omap_gem_describe(struct drm_gem_object *obj, struct seq_file *m)
984         struct omap_gem_object *omap_obj = to_omap_bo(obj);
985         uint64_t off;
987         off = drm_vma_node_start(&obj->vma_node);
989         seq_printf(m, "%08x: %2d (%2d) %08llx %pad (%2d) %p %4d",
990                         omap_obj->flags, obj->name, obj->refcount.refcount.counter,
991                         off, &omap_obj->paddr, omap_obj->paddr_cnt,
992                         omap_obj->vaddr, omap_obj->roll);
994         if (omap_obj->flags & OMAP_BO_TILED) {
995                 seq_printf(m, " %dx%d", omap_obj->width, omap_obj->height);
996                 if (omap_obj->block) {
997                         struct tcm_area *area = &omap_obj->block->area;
998                         seq_printf(m, " (%dx%d, %dx%d)",
999                                         area->p0.x, area->p0.y,
1000                                         area->p1.x, area->p1.y);
1001                 }
1002         } else {
1003                 seq_printf(m, " %d", obj->size);
1004         }
1006         seq_printf(m, "\n");
1009 void omap_gem_describe_objects(struct list_head *list, struct seq_file *m)
1011         struct omap_gem_object *omap_obj;
1012         int count = 0;
1013         size_t size = 0;
1015         list_for_each_entry(omap_obj, list, mm_list) {
1016                 struct drm_gem_object *obj = &omap_obj->base;
1017                 seq_printf(m, "   ");
1018                 omap_gem_describe(obj, m);
1019                 count++;
1020                 size += obj->size;
1021         }
1023         seq_printf(m, "Total %d objects, %zu bytes\n", count, size);
1025 #endif
1027 /* Buffer Synchronization:
1028  */
1030 struct omap_gem_sync_waiter {
1031         struct list_head list;
1032         struct omap_gem_object *omap_obj;
1033         enum omap_gem_op op;
1034         uint32_t read_target, write_target;
1035         /* notify called w/ sync_lock held */
1036         void (*notify)(void *arg);
1037         void *arg;
1038 };
1040 /* list of omap_gem_sync_waiter.. the notify fxn gets called back when
1041  * the read and/or write target count is achieved which can call a user
1042  * callback (ex. to kick 3d and/or 2d), wakeup blocked task (prep for
1043  * cpu access), etc.
1044  */
1045 static LIST_HEAD(waiters);
1047 static inline bool is_waiting(struct omap_gem_sync_waiter *waiter)
1049         struct omap_gem_object *omap_obj = waiter->omap_obj;
1050         if ((waiter->op & OMAP_GEM_READ) &&
1051                         (omap_obj->sync->write_complete < waiter->write_target))
1052                 return true;
1053         if ((waiter->op & OMAP_GEM_WRITE) &&
1054                         (omap_obj->sync->read_complete < waiter->read_target))
1055                 return true;
1056         return false;
1059 /* macro for sync debug.. */
1060 #define SYNCDBG 0
1061 #define SYNC(fmt, ...) do { if (SYNCDBG) \
1062                 printk(KERN_ERR "%s:%d: "fmt"\n", \
1063                                 __func__, __LINE__, ##__VA_ARGS__); \
1064         } while (0)
1067 static void sync_op_update(void)
1069         struct omap_gem_sync_waiter *waiter, *n;
1070         list_for_each_entry_safe(waiter, n, &waiters, list) {
1071                 if (!is_waiting(waiter)) {
1072                         list_del(&waiter->list);
1073                         SYNC("notify: %p", waiter);
1074                         waiter->notify(waiter->arg);
1075                         kfree(waiter);
1076                 }
1077         }
1080 static inline int sync_op(struct drm_gem_object *obj,
1081                 enum omap_gem_op op, bool start)
1083         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1084         int ret = 0;
1086         spin_lock(&sync_lock);
1088         if (!omap_obj->sync) {
1089                 omap_obj->sync = kzalloc(sizeof(*omap_obj->sync), GFP_ATOMIC);
1090                 if (!omap_obj->sync) {
1091                         ret = -ENOMEM;
1092                         goto unlock;
1093                 }
1094         }
1096         if (start) {
1097                 if (op & OMAP_GEM_READ)
1098                         omap_obj->sync->read_pending++;
1099                 if (op & OMAP_GEM_WRITE)
1100                         omap_obj->sync->write_pending++;
1101         } else {
1102                 if (op & OMAP_GEM_READ)
1103                         omap_obj->sync->read_complete++;
1104                 if (op & OMAP_GEM_WRITE)
1105                         omap_obj->sync->write_complete++;
1106                 sync_op_update();
1107         }
1109 unlock:
1110         spin_unlock(&sync_lock);
1112         return ret;
1115 /* it is a bit lame to handle updates in this sort of polling way, but
1116  * in case of PVR, the GPU can directly update read/write complete
1117  * values, and not really tell us which ones it updated.. this also
1118  * means that sync_lock is not quite sufficient.  So we'll need to
1119  * do something a bit better when it comes time to add support for
1120  * separate 2d hw..
1121  */
1122 void omap_gem_op_update(void)
1124         spin_lock(&sync_lock);
1125         sync_op_update();
1126         spin_unlock(&sync_lock);
1129 /* mark the start of read and/or write operation */
1130 int omap_gem_op_start(struct drm_gem_object *obj, enum omap_gem_op op)
1132         return sync_op(obj, op, true);
1135 int omap_gem_op_finish(struct drm_gem_object *obj, enum omap_gem_op op)
1137         return sync_op(obj, op, false);
1140 static DECLARE_WAIT_QUEUE_HEAD(sync_event);
1142 static void sync_notify(void *arg)
1144         struct task_struct **waiter_task = arg;
1145         *waiter_task = NULL;
1146         wake_up_all(&sync_event);
1149 int omap_gem_op_sync(struct drm_gem_object *obj, enum omap_gem_op op)
1151         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1152         int ret = 0;
1153         if (omap_obj->sync) {
1154                 struct task_struct *waiter_task = current;
1155                 struct omap_gem_sync_waiter *waiter =
1156                                 kzalloc(sizeof(*waiter), GFP_KERNEL);
1158                 if (!waiter)
1159                         return -ENOMEM;
1161                 waiter->omap_obj = omap_obj;
1162                 waiter->op = op;
1163                 waiter->read_target = omap_obj->sync->read_pending;
1164                 waiter->write_target = omap_obj->sync->write_pending;
1165                 waiter->notify = sync_notify;
1166                 waiter->arg = &waiter_task;
1168                 spin_lock(&sync_lock);
1169                 if (is_waiting(waiter)) {
1170                         SYNC("waited: %p", waiter);
1171                         list_add_tail(&waiter->list, &waiters);
1172                         spin_unlock(&sync_lock);
1173                         ret = wait_event_interruptible(sync_event,
1174                                         (waiter_task == NULL));
1175                         spin_lock(&sync_lock);
1176                         if (waiter_task) {
1177                                 SYNC("interrupted: %p", waiter);
1178                                 /* we were interrupted */
1179                                 list_del(&waiter->list);
1180                                 waiter_task = NULL;
1181                         } else {
1182                                 /* freed in sync_op_update() */
1183                                 waiter = NULL;
1184                         }
1185                 }
1186                 spin_unlock(&sync_lock);
1188                 if (waiter)
1189                         kfree(waiter);
1190         }
1191         return ret;
1194 /* call fxn(arg), either synchronously or asynchronously if the op
1195  * is currently blocked..  fxn() can be called from any context
1196  *
1197  * (TODO for now fxn is called back from whichever context calls
1198  * omap_gem_op_update().. but this could be better defined later
1199  * if needed)
1200  *
1201  * TODO more code in common w/ _sync()..
1202  */
1203 int omap_gem_op_async(struct drm_gem_object *obj, enum omap_gem_op op,
1204                 void (*fxn)(void *arg), void *arg)
1206         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1207         if (omap_obj->sync) {
1208                 struct omap_gem_sync_waiter *waiter =
1209                                 kzalloc(sizeof(*waiter), GFP_ATOMIC);
1211                 if (!waiter)
1212                         return -ENOMEM;
1214                 waiter->omap_obj = omap_obj;
1215                 waiter->op = op;
1216                 waiter->read_target = omap_obj->sync->read_pending;
1217                 waiter->write_target = omap_obj->sync->write_pending;
1218                 waiter->notify = fxn;
1219                 waiter->arg = arg;
1221                 spin_lock(&sync_lock);
1222                 if (is_waiting(waiter)) {
1223                         SYNC("waited: %p", waiter);
1224                         list_add_tail(&waiter->list, &waiters);
1225                         spin_unlock(&sync_lock);
1226                         return 0;
1227                 }
1229                 spin_unlock(&sync_lock);
1231                 kfree(waiter);
1232         }
1234         /* no waiting.. */
1235         fxn(arg);
1237         return 0;
1240 /* special API so PVR can update the buffer to use a sync-object allocated
1241  * from it's sync-obj heap.  Only used for a newly allocated (from PVR's
1242  * perspective) sync-object, so we overwrite the new syncobj w/ values
1243  * from the already allocated syncobj (if there is one)
1244  */
1245 int omap_gem_set_sync_object(struct drm_gem_object *obj, void *syncobj)
1247         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1248         int ret = 0;
1250         spin_lock(&sync_lock);
1252         if ((omap_obj->flags & OMAP_BO_EXT_SYNC) && !syncobj) {
1253                 /* clearing a previously set syncobj */
1254                 syncobj = kmemdup(omap_obj->sync, sizeof(*omap_obj->sync),
1255                                   GFP_ATOMIC);
1256                 if (!syncobj) {
1257                         ret = -ENOMEM;
1258                         goto unlock;
1259                 }
1260                 omap_obj->flags &= ~OMAP_BO_EXT_SYNC;
1261                 omap_obj->sync = syncobj;
1262         } else if (syncobj && !(omap_obj->flags & OMAP_BO_EXT_SYNC)) {
1263                 /* replacing an existing syncobj */
1264                 if (omap_obj->sync) {
1265                         memcpy(syncobj, omap_obj->sync, sizeof(*omap_obj->sync));
1266                         kfree(omap_obj->sync);
1267                 }
1268                 omap_obj->flags |= OMAP_BO_EXT_SYNC;
1269                 omap_obj->sync = syncobj;
1270         }
1272 unlock:
1273         spin_unlock(&sync_lock);
1274         return ret;
1277 /* don't call directly.. called from GEM core when it is time to actually
1278  * free the object..
1279  */
1280 void omap_gem_free_object(struct drm_gem_object *obj)
1282         struct drm_device *dev = obj->dev;
1283         struct omap_drm_private *priv = dev->dev_private;
1284         struct omap_gem_object *omap_obj = to_omap_bo(obj);
1286         evict(obj);
1288         WARN_ON(!mutex_is_locked(&dev->struct_mutex));
1290         spin_lock(&priv->list_lock);
1291         list_del(&omap_obj->mm_list);
1292         spin_unlock(&priv->list_lock);
1294         drm_gem_free_mmap_offset(obj);
1296         /* this means the object is still pinned.. which really should
1297          * not happen.  I think..
1298          */
1299         WARN_ON(omap_obj->paddr_cnt > 0);
1301         /* don't free externally allocated backing memory */
1302         if (!(omap_obj->flags & OMAP_BO_EXT_MEM)) {
1303                 if (omap_obj->pages)
1304                         omap_gem_detach_pages(obj);
1306                 if (!is_shmem(obj)) {
1307                         dma_free_writecombine(dev->dev, obj->size,
1308                                         omap_obj->vaddr, omap_obj->paddr);
1309                 } else if (omap_obj->vaddr) {
1310                         vunmap(omap_obj->vaddr);
1311                 }
1312         }
1314         /* don't free externally allocated syncobj */
1315         if (!(omap_obj->flags & OMAP_BO_EXT_SYNC))
1316                 kfree(omap_obj->sync);
1318         drm_gem_object_release(obj);
1320         kfree(obj);
1323 /* convenience method to construct a GEM buffer object, and userspace handle */
1324 int omap_gem_new_handle(struct drm_device *dev, struct drm_file *file,
1325                 union omap_gem_size gsize, uint32_t flags, uint32_t *handle)
1327         struct drm_gem_object *obj;
1328         int ret;
1330         obj = omap_gem_new(dev, gsize, flags);
1331         if (!obj)
1332                 return -ENOMEM;
1334         ret = drm_gem_handle_create(file, obj, handle);
1335         if (ret) {
1336                 drm_gem_object_release(obj);
1337                 kfree(obj); /* TODO isn't there a dtor to call? just copying i915 */
1338                 return ret;
1339         }
1341         /* drop reference from allocate - handle holds it now */
1342         drm_gem_object_unreference_unlocked(obj);
1344         return 0;
1347 /* GEM buffer object constructor */
1348 struct drm_gem_object *omap_gem_new(struct drm_device *dev,
1349                 union omap_gem_size gsize, uint32_t flags)
1351         struct omap_drm_private *priv = dev->dev_private;
1352         struct omap_gem_object *omap_obj;
1353         struct drm_gem_object *obj = NULL;
1354         size_t size;
1355         int ret;
1357         if (flags & OMAP_BO_TILED) {
1358                 if (!usergart) {
1359                         dev_err(dev->dev, "Tiled buffers require DMM\n");
1360                         goto fail;
1361                 }
1363                 /* tiled buffers are always shmem paged backed.. when they are
1364                  * scanned out, they are remapped into DMM/TILER
1365                  */
1366                 flags &= ~OMAP_BO_SCANOUT;
1368                 /* currently don't allow cached buffers.. there is some caching
1369                  * stuff that needs to be handled better
1370                  */
1371                 flags &= ~(OMAP_BO_CACHED|OMAP_BO_WC|OMAP_BO_UNCACHED);
1372                 flags |= tiler_get_cpu_cache_flags();
1374                 /* align dimensions to slot boundaries... */
1375                 tiler_align(gem2fmt(flags),
1376                                 &gsize.tiled.width, &gsize.tiled.height);
1378                 /* ...and calculate size based on aligned dimensions */
1379                 size = tiler_size(gem2fmt(flags),
1380                                 gsize.tiled.width, gsize.tiled.height);
1381         } else {
1382                 size = PAGE_ALIGN(gsize.bytes);
1383         }
1385         omap_obj = kzalloc(sizeof(*omap_obj), GFP_KERNEL);
1386         if (!omap_obj)
1387                 goto fail;
1389         spin_lock(&priv->list_lock);
1390         list_add(&omap_obj->mm_list, &priv->obj_list);
1391         spin_unlock(&priv->list_lock);
1393         obj = &omap_obj->base;
1395         if ((flags & OMAP_BO_SCANOUT) && !priv->has_dmm) {
1396                 /* attempt to allocate contiguous memory if we don't
1397                  * have DMM for remappign discontiguous buffers
1398                  */
1399                 omap_obj->vaddr =  dma_alloc_writecombine(dev->dev, size,
1400                                 &omap_obj->paddr, GFP_KERNEL);
1401                 if (!omap_obj->vaddr) {
1402                         spin_lock(&priv->list_lock);
1403                         list_del(&omap_obj->mm_list);
1404                         spin_unlock(&priv->list_lock);
1406                         kfree(omap_obj);
1408                         return NULL;
1409                 }
1411                 flags |= OMAP_BO_DMA;
1412         }
1414         omap_obj->flags = flags;
1416         if (flags & OMAP_BO_TILED) {
1417                 omap_obj->width = gsize.tiled.width;
1418                 omap_obj->height = gsize.tiled.height;
1419         }
1421         ret = 0;
1422         if (flags & (OMAP_BO_DMA|OMAP_BO_EXT_MEM))
1423                 drm_gem_private_object_init(dev, obj, size);
1424         else
1425                 ret = drm_gem_object_init(dev, obj, size);
1427         if (ret)
1428                 goto fail;
1430         return obj;
1432 fail:
1433         if (obj)
1434                 omap_gem_free_object(obj);
1436         return NULL;
1439 /* init/cleanup.. if DMM is used, we need to set some stuff up.. */
1440 void omap_gem_init(struct drm_device *dev)
1442         struct omap_drm_private *priv = dev->dev_private;
1443         const enum tiler_fmt fmts[] = {
1444                         TILFMT_8BIT, TILFMT_16BIT, TILFMT_32BIT
1445         };
1446         int i, j;
1448         if (!dmm_is_available()) {
1449                 /* DMM only supported on OMAP4 and later, so this isn't fatal */
1450                 dev_warn(dev->dev, "DMM not available, disable DMM support\n");
1451                 return;
1452         }
1454         usergart = kcalloc(3, sizeof(*usergart), GFP_KERNEL);
1455         if (!usergart)
1456                 return;
1458         /* reserve 4k aligned/wide regions for userspace mappings: */
1459         for (i = 0; i < ARRAY_SIZE(fmts); i++) {
1460                 uint16_t h = 1, w = PAGE_SIZE >> i;
1461                 tiler_align(fmts[i], &w, &h);
1462                 /* note: since each region is 1 4kb page wide, and minimum
1463                  * number of rows, the height ends up being the same as the
1464                  * # of pages in the region
1465                  */
1466                 usergart[i].height = h;
1467                 usergart[i].height_shift = ilog2(h);
1468                 usergart[i].stride_pfn = tiler_stride(fmts[i], 0) >> PAGE_SHIFT;
1469                 usergart[i].slot_shift = ilog2((PAGE_SIZE / h) >> i);
1470                 for (j = 0; j < NUM_USERGART_ENTRIES; j++) {
1471                         struct usergart_entry *entry = &usergart[i].entry[j];
1472                         struct tiler_block *block =
1473                                         tiler_reserve_2d(fmts[i], w, h,
1474                                                         PAGE_SIZE);
1475                         if (IS_ERR(block)) {
1476                                 dev_err(dev->dev,
1477                                                 "reserve failed: %d, %d, %ld\n",
1478                                                 i, j, PTR_ERR(block));
1479                                 return;
1480                         }
1481                         entry->paddr = tiler_ssptr(block);
1482                         entry->block = block;
1484                         DBG("%d:%d: %dx%d: paddr=%pad stride=%d", i, j, w, h,
1485                                         &entry->paddr,
1486                                         usergart[i].stride_pfn << PAGE_SHIFT);
1487                 }
1488         }
1490         priv->has_dmm = true;
1493 void omap_gem_deinit(struct drm_device *dev)
1495         /* I believe we can rely on there being no more outstanding GEM
1496          * objects which could depend on usergart/dmm at this point.
1497          */
1498         kfree(usergart);