1 /*
2 * drivers/gpu/drm/omapdrm/omap_irq.c
3 *
4 * Copyright (C) 2012 Texas Instruments
5 * Author: Rob Clark <rob.clark@linaro.org>
6 *
7 * This program is free software; you can redistribute it and/or modify it
8 * under the terms of the GNU General Public License version 2 as published by
9 * the Free Software Foundation.
10 *
11 * This program is distributed in the hope that it will be useful, but WITHOUT
12 * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
13 * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for
14 * more details.
15 *
16 * You should have received a copy of the GNU General Public License along with
17 * this program. If not, see <http://www.gnu.org/licenses/>.
18 */
20 #include "omap_drv.h"
22 static DEFINE_SPINLOCK(list_lock);
24 static void omap_irq_error_handler(struct omap_drm_irq *irq,
25 uint32_t irqstatus)
26 {
27 DRM_ERROR("errors: %08x\n", irqstatus);
28 }
30 /* call with list_lock and dispc runtime held */
31 static void omap_irq_update(struct drm_device *dev)
32 {
33 struct omap_drm_private *priv = dev->dev_private;
34 struct omap_drm_irq *irq;
35 uint32_t irqmask = priv->vblank_mask;
37 BUG_ON(!spin_is_locked(&list_lock));
39 list_for_each_entry(irq, &priv->irq_list, node)
40 irqmask |= irq->irqmask;
42 DBG("irqmask=%08x", irqmask);
44 dispc_write_irqenable(irqmask);
45 dispc_read_irqenable(); /* flush posted write */
46 }
48 void omap_irq_register(struct drm_device *dev, struct omap_drm_irq *irq)
49 {
50 struct omap_drm_private *priv = dev->dev_private;
51 unsigned long flags;
53 dispc_runtime_get();
54 spin_lock_irqsave(&list_lock, flags);
56 if (!WARN_ON(irq->registered)) {
57 irq->registered = true;
58 list_add(&irq->node, &priv->irq_list);
59 omap_irq_update(dev);
60 }
62 spin_unlock_irqrestore(&list_lock, flags);
63 dispc_runtime_put();
64 }
66 void omap_irq_unregister(struct drm_device *dev, struct omap_drm_irq *irq)
67 {
68 unsigned long flags;
70 dispc_runtime_get();
71 spin_lock_irqsave(&list_lock, flags);
73 if (!WARN_ON(!irq->registered)) {
74 irq->registered = false;
75 list_del(&irq->node);
76 omap_irq_update(dev);
77 }
79 spin_unlock_irqrestore(&list_lock, flags);
80 dispc_runtime_put();
81 }
83 struct omap_irq_wait {
84 struct omap_drm_irq irq;
85 int count;
86 };
88 static DECLARE_WAIT_QUEUE_HEAD(wait_event);
90 static void wait_irq(struct omap_drm_irq *irq, uint32_t irqstatus)
91 {
92 struct omap_irq_wait *wait =
93 container_of(irq, struct omap_irq_wait, irq);
94 wait->count--;
95 wake_up_all(&wait_event);
96 }
98 struct omap_irq_wait * omap_irq_wait_init(struct drm_device *dev,
99 uint32_t irqmask, int count)
100 {
101 struct omap_irq_wait *wait = kzalloc(sizeof(*wait), GFP_KERNEL);
102 wait->irq.irq = wait_irq;
103 wait->irq.irqmask = irqmask;
104 wait->count = count;
105 omap_irq_register(dev, &wait->irq);
106 return wait;
107 }
109 int omap_irq_wait(struct drm_device *dev, struct omap_irq_wait *wait,
110 unsigned long timeout)
111 {
112 int ret = wait_event_timeout(wait_event, (wait->count <= 0), timeout);
113 omap_irq_unregister(dev, &wait->irq);
114 kfree(wait);
115 if (ret == 0)
116 return -1;
117 return 0;
118 }
120 /**
121 * enable_vblank - enable vblank interrupt events
122 * @dev: DRM device
123 * @crtc: which irq to enable
124 *
125 * Enable vblank interrupts for @crtc. If the device doesn't have
126 * a hardware vblank counter, this routine should be a no-op, since
127 * interrupts will have to stay on to keep the count accurate.
128 *
129 * RETURNS
130 * Zero on success, appropriate errno if the given @crtc's vblank
131 * interrupt cannot be enabled.
132 */
133 int omap_irq_enable_vblank(struct drm_device *dev, int crtc_id)
134 {
135 struct omap_drm_private *priv = dev->dev_private;
136 struct drm_crtc *crtc = priv->crtcs[crtc_id];
137 unsigned long flags;
139 DBG("dev=%p, crtc=%d", dev, crtc_id);
141 dispc_runtime_get();
142 spin_lock_irqsave(&list_lock, flags);
143 priv->vblank_mask |= pipe2vbl(crtc);
144 omap_irq_update(dev);
145 spin_unlock_irqrestore(&list_lock, flags);
146 dispc_runtime_put();
148 return 0;
149 }
151 /**
152 * disable_vblank - disable vblank interrupt events
153 * @dev: DRM device
154 * @crtc: which irq to enable
155 *
156 * Disable vblank interrupts for @crtc. If the device doesn't have
157 * a hardware vblank counter, this routine should be a no-op, since
158 * interrupts will have to stay on to keep the count accurate.
159 */
160 void omap_irq_disable_vblank(struct drm_device *dev, int crtc_id)
161 {
162 struct omap_drm_private *priv = dev->dev_private;
163 struct drm_crtc *crtc = priv->crtcs[crtc_id];
164 unsigned long flags;
166 DBG("dev=%p, crtc=%d", dev, crtc_id);
168 dispc_runtime_get();
169 spin_lock_irqsave(&list_lock, flags);
170 priv->vblank_mask &= ~pipe2vbl(crtc);
171 omap_irq_update(dev);
172 spin_unlock_irqrestore(&list_lock, flags);
173 dispc_runtime_put();
174 }
176 irqreturn_t omap_irq_handler(DRM_IRQ_ARGS)
177 {
178 struct drm_device *dev = (struct drm_device *) arg;
179 struct omap_drm_private *priv = dev->dev_private;
180 struct omap_drm_irq *handler, *n;
181 unsigned long flags;
182 unsigned int id;
183 u32 irqstatus;
185 irqstatus = dispc_read_irqstatus();
186 dispc_clear_irqstatus(irqstatus);
187 dispc_read_irqstatus(); /* flush posted write */
189 VERB("irqs: %08x", irqstatus);
191 for (id = 0; id < priv->num_crtcs; id++) {
192 struct drm_crtc *crtc = priv->crtcs[id];
194 if (irqstatus & pipe2vbl(crtc))
195 drm_handle_vblank(dev, id);
196 }
198 spin_lock_irqsave(&list_lock, flags);
199 list_for_each_entry_safe(handler, n, &priv->irq_list, node) {
200 if (handler->irqmask & irqstatus) {
201 spin_unlock_irqrestore(&list_lock, flags);
202 handler->irq(handler, handler->irqmask & irqstatus);
203 spin_lock_irqsave(&list_lock, flags);
204 }
205 }
206 spin_unlock_irqrestore(&list_lock, flags);
208 return IRQ_HANDLED;
209 }
211 void omap_irq_preinstall(struct drm_device *dev)
212 {
213 DBG("dev=%p", dev);
214 dispc_runtime_get();
215 dispc_clear_irqstatus(0xffffffff);
216 dispc_runtime_put();
217 }
219 int omap_irq_postinstall(struct drm_device *dev)
220 {
221 struct omap_drm_private *priv = dev->dev_private;
222 struct omap_drm_irq *error_handler = &priv->error_handler;
224 DBG("dev=%p", dev);
226 INIT_LIST_HEAD(&priv->irq_list);
228 error_handler->irq = omap_irq_error_handler;
229 error_handler->irqmask = DISPC_IRQ_OCP_ERR;
231 /* for now ignore DISPC_IRQ_SYNC_LOST_DIGIT.. really I think
232 * we just need to ignore it while enabling tv-out
233 */
234 error_handler->irqmask &= ~DISPC_IRQ_SYNC_LOST_DIGIT;
236 omap_irq_register(dev, error_handler);
238 return 0;
239 }
241 void omap_irq_uninstall(struct drm_device *dev)
242 {
243 DBG("dev=%p", dev);
244 // TODO prolly need to call drm_irq_uninstall() somewhere too
245 }
247 /*
248 * We need a special version, instead of just using drm_irq_install(),
249 * because we need to register the irq via omapdss. Once omapdss and
250 * omapdrm are merged together we can assign the dispc hwmod data to
251 * ourselves and drop these and just use drm_irq_{install,uninstall}()
252 */
254 int omap_drm_irq_install(struct drm_device *dev)
255 {
256 int ret;
258 mutex_lock(&dev->struct_mutex);
260 if (dev->irq_enabled) {
261 mutex_unlock(&dev->struct_mutex);
262 return -EBUSY;
263 }
264 dev->irq_enabled = 1;
265 mutex_unlock(&dev->struct_mutex);
267 /* Before installing handler */
268 if (dev->driver->irq_preinstall)
269 dev->driver->irq_preinstall(dev);
271 ret = dispc_request_irq(dev->driver->irq_handler, dev);
273 if (ret < 0) {
274 mutex_lock(&dev->struct_mutex);
275 dev->irq_enabled = 0;
276 mutex_unlock(&dev->struct_mutex);
277 return ret;
278 }
280 /* After installing handler */
281 if (dev->driver->irq_postinstall)
282 ret = dev->driver->irq_postinstall(dev);
284 if (ret < 0) {
285 mutex_lock(&dev->struct_mutex);
286 dev->irq_enabled = 0;
287 mutex_unlock(&dev->struct_mutex);
288 dispc_free_irq(dev);
289 }
291 return ret;
292 }
294 int omap_drm_irq_uninstall(struct drm_device *dev)
295 {
296 unsigned long irqflags;
297 int irq_enabled, i;
299 mutex_lock(&dev->struct_mutex);
300 irq_enabled = dev->irq_enabled;
301 dev->irq_enabled = 0;
302 mutex_unlock(&dev->struct_mutex);
304 /*
305 * Wake up any waiters so they don't hang.
306 */
307 if (dev->num_crtcs) {
308 spin_lock_irqsave(&dev->vbl_lock, irqflags);
309 for (i = 0; i < dev->num_crtcs; i++) {
310 DRM_WAKEUP(&dev->vbl_queue[i]);
311 dev->vblank_enabled[i] = 0;
312 dev->last_vblank[i] =
313 dev->driver->get_vblank_counter(dev, i);
314 }
315 spin_unlock_irqrestore(&dev->vbl_lock, irqflags);
316 }
318 if (!irq_enabled)
319 return -EINVAL;
321 if (dev->driver->irq_uninstall)
322 dev->driver->irq_uninstall(dev);
324 dispc_free_irq(dev);
326 return 0;
327 }