]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - drivers/ide/delkin_cb.c
Merge branch 'drm-nouveau-fixes-3.8' of git://anongit.freedesktop.org/git/nouveau...
[android-sdk/kernel-video.git] / drivers / ide / delkin_cb.c
1 /*
2  *  Created 20 Oct 2004 by Mark Lord
3  *
4  *  Basic support for Delkin/ASKA/Workbit Cardbus CompactFlash adapter
5  *
6  *  Modeled after the 16-bit PCMCIA driver: ide-cs.c
7  *
8  *  This is slightly peculiar, in that it is a PCI driver,
9  *  but is NOT an IDE PCI driver -- the IDE layer does not directly
10  *  support hot insertion/removal of PCI interfaces, so this driver
11  *  is unable to use the IDE PCI interfaces.  Instead, it uses the
12  *  same interfaces as the ide-cs (PCMCIA) driver uses.
13  *  On the plus side, the driver is also smaller/simpler this way.
14  *
15  *  This file is subject to the terms and conditions of the GNU General Public
16  *  License.  See the file COPYING in the main directory of this archive for
17  *  more details.
18  */
20 #include <linux/types.h>
21 #include <linux/module.h>
22 #include <linux/ide.h>
23 #include <linux/init.h>
24 #include <linux/pci.h>
26 #include <asm/io.h>
28 /*
29  * No chip documentation has yet been found,
30  * so these configuration values were pulled from
31  * a running Win98 system using "debug".
32  * This gives around 3MByte/second read performance,
33  * which is about 2/3 of what the chip is capable of.
34  *
35  * There is also a 4KByte mmio region on the card,
36  * but its purpose has yet to be reverse-engineered.
37  */
38 static const u8 setup[] = {
39         0x00, 0x05, 0xbe, 0x01, 0x20, 0x8f, 0x00, 0x00,
40         0xa4, 0x1f, 0xb3, 0x1b, 0x00, 0x00, 0x00, 0x80,
41         0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
42         0x00, 0x00, 0x00, 0x00, 0xa4, 0x83, 0x02, 0x13,
43 };
45 static const struct ide_port_ops delkin_cb_port_ops = {
46         .quirkproc              = ide_undecoded_slave,
47 };
49 static int delkin_cb_init_chipset(struct pci_dev *dev)
50 {
51         unsigned long base = pci_resource_start(dev, 0);
52         int i;
54         outb(0x02, base + 0x1e);        /* set nIEN to block interrupts */
55         inb(base + 0x17);               /* read status to clear interrupts */
57         for (i = 0; i < sizeof(setup); ++i) {
58                 if (setup[i])
59                         outb(setup[i], base + i);
60         }
62         return 0;
63 }
65 static const struct ide_port_info delkin_cb_port_info = {
66         .port_ops               = &delkin_cb_port_ops,
67         .host_flags             = IDE_HFLAG_IO_32BIT | IDE_HFLAG_UNMASK_IRQS |
68                                   IDE_HFLAG_NO_DMA,
69         .irq_flags              = IRQF_SHARED,
70         .init_chipset           = delkin_cb_init_chipset,
71         .chipset                = ide_pci,
72 };
74 static int delkin_cb_probe(struct pci_dev *dev, const struct pci_device_id *id)
75 {
76         struct ide_host *host;
77         unsigned long base;
78         int rc;
79         struct ide_hw hw, *hws[] = { &hw };
81         rc = pci_enable_device(dev);
82         if (rc) {
83                 printk(KERN_ERR "delkin_cb: pci_enable_device failed (%d)\n", rc);
84                 return rc;
85         }
86         rc = pci_request_regions(dev, "delkin_cb");
87         if (rc) {
88                 printk(KERN_ERR "delkin_cb: pci_request_regions failed (%d)\n", rc);
89                 pci_disable_device(dev);
90                 return rc;
91         }
92         base = pci_resource_start(dev, 0);
94         delkin_cb_init_chipset(dev);
96         memset(&hw, 0, sizeof(hw));
97         ide_std_init_ports(&hw, base + 0x10, base + 0x1e);
98         hw.irq = dev->irq;
99         hw.dev = &dev->dev;
101         rc = ide_host_add(&delkin_cb_port_info, hws, 1, &host);
102         if (rc)
103                 goto out_disable;
105         pci_set_drvdata(dev, host);
107         return 0;
109 out_disable:
110         pci_release_regions(dev);
111         pci_disable_device(dev);
112         return rc;
115 static void
116 delkin_cb_remove (struct pci_dev *dev)
118         struct ide_host *host = pci_get_drvdata(dev);
120         ide_host_remove(host);
122         pci_release_regions(dev);
123         pci_disable_device(dev);
126 #ifdef CONFIG_PM
127 static int delkin_cb_suspend(struct pci_dev *dev, pm_message_t state)
129         pci_save_state(dev);
130         pci_disable_device(dev);
131         pci_set_power_state(dev, pci_choose_state(dev, state));
133         return 0;
136 static int delkin_cb_resume(struct pci_dev *dev)
138         struct ide_host *host = pci_get_drvdata(dev);
139         int rc;
141         pci_set_power_state(dev, PCI_D0);
143         rc = pci_enable_device(dev);
144         if (rc)
145                 return rc;
147         pci_restore_state(dev);
148         pci_set_master(dev);
150         if (host->init_chipset)
151                 host->init_chipset(dev);
153         return 0;
155 #else
156 #define delkin_cb_suspend NULL
157 #define delkin_cb_resume NULL
158 #endif
160 static struct pci_device_id delkin_cb_pci_tbl[] = {
161         { 0x1145, 0xf021, PCI_ANY_ID, PCI_ANY_ID, 0, 0, 0},
162         { 0x1145, 0xf024, PCI_ANY_ID, PCI_ANY_ID, 0, 0, 0},
163         { 0, },
164 };
165 MODULE_DEVICE_TABLE(pci, delkin_cb_pci_tbl);
167 static struct pci_driver delkin_cb_pci_driver = {
168         .name           = "Delkin-ASKA-Workbit Cardbus IDE",
169         .id_table       = delkin_cb_pci_tbl,
170         .probe          = delkin_cb_probe,
171         .remove         = delkin_cb_remove,
172         .suspend        = delkin_cb_suspend,
173         .resume         = delkin_cb_resume,
174 };
176 static int __init delkin_cb_init(void)
178         return pci_register_driver(&delkin_cb_pci_driver);
181 static void __exit delkin_cb_exit(void)
183         pci_unregister_driver(&delkin_cb_pci_driver);
186 module_init(delkin_cb_init);
187 module_exit(delkin_cb_exit);
189 MODULE_AUTHOR("Mark Lord");
190 MODULE_DESCRIPTION("Basic support for Delkin/ASKA/Workbit Cardbus IDE");
191 MODULE_LICENSE("GPL");