]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - drivers/isdn/hysdn/hysdn_init.c
Merge branch 'drm-nouveau-fixes-3.8' of git://anongit.freedesktop.org/git/nouveau...
[android-sdk/kernel-video.git] / drivers / isdn / hysdn / hysdn_init.c
1 /* $Id: hysdn_init.c,v 1.6.6.6 2001/09/23 22:24:54 kai Exp $
2  *
3  * Linux driver for HYSDN cards, init functions.
4  *
5  * Author    Werner Cornelius (werner@titro.de) for Hypercope GmbH
6  * Copyright 1999 by Werner Cornelius (werner@titro.de)
7  *
8  * This software may be used and distributed according to the terms
9  * of the GNU General Public License, incorporated herein by reference.
10  *
11  */
13 #include <linux/module.h>
14 #include <linux/init.h>
15 #include <linux/poll.h>
16 #include <linux/vmalloc.h>
17 #include <linux/slab.h>
18 #include <linux/pci.h>
20 #include "hysdn_defs.h"
22 static struct pci_device_id hysdn_pci_tbl[] = {
23         { PCI_VENDOR_ID_HYPERCOPE, PCI_DEVICE_ID_HYPERCOPE_PLX,
24           PCI_ANY_ID, PCI_SUBDEVICE_ID_HYPERCOPE_METRO, 0, 0, BD_METRO },
25         { PCI_VENDOR_ID_HYPERCOPE, PCI_DEVICE_ID_HYPERCOPE_PLX,
26           PCI_ANY_ID, PCI_SUBDEVICE_ID_HYPERCOPE_CHAMP2, 0, 0, BD_CHAMP2 },
27         { PCI_VENDOR_ID_HYPERCOPE, PCI_DEVICE_ID_HYPERCOPE_PLX,
28           PCI_ANY_ID, PCI_SUBDEVICE_ID_HYPERCOPE_ERGO, 0, 0, BD_ERGO },
29         { PCI_VENDOR_ID_HYPERCOPE, PCI_DEVICE_ID_HYPERCOPE_PLX,
30           PCI_ANY_ID, PCI_SUBDEVICE_ID_HYPERCOPE_OLD_ERGO, 0, 0, BD_ERGO },
32         { }                             /* Terminating entry */
33 };
34 MODULE_DEVICE_TABLE(pci, hysdn_pci_tbl);
35 MODULE_DESCRIPTION("ISDN4Linux: Driver for HYSDN cards");
36 MODULE_AUTHOR("Werner Cornelius");
37 MODULE_LICENSE("GPL");
39 static int cardmax;             /* number of found cards */
40 hysdn_card *card_root = NULL;   /* pointer to first card */
41 static hysdn_card *card_last = NULL;    /* pointer to first card */
44 /****************************************************************************/
45 /* The module startup and shutdown code. Only compiled when used as module. */
46 /* Using the driver as module is always advisable, because the booting      */
47 /* image becomes smaller and the driver code is only loaded when needed.    */
48 /* Additionally newer versions may be activated without rebooting.          */
49 /****************************************************************************/
51 /****************************************************************************/
52 /* init_module is called once when the module is loaded to do all necessary */
53 /* things like autodetect...                                                */
54 /* If the return value of this function is 0 the init has been successful   */
55 /* and the module is added to the list in /proc/modules, otherwise an error */
56 /* is assumed and the module will not be kept in memory.                    */
57 /****************************************************************************/
59 static int hysdn_pci_init_one(struct pci_dev *akt_pcidev,
60                               const struct pci_device_id *ent)
61 {
62         hysdn_card *card;
63         int rc;
65         rc = pci_enable_device(akt_pcidev);
66         if (rc)
67                 return rc;
69         if (!(card = kzalloc(sizeof(hysdn_card), GFP_KERNEL))) {
70                 printk(KERN_ERR "HYSDN: unable to alloc device mem \n");
71                 rc = -ENOMEM;
72                 goto err_out;
73         }
74         card->myid = cardmax;   /* set own id */
75         card->bus = akt_pcidev->bus->number;
76         card->devfn = akt_pcidev->devfn;        /* slot + function */
77         card->subsysid = akt_pcidev->subsystem_device;
78         card->irq = akt_pcidev->irq;
79         card->iobase = pci_resource_start(akt_pcidev, PCI_REG_PLX_IO_BASE);
80         card->plxbase = pci_resource_start(akt_pcidev, PCI_REG_PLX_MEM_BASE);
81         card->membase = pci_resource_start(akt_pcidev, PCI_REG_MEMORY_BASE);
82         card->brdtype = BD_NONE;        /* unknown */
83         card->debug_flags = DEF_DEB_FLAGS;      /* set default debug */
84         card->faxchans = 0;     /* default no fax channels */
85         card->bchans = 2;       /* and 2 b-channels */
86         card->brdtype = ent->driver_data;
88         if (ergo_inithardware(card)) {
89                 printk(KERN_WARNING "HYSDN: card at io 0x%04x already in use\n", card->iobase);
90                 rc = -EBUSY;
91                 goto err_out_card;
92         }
94         cardmax++;
95         card->next = NULL;      /*end of chain */
96         if (card_last)
97                 card_last->next = card;         /* pointer to next card */
98         else
99                 card_root = card;
100         card_last = card;       /* new chain end */
102         pci_set_drvdata(akt_pcidev, card);
103         return 0;
105 err_out_card:
106         kfree(card);
107 err_out:
108         pci_disable_device(akt_pcidev);
109         return rc;
112 static void hysdn_pci_remove_one(struct pci_dev *akt_pcidev)
114         hysdn_card *card = pci_get_drvdata(akt_pcidev);
116         pci_set_drvdata(akt_pcidev, NULL);
118         if (card->stopcard)
119                 card->stopcard(card);
121 #ifdef CONFIG_HYSDN_CAPI
122         hycapi_capi_release(card);
123 #endif
125         if (card->releasehardware)
126                 card->releasehardware(card);   /* free all hardware resources */
128         if (card == card_root) {
129                 card_root = card_root->next;
130                 if (!card_root)
131                         card_last = NULL;
132         } else {
133                 hysdn_card *tmp = card_root;
134                 while (tmp) {
135                         if (tmp->next == card)
136                                 tmp->next = card->next;
137                         card_last = tmp;
138                         tmp = tmp->next;
139                 }
140         }
142         kfree(card);
143         pci_disable_device(akt_pcidev);
146 static struct pci_driver hysdn_pci_driver = {
147         .name           = "hysdn",
148         .id_table       = hysdn_pci_tbl,
149         .probe          = hysdn_pci_init_one,
150         .remove         = hysdn_pci_remove_one,
151 };
153 static int hysdn_have_procfs;
155 static int __init
156 hysdn_init(void)
158         int rc;
160         printk(KERN_NOTICE "HYSDN: module loaded\n");
162         rc = pci_register_driver(&hysdn_pci_driver);
163         if (rc)
164                 return rc;
166         printk(KERN_INFO "HYSDN: %d card(s) found.\n", cardmax);
168         if (!hysdn_procconf_init())
169                 hysdn_have_procfs = 1;
171 #ifdef CONFIG_HYSDN_CAPI
172         if (cardmax > 0) {
173                 if (hycapi_init()) {
174                         printk(KERN_ERR "HYCAPI: init failed\n");
176                         if (hysdn_have_procfs)
177                                 hysdn_procconf_release();
179                         pci_unregister_driver(&hysdn_pci_driver);
180                         return -ESPIPE;
181                 }
182         }
183 #endif /* CONFIG_HYSDN_CAPI */
185         return 0;               /* no error */
186 }                               /* init_module */
189 /***********************************************************************/
190 /* cleanup_module is called when the module is released by the kernel. */
191 /* The routine is only called if init_module has been successful and   */
192 /* the module counter has a value of 0. Otherwise this function will   */
193 /* not be called. This function must release all resources still allo- */
194 /* cated as after the return from this function the module code will   */
195 /* be removed from memory.                                             */
196 /***********************************************************************/
197 static void __exit
198 hysdn_exit(void)
200         if (hysdn_have_procfs)
201                 hysdn_procconf_release();
203         pci_unregister_driver(&hysdn_pci_driver);
205 #ifdef CONFIG_HYSDN_CAPI
206         hycapi_cleanup();
207 #endif /* CONFIG_HYSDN_CAPI */
209         printk(KERN_NOTICE "HYSDN: module unloaded\n");
210 }                               /* cleanup_module */
212 module_init(hysdn_init);
213 module_exit(hysdn_exit);