1 #
2 # Misc strange devices
3 #
5 menu "Misc devices"
7 config SENSORS_LIS3LV02D
8 tristate
9 depends on INPUT
10 select INPUT_POLLDEV
11 default n
13 config AD525X_DPOT
14 tristate "Analog Devices Digital Potentiometers"
15 depends on (I2C || SPI) && SYSFS
16 help
17 If you say yes here, you get support for the Analog Devices
18 AD5258, AD5259, AD5251, AD5252, AD5253, AD5254, AD5255
19 AD5160, AD5161, AD5162, AD5165, AD5200, AD5201, AD5203,
20 AD5204, AD5206, AD5207, AD5231, AD5232, AD5233, AD5235,
21 AD5260, AD5262, AD5263, AD5290, AD5291, AD5292, AD5293,
22 AD7376, AD8400, AD8402, AD8403, ADN2850, AD5241, AD5242,
23 AD5243, AD5245, AD5246, AD5247, AD5248, AD5280, AD5282,
24 ADN2860, AD5273, AD5171, AD5170, AD5172, AD5173, AD5270,
25 AD5271, AD5272, AD5274
26 digital potentiometer chips.
28 See Documentation/misc-devices/ad525x_dpot.txt for the
29 userspace interface.
31 This driver can also be built as a module. If so, the module
32 will be called ad525x_dpot.
34 config AD525X_DPOT_I2C
35 tristate "support I2C bus connection"
36 depends on AD525X_DPOT && I2C
37 help
38 Say Y here if you have a digital potentiometers hooked to an I2C bus.
40 To compile this driver as a module, choose M here: the
41 module will be called ad525x_dpot-i2c.
43 config AD525X_DPOT_SPI
44 tristate "support SPI bus connection"
45 depends on AD525X_DPOT && SPI_MASTER
46 help
47 Say Y here if you have a digital potentiometers hooked to an SPI bus.
49 If unsure, say N (but it's safe to say "Y").
51 To compile this driver as a module, choose M here: the
52 module will be called ad525x_dpot-spi.
54 config ATMEL_PWM
55 tristate "Atmel AT32/AT91 PWM support"
56 depends on HAVE_CLK
57 help
58 This option enables device driver support for the PWM channels
59 on certain Atmel processors. Pulse Width Modulation is used for
60 purposes including software controlled power-efficient backlights
61 on LCD displays, motor control, and waveform generation.
63 config ATMEL_TCLIB
64 bool "Atmel AT32/AT91 Timer/Counter Library"
65 depends on (AVR32 || ARCH_AT91)
66 help
67 Select this if you want a library to allocate the Timer/Counter
68 blocks found on many Atmel processors. This facilitates using
69 these blocks by different drivers despite processor differences.
71 config ATMEL_TCB_CLKSRC
72 bool "TC Block Clocksource"
73 depends on ATMEL_TCLIB
74 default y
75 help
76 Select this to get a high precision clocksource based on a
77 TC block with a 5+ MHz base clock rate. Two timer channels
78 are combined to make a single 32-bit timer.
80 When GENERIC_CLOCKEVENTS is defined, the third timer channel
81 may be used as a clock event device supporting oneshot mode
82 (delays of up to two seconds) based on the 32 KiHz clock.
84 config ATMEL_TCB_CLKSRC_BLOCK
85 int
86 depends on ATMEL_TCB_CLKSRC
87 prompt "TC Block" if ARCH_AT91RM9200 || ARCH_AT91SAM9260 || CPU_AT32AP700X
88 default 0
89 range 0 1
90 help
91 Some chips provide more than one TC block, so you have the
92 choice of which one to use for the clock framework. The other
93 TC can be used for other purposes, such as PWM generation and
94 interval timing.
96 config DUMMY_IRQ
97 tristate "Dummy IRQ handler"
98 default n
99 ---help---
100 This module accepts a single 'irq' parameter, which it should register for.
101 The sole purpose of this module is to help with debugging of systems on
102 which spurious IRQs would happen on disabled IRQ vector.
104 config IBM_ASM
105 tristate "Device driver for IBM RSA service processor"
106 depends on X86 && PCI && INPUT
107 ---help---
108 This option enables device driver support for in-band access to the
109 IBM RSA (Condor) service processor in eServer xSeries systems.
110 The ibmasm device driver allows user space application to access
111 ASM (Advanced Systems Management) functions on the service
112 processor. The driver is meant to be used in conjunction with
113 a user space API.
114 The ibmasm driver also enables the OS to use the UART on the
115 service processor board as a regular serial port. To make use of
116 this feature serial driver support (CONFIG_SERIAL_8250) must be
117 enabled.
119 WARNING: This software may not be supported or function
120 correctly on your IBM server. Please consult the IBM ServerProven
121 website <http://www-03.ibm.com/systems/info/x86servers/serverproven/compat/us/>
122 for information on the specific driver level and support statement
123 for your IBM server.
125 config PHANTOM
126 tristate "Sensable PHANToM (PCI)"
127 depends on PCI
128 help
129 Say Y here if you want to build a driver for Sensable PHANToM device.
131 This driver is only for PCI PHANToMs.
133 If you choose to build module, its name will be phantom. If unsure,
134 say N here.
136 config INTEL_MID_PTI
137 tristate "Parallel Trace Interface for MIPI P1149.7 cJTAG standard"
138 depends on PCI && TTY && (X86_INTEL_MID || COMPILE_TEST)
139 default n
140 help
141 The PTI (Parallel Trace Interface) driver directs
142 trace data routed from various parts in the system out
143 through an Intel Penwell PTI port and out of the mobile
144 device for analysis with a debugging tool (Lauterbach or Fido).
146 You should select this driver if the target kernel is meant for
147 an Intel Atom (non-netbook) mobile device containing a MIPI
148 P1149.7 standard implementation.
150 config SGI_IOC4
151 tristate "SGI IOC4 Base IO support"
152 depends on PCI
153 ---help---
154 This option enables basic support for the IOC4 chip on certain
155 SGI IO controller cards (IO9, IO10, and PCI-RT). This option
156 does not enable any specific functions on such a card, but provides
157 necessary infrastructure for other drivers to utilize.
159 If you have an SGI Altix with an IOC4-based card say Y.
160 Otherwise say N.
162 config TIFM_CORE
163 tristate "TI Flash Media interface support"
164 depends on PCI
165 help
166 If you want support for Texas Instruments(R) Flash Media adapters
167 you should select this option and then also choose an appropriate
168 host adapter, such as 'TI Flash Media PCI74xx/PCI76xx host adapter
169 support', if you have a TI PCI74xx compatible card reader, for
170 example.
171 You will also have to select some flash card format drivers. MMC/SD
172 cards are supported via 'MMC/SD Card support: TI Flash Media MMC/SD
173 Interface support (MMC_TIFM_SD)'.
175 To compile this driver as a module, choose M here: the module will
176 be called tifm_core.
178 config TIFM_7XX1
179 tristate "TI Flash Media PCI74xx/PCI76xx host adapter support"
180 depends on PCI && TIFM_CORE
181 default TIFM_CORE
182 help
183 This option enables support for Texas Instruments(R) PCI74xx and
184 PCI76xx families of Flash Media adapters, found in many laptops.
185 To make actual use of the device, you will have to select some
186 flash card format drivers, as outlined in the TIFM_CORE Help.
188 To compile this driver as a module, choose M here: the module will
189 be called tifm_7xx1.
191 config ICS932S401
192 tristate "Integrated Circuits ICS932S401"
193 depends on I2C
194 help
195 If you say yes here you get support for the Integrated Circuits
196 ICS932S401 clock control chips.
198 This driver can also be built as a module. If so, the module
199 will be called ics932s401.
201 config ATMEL_SSC
202 tristate "Device driver for Atmel SSC peripheral"
203 depends on HAS_IOMEM
204 ---help---
205 This option enables device driver support for Atmel Synchronized
206 Serial Communication peripheral (SSC).
208 The SSC peripheral supports a wide variety of serial frame based
209 communications, i.e. I2S, SPI, etc.
211 If unsure, say N.
213 config ENCLOSURE_SERVICES
214 tristate "Enclosure Services"
215 default n
216 help
217 Provides support for intelligent enclosures (bays which
218 contain storage devices). You also need either a host
219 driver (SCSI/ATA) which supports enclosures
220 or a SCSI enclosure device (SES) to use these services.
222 config SGI_XP
223 tristate "Support communication between SGI SSIs"
224 depends on NET
225 depends on (IA64_GENERIC || IA64_SGI_SN2 || IA64_SGI_UV || X86_UV) && SMP
226 select IA64_UNCACHED_ALLOCATOR if IA64_GENERIC || IA64_SGI_SN2
227 select GENERIC_ALLOCATOR if IA64_GENERIC || IA64_SGI_SN2
228 select SGI_GRU if X86_64 && SMP
229 ---help---
230 An SGI machine can be divided into multiple Single System
231 Images which act independently of each other and have
232 hardware based memory protection from the others. Enabling
233 this feature will allow for direct communication between SSIs
234 based on a network adapter and DMA messaging.
236 config CS5535_MFGPT
237 tristate "CS5535/CS5536 Geode Multi-Function General Purpose Timer (MFGPT) support"
238 depends on PCI && X86 && MFD_CS5535
239 default n
240 help
241 This driver provides access to MFGPT functionality for other
242 drivers that need timers. MFGPTs are available in the CS5535 and
243 CS5536 companion chips that are found in AMD Geode and several
244 other platforms. They have a better resolution and max interval
245 than the generic PIT, and are suitable for use as high-res timers.
246 You probably don't want to enable this manually; other drivers that
247 make use of it should enable it.
249 config CS5535_MFGPT_DEFAULT_IRQ
250 int
251 depends on CS5535_MFGPT
252 default 7
253 help
254 MFGPTs on the CS5535 require an interrupt. The selected IRQ
255 can be overridden as a module option as well as by driver that
256 use the cs5535_mfgpt_ API; however, different architectures might
257 want to use a different IRQ by default. This is here for
258 architectures to set as necessary.
260 config CS5535_CLOCK_EVENT_SRC
261 tristate "CS5535/CS5536 high-res timer (MFGPT) events"
262 depends on GENERIC_CLOCKEVENTS && CS5535_MFGPT
263 help
264 This driver provides a clock event source based on the MFGPT
265 timer(s) in the CS5535 and CS5536 companion chips.
266 MFGPTs have a better resolution and max interval than the
267 generic PIT, and are suitable for use as high-res timers.
269 config HP_ILO
270 tristate "Channel interface driver for the HP iLO processor"
271 depends on PCI
272 default n
273 help
274 The channel interface driver allows applications to communicate
275 with iLO management processors present on HP ProLiant servers.
276 Upon loading, the driver creates /dev/hpilo/dXccbN files, which
277 can be used to gather data from the management processor, via
278 read and write system calls.
280 To compile this driver as a module, choose M here: the
281 module will be called hpilo.
283 config SGI_GRU
284 tristate "SGI GRU driver"
285 depends on X86_UV && SMP
286 default n
287 select MMU_NOTIFIER
288 ---help---
289 The GRU is a hardware resource located in the system chipset. The GRU
290 contains memory that can be mmapped into the user address space. This memory is
291 used to communicate with the GRU to perform functions such as load/store,
292 scatter/gather, bcopy, AMOs, etc. The GRU is directly accessed by user
293 instructions using user virtual addresses. GRU instructions (ex., bcopy) use
294 user virtual addresses for operands.
296 If you are not running on a SGI UV system, say N.
298 config SGI_GRU_DEBUG
299 bool "SGI GRU driver debug"
300 depends on SGI_GRU
301 default n
302 ---help---
303 This option enables addition debugging code for the SGI GRU driver. If
304 you are unsure, say N.
306 config APDS9802ALS
307 tristate "Medfield Avago APDS9802 ALS Sensor module"
308 depends on I2C
309 help
310 If you say yes here you get support for the ALS APDS9802 ambient
311 light sensor.
313 This driver can also be built as a module. If so, the module
314 will be called apds9802als.
316 config ISL29003
317 tristate "Intersil ISL29003 ambient light sensor"
318 depends on I2C && SYSFS
319 help
320 If you say yes here you get support for the Intersil ISL29003
321 ambient light sensor.
323 This driver can also be built as a module. If so, the module
324 will be called isl29003.
326 config ISL29020
327 tristate "Intersil ISL29020 ambient light sensor"
328 depends on I2C
329 help
330 If you say yes here you get support for the Intersil ISL29020
331 ambient light sensor.
333 This driver can also be built as a module. If so, the module
334 will be called isl29020.
336 config SENSORS_TSL2550
337 tristate "Taos TSL2550 ambient light sensor"
338 depends on I2C && SYSFS
339 help
340 If you say yes here you get support for the Taos TSL2550
341 ambient light sensor.
343 This driver can also be built as a module. If so, the module
344 will be called tsl2550.
346 config SENSORS_BH1780
347 tristate "ROHM BH1780GLI ambient light sensor"
348 depends on I2C && SYSFS
349 help
350 If you say yes here you get support for the ROHM BH1780GLI
351 ambient light sensor.
353 This driver can also be built as a module. If so, the module
354 will be called bh1780gli.
356 config SENSORS_BH1770
357 tristate "BH1770GLC / SFH7770 combined ALS - Proximity sensor"
358 depends on I2C
359 ---help---
360 Say Y here if you want to build a driver for BH1770GLC (ROHM) or
361 SFH7770 (Osram) combined ambient light and proximity sensor chip.
363 To compile this driver as a module, choose M here: the
364 module will be called bh1770glc. If unsure, say N here.
366 config SENSORS_APDS990X
367 tristate "APDS990X combined als and proximity sensors"
368 depends on I2C
369 default n
370 ---help---
371 Say Y here if you want to build a driver for Avago APDS990x
372 combined ambient light and proximity sensor chip.
374 To compile this driver as a module, choose M here: the
375 module will be called apds990x. If unsure, say N here.
377 config HMC6352
378 tristate "Honeywell HMC6352 compass"
379 depends on I2C
380 help
381 This driver provides support for the Honeywell HMC6352 compass,
382 providing configuration and heading data via sysfs.
384 config DS1682
385 tristate "Dallas DS1682 Total Elapsed Time Recorder with Alarm"
386 depends on I2C
387 help
388 If you say yes here you get support for Dallas Semiconductor
389 DS1682 Total Elapsed Time Recorder.
391 This driver can also be built as a module. If so, the module
392 will be called ds1682.
394 config SPEAR13XX_PCIE_GADGET
395 bool "PCIe gadget support for SPEAr13XX platform"
396 depends on ARCH_SPEAR13XX && BROKEN
397 default n
398 help
399 This option enables gadget support for PCIe controller. If
400 board file defines any controller as PCIe endpoint then a sysfs
401 entry will be created for that controller. User can use these
402 sysfs node to configure PCIe EP as per his requirements.
404 config TI_DAC7512
405 tristate "Texas Instruments DAC7512"
406 depends on SPI && SYSFS
407 help
408 If you say yes here you get support for the Texas Instruments
409 DAC7512 16-bit digital-to-analog converter.
411 This driver can also be built as a module. If so, the module
412 will be called ti_dac7512.
414 config UID_STAT
415 bool "UID based statistics tracking exported to /proc/uid_stat"
416 default n
418 config VMWARE_BALLOON
419 tristate "VMware Balloon Driver"
420 depends on X86 && HYPERVISOR_GUEST
421 help
422 This is VMware physical memory management driver which acts
423 like a "balloon" that can be inflated to reclaim physical pages
424 by reserving them in the guest and invalidating them in the
425 monitor, freeing up the underlying machine pages so they can
426 be allocated to other guests. The balloon can also be deflated
427 to allow the guest to use more physical memory.
429 If unsure, say N.
431 To compile this driver as a module, choose M here: the
432 module will be called vmw_balloon.
434 config ARM_CHARLCD
435 bool "ARM Ltd. Character LCD Driver"
436 depends on PLAT_VERSATILE
437 help
438 This is a driver for the character LCD found on the ARM Ltd.
439 Versatile and RealView Platform Baseboards. It doesn't do
440 very much more than display the text "ARM Linux" on the first
441 line and the Linux version on the second line, but that's
442 still useful.
444 config BMP085
445 bool
446 depends on SYSFS
448 config BMP085_I2C
449 tristate "BMP085 digital pressure sensor on I2C"
450 select BMP085
451 select REGMAP_I2C
452 depends on I2C && SYSFS
453 help
454 Say Y here if you want to support Bosch Sensortec's digital pressure
455 sensor hooked to an I2C bus.
457 To compile this driver as a module, choose M here: the
458 module will be called bmp085-i2c.
460 config BMP085_SPI
461 tristate "BMP085 digital pressure sensor on SPI"
462 select BMP085
463 select REGMAP_SPI
464 depends on SPI_MASTER && SYSFS
465 help
466 Say Y here if you want to support Bosch Sensortec's digital pressure
467 sensor hooked to an SPI bus.
469 To compile this driver as a module, choose M here: the
470 module will be called bmp085-spi.
472 config PCH_PHUB
473 tristate "Intel EG20T PCH/LAPIS Semicon IOH(ML7213/ML7223/ML7831) PHUB"
474 select GENERIC_NET_UTILS
475 depends on PCI
476 help
477 This driver is for PCH(Platform controller Hub) PHUB(Packet Hub) of
478 Intel Topcliff which is an IOH(Input/Output Hub) for x86 embedded
479 processor. The Topcliff has MAC address and Option ROM data in SROM.
480 This driver can access MAC address and Option ROM data in SROM.
482 This driver also can be used for LAPIS Semiconductor's IOH,
483 ML7213/ML7223/ML7831.
484 ML7213 which is for IVI(In-Vehicle Infotainment) use.
485 ML7223 IOH is for MP(Media Phone) use.
486 ML7831 IOH is for general purpose use.
487 ML7213/ML7223/ML7831 is companion chip for Intel Atom E6xx series.
488 ML7213/ML7223/ML7831 is completely compatible for Intel EG20T PCH.
490 To compile this driver as a module, choose M here: the module will
491 be called pch_phub.
493 config USB_SWITCH_FSA9480
494 tristate "FSA9480 USB Switch"
495 depends on I2C
496 help
497 The FSA9480 is a USB port accessory detector and switch.
498 The FSA9480 is fully controlled using I2C and enables USB data,
499 stereo and mono audio, video, microphone and UART data to use
500 a common connector port.
502 config LATTICE_ECP3_CONFIG
503 tristate "Lattice ECP3 FPGA bitstream configuration via SPI"
504 depends on SPI && SYSFS
505 select FW_LOADER
506 default n
507 help
508 This option enables support for bitstream configuration (programming
509 or loading) of the Lattice ECP3 FPGA family via SPI.
511 If unsure, say N.
513 config SRAM
514 bool "Generic on-chip SRAM driver"
515 depends on HAS_IOMEM
516 select GENERIC_ALLOCATOR
517 help
518 This driver allows you to declare a memory region to be managed by
519 the genalloc API. It is supposed to be used for small on-chip SRAM
520 areas found on many SoCs.
522 config UID_CPUTIME
523 tristate "Per-UID cpu time statistics"
524 depends on PROFILING
525 help
526 Per UID based cpu time statistics exported to /proc/uid_cputime
528 source "drivers/misc/c2port/Kconfig"
529 source "drivers/misc/eeprom/Kconfig"
530 source "drivers/misc/cb710/Kconfig"
531 source "drivers/misc/ti-st/Kconfig"
532 source "drivers/misc/lis3lv02d/Kconfig"
533 source "drivers/misc/carma/Kconfig"
534 source "drivers/misc/altera-stapl/Kconfig"
535 source "drivers/misc/mei/Kconfig"
536 source "drivers/misc/vmw_vmci/Kconfig"
537 source "drivers/misc/mic/Kconfig"
538 source "drivers/misc/genwqe/Kconfig"
539 endmenu