1 /*
2 * linux/drivers/mmc/core/sdio_io.c
3 *
4 * Copyright 2007-2008 Pierre Ossman
5 *
6 * This program is free software; you can redistribute it and/or modify
7 * it under the terms of the GNU General Public License as published by
8 * the Free Software Foundation; either version 2 of the License, or (at
9 * your option) any later version.
10 */
12 #include <linux/export.h>
13 #include <linux/mmc/host.h>
14 #include <linux/mmc/card.h>
15 #include <linux/mmc/sdio.h>
16 #include <linux/mmc/sdio_func.h>
18 #include "sdio_ops.h"
20 /**
21 * sdio_claim_host - exclusively claim a bus for a certain SDIO function
22 * @func: SDIO function that will be accessed
23 *
24 * Claim a bus for a set of operations. The SDIO function given
25 * is used to figure out which bus is relevant.
26 */
27 void sdio_claim_host(struct sdio_func *func)
28 {
29 BUG_ON(!func);
30 BUG_ON(!func->card);
32 mmc_claim_host(func->card->host);
33 }
34 EXPORT_SYMBOL_GPL(sdio_claim_host);
36 /**
37 * sdio_release_host - release a bus for a certain SDIO function
38 * @func: SDIO function that was accessed
39 *
40 * Release a bus, allowing others to claim the bus for their
41 * operations.
42 */
43 void sdio_release_host(struct sdio_func *func)
44 {
45 BUG_ON(!func);
46 BUG_ON(!func->card);
48 mmc_release_host(func->card->host);
49 }
50 EXPORT_SYMBOL_GPL(sdio_release_host);
52 /**
53 * sdio_enable_func - enables a SDIO function for usage
54 * @func: SDIO function to enable
55 *
56 * Powers up and activates a SDIO function so that register
57 * access is possible.
58 */
59 int sdio_enable_func(struct sdio_func *func)
60 {
61 int ret;
62 unsigned char reg;
63 unsigned long timeout;
65 BUG_ON(!func);
66 BUG_ON(!func->card);
68 pr_debug("SDIO: Enabling device %s...\n", sdio_func_id(func));
70 ret = mmc_io_rw_direct(func->card, 0, 0, SDIO_CCCR_IOEx, 0, ®);
71 if (ret)
72 goto err;
74 reg |= 1 << func->num;
76 ret = mmc_io_rw_direct(func->card, 1, 0, SDIO_CCCR_IOEx, reg, NULL);
77 if (ret)
78 goto err;
80 timeout = jiffies + msecs_to_jiffies(func->enable_timeout);
82 while (1) {
83 ret = mmc_io_rw_direct(func->card, 0, 0, SDIO_CCCR_IORx, 0, ®);
84 if (ret)
85 goto err;
86 if (reg & (1 << func->num))
87 break;
88 ret = -ETIME;
89 if (time_after(jiffies, timeout))
90 goto err;
91 }
93 pr_debug("SDIO: Enabled device %s\n", sdio_func_id(func));
95 return 0;
97 err:
98 pr_debug("SDIO: Failed to enable device %s\n", sdio_func_id(func));
99 return ret;
100 }
101 EXPORT_SYMBOL_GPL(sdio_enable_func);
103 /**
104 * sdio_disable_func - disable a SDIO function
105 * @func: SDIO function to disable
106 *
107 * Powers down and deactivates a SDIO function. Register access
108 * to this function will fail until the function is reenabled.
109 */
110 int sdio_disable_func(struct sdio_func *func)
111 {
112 int ret;
113 unsigned char reg;
115 BUG_ON(!func);
116 BUG_ON(!func->card);
118 pr_debug("SDIO: Disabling device %s...\n", sdio_func_id(func));
120 ret = mmc_io_rw_direct(func->card, 0, 0, SDIO_CCCR_IOEx, 0, ®);
121 if (ret)
122 goto err;
124 reg &= ~(1 << func->num);
126 ret = mmc_io_rw_direct(func->card, 1, 0, SDIO_CCCR_IOEx, reg, NULL);
127 if (ret)
128 goto err;
130 pr_debug("SDIO: Disabled device %s\n", sdio_func_id(func));
132 return 0;
134 err:
135 pr_debug("SDIO: Failed to disable device %s\n", sdio_func_id(func));
136 return -EIO;
137 }
138 EXPORT_SYMBOL_GPL(sdio_disable_func);
140 /**
141 * sdio_set_block_size - set the block size of an SDIO function
142 * @func: SDIO function to change
143 * @blksz: new block size or 0 to use the default.
144 *
145 * The default block size is the largest supported by both the function
146 * and the host, with a maximum of 512 to ensure that arbitrarily sized
147 * data transfer use the optimal (least) number of commands.
148 *
149 * A driver may call this to override the default block size set by the
150 * core. This can be used to set a block size greater than the maximum
151 * that reported by the card; it is the driver's responsibility to ensure
152 * it uses a value that the card supports.
153 *
154 * Returns 0 on success, -EINVAL if the host does not support the
155 * requested block size, or -EIO (etc.) if one of the resultant FBR block
156 * size register writes failed.
157 *
158 */
159 int sdio_set_block_size(struct sdio_func *func, unsigned blksz)
160 {
161 int ret;
163 if (blksz > func->card->host->max_blk_size)
164 return -EINVAL;
166 if (blksz == 0) {
167 blksz = min(func->max_blksize, func->card->host->max_blk_size);
168 blksz = min(blksz, 512u);
169 }
171 ret = mmc_io_rw_direct(func->card, 1, 0,
172 SDIO_FBR_BASE(func->num) + SDIO_FBR_BLKSIZE,
173 blksz & 0xff, NULL);
174 if (ret)
175 return ret;
176 ret = mmc_io_rw_direct(func->card, 1, 0,
177 SDIO_FBR_BASE(func->num) + SDIO_FBR_BLKSIZE + 1,
178 (blksz >> 8) & 0xff, NULL);
179 if (ret)
180 return ret;
181 func->cur_blksize = blksz;
182 return 0;
183 }
184 EXPORT_SYMBOL_GPL(sdio_set_block_size);
186 /*
187 * Calculate the maximum byte mode transfer size
188 */
189 static inline unsigned int sdio_max_byte_size(struct sdio_func *func)
190 {
191 unsigned mval = func->card->host->max_blk_size;
193 if (mmc_blksz_for_byte_mode(func->card))
194 mval = min(mval, func->cur_blksize);
195 else
196 mval = min(mval, func->max_blksize);
198 if (mmc_card_broken_byte_mode_512(func->card))
199 return min(mval, 511u);
201 return min(mval, 512u); /* maximum size for byte mode */
202 }
204 /**
205 * sdio_align_size - pads a transfer size to a more optimal value
206 * @func: SDIO function
207 * @sz: original transfer size
208 *
209 * Pads the original data size with a number of extra bytes in
210 * order to avoid controller bugs and/or performance hits
211 * (e.g. some controllers revert to PIO for certain sizes).
212 *
213 * If possible, it will also adjust the size so that it can be
214 * handled in just a single request.
215 *
216 * Returns the improved size, which might be unmodified.
217 */
218 unsigned int sdio_align_size(struct sdio_func *func, unsigned int sz)
219 {
220 unsigned int orig_sz;
221 unsigned int blk_sz, byte_sz;
222 unsigned chunk_sz;
224 orig_sz = sz;
226 /*
227 * Do a first check with the controller, in case it
228 * wants to increase the size up to a point where it
229 * might need more than one block.
230 */
231 sz = mmc_align_data_size(func->card, sz);
233 /*
234 * If we can still do this with just a byte transfer, then
235 * we're done.
236 */
237 if (sz <= sdio_max_byte_size(func))
238 return sz;
240 if (func->card->cccr.multi_block) {
241 /*
242 * Check if the transfer is already block aligned
243 */
244 if ((sz % func->cur_blksize) == 0)
245 return sz;
247 /*
248 * Realign it so that it can be done with one request,
249 * and recheck if the controller still likes it.
250 */
251 blk_sz = ((sz + func->cur_blksize - 1) /
252 func->cur_blksize) * func->cur_blksize;
253 blk_sz = mmc_align_data_size(func->card, blk_sz);
255 /*
256 * This value is only good if it is still just
257 * one request.
258 */
259 if ((blk_sz % func->cur_blksize) == 0)
260 return blk_sz;
262 /*
263 * We failed to do one request, but at least try to
264 * pad the remainder properly.
265 */
266 byte_sz = mmc_align_data_size(func->card,
267 sz % func->cur_blksize);
268 if (byte_sz <= sdio_max_byte_size(func)) {
269 blk_sz = sz / func->cur_blksize;
270 return blk_sz * func->cur_blksize + byte_sz;
271 }
272 } else {
273 /*
274 * We need multiple requests, so first check that the
275 * controller can handle the chunk size;
276 */
277 chunk_sz = mmc_align_data_size(func->card,
278 sdio_max_byte_size(func));
279 if (chunk_sz == sdio_max_byte_size(func)) {
280 /*
281 * Fix up the size of the remainder (if any)
282 */
283 byte_sz = orig_sz % chunk_sz;
284 if (byte_sz) {
285 byte_sz = mmc_align_data_size(func->card,
286 byte_sz);
287 }
289 return (orig_sz / chunk_sz) * chunk_sz + byte_sz;
290 }
291 }
293 /*
294 * The controller is simply incapable of transferring the size
295 * we want in decent manner, so just return the original size.
296 */
297 return orig_sz;
298 }
299 EXPORT_SYMBOL_GPL(sdio_align_size);
301 /* Split an arbitrarily sized data transfer into several
302 * IO_RW_EXTENDED commands. */
303 static int sdio_io_rw_ext_helper(struct sdio_func *func, int write,
304 unsigned addr, int incr_addr, u8 *buf, unsigned size)
305 {
306 unsigned remainder = size;
307 unsigned max_blocks;
308 int ret;
310 /* Do the bulk of the transfer using block mode (if supported). */
311 if (func->card->cccr.multi_block && (size > sdio_max_byte_size(func))) {
312 /* Blocks per command is limited by host count, host transfer
313 * size and the maximum for IO_RW_EXTENDED of 511 blocks. */
314 max_blocks = min(func->card->host->max_blk_count, 511u);
316 while (remainder >= func->cur_blksize) {
317 unsigned blocks;
319 blocks = remainder / func->cur_blksize;
320 if (blocks > max_blocks)
321 blocks = max_blocks;
322 size = blocks * func->cur_blksize;
324 ret = mmc_io_rw_extended(func->card, write,
325 func->num, addr, incr_addr, buf,
326 blocks, func->cur_blksize);
327 if (ret)
328 return ret;
330 remainder -= size;
331 buf += size;
332 if (incr_addr)
333 addr += size;
334 }
335 }
337 /* Write the remainder using byte mode. */
338 while (remainder > 0) {
339 size = min(remainder, sdio_max_byte_size(func));
341 /* Indicate byte mode by setting "blocks" = 0 */
342 ret = mmc_io_rw_extended(func->card, write, func->num, addr,
343 incr_addr, buf, 0, size);
344 if (ret)
345 return ret;
347 remainder -= size;
348 buf += size;
349 if (incr_addr)
350 addr += size;
351 }
352 return 0;
353 }
355 /**
356 * sdio_readb - read a single byte from a SDIO function
357 * @func: SDIO function to access
358 * @addr: address to read
359 * @err_ret: optional status value from transfer
360 *
361 * Reads a single byte from the address space of a given SDIO
362 * function. If there is a problem reading the address, 0xff
363 * is returned and @err_ret will contain the error code.
364 */
365 u8 sdio_readb(struct sdio_func *func, unsigned int addr, int *err_ret)
366 {
367 int ret;
368 u8 val;
370 BUG_ON(!func);
372 if (err_ret)
373 *err_ret = 0;
375 ret = mmc_io_rw_direct(func->card, 0, func->num, addr, 0, &val);
376 if (ret) {
377 if (err_ret)
378 *err_ret = ret;
379 return 0xFF;
380 }
382 return val;
383 }
384 EXPORT_SYMBOL_GPL(sdio_readb);
386 /**
387 * sdio_readb_ext - read a single byte from a SDIO function
388 * @func: SDIO function to access
389 * @addr: address to read
390 * @err_ret: optional status value from transfer
391 * @in: value to add to argument
392 *
393 * Reads a single byte from the address space of a given SDIO
394 * function. If there is a problem reading the address, 0xff
395 * is returned and @err_ret will contain the error code.
396 */
397 unsigned char sdio_readb_ext(struct sdio_func *func, unsigned int addr,
398 int *err_ret, unsigned in)
399 {
400 int ret;
401 unsigned char val;
403 BUG_ON(!func);
405 if (err_ret)
406 *err_ret = 0;
408 ret = mmc_io_rw_direct(func->card, 0, func->num, addr, (u8)in, &val);
409 if (ret) {
410 if (err_ret)
411 *err_ret = ret;
412 return 0xFF;
413 }
415 return val;
416 }
417 EXPORT_SYMBOL_GPL(sdio_readb_ext);
419 /**
420 * sdio_writeb - write a single byte to a SDIO function
421 * @func: SDIO function to access
422 * @b: byte to write
423 * @addr: address to write to
424 * @err_ret: optional status value from transfer
425 *
426 * Writes a single byte to the address space of a given SDIO
427 * function. @err_ret will contain the status of the actual
428 * transfer.
429 */
430 void sdio_writeb(struct sdio_func *func, u8 b, unsigned int addr, int *err_ret)
431 {
432 int ret;
434 BUG_ON(!func);
436 ret = mmc_io_rw_direct(func->card, 1, func->num, addr, b, NULL);
437 if (err_ret)
438 *err_ret = ret;
439 }
440 EXPORT_SYMBOL_GPL(sdio_writeb);
442 /**
443 * sdio_writeb_readb - write and read a byte from SDIO function
444 * @func: SDIO function to access
445 * @write_byte: byte to write
446 * @addr: address to write to
447 * @err_ret: optional status value from transfer
448 *
449 * Performs a RAW (Read after Write) operation as defined by SDIO spec -
450 * single byte is written to address space of a given SDIO function and
451 * response is read back from the same address, both using single request.
452 * If there is a problem with the operation, 0xff is returned and
453 * @err_ret will contain the error code.
454 */
455 u8 sdio_writeb_readb(struct sdio_func *func, u8 write_byte,
456 unsigned int addr, int *err_ret)
457 {
458 int ret;
459 u8 val;
461 ret = mmc_io_rw_direct(func->card, 1, func->num, addr,
462 write_byte, &val);
463 if (err_ret)
464 *err_ret = ret;
465 if (ret)
466 val = 0xff;
468 return val;
469 }
470 EXPORT_SYMBOL_GPL(sdio_writeb_readb);
472 /**
473 * sdio_memcpy_fromio - read a chunk of memory from a SDIO function
474 * @func: SDIO function to access
475 * @dst: buffer to store the data
476 * @addr: address to begin reading from
477 * @count: number of bytes to read
478 *
479 * Reads from the address space of a given SDIO function. Return
480 * value indicates if the transfer succeeded or not.
481 */
482 int sdio_memcpy_fromio(struct sdio_func *func, void *dst,
483 unsigned int addr, int count)
484 {
485 return sdio_io_rw_ext_helper(func, 0, addr, 1, dst, count);
486 }
487 EXPORT_SYMBOL_GPL(sdio_memcpy_fromio);
489 /**
490 * sdio_memcpy_toio - write a chunk of memory to a SDIO function
491 * @func: SDIO function to access
492 * @addr: address to start writing to
493 * @src: buffer that contains the data to write
494 * @count: number of bytes to write
495 *
496 * Writes to the address space of a given SDIO function. Return
497 * value indicates if the transfer succeeded or not.
498 */
499 int sdio_memcpy_toio(struct sdio_func *func, unsigned int addr,
500 void *src, int count)
501 {
502 return sdio_io_rw_ext_helper(func, 1, addr, 1, src, count);
503 }
504 EXPORT_SYMBOL_GPL(sdio_memcpy_toio);
506 /**
507 * sdio_readsb - read from a FIFO on a SDIO function
508 * @func: SDIO function to access
509 * @dst: buffer to store the data
510 * @addr: address of (single byte) FIFO
511 * @count: number of bytes to read
512 *
513 * Reads from the specified FIFO of a given SDIO function. Return
514 * value indicates if the transfer succeeded or not.
515 */
516 int sdio_readsb(struct sdio_func *func, void *dst, unsigned int addr,
517 int count)
518 {
519 return sdio_io_rw_ext_helper(func, 0, addr, 0, dst, count);
520 }
521 EXPORT_SYMBOL_GPL(sdio_readsb);
523 /**
524 * sdio_writesb - write to a FIFO of a SDIO function
525 * @func: SDIO function to access
526 * @addr: address of (single byte) FIFO
527 * @src: buffer that contains the data to write
528 * @count: number of bytes to write
529 *
530 * Writes to the specified FIFO of a given SDIO function. Return
531 * value indicates if the transfer succeeded or not.
532 */
533 int sdio_writesb(struct sdio_func *func, unsigned int addr, void *src,
534 int count)
535 {
536 return sdio_io_rw_ext_helper(func, 1, addr, 0, src, count);
537 }
538 EXPORT_SYMBOL_GPL(sdio_writesb);
540 /**
541 * sdio_readw - read a 16 bit integer from a SDIO function
542 * @func: SDIO function to access
543 * @addr: address to read
544 * @err_ret: optional status value from transfer
545 *
546 * Reads a 16 bit integer from the address space of a given SDIO
547 * function. If there is a problem reading the address, 0xffff
548 * is returned and @err_ret will contain the error code.
549 */
550 u16 sdio_readw(struct sdio_func *func, unsigned int addr, int *err_ret)
551 {
552 int ret;
554 if (err_ret)
555 *err_ret = 0;
557 ret = sdio_memcpy_fromio(func, func->tmpbuf, addr, 2);
558 if (ret) {
559 if (err_ret)
560 *err_ret = ret;
561 return 0xFFFF;
562 }
564 return le16_to_cpup((__le16 *)func->tmpbuf);
565 }
566 EXPORT_SYMBOL_GPL(sdio_readw);
568 /**
569 * sdio_writew - write a 16 bit integer to a SDIO function
570 * @func: SDIO function to access
571 * @b: integer to write
572 * @addr: address to write to
573 * @err_ret: optional status value from transfer
574 *
575 * Writes a 16 bit integer to the address space of a given SDIO
576 * function. @err_ret will contain the status of the actual
577 * transfer.
578 */
579 void sdio_writew(struct sdio_func *func, u16 b, unsigned int addr, int *err_ret)
580 {
581 int ret;
583 *(__le16 *)func->tmpbuf = cpu_to_le16(b);
585 ret = sdio_memcpy_toio(func, addr, func->tmpbuf, 2);
586 if (err_ret)
587 *err_ret = ret;
588 }
589 EXPORT_SYMBOL_GPL(sdio_writew);
591 /**
592 * sdio_readl - read a 32 bit integer from a SDIO function
593 * @func: SDIO function to access
594 * @addr: address to read
595 * @err_ret: optional status value from transfer
596 *
597 * Reads a 32 bit integer from the address space of a given SDIO
598 * function. If there is a problem reading the address,
599 * 0xffffffff is returned and @err_ret will contain the error
600 * code.
601 */
602 u32 sdio_readl(struct sdio_func *func, unsigned int addr, int *err_ret)
603 {
604 int ret;
606 if (err_ret)
607 *err_ret = 0;
609 ret = sdio_memcpy_fromio(func, func->tmpbuf, addr, 4);
610 if (ret) {
611 if (err_ret)
612 *err_ret = ret;
613 return 0xFFFFFFFF;
614 }
616 return le32_to_cpup((__le32 *)func->tmpbuf);
617 }
618 EXPORT_SYMBOL_GPL(sdio_readl);
620 /**
621 * sdio_writel - write a 32 bit integer to a SDIO function
622 * @func: SDIO function to access
623 * @b: integer to write
624 * @addr: address to write to
625 * @err_ret: optional status value from transfer
626 *
627 * Writes a 32 bit integer to the address space of a given SDIO
628 * function. @err_ret will contain the status of the actual
629 * transfer.
630 */
631 void sdio_writel(struct sdio_func *func, u32 b, unsigned int addr, int *err_ret)
632 {
633 int ret;
635 *(__le32 *)func->tmpbuf = cpu_to_le32(b);
637 ret = sdio_memcpy_toio(func, addr, func->tmpbuf, 4);
638 if (err_ret)
639 *err_ret = ret;
640 }
641 EXPORT_SYMBOL_GPL(sdio_writel);
643 /**
644 * sdio_f0_readb - read a single byte from SDIO function 0
645 * @func: an SDIO function of the card
646 * @addr: address to read
647 * @err_ret: optional status value from transfer
648 *
649 * Reads a single byte from the address space of SDIO function 0.
650 * If there is a problem reading the address, 0xff is returned
651 * and @err_ret will contain the error code.
652 */
653 unsigned char sdio_f0_readb(struct sdio_func *func, unsigned int addr,
654 int *err_ret)
655 {
656 int ret;
657 unsigned char val;
659 BUG_ON(!func);
661 if (err_ret)
662 *err_ret = 0;
664 ret = mmc_io_rw_direct(func->card, 0, 0, addr, 0, &val);
665 if (ret) {
666 if (err_ret)
667 *err_ret = ret;
668 return 0xFF;
669 }
671 return val;
672 }
673 EXPORT_SYMBOL_GPL(sdio_f0_readb);
675 /**
676 * sdio_f0_writeb - write a single byte to SDIO function 0
677 * @func: an SDIO function of the card
678 * @b: byte to write
679 * @addr: address to write to
680 * @err_ret: optional status value from transfer
681 *
682 * Writes a single byte to the address space of SDIO function 0.
683 * @err_ret will contain the status of the actual transfer.
684 *
685 * Only writes to the vendor specific CCCR registers (0xF0 -
686 * 0xFF) are permiited; @err_ret will be set to -EINVAL for *
687 * writes outside this range.
688 */
689 void sdio_f0_writeb(struct sdio_func *func, unsigned char b, unsigned int addr,
690 int *err_ret)
691 {
692 int ret;
694 BUG_ON(!func);
696 if ((addr < 0xF0 || addr > 0xFF) && (!mmc_card_lenient_fn0(func->card))) {
697 if (err_ret)
698 *err_ret = -EINVAL;
699 return;
700 }
702 ret = mmc_io_rw_direct(func->card, 1, 0, addr, b, NULL);
703 if (err_ret)
704 *err_ret = ret;
705 }
706 EXPORT_SYMBOL_GPL(sdio_f0_writeb);
708 /**
709 * sdio_get_host_pm_caps - get host power management capabilities
710 * @func: SDIO function attached to host
711 *
712 * Returns a capability bitmask corresponding to power management
713 * features supported by the host controller that the card function
714 * might rely upon during a system suspend. The host doesn't need
715 * to be claimed, nor the function active, for this information to be
716 * obtained.
717 */
718 mmc_pm_flag_t sdio_get_host_pm_caps(struct sdio_func *func)
719 {
720 BUG_ON(!func);
721 BUG_ON(!func->card);
723 return func->card->host->pm_caps;
724 }
725 EXPORT_SYMBOL_GPL(sdio_get_host_pm_caps);
727 /**
728 * sdio_set_host_pm_flags - set wanted host power management capabilities
729 * @func: SDIO function attached to host
730 *
731 * Set a capability bitmask corresponding to wanted host controller
732 * power management features for the upcoming suspend state.
733 * This must be called, if needed, each time the suspend method of
734 * the function driver is called, and must contain only bits that
735 * were returned by sdio_get_host_pm_caps().
736 * The host doesn't need to be claimed, nor the function active,
737 * for this information to be set.
738 */
739 int sdio_set_host_pm_flags(struct sdio_func *func, mmc_pm_flag_t flags)
740 {
741 struct mmc_host *host;
743 BUG_ON(!func);
744 BUG_ON(!func->card);
746 host = func->card->host;
748 if (flags & ~host->pm_caps)
749 return -EINVAL;
751 /* function suspend methods are serialized, hence no lock needed */
752 host->pm_flags |= flags;
753 return 0;
754 }
755 EXPORT_SYMBOL_GPL(sdio_set_host_pm_flags);