1 config MTD_NAND_IDS
2 tristate "Include chip ids for known NAND devices."
3 depends on MTD
4 help
5 Useful for NAND drivers that do not use the NAND subsystem but
6 still like to take advantage of the known chip information.
8 config MTD_NAND_ECC
9 tristate
11 config MTD_NAND_ECC_SMC
12 bool "NAND ECC Smart Media byte order"
13 depends on MTD_NAND_ECC
14 default n
15 help
16 Software ECC according to the Smart Media Specification.
17 The original Linux implementation had byte 0 and 1 swapped.
20 menuconfig MTD_NAND
21 tristate "NAND Device Support"
22 depends on MTD
23 select MTD_NAND_IDS
24 select MTD_NAND_ECC
25 help
26 This enables support for accessing all type of NAND flash
27 devices. For further information see
28 <http://www.linux-mtd.infradead.org/doc/nand.html>.
30 if MTD_NAND
32 config MTD_NAND_BCH
33 tristate
34 select BCH
35 depends on MTD_NAND_ECC_BCH
36 default MTD_NAND
38 config MTD_NAND_ECC_BCH
39 bool "Support software BCH ECC"
40 default n
41 help
42 This enables support for software BCH error correction. Binary BCH
43 codes are more powerful and cpu intensive than traditional Hamming
44 ECC codes. They are used with NAND devices requiring more than 1 bit
45 of error correction.
47 config MTD_SM_COMMON
48 tristate
49 default n
51 config MTD_NAND_MUSEUM_IDS
52 bool "Enable chip ids for obsolete ancient NAND devices"
53 default n
54 help
55 Enable this option only when your board has first generation
56 NAND chips (page size 256 byte, erase size 4-8KiB). The IDs
57 of these chips were reused by later, larger chips.
59 config MTD_NAND_DENALI
60 tristate "Support Denali NAND controller"
61 help
62 Enable support for the Denali NAND controller. This should be
63 combined with either the PCI or platform drivers to provide device
64 registration.
66 config MTD_NAND_DENALI_PCI
67 tristate "Support Denali NAND controller on Intel Moorestown"
68 depends on PCI && MTD_NAND_DENALI
69 help
70 Enable the driver for NAND flash on Intel Moorestown, using the
71 Denali NAND controller core.
73 config MTD_NAND_DENALI_DT
74 tristate "Support Denali NAND controller as a DT device"
75 depends on HAVE_CLK && MTD_NAND_DENALI
76 help
77 Enable the driver for NAND flash on platforms using a Denali NAND
78 controller as a DT device.
80 config MTD_NAND_DENALI_SCRATCH_REG_ADDR
81 hex "Denali NAND size scratch register address"
82 default "0xFF108018"
83 depends on MTD_NAND_DENALI_PCI
84 help
85 Some platforms place the NAND chip size in a scratch register
86 because (some versions of) the driver aren't able to automatically
87 determine the size of certain chips. Set the address of the
88 scratch register here to enable this feature. On Intel Moorestown
89 boards, the scratch register is at 0xFF108018.
91 config MTD_NAND_H1900
92 tristate "iPAQ H1900 flash"
93 depends on ARCH_PXA && BROKEN
94 help
95 This enables the driver for the iPAQ h1900 flash.
97 config MTD_NAND_GPIO
98 tristate "GPIO NAND Flash driver"
99 depends on GENERIC_GPIO && ARM
100 help
101 This enables a GPIO based NAND flash driver.
103 config MTD_NAND_AMS_DELTA
104 tristate "NAND Flash device on Amstrad E3"
105 depends on MACH_AMS_DELTA
106 default y
107 help
108 Support for NAND flash on Amstrad E3 (Delta).
110 config MTD_NAND_OMAP2
111 tristate "NAND Flash device on OMAP2, OMAP3 and OMAP4"
112 depends on ARCH_OMAP2PLUS
113 help
114 Support for NAND flash on Texas Instruments OMAP2, OMAP3 and OMAP4
115 platforms.
117 config MTD_NAND_OMAP_BCH
118 depends on MTD_NAND && MTD_NAND_OMAP2 && ARCH_OMAP3
119 bool "Enable support for hardware BCH error correction"
120 default n
121 select BCH
122 select BCH_CONST_PARAMS
123 help
124 Support for hardware BCH error correction.
126 choice
127 prompt "BCH error correction capability"
128 depends on MTD_NAND_OMAP_BCH
130 config MTD_NAND_OMAP_BCH8
131 bool "8 bits / 512 bytes (recommended)"
132 help
133 Support correcting up to 8 bitflips per 512-byte block.
134 This will use 13 bytes of spare area per 512 bytes of page data.
135 This is the recommended mode, as 4-bit mode does not work
136 on some OMAP3 revisions, due to a hardware bug.
138 config MTD_NAND_OMAP_BCH4
139 bool "4 bits / 512 bytes"
140 help
141 Support correcting up to 4 bitflips per 512-byte block.
142 This will use 7 bytes of spare area per 512 bytes of page data.
143 Note that this mode does not work on some OMAP3 revisions, due to a
144 hardware bug. Please check your OMAP datasheet before selecting this
145 mode.
147 endchoice
149 if MTD_NAND_OMAP_BCH
150 config BCH_CONST_M
151 default 13
152 config BCH_CONST_T
153 default 4 if MTD_NAND_OMAP_BCH4
154 default 8 if MTD_NAND_OMAP_BCH8
155 endif
157 config MTD_NAND_RICOH
158 tristate "Ricoh xD card reader"
159 default n
160 depends on PCI
161 select MTD_SM_COMMON
162 help
163 Enable support for Ricoh R5C852 xD card reader
164 You also need to enable ether
165 NAND SSFDC (SmartMedia) read only translation layer' or new
166 expermental, readwrite
167 'SmartMedia/xD new translation layer'
169 config MTD_NAND_AU1550
170 tristate "Au1550/1200 NAND support"
171 depends on MIPS_ALCHEMY
172 help
173 This enables the driver for the NAND flash controller on the
174 AMD/Alchemy 1550 SOC.
176 config MTD_NAND_BF5XX
177 tristate "Blackfin on-chip NAND Flash Controller driver"
178 depends on BF54x || BF52x
179 help
180 This enables the Blackfin on-chip NAND flash controller
182 No board specific support is done by this driver, each board
183 must advertise a platform_device for the driver to attach.
185 This driver can also be built as a module. If so, the module
186 will be called bf5xx-nand.
188 config MTD_NAND_BF5XX_HWECC
189 bool "BF5XX NAND Hardware ECC"
190 default y
191 depends on MTD_NAND_BF5XX
192 help
193 Enable the use of the BF5XX's internal ECC generator when
194 using NAND.
196 config MTD_NAND_BF5XX_BOOTROM_ECC
197 bool "Use Blackfin BootROM ECC Layout"
198 default n
199 depends on MTD_NAND_BF5XX_HWECC
200 help
201 If you wish to modify NAND pages and allow the Blackfin on-chip
202 BootROM to boot from them, say Y here. This is only necessary
203 if you are booting U-Boot out of NAND and you wish to update
204 U-Boot from Linux' userspace. Otherwise, you should say N here.
206 If unsure, say N.
208 config MTD_NAND_RTC_FROM4
209 tristate "Renesas Flash ROM 4-slot interface board (FROM_BOARD4)"
210 depends on SH_SOLUTION_ENGINE
211 select REED_SOLOMON
212 select REED_SOLOMON_DEC8
213 select BITREVERSE
214 help
215 This enables the driver for the Renesas Technology AG-AND
216 flash interface board (FROM_BOARD4)
218 config MTD_NAND_PPCHAMELEONEVB
219 tristate "NAND Flash device on PPChameleonEVB board"
220 depends on PPCHAMELEONEVB && BROKEN
221 help
222 This enables the NAND flash driver on the PPChameleon EVB Board.
224 config MTD_NAND_S3C2410
225 tristate "NAND Flash support for Samsung S3C SoCs"
226 depends on ARCH_S3C24XX || ARCH_S3C64XX
227 help
228 This enables the NAND flash controller on the S3C24xx and S3C64xx
229 SoCs
231 No board specific support is done by this driver, each board
232 must advertise a platform_device for the driver to attach.
234 config MTD_NAND_S3C2410_DEBUG
235 bool "Samsung S3C NAND driver debug"
236 depends on MTD_NAND_S3C2410
237 help
238 Enable debugging of the S3C NAND driver
240 config MTD_NAND_S3C2410_HWECC
241 bool "Samsung S3C NAND Hardware ECC"
242 depends on MTD_NAND_S3C2410
243 help
244 Enable the use of the controller's internal ECC generator when
245 using NAND. Early versions of the chips have had problems with
246 incorrect ECC generation, and if using these, the default of
247 software ECC is preferable.
249 config MTD_NAND_NDFC
250 tristate "NDFC NanD Flash Controller"
251 depends on 4xx
252 select MTD_NAND_ECC_SMC
253 help
254 NDFC Nand Flash Controllers are integrated in IBM/AMCC's 4xx SoCs
256 config MTD_NAND_S3C2410_CLKSTOP
257 bool "Samsung S3C NAND IDLE clock stop"
258 depends on MTD_NAND_S3C2410
259 default n
260 help
261 Stop the clock to the NAND controller when there is no chip
262 selected to save power. This will mean there is a small delay
263 when the is NAND chip selected or released, but will save
264 approximately 5mA of power when there is nothing happening.
266 config MTD_NAND_DISKONCHIP
267 tristate "DiskOnChip 2000, Millennium and Millennium Plus (NAND reimplementation) (EXPERIMENTAL)"
268 depends on EXPERIMENTAL
269 depends on HAS_IOMEM
270 select REED_SOLOMON
271 select REED_SOLOMON_DEC16
272 help
273 This is a reimplementation of M-Systems DiskOnChip 2000,
274 Millennium and Millennium Plus as a standard NAND device driver,
275 as opposed to the earlier self-contained MTD device drivers.
276 This should enable, among other things, proper JFFS2 operation on
277 these devices.
279 config MTD_NAND_DISKONCHIP_PROBE_ADVANCED
280 bool "Advanced detection options for DiskOnChip"
281 depends on MTD_NAND_DISKONCHIP
282 help
283 This option allows you to specify nonstandard address at which to
284 probe for a DiskOnChip, or to change the detection options. You
285 are unlikely to need any of this unless you are using LinuxBIOS.
286 Say 'N'.
288 config MTD_NAND_DISKONCHIP_PROBE_ADDRESS
289 hex "Physical address of DiskOnChip" if MTD_NAND_DISKONCHIP_PROBE_ADVANCED
290 depends on MTD_NAND_DISKONCHIP
291 default "0"
292 ---help---
293 By default, the probe for DiskOnChip devices will look for a
294 DiskOnChip at every multiple of 0x2000 between 0xC8000 and 0xEE000.
295 This option allows you to specify a single address at which to probe
296 for the device, which is useful if you have other devices in that
297 range which get upset when they are probed.
299 (Note that on PowerPC, the normal probe will only check at
300 0xE4000000.)
302 Normally, you should leave this set to zero, to allow the probe at
303 the normal addresses.
305 config MTD_NAND_DISKONCHIP_PROBE_HIGH
306 bool "Probe high addresses"
307 depends on MTD_NAND_DISKONCHIP_PROBE_ADVANCED
308 help
309 By default, the probe for DiskOnChip devices will look for a
310 DiskOnChip at every multiple of 0x2000 between 0xC8000 and 0xEE000.
311 This option changes to make it probe between 0xFFFC8000 and
312 0xFFFEE000. Unless you are using LinuxBIOS, this is unlikely to be
313 useful to you. Say 'N'.
315 config MTD_NAND_DISKONCHIP_BBTWRITE
316 bool "Allow BBT writes on DiskOnChip Millennium and 2000TSOP"
317 depends on MTD_NAND_DISKONCHIP
318 help
319 On DiskOnChip devices shipped with the INFTL filesystem (Millennium
320 and 2000 TSOP/Alon), Linux reserves some space at the end of the
321 device for the Bad Block Table (BBT). If you have existing INFTL
322 data on your device (created by non-Linux tools such as M-Systems'
323 DOS drivers), your data might overlap the area Linux wants to use for
324 the BBT. If this is a concern for you, leave this option disabled and
325 Linux will not write BBT data into this area.
326 The downside of leaving this option disabled is that if bad blocks
327 are detected by Linux, they will not be recorded in the BBT, which
328 could cause future problems.
329 Once you enable this option, new filesystems (INFTL or others, created
330 in Linux or other operating systems) will not use the reserved area.
331 The only reason not to enable this option is to prevent damage to
332 preexisting filesystems.
333 Even if you leave this disabled, you can enable BBT writes at module
334 load time (assuming you build diskonchip as a module) with the module
335 parameter "inftl_bbt_write=1".
337 config MTD_NAND_DOCG4
338 tristate "Support for DiskOnChip G4 (EXPERIMENTAL)"
339 depends on EXPERIMENTAL && HAS_IOMEM
340 select BCH
341 select BITREVERSE
342 help
343 Support for diskonchip G4 nand flash, found in various smartphones and
344 PDAs, among them the Palm Treo680, HTC Prophet and Wizard, Toshiba
345 Portege G900, Asus P526, and O2 XDA Zinc.
347 With this driver you will be able to use UBI and create a ubifs on the
348 device, so you may wish to consider enabling UBI and UBIFS as well.
350 These devices ship with the Mys/Sandisk SAFTL formatting, for which
351 there is currently no mtd parser, so you may want to use command line
352 partitioning to segregate write-protected blocks. On the Treo680, the
353 first five erase blocks (256KiB each) are write-protected, followed
354 by the block containing the saftl partition table. This is probably
355 typical.
357 config MTD_NAND_SHARPSL
358 tristate "Support for NAND Flash on Sharp SL Series (C7xx + others)"
359 depends on ARCH_PXA
361 config MTD_NAND_CAFE
362 tristate "NAND support for OLPC CAFÉ chip"
363 depends on PCI
364 select REED_SOLOMON
365 select REED_SOLOMON_DEC16
366 help
367 Use NAND flash attached to the CAFÉ chip designed for the OLPC
368 laptop.
370 config MTD_NAND_CS553X
371 tristate "NAND support for CS5535/CS5536 (AMD Geode companion chip)"
372 depends on X86_32
373 help
374 The CS553x companion chips for the AMD Geode processor
375 include NAND flash controllers with built-in hardware ECC
376 capabilities; enabling this option will allow you to use
377 these. The driver will check the MSRs to verify that the
378 controller is enabled for NAND, and currently requires that
379 the controller be in MMIO mode.
381 If you say "m", the module will be called cs553x_nand.
383 config MTD_NAND_ATMEL
384 tristate "Support for NAND Flash / SmartMedia on AT91 and AVR32"
385 depends on ARCH_AT91 || AVR32
386 help
387 Enables support for NAND Flash / Smart Media Card interface
388 on Atmel AT91 and AVR32 processors.
390 config MTD_NAND_PXA3xx
391 tristate "Support for NAND flash devices on PXA3xx"
392 depends on PXA3xx || ARCH_MMP
393 help
394 This enables the driver for the NAND flash device found on
395 PXA3xx processors
397 config MTD_NAND_SLC_LPC32XX
398 tristate "NXP LPC32xx SLC Controller"
399 depends on ARCH_LPC32XX
400 help
401 Enables support for NXP's LPC32XX SLC (i.e. for Single Level Cell
402 chips) NAND controller. This is the default for the PHYTEC 3250
403 reference board which contains a NAND256R3A2CZA6 chip.
405 Please check the actual NAND chip connected and its support
406 by the SLC NAND controller.
408 config MTD_NAND_MLC_LPC32XX
409 tristate "NXP LPC32xx MLC Controller"
410 depends on ARCH_LPC32XX
411 help
412 Uses the LPC32XX MLC (i.e. for Multi Level Cell chips) NAND
413 controller. This is the default for the WORK92105 controller
414 board.
416 Please check the actual NAND chip connected and its support
417 by the MLC NAND controller.
419 config MTD_NAND_CM_X270
420 tristate "Support for NAND Flash on CM-X270 modules"
421 depends on MACH_ARMCORE
423 config MTD_NAND_PASEMI
424 tristate "NAND support for PA Semi PWRficient"
425 depends on PPC_PASEMI
426 help
427 Enables support for NAND Flash interface on PA Semi PWRficient
428 based boards
430 config MTD_NAND_TMIO
431 tristate "NAND Flash device on Toshiba Mobile IO Controller"
432 depends on MFD_TMIO
433 help
434 Support for NAND flash connected to a Toshiba Mobile IO
435 Controller in some PDAs, including the Sharp SL6000x.
437 config MTD_NAND_NANDSIM
438 tristate "Support for NAND Flash Simulator"
439 help
440 The simulator may simulate various NAND flash chips for the
441 MTD nand layer.
443 config MTD_NAND_GPMI_NAND
444 tristate "GPMI NAND Flash Controller driver"
445 depends on MTD_NAND && MXS_DMA
446 help
447 Enables NAND Flash support for IMX23, IMX28 or IMX6.
448 The GPMI controller is very powerful, with the help of BCH
449 module, it can do the hardware ECC. The GPMI supports several
450 NAND flashs at the same time. The GPMI may conflicts with other
451 block, such as SD card. So pay attention to it when you enable
452 the GPMI.
454 config MTD_NAND_BCM47XXNFLASH
455 tristate "Support for NAND flash on BCM4706 BCMA bus"
456 depends on BCMA_NFLASH
457 help
458 BCMA bus can have various flash memories attached, they are
459 registered by bcma as platform devices. This enables driver for
460 NAND flash memories. For now only BCM4706 is supported.
462 config MTD_NAND_PLATFORM
463 tristate "Support for generic platform NAND driver"
464 depends on HAS_IOMEM
465 help
466 This implements a generic NAND driver for on-SOC platform
467 devices. You will need to provide platform-specific functions
468 via platform_data.
470 config MTD_ALAUDA
471 tristate "MTD driver for Olympus MAUSB-10 and Fujifilm DPC-R1"
472 depends on USB
473 help
474 These two (and possibly other) Alauda-based cardreaders for
475 SmartMedia and xD allow raw flash access.
477 config MTD_NAND_ORION
478 tristate "NAND Flash support for Marvell Orion SoC"
479 depends on PLAT_ORION
480 help
481 This enables the NAND flash controller on Orion machines.
483 No board specific support is done by this driver, each board
484 must advertise a platform_device for the driver to attach.
486 config MTD_NAND_FSL_ELBC
487 tristate "NAND support for Freescale eLBC controllers"
488 depends on PPC_OF
489 select FSL_LBC
490 help
491 Various Freescale chips, including the 8313, include a NAND Flash
492 Controller Module with built-in hardware ECC capabilities.
493 Enabling this option will enable you to use this to control
494 external NAND devices.
496 config MTD_NAND_FSL_IFC
497 tristate "NAND support for Freescale IFC controller"
498 depends on MTD_NAND && FSL_SOC
499 select FSL_IFC
500 help
501 Various Freescale chips e.g P1010, include a NAND Flash machine
502 with built-in hardware ECC capabilities.
503 Enabling this option will enable you to use this to control
504 external NAND devices.
506 config MTD_NAND_FSL_UPM
507 tristate "Support for NAND on Freescale UPM"
508 depends on PPC_83xx || PPC_85xx
509 select FSL_LBC
510 help
511 Enables support for NAND Flash chips wired onto Freescale PowerPC
512 processor localbus with User-Programmable Machine support.
514 config MTD_NAND_MPC5121_NFC
515 tristate "MPC5121 built-in NAND Flash Controller support"
516 depends on PPC_MPC512x
517 help
518 This enables the driver for the NAND flash controller on the
519 MPC5121 SoC.
521 config MTD_NAND_MXC
522 tristate "MXC NAND support"
523 depends on ARCH_MXC
524 help
525 This enables the driver for the NAND flash controller on the
526 MXC processors.
528 config MTD_NAND_SH_FLCTL
529 tristate "Support for NAND on Renesas SuperH FLCTL"
530 depends on SUPERH || ARCH_SHMOBILE
531 help
532 Several Renesas SuperH CPU has FLCTL. This option enables support
533 for NAND Flash using FLCTL.
535 config MTD_NAND_DAVINCI
536 tristate "Support NAND on DaVinci SoC"
537 depends on ARCH_DAVINCI
538 help
539 Enable the driver for NAND flash chips on Texas Instruments
540 DaVinci processors.
542 config MTD_NAND_TXX9NDFMC
543 tristate "NAND Flash support for TXx9 SoC"
544 depends on SOC_TX4938 || SOC_TX4939
545 help
546 This enables the NAND flash controller on the TXx9 SoCs.
548 config MTD_NAND_SOCRATES
549 tristate "Support for NAND on Socrates board"
550 depends on SOCRATES
551 help
552 Enables support for NAND Flash chips wired onto Socrates board.
554 config MTD_NAND_NUC900
555 tristate "Support for NAND on Nuvoton NUC9xx/w90p910 evaluation boards."
556 depends on ARCH_W90X900
557 help
558 This enables the driver for the NAND Flash on evaluation board based
559 on w90p910 / NUC9xx.
561 config MTD_NAND_JZ4740
562 tristate "Support for JZ4740 SoC NAND controller"
563 depends on MACH_JZ4740
564 help
565 Enables support for NAND Flash on JZ4740 SoC based boards.
567 config MTD_NAND_FSMC
568 tristate "Support for NAND on ST Micros FSMC"
569 depends on PLAT_SPEAR || ARCH_NOMADIK || ARCH_U8500 || MACH_U300
570 help
571 Enables support for NAND Flash chips on the ST Microelectronics
572 Flexible Static Memory Controller (FSMC)
574 config MTD_NAND_XWAY
575 tristate "Support for NAND on Lantiq XWAY SoC"
576 depends on LANTIQ && SOC_TYPE_XWAY
577 select MTD_NAND_PLATFORM
578 help
579 Enables support for NAND Flash chips on Lantiq XWAY SoCs. NAND is attached
580 to the External Bus Unit (EBU).
582 endif # MTD_NAND