1 /* A network driver using virtio.
2 *
3 * Copyright 2007 Rusty Russell <rusty@rustcorp.com.au> IBM Corporation
4 *
5 * This program is free software; you can redistribute it and/or modify
6 * it under the terms of the GNU General Public License as published by
7 * the Free Software Foundation; either version 2 of the License, or
8 * (at your option) any later version.
9 *
10 * This program is distributed in the hope that it will be useful,
11 * but WITHOUT ANY WARRANTY; without even the implied warranty of
12 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
13 * GNU General Public License for more details.
14 *
15 * You should have received a copy of the GNU General Public License
16 * along with this program; if not, write to the Free Software
17 * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA
18 */
19 //#define DEBUG
20 #include <linux/netdevice.h>
21 #include <linux/etherdevice.h>
22 #include <linux/ethtool.h>
23 #include <linux/module.h>
24 #include <linux/virtio.h>
25 #include <linux/virtio_net.h>
26 #include <linux/scatterlist.h>
27 #include <linux/if_vlan.h>
28 #include <linux/slab.h>
29 #include <linux/cpu.h>
31 static int napi_weight = 128;
32 module_param(napi_weight, int, 0444);
34 static bool csum = true, gso = true;
35 module_param(csum, bool, 0444);
36 module_param(gso, bool, 0444);
38 /* FIXME: MTU in config. */
39 #define MAX_PACKET_LEN (ETH_HLEN + VLAN_HLEN + ETH_DATA_LEN)
40 #define GOOD_COPY_LEN 128
42 #define VIRTNET_SEND_COMMAND_SG_MAX 2
43 #define VIRTNET_DRIVER_VERSION "1.0.0"
45 struct virtnet_stats {
46 struct u64_stats_sync tx_syncp;
47 struct u64_stats_sync rx_syncp;
48 u64 tx_bytes;
49 u64 tx_packets;
51 u64 rx_bytes;
52 u64 rx_packets;
53 };
55 /* Internal representation of a send virtqueue */
56 struct send_queue {
57 /* Virtqueue associated with this send _queue */
58 struct virtqueue *vq;
60 /* TX: fragments + linear part + virtio header */
61 struct scatterlist sg[MAX_SKB_FRAGS + 2];
63 /* Name of the send queue: output.$index */
64 char name[40];
65 };
67 /* Internal representation of a receive virtqueue */
68 struct receive_queue {
69 /* Virtqueue associated with this receive_queue */
70 struct virtqueue *vq;
72 struct napi_struct napi;
74 /* Number of input buffers, and max we've ever had. */
75 unsigned int num, max;
77 /* Chain pages by the private ptr. */
78 struct page *pages;
80 /* RX: fragments + linear part + virtio header */
81 struct scatterlist sg[MAX_SKB_FRAGS + 2];
83 /* Name of this receive queue: input.$index */
84 char name[40];
85 };
87 struct virtnet_info {
88 struct virtio_device *vdev;
89 struct virtqueue *cvq;
90 struct net_device *dev;
91 struct send_queue *sq;
92 struct receive_queue *rq;
93 unsigned int status;
95 /* Max # of queue pairs supported by the device */
96 u16 max_queue_pairs;
98 /* # of queue pairs currently used by the driver */
99 u16 curr_queue_pairs;
101 /* I like... big packets and I cannot lie! */
102 bool big_packets;
104 /* Host will merge rx buffers for big packets (shake it! shake it!) */
105 bool mergeable_rx_bufs;
107 /* Has control virtqueue */
108 bool has_cvq;
110 /* enable config space updates */
111 bool config_enable;
113 /* Active statistics */
114 struct virtnet_stats __percpu *stats;
116 /* Work struct for refilling if we run low on memory. */
117 struct delayed_work refill;
119 /* Work struct for config space updates */
120 struct work_struct config_work;
122 /* Lock for config space updates */
123 struct mutex config_lock;
125 /* Does the affinity hint is set for virtqueues? */
126 bool affinity_hint_set;
128 /* Per-cpu variable to show the mapping from CPU to virtqueue */
129 int __percpu *vq_index;
131 /* CPU hot plug notifier */
132 struct notifier_block nb;
133 };
135 struct skb_vnet_hdr {
136 union {
137 struct virtio_net_hdr hdr;
138 struct virtio_net_hdr_mrg_rxbuf mhdr;
139 };
140 };
142 struct padded_vnet_hdr {
143 struct virtio_net_hdr hdr;
144 /*
145 * virtio_net_hdr should be in a separated sg buffer because of a
146 * QEMU bug, and data sg buffer shares same page with this header sg.
147 * This padding makes next sg 16 byte aligned after virtio_net_hdr.
148 */
149 char padding[6];
150 };
152 /* Converting between virtqueue no. and kernel tx/rx queue no.
153 * 0:rx0 1:tx0 2:rx1 3:tx1 ... 2N:rxN 2N+1:txN 2N+2:cvq
154 */
155 static int vq2txq(struct virtqueue *vq)
156 {
157 return (virtqueue_get_queue_index(vq) - 1) / 2;
158 }
160 static int txq2vq(int txq)
161 {
162 return txq * 2 + 1;
163 }
165 static int vq2rxq(struct virtqueue *vq)
166 {
167 return virtqueue_get_queue_index(vq) / 2;
168 }
170 static int rxq2vq(int rxq)
171 {
172 return rxq * 2;
173 }
175 static inline struct skb_vnet_hdr *skb_vnet_hdr(struct sk_buff *skb)
176 {
177 return (struct skb_vnet_hdr *)skb->cb;
178 }
180 /*
181 * private is used to chain pages for big packets, put the whole
182 * most recent used list in the beginning for reuse
183 */
184 static void give_pages(struct receive_queue *rq, struct page *page)
185 {
186 struct page *end;
188 /* Find end of list, sew whole thing into vi->rq.pages. */
189 for (end = page; end->private; end = (struct page *)end->private);
190 end->private = (unsigned long)rq->pages;
191 rq->pages = page;
192 }
194 static struct page *get_a_page(struct receive_queue *rq, gfp_t gfp_mask)
195 {
196 struct page *p = rq->pages;
198 if (p) {
199 rq->pages = (struct page *)p->private;
200 /* clear private here, it is used to chain pages */
201 p->private = 0;
202 } else
203 p = alloc_page(gfp_mask);
204 return p;
205 }
207 static void skb_xmit_done(struct virtqueue *vq)
208 {
209 struct virtnet_info *vi = vq->vdev->priv;
211 /* Suppress further interrupts. */
212 virtqueue_disable_cb(vq);
214 /* We were probably waiting for more output buffers. */
215 netif_wake_subqueue(vi->dev, vq2txq(vq));
216 }
218 static void set_skb_frag(struct sk_buff *skb, struct page *page,
219 unsigned int offset, unsigned int *len)
220 {
221 int size = min((unsigned)PAGE_SIZE - offset, *len);
222 int i = skb_shinfo(skb)->nr_frags;
224 __skb_fill_page_desc(skb, i, page, offset, size);
226 skb->data_len += size;
227 skb->len += size;
228 skb->truesize += PAGE_SIZE;
229 skb_shinfo(skb)->nr_frags++;
230 *len -= size;
231 }
233 /* Called from bottom half context */
234 static struct sk_buff *page_to_skb(struct receive_queue *rq,
235 struct page *page, unsigned int len)
236 {
237 struct virtnet_info *vi = rq->vq->vdev->priv;
238 struct sk_buff *skb;
239 struct skb_vnet_hdr *hdr;
240 unsigned int copy, hdr_len, offset;
241 char *p;
243 p = page_address(page);
245 /* copy small packet so we can reuse these pages for small data */
246 skb = netdev_alloc_skb_ip_align(vi->dev, GOOD_COPY_LEN);
247 if (unlikely(!skb))
248 return NULL;
250 hdr = skb_vnet_hdr(skb);
252 if (vi->mergeable_rx_bufs) {
253 hdr_len = sizeof hdr->mhdr;
254 offset = hdr_len;
255 } else {
256 hdr_len = sizeof hdr->hdr;
257 offset = sizeof(struct padded_vnet_hdr);
258 }
260 memcpy(hdr, p, hdr_len);
262 len -= hdr_len;
263 p += offset;
265 copy = len;
266 if (copy > skb_tailroom(skb))
267 copy = skb_tailroom(skb);
268 memcpy(skb_put(skb, copy), p, copy);
270 len -= copy;
271 offset += copy;
273 /*
274 * Verify that we can indeed put this data into a skb.
275 * This is here to handle cases when the device erroneously
276 * tries to receive more than is possible. This is usually
277 * the case of a broken device.
278 */
279 if (unlikely(len > MAX_SKB_FRAGS * PAGE_SIZE)) {
280 net_dbg_ratelimited("%s: too much data\n", skb->dev->name);
281 dev_kfree_skb(skb);
282 return NULL;
283 }
285 while (len) {
286 set_skb_frag(skb, page, offset, &len);
287 page = (struct page *)page->private;
288 offset = 0;
289 }
291 if (page)
292 give_pages(rq, page);
294 return skb;
295 }
297 static int receive_mergeable(struct receive_queue *rq, struct sk_buff *skb)
298 {
299 struct skb_vnet_hdr *hdr = skb_vnet_hdr(skb);
300 struct page *page;
301 int num_buf, i, len;
303 num_buf = hdr->mhdr.num_buffers;
304 while (--num_buf) {
305 i = skb_shinfo(skb)->nr_frags;
306 if (i >= MAX_SKB_FRAGS) {
307 pr_debug("%s: packet too long\n", skb->dev->name);
308 skb->dev->stats.rx_length_errors++;
309 return -EINVAL;
310 }
311 page = virtqueue_get_buf(rq->vq, &len);
312 if (!page) {
313 pr_debug("%s: rx error: %d buffers missing\n",
314 skb->dev->name, hdr->mhdr.num_buffers);
315 skb->dev->stats.rx_length_errors++;
316 return -EINVAL;
317 }
319 if (len > PAGE_SIZE)
320 len = PAGE_SIZE;
322 set_skb_frag(skb, page, 0, &len);
324 --rq->num;
325 }
326 return 0;
327 }
329 static void receive_buf(struct receive_queue *rq, void *buf, unsigned int len)
330 {
331 struct virtnet_info *vi = rq->vq->vdev->priv;
332 struct net_device *dev = vi->dev;
333 struct virtnet_stats *stats = this_cpu_ptr(vi->stats);
334 struct sk_buff *skb;
335 struct page *page;
336 struct skb_vnet_hdr *hdr;
338 if (unlikely(len < sizeof(struct virtio_net_hdr) + ETH_HLEN)) {
339 pr_debug("%s: short packet %i\n", dev->name, len);
340 dev->stats.rx_length_errors++;
341 if (vi->mergeable_rx_bufs || vi->big_packets)
342 give_pages(rq, buf);
343 else
344 dev_kfree_skb(buf);
345 return;
346 }
348 if (!vi->mergeable_rx_bufs && !vi->big_packets) {
349 skb = buf;
350 len -= sizeof(struct virtio_net_hdr);
351 skb_trim(skb, len);
352 } else {
353 page = buf;
354 skb = page_to_skb(rq, page, len);
355 if (unlikely(!skb)) {
356 dev->stats.rx_dropped++;
357 give_pages(rq, page);
358 return;
359 }
360 if (vi->mergeable_rx_bufs)
361 if (receive_mergeable(rq, skb)) {
362 dev_kfree_skb(skb);
363 return;
364 }
365 }
367 hdr = skb_vnet_hdr(skb);
369 u64_stats_update_begin(&stats->rx_syncp);
370 stats->rx_bytes += skb->len;
371 stats->rx_packets++;
372 u64_stats_update_end(&stats->rx_syncp);
374 if (hdr->hdr.flags & VIRTIO_NET_HDR_F_NEEDS_CSUM) {
375 pr_debug("Needs csum!\n");
376 if (!skb_partial_csum_set(skb,
377 hdr->hdr.csum_start,
378 hdr->hdr.csum_offset))
379 goto frame_err;
380 } else if (hdr->hdr.flags & VIRTIO_NET_HDR_F_DATA_VALID) {
381 skb->ip_summed = CHECKSUM_UNNECESSARY;
382 }
384 skb->protocol = eth_type_trans(skb, dev);
385 pr_debug("Receiving skb proto 0x%04x len %i type %i\n",
386 ntohs(skb->protocol), skb->len, skb->pkt_type);
388 if (hdr->hdr.gso_type != VIRTIO_NET_HDR_GSO_NONE) {
389 pr_debug("GSO!\n");
390 switch (hdr->hdr.gso_type & ~VIRTIO_NET_HDR_GSO_ECN) {
391 case VIRTIO_NET_HDR_GSO_TCPV4:
392 skb_shinfo(skb)->gso_type = SKB_GSO_TCPV4;
393 break;
394 case VIRTIO_NET_HDR_GSO_UDP:
395 skb_shinfo(skb)->gso_type = SKB_GSO_UDP;
396 break;
397 case VIRTIO_NET_HDR_GSO_TCPV6:
398 skb_shinfo(skb)->gso_type = SKB_GSO_TCPV6;
399 break;
400 default:
401 net_warn_ratelimited("%s: bad gso type %u.\n",
402 dev->name, hdr->hdr.gso_type);
403 goto frame_err;
404 }
406 if (hdr->hdr.gso_type & VIRTIO_NET_HDR_GSO_ECN)
407 skb_shinfo(skb)->gso_type |= SKB_GSO_TCP_ECN;
409 skb_shinfo(skb)->gso_size = hdr->hdr.gso_size;
410 if (skb_shinfo(skb)->gso_size == 0) {
411 net_warn_ratelimited("%s: zero gso size.\n", dev->name);
412 goto frame_err;
413 }
415 /* Header must be checked, and gso_segs computed. */
416 skb_shinfo(skb)->gso_type |= SKB_GSO_DODGY;
417 skb_shinfo(skb)->gso_segs = 0;
418 }
420 netif_receive_skb(skb);
421 return;
423 frame_err:
424 dev->stats.rx_frame_errors++;
425 dev_kfree_skb(skb);
426 }
428 static int add_recvbuf_small(struct receive_queue *rq, gfp_t gfp)
429 {
430 struct virtnet_info *vi = rq->vq->vdev->priv;
431 struct sk_buff *skb;
432 struct skb_vnet_hdr *hdr;
433 int err;
435 skb = __netdev_alloc_skb_ip_align(vi->dev, MAX_PACKET_LEN, gfp);
436 if (unlikely(!skb))
437 return -ENOMEM;
439 skb_put(skb, MAX_PACKET_LEN);
441 hdr = skb_vnet_hdr(skb);
442 sg_set_buf(rq->sg, &hdr->hdr, sizeof hdr->hdr);
444 skb_to_sgvec(skb, rq->sg + 1, 0, skb->len);
446 err = virtqueue_add_buf(rq->vq, rq->sg, 0, 2, skb, gfp);
447 if (err < 0)
448 dev_kfree_skb(skb);
450 return err;
451 }
453 static int add_recvbuf_big(struct receive_queue *rq, gfp_t gfp)
454 {
455 struct page *first, *list = NULL;
456 char *p;
457 int i, err, offset;
459 /* page in rq->sg[MAX_SKB_FRAGS + 1] is list tail */
460 for (i = MAX_SKB_FRAGS + 1; i > 1; --i) {
461 first = get_a_page(rq, gfp);
462 if (!first) {
463 if (list)
464 give_pages(rq, list);
465 return -ENOMEM;
466 }
467 sg_set_buf(&rq->sg[i], page_address(first), PAGE_SIZE);
469 /* chain new page in list head to match sg */
470 first->private = (unsigned long)list;
471 list = first;
472 }
474 first = get_a_page(rq, gfp);
475 if (!first) {
476 give_pages(rq, list);
477 return -ENOMEM;
478 }
479 p = page_address(first);
481 /* rq->sg[0], rq->sg[1] share the same page */
482 /* a separated rq->sg[0] for virtio_net_hdr only due to QEMU bug */
483 sg_set_buf(&rq->sg[0], p, sizeof(struct virtio_net_hdr));
485 /* rq->sg[1] for data packet, from offset */
486 offset = sizeof(struct padded_vnet_hdr);
487 sg_set_buf(&rq->sg[1], p + offset, PAGE_SIZE - offset);
489 /* chain first in list head */
490 first->private = (unsigned long)list;
491 err = virtqueue_add_buf(rq->vq, rq->sg, 0, MAX_SKB_FRAGS + 2,
492 first, gfp);
493 if (err < 0)
494 give_pages(rq, first);
496 return err;
497 }
499 static int add_recvbuf_mergeable(struct receive_queue *rq, gfp_t gfp)
500 {
501 struct page *page;
502 int err;
504 page = get_a_page(rq, gfp);
505 if (!page)
506 return -ENOMEM;
508 sg_init_one(rq->sg, page_address(page), PAGE_SIZE);
510 err = virtqueue_add_buf(rq->vq, rq->sg, 0, 1, page, gfp);
511 if (err < 0)
512 give_pages(rq, page);
514 return err;
515 }
517 /*
518 * Returns false if we couldn't fill entirely (OOM).
519 *
520 * Normally run in the receive path, but can also be run from ndo_open
521 * before we're receiving packets, or from refill_work which is
522 * careful to disable receiving (using napi_disable).
523 */
524 static bool try_fill_recv(struct receive_queue *rq, gfp_t gfp)
525 {
526 struct virtnet_info *vi = rq->vq->vdev->priv;
527 int err;
528 bool oom;
530 do {
531 if (vi->mergeable_rx_bufs)
532 err = add_recvbuf_mergeable(rq, gfp);
533 else if (vi->big_packets)
534 err = add_recvbuf_big(rq, gfp);
535 else
536 err = add_recvbuf_small(rq, gfp);
538 oom = err == -ENOMEM;
539 if (err)
540 break;
541 ++rq->num;
542 } while (rq->vq->num_free);
543 if (unlikely(rq->num > rq->max))
544 rq->max = rq->num;
545 virtqueue_kick(rq->vq);
546 return !oom;
547 }
549 static void skb_recv_done(struct virtqueue *rvq)
550 {
551 struct virtnet_info *vi = rvq->vdev->priv;
552 struct receive_queue *rq = &vi->rq[vq2rxq(rvq)];
554 /* Schedule NAPI, Suppress further interrupts if successful. */
555 if (napi_schedule_prep(&rq->napi)) {
556 virtqueue_disable_cb(rvq);
557 __napi_schedule(&rq->napi);
558 }
559 }
561 static void virtnet_napi_enable(struct receive_queue *rq)
562 {
563 napi_enable(&rq->napi);
565 /* If all buffers were filled by other side before we napi_enabled, we
566 * won't get another interrupt, so process any outstanding packets
567 * now. virtnet_poll wants re-enable the queue, so we disable here.
568 * We synchronize against interrupts via NAPI_STATE_SCHED */
569 if (napi_schedule_prep(&rq->napi)) {
570 virtqueue_disable_cb(rq->vq);
571 local_bh_disable();
572 __napi_schedule(&rq->napi);
573 local_bh_enable();
574 }
575 }
577 static void refill_work(struct work_struct *work)
578 {
579 struct virtnet_info *vi =
580 container_of(work, struct virtnet_info, refill.work);
581 bool still_empty;
582 int i;
584 for (i = 0; i < vi->max_queue_pairs; i++) {
585 struct receive_queue *rq = &vi->rq[i];
587 napi_disable(&rq->napi);
588 still_empty = !try_fill_recv(rq, GFP_KERNEL);
589 virtnet_napi_enable(rq);
591 /* In theory, this can happen: if we don't get any buffers in
592 * we will *never* try to fill again.
593 */
594 if (still_empty)
595 schedule_delayed_work(&vi->refill, HZ/2);
596 }
597 }
599 static int virtnet_poll(struct napi_struct *napi, int budget)
600 {
601 struct receive_queue *rq =
602 container_of(napi, struct receive_queue, napi);
603 struct virtnet_info *vi = rq->vq->vdev->priv;
604 void *buf;
605 unsigned int len, received = 0;
607 again:
608 while (received < budget &&
609 (buf = virtqueue_get_buf(rq->vq, &len)) != NULL) {
610 receive_buf(rq, buf, len);
611 --rq->num;
612 received++;
613 }
615 if (rq->num < rq->max / 2) {
616 if (!try_fill_recv(rq, GFP_ATOMIC))
617 schedule_delayed_work(&vi->refill, 0);
618 }
620 /* Out of packets? */
621 if (received < budget) {
622 napi_complete(napi);
623 if (unlikely(!virtqueue_enable_cb(rq->vq)) &&
624 napi_schedule_prep(napi)) {
625 virtqueue_disable_cb(rq->vq);
626 __napi_schedule(napi);
627 goto again;
628 }
629 }
631 return received;
632 }
634 static int virtnet_open(struct net_device *dev)
635 {
636 struct virtnet_info *vi = netdev_priv(dev);
637 int i;
639 for (i = 0; i < vi->max_queue_pairs; i++) {
640 /* Make sure we have some buffers: if oom use wq. */
641 if (!try_fill_recv(&vi->rq[i], GFP_KERNEL))
642 schedule_delayed_work(&vi->refill, 0);
643 virtnet_napi_enable(&vi->rq[i]);
644 }
646 return 0;
647 }
649 static void free_old_xmit_skbs(struct send_queue *sq)
650 {
651 struct sk_buff *skb;
652 unsigned int len;
653 struct virtnet_info *vi = sq->vq->vdev->priv;
654 struct virtnet_stats *stats = this_cpu_ptr(vi->stats);
656 while ((skb = virtqueue_get_buf(sq->vq, &len)) != NULL) {
657 pr_debug("Sent skb %p\n", skb);
659 u64_stats_update_begin(&stats->tx_syncp);
660 stats->tx_bytes += skb->len;
661 stats->tx_packets++;
662 u64_stats_update_end(&stats->tx_syncp);
664 dev_kfree_skb_any(skb);
665 }
666 }
668 static int xmit_skb(struct send_queue *sq, struct sk_buff *skb)
669 {
670 struct skb_vnet_hdr *hdr = skb_vnet_hdr(skb);
671 const unsigned char *dest = ((struct ethhdr *)skb->data)->h_dest;
672 struct virtnet_info *vi = sq->vq->vdev->priv;
673 unsigned num_sg;
675 pr_debug("%s: xmit %p %pM\n", vi->dev->name, skb, dest);
677 if (skb->ip_summed == CHECKSUM_PARTIAL) {
678 hdr->hdr.flags = VIRTIO_NET_HDR_F_NEEDS_CSUM;
679 hdr->hdr.csum_start = skb_checksum_start_offset(skb);
680 hdr->hdr.csum_offset = skb->csum_offset;
681 } else {
682 hdr->hdr.flags = 0;
683 hdr->hdr.csum_offset = hdr->hdr.csum_start = 0;
684 }
686 if (skb_is_gso(skb)) {
687 hdr->hdr.hdr_len = skb_headlen(skb);
688 hdr->hdr.gso_size = skb_shinfo(skb)->gso_size;
689 if (skb_shinfo(skb)->gso_type & SKB_GSO_TCPV4)
690 hdr->hdr.gso_type = VIRTIO_NET_HDR_GSO_TCPV4;
691 else if (skb_shinfo(skb)->gso_type & SKB_GSO_TCPV6)
692 hdr->hdr.gso_type = VIRTIO_NET_HDR_GSO_TCPV6;
693 else if (skb_shinfo(skb)->gso_type & SKB_GSO_UDP)
694 hdr->hdr.gso_type = VIRTIO_NET_HDR_GSO_UDP;
695 else
696 BUG();
697 if (skb_shinfo(skb)->gso_type & SKB_GSO_TCP_ECN)
698 hdr->hdr.gso_type |= VIRTIO_NET_HDR_GSO_ECN;
699 } else {
700 hdr->hdr.gso_type = VIRTIO_NET_HDR_GSO_NONE;
701 hdr->hdr.gso_size = hdr->hdr.hdr_len = 0;
702 }
704 hdr->mhdr.num_buffers = 0;
706 /* Encode metadata header at front. */
707 if (vi->mergeable_rx_bufs)
708 sg_set_buf(sq->sg, &hdr->mhdr, sizeof hdr->mhdr);
709 else
710 sg_set_buf(sq->sg, &hdr->hdr, sizeof hdr->hdr);
712 num_sg = skb_to_sgvec(skb, sq->sg + 1, 0, skb->len) + 1;
713 return virtqueue_add_buf(sq->vq, sq->sg, num_sg,
714 0, skb, GFP_ATOMIC);
715 }
717 static netdev_tx_t start_xmit(struct sk_buff *skb, struct net_device *dev)
718 {
719 struct virtnet_info *vi = netdev_priv(dev);
720 int qnum = skb_get_queue_mapping(skb);
721 struct send_queue *sq = &vi->sq[qnum];
722 int err;
724 /* Free up any pending old buffers before queueing new ones. */
725 free_old_xmit_skbs(sq);
727 /* Try to transmit */
728 err = xmit_skb(sq, skb);
730 /* This should not happen! */
731 if (unlikely(err)) {
732 dev->stats.tx_fifo_errors++;
733 if (net_ratelimit())
734 dev_warn(&dev->dev,
735 "Unexpected TXQ (%d) queue failure: %d\n", qnum, err);
736 dev->stats.tx_dropped++;
737 kfree_skb(skb);
738 return NETDEV_TX_OK;
739 }
740 virtqueue_kick(sq->vq);
742 /* Don't wait up for transmitted skbs to be freed. */
743 skb_orphan(skb);
744 nf_reset(skb);
746 /* Apparently nice girls don't return TX_BUSY; stop the queue
747 * before it gets out of hand. Naturally, this wastes entries. */
748 if (sq->vq->num_free < 2+MAX_SKB_FRAGS) {
749 netif_stop_subqueue(dev, qnum);
750 if (unlikely(!virtqueue_enable_cb_delayed(sq->vq))) {
751 /* More just got used, free them then recheck. */
752 free_old_xmit_skbs(sq);
753 if (sq->vq->num_free >= 2+MAX_SKB_FRAGS) {
754 netif_start_subqueue(dev, qnum);
755 virtqueue_disable_cb(sq->vq);
756 }
757 }
758 }
760 return NETDEV_TX_OK;
761 }
763 static int virtnet_set_mac_address(struct net_device *dev, void *p)
764 {
765 struct virtnet_info *vi = netdev_priv(dev);
766 struct virtio_device *vdev = vi->vdev;
767 int ret;
769 ret = eth_mac_addr(dev, p);
770 if (ret)
771 return ret;
773 if (virtio_has_feature(vdev, VIRTIO_NET_F_MAC))
774 vdev->config->set(vdev, offsetof(struct virtio_net_config, mac),
775 dev->dev_addr, dev->addr_len);
777 return 0;
778 }
780 static struct rtnl_link_stats64 *virtnet_stats(struct net_device *dev,
781 struct rtnl_link_stats64 *tot)
782 {
783 struct virtnet_info *vi = netdev_priv(dev);
784 int cpu;
785 unsigned int start;
787 for_each_possible_cpu(cpu) {
788 struct virtnet_stats *stats = per_cpu_ptr(vi->stats, cpu);
789 u64 tpackets, tbytes, rpackets, rbytes;
791 do {
792 start = u64_stats_fetch_begin_bh(&stats->tx_syncp);
793 tpackets = stats->tx_packets;
794 tbytes = stats->tx_bytes;
795 } while (u64_stats_fetch_retry_bh(&stats->tx_syncp, start));
797 do {
798 start = u64_stats_fetch_begin_bh(&stats->rx_syncp);
799 rpackets = stats->rx_packets;
800 rbytes = stats->rx_bytes;
801 } while (u64_stats_fetch_retry_bh(&stats->rx_syncp, start));
803 tot->rx_packets += rpackets;
804 tot->tx_packets += tpackets;
805 tot->rx_bytes += rbytes;
806 tot->tx_bytes += tbytes;
807 }
809 tot->tx_dropped = dev->stats.tx_dropped;
810 tot->tx_fifo_errors = dev->stats.tx_fifo_errors;
811 tot->rx_dropped = dev->stats.rx_dropped;
812 tot->rx_length_errors = dev->stats.rx_length_errors;
813 tot->rx_frame_errors = dev->stats.rx_frame_errors;
815 return tot;
816 }
818 #ifdef CONFIG_NET_POLL_CONTROLLER
819 static void virtnet_netpoll(struct net_device *dev)
820 {
821 struct virtnet_info *vi = netdev_priv(dev);
822 int i;
824 for (i = 0; i < vi->curr_queue_pairs; i++)
825 napi_schedule(&vi->rq[i].napi);
826 }
827 #endif
829 /*
830 * Send command via the control virtqueue and check status. Commands
831 * supported by the hypervisor, as indicated by feature bits, should
832 * never fail unless improperly formated.
833 */
834 static bool virtnet_send_command(struct virtnet_info *vi, u8 class, u8 cmd,
835 struct scatterlist *data, int out, int in)
836 {
837 struct scatterlist *s, sg[VIRTNET_SEND_COMMAND_SG_MAX + 2];
838 struct virtio_net_ctrl_hdr ctrl;
839 virtio_net_ctrl_ack status = ~0;
840 unsigned int tmp;
841 int i;
843 /* Caller should know better */
844 BUG_ON(!virtio_has_feature(vi->vdev, VIRTIO_NET_F_CTRL_VQ) ||
845 (out + in > VIRTNET_SEND_COMMAND_SG_MAX));
847 out++; /* Add header */
848 in++; /* Add return status */
850 ctrl.class = class;
851 ctrl.cmd = cmd;
853 sg_init_table(sg, out + in);
855 sg_set_buf(&sg[0], &ctrl, sizeof(ctrl));
856 for_each_sg(data, s, out + in - 2, i)
857 sg_set_buf(&sg[i + 1], sg_virt(s), s->length);
858 sg_set_buf(&sg[out + in - 1], &status, sizeof(status));
860 BUG_ON(virtqueue_add_buf(vi->cvq, sg, out, in, vi, GFP_ATOMIC) < 0);
862 virtqueue_kick(vi->cvq);
864 /*
865 * Spin for a response, the kick causes an ioport write, trapping
866 * into the hypervisor, so the request should be handled immediately.
867 */
868 while (!virtqueue_get_buf(vi->cvq, &tmp))
869 cpu_relax();
871 return status == VIRTIO_NET_OK;
872 }
874 static void virtnet_ack_link_announce(struct virtnet_info *vi)
875 {
876 rtnl_lock();
877 if (!virtnet_send_command(vi, VIRTIO_NET_CTRL_ANNOUNCE,
878 VIRTIO_NET_CTRL_ANNOUNCE_ACK, NULL,
879 0, 0))
880 dev_warn(&vi->dev->dev, "Failed to ack link announce.\n");
881 rtnl_unlock();
882 }
884 static int virtnet_set_queues(struct virtnet_info *vi, u16 queue_pairs)
885 {
886 struct scatterlist sg;
887 struct virtio_net_ctrl_mq s;
888 struct net_device *dev = vi->dev;
890 if (!vi->has_cvq || !virtio_has_feature(vi->vdev, VIRTIO_NET_F_MQ))
891 return 0;
893 s.virtqueue_pairs = queue_pairs;
894 sg_init_one(&sg, &s, sizeof(s));
896 if (!virtnet_send_command(vi, VIRTIO_NET_CTRL_MQ,
897 VIRTIO_NET_CTRL_MQ_VQ_PAIRS_SET, &sg, 1, 0)){
898 dev_warn(&dev->dev, "Fail to set num of queue pairs to %d\n",
899 queue_pairs);
900 return -EINVAL;
901 } else
902 vi->curr_queue_pairs = queue_pairs;
904 return 0;
905 }
907 static int virtnet_close(struct net_device *dev)
908 {
909 struct virtnet_info *vi = netdev_priv(dev);
910 int i;
912 /* Make sure refill_work doesn't re-enable napi! */
913 cancel_delayed_work_sync(&vi->refill);
915 for (i = 0; i < vi->max_queue_pairs; i++)
916 napi_disable(&vi->rq[i].napi);
918 return 0;
919 }
921 static void virtnet_set_rx_mode(struct net_device *dev)
922 {
923 struct virtnet_info *vi = netdev_priv(dev);
924 struct scatterlist sg[2];
925 u8 promisc, allmulti;
926 struct virtio_net_ctrl_mac *mac_data;
927 struct netdev_hw_addr *ha;
928 int uc_count;
929 int mc_count;
930 void *buf;
931 int i;
933 /* We can't dynamicaly set ndo_set_rx_mode, so return gracefully */
934 if (!virtio_has_feature(vi->vdev, VIRTIO_NET_F_CTRL_RX))
935 return;
937 promisc = ((dev->flags & IFF_PROMISC) != 0);
938 allmulti = ((dev->flags & IFF_ALLMULTI) != 0);
940 sg_init_one(sg, &promisc, sizeof(promisc));
942 if (!virtnet_send_command(vi, VIRTIO_NET_CTRL_RX,
943 VIRTIO_NET_CTRL_RX_PROMISC,
944 sg, 1, 0))
945 dev_warn(&dev->dev, "Failed to %sable promisc mode.\n",
946 promisc ? "en" : "dis");
948 sg_init_one(sg, &allmulti, sizeof(allmulti));
950 if (!virtnet_send_command(vi, VIRTIO_NET_CTRL_RX,
951 VIRTIO_NET_CTRL_RX_ALLMULTI,
952 sg, 1, 0))
953 dev_warn(&dev->dev, "Failed to %sable allmulti mode.\n",
954 allmulti ? "en" : "dis");
956 uc_count = netdev_uc_count(dev);
957 mc_count = netdev_mc_count(dev);
958 /* MAC filter - use one buffer for both lists */
959 buf = kzalloc(((uc_count + mc_count) * ETH_ALEN) +
960 (2 * sizeof(mac_data->entries)), GFP_ATOMIC);
961 mac_data = buf;
962 if (!buf) {
963 dev_warn(&dev->dev, "No memory for MAC address buffer\n");
964 return;
965 }
967 sg_init_table(sg, 2);
969 /* Store the unicast list and count in the front of the buffer */
970 mac_data->entries = uc_count;
971 i = 0;
972 netdev_for_each_uc_addr(ha, dev)
973 memcpy(&mac_data->macs[i++][0], ha->addr, ETH_ALEN);
975 sg_set_buf(&sg[0], mac_data,
976 sizeof(mac_data->entries) + (uc_count * ETH_ALEN));
978 /* multicast list and count fill the end */
979 mac_data = (void *)&mac_data->macs[uc_count][0];
981 mac_data->entries = mc_count;
982 i = 0;
983 netdev_for_each_mc_addr(ha, dev)
984 memcpy(&mac_data->macs[i++][0], ha->addr, ETH_ALEN);
986 sg_set_buf(&sg[1], mac_data,
987 sizeof(mac_data->entries) + (mc_count * ETH_ALEN));
989 if (!virtnet_send_command(vi, VIRTIO_NET_CTRL_MAC,
990 VIRTIO_NET_CTRL_MAC_TABLE_SET,
991 sg, 2, 0))
992 dev_warn(&dev->dev, "Failed to set MAC fitler table.\n");
994 kfree(buf);
995 }
997 static int virtnet_vlan_rx_add_vid(struct net_device *dev, u16 vid)
998 {
999 struct virtnet_info *vi = netdev_priv(dev);
1000 struct scatterlist sg;
1002 sg_init_one(&sg, &vid, sizeof(vid));
1004 if (!virtnet_send_command(vi, VIRTIO_NET_CTRL_VLAN,
1005 VIRTIO_NET_CTRL_VLAN_ADD, &sg, 1, 0))
1006 dev_warn(&dev->dev, "Failed to add VLAN ID %d.\n", vid);
1007 return 0;
1008 }
1010 static int virtnet_vlan_rx_kill_vid(struct net_device *dev, u16 vid)
1011 {
1012 struct virtnet_info *vi = netdev_priv(dev);
1013 struct scatterlist sg;
1015 sg_init_one(&sg, &vid, sizeof(vid));
1017 if (!virtnet_send_command(vi, VIRTIO_NET_CTRL_VLAN,
1018 VIRTIO_NET_CTRL_VLAN_DEL, &sg, 1, 0))
1019 dev_warn(&dev->dev, "Failed to kill VLAN ID %d.\n", vid);
1020 return 0;
1021 }
1023 static void virtnet_clean_affinity(struct virtnet_info *vi, long hcpu)
1024 {
1025 int i;
1026 int cpu;
1028 if (vi->affinity_hint_set) {
1029 for (i = 0; i < vi->max_queue_pairs; i++) {
1030 virtqueue_set_affinity(vi->rq[i].vq, -1);
1031 virtqueue_set_affinity(vi->sq[i].vq, -1);
1032 }
1034 vi->affinity_hint_set = false;
1035 }
1037 i = 0;
1038 for_each_online_cpu(cpu) {
1039 if (cpu == hcpu) {
1040 *per_cpu_ptr(vi->vq_index, cpu) = -1;
1041 } else {
1042 *per_cpu_ptr(vi->vq_index, cpu) =
1043 ++i % vi->curr_queue_pairs;
1044 }
1045 }
1046 }
1048 static void virtnet_set_affinity(struct virtnet_info *vi)
1049 {
1050 int i;
1051 int cpu;
1053 /* In multiqueue mode, when the number of cpu is equal to the number of
1054 * queue pairs, we let the queue pairs to be private to one cpu by
1055 * setting the affinity hint to eliminate the contention.
1056 */
1057 if (vi->curr_queue_pairs == 1 ||
1058 vi->max_queue_pairs != num_online_cpus()) {
1059 virtnet_clean_affinity(vi, -1);
1060 return;
1061 }
1063 i = 0;
1064 for_each_online_cpu(cpu) {
1065 virtqueue_set_affinity(vi->rq[i].vq, cpu);
1066 virtqueue_set_affinity(vi->sq[i].vq, cpu);
1067 *per_cpu_ptr(vi->vq_index, cpu) = i;
1068 i++;
1069 }
1071 vi->affinity_hint_set = true;
1072 }
1074 static int virtnet_cpu_callback(struct notifier_block *nfb,
1075 unsigned long action, void *hcpu)
1076 {
1077 struct virtnet_info *vi = container_of(nfb, struct virtnet_info, nb);
1079 switch(action & ~CPU_TASKS_FROZEN) {
1080 case CPU_ONLINE:
1081 case CPU_DOWN_FAILED:
1082 case CPU_DEAD:
1083 virtnet_set_affinity(vi);
1084 break;
1085 case CPU_DOWN_PREPARE:
1086 virtnet_clean_affinity(vi, (long)hcpu);
1087 break;
1088 default:
1089 break;
1090 }
1091 return NOTIFY_OK;
1092 }
1094 static void virtnet_get_ringparam(struct net_device *dev,
1095 struct ethtool_ringparam *ring)
1096 {
1097 struct virtnet_info *vi = netdev_priv(dev);
1099 ring->rx_max_pending = virtqueue_get_vring_size(vi->rq[0].vq);
1100 ring->tx_max_pending = virtqueue_get_vring_size(vi->sq[0].vq);
1101 ring->rx_pending = ring->rx_max_pending;
1102 ring->tx_pending = ring->tx_max_pending;
1103 }
1106 static void virtnet_get_drvinfo(struct net_device *dev,
1107 struct ethtool_drvinfo *info)
1108 {
1109 struct virtnet_info *vi = netdev_priv(dev);
1110 struct virtio_device *vdev = vi->vdev;
1112 strlcpy(info->driver, KBUILD_MODNAME, sizeof(info->driver));
1113 strlcpy(info->version, VIRTNET_DRIVER_VERSION, sizeof(info->version));
1114 strlcpy(info->bus_info, virtio_bus_name(vdev), sizeof(info->bus_info));
1116 }
1118 /* TODO: Eliminate OOO packets during switching */
1119 static int virtnet_set_channels(struct net_device *dev,
1120 struct ethtool_channels *channels)
1121 {
1122 struct virtnet_info *vi = netdev_priv(dev);
1123 u16 queue_pairs = channels->combined_count;
1124 int err;
1126 /* We don't support separate rx/tx channels.
1127 * We don't allow setting 'other' channels.
1128 */
1129 if (channels->rx_count || channels->tx_count || channels->other_count)
1130 return -EINVAL;
1132 if (queue_pairs > vi->max_queue_pairs)
1133 return -EINVAL;
1135 get_online_cpus();
1136 err = virtnet_set_queues(vi, queue_pairs);
1137 if (!err) {
1138 netif_set_real_num_tx_queues(dev, queue_pairs);
1139 netif_set_real_num_rx_queues(dev, queue_pairs);
1141 virtnet_set_affinity(vi);
1142 }
1143 put_online_cpus();
1145 return err;
1146 }
1148 static void virtnet_get_channels(struct net_device *dev,
1149 struct ethtool_channels *channels)
1150 {
1151 struct virtnet_info *vi = netdev_priv(dev);
1153 channels->combined_count = vi->curr_queue_pairs;
1154 channels->max_combined = vi->max_queue_pairs;
1155 channels->max_other = 0;
1156 channels->rx_count = 0;
1157 channels->tx_count = 0;
1158 channels->other_count = 0;
1159 }
1161 static const struct ethtool_ops virtnet_ethtool_ops = {
1162 .get_drvinfo = virtnet_get_drvinfo,
1163 .get_link = ethtool_op_get_link,
1164 .get_ringparam = virtnet_get_ringparam,
1165 .set_channels = virtnet_set_channels,
1166 .get_channels = virtnet_get_channels,
1167 };
1169 #define MIN_MTU 68
1170 #define MAX_MTU 65535
1172 static int virtnet_change_mtu(struct net_device *dev, int new_mtu)
1173 {
1174 if (new_mtu < MIN_MTU || new_mtu > MAX_MTU)
1175 return -EINVAL;
1176 dev->mtu = new_mtu;
1177 return 0;
1178 }
1180 /* To avoid contending a lock hold by a vcpu who would exit to host, select the
1181 * txq based on the processor id.
1182 */
1183 static u16 virtnet_select_queue(struct net_device *dev, struct sk_buff *skb)
1184 {
1185 int txq;
1186 struct virtnet_info *vi = netdev_priv(dev);
1188 if (skb_rx_queue_recorded(skb)) {
1189 txq = skb_get_rx_queue(skb);
1190 } else {
1191 txq = *__this_cpu_ptr(vi->vq_index);
1192 if (txq == -1)
1193 txq = 0;
1194 }
1196 while (unlikely(txq >= dev->real_num_tx_queues))
1197 txq -= dev->real_num_tx_queues;
1199 return txq;
1200 }
1202 static const struct net_device_ops virtnet_netdev = {
1203 .ndo_open = virtnet_open,
1204 .ndo_stop = virtnet_close,
1205 .ndo_start_xmit = start_xmit,
1206 .ndo_validate_addr = eth_validate_addr,
1207 .ndo_set_mac_address = virtnet_set_mac_address,
1208 .ndo_set_rx_mode = virtnet_set_rx_mode,
1209 .ndo_change_mtu = virtnet_change_mtu,
1210 .ndo_get_stats64 = virtnet_stats,
1211 .ndo_vlan_rx_add_vid = virtnet_vlan_rx_add_vid,
1212 .ndo_vlan_rx_kill_vid = virtnet_vlan_rx_kill_vid,
1213 .ndo_select_queue = virtnet_select_queue,
1214 #ifdef CONFIG_NET_POLL_CONTROLLER
1215 .ndo_poll_controller = virtnet_netpoll,
1216 #endif
1217 };
1219 static void virtnet_config_changed_work(struct work_struct *work)
1220 {
1221 struct virtnet_info *vi =
1222 container_of(work, struct virtnet_info, config_work);
1223 u16 v;
1225 mutex_lock(&vi->config_lock);
1226 if (!vi->config_enable)
1227 goto done;
1229 if (virtio_config_val(vi->vdev, VIRTIO_NET_F_STATUS,
1230 offsetof(struct virtio_net_config, status),
1231 &v) < 0)
1232 goto done;
1234 if (v & VIRTIO_NET_S_ANNOUNCE) {
1235 netdev_notify_peers(vi->dev);
1236 virtnet_ack_link_announce(vi);
1237 }
1239 /* Ignore unknown (future) status bits */
1240 v &= VIRTIO_NET_S_LINK_UP;
1242 if (vi->status == v)
1243 goto done;
1245 vi->status = v;
1247 if (vi->status & VIRTIO_NET_S_LINK_UP) {
1248 netif_carrier_on(vi->dev);
1249 netif_tx_wake_all_queues(vi->dev);
1250 } else {
1251 netif_carrier_off(vi->dev);
1252 netif_tx_stop_all_queues(vi->dev);
1253 }
1254 done:
1255 mutex_unlock(&vi->config_lock);
1256 }
1258 static void virtnet_config_changed(struct virtio_device *vdev)
1259 {
1260 struct virtnet_info *vi = vdev->priv;
1262 schedule_work(&vi->config_work);
1263 }
1265 static void virtnet_free_queues(struct virtnet_info *vi)
1266 {
1267 kfree(vi->rq);
1268 kfree(vi->sq);
1269 }
1271 static void free_receive_bufs(struct virtnet_info *vi)
1272 {
1273 int i;
1275 for (i = 0; i < vi->max_queue_pairs; i++) {
1276 while (vi->rq[i].pages)
1277 __free_pages(get_a_page(&vi->rq[i], GFP_KERNEL), 0);
1278 }
1279 }
1281 static void free_unused_bufs(struct virtnet_info *vi)
1282 {
1283 void *buf;
1284 int i;
1286 for (i = 0; i < vi->max_queue_pairs; i++) {
1287 struct virtqueue *vq = vi->sq[i].vq;
1288 while ((buf = virtqueue_detach_unused_buf(vq)) != NULL)
1289 dev_kfree_skb(buf);
1290 }
1292 for (i = 0; i < vi->max_queue_pairs; i++) {
1293 struct virtqueue *vq = vi->rq[i].vq;
1295 while ((buf = virtqueue_detach_unused_buf(vq)) != NULL) {
1296 if (vi->mergeable_rx_bufs || vi->big_packets)
1297 give_pages(&vi->rq[i], buf);
1298 else
1299 dev_kfree_skb(buf);
1300 --vi->rq[i].num;
1301 }
1302 BUG_ON(vi->rq[i].num != 0);
1303 }
1304 }
1306 static void virtnet_del_vqs(struct virtnet_info *vi)
1307 {
1308 struct virtio_device *vdev = vi->vdev;
1310 virtnet_clean_affinity(vi, -1);
1312 vdev->config->del_vqs(vdev);
1314 virtnet_free_queues(vi);
1315 }
1317 static int virtnet_find_vqs(struct virtnet_info *vi)
1318 {
1319 vq_callback_t **callbacks;
1320 struct virtqueue **vqs;
1321 int ret = -ENOMEM;
1322 int i, total_vqs;
1323 const char **names;
1325 /* We expect 1 RX virtqueue followed by 1 TX virtqueue, followed by
1326 * possible N-1 RX/TX queue pairs used in multiqueue mode, followed by
1327 * possible control vq.
1328 */
1329 total_vqs = vi->max_queue_pairs * 2 +
1330 virtio_has_feature(vi->vdev, VIRTIO_NET_F_CTRL_VQ);
1332 /* Allocate space for find_vqs parameters */
1333 vqs = kzalloc(total_vqs * sizeof(*vqs), GFP_KERNEL);
1334 if (!vqs)
1335 goto err_vq;
1336 callbacks = kmalloc(total_vqs * sizeof(*callbacks), GFP_KERNEL);
1337 if (!callbacks)
1338 goto err_callback;
1339 names = kmalloc(total_vqs * sizeof(*names), GFP_KERNEL);
1340 if (!names)
1341 goto err_names;
1343 /* Parameters for control virtqueue, if any */
1344 if (vi->has_cvq) {
1345 callbacks[total_vqs - 1] = NULL;
1346 names[total_vqs - 1] = "control";
1347 }
1349 /* Allocate/initialize parameters for send/receive virtqueues */
1350 for (i = 0; i < vi->max_queue_pairs; i++) {
1351 callbacks[rxq2vq(i)] = skb_recv_done;
1352 callbacks[txq2vq(i)] = skb_xmit_done;
1353 sprintf(vi->rq[i].name, "input.%d", i);
1354 sprintf(vi->sq[i].name, "output.%d", i);
1355 names[rxq2vq(i)] = vi->rq[i].name;
1356 names[txq2vq(i)] = vi->sq[i].name;
1357 }
1359 ret = vi->vdev->config->find_vqs(vi->vdev, total_vqs, vqs, callbacks,
1360 names);
1361 if (ret)
1362 goto err_find;
1364 if (vi->has_cvq) {
1365 vi->cvq = vqs[total_vqs - 1];
1366 if (virtio_has_feature(vi->vdev, VIRTIO_NET_F_CTRL_VLAN))
1367 vi->dev->features |= NETIF_F_HW_VLAN_FILTER;
1368 }
1370 for (i = 0; i < vi->max_queue_pairs; i++) {
1371 vi->rq[i].vq = vqs[rxq2vq(i)];
1372 vi->sq[i].vq = vqs[txq2vq(i)];
1373 }
1375 kfree(names);
1376 kfree(callbacks);
1377 kfree(vqs);
1379 return 0;
1381 err_find:
1382 kfree(names);
1383 err_names:
1384 kfree(callbacks);
1385 err_callback:
1386 kfree(vqs);
1387 err_vq:
1388 return ret;
1389 }
1391 static int virtnet_alloc_queues(struct virtnet_info *vi)
1392 {
1393 int i;
1395 vi->sq = kzalloc(sizeof(*vi->sq) * vi->max_queue_pairs, GFP_KERNEL);
1396 if (!vi->sq)
1397 goto err_sq;
1398 vi->rq = kzalloc(sizeof(*vi->rq) * vi->max_queue_pairs, GFP_KERNEL);
1399 if (!vi->rq)
1400 goto err_rq;
1402 INIT_DELAYED_WORK(&vi->refill, refill_work);
1403 for (i = 0; i < vi->max_queue_pairs; i++) {
1404 vi->rq[i].pages = NULL;
1405 netif_napi_add(vi->dev, &vi->rq[i].napi, virtnet_poll,
1406 napi_weight);
1408 sg_init_table(vi->rq[i].sg, ARRAY_SIZE(vi->rq[i].sg));
1409 sg_init_table(vi->sq[i].sg, ARRAY_SIZE(vi->sq[i].sg));
1410 }
1412 return 0;
1414 err_rq:
1415 kfree(vi->sq);
1416 err_sq:
1417 return -ENOMEM;
1418 }
1420 static int init_vqs(struct virtnet_info *vi)
1421 {
1422 int ret;
1424 /* Allocate send & receive queues */
1425 ret = virtnet_alloc_queues(vi);
1426 if (ret)
1427 goto err;
1429 ret = virtnet_find_vqs(vi);
1430 if (ret)
1431 goto err_free;
1433 get_online_cpus();
1434 virtnet_set_affinity(vi);
1435 put_online_cpus();
1437 return 0;
1439 err_free:
1440 virtnet_free_queues(vi);
1441 err:
1442 return ret;
1443 }
1445 static int virtnet_probe(struct virtio_device *vdev)
1446 {
1447 int i, err;
1448 struct net_device *dev;
1449 struct virtnet_info *vi;
1450 u16 max_queue_pairs;
1452 /* Find if host supports multiqueue virtio_net device */
1453 err = virtio_config_val(vdev, VIRTIO_NET_F_MQ,
1454 offsetof(struct virtio_net_config,
1455 max_virtqueue_pairs), &max_queue_pairs);
1457 /* We need at least 2 queue's */
1458 if (err || max_queue_pairs < VIRTIO_NET_CTRL_MQ_VQ_PAIRS_MIN ||
1459 max_queue_pairs > VIRTIO_NET_CTRL_MQ_VQ_PAIRS_MAX ||
1460 !virtio_has_feature(vdev, VIRTIO_NET_F_CTRL_VQ))
1461 max_queue_pairs = 1;
1463 /* Allocate ourselves a network device with room for our info */
1464 dev = alloc_etherdev_mq(sizeof(struct virtnet_info), max_queue_pairs);
1465 if (!dev)
1466 return -ENOMEM;
1468 /* Set up network device as normal. */
1469 dev->priv_flags |= IFF_UNICAST_FLT | IFF_LIVE_ADDR_CHANGE;
1470 dev->netdev_ops = &virtnet_netdev;
1471 dev->features = NETIF_F_HIGHDMA;
1473 SET_ETHTOOL_OPS(dev, &virtnet_ethtool_ops);
1474 SET_NETDEV_DEV(dev, &vdev->dev);
1476 /* Do we support "hardware" checksums? */
1477 if (virtio_has_feature(vdev, VIRTIO_NET_F_CSUM)) {
1478 /* This opens up the world of extra features. */
1479 dev->hw_features |= NETIF_F_HW_CSUM|NETIF_F_SG|NETIF_F_FRAGLIST;
1480 if (csum)
1481 dev->features |= NETIF_F_HW_CSUM|NETIF_F_SG|NETIF_F_FRAGLIST;
1483 if (virtio_has_feature(vdev, VIRTIO_NET_F_GSO)) {
1484 dev->hw_features |= NETIF_F_TSO | NETIF_F_UFO
1485 | NETIF_F_TSO_ECN | NETIF_F_TSO6;
1486 }
1487 /* Individual feature bits: what can host handle? */
1488 if (virtio_has_feature(vdev, VIRTIO_NET_F_HOST_TSO4))
1489 dev->hw_features |= NETIF_F_TSO;
1490 if (virtio_has_feature(vdev, VIRTIO_NET_F_HOST_TSO6))
1491 dev->hw_features |= NETIF_F_TSO6;
1492 if (virtio_has_feature(vdev, VIRTIO_NET_F_HOST_ECN))
1493 dev->hw_features |= NETIF_F_TSO_ECN;
1494 if (virtio_has_feature(vdev, VIRTIO_NET_F_HOST_UFO))
1495 dev->hw_features |= NETIF_F_UFO;
1497 if (gso)
1498 dev->features |= dev->hw_features & (NETIF_F_ALL_TSO|NETIF_F_UFO);
1499 /* (!csum && gso) case will be fixed by register_netdev() */
1500 }
1502 /* Configuration may specify what MAC to use. Otherwise random. */
1503 if (virtio_config_val_len(vdev, VIRTIO_NET_F_MAC,
1504 offsetof(struct virtio_net_config, mac),
1505 dev->dev_addr, dev->addr_len) < 0)
1506 eth_hw_addr_random(dev);
1508 /* Set up our device-specific information */
1509 vi = netdev_priv(dev);
1510 vi->dev = dev;
1511 vi->vdev = vdev;
1512 vdev->priv = vi;
1513 vi->stats = alloc_percpu(struct virtnet_stats);
1514 err = -ENOMEM;
1515 if (vi->stats == NULL)
1516 goto free;
1518 vi->vq_index = alloc_percpu(int);
1519 if (vi->vq_index == NULL)
1520 goto free_stats;
1522 mutex_init(&vi->config_lock);
1523 vi->config_enable = true;
1524 INIT_WORK(&vi->config_work, virtnet_config_changed_work);
1526 /* If we can receive ANY GSO packets, we must allocate large ones. */
1527 if (virtio_has_feature(vdev, VIRTIO_NET_F_GUEST_TSO4) ||
1528 virtio_has_feature(vdev, VIRTIO_NET_F_GUEST_TSO6) ||
1529 virtio_has_feature(vdev, VIRTIO_NET_F_GUEST_ECN))
1530 vi->big_packets = true;
1532 if (virtio_has_feature(vdev, VIRTIO_NET_F_MRG_RXBUF))
1533 vi->mergeable_rx_bufs = true;
1535 if (virtio_has_feature(vdev, VIRTIO_NET_F_CTRL_VQ))
1536 vi->has_cvq = true;
1538 /* Use single tx/rx queue pair as default */
1539 vi->curr_queue_pairs = 1;
1540 vi->max_queue_pairs = max_queue_pairs;
1542 /* Allocate/initialize the rx/tx queues, and invoke find_vqs */
1543 err = init_vqs(vi);
1544 if (err)
1545 goto free_index;
1547 netif_set_real_num_tx_queues(dev, 1);
1548 netif_set_real_num_rx_queues(dev, 1);
1550 err = register_netdev(dev);
1551 if (err) {
1552 pr_debug("virtio_net: registering device failed\n");
1553 goto free_vqs;
1554 }
1556 /* Last of all, set up some receive buffers. */
1557 for (i = 0; i < vi->max_queue_pairs; i++) {
1558 try_fill_recv(&vi->rq[i], GFP_KERNEL);
1560 /* If we didn't even get one input buffer, we're useless. */
1561 if (vi->rq[i].num == 0) {
1562 free_unused_bufs(vi);
1563 err = -ENOMEM;
1564 goto free_recv_bufs;
1565 }
1566 }
1568 vi->nb.notifier_call = &virtnet_cpu_callback;
1569 err = register_hotcpu_notifier(&vi->nb);
1570 if (err) {
1571 pr_debug("virtio_net: registering cpu notifier failed\n");
1572 goto free_recv_bufs;
1573 }
1575 /* Assume link up if device can't report link status,
1576 otherwise get link status from config. */
1577 if (virtio_has_feature(vi->vdev, VIRTIO_NET_F_STATUS)) {
1578 netif_carrier_off(dev);
1579 schedule_work(&vi->config_work);
1580 } else {
1581 vi->status = VIRTIO_NET_S_LINK_UP;
1582 netif_carrier_on(dev);
1583 }
1585 pr_debug("virtnet: registered device %s with %d RX and TX vq's\n",
1586 dev->name, max_queue_pairs);
1588 return 0;
1590 free_recv_bufs:
1591 free_receive_bufs(vi);
1592 unregister_netdev(dev);
1593 free_vqs:
1594 cancel_delayed_work_sync(&vi->refill);
1595 virtnet_del_vqs(vi);
1596 free_index:
1597 free_percpu(vi->vq_index);
1598 free_stats:
1599 free_percpu(vi->stats);
1600 free:
1601 free_netdev(dev);
1602 return err;
1603 }
1605 static void remove_vq_common(struct virtnet_info *vi)
1606 {
1607 vi->vdev->config->reset(vi->vdev);
1609 /* Free unused buffers in both send and recv, if any. */
1610 free_unused_bufs(vi);
1612 free_receive_bufs(vi);
1614 virtnet_del_vqs(vi);
1615 }
1617 static void virtnet_remove(struct virtio_device *vdev)
1618 {
1619 struct virtnet_info *vi = vdev->priv;
1621 unregister_hotcpu_notifier(&vi->nb);
1623 /* Prevent config work handler from accessing the device. */
1624 mutex_lock(&vi->config_lock);
1625 vi->config_enable = false;
1626 mutex_unlock(&vi->config_lock);
1628 unregister_netdev(vi->dev);
1630 remove_vq_common(vi);
1632 flush_work(&vi->config_work);
1634 free_percpu(vi->vq_index);
1635 free_percpu(vi->stats);
1636 free_netdev(vi->dev);
1637 }
1639 #ifdef CONFIG_PM
1640 static int virtnet_freeze(struct virtio_device *vdev)
1641 {
1642 struct virtnet_info *vi = vdev->priv;
1643 int i;
1645 /* Prevent config work handler from accessing the device */
1646 mutex_lock(&vi->config_lock);
1647 vi->config_enable = false;
1648 mutex_unlock(&vi->config_lock);
1650 netif_device_detach(vi->dev);
1651 cancel_delayed_work_sync(&vi->refill);
1653 if (netif_running(vi->dev))
1654 for (i = 0; i < vi->max_queue_pairs; i++) {
1655 napi_disable(&vi->rq[i].napi);
1656 netif_napi_del(&vi->rq[i].napi);
1657 }
1659 remove_vq_common(vi);
1661 flush_work(&vi->config_work);
1663 return 0;
1664 }
1666 static int virtnet_restore(struct virtio_device *vdev)
1667 {
1668 struct virtnet_info *vi = vdev->priv;
1669 int err, i;
1671 err = init_vqs(vi);
1672 if (err)
1673 return err;
1675 if (netif_running(vi->dev))
1676 for (i = 0; i < vi->max_queue_pairs; i++)
1677 virtnet_napi_enable(&vi->rq[i]);
1679 netif_device_attach(vi->dev);
1681 for (i = 0; i < vi->max_queue_pairs; i++)
1682 if (!try_fill_recv(&vi->rq[i], GFP_KERNEL))
1683 schedule_delayed_work(&vi->refill, 0);
1685 mutex_lock(&vi->config_lock);
1686 vi->config_enable = true;
1687 mutex_unlock(&vi->config_lock);
1689 virtnet_set_queues(vi, vi->curr_queue_pairs);
1691 return 0;
1692 }
1693 #endif
1695 static struct virtio_device_id id_table[] = {
1696 { VIRTIO_ID_NET, VIRTIO_DEV_ANY_ID },
1697 { 0 },
1698 };
1700 static unsigned int features[] = {
1701 VIRTIO_NET_F_CSUM, VIRTIO_NET_F_GUEST_CSUM,
1702 VIRTIO_NET_F_GSO, VIRTIO_NET_F_MAC,
1703 VIRTIO_NET_F_HOST_TSO4, VIRTIO_NET_F_HOST_UFO, VIRTIO_NET_F_HOST_TSO6,
1704 VIRTIO_NET_F_HOST_ECN, VIRTIO_NET_F_GUEST_TSO4, VIRTIO_NET_F_GUEST_TSO6,
1705 VIRTIO_NET_F_GUEST_ECN, VIRTIO_NET_F_GUEST_UFO,
1706 VIRTIO_NET_F_MRG_RXBUF, VIRTIO_NET_F_STATUS, VIRTIO_NET_F_CTRL_VQ,
1707 VIRTIO_NET_F_CTRL_RX, VIRTIO_NET_F_CTRL_VLAN,
1708 VIRTIO_NET_F_GUEST_ANNOUNCE, VIRTIO_NET_F_MQ,
1709 };
1711 static struct virtio_driver virtio_net_driver = {
1712 .feature_table = features,
1713 .feature_table_size = ARRAY_SIZE(features),
1714 .driver.name = KBUILD_MODNAME,
1715 .driver.owner = THIS_MODULE,
1716 .id_table = id_table,
1717 .probe = virtnet_probe,
1718 .remove = virtnet_remove,
1719 .config_changed = virtnet_config_changed,
1720 #ifdef CONFIG_PM
1721 .freeze = virtnet_freeze,
1722 .restore = virtnet_restore,
1723 #endif
1724 };
1726 static int __init init(void)
1727 {
1728 return register_virtio_driver(&virtio_net_driver);
1729 }
1731 static void __exit fini(void)
1732 {
1733 unregister_virtio_driver(&virtio_net_driver);
1734 }
1735 module_init(init);
1736 module_exit(fini);
1738 MODULE_DEVICE_TABLE(virtio, id_table);
1739 MODULE_DESCRIPTION("Virtio network driver");
1740 MODULE_LICENSE("GPL");