1 /*
2 * drivers/staging/omapdrm/omap_irq.c
3 *
4 * Copyright (C) 2012 Texas Instruments
5 * Author: Rob Clark <rob.clark@linaro.org>
6 *
7 * This program is free software; you can redistribute it and/or modify it
8 * under the terms of the GNU General Public License version 2 as published by
9 * the Free Software Foundation.
10 *
11 * This program is distributed in the hope that it will be useful, but WITHOUT
12 * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
13 * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for
14 * more details.
15 *
16 * You should have received a copy of the GNU General Public License along with
17 * this program. If not, see <http://www.gnu.org/licenses/>.
18 */
20 #include "omap_drv.h"
22 static DEFINE_SPINLOCK(list_lock);
24 static void omap_irq_error_handler(struct omap_drm_irq *irq,
25 uint32_t irqstatus)
26 {
27 DRM_ERROR("errors: %08x\n", irqstatus);
28 }
30 /* call with list_lock and dispc runtime held */
31 static void omap_irq_update(struct drm_device *dev)
32 {
33 struct omap_drm_private *priv = dev->dev_private;
34 struct omap_drm_irq *irq;
35 uint32_t irqmask = priv->vblank_mask;
37 BUG_ON(!spin_is_locked(&list_lock));
39 list_for_each_entry(irq, &priv->irq_list, node)
40 irqmask |= irq->irqmask;
42 DBG("irqmask=%08x", irqmask);
44 dispc_write_irqenable(irqmask);
45 dispc_read_irqenable(); /* flush posted write */
46 }
48 void omap_irq_register(struct drm_device *dev, struct omap_drm_irq *irq)
49 {
50 struct omap_drm_private *priv = dev->dev_private;
51 unsigned long flags;
53 dispc_runtime_get();
54 spin_lock_irqsave(&list_lock, flags);
56 if (!WARN_ON(irq->registered)) {
57 irq->registered = true;
58 list_add(&irq->node, &priv->irq_list);
59 omap_irq_update(dev);
60 }
62 spin_unlock_irqrestore(&list_lock, flags);
63 dispc_runtime_put();
64 }
66 void omap_irq_unregister(struct drm_device *dev, struct omap_drm_irq *irq)
67 {
68 unsigned long flags;
70 dispc_runtime_get();
71 spin_lock_irqsave(&list_lock, flags);
73 if (!WARN_ON(!irq->registered)) {
74 irq->registered = false;
75 list_del(&irq->node);
76 omap_irq_update(dev);
77 }
79 spin_unlock_irqrestore(&list_lock, flags);
80 dispc_runtime_put();
81 }
83 struct omap_irq_wait {
84 struct omap_drm_irq irq;
85 int count;
86 };
88 static DECLARE_WAIT_QUEUE_HEAD(wait_event);
90 static void wait_irq(struct omap_drm_irq *irq, uint32_t irqstatus)
91 {
92 struct omap_irq_wait *wait =
93 container_of(irq, struct omap_irq_wait, irq);
94 wait->count--;
95 wake_up_all(&wait_event);
96 }
98 struct omap_irq_wait * omap_irq_wait_init(struct drm_device *dev,
99 uint32_t irqmask, int count)
100 {
101 struct omap_irq_wait *wait = kzalloc(sizeof(*wait), GFP_KERNEL);
102 wait->irq.irq = wait_irq;
103 wait->irq.irqmask = irqmask;
104 wait->count = count;
105 omap_irq_register(dev, &wait->irq);
106 return wait;
107 }
109 int omap_irq_wait(struct drm_device *dev, struct omap_irq_wait *wait,
110 unsigned long timeout)
111 {
112 int ret = wait_event_timeout(wait_event, (wait->count <= 0), timeout);
113 omap_irq_unregister(dev, &wait->irq);
114 kfree(wait);
115 if (ret == 0)
116 return -1;
117 return 0;
118 }
120 /**
121 * enable_vblank - enable vblank interrupt events
122 * @dev: DRM device
123 * @crtc: which irq to enable
124 *
125 * Enable vblank interrupts for @crtc. If the device doesn't have
126 * a hardware vblank counter, this routine should be a no-op, since
127 * interrupts will have to stay on to keep the count accurate.
128 *
129 * RETURNS
130 * Zero on success, appropriate errno if the given @crtc's vblank
131 * interrupt cannot be enabled.
132 */
133 int omap_irq_enable_vblank(struct drm_device *dev, int crtc)
134 {
135 struct omap_drm_private *priv = dev->dev_private;
136 unsigned long flags;
138 DBG("dev=%p, crtc=%d", dev, crtc);
140 dispc_runtime_get();
141 spin_lock_irqsave(&list_lock, flags);
142 priv->vblank_mask |= pipe2vbl(crtc);
143 omap_irq_update(dev);
144 spin_unlock_irqrestore(&list_lock, flags);
145 dispc_runtime_put();
147 return 0;
148 }
150 /**
151 * disable_vblank - disable vblank interrupt events
152 * @dev: DRM device
153 * @crtc: which irq to enable
154 *
155 * Disable vblank interrupts for @crtc. If the device doesn't have
156 * a hardware vblank counter, this routine should be a no-op, since
157 * interrupts will have to stay on to keep the count accurate.
158 */
159 void omap_irq_disable_vblank(struct drm_device *dev, int crtc)
160 {
161 struct omap_drm_private *priv = dev->dev_private;
162 unsigned long flags;
164 DBG("dev=%p, crtc=%d", dev, crtc);
166 dispc_runtime_get();
167 spin_lock_irqsave(&list_lock, flags);
168 priv->vblank_mask &= ~pipe2vbl(crtc);
169 omap_irq_update(dev);
170 spin_unlock_irqrestore(&list_lock, flags);
171 dispc_runtime_put();
172 }
174 irqreturn_t omap_irq_handler(DRM_IRQ_ARGS)
175 {
176 struct drm_device *dev = (struct drm_device *) arg;
177 struct omap_drm_private *priv = dev->dev_private;
178 struct omap_drm_irq *handler, *n;
179 unsigned long flags;
180 unsigned int id;
181 u32 irqstatus;
183 irqstatus = dispc_read_irqstatus();
184 dispc_clear_irqstatus(irqstatus);
185 dispc_read_irqstatus(); /* flush posted write */
187 VERB("irqs: %08x", irqstatus);
189 for (id = 0; id < priv->num_crtcs; id++)
190 if (irqstatus & pipe2vbl(id))
191 drm_handle_vblank(dev, id);
193 spin_lock_irqsave(&list_lock, flags);
194 list_for_each_entry_safe(handler, n, &priv->irq_list, node) {
195 if (handler->irqmask & irqstatus) {
196 spin_unlock_irqrestore(&list_lock, flags);
197 handler->irq(handler, handler->irqmask & irqstatus);
198 spin_lock_irqsave(&list_lock, flags);
199 }
200 }
201 spin_unlock_irqrestore(&list_lock, flags);
203 return IRQ_HANDLED;
204 }
206 void omap_irq_preinstall(struct drm_device *dev)
207 {
208 DBG("dev=%p", dev);
209 dispc_runtime_get();
210 dispc_clear_irqstatus(0xffffffff);
211 dispc_runtime_put();
212 }
214 int omap_irq_postinstall(struct drm_device *dev)
215 {
216 struct omap_drm_private *priv = dev->dev_private;
217 struct omap_drm_irq *error_handler = &priv->error_handler;
219 DBG("dev=%p", dev);
221 INIT_LIST_HEAD(&priv->irq_list);
223 error_handler->irq = omap_irq_error_handler;
224 error_handler->irqmask = DISPC_IRQ_OCP_ERR;
226 /* for now ignore DISPC_IRQ_SYNC_LOST_DIGIT.. really I think
227 * we just need to ignore it while enabling tv-out
228 */
229 error_handler->irqmask &= ~DISPC_IRQ_SYNC_LOST_DIGIT;
231 omap_irq_register(dev, error_handler);
233 return 0;
234 }
236 void omap_irq_uninstall(struct drm_device *dev)
237 {
238 DBG("dev=%p", dev);
239 // TODO prolly need to call drm_irq_uninstall() somewhere too
240 }
242 /*
243 * We need a special version, instead of just using drm_irq_install(),
244 * because we need to register the irq via omapdss. Once omapdss and
245 * omapdrm are merged together we can assign the dispc hwmod data to
246 * ourselves and drop these and just use drm_irq_{install,uninstall}()
247 */
249 int omap_drm_irq_install(struct drm_device *dev)
250 {
251 int ret;
253 mutex_lock(&dev->struct_mutex);
255 if (dev->irq_enabled) {
256 mutex_unlock(&dev->struct_mutex);
257 return -EBUSY;
258 }
259 dev->irq_enabled = 1;
260 mutex_unlock(&dev->struct_mutex);
262 /* Before installing handler */
263 if (dev->driver->irq_preinstall)
264 dev->driver->irq_preinstall(dev);
266 ret = dispc_request_irq(dev->driver->irq_handler, dev);
268 if (ret < 0) {
269 mutex_lock(&dev->struct_mutex);
270 dev->irq_enabled = 0;
271 mutex_unlock(&dev->struct_mutex);
272 return ret;
273 }
275 /* After installing handler */
276 if (dev->driver->irq_postinstall)
277 ret = dev->driver->irq_postinstall(dev);
279 if (ret < 0) {
280 mutex_lock(&dev->struct_mutex);
281 dev->irq_enabled = 0;
282 mutex_unlock(&dev->struct_mutex);
283 dispc_free_irq(dev);
284 }
286 return ret;
287 }
289 int omap_drm_irq_uninstall(struct drm_device *dev)
290 {
291 unsigned long irqflags;
292 int irq_enabled, i;
294 mutex_lock(&dev->struct_mutex);
295 irq_enabled = dev->irq_enabled;
296 dev->irq_enabled = 0;
297 mutex_unlock(&dev->struct_mutex);
299 /*
300 * Wake up any waiters so they don't hang.
301 */
302 if (dev->num_crtcs) {
303 spin_lock_irqsave(&dev->vbl_lock, irqflags);
304 for (i = 0; i < dev->num_crtcs; i++) {
305 DRM_WAKEUP(&dev->vbl_queue[i]);
306 dev->vblank_enabled[i] = 0;
307 dev->last_vblank[i] =
308 dev->driver->get_vblank_counter(dev, i);
309 }
310 spin_unlock_irqrestore(&dev->vbl_lock, irqflags);
311 }
313 if (!irq_enabled)
314 return -EINVAL;
316 if (dev->driver->irq_uninstall)
317 dev->driver->irq_uninstall(dev);
319 dispc_free_irq(dev);
321 return 0;
322 }