1 /*
2 * Generic driver for the MPSC (UART mode) on Marvell parts (e.g., GT64240,
3 * GT64260, MV64340, MV64360, GT96100, ... ).
4 *
5 * Author: Mark A. Greer <mgreer@mvista.com>
6 *
7 * Based on an old MPSC driver that was in the linuxppc tree. It appears to
8 * have been created by Chris Zankel (formerly of MontaVista) but there
9 * is no proper Copyright so I'm not sure. Apparently, parts were also
10 * taken from PPCBoot (now U-Boot). Also based on drivers/serial/8250.c
11 * by Russell King.
12 *
13 * 2004 (c) MontaVista, Software, Inc. This file is licensed under
14 * the terms of the GNU General Public License version 2. This program
15 * is licensed "as is" without any warranty of any kind, whether express
16 * or implied.
17 */
18 /*
19 * The MPSC interface is much like a typical network controller's interface.
20 * That is, you set up separate rings of descriptors for transmitting and
21 * receiving data. There is also a pool of buffers with (one buffer per
22 * descriptor) that incoming data are dma'd into or outgoing data are dma'd
23 * out of.
24 *
25 * The MPSC requires two other controllers to be able to work. The Baud Rate
26 * Generator (BRG) provides a clock at programmable frequencies which determines
27 * the baud rate. The Serial DMA Controller (SDMA) takes incoming data from the
28 * MPSC and DMA's it into memory or DMA's outgoing data and passes it to the
29 * MPSC. It is actually the SDMA interrupt that the driver uses to keep the
30 * transmit and receive "engines" going (i.e., indicate data has been
31 * transmitted or received).
32 *
33 * NOTES:
34 *
35 * 1) Some chips have an erratum where several regs cannot be
36 * read. To work around that, we keep a local copy of those regs in
37 * 'mpsc_port_info'.
38 *
39 * 2) Some chips have an erratum where the ctlr will hang when the SDMA ctlr
40 * accesses system mem with coherency enabled. For that reason, the driver
41 * assumes that coherency for that ctlr has been disabled. This means
42 * that when in a cache coherent system, the driver has to manually manage
43 * the data cache on the areas that it touches because the dma_* macro are
44 * basically no-ops.
45 *
46 * 3) There is an erratum (on PPC) where you can't use the instruction to do
47 * a DMA_TO_DEVICE/cache clean so DMA_BIDIRECTIONAL/flushes are used in places
48 * where a DMA_TO_DEVICE/clean would have [otherwise] sufficed.
49 *
50 * 4) AFAICT, hardware flow control isn't supported by the controller --MAG.
51 */
54 #if defined(CONFIG_SERIAL_MPSC_CONSOLE) && defined(CONFIG_MAGIC_SYSRQ)
55 #define SUPPORT_SYSRQ
56 #endif
58 #include <linux/module.h>
59 #include <linux/moduleparam.h>
60 #include <linux/tty.h>
61 #include <linux/tty_flip.h>
62 #include <linux/ioport.h>
63 #include <linux/init.h>
64 #include <linux/console.h>
65 #include <linux/sysrq.h>
66 #include <linux/serial.h>
67 #include <linux/serial_core.h>
68 #include <linux/delay.h>
69 #include <linux/device.h>
70 #include <linux/dma-mapping.h>
71 #include <linux/mv643xx.h>
72 #include <linux/platform_device.h>
73 #include <linux/gfp.h>
75 #include <asm/io.h>
76 #include <asm/irq.h>
78 #define MPSC_NUM_CTLRS 2
80 /*
81 * Descriptors and buffers must be cache line aligned.
82 * Buffers lengths must be multiple of cache line size.
83 * Number of Tx & Rx descriptors must be powers of 2.
84 */
85 #define MPSC_RXR_ENTRIES 32
86 #define MPSC_RXRE_SIZE dma_get_cache_alignment()
87 #define MPSC_RXR_SIZE (MPSC_RXR_ENTRIES * MPSC_RXRE_SIZE)
88 #define MPSC_RXBE_SIZE dma_get_cache_alignment()
89 #define MPSC_RXB_SIZE (MPSC_RXR_ENTRIES * MPSC_RXBE_SIZE)
91 #define MPSC_TXR_ENTRIES 32
92 #define MPSC_TXRE_SIZE dma_get_cache_alignment()
93 #define MPSC_TXR_SIZE (MPSC_TXR_ENTRIES * MPSC_TXRE_SIZE)
94 #define MPSC_TXBE_SIZE dma_get_cache_alignment()
95 #define MPSC_TXB_SIZE (MPSC_TXR_ENTRIES * MPSC_TXBE_SIZE)
97 #define MPSC_DMA_ALLOC_SIZE (MPSC_RXR_SIZE + MPSC_RXB_SIZE + MPSC_TXR_SIZE \
98 + MPSC_TXB_SIZE + dma_get_cache_alignment() /* for alignment */)
100 /* Rx and Tx Ring entry descriptors -- assume entry size is <= cacheline size */
101 struct mpsc_rx_desc {
102 u16 bufsize;
103 u16 bytecnt;
104 u32 cmdstat;
105 u32 link;
106 u32 buf_ptr;
107 } __attribute((packed));
109 struct mpsc_tx_desc {
110 u16 bytecnt;
111 u16 shadow;
112 u32 cmdstat;
113 u32 link;
114 u32 buf_ptr;
115 } __attribute((packed));
117 /*
118 * Some regs that have the erratum that you can't read them are are shared
119 * between the two MPSC controllers. This struct contains those shared regs.
120 */
121 struct mpsc_shared_regs {
122 phys_addr_t mpsc_routing_base_p;
123 phys_addr_t sdma_intr_base_p;
125 void __iomem *mpsc_routing_base;
126 void __iomem *sdma_intr_base;
128 u32 MPSC_MRR_m;
129 u32 MPSC_RCRR_m;
130 u32 MPSC_TCRR_m;
131 u32 SDMA_INTR_CAUSE_m;
132 u32 SDMA_INTR_MASK_m;
133 };
135 /* The main driver data structure */
136 struct mpsc_port_info {
137 struct uart_port port; /* Overlay uart_port structure */
139 /* Internal driver state for this ctlr */
140 u8 ready;
141 u8 rcv_data;
142 tcflag_t c_iflag; /* save termios->c_iflag */
143 tcflag_t c_cflag; /* save termios->c_cflag */
145 /* Info passed in from platform */
146 u8 mirror_regs; /* Need to mirror regs? */
147 u8 cache_mgmt; /* Need manual cache mgmt? */
148 u8 brg_can_tune; /* BRG has baud tuning? */
149 u32 brg_clk_src;
150 u16 mpsc_max_idle;
151 int default_baud;
152 int default_bits;
153 int default_parity;
154 int default_flow;
156 /* Physical addresses of various blocks of registers (from platform) */
157 phys_addr_t mpsc_base_p;
158 phys_addr_t sdma_base_p;
159 phys_addr_t brg_base_p;
161 /* Virtual addresses of various blocks of registers (from platform) */
162 void __iomem *mpsc_base;
163 void __iomem *sdma_base;
164 void __iomem *brg_base;
166 /* Descriptor ring and buffer allocations */
167 void *dma_region;
168 dma_addr_t dma_region_p;
170 dma_addr_t rxr; /* Rx descriptor ring */
171 dma_addr_t rxr_p; /* Phys addr of rxr */
172 u8 *rxb; /* Rx Ring I/O buf */
173 u8 *rxb_p; /* Phys addr of rxb */
174 u32 rxr_posn; /* First desc w/ Rx data */
176 dma_addr_t txr; /* Tx descriptor ring */
177 dma_addr_t txr_p; /* Phys addr of txr */
178 u8 *txb; /* Tx Ring I/O buf */
179 u8 *txb_p; /* Phys addr of txb */
180 int txr_head; /* Where new data goes */
181 int txr_tail; /* Where sent data comes off */
182 spinlock_t tx_lock; /* transmit lock */
184 /* Mirrored values of regs we can't read (if 'mirror_regs' set) */
185 u32 MPSC_MPCR_m;
186 u32 MPSC_CHR_1_m;
187 u32 MPSC_CHR_2_m;
188 u32 MPSC_CHR_10_m;
189 u32 BRG_BCR_m;
190 struct mpsc_shared_regs *shared_regs;
191 };
193 /* Hooks to platform-specific code */
194 int mpsc_platform_register_driver(void);
195 void mpsc_platform_unregister_driver(void);
197 /* Hooks back in to mpsc common to be called by platform-specific code */
198 struct mpsc_port_info *mpsc_device_probe(int index);
199 struct mpsc_port_info *mpsc_device_remove(int index);
201 /* Main MPSC Configuration Register Offsets */
202 #define MPSC_MMCRL 0x0000
203 #define MPSC_MMCRH 0x0004
204 #define MPSC_MPCR 0x0008
205 #define MPSC_CHR_1 0x000c
206 #define MPSC_CHR_2 0x0010
207 #define MPSC_CHR_3 0x0014
208 #define MPSC_CHR_4 0x0018
209 #define MPSC_CHR_5 0x001c
210 #define MPSC_CHR_6 0x0020
211 #define MPSC_CHR_7 0x0024
212 #define MPSC_CHR_8 0x0028
213 #define MPSC_CHR_9 0x002c
214 #define MPSC_CHR_10 0x0030
215 #define MPSC_CHR_11 0x0034
217 #define MPSC_MPCR_FRZ (1 << 9)
218 #define MPSC_MPCR_CL_5 0
219 #define MPSC_MPCR_CL_6 1
220 #define MPSC_MPCR_CL_7 2
221 #define MPSC_MPCR_CL_8 3
222 #define MPSC_MPCR_SBL_1 0
223 #define MPSC_MPCR_SBL_2 1
225 #define MPSC_CHR_2_TEV (1<<1)
226 #define MPSC_CHR_2_TA (1<<7)
227 #define MPSC_CHR_2_TTCS (1<<9)
228 #define MPSC_CHR_2_REV (1<<17)
229 #define MPSC_CHR_2_RA (1<<23)
230 #define MPSC_CHR_2_CRD (1<<25)
231 #define MPSC_CHR_2_EH (1<<31)
232 #define MPSC_CHR_2_PAR_ODD 0
233 #define MPSC_CHR_2_PAR_SPACE 1
234 #define MPSC_CHR_2_PAR_EVEN 2
235 #define MPSC_CHR_2_PAR_MARK 3
237 /* MPSC Signal Routing */
238 #define MPSC_MRR 0x0000
239 #define MPSC_RCRR 0x0004
240 #define MPSC_TCRR 0x0008
242 /* Serial DMA Controller Interface Registers */
243 #define SDMA_SDC 0x0000
244 #define SDMA_SDCM 0x0008
245 #define SDMA_RX_DESC 0x0800
246 #define SDMA_RX_BUF_PTR 0x0808
247 #define SDMA_SCRDP 0x0810
248 #define SDMA_TX_DESC 0x0c00
249 #define SDMA_SCTDP 0x0c10
250 #define SDMA_SFTDP 0x0c14
252 #define SDMA_DESC_CMDSTAT_PE (1<<0)
253 #define SDMA_DESC_CMDSTAT_CDL (1<<1)
254 #define SDMA_DESC_CMDSTAT_FR (1<<3)
255 #define SDMA_DESC_CMDSTAT_OR (1<<6)
256 #define SDMA_DESC_CMDSTAT_BR (1<<9)
257 #define SDMA_DESC_CMDSTAT_MI (1<<10)
258 #define SDMA_DESC_CMDSTAT_A (1<<11)
259 #define SDMA_DESC_CMDSTAT_AM (1<<12)
260 #define SDMA_DESC_CMDSTAT_CT (1<<13)
261 #define SDMA_DESC_CMDSTAT_C (1<<14)
262 #define SDMA_DESC_CMDSTAT_ES (1<<15)
263 #define SDMA_DESC_CMDSTAT_L (1<<16)
264 #define SDMA_DESC_CMDSTAT_F (1<<17)
265 #define SDMA_DESC_CMDSTAT_P (1<<18)
266 #define SDMA_DESC_CMDSTAT_EI (1<<23)
267 #define SDMA_DESC_CMDSTAT_O (1<<31)
269 #define SDMA_DESC_DFLT (SDMA_DESC_CMDSTAT_O \
270 | SDMA_DESC_CMDSTAT_EI)
272 #define SDMA_SDC_RFT (1<<0)
273 #define SDMA_SDC_SFM (1<<1)
274 #define SDMA_SDC_BLMR (1<<6)
275 #define SDMA_SDC_BLMT (1<<7)
276 #define SDMA_SDC_POVR (1<<8)
277 #define SDMA_SDC_RIFB (1<<9)
279 #define SDMA_SDCM_ERD (1<<7)
280 #define SDMA_SDCM_AR (1<<15)
281 #define SDMA_SDCM_STD (1<<16)
282 #define SDMA_SDCM_TXD (1<<23)
283 #define SDMA_SDCM_AT (1<<31)
285 #define SDMA_0_CAUSE_RXBUF (1<<0)
286 #define SDMA_0_CAUSE_RXERR (1<<1)
287 #define SDMA_0_CAUSE_TXBUF (1<<2)
288 #define SDMA_0_CAUSE_TXEND (1<<3)
289 #define SDMA_1_CAUSE_RXBUF (1<<8)
290 #define SDMA_1_CAUSE_RXERR (1<<9)
291 #define SDMA_1_CAUSE_TXBUF (1<<10)
292 #define SDMA_1_CAUSE_TXEND (1<<11)
294 #define SDMA_CAUSE_RX_MASK (SDMA_0_CAUSE_RXBUF | SDMA_0_CAUSE_RXERR \
295 | SDMA_1_CAUSE_RXBUF | SDMA_1_CAUSE_RXERR)
296 #define SDMA_CAUSE_TX_MASK (SDMA_0_CAUSE_TXBUF | SDMA_0_CAUSE_TXEND \
297 | SDMA_1_CAUSE_TXBUF | SDMA_1_CAUSE_TXEND)
299 /* SDMA Interrupt registers */
300 #define SDMA_INTR_CAUSE 0x0000
301 #define SDMA_INTR_MASK 0x0080
303 /* Baud Rate Generator Interface Registers */
304 #define BRG_BCR 0x0000
305 #define BRG_BTR 0x0004
307 /*
308 * Define how this driver is known to the outside (we've been assigned a
309 * range on the "Low-density serial ports" major).
310 */
311 #define MPSC_MAJOR 204
312 #define MPSC_MINOR_START 44
313 #define MPSC_DRIVER_NAME "MPSC"
314 #define MPSC_DEV_NAME "ttyMM"
315 #define MPSC_VERSION "1.00"
317 static struct mpsc_port_info mpsc_ports[MPSC_NUM_CTLRS];
318 static struct mpsc_shared_regs mpsc_shared_regs;
319 static struct uart_driver mpsc_reg;
321 static void mpsc_start_rx(struct mpsc_port_info *pi);
322 static void mpsc_free_ring_mem(struct mpsc_port_info *pi);
323 static void mpsc_release_port(struct uart_port *port);
324 /*
325 ******************************************************************************
326 *
327 * Baud Rate Generator Routines (BRG)
328 *
329 ******************************************************************************
330 */
331 static void mpsc_brg_init(struct mpsc_port_info *pi, u32 clk_src)
332 {
333 u32 v;
335 v = (pi->mirror_regs) ? pi->BRG_BCR_m : readl(pi->brg_base + BRG_BCR);
336 v = (v & ~(0xf << 18)) | ((clk_src & 0xf) << 18);
338 if (pi->brg_can_tune)
339 v &= ~(1 << 25);
341 if (pi->mirror_regs)
342 pi->BRG_BCR_m = v;
343 writel(v, pi->brg_base + BRG_BCR);
345 writel(readl(pi->brg_base + BRG_BTR) & 0xffff0000,
346 pi->brg_base + BRG_BTR);
347 }
349 static void mpsc_brg_enable(struct mpsc_port_info *pi)
350 {
351 u32 v;
353 v = (pi->mirror_regs) ? pi->BRG_BCR_m : readl(pi->brg_base + BRG_BCR);
354 v |= (1 << 16);
356 if (pi->mirror_regs)
357 pi->BRG_BCR_m = v;
358 writel(v, pi->brg_base + BRG_BCR);
359 }
361 static void mpsc_brg_disable(struct mpsc_port_info *pi)
362 {
363 u32 v;
365 v = (pi->mirror_regs) ? pi->BRG_BCR_m : readl(pi->brg_base + BRG_BCR);
366 v &= ~(1 << 16);
368 if (pi->mirror_regs)
369 pi->BRG_BCR_m = v;
370 writel(v, pi->brg_base + BRG_BCR);
371 }
373 /*
374 * To set the baud, we adjust the CDV field in the BRG_BCR reg.
375 * From manual: Baud = clk / ((CDV+1)*2) ==> CDV = (clk / (baud*2)) - 1.
376 * However, the input clock is divided by 16 in the MPSC b/c of how
377 * 'MPSC_MMCRH' was set up so we have to divide the 'clk' used in our
378 * calculation by 16 to account for that. So the real calculation
379 * that accounts for the way the mpsc is set up is:
380 * CDV = (clk / (baud*2*16)) - 1 ==> CDV = (clk / (baud << 5)) - 1.
381 */
382 static void mpsc_set_baudrate(struct mpsc_port_info *pi, u32 baud)
383 {
384 u32 cdv = (pi->port.uartclk / (baud << 5)) - 1;
385 u32 v;
387 mpsc_brg_disable(pi);
388 v = (pi->mirror_regs) ? pi->BRG_BCR_m : readl(pi->brg_base + BRG_BCR);
389 v = (v & 0xffff0000) | (cdv & 0xffff);
391 if (pi->mirror_regs)
392 pi->BRG_BCR_m = v;
393 writel(v, pi->brg_base + BRG_BCR);
394 mpsc_brg_enable(pi);
395 }
397 /*
398 ******************************************************************************
399 *
400 * Serial DMA Routines (SDMA)
401 *
402 ******************************************************************************
403 */
405 static void mpsc_sdma_burstsize(struct mpsc_port_info *pi, u32 burst_size)
406 {
407 u32 v;
409 pr_debug("mpsc_sdma_burstsize[%d]: burst_size: %d\n",
410 pi->port.line, burst_size);
412 burst_size >>= 3; /* Divide by 8 b/c reg values are 8-byte chunks */
414 if (burst_size < 2)
415 v = 0x0; /* 1 64-bit word */
416 else if (burst_size < 4)
417 v = 0x1; /* 2 64-bit words */
418 else if (burst_size < 8)
419 v = 0x2; /* 4 64-bit words */
420 else
421 v = 0x3; /* 8 64-bit words */
423 writel((readl(pi->sdma_base + SDMA_SDC) & (0x3 << 12)) | (v << 12),
424 pi->sdma_base + SDMA_SDC);
425 }
427 static void mpsc_sdma_init(struct mpsc_port_info *pi, u32 burst_size)
428 {
429 pr_debug("mpsc_sdma_init[%d]: burst_size: %d\n", pi->port.line,
430 burst_size);
432 writel((readl(pi->sdma_base + SDMA_SDC) & 0x3ff) | 0x03f,
433 pi->sdma_base + SDMA_SDC);
434 mpsc_sdma_burstsize(pi, burst_size);
435 }
437 static u32 mpsc_sdma_intr_mask(struct mpsc_port_info *pi, u32 mask)
438 {
439 u32 old, v;
441 pr_debug("mpsc_sdma_intr_mask[%d]: mask: 0x%x\n", pi->port.line, mask);
443 old = v = (pi->mirror_regs) ? pi->shared_regs->SDMA_INTR_MASK_m :
444 readl(pi->shared_regs->sdma_intr_base + SDMA_INTR_MASK);
446 mask &= 0xf;
447 if (pi->port.line)
448 mask <<= 8;
449 v &= ~mask;
451 if (pi->mirror_regs)
452 pi->shared_regs->SDMA_INTR_MASK_m = v;
453 writel(v, pi->shared_regs->sdma_intr_base + SDMA_INTR_MASK);
455 if (pi->port.line)
456 old >>= 8;
457 return old & 0xf;
458 }
460 static void mpsc_sdma_intr_unmask(struct mpsc_port_info *pi, u32 mask)
461 {
462 u32 v;
464 pr_debug("mpsc_sdma_intr_unmask[%d]: mask: 0x%x\n", pi->port.line,mask);
466 v = (pi->mirror_regs) ? pi->shared_regs->SDMA_INTR_MASK_m
467 : readl(pi->shared_regs->sdma_intr_base + SDMA_INTR_MASK);
469 mask &= 0xf;
470 if (pi->port.line)
471 mask <<= 8;
472 v |= mask;
474 if (pi->mirror_regs)
475 pi->shared_regs->SDMA_INTR_MASK_m = v;
476 writel(v, pi->shared_regs->sdma_intr_base + SDMA_INTR_MASK);
477 }
479 static void mpsc_sdma_intr_ack(struct mpsc_port_info *pi)
480 {
481 pr_debug("mpsc_sdma_intr_ack[%d]: Acknowledging IRQ\n", pi->port.line);
483 if (pi->mirror_regs)
484 pi->shared_regs->SDMA_INTR_CAUSE_m = 0;
485 writeb(0x00, pi->shared_regs->sdma_intr_base + SDMA_INTR_CAUSE
486 + pi->port.line);
487 }
489 static void mpsc_sdma_set_rx_ring(struct mpsc_port_info *pi,
490 struct mpsc_rx_desc *rxre_p)
491 {
492 pr_debug("mpsc_sdma_set_rx_ring[%d]: rxre_p: 0x%x\n",
493 pi->port.line, (u32)rxre_p);
495 writel((u32)rxre_p, pi->sdma_base + SDMA_SCRDP);
496 }
498 static void mpsc_sdma_set_tx_ring(struct mpsc_port_info *pi,
499 struct mpsc_tx_desc *txre_p)
500 {
501 writel((u32)txre_p, pi->sdma_base + SDMA_SFTDP);
502 writel((u32)txre_p, pi->sdma_base + SDMA_SCTDP);
503 }
505 static void mpsc_sdma_cmd(struct mpsc_port_info *pi, u32 val)
506 {
507 u32 v;
509 v = readl(pi->sdma_base + SDMA_SDCM);
510 if (val)
511 v |= val;
512 else
513 v = 0;
514 wmb();
515 writel(v, pi->sdma_base + SDMA_SDCM);
516 wmb();
517 }
519 static uint mpsc_sdma_tx_active(struct mpsc_port_info *pi)
520 {
521 return readl(pi->sdma_base + SDMA_SDCM) & SDMA_SDCM_TXD;
522 }
524 static void mpsc_sdma_start_tx(struct mpsc_port_info *pi)
525 {
526 struct mpsc_tx_desc *txre, *txre_p;
528 /* If tx isn't running & there's a desc ready to go, start it */
529 if (!mpsc_sdma_tx_active(pi)) {
530 txre = (struct mpsc_tx_desc *)(pi->txr
531 + (pi->txr_tail * MPSC_TXRE_SIZE));
532 dma_cache_sync(pi->port.dev, (void *)txre, MPSC_TXRE_SIZE,
533 DMA_FROM_DEVICE);
534 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
535 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
536 invalidate_dcache_range((ulong)txre,
537 (ulong)txre + MPSC_TXRE_SIZE);
538 #endif
540 if (be32_to_cpu(txre->cmdstat) & SDMA_DESC_CMDSTAT_O) {
541 txre_p = (struct mpsc_tx_desc *)
542 (pi->txr_p + (pi->txr_tail * MPSC_TXRE_SIZE));
544 mpsc_sdma_set_tx_ring(pi, txre_p);
545 mpsc_sdma_cmd(pi, SDMA_SDCM_STD | SDMA_SDCM_TXD);
546 }
547 }
548 }
550 static void mpsc_sdma_stop(struct mpsc_port_info *pi)
551 {
552 pr_debug("mpsc_sdma_stop[%d]: Stopping SDMA\n", pi->port.line);
554 /* Abort any SDMA transfers */
555 mpsc_sdma_cmd(pi, 0);
556 mpsc_sdma_cmd(pi, SDMA_SDCM_AR | SDMA_SDCM_AT);
558 /* Clear the SDMA current and first TX and RX pointers */
559 mpsc_sdma_set_tx_ring(pi, NULL);
560 mpsc_sdma_set_rx_ring(pi, NULL);
562 /* Disable interrupts */
563 mpsc_sdma_intr_mask(pi, 0xf);
564 mpsc_sdma_intr_ack(pi);
565 }
567 /*
568 ******************************************************************************
569 *
570 * Multi-Protocol Serial Controller Routines (MPSC)
571 *
572 ******************************************************************************
573 */
575 static void mpsc_hw_init(struct mpsc_port_info *pi)
576 {
577 u32 v;
579 pr_debug("mpsc_hw_init[%d]: Initializing hardware\n", pi->port.line);
581 /* Set up clock routing */
582 if (pi->mirror_regs) {
583 v = pi->shared_regs->MPSC_MRR_m;
584 v &= ~0x1c7;
585 pi->shared_regs->MPSC_MRR_m = v;
586 writel(v, pi->shared_regs->mpsc_routing_base + MPSC_MRR);
588 v = pi->shared_regs->MPSC_RCRR_m;
589 v = (v & ~0xf0f) | 0x100;
590 pi->shared_regs->MPSC_RCRR_m = v;
591 writel(v, pi->shared_regs->mpsc_routing_base + MPSC_RCRR);
593 v = pi->shared_regs->MPSC_TCRR_m;
594 v = (v & ~0xf0f) | 0x100;
595 pi->shared_regs->MPSC_TCRR_m = v;
596 writel(v, pi->shared_regs->mpsc_routing_base + MPSC_TCRR);
597 } else {
598 v = readl(pi->shared_regs->mpsc_routing_base + MPSC_MRR);
599 v &= ~0x1c7;
600 writel(v, pi->shared_regs->mpsc_routing_base + MPSC_MRR);
602 v = readl(pi->shared_regs->mpsc_routing_base + MPSC_RCRR);
603 v = (v & ~0xf0f) | 0x100;
604 writel(v, pi->shared_regs->mpsc_routing_base + MPSC_RCRR);
606 v = readl(pi->shared_regs->mpsc_routing_base + MPSC_TCRR);
607 v = (v & ~0xf0f) | 0x100;
608 writel(v, pi->shared_regs->mpsc_routing_base + MPSC_TCRR);
609 }
611 /* Put MPSC in UART mode & enabel Tx/Rx egines */
612 writel(0x000004c4, pi->mpsc_base + MPSC_MMCRL);
614 /* No preamble, 16x divider, low-latency, */
615 writel(0x04400400, pi->mpsc_base + MPSC_MMCRH);
616 mpsc_set_baudrate(pi, pi->default_baud);
618 if (pi->mirror_regs) {
619 pi->MPSC_CHR_1_m = 0;
620 pi->MPSC_CHR_2_m = 0;
621 }
622 writel(0, pi->mpsc_base + MPSC_CHR_1);
623 writel(0, pi->mpsc_base + MPSC_CHR_2);
624 writel(pi->mpsc_max_idle, pi->mpsc_base + MPSC_CHR_3);
625 writel(0, pi->mpsc_base + MPSC_CHR_4);
626 writel(0, pi->mpsc_base + MPSC_CHR_5);
627 writel(0, pi->mpsc_base + MPSC_CHR_6);
628 writel(0, pi->mpsc_base + MPSC_CHR_7);
629 writel(0, pi->mpsc_base + MPSC_CHR_8);
630 writel(0, pi->mpsc_base + MPSC_CHR_9);
631 writel(0, pi->mpsc_base + MPSC_CHR_10);
632 }
634 static void mpsc_enter_hunt(struct mpsc_port_info *pi)
635 {
636 pr_debug("mpsc_enter_hunt[%d]: Hunting...\n", pi->port.line);
638 if (pi->mirror_regs) {
639 writel(pi->MPSC_CHR_2_m | MPSC_CHR_2_EH,
640 pi->mpsc_base + MPSC_CHR_2);
641 /* Erratum prevents reading CHR_2 so just delay for a while */
642 udelay(100);
643 } else {
644 writel(readl(pi->mpsc_base + MPSC_CHR_2) | MPSC_CHR_2_EH,
645 pi->mpsc_base + MPSC_CHR_2);
647 while (readl(pi->mpsc_base + MPSC_CHR_2) & MPSC_CHR_2_EH)
648 udelay(10);
649 }
650 }
652 static void mpsc_freeze(struct mpsc_port_info *pi)
653 {
654 u32 v;
656 pr_debug("mpsc_freeze[%d]: Freezing\n", pi->port.line);
658 v = (pi->mirror_regs) ? pi->MPSC_MPCR_m :
659 readl(pi->mpsc_base + MPSC_MPCR);
660 v |= MPSC_MPCR_FRZ;
662 if (pi->mirror_regs)
663 pi->MPSC_MPCR_m = v;
664 writel(v, pi->mpsc_base + MPSC_MPCR);
665 }
667 static void mpsc_unfreeze(struct mpsc_port_info *pi)
668 {
669 u32 v;
671 v = (pi->mirror_regs) ? pi->MPSC_MPCR_m :
672 readl(pi->mpsc_base + MPSC_MPCR);
673 v &= ~MPSC_MPCR_FRZ;
675 if (pi->mirror_regs)
676 pi->MPSC_MPCR_m = v;
677 writel(v, pi->mpsc_base + MPSC_MPCR);
679 pr_debug("mpsc_unfreeze[%d]: Unfrozen\n", pi->port.line);
680 }
682 static void mpsc_set_char_length(struct mpsc_port_info *pi, u32 len)
683 {
684 u32 v;
686 pr_debug("mpsc_set_char_length[%d]: char len: %d\n", pi->port.line,len);
688 v = (pi->mirror_regs) ? pi->MPSC_MPCR_m :
689 readl(pi->mpsc_base + MPSC_MPCR);
690 v = (v & ~(0x3 << 12)) | ((len & 0x3) << 12);
692 if (pi->mirror_regs)
693 pi->MPSC_MPCR_m = v;
694 writel(v, pi->mpsc_base + MPSC_MPCR);
695 }
697 static void mpsc_set_stop_bit_length(struct mpsc_port_info *pi, u32 len)
698 {
699 u32 v;
701 pr_debug("mpsc_set_stop_bit_length[%d]: stop bits: %d\n",
702 pi->port.line, len);
704 v = (pi->mirror_regs) ? pi->MPSC_MPCR_m :
705 readl(pi->mpsc_base + MPSC_MPCR);
707 v = (v & ~(1 << 14)) | ((len & 0x1) << 14);
709 if (pi->mirror_regs)
710 pi->MPSC_MPCR_m = v;
711 writel(v, pi->mpsc_base + MPSC_MPCR);
712 }
714 static void mpsc_set_parity(struct mpsc_port_info *pi, u32 p)
715 {
716 u32 v;
718 pr_debug("mpsc_set_parity[%d]: parity bits: 0x%x\n", pi->port.line, p);
720 v = (pi->mirror_regs) ? pi->MPSC_CHR_2_m :
721 readl(pi->mpsc_base + MPSC_CHR_2);
723 p &= 0x3;
724 v = (v & ~0xc000c) | (p << 18) | (p << 2);
726 if (pi->mirror_regs)
727 pi->MPSC_CHR_2_m = v;
728 writel(v, pi->mpsc_base + MPSC_CHR_2);
729 }
731 /*
732 ******************************************************************************
733 *
734 * Driver Init Routines
735 *
736 ******************************************************************************
737 */
739 static void mpsc_init_hw(struct mpsc_port_info *pi)
740 {
741 pr_debug("mpsc_init_hw[%d]: Initializing\n", pi->port.line);
743 mpsc_brg_init(pi, pi->brg_clk_src);
744 mpsc_brg_enable(pi);
745 mpsc_sdma_init(pi, dma_get_cache_alignment()); /* burst a cacheline */
746 mpsc_sdma_stop(pi);
747 mpsc_hw_init(pi);
748 }
750 static int mpsc_alloc_ring_mem(struct mpsc_port_info *pi)
751 {
752 int rc = 0;
754 pr_debug("mpsc_alloc_ring_mem[%d]: Allocating ring mem\n",
755 pi->port.line);
757 if (!pi->dma_region) {
758 if (!dma_supported(pi->port.dev, 0xffffffff)) {
759 printk(KERN_ERR "MPSC: Inadequate DMA support\n");
760 rc = -ENXIO;
761 } else if ((pi->dma_region = dma_alloc_noncoherent(pi->port.dev,
762 MPSC_DMA_ALLOC_SIZE,
763 &pi->dma_region_p, GFP_KERNEL))
764 == NULL) {
765 printk(KERN_ERR "MPSC: Can't alloc Desc region\n");
766 rc = -ENOMEM;
767 }
768 }
770 return rc;
771 }
773 static void mpsc_free_ring_mem(struct mpsc_port_info *pi)
774 {
775 pr_debug("mpsc_free_ring_mem[%d]: Freeing ring mem\n", pi->port.line);
777 if (pi->dma_region) {
778 dma_free_noncoherent(pi->port.dev, MPSC_DMA_ALLOC_SIZE,
779 pi->dma_region, pi->dma_region_p);
780 pi->dma_region = NULL;
781 pi->dma_region_p = (dma_addr_t)NULL;
782 }
783 }
785 static void mpsc_init_rings(struct mpsc_port_info *pi)
786 {
787 struct mpsc_rx_desc *rxre;
788 struct mpsc_tx_desc *txre;
789 dma_addr_t dp, dp_p;
790 u8 *bp, *bp_p;
791 int i;
793 pr_debug("mpsc_init_rings[%d]: Initializing rings\n", pi->port.line);
795 BUG_ON(pi->dma_region == NULL);
797 memset(pi->dma_region, 0, MPSC_DMA_ALLOC_SIZE);
799 /*
800 * Descriptors & buffers are multiples of cacheline size and must be
801 * cacheline aligned.
802 */
803 dp = ALIGN((u32)pi->dma_region, dma_get_cache_alignment());
804 dp_p = ALIGN((u32)pi->dma_region_p, dma_get_cache_alignment());
806 /*
807 * Partition dma region into rx ring descriptor, rx buffers,
808 * tx ring descriptors, and tx buffers.
809 */
810 pi->rxr = dp;
811 pi->rxr_p = dp_p;
812 dp += MPSC_RXR_SIZE;
813 dp_p += MPSC_RXR_SIZE;
815 pi->rxb = (u8 *)dp;
816 pi->rxb_p = (u8 *)dp_p;
817 dp += MPSC_RXB_SIZE;
818 dp_p += MPSC_RXB_SIZE;
820 pi->rxr_posn = 0;
822 pi->txr = dp;
823 pi->txr_p = dp_p;
824 dp += MPSC_TXR_SIZE;
825 dp_p += MPSC_TXR_SIZE;
827 pi->txb = (u8 *)dp;
828 pi->txb_p = (u8 *)dp_p;
830 pi->txr_head = 0;
831 pi->txr_tail = 0;
833 /* Init rx ring descriptors */
834 dp = pi->rxr;
835 dp_p = pi->rxr_p;
836 bp = pi->rxb;
837 bp_p = pi->rxb_p;
839 for (i = 0; i < MPSC_RXR_ENTRIES; i++) {
840 rxre = (struct mpsc_rx_desc *)dp;
842 rxre->bufsize = cpu_to_be16(MPSC_RXBE_SIZE);
843 rxre->bytecnt = cpu_to_be16(0);
844 rxre->cmdstat = cpu_to_be32(SDMA_DESC_CMDSTAT_O
845 | SDMA_DESC_CMDSTAT_EI | SDMA_DESC_CMDSTAT_F
846 | SDMA_DESC_CMDSTAT_L);
847 rxre->link = cpu_to_be32(dp_p + MPSC_RXRE_SIZE);
848 rxre->buf_ptr = cpu_to_be32(bp_p);
850 dp += MPSC_RXRE_SIZE;
851 dp_p += MPSC_RXRE_SIZE;
852 bp += MPSC_RXBE_SIZE;
853 bp_p += MPSC_RXBE_SIZE;
854 }
855 rxre->link = cpu_to_be32(pi->rxr_p); /* Wrap last back to first */
857 /* Init tx ring descriptors */
858 dp = pi->txr;
859 dp_p = pi->txr_p;
860 bp = pi->txb;
861 bp_p = pi->txb_p;
863 for (i = 0; i < MPSC_TXR_ENTRIES; i++) {
864 txre = (struct mpsc_tx_desc *)dp;
866 txre->link = cpu_to_be32(dp_p + MPSC_TXRE_SIZE);
867 txre->buf_ptr = cpu_to_be32(bp_p);
869 dp += MPSC_TXRE_SIZE;
870 dp_p += MPSC_TXRE_SIZE;
871 bp += MPSC_TXBE_SIZE;
872 bp_p += MPSC_TXBE_SIZE;
873 }
874 txre->link = cpu_to_be32(pi->txr_p); /* Wrap last back to first */
876 dma_cache_sync(pi->port.dev, (void *)pi->dma_region,
877 MPSC_DMA_ALLOC_SIZE, DMA_BIDIRECTIONAL);
878 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
879 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
880 flush_dcache_range((ulong)pi->dma_region,
881 (ulong)pi->dma_region
882 + MPSC_DMA_ALLOC_SIZE);
883 #endif
885 return;
886 }
888 static void mpsc_uninit_rings(struct mpsc_port_info *pi)
889 {
890 pr_debug("mpsc_uninit_rings[%d]: Uninitializing rings\n",pi->port.line);
892 BUG_ON(pi->dma_region == NULL);
894 pi->rxr = 0;
895 pi->rxr_p = 0;
896 pi->rxb = NULL;
897 pi->rxb_p = NULL;
898 pi->rxr_posn = 0;
900 pi->txr = 0;
901 pi->txr_p = 0;
902 pi->txb = NULL;
903 pi->txb_p = NULL;
904 pi->txr_head = 0;
905 pi->txr_tail = 0;
906 }
908 static int mpsc_make_ready(struct mpsc_port_info *pi)
909 {
910 int rc;
912 pr_debug("mpsc_make_ready[%d]: Making cltr ready\n", pi->port.line);
914 if (!pi->ready) {
915 mpsc_init_hw(pi);
916 if ((rc = mpsc_alloc_ring_mem(pi)))
917 return rc;
918 mpsc_init_rings(pi);
919 pi->ready = 1;
920 }
922 return 0;
923 }
925 #ifdef CONFIG_CONSOLE_POLL
926 static int serial_polled;
927 #endif
929 /*
930 ******************************************************************************
931 *
932 * Interrupt Handling Routines
933 *
934 ******************************************************************************
935 */
937 static int mpsc_rx_intr(struct mpsc_port_info *pi)
938 {
939 struct mpsc_rx_desc *rxre;
940 struct tty_struct *tty = pi->port.state->port.tty;
941 u32 cmdstat, bytes_in, i;
942 int rc = 0;
943 u8 *bp;
944 char flag = TTY_NORMAL;
946 pr_debug("mpsc_rx_intr[%d]: Handling Rx intr\n", pi->port.line);
948 rxre = (struct mpsc_rx_desc *)(pi->rxr + (pi->rxr_posn*MPSC_RXRE_SIZE));
950 dma_cache_sync(pi->port.dev, (void *)rxre, MPSC_RXRE_SIZE,
951 DMA_FROM_DEVICE);
952 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
953 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
954 invalidate_dcache_range((ulong)rxre,
955 (ulong)rxre + MPSC_RXRE_SIZE);
956 #endif
958 /*
959 * Loop through Rx descriptors handling ones that have been completed.
960 */
961 while (!((cmdstat = be32_to_cpu(rxre->cmdstat))
962 & SDMA_DESC_CMDSTAT_O)) {
963 bytes_in = be16_to_cpu(rxre->bytecnt);
964 #ifdef CONFIG_CONSOLE_POLL
965 if (unlikely(serial_polled)) {
966 serial_polled = 0;
967 return 0;
968 }
969 #endif
970 /* Following use of tty struct directly is deprecated */
971 if (unlikely(tty_buffer_request_room(tty, bytes_in)
972 < bytes_in)) {
973 if (tty->low_latency)
974 tty_flip_buffer_push(tty);
975 /*
976 * If this failed then we will throw away the bytes
977 * but must do so to clear interrupts.
978 */
979 }
981 bp = pi->rxb + (pi->rxr_posn * MPSC_RXBE_SIZE);
982 dma_cache_sync(pi->port.dev, (void *)bp, MPSC_RXBE_SIZE,
983 DMA_FROM_DEVICE);
984 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
985 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
986 invalidate_dcache_range((ulong)bp,
987 (ulong)bp + MPSC_RXBE_SIZE);
988 #endif
990 /*
991 * Other than for parity error, the manual provides little
992 * info on what data will be in a frame flagged by any of
993 * these errors. For parity error, it is the last byte in
994 * the buffer that had the error. As for the rest, I guess
995 * we'll assume there is no data in the buffer.
996 * If there is...it gets lost.
997 */
998 if (unlikely(cmdstat & (SDMA_DESC_CMDSTAT_BR
999 | SDMA_DESC_CMDSTAT_FR
1000 | SDMA_DESC_CMDSTAT_OR))) {
1002 pi->port.icount.rx++;
1004 if (cmdstat & SDMA_DESC_CMDSTAT_BR) { /* Break */
1005 pi->port.icount.brk++;
1007 if (uart_handle_break(&pi->port))
1008 goto next_frame;
1009 } else if (cmdstat & SDMA_DESC_CMDSTAT_FR) {
1010 pi->port.icount.frame++;
1011 } else if (cmdstat & SDMA_DESC_CMDSTAT_OR) {
1012 pi->port.icount.overrun++;
1013 }
1015 cmdstat &= pi->port.read_status_mask;
1017 if (cmdstat & SDMA_DESC_CMDSTAT_BR)
1018 flag = TTY_BREAK;
1019 else if (cmdstat & SDMA_DESC_CMDSTAT_FR)
1020 flag = TTY_FRAME;
1021 else if (cmdstat & SDMA_DESC_CMDSTAT_OR)
1022 flag = TTY_OVERRUN;
1023 else if (cmdstat & SDMA_DESC_CMDSTAT_PE)
1024 flag = TTY_PARITY;
1025 }
1027 if (uart_handle_sysrq_char(&pi->port, *bp)) {
1028 bp++;
1029 bytes_in--;
1030 #ifdef CONFIG_CONSOLE_POLL
1031 if (unlikely(serial_polled)) {
1032 serial_polled = 0;
1033 return 0;
1034 }
1035 #endif
1036 goto next_frame;
1037 }
1039 if ((unlikely(cmdstat & (SDMA_DESC_CMDSTAT_BR
1040 | SDMA_DESC_CMDSTAT_FR
1041 | SDMA_DESC_CMDSTAT_OR)))
1042 && !(cmdstat & pi->port.ignore_status_mask)) {
1043 tty_insert_flip_char(tty, *bp, flag);
1044 } else {
1045 for (i=0; i<bytes_in; i++)
1046 tty_insert_flip_char(tty, *bp++, TTY_NORMAL);
1048 pi->port.icount.rx += bytes_in;
1049 }
1051 next_frame:
1052 rxre->bytecnt = cpu_to_be16(0);
1053 wmb();
1054 rxre->cmdstat = cpu_to_be32(SDMA_DESC_CMDSTAT_O
1055 | SDMA_DESC_CMDSTAT_EI | SDMA_DESC_CMDSTAT_F
1056 | SDMA_DESC_CMDSTAT_L);
1057 wmb();
1058 dma_cache_sync(pi->port.dev, (void *)rxre, MPSC_RXRE_SIZE,
1059 DMA_BIDIRECTIONAL);
1060 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
1061 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
1062 flush_dcache_range((ulong)rxre,
1063 (ulong)rxre + MPSC_RXRE_SIZE);
1064 #endif
1066 /* Advance to next descriptor */
1067 pi->rxr_posn = (pi->rxr_posn + 1) & (MPSC_RXR_ENTRIES - 1);
1068 rxre = (struct mpsc_rx_desc *)
1069 (pi->rxr + (pi->rxr_posn * MPSC_RXRE_SIZE));
1070 dma_cache_sync(pi->port.dev, (void *)rxre, MPSC_RXRE_SIZE,
1071 DMA_FROM_DEVICE);
1072 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
1073 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
1074 invalidate_dcache_range((ulong)rxre,
1075 (ulong)rxre + MPSC_RXRE_SIZE);
1076 #endif
1077 rc = 1;
1078 }
1080 /* Restart rx engine, if its stopped */
1081 if ((readl(pi->sdma_base + SDMA_SDCM) & SDMA_SDCM_ERD) == 0)
1082 mpsc_start_rx(pi);
1084 tty_flip_buffer_push(tty);
1085 return rc;
1086 }
1088 static void mpsc_setup_tx_desc(struct mpsc_port_info *pi, u32 count, u32 intr)
1089 {
1090 struct mpsc_tx_desc *txre;
1092 txre = (struct mpsc_tx_desc *)(pi->txr
1093 + (pi->txr_head * MPSC_TXRE_SIZE));
1095 txre->bytecnt = cpu_to_be16(count);
1096 txre->shadow = txre->bytecnt;
1097 wmb(); /* ensure cmdstat is last field updated */
1098 txre->cmdstat = cpu_to_be32(SDMA_DESC_CMDSTAT_O | SDMA_DESC_CMDSTAT_F
1099 | SDMA_DESC_CMDSTAT_L
1100 | ((intr) ? SDMA_DESC_CMDSTAT_EI : 0));
1101 wmb();
1102 dma_cache_sync(pi->port.dev, (void *)txre, MPSC_TXRE_SIZE,
1103 DMA_BIDIRECTIONAL);
1104 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
1105 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
1106 flush_dcache_range((ulong)txre,
1107 (ulong)txre + MPSC_TXRE_SIZE);
1108 #endif
1109 }
1111 static void mpsc_copy_tx_data(struct mpsc_port_info *pi)
1112 {
1113 struct circ_buf *xmit = &pi->port.state->xmit;
1114 u8 *bp;
1115 u32 i;
1117 /* Make sure the desc ring isn't full */
1118 while (CIRC_CNT(pi->txr_head, pi->txr_tail, MPSC_TXR_ENTRIES)
1119 < (MPSC_TXR_ENTRIES - 1)) {
1120 if (pi->port.x_char) {
1121 /*
1122 * Ideally, we should use the TCS field in
1123 * CHR_1 to put the x_char out immediately but
1124 * errata prevents us from being able to read
1125 * CHR_2 to know that its safe to write to
1126 * CHR_1. Instead, just put it in-band with
1127 * all the other Tx data.
1128 */
1129 bp = pi->txb + (pi->txr_head * MPSC_TXBE_SIZE);
1130 *bp = pi->port.x_char;
1131 pi->port.x_char = 0;
1132 i = 1;
1133 } else if (!uart_circ_empty(xmit)
1134 && !uart_tx_stopped(&pi->port)) {
1135 i = min((u32)MPSC_TXBE_SIZE,
1136 (u32)uart_circ_chars_pending(xmit));
1137 i = min(i, (u32)CIRC_CNT_TO_END(xmit->head, xmit->tail,
1138 UART_XMIT_SIZE));
1139 bp = pi->txb + (pi->txr_head * MPSC_TXBE_SIZE);
1140 memcpy(bp, &xmit->buf[xmit->tail], i);
1141 xmit->tail = (xmit->tail + i) & (UART_XMIT_SIZE - 1);
1143 if (uart_circ_chars_pending(xmit) < WAKEUP_CHARS)
1144 uart_write_wakeup(&pi->port);
1145 } else { /* All tx data copied into ring bufs */
1146 return;
1147 }
1149 dma_cache_sync(pi->port.dev, (void *)bp, MPSC_TXBE_SIZE,
1150 DMA_BIDIRECTIONAL);
1151 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
1152 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
1153 flush_dcache_range((ulong)bp,
1154 (ulong)bp + MPSC_TXBE_SIZE);
1155 #endif
1156 mpsc_setup_tx_desc(pi, i, 1);
1158 /* Advance to next descriptor */
1159 pi->txr_head = (pi->txr_head + 1) & (MPSC_TXR_ENTRIES - 1);
1160 }
1161 }
1163 static int mpsc_tx_intr(struct mpsc_port_info *pi)
1164 {
1165 struct mpsc_tx_desc *txre;
1166 int rc = 0;
1167 unsigned long iflags;
1169 spin_lock_irqsave(&pi->tx_lock, iflags);
1171 if (!mpsc_sdma_tx_active(pi)) {
1172 txre = (struct mpsc_tx_desc *)(pi->txr
1173 + (pi->txr_tail * MPSC_TXRE_SIZE));
1175 dma_cache_sync(pi->port.dev, (void *)txre, MPSC_TXRE_SIZE,
1176 DMA_FROM_DEVICE);
1177 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
1178 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
1179 invalidate_dcache_range((ulong)txre,
1180 (ulong)txre + MPSC_TXRE_SIZE);
1181 #endif
1183 while (!(be32_to_cpu(txre->cmdstat) & SDMA_DESC_CMDSTAT_O)) {
1184 rc = 1;
1185 pi->port.icount.tx += be16_to_cpu(txre->bytecnt);
1186 pi->txr_tail = (pi->txr_tail+1) & (MPSC_TXR_ENTRIES-1);
1188 /* If no more data to tx, fall out of loop */
1189 if (pi->txr_head == pi->txr_tail)
1190 break;
1192 txre = (struct mpsc_tx_desc *)(pi->txr
1193 + (pi->txr_tail * MPSC_TXRE_SIZE));
1194 dma_cache_sync(pi->port.dev, (void *)txre,
1195 MPSC_TXRE_SIZE, DMA_FROM_DEVICE);
1196 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
1197 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
1198 invalidate_dcache_range((ulong)txre,
1199 (ulong)txre + MPSC_TXRE_SIZE);
1200 #endif
1201 }
1203 mpsc_copy_tx_data(pi);
1204 mpsc_sdma_start_tx(pi); /* start next desc if ready */
1205 }
1207 spin_unlock_irqrestore(&pi->tx_lock, iflags);
1208 return rc;
1209 }
1211 /*
1212 * This is the driver's interrupt handler. To avoid a race, we first clear
1213 * the interrupt, then handle any completed Rx/Tx descriptors. When done
1214 * handling those descriptors, we restart the Rx/Tx engines if they're stopped.
1215 */
1216 static irqreturn_t mpsc_sdma_intr(int irq, void *dev_id)
1217 {
1218 struct mpsc_port_info *pi = dev_id;
1219 ulong iflags;
1220 int rc = IRQ_NONE;
1222 pr_debug("mpsc_sdma_intr[%d]: SDMA Interrupt Received\n",pi->port.line);
1224 spin_lock_irqsave(&pi->port.lock, iflags);
1225 mpsc_sdma_intr_ack(pi);
1226 if (mpsc_rx_intr(pi))
1227 rc = IRQ_HANDLED;
1228 if (mpsc_tx_intr(pi))
1229 rc = IRQ_HANDLED;
1230 spin_unlock_irqrestore(&pi->port.lock, iflags);
1232 pr_debug("mpsc_sdma_intr[%d]: SDMA Interrupt Handled\n", pi->port.line);
1233 return rc;
1234 }
1236 /*
1237 ******************************************************************************
1238 *
1239 * serial_core.c Interface routines
1240 *
1241 ******************************************************************************
1242 */
1243 static uint mpsc_tx_empty(struct uart_port *port)
1244 {
1245 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1246 ulong iflags;
1247 uint rc;
1249 spin_lock_irqsave(&pi->port.lock, iflags);
1250 rc = mpsc_sdma_tx_active(pi) ? 0 : TIOCSER_TEMT;
1251 spin_unlock_irqrestore(&pi->port.lock, iflags);
1253 return rc;
1254 }
1256 static void mpsc_set_mctrl(struct uart_port *port, uint mctrl)
1257 {
1258 /* Have no way to set modem control lines AFAICT */
1259 }
1261 static uint mpsc_get_mctrl(struct uart_port *port)
1262 {
1263 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1264 u32 mflags, status;
1266 status = (pi->mirror_regs) ? pi->MPSC_CHR_10_m
1267 : readl(pi->mpsc_base + MPSC_CHR_10);
1269 mflags = 0;
1270 if (status & 0x1)
1271 mflags |= TIOCM_CTS;
1272 if (status & 0x2)
1273 mflags |= TIOCM_CAR;
1275 return mflags | TIOCM_DSR; /* No way to tell if DSR asserted */
1276 }
1278 static void mpsc_stop_tx(struct uart_port *port)
1279 {
1280 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1282 pr_debug("mpsc_stop_tx[%d]\n", port->line);
1284 mpsc_freeze(pi);
1285 }
1287 static void mpsc_start_tx(struct uart_port *port)
1288 {
1289 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1290 unsigned long iflags;
1292 spin_lock_irqsave(&pi->tx_lock, iflags);
1294 mpsc_unfreeze(pi);
1295 mpsc_copy_tx_data(pi);
1296 mpsc_sdma_start_tx(pi);
1298 spin_unlock_irqrestore(&pi->tx_lock, iflags);
1300 pr_debug("mpsc_start_tx[%d]\n", port->line);
1301 }
1303 static void mpsc_start_rx(struct mpsc_port_info *pi)
1304 {
1305 pr_debug("mpsc_start_rx[%d]: Starting...\n", pi->port.line);
1307 if (pi->rcv_data) {
1308 mpsc_enter_hunt(pi);
1309 mpsc_sdma_cmd(pi, SDMA_SDCM_ERD);
1310 }
1311 }
1313 static void mpsc_stop_rx(struct uart_port *port)
1314 {
1315 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1317 pr_debug("mpsc_stop_rx[%d]: Stopping...\n", port->line);
1319 if (pi->mirror_regs) {
1320 writel(pi->MPSC_CHR_2_m | MPSC_CHR_2_RA,
1321 pi->mpsc_base + MPSC_CHR_2);
1322 /* Erratum prevents reading CHR_2 so just delay for a while */
1323 udelay(100);
1324 } else {
1325 writel(readl(pi->mpsc_base + MPSC_CHR_2) | MPSC_CHR_2_RA,
1326 pi->mpsc_base + MPSC_CHR_2);
1328 while (readl(pi->mpsc_base + MPSC_CHR_2) & MPSC_CHR_2_RA)
1329 udelay(10);
1330 }
1332 mpsc_sdma_cmd(pi, SDMA_SDCM_AR);
1333 }
1335 static void mpsc_enable_ms(struct uart_port *port)
1336 {
1337 }
1339 static void mpsc_break_ctl(struct uart_port *port, int ctl)
1340 {
1341 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1342 ulong flags;
1343 u32 v;
1345 v = ctl ? 0x00ff0000 : 0;
1347 spin_lock_irqsave(&pi->port.lock, flags);
1348 if (pi->mirror_regs)
1349 pi->MPSC_CHR_1_m = v;
1350 writel(v, pi->mpsc_base + MPSC_CHR_1);
1351 spin_unlock_irqrestore(&pi->port.lock, flags);
1352 }
1354 static int mpsc_startup(struct uart_port *port)
1355 {
1356 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1357 u32 flag = 0;
1358 int rc;
1360 pr_debug("mpsc_startup[%d]: Starting up MPSC, irq: %d\n",
1361 port->line, pi->port.irq);
1363 if ((rc = mpsc_make_ready(pi)) == 0) {
1364 /* Setup IRQ handler */
1365 mpsc_sdma_intr_ack(pi);
1367 /* If irq's are shared, need to set flag */
1368 if (mpsc_ports[0].port.irq == mpsc_ports[1].port.irq)
1369 flag = IRQF_SHARED;
1371 if (request_irq(pi->port.irq, mpsc_sdma_intr, flag,
1372 "mpsc-sdma", pi))
1373 printk(KERN_ERR "MPSC: Can't get SDMA IRQ %d\n",
1374 pi->port.irq);
1376 mpsc_sdma_intr_unmask(pi, 0xf);
1377 mpsc_sdma_set_rx_ring(pi, (struct mpsc_rx_desc *)(pi->rxr_p
1378 + (pi->rxr_posn * MPSC_RXRE_SIZE)));
1379 }
1381 return rc;
1382 }
1384 static void mpsc_shutdown(struct uart_port *port)
1385 {
1386 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1388 pr_debug("mpsc_shutdown[%d]: Shutting down MPSC\n", port->line);
1390 mpsc_sdma_stop(pi);
1391 free_irq(pi->port.irq, pi);
1392 }
1394 static void mpsc_set_termios(struct uart_port *port, struct ktermios *termios,
1395 struct ktermios *old)
1396 {
1397 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1398 u32 baud;
1399 ulong flags;
1400 u32 chr_bits, stop_bits, par;
1402 pi->c_iflag = termios->c_iflag;
1403 pi->c_cflag = termios->c_cflag;
1405 switch (termios->c_cflag & CSIZE) {
1406 case CS5:
1407 chr_bits = MPSC_MPCR_CL_5;
1408 break;
1409 case CS6:
1410 chr_bits = MPSC_MPCR_CL_6;
1411 break;
1412 case CS7:
1413 chr_bits = MPSC_MPCR_CL_7;
1414 break;
1415 case CS8:
1416 default:
1417 chr_bits = MPSC_MPCR_CL_8;
1418 break;
1419 }
1421 if (termios->c_cflag & CSTOPB)
1422 stop_bits = MPSC_MPCR_SBL_2;
1423 else
1424 stop_bits = MPSC_MPCR_SBL_1;
1426 par = MPSC_CHR_2_PAR_EVEN;
1427 if (termios->c_cflag & PARENB)
1428 if (termios->c_cflag & PARODD)
1429 par = MPSC_CHR_2_PAR_ODD;
1430 #ifdef CMSPAR
1431 if (termios->c_cflag & CMSPAR) {
1432 if (termios->c_cflag & PARODD)
1433 par = MPSC_CHR_2_PAR_MARK;
1434 else
1435 par = MPSC_CHR_2_PAR_SPACE;
1436 }
1437 #endif
1439 baud = uart_get_baud_rate(port, termios, old, 0, port->uartclk);
1441 spin_lock_irqsave(&pi->port.lock, flags);
1443 uart_update_timeout(port, termios->c_cflag, baud);
1445 mpsc_set_char_length(pi, chr_bits);
1446 mpsc_set_stop_bit_length(pi, stop_bits);
1447 mpsc_set_parity(pi, par);
1448 mpsc_set_baudrate(pi, baud);
1450 /* Characters/events to read */
1451 pi->port.read_status_mask = SDMA_DESC_CMDSTAT_OR;
1453 if (termios->c_iflag & INPCK)
1454 pi->port.read_status_mask |= SDMA_DESC_CMDSTAT_PE
1455 | SDMA_DESC_CMDSTAT_FR;
1457 if (termios->c_iflag & (BRKINT | PARMRK))
1458 pi->port.read_status_mask |= SDMA_DESC_CMDSTAT_BR;
1460 /* Characters/events to ignore */
1461 pi->port.ignore_status_mask = 0;
1463 if (termios->c_iflag & IGNPAR)
1464 pi->port.ignore_status_mask |= SDMA_DESC_CMDSTAT_PE
1465 | SDMA_DESC_CMDSTAT_FR;
1467 if (termios->c_iflag & IGNBRK) {
1468 pi->port.ignore_status_mask |= SDMA_DESC_CMDSTAT_BR;
1470 if (termios->c_iflag & IGNPAR)
1471 pi->port.ignore_status_mask |= SDMA_DESC_CMDSTAT_OR;
1472 }
1474 if ((termios->c_cflag & CREAD)) {
1475 if (!pi->rcv_data) {
1476 pi->rcv_data = 1;
1477 mpsc_start_rx(pi);
1478 }
1479 } else if (pi->rcv_data) {
1480 mpsc_stop_rx(port);
1481 pi->rcv_data = 0;
1482 }
1484 spin_unlock_irqrestore(&pi->port.lock, flags);
1485 }
1487 static const char *mpsc_type(struct uart_port *port)
1488 {
1489 pr_debug("mpsc_type[%d]: port type: %s\n", port->line,MPSC_DRIVER_NAME);
1490 return MPSC_DRIVER_NAME;
1491 }
1493 static int mpsc_request_port(struct uart_port *port)
1494 {
1495 /* Should make chip/platform specific call */
1496 return 0;
1497 }
1499 static void mpsc_release_port(struct uart_port *port)
1500 {
1501 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1503 if (pi->ready) {
1504 mpsc_uninit_rings(pi);
1505 mpsc_free_ring_mem(pi);
1506 pi->ready = 0;
1507 }
1508 }
1510 static void mpsc_config_port(struct uart_port *port, int flags)
1511 {
1512 }
1514 static int mpsc_verify_port(struct uart_port *port, struct serial_struct *ser)
1515 {
1516 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1517 int rc = 0;
1519 pr_debug("mpsc_verify_port[%d]: Verifying port data\n", pi->port.line);
1521 if (ser->type != PORT_UNKNOWN && ser->type != PORT_MPSC)
1522 rc = -EINVAL;
1523 else if (pi->port.irq != ser->irq)
1524 rc = -EINVAL;
1525 else if (ser->io_type != SERIAL_IO_MEM)
1526 rc = -EINVAL;
1527 else if (pi->port.uartclk / 16 != ser->baud_base) /* Not sure */
1528 rc = -EINVAL;
1529 else if ((void *)pi->port.mapbase != ser->iomem_base)
1530 rc = -EINVAL;
1531 else if (pi->port.iobase != ser->port)
1532 rc = -EINVAL;
1533 else if (ser->hub6 != 0)
1534 rc = -EINVAL;
1536 return rc;
1537 }
1538 #ifdef CONFIG_CONSOLE_POLL
1539 /* Serial polling routines for writing and reading from the uart while
1540 * in an interrupt or debug context.
1541 */
1543 static char poll_buf[2048];
1544 static int poll_ptr;
1545 static int poll_cnt;
1546 static void mpsc_put_poll_char(struct uart_port *port,
1547 unsigned char c);
1549 static int mpsc_get_poll_char(struct uart_port *port)
1550 {
1551 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1552 struct mpsc_rx_desc *rxre;
1553 u32 cmdstat, bytes_in, i;
1554 u8 *bp;
1556 if (!serial_polled)
1557 serial_polled = 1;
1559 pr_debug("mpsc_rx_intr[%d]: Handling Rx intr\n", pi->port.line);
1561 if (poll_cnt) {
1562 poll_cnt--;
1563 return poll_buf[poll_ptr++];
1564 }
1565 poll_ptr = 0;
1566 poll_cnt = 0;
1568 while (poll_cnt == 0) {
1569 rxre = (struct mpsc_rx_desc *)(pi->rxr +
1570 (pi->rxr_posn*MPSC_RXRE_SIZE));
1571 dma_cache_sync(pi->port.dev, (void *)rxre,
1572 MPSC_RXRE_SIZE, DMA_FROM_DEVICE);
1573 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
1574 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
1575 invalidate_dcache_range((ulong)rxre,
1576 (ulong)rxre + MPSC_RXRE_SIZE);
1577 #endif
1578 /*
1579 * Loop through Rx descriptors handling ones that have
1580 * been completed.
1581 */
1582 while (poll_cnt == 0 &&
1583 !((cmdstat = be32_to_cpu(rxre->cmdstat)) &
1584 SDMA_DESC_CMDSTAT_O)){
1585 bytes_in = be16_to_cpu(rxre->bytecnt);
1586 bp = pi->rxb + (pi->rxr_posn * MPSC_RXBE_SIZE);
1587 dma_cache_sync(pi->port.dev, (void *) bp,
1588 MPSC_RXBE_SIZE, DMA_FROM_DEVICE);
1589 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
1590 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
1591 invalidate_dcache_range((ulong)bp,
1592 (ulong)bp + MPSC_RXBE_SIZE);
1593 #endif
1594 if ((unlikely(cmdstat & (SDMA_DESC_CMDSTAT_BR |
1595 SDMA_DESC_CMDSTAT_FR | SDMA_DESC_CMDSTAT_OR))) &&
1596 !(cmdstat & pi->port.ignore_status_mask)) {
1597 poll_buf[poll_cnt] = *bp;
1598 poll_cnt++;
1599 } else {
1600 for (i = 0; i < bytes_in; i++) {
1601 poll_buf[poll_cnt] = *bp++;
1602 poll_cnt++;
1603 }
1604 pi->port.icount.rx += bytes_in;
1605 }
1606 rxre->bytecnt = cpu_to_be16(0);
1607 wmb();
1608 rxre->cmdstat = cpu_to_be32(SDMA_DESC_CMDSTAT_O |
1609 SDMA_DESC_CMDSTAT_EI |
1610 SDMA_DESC_CMDSTAT_F |
1611 SDMA_DESC_CMDSTAT_L);
1612 wmb();
1613 dma_cache_sync(pi->port.dev, (void *)rxre,
1614 MPSC_RXRE_SIZE, DMA_BIDIRECTIONAL);
1615 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
1616 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
1617 flush_dcache_range((ulong)rxre,
1618 (ulong)rxre + MPSC_RXRE_SIZE);
1619 #endif
1621 /* Advance to next descriptor */
1622 pi->rxr_posn = (pi->rxr_posn + 1) &
1623 (MPSC_RXR_ENTRIES - 1);
1624 rxre = (struct mpsc_rx_desc *)(pi->rxr +
1625 (pi->rxr_posn * MPSC_RXRE_SIZE));
1626 dma_cache_sync(pi->port.dev, (void *)rxre,
1627 MPSC_RXRE_SIZE, DMA_FROM_DEVICE);
1628 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
1629 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
1630 invalidate_dcache_range((ulong)rxre,
1631 (ulong)rxre + MPSC_RXRE_SIZE);
1632 #endif
1633 }
1635 /* Restart rx engine, if its stopped */
1636 if ((readl(pi->sdma_base + SDMA_SDCM) & SDMA_SDCM_ERD) == 0)
1637 mpsc_start_rx(pi);
1638 }
1639 if (poll_cnt) {
1640 poll_cnt--;
1641 return poll_buf[poll_ptr++];
1642 }
1644 return 0;
1645 }
1648 static void mpsc_put_poll_char(struct uart_port *port,
1649 unsigned char c)
1650 {
1651 struct mpsc_port_info *pi = (struct mpsc_port_info *)port;
1652 u32 data;
1654 data = readl(pi->mpsc_base + MPSC_MPCR);
1655 writeb(c, pi->mpsc_base + MPSC_CHR_1);
1656 mb();
1657 data = readl(pi->mpsc_base + MPSC_CHR_2);
1658 data |= MPSC_CHR_2_TTCS;
1659 writel(data, pi->mpsc_base + MPSC_CHR_2);
1660 mb();
1662 while (readl(pi->mpsc_base + MPSC_CHR_2) & MPSC_CHR_2_TTCS);
1663 }
1664 #endif
1666 static struct uart_ops mpsc_pops = {
1667 .tx_empty = mpsc_tx_empty,
1668 .set_mctrl = mpsc_set_mctrl,
1669 .get_mctrl = mpsc_get_mctrl,
1670 .stop_tx = mpsc_stop_tx,
1671 .start_tx = mpsc_start_tx,
1672 .stop_rx = mpsc_stop_rx,
1673 .enable_ms = mpsc_enable_ms,
1674 .break_ctl = mpsc_break_ctl,
1675 .startup = mpsc_startup,
1676 .shutdown = mpsc_shutdown,
1677 .set_termios = mpsc_set_termios,
1678 .type = mpsc_type,
1679 .release_port = mpsc_release_port,
1680 .request_port = mpsc_request_port,
1681 .config_port = mpsc_config_port,
1682 .verify_port = mpsc_verify_port,
1683 #ifdef CONFIG_CONSOLE_POLL
1684 .poll_get_char = mpsc_get_poll_char,
1685 .poll_put_char = mpsc_put_poll_char,
1686 #endif
1687 };
1689 /*
1690 ******************************************************************************
1691 *
1692 * Console Interface Routines
1693 *
1694 ******************************************************************************
1695 */
1697 #ifdef CONFIG_SERIAL_MPSC_CONSOLE
1698 static void mpsc_console_write(struct console *co, const char *s, uint count)
1699 {
1700 struct mpsc_port_info *pi = &mpsc_ports[co->index];
1701 u8 *bp, *dp, add_cr = 0;
1702 int i;
1703 unsigned long iflags;
1705 spin_lock_irqsave(&pi->tx_lock, iflags);
1707 while (pi->txr_head != pi->txr_tail) {
1708 while (mpsc_sdma_tx_active(pi))
1709 udelay(100);
1710 mpsc_sdma_intr_ack(pi);
1711 mpsc_tx_intr(pi);
1712 }
1714 while (mpsc_sdma_tx_active(pi))
1715 udelay(100);
1717 while (count > 0) {
1718 bp = dp = pi->txb + (pi->txr_head * MPSC_TXBE_SIZE);
1720 for (i = 0; i < MPSC_TXBE_SIZE; i++) {
1721 if (count == 0)
1722 break;
1724 if (add_cr) {
1725 *(dp++) = '\r';
1726 add_cr = 0;
1727 } else {
1728 *(dp++) = *s;
1730 if (*(s++) == '\n') { /* add '\r' after '\n' */
1731 add_cr = 1;
1732 count++;
1733 }
1734 }
1736 count--;
1737 }
1739 dma_cache_sync(pi->port.dev, (void *)bp, MPSC_TXBE_SIZE,
1740 DMA_BIDIRECTIONAL);
1741 #if defined(CONFIG_PPC32) && !defined(CONFIG_NOT_COHERENT_CACHE)
1742 if (pi->cache_mgmt) /* GT642[46]0 Res #COMM-2 */
1743 flush_dcache_range((ulong)bp,
1744 (ulong)bp + MPSC_TXBE_SIZE);
1745 #endif
1746 mpsc_setup_tx_desc(pi, i, 0);
1747 pi->txr_head = (pi->txr_head + 1) & (MPSC_TXR_ENTRIES - 1);
1748 mpsc_sdma_start_tx(pi);
1750 while (mpsc_sdma_tx_active(pi))
1751 udelay(100);
1753 pi->txr_tail = (pi->txr_tail + 1) & (MPSC_TXR_ENTRIES - 1);
1754 }
1756 spin_unlock_irqrestore(&pi->tx_lock, iflags);
1757 }
1759 static int __init mpsc_console_setup(struct console *co, char *options)
1760 {
1761 struct mpsc_port_info *pi;
1762 int baud, bits, parity, flow;
1764 pr_debug("mpsc_console_setup[%d]: options: %s\n", co->index, options);
1766 if (co->index >= MPSC_NUM_CTLRS)
1767 co->index = 0;
1769 pi = &mpsc_ports[co->index];
1771 baud = pi->default_baud;
1772 bits = pi->default_bits;
1773 parity = pi->default_parity;
1774 flow = pi->default_flow;
1776 if (!pi->port.ops)
1777 return -ENODEV;
1779 spin_lock_init(&pi->port.lock); /* Temporary fix--copied from 8250.c */
1781 if (options)
1782 uart_parse_options(options, &baud, &parity, &bits, &flow);
1784 return uart_set_options(&pi->port, co, baud, parity, bits, flow);
1785 }
1787 static struct console mpsc_console = {
1788 .name = MPSC_DEV_NAME,
1789 .write = mpsc_console_write,
1790 .device = uart_console_device,
1791 .setup = mpsc_console_setup,
1792 .flags = CON_PRINTBUFFER,
1793 .index = -1,
1794 .data = &mpsc_reg,
1795 };
1797 static int __init mpsc_late_console_init(void)
1798 {
1799 pr_debug("mpsc_late_console_init: Enter\n");
1801 if (!(mpsc_console.flags & CON_ENABLED))
1802 register_console(&mpsc_console);
1803 return 0;
1804 }
1806 late_initcall(mpsc_late_console_init);
1808 #define MPSC_CONSOLE &mpsc_console
1809 #else
1810 #define MPSC_CONSOLE NULL
1811 #endif
1812 /*
1813 ******************************************************************************
1814 *
1815 * Dummy Platform Driver to extract & map shared register regions
1816 *
1817 ******************************************************************************
1818 */
1819 static void mpsc_resource_err(char *s)
1820 {
1821 printk(KERN_WARNING "MPSC: Platform device resource error in %s\n", s);
1822 }
1824 static int mpsc_shared_map_regs(struct platform_device *pd)
1825 {
1826 struct resource *r;
1828 if ((r = platform_get_resource(pd, IORESOURCE_MEM,
1829 MPSC_ROUTING_BASE_ORDER))
1830 && request_mem_region(r->start,
1831 MPSC_ROUTING_REG_BLOCK_SIZE,
1832 "mpsc_routing_regs")) {
1833 mpsc_shared_regs.mpsc_routing_base = ioremap(r->start,
1834 MPSC_ROUTING_REG_BLOCK_SIZE);
1835 mpsc_shared_regs.mpsc_routing_base_p = r->start;
1836 } else {
1837 mpsc_resource_err("MPSC routing base");
1838 return -ENOMEM;
1839 }
1841 if ((r = platform_get_resource(pd, IORESOURCE_MEM,
1842 MPSC_SDMA_INTR_BASE_ORDER))
1843 && request_mem_region(r->start,
1844 MPSC_SDMA_INTR_REG_BLOCK_SIZE,
1845 "sdma_intr_regs")) {
1846 mpsc_shared_regs.sdma_intr_base = ioremap(r->start,
1847 MPSC_SDMA_INTR_REG_BLOCK_SIZE);
1848 mpsc_shared_regs.sdma_intr_base_p = r->start;
1849 } else {
1850 iounmap(mpsc_shared_regs.mpsc_routing_base);
1851 release_mem_region(mpsc_shared_regs.mpsc_routing_base_p,
1852 MPSC_ROUTING_REG_BLOCK_SIZE);
1853 mpsc_resource_err("SDMA intr base");
1854 return -ENOMEM;
1855 }
1857 return 0;
1858 }
1860 static void mpsc_shared_unmap_regs(void)
1861 {
1862 if (!mpsc_shared_regs.mpsc_routing_base) {
1863 iounmap(mpsc_shared_regs.mpsc_routing_base);
1864 release_mem_region(mpsc_shared_regs.mpsc_routing_base_p,
1865 MPSC_ROUTING_REG_BLOCK_SIZE);
1866 }
1867 if (!mpsc_shared_regs.sdma_intr_base) {
1868 iounmap(mpsc_shared_regs.sdma_intr_base);
1869 release_mem_region(mpsc_shared_regs.sdma_intr_base_p,
1870 MPSC_SDMA_INTR_REG_BLOCK_SIZE);
1871 }
1873 mpsc_shared_regs.mpsc_routing_base = NULL;
1874 mpsc_shared_regs.sdma_intr_base = NULL;
1876 mpsc_shared_regs.mpsc_routing_base_p = 0;
1877 mpsc_shared_regs.sdma_intr_base_p = 0;
1878 }
1880 static int mpsc_shared_drv_probe(struct platform_device *dev)
1881 {
1882 struct mpsc_shared_pdata *pdata;
1883 int rc = -ENODEV;
1885 if (dev->id == 0) {
1886 if (!(rc = mpsc_shared_map_regs(dev))) {
1887 pdata = (struct mpsc_shared_pdata *)
1888 dev->dev.platform_data;
1890 mpsc_shared_regs.MPSC_MRR_m = pdata->mrr_val;
1891 mpsc_shared_regs.MPSC_RCRR_m= pdata->rcrr_val;
1892 mpsc_shared_regs.MPSC_TCRR_m= pdata->tcrr_val;
1893 mpsc_shared_regs.SDMA_INTR_CAUSE_m =
1894 pdata->intr_cause_val;
1895 mpsc_shared_regs.SDMA_INTR_MASK_m =
1896 pdata->intr_mask_val;
1898 rc = 0;
1899 }
1900 }
1902 return rc;
1903 }
1905 static int mpsc_shared_drv_remove(struct platform_device *dev)
1906 {
1907 int rc = -ENODEV;
1909 if (dev->id == 0) {
1910 mpsc_shared_unmap_regs();
1911 mpsc_shared_regs.MPSC_MRR_m = 0;
1912 mpsc_shared_regs.MPSC_RCRR_m = 0;
1913 mpsc_shared_regs.MPSC_TCRR_m = 0;
1914 mpsc_shared_regs.SDMA_INTR_CAUSE_m = 0;
1915 mpsc_shared_regs.SDMA_INTR_MASK_m = 0;
1916 rc = 0;
1917 }
1919 return rc;
1920 }
1922 static struct platform_driver mpsc_shared_driver = {
1923 .probe = mpsc_shared_drv_probe,
1924 .remove = mpsc_shared_drv_remove,
1925 .driver = {
1926 .name = MPSC_SHARED_NAME,
1927 },
1928 };
1930 /*
1931 ******************************************************************************
1932 *
1933 * Driver Interface Routines
1934 *
1935 ******************************************************************************
1936 */
1937 static struct uart_driver mpsc_reg = {
1938 .owner = THIS_MODULE,
1939 .driver_name = MPSC_DRIVER_NAME,
1940 .dev_name = MPSC_DEV_NAME,
1941 .major = MPSC_MAJOR,
1942 .minor = MPSC_MINOR_START,
1943 .nr = MPSC_NUM_CTLRS,
1944 .cons = MPSC_CONSOLE,
1945 };
1947 static int mpsc_drv_map_regs(struct mpsc_port_info *pi,
1948 struct platform_device *pd)
1949 {
1950 struct resource *r;
1952 if ((r = platform_get_resource(pd, IORESOURCE_MEM, MPSC_BASE_ORDER))
1953 && request_mem_region(r->start, MPSC_REG_BLOCK_SIZE,
1954 "mpsc_regs")) {
1955 pi->mpsc_base = ioremap(r->start, MPSC_REG_BLOCK_SIZE);
1956 pi->mpsc_base_p = r->start;
1957 } else {
1958 mpsc_resource_err("MPSC base");
1959 goto err;
1960 }
1962 if ((r = platform_get_resource(pd, IORESOURCE_MEM,
1963 MPSC_SDMA_BASE_ORDER))
1964 && request_mem_region(r->start,
1965 MPSC_SDMA_REG_BLOCK_SIZE, "sdma_regs")) {
1966 pi->sdma_base = ioremap(r->start,MPSC_SDMA_REG_BLOCK_SIZE);
1967 pi->sdma_base_p = r->start;
1968 } else {
1969 mpsc_resource_err("SDMA base");
1970 if (pi->mpsc_base) {
1971 iounmap(pi->mpsc_base);
1972 pi->mpsc_base = NULL;
1973 }
1974 goto err;
1975 }
1977 if ((r = platform_get_resource(pd,IORESOURCE_MEM,MPSC_BRG_BASE_ORDER))
1978 && request_mem_region(r->start,
1979 MPSC_BRG_REG_BLOCK_SIZE, "brg_regs")) {
1980 pi->brg_base = ioremap(r->start, MPSC_BRG_REG_BLOCK_SIZE);
1981 pi->brg_base_p = r->start;
1982 } else {
1983 mpsc_resource_err("BRG base");
1984 if (pi->mpsc_base) {
1985 iounmap(pi->mpsc_base);
1986 pi->mpsc_base = NULL;
1987 }
1988 if (pi->sdma_base) {
1989 iounmap(pi->sdma_base);
1990 pi->sdma_base = NULL;
1991 }
1992 goto err;
1993 }
1994 return 0;
1996 err:
1997 return -ENOMEM;
1998 }
2000 static void mpsc_drv_unmap_regs(struct mpsc_port_info *pi)
2001 {
2002 if (!pi->mpsc_base) {
2003 iounmap(pi->mpsc_base);
2004 release_mem_region(pi->mpsc_base_p, MPSC_REG_BLOCK_SIZE);
2005 }
2006 if (!pi->sdma_base) {
2007 iounmap(pi->sdma_base);
2008 release_mem_region(pi->sdma_base_p, MPSC_SDMA_REG_BLOCK_SIZE);
2009 }
2010 if (!pi->brg_base) {
2011 iounmap(pi->brg_base);
2012 release_mem_region(pi->brg_base_p, MPSC_BRG_REG_BLOCK_SIZE);
2013 }
2015 pi->mpsc_base = NULL;
2016 pi->sdma_base = NULL;
2017 pi->brg_base = NULL;
2019 pi->mpsc_base_p = 0;
2020 pi->sdma_base_p = 0;
2021 pi->brg_base_p = 0;
2022 }
2024 static void mpsc_drv_get_platform_data(struct mpsc_port_info *pi,
2025 struct platform_device *pd, int num)
2026 {
2027 struct mpsc_pdata *pdata;
2029 pdata = (struct mpsc_pdata *)pd->dev.platform_data;
2031 pi->port.uartclk = pdata->brg_clk_freq;
2032 pi->port.iotype = UPIO_MEM;
2033 pi->port.line = num;
2034 pi->port.type = PORT_MPSC;
2035 pi->port.fifosize = MPSC_TXBE_SIZE;
2036 pi->port.membase = pi->mpsc_base;
2037 pi->port.mapbase = (ulong)pi->mpsc_base;
2038 pi->port.ops = &mpsc_pops;
2040 pi->mirror_regs = pdata->mirror_regs;
2041 pi->cache_mgmt = pdata->cache_mgmt;
2042 pi->brg_can_tune = pdata->brg_can_tune;
2043 pi->brg_clk_src = pdata->brg_clk_src;
2044 pi->mpsc_max_idle = pdata->max_idle;
2045 pi->default_baud = pdata->default_baud;
2046 pi->default_bits = pdata->default_bits;
2047 pi->default_parity = pdata->default_parity;
2048 pi->default_flow = pdata->default_flow;
2050 /* Initial values of mirrored regs */
2051 pi->MPSC_CHR_1_m = pdata->chr_1_val;
2052 pi->MPSC_CHR_2_m = pdata->chr_2_val;
2053 pi->MPSC_CHR_10_m = pdata->chr_10_val;
2054 pi->MPSC_MPCR_m = pdata->mpcr_val;
2055 pi->BRG_BCR_m = pdata->bcr_val;
2057 pi->shared_regs = &mpsc_shared_regs;
2059 pi->port.irq = platform_get_irq(pd, 0);
2060 }
2062 static int mpsc_drv_probe(struct platform_device *dev)
2063 {
2064 struct mpsc_port_info *pi;
2065 int rc = -ENODEV;
2067 pr_debug("mpsc_drv_probe: Adding MPSC %d\n", dev->id);
2069 if (dev->id < MPSC_NUM_CTLRS) {
2070 pi = &mpsc_ports[dev->id];
2072 if (!(rc = mpsc_drv_map_regs(pi, dev))) {
2073 mpsc_drv_get_platform_data(pi, dev, dev->id);
2074 pi->port.dev = &dev->dev;
2076 if (!(rc = mpsc_make_ready(pi))) {
2077 spin_lock_init(&pi->tx_lock);
2078 if (!(rc = uart_add_one_port(&mpsc_reg,
2079 &pi->port))) {
2080 rc = 0;
2081 } else {
2082 mpsc_release_port((struct uart_port *)
2083 pi);
2084 mpsc_drv_unmap_regs(pi);
2085 }
2086 } else {
2087 mpsc_drv_unmap_regs(pi);
2088 }
2089 }
2090 }
2092 return rc;
2093 }
2095 static int mpsc_drv_remove(struct platform_device *dev)
2096 {
2097 pr_debug("mpsc_drv_exit: Removing MPSC %d\n", dev->id);
2099 if (dev->id < MPSC_NUM_CTLRS) {
2100 uart_remove_one_port(&mpsc_reg, &mpsc_ports[dev->id].port);
2101 mpsc_release_port((struct uart_port *)
2102 &mpsc_ports[dev->id].port);
2103 mpsc_drv_unmap_regs(&mpsc_ports[dev->id]);
2104 return 0;
2105 } else {
2106 return -ENODEV;
2107 }
2108 }
2110 static struct platform_driver mpsc_driver = {
2111 .probe = mpsc_drv_probe,
2112 .remove = mpsc_drv_remove,
2113 .driver = {
2114 .name = MPSC_CTLR_NAME,
2115 .owner = THIS_MODULE,
2116 },
2117 };
2119 static int __init mpsc_drv_init(void)
2120 {
2121 int rc;
2123 printk(KERN_INFO "Serial: MPSC driver\n");
2125 memset(mpsc_ports, 0, sizeof(mpsc_ports));
2126 memset(&mpsc_shared_regs, 0, sizeof(mpsc_shared_regs));
2128 if (!(rc = uart_register_driver(&mpsc_reg))) {
2129 if (!(rc = platform_driver_register(&mpsc_shared_driver))) {
2130 if ((rc = platform_driver_register(&mpsc_driver))) {
2131 platform_driver_unregister(&mpsc_shared_driver);
2132 uart_unregister_driver(&mpsc_reg);
2133 }
2134 } else {
2135 uart_unregister_driver(&mpsc_reg);
2136 }
2137 }
2139 return rc;
2140 }
2142 static void __exit mpsc_drv_exit(void)
2143 {
2144 platform_driver_unregister(&mpsc_driver);
2145 platform_driver_unregister(&mpsc_shared_driver);
2146 uart_unregister_driver(&mpsc_reg);
2147 memset(mpsc_ports, 0, sizeof(mpsc_ports));
2148 memset(&mpsc_shared_regs, 0, sizeof(mpsc_shared_regs));
2149 }
2151 module_init(mpsc_drv_init);
2152 module_exit(mpsc_drv_exit);
2154 MODULE_AUTHOR("Mark A. Greer <mgreer@mvista.com>");
2155 MODULE_DESCRIPTION("Generic Marvell MPSC serial/UART driver");
2156 MODULE_VERSION(MPSC_VERSION);
2157 MODULE_LICENSE("GPL");
2158 MODULE_ALIAS_CHARDEV_MAJOR(MPSC_MAJOR);
2159 MODULE_ALIAS("platform:" MPSC_CTLR_NAME);