1 /*
2 * Tty buffer allocation management
3 */
5 #include <linux/types.h>
6 #include <linux/errno.h>
7 #include <linux/tty.h>
8 #include <linux/tty_driver.h>
9 #include <linux/tty_flip.h>
10 #include <linux/timer.h>
11 #include <linux/string.h>
12 #include <linux/slab.h>
13 #include <linux/sched.h>
14 #include <linux/wait.h>
15 #include <linux/bitops.h>
16 #include <linux/delay.h>
17 #include <linux/module.h>
18 #include <linux/ratelimit.h>
21 #define MIN_TTYB_SIZE 256
22 #define TTYB_ALIGN_MASK 255
24 /*
25 * Byte threshold to limit memory consumption for flip buffers.
26 * The actual memory limit is > 2x this amount.
27 */
28 #define TTYB_DEFAULT_MEM_LIMIT 65536
30 /*
31 * We default to dicing tty buffer allocations to this many characters
32 * in order to avoid multiple page allocations. We know the size of
33 * tty_buffer itself but it must also be taken into account that the
34 * the buffer is 256 byte aligned. See tty_buffer_find for the allocation
35 * logic this must match
36 */
38 #define TTY_BUFFER_PAGE (((PAGE_SIZE - sizeof(struct tty_buffer)) / 2) & ~0xFF)
41 /**
42 * tty_buffer_lock_exclusive - gain exclusive access to buffer
43 * tty_buffer_unlock_exclusive - release exclusive access
44 *
45 * @port - tty_port owning the flip buffer
46 *
47 * Guarantees safe use of the line discipline's receive_buf() method by
48 * excluding the buffer work and any pending flush from using the flip
49 * buffer. Data can continue to be added concurrently to the flip buffer
50 * from the driver side.
51 *
52 * On release, the buffer work is restarted if there is data in the
53 * flip buffer
54 */
56 void tty_buffer_lock_exclusive(struct tty_port *port)
57 {
58 struct tty_bufhead *buf = &port->buf;
60 atomic_inc(&buf->priority);
61 mutex_lock(&buf->lock);
62 }
63 EXPORT_SYMBOL_GPL(tty_buffer_lock_exclusive);
65 void tty_buffer_unlock_exclusive(struct tty_port *port)
66 {
67 struct tty_bufhead *buf = &port->buf;
68 int restart;
70 restart = buf->head->commit != buf->head->read;
72 atomic_dec(&buf->priority);
73 mutex_unlock(&buf->lock);
74 if (restart)
75 queue_work(system_unbound_wq, &buf->work);
76 }
77 EXPORT_SYMBOL_GPL(tty_buffer_unlock_exclusive);
79 /**
80 * tty_buffer_space_avail - return unused buffer space
81 * @port - tty_port owning the flip buffer
82 *
83 * Returns the # of bytes which can be written by the driver without
84 * reaching the buffer limit.
85 *
86 * Note: this does not guarantee that memory is available to write
87 * the returned # of bytes (use tty_prepare_flip_string_xxx() to
88 * pre-allocate if memory guarantee is required).
89 */
91 int tty_buffer_space_avail(struct tty_port *port)
92 {
93 int space = port->buf.mem_limit - atomic_read(&port->buf.mem_used);
94 return max(space, 0);
95 }
96 EXPORT_SYMBOL_GPL(tty_buffer_space_avail);
98 static void tty_buffer_reset(struct tty_buffer *p, size_t size)
99 {
100 p->used = 0;
101 p->size = size;
102 p->next = NULL;
103 p->commit = 0;
104 p->read = 0;
105 p->flags = 0;
106 }
108 /**
109 * tty_buffer_free_all - free buffers used by a tty
110 * @tty: tty to free from
111 *
112 * Remove all the buffers pending on a tty whether queued with data
113 * or in the free ring. Must be called when the tty is no longer in use
114 */
116 void tty_buffer_free_all(struct tty_port *port)
117 {
118 struct tty_bufhead *buf = &port->buf;
119 struct tty_buffer *p, *next;
120 struct llist_node *llist;
122 while ((p = buf->head) != NULL) {
123 buf->head = p->next;
124 if (p->size > 0)
125 kfree(p);
126 }
127 llist = llist_del_all(&buf->free);
128 llist_for_each_entry_safe(p, next, llist, free)
129 kfree(p);
131 tty_buffer_reset(&buf->sentinel, 0);
132 buf->head = &buf->sentinel;
133 buf->tail = &buf->sentinel;
135 atomic_set(&buf->mem_used, 0);
136 }
138 /**
139 * tty_buffer_alloc - allocate a tty buffer
140 * @tty: tty device
141 * @size: desired size (characters)
142 *
143 * Allocate a new tty buffer to hold the desired number of characters.
144 * We round our buffers off in 256 character chunks to get better
145 * allocation behaviour.
146 * Return NULL if out of memory or the allocation would exceed the
147 * per device queue
148 */
150 static struct tty_buffer *tty_buffer_alloc(struct tty_port *port, size_t size)
151 {
152 struct llist_node *free;
153 struct tty_buffer *p;
155 /* Round the buffer size out */
156 size = __ALIGN_MASK(size, TTYB_ALIGN_MASK);
158 if (size <= MIN_TTYB_SIZE) {
159 free = llist_del_first(&port->buf.free);
160 if (free) {
161 p = llist_entry(free, struct tty_buffer, free);
162 goto found;
163 }
164 }
166 /* Should possibly check if this fails for the largest buffer we
167 have queued and recycle that ? */
168 if (atomic_read(&port->buf.mem_used) > port->buf.mem_limit)
169 return NULL;
170 p = kmalloc(sizeof(struct tty_buffer) + 2 * size, GFP_ATOMIC);
171 if (p == NULL)
172 return NULL;
174 found:
175 tty_buffer_reset(p, size);
176 atomic_add(size, &port->buf.mem_used);
177 return p;
178 }
180 /**
181 * tty_buffer_free - free a tty buffer
182 * @tty: tty owning the buffer
183 * @b: the buffer to free
184 *
185 * Free a tty buffer, or add it to the free list according to our
186 * internal strategy
187 */
189 static void tty_buffer_free(struct tty_port *port, struct tty_buffer *b)
190 {
191 struct tty_bufhead *buf = &port->buf;
193 /* Dumb strategy for now - should keep some stats */
194 WARN_ON(atomic_sub_return(b->size, &buf->mem_used) < 0);
196 if (b->size > MIN_TTYB_SIZE)
197 kfree(b);
198 else if (b->size > 0)
199 llist_add(&b->free, &buf->free);
200 }
202 /**
203 * tty_buffer_flush - flush full tty buffers
204 * @tty: tty to flush
205 *
206 * flush all the buffers containing receive data.
207 *
208 * Locking: takes buffer lock to ensure single-threaded flip buffer
209 * 'consumer'
210 */
212 void tty_buffer_flush(struct tty_struct *tty)
213 {
214 struct tty_port *port = tty->port;
215 struct tty_bufhead *buf = &port->buf;
216 struct tty_buffer *next;
218 atomic_inc(&buf->priority);
220 mutex_lock(&buf->lock);
221 while ((next = buf->head->next) != NULL) {
222 tty_buffer_free(port, buf->head);
223 buf->head = next;
224 }
225 buf->head->read = buf->head->commit;
226 atomic_dec(&buf->priority);
227 mutex_unlock(&buf->lock);
228 }
230 /**
231 * tty_buffer_request_room - grow tty buffer if needed
232 * @tty: tty structure
233 * @size: size desired
234 * @flags: buffer flags if new buffer allocated (default = 0)
235 *
236 * Make at least size bytes of linear space available for the tty
237 * buffer. If we fail return the size we managed to find.
238 *
239 * Will change over to a new buffer if the current buffer is encoded as
240 * TTY_NORMAL (so has no flags buffer) and the new buffer requires
241 * a flags buffer.
242 */
243 static int __tty_buffer_request_room(struct tty_port *port, size_t size,
244 int flags)
245 {
246 struct tty_bufhead *buf = &port->buf;
247 struct tty_buffer *b, *n;
248 int left, change;
250 b = buf->tail;
251 if (b->flags & TTYB_NORMAL)
252 left = 2 * b->size - b->used;
253 else
254 left = b->size - b->used;
256 change = (b->flags & TTYB_NORMAL) && (~flags & TTYB_NORMAL);
257 if (change || left < size) {
258 /* This is the slow path - looking for new buffers to use */
259 if ((n = tty_buffer_alloc(port, size)) != NULL) {
260 n->flags = flags;
261 buf->tail = n;
262 b->commit = b->used;
263 /* paired w/ barrier in flush_to_ldisc(); ensures the
264 * latest commit value can be read before the head is
265 * advanced to the next buffer
266 */
267 smp_wmb();
268 b->next = n;
269 } else if (change)
270 size = 0;
271 else
272 size = left;
273 }
274 return size;
275 }
277 int tty_buffer_request_room(struct tty_port *port, size_t size)
278 {
279 return __tty_buffer_request_room(port, size, 0);
280 }
281 EXPORT_SYMBOL_GPL(tty_buffer_request_room);
283 /**
284 * tty_insert_flip_string_fixed_flag - Add characters to the tty buffer
285 * @port: tty port
286 * @chars: characters
287 * @flag: flag value for each character
288 * @size: size
289 *
290 * Queue a series of bytes to the tty buffering. All the characters
291 * passed are marked with the supplied flag. Returns the number added.
292 */
294 int tty_insert_flip_string_fixed_flag(struct tty_port *port,
295 const unsigned char *chars, char flag, size_t size)
296 {
297 int copied = 0;
298 do {
299 int goal = min_t(size_t, size - copied, TTY_BUFFER_PAGE);
300 int flags = (flag == TTY_NORMAL) ? TTYB_NORMAL : 0;
301 int space = __tty_buffer_request_room(port, goal, flags);
302 struct tty_buffer *tb = port->buf.tail;
303 if (unlikely(space == 0))
304 break;
305 memcpy(char_buf_ptr(tb, tb->used), chars, space);
306 if (~tb->flags & TTYB_NORMAL)
307 memset(flag_buf_ptr(tb, tb->used), flag, space);
308 tb->used += space;
309 copied += space;
310 chars += space;
311 /* There is a small chance that we need to split the data over
312 several buffers. If this is the case we must loop */
313 } while (unlikely(size > copied));
314 return copied;
315 }
316 EXPORT_SYMBOL(tty_insert_flip_string_fixed_flag);
318 /**
319 * tty_insert_flip_string_flags - Add characters to the tty buffer
320 * @port: tty port
321 * @chars: characters
322 * @flags: flag bytes
323 * @size: size
324 *
325 * Queue a series of bytes to the tty buffering. For each character
326 * the flags array indicates the status of the character. Returns the
327 * number added.
328 */
330 int tty_insert_flip_string_flags(struct tty_port *port,
331 const unsigned char *chars, const char *flags, size_t size)
332 {
333 int copied = 0;
334 do {
335 int goal = min_t(size_t, size - copied, TTY_BUFFER_PAGE);
336 int space = tty_buffer_request_room(port, goal);
337 struct tty_buffer *tb = port->buf.tail;
338 if (unlikely(space == 0))
339 break;
340 memcpy(char_buf_ptr(tb, tb->used), chars, space);
341 memcpy(flag_buf_ptr(tb, tb->used), flags, space);
342 tb->used += space;
343 copied += space;
344 chars += space;
345 flags += space;
346 /* There is a small chance that we need to split the data over
347 several buffers. If this is the case we must loop */
348 } while (unlikely(size > copied));
349 return copied;
350 }
351 EXPORT_SYMBOL(tty_insert_flip_string_flags);
353 /**
354 * tty_schedule_flip - push characters to ldisc
355 * @port: tty port to push from
356 *
357 * Takes any pending buffers and transfers their ownership to the
358 * ldisc side of the queue. It then schedules those characters for
359 * processing by the line discipline.
360 */
362 void tty_schedule_flip(struct tty_port *port)
363 {
364 struct tty_bufhead *buf = &port->buf;
366 buf->tail->commit = buf->tail->used;
367 schedule_work(&buf->work);
368 }
369 EXPORT_SYMBOL(tty_schedule_flip);
371 /**
372 * tty_prepare_flip_string - make room for characters
373 * @port: tty port
374 * @chars: return pointer for character write area
375 * @size: desired size
376 *
377 * Prepare a block of space in the buffer for data. Returns the length
378 * available and buffer pointer to the space which is now allocated and
379 * accounted for as ready for normal characters. This is used for drivers
380 * that need their own block copy routines into the buffer. There is no
381 * guarantee the buffer is a DMA target!
382 */
384 int tty_prepare_flip_string(struct tty_port *port, unsigned char **chars,
385 size_t size)
386 {
387 int space = __tty_buffer_request_room(port, size, TTYB_NORMAL);
388 if (likely(space)) {
389 struct tty_buffer *tb = port->buf.tail;
390 *chars = char_buf_ptr(tb, tb->used);
391 if (~tb->flags & TTYB_NORMAL)
392 memset(flag_buf_ptr(tb, tb->used), TTY_NORMAL, space);
393 tb->used += space;
394 }
395 return space;
396 }
397 EXPORT_SYMBOL_GPL(tty_prepare_flip_string);
400 static int
401 receive_buf(struct tty_struct *tty, struct tty_buffer *head, int count)
402 {
403 struct tty_ldisc *disc = tty->ldisc;
404 unsigned char *p = char_buf_ptr(head, head->read);
405 char *f = NULL;
407 if (~head->flags & TTYB_NORMAL)
408 f = flag_buf_ptr(head, head->read);
410 if (disc->ops->receive_buf2)
411 count = disc->ops->receive_buf2(tty, p, f, count);
412 else {
413 count = min_t(int, count, tty->receive_room);
414 if (count)
415 disc->ops->receive_buf(tty, p, f, count);
416 }
417 head->read += count;
418 return count;
419 }
421 /**
422 * flush_to_ldisc
423 * @work: tty structure passed from work queue.
424 *
425 * This routine is called out of the software interrupt to flush data
426 * from the buffer chain to the line discipline.
427 *
428 * The receive_buf method is single threaded for each tty instance.
429 *
430 * Locking: takes buffer lock to ensure single-threaded flip buffer
431 * 'consumer'
432 */
434 static void flush_to_ldisc(struct work_struct *work)
435 {
436 struct tty_port *port = container_of(work, struct tty_port, buf.work);
437 struct tty_bufhead *buf = &port->buf;
438 struct tty_struct *tty;
439 struct tty_ldisc *disc;
441 tty = port->itty;
442 if (tty == NULL)
443 return;
445 disc = tty_ldisc_ref(tty);
446 if (disc == NULL)
447 return;
449 mutex_lock(&buf->lock);
451 while (1) {
452 struct tty_buffer *head = buf->head;
453 struct tty_buffer *next;
454 int count;
456 /* Ldisc or user is trying to gain exclusive access */
457 if (atomic_read(&buf->priority))
458 break;
460 next = head->next;
461 /* paired w/ barrier in __tty_buffer_request_room();
462 * ensures commit value read is not stale if the head
463 * is advancing to the next buffer
464 */
465 smp_rmb();
466 count = head->commit - head->read;
467 if (!count) {
468 if (next == NULL)
469 break;
470 buf->head = next;
471 tty_buffer_free(port, head);
472 continue;
473 }
475 count = receive_buf(tty, head, count);
476 if (!count)
477 break;
478 }
480 mutex_unlock(&buf->lock);
482 tty_ldisc_deref(disc);
483 }
485 /**
486 * tty_flush_to_ldisc
487 * @tty: tty to push
488 *
489 * Push the terminal flip buffers to the line discipline.
490 *
491 * Must not be called from IRQ context.
492 */
493 void tty_flush_to_ldisc(struct tty_struct *tty)
494 {
495 flush_work(&tty->port->buf.work);
496 }
498 /**
499 * tty_flip_buffer_push - terminal
500 * @port: tty port to push
501 *
502 * Queue a push of the terminal flip buffers to the line discipline.
503 * Can be called from IRQ/atomic context.
504 *
505 * In the event of the queue being busy for flipping the work will be
506 * held off and retried later.
507 */
509 void tty_flip_buffer_push(struct tty_port *port)
510 {
511 tty_schedule_flip(port);
512 }
513 EXPORT_SYMBOL(tty_flip_buffer_push);
515 /**
516 * tty_buffer_init - prepare a tty buffer structure
517 * @tty: tty to initialise
518 *
519 * Set up the initial state of the buffer management for a tty device.
520 * Must be called before the other tty buffer functions are used.
521 */
523 void tty_buffer_init(struct tty_port *port)
524 {
525 struct tty_bufhead *buf = &port->buf;
527 mutex_init(&buf->lock);
528 tty_buffer_reset(&buf->sentinel, 0);
529 buf->head = &buf->sentinel;
530 buf->tail = &buf->sentinel;
531 init_llist_head(&buf->free);
532 atomic_set(&buf->mem_used, 0);
533 atomic_set(&buf->priority, 0);
534 INIT_WORK(&buf->work, flush_to_ldisc);
535 buf->mem_limit = TTYB_DEFAULT_MEM_LIMIT;
536 }
538 /**
539 * tty_buffer_set_limit - change the tty buffer memory limit
540 * @port: tty port to change
541 *
542 * Change the tty buffer memory limit.
543 * Must be called before the other tty buffer functions are used.
544 */
546 int tty_buffer_set_limit(struct tty_port *port, int limit)
547 {
548 if (limit < MIN_TTYB_SIZE)
549 return -EINVAL;
550 port->buf.mem_limit = limit;
551 return 0;
552 }
553 EXPORT_SYMBOL_GPL(tty_buffer_set_limit);