1 /*
2 * 32-bit compatibility support for ELF format executables and core dumps.
3 *
4 * Copyright (C) 2007 Red Hat, Inc. All rights reserved.
5 *
6 * This copyrighted material is made available to anyone wishing to use,
7 * modify, copy, or redistribute it subject to the terms and conditions
8 * of the GNU General Public License v.2.
9 *
10 * Red Hat Author: Roland McGrath.
11 *
12 * This file is used in a 64-bit kernel that wants to support 32-bit ELF.
13 * asm/elf.h is responsible for defining the compat_* and COMPAT_* macros
14 * used below, with definitions appropriate for 32-bit ABI compatibility.
15 *
16 * We use macros to rename the ABI types and machine-dependent
17 * functions used in binfmt_elf.c to compat versions.
18 */
20 #include <linux/elfcore-compat.h>
21 #include <linux/time.h>
23 /*
24 * Rename the basic ELF layout types to refer to the 32-bit class of files.
25 */
26 #undef ELF_CLASS
27 #define ELF_CLASS ELFCLASS32
29 #undef elfhdr
30 #undef elf_phdr
31 #undef elf_shdr
32 #undef elf_note
33 #undef elf_addr_t
34 #define elfhdr elf32_hdr
35 #define elf_phdr elf32_phdr
36 #define elf_shdr elf32_shdr
37 #define elf_note elf32_note
38 #define elf_addr_t Elf32_Addr
40 /*
41 * Some data types as stored in coredump.
42 */
43 #define user_long_t compat_long_t
44 #define user_siginfo_t compat_siginfo_t
45 #define copy_siginfo_to_user copy_siginfo_to_user32
47 /*
48 * The machine-dependent core note format types are defined in elfcore-compat.h,
49 * which requires asm/elf.h to define compat_elf_gregset_t et al.
50 */
51 #define elf_prstatus compat_elf_prstatus
52 #define elf_prpsinfo compat_elf_prpsinfo
54 /*
55 * Compat version of cputime_to_compat_timeval, perhaps this
56 * should be an inline in <linux/compat.h>.
57 */
58 static void cputime_to_compat_timeval(const cputime_t cputime,
59 struct compat_timeval *value)
60 {
61 struct timeval tv;
62 cputime_to_timeval(cputime, &tv);
63 value->tv_sec = tv.tv_sec;
64 value->tv_usec = tv.tv_usec;
65 }
67 #undef cputime_to_timeval
68 #define cputime_to_timeval cputime_to_compat_timeval
71 /*
72 * To use this file, asm/elf.h must define compat_elf_check_arch.
73 * The other following macros can be defined if the compat versions
74 * differ from the native ones, or omitted when they match.
75 */
77 #undef ELF_ARCH
78 #undef elf_check_arch
79 #define elf_check_arch compat_elf_check_arch
81 #ifdef COMPAT_ELF_PLATFORM
82 #undef ELF_PLATFORM
83 #define ELF_PLATFORM COMPAT_ELF_PLATFORM
84 #endif
86 #ifdef COMPAT_ELF_HWCAP
87 #undef ELF_HWCAP
88 #define ELF_HWCAP COMPAT_ELF_HWCAP
89 #endif
91 #ifdef COMPAT_ARCH_DLINFO
92 #undef ARCH_DLINFO
93 #define ARCH_DLINFO COMPAT_ARCH_DLINFO
94 #endif
96 #ifdef COMPAT_ELF_ET_DYN_BASE
97 #undef ELF_ET_DYN_BASE
98 #define ELF_ET_DYN_BASE COMPAT_ELF_ET_DYN_BASE
99 #endif
101 #ifdef COMPAT_ELF_EXEC_PAGESIZE
102 #undef ELF_EXEC_PAGESIZE
103 #define ELF_EXEC_PAGESIZE COMPAT_ELF_EXEC_PAGESIZE
104 #endif
106 #ifdef COMPAT_ELF_PLAT_INIT
107 #undef ELF_PLAT_INIT
108 #define ELF_PLAT_INIT COMPAT_ELF_PLAT_INIT
109 #endif
111 #ifdef COMPAT_SET_PERSONALITY
112 #undef SET_PERSONALITY
113 #define SET_PERSONALITY COMPAT_SET_PERSONALITY
114 #endif
116 #ifdef compat_start_thread
117 #undef start_thread
118 #define start_thread compat_start_thread
119 #endif
121 #ifdef compat_arch_setup_additional_pages
122 #undef ARCH_HAS_SETUP_ADDITIONAL_PAGES
123 #define ARCH_HAS_SETUP_ADDITIONAL_PAGES 1
124 #undef arch_setup_additional_pages
125 #define arch_setup_additional_pages compat_arch_setup_additional_pages
126 #endif
128 /*
129 * Rename a few of the symbols that binfmt_elf.c will define.
130 * These are all local so the names don't really matter, but it
131 * might make some debugging less confusing not to duplicate them.
132 */
133 #define elf_format compat_elf_format
134 #define init_elf_binfmt init_compat_elf_binfmt
135 #define exit_elf_binfmt exit_compat_elf_binfmt
137 /*
138 * We share all the actual code with the native (64-bit) version.
139 */
140 #include "binfmt_elf.c"